This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] LP-AM263:在 Windows 11上使用 CCS12.8.1时无法访问 DAP 错误1170

Guru**** 2482225 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1504660/lp-am263-unable-to-access-dap-error-1170-with-ccs12-8-1-on-windows-11

器件型号:LP-AM263

工具/软件:

您好、

在窗口11计算机上、我运行 CCS 12.8.1、连接到 AM263x LP R5F0_0内核时收到以下错误。  

连接到目标时出错:
(错误-1170 @ 0x0)
无法访问 DAP。 重置器件、然后重试此操作。 如果错误仍然存在、请确认配置、对电路板进行下电上电、和/或尝试更可靠的 JTAG 设置(例如下 TCLK)。
(仿真包20.0.0.3178)

为此、目标配置是用一个精简的1MHz TCLK 创建的。

启动目标配置时没有问题、连接到 R5F 内核时会发生错误。

这是日志

[Start: Texas Instruments XDS110 USB Debug Probe_0]

Execute the command:

%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -S integrity

[Result]


-----[Print the board config pathname(s)]------------------------------------

C:\Users\a0192896\AppData\Local\TEXASI~1\
    CCS\ccs1281\0\0\BrdDat\testBoard.dat

-----[Print the reset-command software log-file]-----------------------------

This utility has selected a 100/110/510 class product.
This utility will load the adapter 'jioxds110.dll'.
The library build date was 'Sep 26 2024'.
The library build time was '10:09:41'.
The library package version is '20.0.0.3178'.
The library component version is '35.35.0.0'.
The controller does not use a programmable FPGA.
The controller has a version number of '5' (0x00000005).
The controller has an insertion length of '0' (0x00000000).
This utility will attempt to reset the controller.
This utility has successfully reset the controller.

-----[Print the reset-command hardware log-file]-----------------------------

The scan-path will be reset by toggling the JTAG TRST signal.
The controller is the XDS110 with USB interface.
The link from controller to target is direct (without cable).
The software is configured for XDS110 features.
The controller cannot monitor the value on the EMU[0] pin.
The controller cannot monitor the value on the EMU[1] pin.
The controller cannot control the timing on output pins.
The controller cannot control the timing on input pins.
The scan-path link-delay has been set to exactly '0' (0x0000).

-----[An error has occurred and this utility has aborted]--------------------

This error is generated by TI's USCIF driver or utilities.

The value is '-233' (0xffffff17).
The title is 'SC_ERR_PATH_BROKEN'.

The explanation is:
The JTAG IR and DR scan-paths cannot circulate bits, they may be broken.
An attempt to scan the JTAG scan-path has failed.
The target's JTAG scan-path appears to be broken
with a stuck-at-ones or stuck-at-zero fault.

[End: Texas Instruments XDS110 USB Debug Probe_0]

非常有趣的是、当测试 CCS12.8.1在 Linux 计算机上运行且目标配置相同的同一电路板时、一切都正常工作。

任何想法都是非常感激的。

谢谢!

-- Gunter

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好 Gunter、

    他们是否尝试过使用不同的 USB 电缆? 我发现这种情况有时是由于 USB 电缆故障导致的、通常是 EVM 随附的电缆。

    我们会让调试专家审查一下、但希望提供该初始输入。

    此致、

    Ralph Jacobi

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好 Gunter、

    除了 Ralph 的建议外、请参阅   调试 JTAG 指南的"无法访问 DAP"部分

    如果错误仍然存在、请告诉我。

    此致、

    Brennan