This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] DRA821U:是否可以通过此配置使用所有4个串行器/解串器通道?

Guru**** 2455560 points
Other Parts Discussed in Thread: DRA821U

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1510218/dra821u-can-is-use-all-4-serdes-lanes-with-this-configuration

器件型号:DRA821U
主题: DRA821中讨论的其他器件

工具/软件:

我使用的是 DRA821U、并且对数据表中的注释存在一些问题。
DRA821数据表的第3页有一条底线、内容如下:
  "b. SGMII、USB3.0和 PCIE 共用总共四个串行器/解串器通道。 最多可同时使用三个 IP (例如 SGMII 和 USB)中的两个。"

我要同时使用所有4个串行器/解串器通道、这是否可行?
  通道0:PCIe 通道0
  通道1:SGMII 通道4
  通道2:SGMII 通道1
  通道3:USB 3.0

谢谢、

Steve