This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] SK-AM62-LP:UART uniflash 不适用于 HS-SE 器件

Guru**** 2343770 points
Other Parts Discussed in Thread: UNIFLASH
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1505029/sk-am62-lp-uart-uniflash-not-working-for-hs-se-device

器件型号:SK-AM62-LP
Thread 中讨论的其他器件:UNIFLASH

工具/软件:

大家好、我尝试使用 mcu_plus_sdk_am62x_11_00_00_16工具套件中的 python UART uniflash 工具。

我已将密钥放入 tools/boot/signing/custMpk_am62x.pem 文件中、并使用` make device=am62x device_type=HS -sk`编译整个 SDK

但是、在刷写 uniflash_stage1文件时仍会获得以下输出:

(.venv) [fred441a@FSH-arch boot]$ python uart_uniflash.py -p /dev/ttyUSB0 --cfg=sbl_prebuilt/am62x-sk-lp/default_sbl_ospi_nand_hs.cfg

Parsing config file ...
Parsing config file ... SUCCESS. Found 9 command(s) !!!

Executing command 1 of 9 ...
Found flash writer ... sending sbl_prebuilt/am62x-sk-lp/sbl_uart_uniflash_stage1.release.hs.tiimage
Sending sbl_prebuilt/am62x-sk-lp/sbl_uart_uniflash_stage1.release.hs.tiimage:   0%|      | 0/266850 [00:00<?, ?bytes/s]send error: expected NAK, CRC, EOT or CAN; got b'\x00'
Sent flashwriter sbl_prebuilt/am62x-sk-lp/sbl_uart_uniflash_stage1.release.hs.tiimage of size 266850 bytes in 25.09s.

Executing command 2 of 9 ...
Command arguments : --file=../../examples/drivers/boot/sbl_uart_uniflash_multistage/sbl_uart_uniflash_stage2/am62x-sk-lp/r5fss0-0_nortos/ti-arm-clang/sbl_uart_uniflash_stage2.release.appimage.hs --operation=flash --flash-offset=0x0
Sending ../../examples/drivers/boot/sbl_uart_uniflash_multistage/sbl_uart_uniflash_stage2/am62x-sk-lp/r5fss0-0_nortos/tsend error: expected NAK, CRC, EOT or CAN; got b'0'
send error: expected NAK, CRC, EOT or CAN; got b'2'
send error: expected NAK, CRC, EOT or CAN; got b'0'
send error: expected NAK, CRC, EOT or CAN; got b'0'
send error: expected NAK, CRC, EOT or CAN; got b'0'
send error: expected NAK, CRC, EOT or CAN; got b'0'
send error: expected NAK, CRC, EOT or CAN; got b'0'
send error: expected NAK, CRC, EOT or CAN; got b'0'
send error: expected NAK, CRC, EOT or CAN; got b'0'
send error: expected NAK, CRC, EOT or CAN; got b'1'
send error: expected NAK, CRC, EOT or CAN; got b'1'
send error: error_count reached 10, aborting.
Sending ../../examples/drivers/boot/sbl_uart_uniflash_multistage/sbl_uart_uniflash_stage2/am62x-sk-lp/r5fss0-0_nortos/t
[ERROR] XMODEM send failed, no response OR incorrect response from EVM OR cancelled by user,
Power cycle EVM and run this script again !!!

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好:

    请告知我们、此问题是否仍可供我们采取进一步行动。

    谢谢!