This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] AM625:AM62x 启用 LVDS 异常

Guru**** 2335430 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1512969/am625-am62x-enables-lvds-exception

器件型号:AM625

工具/软件:

问题描述:

  在 DTS 中启动 LVDS 时、背光 PWM 无法输出。 可能的原因是什么? 是 defconfig 还是 dts 异常?

我的 DTS 配置:

#include <dt-bindings/pwm/pwm.h>
#include <dt-bindings/gpio/gpio.h>
#include <dt-bindings/interrupt-controller/irq.h>
#include "k3-pinctrl.h"
#include "k3-am62x-sk-common.dtsi"

&{/} {  
    backlight_lvds: backlight-lvds {
        compatible = "pwm-backlight";
        pwms = <&epwm1 1 20000 0>;
        brightness-levels = <
              0  20  20  21  21  22  22  23
             23  24  24  25  25  26  26  27
             27  28  28  29  29  30  30  31
             31  32  32  33  33  34  34  35
             35  36  36  37  37  38  38  39
             40  41  42  43  44  45  46  47
             48  49  50  51  52  53  54  55
             56  57  58  59  60  61  62  63
             64  65  66  67  68  69  70  71
             72  73  74  75  76  77  78  79
             80  81  82  83  84  85  86  87
             88  89  90  91  92  93  94  95
             96  97  98  99 100 101 102 103
            104 105 106 107 108 109 110 111
            112 113 114 115 116 117 118 119
            120 121 122 123 124 125 126 127
            128 129 130 131 132 133 134 135
            136 137 138 139 140 141 142 143
            144 145 146 147 148 149 150 151
            152 153 154 155 156 157 158 159
            160 161 162 163 164 165 166 167
            168 169 170 171 172 173 174 175
            176 177 178 179 180 181 182 183
            184 185 186 187 188 189 190 191
            192 193 194 195 196 197 198 199
            200 201 202 203 204 205 206 207
            208 209 210 211 212 213 214 215
            216 217 218 219 220 221 222 223
            224 225 226 227 228 229 230 231
            232 233 234 235 236 237 238 239
            240 241 242 243 244 245 246 247
            248 249 250 251 252 253 254 255
            >;
        default-brightness-level = <255>;
    };


    panel_lvds: panel_lvds {
        compatible = "panel-lvds";
        backlight = <&backlight_lvds>;
        lable = "LVDS";
        data-mapping = "vesa-24";
        width-mm = <229>;
        height-mm = <149>;

        panel-timing {
            clock-frequency = <71100000>;
            hactive = <1280>;
            vactive = <800>;

            hback-porch = <88>;
            hfront-porch = <70>;

            vback-porch = <21>;
            vfront-porch = <15>;

            hsync-len = <4>;
            vsync-len = <4>;

            hsync-active = <0>;
            vsync-active = <0>;

            de-active = <0>;
            pixelclk-active = <0>;
        };

        port@0 {
            lvds_in0: endpoint {
                remote-endpoint = <&lvds_out0>;
            };
        };
    };
};

&dss_ports {
    #address-cells = <1>;
    #size-cells = <0>;

    port@0 {
        reg = <0>;
        lvds_out0: endpoint {
            remote-endpoint = <&lvds_in0>;
        };
    };
};

&dss {
    pinctrl-names = "default";
    pinctrl-0 = <&main_oldi0_pins_default &main_dss0_pins_default>;
    status  = "okay";
};

&epwm1 {
    pinctrl-names = "default";
    pinctrl-0 = <&main_epwm1_a_pins_default>;
    status  = "okay";
};

&main_pmx0 {
    main_epwm1_a_pins_default: main-epwm1-a-pins-default {
        pinctrl-single,pins = <
            AM62X_IOPAD(0x19c, PIN_OUTPUT, 6) /* (B18) MCASP0_AXR1.EHRPWM1_A */			
        >;
    };

	main_oldi0_pins_default: main-oldi0-pins-default {
        pinctrl-single,pins = <
            AM62X_IOPAD(0x0260, PIN_OUTPUT, 0) /* (AA5) OLDI0_A0N */
            AM62X_IOPAD(0x025c, PIN_OUTPUT, 0) /* (Y6) OLDI0_A0P */
            AM62X_IOPAD(0x0268, PIN_OUTPUT, 0) /* (AD3) OLDI0_A1N */
            AM62X_IOPAD(0x0264, PIN_OUTPUT, 0) /* (AB4) OLDI0_A1P */
            AM62X_IOPAD(0x0270, PIN_OUTPUT, 0) /* (Y8) OLDI0_A2N */
            AM62X_IOPAD(0x026c, PIN_OUTPUT, 0) /* (AA8) OLDI0_A2P */
            AM62X_IOPAD(0x0278, PIN_OUTPUT, 0) /* (AB6) OLDI0_A3N */
            AM62X_IOPAD(0x0274, PIN_OUTPUT, 0) /* (AA7) OLDI0_A3P */
            AM62X_IOPAD(0x0280, PIN_OUTPUT, 0) /* (AC6) OLDI0_A4N */
            AM62X_IOPAD(0x027c, PIN_OUTPUT, 0) /* (AC5) OLDI0_A4P */
            AM62X_IOPAD(0x0288, PIN_OUTPUT, 0) /* (AE5) OLDI0_A5N */
            AM62X_IOPAD(0x0284, PIN_OUTPUT, 0) /* (AD6) OLDI0_A5P */
            AM62X_IOPAD(0x0290, PIN_OUTPUT, 0) /* (AE6) OLDI0_A6N */
            AM62X_IOPAD(0x028c, PIN_OUTPUT, 0) /* (AD7) OLDI0_A6P */
            AM62X_IOPAD(0x0298, PIN_OUTPUT, 0) /* (AD8) OLDI0_A7N */
            AM62X_IOPAD(0x0294, PIN_OUTPUT, 0) /* (AE7) OLDI0_A7P */
            AM62X_IOPAD(0x02a0, PIN_OUTPUT, 0) /* (AD4) OLDI0_CLK0N */
            AM62X_IOPAD(0x029c, PIN_OUTPUT, 0) /* (AE3) OLDI0_CLK0P */
            AM62X_IOPAD(0x02a8, PIN_OUTPUT, 0) /* (AE4) OLDI0_CLK1N */
            AM62X_IOPAD(0x02a4, PIN_OUTPUT, 0) /* (AD5) OLDI0_CLK1P */
        >;
    };
};

系统log:μ s

root@sbc7138:~# cat /sys/kernel/debug/gpio
gpiochip2: GPIOs 344-367, parent: i2c/1-0022, 1-0022, can sleep:
 gpio-344 (GPIO_CPSW2_RST      )
 gpio-345 (GPIO_CPSW1_RST      )
 gpio-346 (PRU_DETECT          )
 gpio-347 (MMC1_SD_EN          |regulator-3         ) out lo 
 gpio-348 (VPP_LDO_EN          )
 gpio-349 (EXP_PS_3V3_En       )
 gpio-350 (EXP_PS_5V0_En       )
 gpio-351 (EXP_HAT_DETECT      )
 gpio-352 (GPIO_AUD_RSTn       )
 gpio-353 (GPIO_eMMC_RSTn      )
 gpio-354 (UART1_FET_BUF_EN    )
 gpio-355 (WL_LT_EN            |regulator-6         ) out lo ACTIVE LOW
 gpio-356 (GPIO_HDMI_RSTn      )
 gpio-357 (CSI_GPIO1           )
 gpio-358 (CSI_GPIO2           )
 gpio-359 (PRU_3V3_EN          )
 gpio-360 (HDMI_INTn           )
 gpio-361 (PD_I2C_IRQ          )
 gpio-362 (MCASP1_FET_EN       )
 gpio-363 (MCASP1_BUF_BT_EN    )
 gpio-364 (MCASP1_FET_SEL      )
 gpio-365 (UART1_FET_SEL       )
 gpio-366 (TSINT#              )
 gpio-367 (IO_EXP_TEST_LED     )

gpiochip1: GPIOs 368-419, parent: platform/601000.gpio, 601000.gpio:
 gpio-417 (                    |heartbeat           ) out lo 

gpiochip0: GPIOs 420-511, parent: platform/600000.gpio, 600000.gpio:
 gpio-451 (                    |tlv71033            ) out lo 
 gpio-491 (                    |regulator-7         ) out lo 
root@sbc7138:~# 
root@sbc7138:~# 
root@sbc7138:~# cat /sys/kernel/debug/pinctrl/f4000.pinctrl-pinctrl-single/pinmux-pins | grep pwm
pin 103 (PIN103): 23010000.pwm (GPIO UNCLAIMED) function main-epwm1-a-pins-default group main-epwm1-a-pins-default
root@sbc7138:~# 
root@sbc7138:~# dmesg | grep pwm
[   17.659335] pwm-backlight backlight-lvds: supply power not found, using dummy regulator
[   18.450811] Modules linked in: videobuf2_dma_contig m_can_platform m_can rti_wdt(+) syscopyarea videobuf2_memops sysfillrect sysimgblt fb_sys_fops videobuf2_v4l2 ti_k3_m4_remoteproc(+) videobuf2_common v4l2_async ti_k3_common can_dev drm videodev snd_soc_davinci_mcasp snd_soc_tlv320aic3x_i2c snd_soc_ti_udma snd_soc_tlv320aic3x cdns_dphy_rx snd_soc_ti_edma pruss sa2ul mcrc drm_panel_orientation_quirks snd_soc_ti_sdma mc pwm_bl optee_rng rng_core pwm_tiehrpwm ip_tables x_tables ipv6
root@sbc7138:~# 

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    添加日志:

    root@sbc7138:~# dmesg | grep dss
    [   10.444403] platform 30200000.dss: Fixed dependency cycle(s) with /bus@f0000/i2c@20010000/sii9022@3b
    [   10.474710] platform 30200000.dss: Fixed dependency cycle(s) with /panel_lvds
    [   10.482071] platform panel_lvds: Fixed dependency cycle(s) with /bus@f0000/dss@30200000
    [   11.215104] platform 30200000.dss: Fixed dependency cycle(s) with /bus@f0000/i2c@20010000/sii9022@3b
    [   11.230782] i2c 1-003b: Fixed dependency cycle(s) with /bus@f0000/dss@30200000
    [   18.991271] Modules linked in: ti_k3_r5_remoteproc(+) rti_wdt(+) k3_j72xx_bandgap(+) j721e_csi2rx videobuf2_dma_contig tidss sii902x drm_dma_helper videobuf2_memops videobuf2_v4l2 m_can_platform videobuf2_common drm_kms_helper v4l2_async m_can ti_k3_m4_remoteproc syscopyarea sysfillrect sysimgblt fb_sys_fops ti_k3_common videodev can_dev drm pruss mcrc sa2ul snd_soc_davinci_mcasp snd_soc_ti_udma snd_soc_ti_edma mc cdns_dphy_rx snd_soc_ti_sdma snd_soc_tlv320aic3x_i2c pwm_tiehrpwm snd_soc_tlv320aic3x drm_panel_orientation_quirks optee_rng rng_core pwm_bl ip_tables x_tables ipv6
    [   32.872677] platform 30200000.dss: deferred probe pending

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您使用的是哪个 SDK?
    您能否参考 SDK 中的这个示例: https://git.ti.com/cgit/ti-linux-kernel/ti-linux-kernel/tree/arch/arm64/boot/dts/ti/k3-am625-sk-microtips-mf101hie-panel.dtso?h=ti-linux-6.12.y 并以这种方式创建 DTS、面板时序在 panel-simple.c 或等效器件中定义。

    您使用的是单链路还是双链路 LVDS?
    这是定制板吗?
    同时分享以下成果:

    kmsprint
    modetest -M tidss
    kmstest

    运行 kmstest 时、还可以分享您在屏幕上看到的内容。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

      非常感谢您的答复。 我还没有到达 LVDS 显示部分。 目前、PWM 背光没有输出。

      我必须手动执行命令来控制它、以便激活背光。

      这可能是背光驱动器出现问题吗?

    cat /sys/class/backlight/backlight-lvds/actual_brightness
    255
    root@sbc7138:~# 
    root@sbc7138:~# cat /sys/class/backlight/backlight-lvds/bl_power
    4
    root@sbc7138:~# 
    root@sbc7138:~# cat /sys/kernel/debug/pwm
    platform/23010000.pwm, 2 PWM devices
     pwm-0   (backlight-lvds      ): requested period: 1000000 ns duty: 0 ns polarity: normal
     pwm-1   ((null)              ): period: 0 ns duty: 0 ns polarity: normal
    root@sbc7138:~# 
    root@sbc7138:~# 
    root@sbc7138:~# dmesg | grep pwm
    [   10.454584] platform 23010000.pwm: Fixed dependency cycle(s) with /bus@f0000/pwm@23010000
    root@sbc7138:~# 
    root@sbc7138:~# echo 0 > /sys/class/backlight/backlight-lvds/bl_power
    root@sbc7138:~# 
    root@sbc7138:~# cat /sys/kernel/debug/pwm
    platform/23010000.pwm, 2 PWM devices
     pwm-0   (backlight-lvds      ): requested enabled period: 1000000 ns duty: 1000000 ns polarity: normal
     pwm-1   ((null)              ): period: 0 ns duty: 0 ns polarity: normal
    root@sbc7138:~# 
    root@sbc7138:~# dmesg | grep backlight
    root@sbc7138:~# 

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    让我在即将到来的星期一之前回复您

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    好的、 非常感谢。我将添加一些更多日志。

    root@sbc7138:~# dmesg | grep pwm
    [   10.454636] platform 23010000.pwm: Fixed dependency cycle(s) with /bus@f0000/pwm@23010000
    root@sbc7138:~# 
    root@sbc7138:~# dmesg | grep backlight
    root@sbc7138:~# 
    root@sbc7138:~# dmesg | grep lvds
    [   10.464265] platform 30200000.dss: Fixed dependency cycle(s) with /panel_lvds
    [   10.471622] platform panel_lvds: Fixed dependency cycle(s) with /bus@f0000/dss@30200000
    root@sbc7138:~# 
    root@sbc7138:~# dmesg | grep dss
    [   10.464265] platform 30200000.dss: Fixed dependency cycle(s) with /panel_lvds
    [   10.471622] platform panel_lvds: Fixed dependency cycle(s) with /bus@f0000/dss@30200000
    [   19.314492] Modules linked in: rtc_ti_k3(+) dwc3_am62 ti_k3_r5_remoteproc(+) k3_j72xx_bandgap(+) rti_wdt(+) tidss m_can_platform m_can ti_k3_m4_remoteproc ti_k3_common drm_dma_helper j721e_csi2rx can_dev drm_kms_helper syscopyarea videobuf2_dma_contig sysfillrect sysimgblt fb_sys_fops videobuf2_memops snd_soc_davinci_mcasp videobuf2_v4l2 snd_soc_ti_udma videobuf2_common snd_soc_ti_edma v4l2_async drm cdns_dphy_rx pruss snd_soc_ti_sdma videodev mc sa2ul mcrc drm_panel_orientation_quirks snd_soc_tlv320aic3x_i2c snd_soc_tlv320aic3x optee_rng rng_core ip_tables x_tables ipv6
    [   19.646650] [drm] Initialized tidss 1.0.0 20180215 for 30200000.dss on minor 0
    [   19.770502] tidss 30200000.dss: [drm] fb0: tidssdrmfb frame buffer device
    root@sbc7138:~# 
    root@sbc7138:~# lsmod | grep lvds
    panel_lvds             16384  0
    drm                   561152  5 drm_kms_helper,drm_dma_helper,tidss,panel_lvds
    root@sbc7138:~# 
    root@sbc7138:~# lsmod | grep pwm
    root@sbc7138:~# 

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

     我现在修改了我的 dts 文件。 背光现在可以亮起。

     系统已识别 LVDS 设备、但没有显示输出。

     这里也没有用于测试 LVDS 的 CLK 信号。

    以下是我的 DTS:

    #include <dt-bindings/pwm/pwm.h>
    #include <dt-bindings/gpio/gpio.h>
    #include <dt-bindings/interrupt-controller/irq.h>
    #include "k3-pinctrl.h"
    #include "k3-am62x-sk-common.dtsi"
    
    &{/} {  
        backlight_lvds: backlight-lvds {
    		compatible = "pwm-backlight";
    		pwms = <&epwm1 0 1000000 0>; 
    		brightness-levels = <
                  0  20  20  21  21  22  22  23
                 23  24  24  25  25  26  26  27
                 27  28  28  29  29  30  30  31
                 31  32  32  33  33  34  34  35
                 35  36  36  37  37  38  38  39
                 40  41  42  43  44  45  46  47
                 48  49  50  51  52  53  54  55
                 56  57  58  59  60  61  62  63
                 64  65  66  67  68  69  70  71
                 72  73  74  75  76  77  78  79
                 80  81  82  83  84  85  86  87
                 88  89  90  91  92  93  94  95
                 96  97  98  99 100 101 102 103
                104 105 106 107 108 109 110 111
                112 113 114 115 116 117 118 119
                120 121 122 123 124 125 126 127
                128 129 130 131 132 133 134 135
                136 137 138 139 140 141 142 143
                144 145 146 147 148 149 150 151
                152 153 154 155 156 157 158 159
                160 161 162 163 164 165 166 167
                168 169 170 171 172 173 174 175
                176 177 178 179 180 181 182 183
                184 185 186 187 188 189 190 191
                192 193 194 195 196 197 198 199
                200 201 202 203 204 205 206 207
                208 209 210 211 212 213 214 215
                216 217 218 219 220 221 222 223
                224 225 226 227 228 229 230 231
                232 233 234 235 236 237 238 239
                240 241 242 243 244 245 246 247
                248 249 250 251 252 253 254 255
            >;
            default-brightness-level = <255>;
    		enable-gpios = <&main_gpio0 41 GPIO_ACTIVE_HIGH>; 
    		power-supply = <&vcc_3v3_sys>;	
        };
    
    
        panel_lvds: panel_lvds {
            compatible = "microtips,mf-101hiebcaf0", "panel-simple";
            backlight = <&backlight_lvds>;
            lable = "LVDS";
            data-mapping = "vesa-24";
            width-mm = <229>;
            height-mm = <149>;
    		
            panel-timing {
                clock-frequency = <71100000>;
                hactive = <1280>;
                vactive = <800>;
    
                hback-porch = <88>;
                hfront-porch = <70>;
    
                vback-porch = <21>;
                vfront-porch = <15>;
    
                hsync-len = <4>;
                vsync-len = <4>;
    
                hsync-active = <0>;
                vsync-active = <0>;
    
                de-active = <0>;
                pixelclk-active = <0>;
            };
    
    		ports {
    			port@0 {
    				lvds_in0: endpoint {
    					remote-endpoint = <&lvds_out0>;
    				};
    			};
    		};
        };
    };
    
    &dss {
        pinctrl-names = "default";
        pinctrl-0 = <&main_oldi0_pins_default>;
        status  = "okay";
    };
    
    &dss_ports {
        port@0 {
            reg = <0>;
            lvds_out0: endpoint {
                remote-endpoint = <&lvds_in0>;
            };
        };
    };
    
    &epwm1 {
        pinctrl-names = "default";
    	pwms = <&epwm1 0 20000 0>; 
        pinctrl-0 = <&main_epwm1_a_pins_default>;
        status  = "okay";
    };
    
    &main_pmx0 {
        main_epwm1_a_pins_default: main-epwm1-a-pins-default {
            pinctrl-single,pins = <
                AM62X_IOPAD(0x19c, PIN_OUTPUT, 6) /* (B18) MCASP0_AXR1.EHRPWM1_A */			
            >;
        };
    
    	pwmenable_pins_default: pwmenable-default-pins {
    		pinctrl-single,pins = <
    			/* PWM pin set */
    			AM62X_IOPAD(0x0094, PIN_INPUT_PULLDOWN, 7) /* (N20) GPMC0_BE1n.GPIO0_36  sbc7138-AM6254_BKLT_PWM_DC_SEL */
    			AM62X_IOPAD(0x00a4, PIN_INPUT_PULLDOWN, 7) /* (M22) GPMC0_DIR.GPIO0_40   sbc7138-AM6254_BKLT_PWM_VO_EN  */
    			AM62X_IOPAD(0x00a8, PIN_INPUT_PULLUP, 7) /* (M21) GPMC0_CSn0.GPIO0_41    sbc7138-AM6254_BKLT_ON         */
    			AM62X_IOPAD(0x00ac, PIN_INPUT_PULLDOWN, 7) /* (L21) GPMC0_CSn1.GPIO0_42  sbc7138-AM6254_BKLT_EN_VO_SEL  */
    			/* PWM pin set END */
    		>;
    	};
    
    	main_oldi0_pins_default: main-oldi0-pins-default {
            pinctrl-single,pins = <
                AM62X_IOPAD(0x0260, PIN_OUTPUT, 0) /* (AA5) OLDI0_A0N */
                AM62X_IOPAD(0x025c, PIN_OUTPUT, 0) /* (Y6) OLDI0_A0P */
                AM62X_IOPAD(0x0268, PIN_OUTPUT, 0) /* (AD3) OLDI0_A1N */
                AM62X_IOPAD(0x0264, PIN_OUTPUT, 0) /* (AB4) OLDI0_A1P */
                AM62X_IOPAD(0x0270, PIN_OUTPUT, 0) /* (Y8) OLDI0_A2N */
                AM62X_IOPAD(0x026c, PIN_OUTPUT, 0) /* (AA8) OLDI0_A2P */
                AM62X_IOPAD(0x0278, PIN_OUTPUT, 0) /* (AB6) OLDI0_A3N */
                AM62X_IOPAD(0x0274, PIN_OUTPUT, 0) /* (AA7) OLDI0_A3P */
                AM62X_IOPAD(0x0280, PIN_OUTPUT, 0) /* (AC6) OLDI0_A4N */
                AM62X_IOPAD(0x027c, PIN_OUTPUT, 0) /* (AC5) OLDI0_A4P */
                AM62X_IOPAD(0x0288, PIN_OUTPUT, 0) /* (AE5) OLDI0_A5N */
                AM62X_IOPAD(0x0284, PIN_OUTPUT, 0) /* (AD6) OLDI0_A5P */
                AM62X_IOPAD(0x0290, PIN_OUTPUT, 0) /* (AE6) OLDI0_A6N */
                AM62X_IOPAD(0x028c, PIN_OUTPUT, 0) /* (AD7) OLDI0_A6P */
                AM62X_IOPAD(0x0298, PIN_OUTPUT, 0) /* (AD8) OLDI0_A7N */
                AM62X_IOPAD(0x0294, PIN_OUTPUT, 0) /* (AE7) OLDI0_A7P */
                AM62X_IOPAD(0x02a0, PIN_OUTPUT, 0) /* (AD4) OLDI0_CLK0N */
                AM62X_IOPAD(0x029c, PIN_OUTPUT, 0) /* (AE3) OLDI0_CLK0P */
                AM62X_IOPAD(0x02a8, PIN_OUTPUT, 0) /* (AE4) OLDI0_CLK1N */
                AM62X_IOPAD(0x02a4, PIN_OUTPUT, 0) /* (AD5) OLDI0_CLK1P */
            >;
        };
    };

    日志:

    Debian GNU/Linux comes with ABSOLUTELY NO WARRANTY, to the extent
    permitted by applicable law.
    root@sbc7138:~# [   25.122925] broken atomic modeset userspace detected, disabling atomic
    [   26.731398] broken atomic modeset userspace detected, disabling atomic
    
    root@sbc7138:~# cat /sys/kernel/debug/pwm
    platform/23010000.pwm, 2 PWM devices
     pwm-0   (backlight-lvds      ): requested enabled period: 1000000 ns duty: 1000000 ns polarity: normal
     pwm-1   ((null)              ): period: 0 ns duty: 0 ns polarity: normal
    root@sbc7138:~# 
    root@sbc7138:~# cat /sys/class/backlight/backlight-lvds/actual_brightness
    255
    root@sbc7138:~# 
    root@sbc7138:~# cat /sys/class/backlight/backlight-lvds/bl_power
    0
    root@sbc7138:~# 
    root@sbc7138:~# ls /sys/kernel/debug/dri/0/
    clients  crtc-0  framebuffer  gem_names  internal_clients  LVDS-1  name  state
    root@sbc7138:~# 
    root@sbc7138:~# dmesg | grep lvds
    [   10.464293] platform 30200000.dss: Fixed dependency cycle(s) with /panel_lvds
    [   10.471646] platform panel_lvds: Fixed dependency cycle(s) with /bus@f0000/dss@30200000
    [   19.534586] panel-simple panel_lvds: supply power not found, using dummy regulator
    [   20.312009] panel-simple panel_lvds: Reject override mode: panel has a fixed mode
    root@sbc7138:~# 
    root@sbc7138:~# dmesg | grep dss
    [   10.464293] platform 30200000.dss: Fixed dependency cycle(s) with /panel_lvds
    [   10.471646] platform panel_lvds: Fixed dependency cycle(s) with /bus@f0000/dss@30200000
    [   19.069174] Modules linked in: rtc_ti_k3(+) dwc3_am62(+) ti_k3_r5_remoteproc(+) rti_wdt(+) tidss ti_k3_m4_remoteproc ti_k3_common drm_dma_helper j721e_csi2rx m_can_platform videobuf2_dma_contig m_can videobuf2_memops drm_kms_helper videobuf2_v4l2 videobuf2_common can_dev syscopyarea sysfillrect sysimgblt v4l2_async fb_sys_fops drm snd_soc_davinci_mcasp videodev cdns_dphy_rx drm_panel_orientation_quirks mcrc snd_soc_ti_udma sa2ul snd_soc_ti_edma mc snd_soc_ti_sdma pruss snd_soc_tlv320aic3x_i2c snd_soc_tlv320aic3x optee_rng rng_core ip_tables x_tables ipv6
    [   19.834675] Modules linked in: panel_simple(+) k3_j72xx_bandgap(+) phy_can_transceiver(+) rtc_ti_k3 dwc3_am62 ti_k3_r5_remoteproc rti_wdt(+) tidss ti_k3_m4_remoteproc ti_k3_common drm_dma_helper j721e_csi2rx m_can_platform videobuf2_dma_contig m_can videobuf2_memops drm_kms_helper videobuf2_v4l2 videobuf2_common can_dev syscopyarea sysfillrect sysimgblt v4l2_async fb_sys_fops drm snd_soc_davinci_mcasp videodev cdns_dphy_rx drm_panel_orientation_quirks mcrc snd_soc_ti_udma sa2ul snd_soc_ti_edma mc snd_soc_ti_sdma pruss snd_soc_tlv320aic3x_i2c snd_soc_tlv320aic3x optee_rng rng_core ip_tables x_tables ipv6
    [   20.335896] [drm] Initialized tidss 1.0.0 20180215 for 30200000.dss on minor 0
    [   20.498160] tidss 30200000.dss: [drm] fb0: tidssdrmfb frame buffer device
    root@sbc7138:~# 
    root@sbc7138:~# dmesg | grep pwm
    [   10.454636] platform 23010000.pwm: Fixed dependency cycle(s) with /bus@f0000/pwm@23010000
    root@sbc7138:~# 
    root@sbc7138:~# lsmod | grep lvds
    root@sbc7138:~# 
    root@sbc7138:~# lsmod | grep pwm
    root@sbc7138:~# 

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    添加日志:

    root@sbc7138:~# lsmod | grep panel
    panel_simple           86016  0
    drm                   561152  5 drm_kms_helper,panel_simple,drm_dma_helper,tidss
    drm_panel_orientation_quirks    28672  1 drm
    root@sbc7138:~# 
    root@sbc7138:~# dmesg | grep panel
    [   10.464202] platform 30200000.dss: Fixed dependency cycle(s) with /panel_lvds
    [   10.471557] platform panel_lvds: Fixed dependency cycle(s) with /bus@f0000/dss@30200000
    [   19.212795] Modules linked in: ti_k3_r5_remoteproc(+) rti_wdt(+) drm_dma_helper drm_kms_helper syscopyarea sysfillrect sysimgblt fb_sys_fops j721e_csi2rx m_can_platform m_can videobuf2_dma_contig drm can_dev videobuf2_memops videobuf2_v4l2 ti_k3_m4_remoteproc(+) ti_k3_common videobuf2_common sa2ul v4l2_async drm_panel_orientation_quirks mcrc pruss snd_soc_davinci_mcasp snd_soc_ti_udma videodev snd_soc_ti_edma snd_soc_ti_sdma mc cdns_dphy_rx snd_soc_tlv320aic3x_i2c snd_soc_tlv320aic3x optee_rng rng_core ip_tables x_tables ipv6
    [   19.839848] panel-simple panel_lvds: supply power not found, using dummy regulator
    [   19.882062] WARNING: CPU: 1 PID: 189 at drivers/gpu/drm/panel/panel-simple.c:519 panel_simple_parse_panel_timing_node+0x1e4/0x1fc [panel_simple]
    [   19.895075] Modules linked in: panel_simple(+) phy_can_transceiver k3_j72xx_bandgap dwc3_am62 rtc_ti_k3 tidss ti_k3_r5_remoteproc rti_wdt(+) drm_dma_helper drm_kms_helper syscopyarea sysfillrect sysimgblt fb_sys_fops j721e_csi2rx m_can_platform m_can videobuf2_dma_contig drm can_dev videobuf2_memops videobuf2_v4l2 ti_k3_m4_remoteproc ti_k3_common videobuf2_common sa2ul v4l2_async drm_panel_orientation_quirks mcrc pruss snd_soc_davinci_mcasp snd_soc_ti_udma videodev snd_soc_ti_edma snd_soc_ti_sdma mc cdns_dphy_rx snd_soc_tlv320aic3x_i2c snd_soc_tlv320aic3x optee_rng rng_core ip_tables x_tables ipv6
    [   19.976065] pc : panel_simple_parse_panel_timing_node+0x1e4/0x1fc [panel_simple]
    [   19.983495] lr : panel_simple_probe+0x2b8/0x3b0 [panel_simple]
    [   20.066315]  panel_simple_parse_panel_timing_node+0x1e4/0x1fc [panel_simple]
    [   20.073371]  panel_simple_probe+0x2b8/0x3b0 [panel_simple]
    [   20.078865]  panel_simple_platform_probe+0x34/0x4c [panel_simple]
    [   20.124275]  panel_simple_init+0x30/0x1000 [panel_simple]
    [   20.296907] panel-simple panel_lvds: Reject override mode: panel has a fixed mode
    root@sbc7138:~# 

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我现在修改了它‘ Compatible ="panel-LVDS";"

    LVDS 驱动器已更改为 panel_dlvs.ko、背光亮度现在可通过命令控制。

    但是、LVDS 仍然没有输出、也没有 CLK

    Log:

    [   24.156417] broken atomic modeset userspace detected, disabling atomic
    root@sbc7138:~# [   25.529282] broken atomic modeset userspace detected, disabling atomic
    
    root@sbc7138:~# lsmod | grep panel
    panel_lvds             16384  0
    drm                   561152  5 drm_kms_helper,drm_dma_helper,tidss,panel_lvds
    drm_panel_orientation_quirks    28672  1 drm
    root@sbc7138:~# 
    root@sbc7138:~# dmesg | grep panel
    [   10.464298] platform 30200000.dss: Fixed dependency cycle(s) with /panel_lvds
    [   10.471654] platform panel_lvds: Fixed dependency cycle(s) with /bus@f0000/dss@30200000
    [   19.150838] Modules linked in: k3_j72xx_bandgap(+) ti_k3_r5_remoteproc(+) dwc3_am62(+) rtc_ti_k3(+) rti_wdt(+) tidss drm_dma_helper j721e_csi2rx videobuf2_dma_contig drm_kms_helper m_can_platform m_can videobuf2_memops syscopyarea sysfillrect videobuf2_v4l2 sysimgblt videobuf2_common fb_sys_fops v4l2_async ti_k3_m4_remoteproc ti_k3_common can_dev videodev drm snd_soc_davinci_mcasp mcrc snd_soc_ti_udma sa2ul drm_panel_orientation_quirks cdns_dphy_rx snd_soc_ti_edma mc pruss snd_soc_ti_sdma snd_soc_tlv320aic3x_i2c snd_soc_tlv320aic3x optee_rng rng_core ip_tables x_tables ipv6
    root@sbc7138:~# 
    root@sbc7138:~# echo "LVDS-1: 1280x720@60" > /sys/kernel/debug/dri/0/force_connector
    -bash: /sys/kernel/debug/dri/0/force_connector: limited authority
    root@sbc7138:~# 
    root@sbc7138:~# cat /sys/kernel/debug/dri/0/LVDS-1/status
    cat: /sys/kernel/debug/dri/0/LVDS-1/status: There is no such file or directory
    root@sbc7138:~# 
    root@sbc7138:~# ls /sys/kernel/debug/dri/0/LVDS-1/
    edid_override  force  output_bpc  vrr_range
    root@sbc7138:~# 
    root@sbc7138:~# cat /sys/class/backlight/backlight-lvds/max_brightness
    255
    root@sbc7138:~# cat /sys/class/backlight/backlight-lvds/brightness
    255
    root@sbc7138:~# 
    root@sbc7138:~# echo 128 > /sys/class/backlight/backlight-lvds/brightness
    root@sbc7138:~# 
    root@sbc7138:~# echo 1 > /sys/class/backlight/backlight-lvds/brightness
    root@sbc7138:~# 
    root@sbc7138:~# echo 255 > /sys/class/backlight/backlight-lvds/brightness
    root@sbc7138:~# 
    root@sbc7138:~# ls /sys/kernel/debug/dri/0/LVDS-1/
    edid_override  force  output_bpc  vrr_range

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    由于现在您正在尝试配置 LVDS、我将再次向您询问相同的问题:

    您使用的是哪个 SDK?
    您能否参考 SDK 中的这个示例: https://git.ti.com/cgit/ti-linux-kernel/ti-linux-kernel/tree/arch/arm64/boot/dts/ti/k3-am625-sk-microtips-mf101hie-panel.dtso?h=ti-linux-6.12.y 并以这种方式创建 DTS、面板时序在 panel-simple.c 或等效器件中定义。

    您使用的是单链路还是双链路 LVDS?
    这是定制板吗?
    同时分享以下成果:

    kmsprint
    modetest -M tidss
    kmstest

    运行 kmstest 时、还可以分享您在屏幕上看到的内容。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    *好、我使用的 SDK 版本是:  ti-processor-sdk-linux-am62xx-evm-09.02.01.10-Linux-x86-Install.bin

    *是、这是一个 定制的电路板。

    *我使用的是单链路 LVDS。

    *我运行 kmstest 工具,但没有找到它。 我认为这应该是因为我自己重建了一个 Debian 系统。 这些工具可以在 SDK 中找到吗? 我没有找到它们。

    rxw@PowerEdge-T440:~/sbc7138/board-support$ 
    rxw@PowerEdge-T440:~/sbc7138/board-support$ find -name kmsprint
    rxw@PowerEdge-T440:~/sbc7138/board-support$ 
    rxw@PowerEdge-T440:~/sbc7138/board-support$ find -name kmstest
    rxw@PowerEdge-T440:~/sbc7138/board-support$ 
    rxw@PowerEdge-T440:~/sbc7138/board-support$ find -name modetest
    rxw@PowerEdge-T440:~/sbc7138/board-support$ 
    

    root@sbc7138:~# kmsprint
    -bash: kmsprint:Command Not found
    root@sbc7138:~# 
    root@sbc7138:~# modetest -M tidss
    -bash: modetest:Command Not found
    root@sbc7138:~# 
    root@sbc7138:~# kmstest
    -bash: kmstest:Command Not found
    root@sbc7138:~# 
    root@sbc7138:~# lsmod | grep km
    drm_kms_helper        184320  4 drm_dma_helper,tidss
    syscopyarea            16384  1 drm_kms_helper
    sysfillrect            16384  1 drm_kms_helper
    sysimgblt              16384  1 drm_kms_helper
    fb_sys_fops            16384  1 drm_kms_helper
    drm                   561152  5 drm_kms_helper,drm_dma_helper,tidss,panel_lvds
    root@sbc7138:~# 

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我尝试引用: git.ti.com/.../k3-am625-sk-microtips-mf101hie-pane L.toso?h=ti-linux-6.12.y、但存在编译异常。 它没有 oldi0和 oldi1

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    这是我的最新日志。 根据日志、LVDS 已正常初始化。 目前、已测量 CLK 和数据信号、但仍然没有显示。

    Debian GNU/Linux comes with ABSOLUTELY NO WARRANTY, to the extent
    permitted by applicable law.
    [   24.425543] broken atomic modeset userspace detected, disabling atomic
    root@sbc7138:~# [   25.951321] broken atomic modeset userspace detected, disabling atomic
    
    root@sbc7138:~# 
    root@sbc7138:~# dmesg | grep lvds
    [   10.464313] platform 30200000.dss: Fixed dependency cycle(s) with /panel_lvds
    [   10.471669] platform panel_lvds: Fixed dependency cycle(s) with /bus@f0000/dss@30200000
    root@sbc7138:~# 
    root@sbc7138:~# dmesg | grep panel
    [   10.464313] platform 30200000.dss: Fixed dependency cycle(s) with /panel_lvds
    [   10.471669] platform panel_lvds: Fixed dependency cycle(s) with /bus@f0000/dss@30200000
    [   19.051048] Modules linked in: k3_j72xx_bandgap(+) rtc_ti_k3(+) rti_wdt(+) tidss ti_k3_m4_remoteproc(+) can_dev drm_dma_helper j721e_csi2rx drm_kms_helper videobuf2_dma_contig syscopyarea ti_k3_common videobuf2_memops videobuf2_v4l2 sysfillrect videobuf2_common sysimgblt v4l2_async fb_sys_fops mcrc snd_soc_davinci_mcasp drm videodev sa2ul snd_soc_ti_udma drm_panel_orientation_quirks cdns_dphy_rx snd_soc_ti_edma snd_soc_ti_sdma pruss mc snd_soc_tlv320aic3x_i2c snd_soc_tlv320aic3x optee_rng rng_core ip_tables x_tables ipv6
    root@sbc7138:~# 
    root@sbc7138:~# dmesg | grep drm
    [   19.051048] Modules linked in: k3_j72xx_bandgap(+) rtc_ti_k3(+) rti_wdt(+) tidss ti_k3_m4_remoteproc(+) can_dev drm_dma_helper j721e_csi2rx drm_kms_helper videobuf2_dma_contig syscopyarea ti_k3_common videobuf2_memops videobuf2_v4l2 sysfillrect videobuf2_common sysimgblt v4l2_async fb_sys_fops mcrc snd_soc_davinci_mcasp drm videodev sa2ul snd_soc_ti_udma drm_panel_orientation_quirks cdns_dphy_rx snd_soc_ti_edma snd_soc_ti_sdma pruss mc snd_soc_tlv320aic3x_i2c snd_soc_tlv320aic3x optee_rng rng_core ip_tables x_tables ipv6
    [   19.897052] [drm] Initialized tidss 1.0.0 20180215 for 30200000.dss on minor 0
    [   19.951426] tidss 30200000.dss: [drm] fb0: tidssdrmfb frame buffer device
    root@sbc7138:~# 
    root@sbc7138:~# dmesg | grep dss
    [   10.464313] platform 30200000.dss: Fixed dependency cycle(s) with /panel_lvds
    [   10.471669] platform panel_lvds: Fixed dependency cycle(s) with /bus@f0000/dss@30200000
    [   19.051048] Modules linked in: k3_j72xx_bandgap(+) rtc_ti_k3(+) rti_wdt(+) tidss ti_k3_m4_remoteproc(+) can_dev drm_dma_helper j721e_csi2rx drm_kms_helper videobuf2_dma_contig syscopyarea ti_k3_common videobuf2_memops videobuf2_v4l2 sysfillrect videobuf2_common sysimgblt v4l2_async fb_sys_fops mcrc snd_soc_davinci_mcasp drm videodev sa2ul snd_soc_ti_udma drm_panel_orientation_quirks cdns_dphy_rx snd_soc_ti_edma snd_soc_ti_sdma pruss mc snd_soc_tlv320aic3x_i2c snd_soc_tlv320aic3x optee_rng rng_core ip_tables x_tables ipv6
    [   19.897052] [drm] Initialized tidss 1.0.0 20180215 for 30200000.dss on minor 0
    [   19.951426] tidss 30200000.dss: [drm] fb0: tidssdrmfb frame buffer device
    root@sbc7138:~# 
    root@sbc7138:~# ls /sys/kernel/debug/dri/0
    clients  crtc-0  framebuffer  gem_names  internal_clients  LVDS-1  name  state
    root@sbc7138:~# 
    root@sbc7138:~# cat /sys/kernel/debug/dri/0/state
    plane[31]: plane-0
            crtc=crtc-0
            fb=48
                    allocated by = [fbcon]
                    refcount=2
                    format=XR24 little-endian (0x34325258)
                    modifier=0x0
                    size=1280x800
                    layers:
                            size[0]=1280x800
                            pitch[0]=5120
                            offset[0]=0
                            obj[0]:
                                    name=0
                                    refcount=3
                                    start=00100000
                                    size=4096000
                                    imported=no
                                    dma_addr=0x00000000f8200000
                                    vaddr=0000000016a01b1d
            crtc-pos=1280x800+0+0
            src-pos=1280.000000x800.000000+0.000000+0.000000
            rotation=1
            normalized-zpos=0
            color-encoding=ITU-R BT.601 YCbCr
            color-range=YCbCr full range
    plane[41]: plane-1
            crtc=(null)
            fb=0
            crtc-pos=0x0+0+0
            src-pos=0.000000x0.000000+0.000000+0.000000
            rotation=1
            normalized-zpos=1
            color-encoding=ITU-R BT.601 YCbCr
            color-range=YCbCr full range
    crtc[38]: crtc-0
            enable=1
            active=1
            self_refresh_active=0
            planes_changed=1
            mode_changed=0
            active_changed=0
            connectors_changed=0
            color_mgmt_changed=0
            plane_mask=1
            connector_mask=1
            encoder_mask=1
            mode: "1280x800": 59 71100 1280 1350 1354 1442 800 815 819 840 0x48 0xa
    connector[40]: LVDS-1
            crtc=crtc-0
            self_refresh_aware=0
            max_requested_bpc=0
    root@sbc7138:~# 
    root@sbc7138:~# 
    root@sbc7138:~# ls /sys/kernel/debug/dri/0/LVDS-1/
    edid_override  force  output_bpc  vrr_range
    root@sbc7138:~# 
    root@sbc7138:~# cat /sys/kernel/debug/dri/0/LVDS-1/force
    unspecified
    root@sbc7138:~# 
    root@sbc7138:~# echo on > /sys/kernel/debug/dri/0/LVDS-1/force
    root@sbc7138:~# 
    root@sbc7138:~# cat /sys/kernel/debug/dri/0/LVDS-1/force
    on
    root@sbc7138:~# 

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    使用此处生成的 modetest 二进制文件: https://software-dl.ti.com/processor-sdk-linux/esd/AM62X/latest/exports/docs/linux/How_to_Guides/Target/How_to_boot_quickly.html#additional-notes 

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我找不到要从此处下载的工具。 我尝试在 SDK 中使用文件系统。 当我替换 SDK 的文件系统时、可以显示 LVDS。 似乎是由于文件系统造成的。 因为我是 dtb、Image ko 文件与之前都相同。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、

    请使用以下链接中提供的"modetest"下载按钮:


    根据您的评论、您的问题是否已解决?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    是的、我的问题已经解决。 我重新编译了一个文件系统、现在 LVDS 可以正常显示。 非常感谢您的答复