This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] PROCESSOR-SDK-AM62X:SDK11:引导停止且没有错误消息-已在 SDK10上使用

Guru**** 2378650 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1517081/processor-sdk-am62x-sdk11-boot-stopping-without-error-messages---worked-on-sdk10

器件型号:PROCESSOR-SDK-AM62X

工具/软件:

我刚刚从10.01.10.04更新为最新的11.00.09.04、现在我无法再次启动电路板。 引导通过 U-boot 进入内核、但在出现任何错误消息之前挂起、我想这可能会在从 u-boot 2024.04更改为2025.01时有一些需要做的事情。 我只是尝试先更改引导加载程序。 内核和文件系统仍然与我在 SDK 10中使用的相同。 我也快速尝试了更新的内核,但它没有改变任何东西。 以下是引导日志:

U-Boot SPL 2025.01-gcd91d7360181-dirty (May 21 2025 - 16:23:48 +0200)
SYSFW ABI: 4.0 (firmware rev 0x000b '11.0.7--v11.00.07 (Fancy Rat)')
SPL initial stack usage: 1952 bytes
Trying to boot from MMC2


U-Boot 2025.01-gcd91d7360181-dirty (May 21 2025 - 16:23:48 +0200)

SoC:   AM62X SR1.0 GP
Model: MYiR SOM AM62x
DRAM:  2 GiB
Core:  80 devices, 32 uclasses, devicetree: separate
MMC:   mmc@fa10000: 0, mmc@fa00000: 1
Loading Environment from nowhere... OK
In:    serial
Out:   serial
Err:   serial
BUCK1: vdd_core is 0.85v
Net:   eth0: ethernet@8000000port@1

Hit any key to stop autoboot:  0
switch to partitions #0, OK
mmc1 is current device
SD/MMC found on device 1
Failed to load 'uEnv.txt'
27144704 bytes read in 1084 ms (23.9 MiB/s)
63393 bytes read in 8 ms (7.6 MiB/s)
Working FDT set to 88000000
## Flattened Device Tree blob at 88000000
   Booting using the fdt blob at 0x88000000
Working FDT set to 88000000
   Loading Device Tree to 000000008feed000, end 000000008fffffff ... OK
Working FDT set to 8feed000

Starting kernel ...

[    0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
[    0.000000] Linux version 6.6.58-ti-01497-ga7758da17c28-dirty (oe-user@oe-host) (aarch64-poky-linux-gcc (GCC) 13.3.0, GNU ld (GNU Binutils) 2.42.0.20240723) #1 SMP PREEMPT Wed Nov 27 13:23:15 UTC 2024
[    0.000000] KASLR disabled due to lack of seed
[    0.000000] Machine model: Texas Instruments K3 AM625 SoC
[    0.000000] earlycon: ns16550a0 at MMIO32 0x0000000002800000 (options '')
[    0.000000] printk: bootconsole [ns16550a0] enabled
[    0.000000] efi: UEFI not found.
[    0.000000] Reserved memory: created CMA memory pool at 0x00000000f8000000, size 128 MiB
[    0.000000] OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x00000000f8000000..0x00000000ffffffff (131072 KiB) map reusable linux,cma
[    0.000000] OF: reserved mem: 0x000000009c700000..0x000000009c7fffff (1024 KiB) map non-reusable ramoops@9c700000
[    0.000000] Reserved memory: created DMA memory pool at 0x000000009c800000, size 3 MiB
[    0.000000] OF: reserved mem: initialized node ipc-memories@9c800000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x000000009c800000..0x000000009cafffff (3072 KiB) nomap non-reusable ipc-memories@9c800000
[    0.000000] Reserved memory: created DMA memory pool at 0x000000009cb00000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node m4f-dma-memory@9cb00000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x000000009cb00000..0x000000009cbfffff (1024 KiB) nomap non-reusable m4f-dma-memory@9cb00000
[    0.000000] Reserved memory: created DMA memory pool at 0x000000009cc00000, size 14 MiB
[    0.000000] OF: reserved mem: initialized node m4f-memory@9cc00000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x000000009cc00000..0x000000009d9fffff (14336 KiB) nomap non-reusable m4f-memory@9cc00000
[    0.000000] Reserved memory: created DMA memory pool at 0x000000009da00000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node r5f-dma-memory@9da00000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x000000009da00000..0x000000009dafffff (1024 KiB) nomap non-reusable r5f-dma-memory@9da00000
[    0.000000] Reserved memory: created DMA memory pool at 0x000000009db00000, size 12 MiB
[    0.000000] OF: reserved mem: initialized node r5f-memory@9db00000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x000000009db00000..0x000000009e6fffff (12288 KiB) nomap non-reusable r5f-memory@9db00000
[    0.000000] OF: reserved mem: 0x000000009e780000..0x000000009e7fffff (512 KiB) nomap non-reusable tfa@9e780000
[    0.000000] OF: reserved mem: 0x000000009e800000..0x000000009fffffff (24576 KiB) nomap non-reusable optee@9e800000
[    0.000000] Zone ranges:
[    0.000000]   DMA      [mem 0x0000000080000000-0x00000000ffffffff]
[    0.000000]   DMA32    empty
[    0.000000]   Normal   empty
[    0.000000] Movable zone start for each node
[    0.000000] Early memory node ranges
[    0.000000]   node   0: [mem 0x0000000080000000-0x000000009c7fffff]
[    0.000000]   node   0: [mem 0x000000009c800000-0x000000009e6fffff]
[    0.000000]   node   0: [mem 0x000000009e700000-0x000000009e77ffff]
[    0.000000]   node   0: [mem 0x000000009e780000-0x000000009fffffff]
[    0.000000]   node   0: [mem 0x00000000a0000000-0x00000000ffffffff]
[    0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000000ffffffff]
[    0.000000] psci: probing for conduit method from DT.
[    0.000000] psci: PSCIv1.1 detected in firmware.
[    0.000000] psci: Using standard PSCI v0.2 function IDs
[    0.000000] psci: Trusted OS migration not required
[    0.000000] psci: SMC Calling Convention v1.5
[    0.000000] percpu: Embedded 29 pages/cpu s80552 r8192 d30040 u118784
[    0.000000] Detected VIPT I-cache on CPU0
[    0.000000] CPU features: detected: GIC system register CPU interface
[    0.000000] CPU features: detected: ARM erratum 845719
[    0.000000] alternatives: applying boot alternatives
[    0.000000] Kernel command line: console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000 mtdparts=spi-nand0:512k(ospi_nand.tiboot3),2m(ospi_nand.tispl),4m(ospi_nand.u-boot),256k(ospi_nand.env),256k(ospi_nand.env.backup),98048k@32m(ospi_nand.rootfs),256k@130816k(ospi_nand.phypattern) root=PARTUUID=076c4a2a-02 rw rootfstype=ext4 rootwait
[    0.000000] Dentry cache hash table entries: 262144 (order: 9, 2097152 bytes, linear)
[    0.000000] Inode-cache hash table entries: 131072 (order: 8, 1048576 bytes, linear)
[    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 516096
[    0.000000] mem auto-init: stack:all(zero), heap alloc:off, heap free:off
[    0.000000] software IO TLB: area num 2.
[    0.000000] software IO TLB: mapped [mem 0x00000000f1800000-0x00000000f5800000] (64MB)
[    0.000000] Memory: 1774428K/2097152K available (14144K kernel code, 2252K rwdata, 4920K rodata, 5056K init, 517K bss, 191652K reserved, 131072K cma-reserved)
[    0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
[    0.000000] ftrace: allocating 46447 entries in 182 pages
[    0.000000] ftrace: allocated 182 pages with 5 groups
[    0.000000] trace event string verifier disabled
[    0.000000] rcu: Preemptible hierarchical RCU implementation.
[    0.000000] rcu:     RCU event tracing is enabled.
[    0.000000] rcu:     RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=2.
[    0.000000]  Trampoline variant of Tasks RCU enabled.
[    0.000000]  Rude variant of Tasks RCU enabled.
[    0.000000]  Tracing variant of Tasks RCU enabled.
[    0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[    0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2
[    0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[    0.000000] GICv3: GIC: Using split EOI/Deactivate mode
[    0.000000] GICv3: 256 SPIs implemented
[    0.000000] GICv3: 0 Extended SPIs implemented
[    0.000000] Root IRQ handler: gic_handle_irq
[    0.000000] GICv3: GICv3 features: 16 PPIs
[    0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000001880000
[    0.000000] ITS [mem 0x01820000-0x0182ffff]
[    0.000000] GIC: enabling workaround for ITS: Socionext Synquacer pre-ITS
[    0.000000] ITS@0x0000000001820000: Devices Table too large, reduce ids 20->19
[    0.000000] ITS@0x0000000001820000: allocated 524288 Devices @80800000 (flat, esz 8, psz 64K, shr 0)
[    0.000000] ITS: using cache flushing for cmd queue
[    0.000000] GICv3: using LPI property table @0x0000000080180000
[    0.000000] GIC: using cache flushing for LPI property table
[    0.000000] GICv3: CPU0: using allocated LPI pending table @0x0000000080190000
[    0.000000] rcu: srcu_init: Setting srcu_struct sizes based on contention.
[    0.000000] arch_timer: cp15 timer(s) running at 200.00MHz (phys).
[    0.000000] clocksource: arch_sys_counter: mask: 0x3ffffffffffffff max_cycles: 0x2e2049d3e8, max_idle_ns: 440795210634 ns
[    0.000001] sched_clock: 58 bits at 200MHz, resolution 5ns, wraps every 4398046511102ns

有什么想法,为什么和它停止的地方?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、

    我其实不知道什么会导致这个停止。

    我尝试在 AM62x EVM 上使用 SDK11.0 U-Boot 引导 SDK10.0内核、并成功引导至 Linux 登录提示符。 因此、我认为您将 u-boot 2025.01与 SDK10.1内核混合并不会导致此引导问题。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我厌倦了新的内核(因为我得到它引导与旧的 u-boot ),没有变化。 我是否必须更改设备树上的内容? 是否有必要的更改? 可能有些时钟未正确初始化? 我还提高了日志级别、但没有收到更多消息。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、

    我想不到 U-boot 2025.01中会导致问题的任何变化。

    您是否在平台上使用 main uart0作为 Linux 控制台? 不同的 UART 端口?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    是的、我使用 MAIN_uart0作为控制台端口。  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您的电路板是否有 JTAG 连接? 您能否在 CCS 中连接到 A53_0以查看 PC 寄存器所在的位置?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我为 am62x 开发板编译了 u-boot、然后我就能够启动了。 现在、我必须了解问题是我的配置还是设备树。