This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] PROCESSOR-SDK-J7200:使用 SDK-LINUX-version 10.01.08.01 运行与 Linux 并行的 MCU-APP

Guru**** 2468610 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1525863/processor-sdk-j7200-running-an-mcu-app-in-parallel-to-linux-using-sdk-linux-version-10-01-08-01

器件型号:PROCESSOR-SDK-J7200

工具/软件:

您好、专家、

我们有 J7200 评估板、需要与定制 MCU-R5F-firmware 并行运行 Linux。 为了实现这一目标、我们讨论了从 J7200-Linux-SDK(版本 10.01.08.01)构建 U-Boot 和 SPL、因为按照我们的理解、文件 tispl.bin 包含适用于 MCU 单元的应用、即根据 SDK 软件开发人员指南中的 3.1.1.1 构建的 R5 DM FW。

那么、我们的问题是、要在 Linux 并行使用我们的自定义 MCU-R5F-application、需要做什么?

或者、您是否知道在哪里可以找到合适的指导方法或示例?

到目前为止、我们发现的关于这个主题的许多信息似乎有些过时。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好:

    根据上述说明、我了解到您希望构建自己的自定义 DM 二进制文件以在 MCU 域 R5F 上运行。

    您希望在区经理的基础上介绍哪些附加功能?

    此致、

    Keerthy  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    好的、现在我想办法了、如何使 r5-mcu 应用程序使用 SPL 运行:我基本上在 k3-j7200-binman.dtsi-file 中将其设置为 ti-dm。

    不过、我遇到了另一个问题:在使用 RTOS-SDK 构建的自定义二进制文件时、引导过程会失败、而不是默认的二进制文件 (board-support/prebuilt-images/ti-dm/j7200/ipc_echo_testb_mcu1_0_release_strip.xer5f)。

     

    U-Boot SPL 2024.04-ti-ga970f6e51043 (Nov 13 2024 - 14:26:23 +0000)
    SYSFW ABI: 4.0 (firmware rev 0x000a '10.1.6--v10.01.06 (Fiery Fox)')
    Trying to boot from MMC2
    Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
    Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
    Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
    Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
    Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
    Loading Environment from nowhere... OK
    ## No elf image at address 0x89000000
    Starting ATF on ARM64 core...
    
    NOTICE:  BL31: v2.12.0(release):11.00.09-dirty
    NOTICE:  BL31: Built : 12:35:58, Mar 24 2025
    ERROR:   Timeout waiting for thread SP_RESPONSE to fill
    ERROR:   Thread SP_RESPONSE verification failed (-60)
    ERROR:   Message receive failed (-60)
    ERROR:   Failed to get response (-60)
    ERROR:   Transfer send failed (-60)
    ERROR:   Timeout waiting for thread SP_RESPONSE to fill
    ERROR:   Thread SP_RESPONSE verification failed (-60)
    ERROR:   Message receive failed (-60)
    ERROR:   Failed to get response (-60)
    ERROR:   Transfer send failed (-60)
    ERROR:   Unable to query firmware capabilities (-60)
    I/TC:
    I/TC: OP-TEE version: 4.5.0-73-gef1ebdc23-dev (gcc version 13.3.0 (GCC)) #1 Tue Feb  4 11:33:18 UTC 2025 aarch64
    I/TC: WARNING: This OP-TEE configuration might be insecure!
    I/TC: WARNING: Please check optee.readthedocs.io/.../porting_guidelines.html
    I/TC: Primary CPU initializing
    I/TC: GIC redistributor base address not provided
    I/TC: Assuming default GIC group status and modifier
    E/TC:0 0 k3_sec_proxy_verify_thread:108 Queue is busy
    E/TC:0 0 k3_sec_proxy_recv:196 Thread SEC_PROXY_RESPONSE_THREAD verification failed. ret = -65523
    E/TC:0 0 ti_sci_do_xfer:120 Message receive failed (-65523)
    E/TC:0 0 ti_sci_init:480 Unable to communicate with control firmware (-65523)
    E/TC:0 0 do_init_calls:22 early_initcall __text_start + 0x00072db8 failed
    E/TC:0 0 k3_sec_proxy_verify_thread:108 Queue is busy
    E/TC:0 0 k3_sec_proxy_recv:196 Thread SEC_PROXY_RESPONSE_THREAD verification failed. ret = -65523
    E/TC:0 0 ti_sci_do_xfer:120 Message receive failed (-65523)
    E/TC:0 0 sa2ul_init:61 Failed to get SA2UL device
    E/TC:0 0 do_init_calls:22 service_initcall __text_start + 0x00073120 failed
    E/TC:0 0 k3_sec_proxy_verify_thread:108 Queue is busy
    E/TC:0 0 k3_sec_proxy_recv:196 Thread SEC_PROXY_RESPONSE_THREAD verification failed. ret = -65523
    E/TC:0 0 ti_sci_do_xfer:120 Message receive failed (-65523)
    E/TC:0 0 k3_sec_proxy_verify_thread:108 Queue is busy
    E/TC:0 0 k3_sec_proxy_recv:196 Thread SEC_PROXY_RESPONSE_THREAD verification failed. ret = -65523
    E/TC:0 0 ti_sci_do_xfer:120 Message receive failed (-65523)
    E/TC:0 0 k3_sec_proxy_verify_thread:108 Queue is busy
    E/TC:0 0 k3_sec_proxy_recv:196 Thread SEC_PROXY_RESPONSE_THREAD verification failed. ret = -65523
    E/TC:0 0 ti_sci_do_xfer:120 Message receive failed (-65523)
    E/TC:0 0 tee_otp_get_hw_unique_key:104 Could not get HUK
    E/TC:0 0 do_init_calls:22 service_initcall __text_start + 0x00073148 failed
    E/TC:0 0
    E/TC:0 0 Core data-abort at address 0x14 (translation fault)
    E/TC:0 0  esr 0x96000005  ttbr0 0x9e8af000   ttbr1 0x00000000   cidr 0x0
    E/TC:0 0  cpu #0          cpsr 0x600003c4
    E/TC:0 0  x0  000000009e877000 x1  0000000000000000
    E/TC:0 0  x2  0000000000000000 x3  0000000000000000
    E/TC:0 0  x4  0000000000000030 x5  000000009e876d78
    E/TC:0 0  x6  00000000fffffff0 x7  00000000ffffffe8
    E/TC:0 0  x8  0000000000000008 x9  000000009e89fd00
    E/TC:0 0  x10 000000009e884040 x11 0000000000000008
    E/TC:0 0  x12 0000000000000020 x13 000000009e89fc70
    E/TC:0 0  x14 0000000000000000 x15 0000000000000000
    E/TC:0 0  x16 000000009e81c26c x17 0000000000000000
    E/TC:0 0  x18 0000000000000000 x19 000000009e8a0000
    E/TC:0 0  x20 000000009e8a0008 x21 000000009e877000
    E/TC:0 0  x22 000000009e877000 x23 000000009e877ef0
    E/TC:0 0  x24 000000009e876db0 x25 0000000000000000
    E/TC:0 0  x26 0000000000000000 x27 0000000000000000
    E/TC:0 0  x28 0000000000000000 x29 000000009e89ff90
    E/TC:0 0  x30 000000009e816984 elr 000000009e816994
    E/TC:0 0  sp_el0 000000009e89ff90
    E/TC:0 0 TEE load address @ 0x9e800000
    E/TC:0 0 Call stack:
    E/TC:0 0  0x9e816994
    E/TC:0 0  0x9e807c88
    E/TC:0 0  0x9e821d3c
    E/TC:0 0 Panic 'unhandled pageable abort' at /usr/src/debug/optee-os/4.5.0+git/core/arch/arm/kernel/abort.c:582 <abort_handler>
    E/TC:0 0 TEE load address @ 0x9e800000
    E/TC:0 0 Call stack:
    E/TC:0 0  0x9e8080fc
    E/TC:0 0  0x9e81e7d4
    E/TC:0 0  0x9e807854
    E/TC:0 0  0x9e804a68

    您是否知道如何解决该问题?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、

    您能否撤消任何自定义更改并仅构建默认  ipc_echo_testb_mcu1_0_release_strip.xer5f?

    然后尝试启动。 它应该会启动。 上述崩溃最有可能是因为 DM(设备管理器也称为 ipc_echo_testb_mcu1_0_release_strip.xer5f) 无法正常工作并且无法响应其他内核请求。

    - Keerthy