This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] AM623:运行 CQE 恢复

Guru**** 2469960 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1525151/am623-running-cqe-recovery

器件型号:AM623

工具/软件:

尊敬的专家

这是对该线程的扩展讨论、因为原始线程被锁定。

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1504295/am623-mmc0-running-cqe-recovery-problem

(1) 问题:我们发现 Linux UART 日志输出“mmc0:正在运行 CQE 恢复“,并且一些文件崩溃。 eMMC 在 HS200 上运行、我们已经确保在 uboot / Linux DTS 中禁用 DDR 模式、因为 AM62 不支持 eMMC DDR 模式。

(2) SDK:10.01.10.04

(3) eMMC 部件: THGBMUG6C1LBAIL (KIOXIA)

(4) SDIO0 (eMMC) 信号完整性:HS200 通过(硬件)

(5) SDIO0 (eMMC) 开关特性: HS200 Pass(硬件)

(6) 线索:如果我们降低速度到 HS 模式,“ CQE 恢复“消失

(7) 并非每块电路板都有相同的问题、据我所知、故障率约为 15%、我们仍在跟踪。  

(8) 错误日志。

日志 1 :  

[    4.711702] mmc0: running CQE recovery
[    4.735046] mmc0: running CQE recovery
[    4.758311] mmc0: running CQE recovery
[    4.766138] I/O error, dev mmcblk0, sector 102744 op 0x0:(READ) flags 0x3000 phys_seg 1 prio class 2
[    4.775291] EXT4-fs warning (device mmcblk0p1): htree_dirblock_to_tree:1082: inode #880: lblock 0: comm
systemd: error -5 reading directory block
[    4.788391] systemd[1]: tmp.mount: Failed to check directory /tmp: Input/output error
[    4.815487] mmc0: running CQE recovery
[    4.838846] mmc0: running CQE recovery
[    4.862113] mmc0: running CQE recovery
[    4.869930] I/O error, dev mmcblk0, sector 291832 op 0x0:(READ) flags 0x0 phys_seg 1 prio class 2

日志 2 :  

[   11.193981] mmc0: running CQE recovery
[   11.199428] Buffer I/O error on dev mmcblk0p1, logical block 0, lost sync page write
[   11.207195] EXT4-fs (mmcblk0p1): I/O error while writing superblock
[   11.229373] mmc0: running CQE recovery
[   11.252665] mmc0: running CQE recovery
[   11.275931] mmc0: running CQE recovery

第 3 章:我的心  

[    1.309542] mmc0: Command Queue Engine enabled
[    1.314030] mmc0: new HS200 MMC card at address 0001
[    1.319843] mmcblk0: mmc0:0001 008GB1 1.16 GiB
[    1.325811] mmc0: running CQE recovery
[    1.332062] mmc0: running CQE recovery
[    1.338170] GPT:Primary header thinks Alt. header is not at the end of the disk.
[    1.345632] GPT:2113535 != 2441215
[    1.349132] GPT:Alternate GPT header not at the end of the disk.
[    1.355233] GPT:2113535 != 2441215
[    1.358647] GPT: Use GNU Parted to correct GPT errors.
[    1.363807]  mmcblk0: p1 p2
[    1.367355] mmcblk0boot0: mmc0:0001 008GB1 4.00 MiB
[    1.373287] mmcblk0boot1: mmc0:0001 008GB1 4.00 MiB
[    1.379213] mmcblk0gp0: mmc0:0001 008GB1 2.55 GiB
[    1.385927] mmc0: running CQE recovery
[    1.392012] mmc0: running CQE recovery
[    1.397284] mmc0: running CQE recovery
[    1.402967]  mmcblk0gp0: p1 p2
[    1.406607] mmcblk0rpmb: mmc0:0001 008GB1 4.00 MiB, chardev (243:0)
[    1.474043] mmc2: Failed to initialize a non-removable card
[    2.730108] sdhci-am654 fa00000.mmc: Power on failed
[    2.771213] mmc1: SDHCI controller on fa00000.mmc [fa00000.mmc] using ADMA 64-bit
[    2.780358] mmc0: running CQE recovery
[    2.785587] mmc0: running CQE recovery
[    2.791585] mmc0: running CQE recovery\

第 4 章:我的心  

 1.205849] mmc2: CQHCI version 5.10
[    1.230661] mmc0: SDHCI controller on fa10000.mmc [fa10000.mmc] using ADMA 64-bit
[    1.238247] mmc2: SDHCI controller on fa20000.mmc [fa20000.mmc] using ADMA 64-bit
[    1.316005] mmc0: Command Queue Engine enabled
[    1.320483] mmc0: new HS200 MMC card at address 0001
[    1.326164] mmcblk0: mmc0:0001 008GB1 1.16 GiB
[    1.332067] mmc0: running CQE recovery
[    1.337534] mmc0: running CQE recovery
[    1.343268] mmc0: running CQE recovery
[    1.347344] I/O error, dev mmcblk0, sector 0 op 0x0:(READ) flags 0x0 phys_seg 1 prio class 2
[    1.355843] Buffer I/O error on dev mmcblk0, logical block 0, async page read

几个问题:  

(1) 据我所知、大多数已由 SDK  10.01.10.04 解决的 eMMC“CQE 恢复“错误都不是吗?

因为我认为 SDK 10.01.10.04 应该会更新有关 EXT_EP-12086 的补丁

https://sir.ext.ti.com/jira/browse/EXT_EP-12086?jql=text%20~%20%22running%20CQE%20recovery%22

(2) 如何跟踪我们针对 eMMC 问题进行了任何修改的 uboot / Linux 代码? 因为我想逐个检查...

(3) SDK 11 与 SDK 10.01.10.04 之间关于 eMMC 代码更新有何差异(更新)? 我还跟踪了该主题、似乎仍然在通过 SDK11 来跟踪 eMMC 问题

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1513257/am623-copy-files-to-emmc-trigger-cqe-error/5846867?tisearch=e2e-sitesearch&keymatch=am62%2525252520mmc0%2525252520running%2525252520CQE%2525252520recovery#5846867

 

我们需要一些调试方向、需要您的建议。

非常感谢

Gibbs