This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] 处理器-SDK-AM437X:AM437X + wq9101 使用 Bluez protoco 连接 PC 蓝牙:连接失败:org.bluez.Error.failed br-connection-profile-unavailable

Guru**** 2473260 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1530822/-sdk-am437x-am437x-wq9101-use-bluez-protoco-to-connect-pc-bluetooth-failed-to-connect-org-bluez-error-failed-br-connection-profile-unavailable

器件型号:PROCESSOR-SDK-AM437X

工具/软件:

硬件架构:μ s

TI AM437x(__LW_AT__ARM Cortex-A9)作为主处理器。

wq9101 Wi-Fi/BT 芯片连接接口为 UART

软件堆栈:μ s

Bluez 协议:用于蓝牙通信。

错误信使:μ s

ROOT@AM437X-EVM:~# sudo bluetoothctl connect 58:1C:F8:A4:F2:C1
尝试连接到 58:1C:F8:A4:F2:C1
连接失败:org.bluez.Error.failed br-connection-profile-unavailable

这个错误怎么处理呢?μ s