工具/软件:
TI 团队大家好、
我的一个自定义模型在 TIDL ONNX Runtime Execution Provider 进行推理时卡住了。
您能否提供有关对此问题进行故障排除的提示或建议?
该模型是使用 TIDL 编译器编译的自定义 ONNX 模型。
编译成功完成。
-使用 x86 仿真器模式进行推理:**Success **
-对 EVM 的推理:**失败**
请查看下面的日志输出:
libtidl_onnxrt_EP loaded 0x270aad80 Final number of subgraphs created are : 16, - Offloaded Nodes - 380, Total Nodes - 420 APP: Init ... !!! 52967.375819 s: MEM: Init ... !!! 52967.375894 s: MEM: Initialized DMA HEAP (fd=5) !!! 52967.376090 s: MEM: Init ... Done !!! 52967.376124 s: IPC: Init ... !!! 52967.394312 s: IPC: Init ... Done !!! REMOTE_SERVICE: Init ... !!! REMOTE_SERVICE: Init ... Done !!! 52967.398984 s: GTC Frequency = 200 MHz APP: Init ... Done !!! 52967.399171 s: VX_ZONE_INFO: Globally Enabled VX_ZONE_ERROR 52967.399201 s: VX_ZONE_INFO: Globally Enabled VX_ZONE_WARNING 52967.399211 s: VX_ZONE_INFO: Globally Enabled VX_ZONE_INFO 52967.400335 s: VX_ZONE_INFO: [tivxPlatformCreateTargetId:134] Added target MPU-0 52967.401090 s: VX_ZONE_INFO: [tivxPlatformCreateTargetId:134] Added target MPU-1 52967.401509 s: VX_ZONE_INFO: [tivxPlatformCreateTargetId:134] Added target MPU-2 52967.402237 s: VX_ZONE_INFO: [tivxPlatformCreateTargetId:134] Added target MPU-3 52967.402335 s: VX_ZONE_INFO: [tivxInitLocal:126] Initialization Done !!! 52967.402374 s: VX_ZONE_INFO: Globally Disabled VX_ZONE_INFO 52967.817573 s: VX_ZONE_ERROR: [ownContextSendCmd:912] Command ack message returned failure cmd_status: -1 52967.817842 s: VX_ZONE_ERROR: [ownNodeKernelInit:604] Target kernel, TIVX_CMD_NODE_CREATE failed for node TIDLNode 52967.817871 s: VX_ZONE_ERROR: [ownNodeKernelInit:605] Please be sure the target callbacks have been registered for this core 52967.817881 s: VX_ZONE_ERROR: [ownNodeKernelInit:606] If the target callbacks have been registered, please ensure no errors are occurring within the create callback of this k 52967.817898 s: VX_ZONE_ERROR: [ownGraphNodeKernelInit:690] kernel init for node 0, kernel com.ti.tidl:4:3 ... failed !!! 52967.817964 s: VX_ZONE_ERROR: [ TIDL subgraph cls_signal ] Node kernel init failed 52967.817976 s: VX_ZONE_ERROR: [ TIDL subgraph cls_signal ] Graph verify failed TIDL_RT_OVX: ERROR: Verifying TIDL graph ... Failed !!! TIDL_RT_OVX: ERROR: Verify OpenVX graph failed
推理应用程序是我们自己使用 ONNX Runtime API 的自定义 Python 程序、具有以下执行提供程序列表:
`EP_LIST =[“TIDLExecutionProvider",“,"CPUExecutionProvider"]、"CPUExecutionProvider"]`“`</s>“
提前感谢您的支持。