This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] SK-AM62A-LP:在 SDK 10.01 上引导挂起、在 SDK 09.02 上工作正常

Guru**** 2477255 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1535625/sk-am62a-lp-boot-hangs-on-sdk-10-01-works-fine-on-sdk-09-02

器件型号:SK-AM62A-LP


工具/软件:

您好、

我刷写了 SDK 10.01 中的预编译映像、并注意到以下 U-Boot 消息。

U-Boot 2024.04-ti-ga970f6e51043 (Nov 13 2024 - 14:26:23 +0000)
   
SoC:   AM62AX SR1.0 HS-FS
Model: Texas Instruments AM62A7 SK
DRAM:  2 GiB (effective 4 GiB)
Core:  87 devices, 30 uclasses, devicetree: separate
MMC:   mmc@fa10000: 0, mmc@fa00000: 1
Loading Environment from nowhere... OK
In:    serial@2800000
Out:   serial@2800000
Err:   serial@2800000
Net:   eth0: ethernet@8000000port@1

但是、系统在引导期间卡住。

switch to partitions #0, OK
mmc1 is current device
** No partition table - mmc 1 **
** No partition table - mmc 1 **
Couldn't find partition mmc 1:2
Can't set block device
** No partition table - mmc 1 **
Couldn't find partition mmc 1:2
Can't set block device
libfdt fdt_check_header(): FDT_ERR_BADMAGIC
No FDT memory address configured. Please configure
the FDT address via "fdt addr <address>" command.
Aborting!
Bad Linux ARM64 Image magic!
Scanning for bootflows in all bootdevs
Seq  Method       State   Uclass    Part  Name                      Filename
---  -----------  ------  --------  ----  ------------------------  ----------------
Scanning global bootmeth 'efi_mgr':
No EFI system partition
No EFI system partition
Failed to persist EFI variables
No EFI system partition
Failed to persist EFI variables
No EFI system partition
Failed to persist EFI variables
No EFI system partition
Failed to persist EFI variables
No EFI system partition
Failed to persist EFI variables
  0  efi_mgr      ready   (none)       0  <NULL>
** Booting bootflow '<NULL>' with efi_mgr
Loading Boot0000 'mmc 1' failed
Loading Boot0001 'mmc 0' failed
EFI boot manager: Cannot load any image
Boot failed (err=-14)
Scanning bootdev 'mmc@fa00000.bootdev':
Scanning bootdev 'mmc@fa10000.bootdev':
Bus usb@31100000: generic_phy_get_bulk : no phys property

我自己也构建了 SDK 10.01 映像、它显示了相同 U-Boot 消息下的相同行为。

但是、当我从 SDK 09.02 刷写预编译映像时、电路板会启动并正常工作。

对于如何调试该问题、您有何建议?

谢谢。