This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] AM62A7-Q1:tiovxmosiac 错误

Guru**** 2589300 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1542808/am62a7-q1-tiovxmosiac-error

器件型号:AM62A7-Q1


工具/软件:

当通过 gstreamer 使用 tiovxmosaic 时、我得到以下错误。

在 SK 板上、该命令工作正常。

我们使用 SDK 版本 10、而是使用定制板、而不是 SK 板。

我应该检查什么?

GST:

gst-launch-1.0 \
v4l2src device=/dev/video4 io-mode=5 ! queue max-size-buffers=1 leaky=2 ! video/x-raw,width=1920,height=1080,framerate=30/1,format=UYVY ! \
tiovxdlcolorconvert ! \
video/x-raw,format=NV12, width=1920,height=1080 ! textoverlay text="VIDEO4 (/dev/video4)" ! queue ! mosaic.sink_0 \
v4l2src device=/dev/video3 io-mode=5  ! queue max-size-buffers=1 leaky=2 ! video/x-raw,width=1920,height=1080,framerate=30/1,format=UYVY ! \
tiovxdlcolorconvert ! \
video/x-raw,format=NV12, width=1920,height=1080 ! textoverlay text="VIDEO3 (/dev/video3)" ! queue ! mosaic.sink_1 \
tiovxmosaic name=mosaic \
sink_0::startx="<0>" sink_0::starty="<0>" sink_0::widths="<1920>" sink_0::heights="<540>" \
sink_1::startx="<0>" sink_1::starty="<540>" sink_1::widths="<1920>" sink_1::heights="<540>" ! \
queue ! video/x-raw, width=1920, height=1080 ! queue ! kmssink driver-name=tidss sync=false force-modesetting=true

APP: Init ... !!!
   969.185955 s: MEM: Init ... !!!
   969.186021 s: MEM: Initialized DMA HEAP (fd=8) !!!
   969.186171 s: MEM: Init ... Done !!!
   969.186186 s: IPC: Init ... !!!
   969.204608 s: IPC: Init ... Done !!!
REMOTE_SERVICE: Init ... !!!
REMOTE_SERVICE: Init ... Done !!!
   969.209618 s: GTC Frequency = 200 MHz
APP: Init ... Done !!!
   969.209751 s:  VX_ZONE_INFO: Globally Enabled VX_ZONE_ERROR
   969.209770 s:  VX_ZONE_INFO: Globally Enabled VX_ZONE_WARNING
   969.209781 s:  VX_ZONE_INFO: Globally Enabled VX_ZONE_INFO
   969.210951 s:  VX_ZONE_INFO: [tivxPlatformCreateTargetId:134] Added target MPU-0 
   969.211281 s:  VX_ZONE_INFO: [tivxPlatformCreateTargetId:134] Added target MPU-1 
   969.211562 s:  VX_ZONE_INFO: [tivxPlatformCreateTargetId:134] Added target MPU-2 
   969.211804 s:  VX_ZONE_INFO: [tivxPlatformCreateTargetId:134] Added target MPU-3 
   969.211838 s:  VX_ZONE_INFO: [tivxInitLocal:126] Initialization Done !!!
   969.211852 s:  VX_ZONE_INFO: Globally Disabled VX_ZONE_INFO
Setting pipeline to PAUSED ...
Pipeline is live and does not need PREROLL ...
Pipeline is PREROLLED ...
Setting pipeline to PLAYING ...
New clock: GstSystemClock
[  957.770331] max96712 1-0029: max96712_get_vc_maps: VC map for port 0 is 0x04
[  957.777418] max96712 1-0029: Mapping sink 0/0 to output VC 0, type 2,30 
[  957.784134] max96712 1-0029: Mapping sink 0/1 to output VC 1, type 2,30 
[  957.790849] max96712 1-0029: max96712_get_vc_maps: VC map for port 0 is 0x04
[  957.797925] max96712 1-0029: Mapping sink 0/0 to output VC 0, type 2,30 
[  957.804637] max96712 1-0029: Mapping sink 0/1 to output VC 1, type 2,30 
[  957.811389] max96712 1-0029: enable streaming (0) 
[  957.816211] max96712 1-0029: Prepare for streaming
[  957.821012] max96712 1-0029: max96712_get_vc_maps: VC map for port 0 is 0x04
[  957.828069] max96712 1-0029: enable tx port 0
[  957.833446] max96712 1-0029: enable rx port 0
[  957.837822] max96712 1-0029: enable RX port 0 streams 0x3
[  957.843234] max9295E 1-0042: enable streaming 
   969.566105 s:  VX_ZONE_ERROR: [ownContextSendCmd:912] Command ack message returned failure cmd_status: -1
   969.566171 s:  VX_ZONE_ERROR: [ownNodeKernelInit:604] Target kernel, TIVX_CMD_NODE_CREATE failed for node img_mosaic_node
   969.566196 s:  VX_ZONE_ERROR: [ownNodeKernelInit:605] Please be sure the target callbacks have been registered for this core
   969.566208 s:  VX_ZONE_ERROR: [ownNodeKernelInit:606] If the target callbacks have been registered, please ensure no errors are occurring within the create callback of this kernel
   969.566225 s:  VX_ZONE_ERROR: [ownGraphNodeKernelInit:690] kernel init for node 0, kernel com.ti.img_proc.img.mosaic:2 ... failed !!!
   969.566252 s:  VX_ZONE_ERROR: [ graph_135 ] Node kernel init failed
   969.566264 s:  VX_ZONE_ERROR: [ graph_135 ] Graph verify failed
   969.566469 s:  VX_ZONE_ERROR: [ownReleaseReferenceInt:747] Invalid reference
ERROR: from element /GstPipeline:pipeline0/GstTIOVXMosaic:mosaic: Unable to init TIOVX module
Additional debug info:
/usr/src/debug/edgeai-gst-plugins/1.0.0/gst-libs/gst/tiovx/gs[  958.028382] max96712 1-0029: disable streaming (1) 
ttiovxmiso.c(1512): gst_tiovx_miso_negotiated_src_caps (): /GstP[  958.036344] max96712 1-0029: disable RX port 0 streams 0x3
ipeline:pipeline0/GstTIOVXMosaic:mosaic
Execution ended after 0[  958.047355] max9295E 1-0042: disable streaming 
:00:00.183445765
Setting pipeline to NULL ...
[  958.057425] max96712 1-0029: disable rx port 0
[  958.065998] max96712 1-0029: disable tx port 0
Freeing pipeline ...
   969.782587 s:  VX_ZONE_WARNING: [vxReleaseContext:1275] Found a reference 0xffff882ea970 of type 00000816 at external count 1, internal count 0, releasing it
   969.782666 s:  VX_ZONE_WARNING: [vxReleaseContext:1277] Releasing reference (name=mosaic_node_config) now as a part of garbage collection
   969.782760 s:  VX_ZONE_WARNING: [vxReleaseContext:1275] Found a reference 0xffff88321e50 of type 0000080f at external count 1, internal count 0, releasing it
   969.782774 s:  VX_ZONE_WARNING: [vxReleaseContext:1277] Releasing reference (name=mosaic_node_background_image_0) now as a part of garbage collection
   969.782795 s:  VX_ZONE_WARNING: [vxReleaseContext:1275] Found a reference 0xffff8839cdd0 of type 00000813 at external count 1, internal count 0, releasing it
   969.782808 s:  VX_ZONE_WARNING: [vxReleaseContext:1277] Releasing reference (name=object_array_129) now as a part of garbage collection
   969.782829 s:  VX_ZONE_WARNING: [vxReleaseContext:1275] Found a reference 0xffff88322120 of type 0000080f at external count 1, internal count 0, releasing it
   969.782842 s:  VX_ZONE_WARNING: [vxReleaseContext:1277] Releasing reference (name=image_130) now as a part of garbage collection
   969.783133 s:  VX_ZONE_WARNING: [vxReleaseContext:1275] Found a reference 0xffff8839cf80 of type 00000813 at external count 1, internal count 0, releasing it
   969.783149 s:  VX_ZONE_WARNING: [vxReleaseContext:1277] Releasing reference (name=object_array_131) now as a part of garbage collection
   969.783169 s:  VX_ZONE_WARNING: [vxReleaseContext:1275] Found a reference 0xffff883223f0 of type 0000080f at external count 1, internal count 0, releasing it
   969.783182 s:  VX_ZONE_WARNING: [vxReleaseContext:1277] Releasing reference (name=image_132) now as a part of garbage collection
   969.783480 s:  VX_ZONE_WARNING: [vxReleaseContext:1275] Found a reference 0xffff883226c0 of type 0000080f at external count 1, internal count 0, releasing it
   969.783495 s:  VX_ZONE_WARNING: [vxReleaseContext:1277] Releasing reference (name=mosaic_node_output_image_0) now as a part of garbage collection
   969.783787 s:  VX_ZONE_WARNING: [vxReleaseContext:1275] Found a reference 0xffff882a95b0 of type 00000804 at external count 1, internal count 1, releasing it
   969.783802 s:  VX_ZONE_WARNING: [vxReleaseContext:1277] Releasing reference (name=com.ti.img_proc.img.mosaic:2) now as a part of garbage collection
   969.783816 s:  VX_ZONE_WARNING: [vxReleaseContext:1297] A kernel with name com.ti.img_proc.img.mosaic:2 has not been removed, possibly due to a kernel module not being unloaded.
   969.783828 s:  VX_ZONE_WARNING: [vxReleaseContext:1298] Removing as a part of garbage collection

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尝试使用 tiovxmultiscaler 将每个流高度降低到 540。 你进入了错误高度的马赛克。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Kim:

    您的电路板和 AM62A SK 板之间的主要差异是什么? 您是否使用相同大小的 DDR?  

     bas Vermeulen , tiovxmosaic 可以重新缩放图像如果 tiovxmultiscaler 没有使用。

    此致、

    建中

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    你(们)好

    对于 DDR、我们使用与 SK 板相同的产品。

    MT53E1G32D2FW-046 AUT:B

    我从 SK 板上移除了许多器件。

    您是否有任何可疑之处?

    此致、

    Kim

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Kim:

    SW 如何? 您对 SDK 进行了哪些更改? 日志中的错误表明 OpenVX 有问题。

    此致、

    建中

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    是可能的。 您的 DDR 大小是多少? 您是否更改了存储器映射?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    抱歉、我忘记了您使用的是与 SK 板相同的 DDR

    [引述 userid=“596322" url="“ url="~“~/support/processors-group/processors/f/processors-forum/1542808/am62a7-q1-tiovxmosiac-error/5936608

    对于 DDR、我们使用与 SK 板相同的产品。

    MT53E1G32D2FW-046 AUT:B

    [/报价]

    问题是、您是否更改了存储器映射?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    你(们)好

    在 uboot 中使用 boot 命令引导时出现上述症状。

    evkit 也出现了此症状。

    如上所述、继续操作的原因是硬件架构。

    正常引导期间不会出现此问题。