This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] AM6442:器件树保留存储器节点

Guru**** 2595805 points
Other Parts Discussed in Thread: AM6442

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1547497/am6442-device-tree-reserved-memory-nodes

器件型号:AM6442


工具/软件:

您好:

我最近遇到了 am6442 上的内核启动的一个奇怪问题。 我正在使用 Yocto 为 AM6442 构建映像;该构建将 phytec-Linux fork 用于内核源。

我的问题是内核似乎没有消耗正确的设备树 blob。 我不能肯定这其实是根本原因、但我会概述这个问题、也许有人更倾向于做什么。

我正在使用的主设备树源是  /arch/arm64/boot/dts/ti/k3-am642-phyboard-electra-rdk.dts.  我通过 Yocto 中的补丁、对此器件树进行了几次编辑、以满足我的特定需求。 内核编辑是两个额外的保留存储器区域:


From 7058d3dc228615c43bd81bf9f737ada18a93a75b Mon Sep 17 00:00:00 2001
From: jweyer <jweyer@aecontrols.com>
Date: Thu, 12 Jun 2025 13:58:18 -0700
Subject: [PATCH] apc reserved buff

---
 .../boot/dts/ti/k3-am64-phycore-som.dtsi      | 29 +++++++++++++++++++
 1 file changed, 29 insertions(+)

diff --git a/arch/arm64/boot/dts/ti/k3-am64-phycore-som.dtsi b/arch/arm64/boot/dts/ti/k3-am64-phycore-som.dtsi
index e8d1b88651e7..0e1447b382ee 100644
--- a/arch/arm64/boot/dts/ti/k3-am64-phycore-som.dtsi
+++ b/arch/arm64/boot/dts/ti/k3-am64-phycore-som.dtsi
@@ -105,8 +105,37 @@ rtos_ipc_memory_region: ipc-memories@a5000000 {
 			alignment = <0x1000>;
 			no-map;
 		};
+
+		/* 
+        * apc reserved memory 
+ 		 *  desc: contigous buffer for apc buffers.
+ 		 * 	region: 0xa58000000 - 0xb5800000
+ 		 * 	size: 100 MiB
+ 		 */
+ 		apc_memory_region: apc-memory@a5800000 {
+ 			reg = <0x00 0xa5800000 0x00 0x10000000>;
+ 			alignment = <0x1000>;
+ 			no-map;
+ 		};
+ 
+ 		/* 
+        * jailhouse reserved memory 
+ 		 *  desc: memory hypervisor and inmate
+ 		 * 	region: 0xdfa00000 - 0xeae00000
+ 		 * 	size: 180 MiB
+ 		 */
+ 		jailhouse_mem: jailhouse@dfa00000 {
+ 			reg = <0x0 0xdfa00000 0x0 0x00b400000>; 
+ 			alignment = <0x1000>;
+ 			no-map;
+ 		};
 	};
 
+  	apc {
+ 		compatible = "apc-memory";
+ 		memory-region = <&apc_memory_region>;
+ 	};
+
 	leds {
 		compatible = "gpio-leds";
 		pinctrl-names = "default";
-- 
2.25.1

这一切都可以正常工作;我已通过对 Yocto 映像部署目录中的设备树 blob 进行解压缩来验证我的补丁是否已应用到设备树。 然后、我在 AM6442 上安装映像、并且未预留存储器。 我通过`dmesg`检查了是否有任何错误、但似乎没有任何创建区域的尝试。 我最初认为 U-boot 和/或内核正在使用错误的设备树 blob;但是、我进行了检查 /boot/  一切似乎都正确:

root@aec-am6442:boot# ls
 EFI
 Image
'System Volume Information'
 k3-am642-phyboard-electra-gpio-fan.dtbo
 k3-am642-phyboard-electra-pcie-usb2.dtbo
 k3-am642-phyboard-electra-rdk.dtb
 k3-am642-phyboard-electra-x27-gpio1-spi1-uart3.dtbo
 oftree
 tiboot3.bin
 tispl.bin
 u-boot.img

我解析 oftree 和 k3-am642-phyboard-Electra-RDK.dtb、它们都有我保留的内存节点。 我还在引导期间停止了 U-boot 并确定了这一点 fdtfile=oftree 。 启动后、我进行检查  /proc/device-tree/reserved-memory  并且我的保留内存节点未显示:

root@aec-am6442:reserved-memory# ls
'#address-cells'           phandle                   r5f-memory@a1100000
'#size-cells'              r5f-dma-memory@a0000000   r5f-memory@a2100000
 m4f-dma-memory@a4000000   r5f-dma-memory@a1000000   r5f-memory@a3100000
 m4f-memory@a4100000       r5f-dma-memory@a2000000   ranges
 name                      r5f-dma-memory@a3000000
 optee@9e800000            r5f-memory@a0100000

 

仔细检查我使用的这些结果  `dtc -i fs`创建 DTS 文件并检查此文件、已验证保留的存储器节点是否不存在。 我还检查了  /proc/device-tree/compatible  看起来正常:

phytec,am642-phyboard-electra-rdkphytec,am64-phycore-somti,am642



因此、似乎内核和 u-boot 使用了正确的器件树;但我的内存节点并不存在。 内存保留是否可能以静默方式失败? 以下是我的相关`dmesg` output:

[    0.000000] OF: reserved mem: 0x000000009e800000..0x000000009fffffff (24576 KiB) nomap non-reusable optee@9e800000
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a0000000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node r5f-dma-memory@a0000000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x00000000a0000000..0x00000000a00fffff (1024 KiB) nomap non-reusable r5f-dma-memory@a0000000
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a0100000, size 15 MiB
[    0.000000] OF: reserved mem: initialized node r5f-memory@a0100000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x00000000a0100000..0x00000000a0ffffff (15360 KiB) nomap non-reusable r5f-memory@a0100000
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a1000000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node r5f-dma-memory@a1000000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x00000000a1000000..0x00000000a10fffff (1024 KiB) nomap non-reusable r5f-dma-memory@a1000000
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a1100000, size 15 MiB
[    0.000000] OF: reserved mem: initialized node r5f-memory@a1100000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x00000000a1100000..0x00000000a1ffffff (15360 KiB) nomap non-reusable r5f-memory@a1100000
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a2000000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node r5f-dma-memory@a2000000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x00000000a2000000..0x00000000a20fffff (1024 KiB) nomap non-reusable r5f-dma-memory@a2000000
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a2100000, size 15 MiB
[    0.000000] OF: reserved mem: initialized node r5f-memory@a2100000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x00000000a2100000..0x00000000a2ffffff (15360 KiB) nomap non-reusable r5f-memory@a2100000
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a3000000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node r5f-dma-memory@a3000000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x00000000a3000000..0x00000000a30fffff (1024 KiB) nomap non-reusable r5f-dma-memory@a3000000
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a3100000, size 15 MiB
[    0.000000] OF: reserved mem: initialized node r5f-memory@a3100000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x00000000a3100000..0x00000000a3ffffff (15360 KiB) nomap non-reusable r5f-memory@a3100000
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a4000000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node m4f-dma-memory@a4000000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x00000000a4000000..0x00000000a40fffff (1024 KiB) nomap non-reusable m4f-dma-memory@a4000000
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a4100000, size 15 MiB
[    0.000000] OF: reserved mem: initialized node m4f-memory@a4100000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x00000000a4100000..0x00000000a4ffffff (15360 KiB) nomap non-reusable m4f-memory@a4100000
 

我以前有内存保留失败了,通常`dmesg`表示此失败,所以似乎内核甚至没有尝试。 我以前使用过这个精确的过程、一切都按预期运行。

对我在这里可能出错的地方有什么想法吗? 此外、任何关于如何进一步调试此问题的想法都将非常感谢!

感谢您的帮助、

- Jared

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好 Jared、

    对延迟深表歉意。

    我正在将您的问题发送给我们的专家。 请期待尽快答复。

    此致、

    Suren

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Suren、

    我与 Phytec 一直保持联系、并与他们解决了问题。

    抱歉不让你们在循环中

    谢谢、

    Jared

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    感谢 Jared 的更新。

    关闭螺纹。  

    此致、

    Suren