This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TDA4VM:在启动期间卡住

Guru**** 2616165 points

Other Parts Discussed in Thread: TDA4VM

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1553347/tda4vm-stuck-during-startup

器件型号:TDA4VM


工具/软件:

大家好

我们使用 SDK 10 定制板。

在下电上电测试期间,发现了引导故障问题 — 系统在次级程序加载程序 (SPL) 阶段挂起、而未成功初始化 U-Boot。

日志:

[2025-08-13 20:41:08.451] U-Boot SPL 2024.04-ti-g46475e143ccd (Jul 23 2025 - 02:54:35 +0000)
[2025-08-13 20:41:08.491] SYSFW ABI: 4.0 (firmware rev 0x000a '10.0.8--v10.00.08 (Fiery Fox)')
[2025-08-13 20:41:08.540] Trying to boot from SPI
[2025-08-13 20:41:08.554] Boot MCU1_0 from Partition B!   
[2025-08-13 20:41:08.603] Authentication passed
[2025-08-13 20:41:08.603] Authentication passed
[2025-08-13 20:41:08.619] Authentication passed
[2025-08-13 20:41:08.646] Loading Environment from nowhere... OK
[2025-08-13 20:41:08.646] Authentication passed
[2025-08-13 20:41:08.646] Authentication passed
[2025-08-13 20:41:08.680] Starting ATF on ARM64 core...
[2025-08-13 20:41:08.680] 
[2025-08-13 20:41:08.680] NOTICE:  BL31: v2.10.0(release):v2.10.0-367-g00f1ec6b87-dirty
[2025-08-13 20:41:08.680] NOTICE:  BL31: Built : 16:09:05, Feb  9 2024
[2025-08-13 20:41:08.695] I/TC: 
[2025-08-13 20:41:08.696] I/TC: OP-TEE version: 4.2.0-dev (gcc version 13.3.0 (GCC)) #1 Fri Apr 12 09:51:21 UTC 2024 aarch64
[2025-08-13 20:41:08.773] I/TC: WARNING: This OP-TEE configuration might be insecure!
[2025-08-13 20:41:08.773] I/TC: WARNING: Please check optee.readthedocs.io/.../porting_guidelines.html
[2025-08-13 20:41:08.773] I/TC: Primary CPU initializing
[2025-08-13 20:41:08.773] I/TC: GIC redistributor base address not provided
[2025-08-13 20:41:08.773] I/TC: Assuming default GIC group status and modifier
[2025-08-13 20:41:08.773] I/TC: SYSFW ABI: 4.0 (firmware rev 0x000a '10.0.8--v10.00.08 (Fiery Fox)')
[2025-08-13 20:41:08.773] I/TC: HUK Initialized
[2025-08-13 20:41:08.773] I/TC: Activated SA2UL device
[2025-08-13 20:41:08.773] I/TC: Enabled firewalls for SA2UL TRNG device
[2025-08-13 20:41:08.773] I/TC: SA2UL TRNG initialized
[2025-08-13 20:41:08.773] I/TC: SA2UL Drivers initialized
[2025-08-13 20:41:08.773] I/TC: Primary CPU switching to normal world boot
[2025-08-13 20:41:08.917] 
[2025-08-13 20:41:08.917] U-Boot SPL 2024.04-ti-gcf9543435d2b (Aug 07 2025 - 06:25:51 +0000)
[2025-08-13 20:41:08.917] SYSFW ABI: 4.0 (firmware rev 0x000a '10.0.8--v10.00.08 (Fiery Fox)')
[2025-08-13 20:41:09.036] Detected: J7X-BASE-CPB rev E3
[2025-08-13 20:41:09.036] Detected: J7X-VSC8514-ETH rev E2
[2025-08-13 20:41:09.036] Trying to boot from SPI
[2025-08-13 20:41:09.036] k3-navss-ringacc ringacc@2b800000: Ring Accelerator probed rings:286, gp-rings[96,20] sci-dev-id:235
[2025-08-13 20:41:09.036] k3-navss-ringacc ringacc@2b800000: dma-ring-reset-quirk: disabled
[2025-08-13 20:41:09.036] jedec_spi_nor flash@0: non-uniform erase sector maps are not supported yet.
[2025-08-13 20:41:09.068] Authentication passed
[2025-08-13 20:41:09.084] Authentication passed
[2025-08-13 20:43:09.321] 
[2025-08-13 20:43:09.321] U-Boot SPL 2024.04-ti-g46475e143ccd (Jul 23 2025 - 02:54:35 +0000)

正常启动日志:

[2025-08-13 20:43:09.321] U-Boot SPL 2024.04-ti-g46475e143ccd (Jul 23 2025 - 02:54:35 +0000)
[2025-08-13 20:43:09.380] SYSFW ABI: 4.0 (firmware rev 0x000a '10.0.8--v10.00.08 (Fiery Fox)')
[2025-08-13 20:43:09.428] Trying to boot from SPI
[2025-08-13 20:43:09.444] Boot MCU1_0 from Partition B!   
[2025-08-13 20:43:09.492] Authentication passed
[2025-08-13 20:43:09.492] Authentication passed
[2025-08-13 20:43:09.508] Authentication passed
[2025-08-13 20:43:09.536] Loading Environment from nowhere... OK
[2025-08-13 20:43:09.536] Authentication passed
[2025-08-13 20:43:09.536] Authentication passed
[2025-08-13 20:43:09.569] Starting ATF on ARM64 core...
[2025-08-13 20:43:09.569] 
[2025-08-13 20:43:09.569] NOTICE:  BL31: v2.10.0(release):v2.10.0-367-g00f1ec6b87-dirty
[2025-08-13 20:43:09.569] NOTICE:  BL31: Built : 16:09:05, Feb  9 2024
[2025-08-13 20:43:09.585] I/TC: 
[2025-08-13 20:43:09.585] I/TC: OP-TEE version: 4.2.0-dev (gcc version 13.3.0 (GCC)) #1 Fri Apr 12 09:51:21 UTC 2024 aarch64
[2025-08-13 20:43:09.659] I/TC: WARNING: This OP-TEE configuration might be insecure!
[2025-08-13 20:43:09.659] I/TC: WARNING: Please check optee.readthedocs.io/.../porting_guidelines.html
[2025-08-13 20:43:09.659] I/TC: Primary CPU initializing
[2025-08-13 20:43:09.659] I/TC: GIC redistributor base address not provided
[2025-08-13 20:43:09.659] I/TC: Assuming default GIC group status and modifier
[2025-08-13 20:43:09.659] I/TC: SYSFW ABI: 4.0 (firmware rev 0x000a '10.0.8--v10.00.08 (Fiery Fox)')
[2025-08-13 20:43:09.659] I/TC: HUK Initialized
[2025-08-13 20:43:09.659] I/TC: Activated SA2UL device
[2025-08-13 20:43:09.659] I/TC: Enabled firewalls for SA2UL TRNG device
[2025-08-13 20:43:09.659] I/TC: SA2UL TRNG initialized
[2025-08-13 20:43:09.659] I/TC: SA2UL Drivers initialized
[2025-08-13 20:43:09.659] I/TC: Primary CPU switching to normal world boot
[2025-08-13 20:43:09.812] 
[2025-08-13 20:43:09.812] U-Boot SPL 2024.04-ti-gcf9543435d2b (Aug 07 2025 - 06:25:51 +0000)
[2025-08-13 20:43:09.812] SYSFW ABI: 4.0 (firmware rev 0x000a '10.0.8--v10.00.08 (Fiery Fox)')
[2025-08-13 20:43:09.926] Detected: J7X-BASE-CPB rev E3
[2025-08-13 20:43:09.926] Detected: J7X-VSC8514-ETH rev E2
[2025-08-13 20:43:09.926] Trying to boot from SPI
[2025-08-13 20:43:09.926] k3-navss-ringacc ringacc@2b800000: Ring Accelerator probed rings:286, gp-rings[96,20] sci-dev-id:235
[2025-08-13 20:43:09.926] k3-navss-ringacc ringacc@2b800000: dma-ring-reset-quirk: disabled
[2025-08-13 20:43:09.926] jedec_spi_nor flash@0: non-uniform erase sector maps are not supported yet.
[2025-08-13 20:43:09.959] Authentication passed
[2025-08-13 20:43:09.974] Authentication passed
[2025-08-13 20:43:10.968] 
[2025-08-13 20:43:10.968] 
[2025-08-13 20:43:10.968] U-Boot 2024.04-ti-gcf9543435d2b (Aug 07 2025 - 06:25:51 +0000)
[2025-08-13 20:43:10.968] 
[2025-08-13 20:43:10.968] SoC:   J721E SR2.0 HS-FS
[2025-08-13 20:43:10.968] Model: Texas Instruments J721e EVM
[2025-08-13 20:43:10.968] Board: J721EX-PM2-SOM rev E8
[2025-08-13 20:43:10.968] DRAM:  2 GiB (effective 4 GiB)
[2025-08-13 20:43:11.523] Core:  115 devices, 34 uclasses, devicetree: separate
[2025-08-13 20:43:11.523] Flash: 0 Bytes
[2025-08-13 20:43:11.523] MMC:   mmc@4f80000: 0, mmc@4fb0000: 1
[2025-08-13 20:43:11.523] Loading Environment from nowhere... OK
[2025-08-13 20:43:11.523] In:    serial@2800000
[2025-08-13 20:43:11.523] Out:   serial@2800000
[2025-08-13 20:43:11.523] Err:   serial@2800000
[2025-08-13 20:43:11.523] am65_cpsw_nuss ethernet@46000000: K3 CPSW: nuss_ver: 0x6BA00101 cpsw_ver: 0x6BA80100 ale_ver: 0x00293904 Ports:1
[2025-08-13 20:43:11.523] Detected: J7X-BASE-CPB rev E3
[2025-08-13 20:43:11.523] Detected: J7X-VSC8514-ETH rev E2
[2025-08-13 20:43:11.523] Net:   PHY PassiveMode: 0x0000 
[2025-08-13 20:43:11.619] eth0: ethernet@46000000port@1
[2025-08-13 20:43:11.667] k3-navss-ringacc ringacc@2b800000: Ring Accelerator probed rings:286, gp-rings[96,20] sci-dev-id:235
[2025-08-13 20:43:11.667] k3-navss-ringacc ringacc@2b800000: dma-ring-reset-quirk: disabled
[2025-08-13 20:43:11.667] jedec_spi_nor flash@0: non-uniform erase sector maps are not supported yet.
[2025-08-13 20:43:12.002] SF: Detected s28hs512t with page size 256 Bytes, erase size 256 KiB, total 64 MiB
[2025-08-13 20:43:12.044] device 0 offset 0x680000, size 0x9
[2025-08-13 20:43:12.044] SF: 9 bytes @ 0x680000 Read: OK
[2025-08-13 20:43:12.044] The current system is on Partition B, set bootpart 0:2.
[2025-08-13 20:43:12.044] device 0 offset 0x3f80000, size 0x40000
[2025-08-13 20:43:12.044] SF: 262144 bytes @ 0x3f80000 Read: OK
[2025-08-13 20:43:12.044] Hit any key to stop autoboot:  2  1  0 
[2025-08-13 20:43:14.199] Device at ufs@4e84000 up at:cdns-ufs-pltfm ufs@4e84000: [RX, TX]: gear=[3, 3], lane[2, 2], pwr[FAST MODE, FAST MODE], rate = 2
[2025-08-13 20:43:14.224] scanning bus for devices...

除了这个问题,我仍然有一些技术问题:

标有红色的编号项目 (1、2、3) 分别指示引导顺序的哪些阶段?

BR

中断

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好:

    1 --> R5 SPL
    2 -->A72 SPL
    3 -->A72 U-Boot。

    基于 U-Boot 的引导流程为:

    R5 SPL --> A72 ATF --> A72 OP-TEE --> A72 SPL --> A72 U-Boot。

    失败再现率是多少? 我假设您有定制的 TDA4VM 板。 当您看到故障情况时、是否能够将调试器/JTAG 连接到 A72?

    - Keerthy