Thread 中讨论的其他器件:UNIFLASH
工具/软件:
您好 TI:
我遇到 Linux 无法 在 AM62P-LP EVM 板上启动的问题、我在 R5 内核上运行演示“dss display test“(MCU SDK 版本为 mcu_plus_sdk_am62px_11_00_00_16)、 然后 A53 正在运行、 Linux 在 tidss_probe 期间崩溃。 Linux SDK 版本为 11.01。
[ 7.385909] NET: Registered PF_BLUETOOTH protocol family
[ 7.390406] Modules linked in: videobuf2_memops k3_j72xx_bandgap(+) bluetooth(+) rtc_ti_k3(+) snd_soc_tlv320aic3x(+) ecdh_generic videobuf2_common sii902x(+) tps6598x(+) tidss(+) videodev ecc drm_dma_helper rfkill snd_soc_davinci_mcasp(+) typec mc snd_soc_ti_udma snd_soc_ti_edma drm_display_helper pwm_tiehrpwm sa2ul
[ 7.395781] Bluetooth: HCI device and connection manager initialized
[ 7.395803] Bluetooth: HCI socket layer initialized
[ 7.423709] snd_soc_ti_sdma mcrc64 omap_hwspinlock omap_mailbox drm_kms_helper pwm_tiecap cryptodev(O) fuse drm drm_panel_orientation_quirks backlight ipv6
[ 7.423753] CPU: 3 UID: 0 PID: 213 Comm: (udev-worker) Tainted: G O 6.12.35-ti-00915-ge3e551586dfa #1
[ 7.430107] Bluetooth: L2CAP socket layer initialized
[ 7.434951] Tainted: [O]=OOT_MODULE
[ 7.434954] Hardware name: Texas Instruments AM62P5 SK (DT)
[ 7.434959] pstate: 00000005 (nzcv daif -PAN -UAO -TCO -DIT -SSBS BTYPE=--)
[ 7.448947] Bluetooth: SCO socket layer initialized
[ 7.459496] pc : device_link_put_kref+0x14/0x114
[ 7.489991] lr : device_link_del+0x30/0x48
[ 7.494092] sp : ffff800082be37f0
[ 7.497398] x29: ffff800082be37f0 x28: 0000000000000000 x27: 0000000000000000
[ 7.504541] x26: ffff800081577490 x25: ffff800082be3bb0 x24: ffff000806d42140
[ 7.511686] x23: ffff000801235c00 x22: ffff000801235c10 x21: 0000000000000008
[ 7.518814] x20: 0000000000000008 x19: 0000000000000008 x18: 0000000000001000
[ 7.525946] x17: 0000000000000000 x16: ffff800080e47780 x15: 014b111ea69f1b38
[ 7.533076] x14: 0000000000000004 x13: ffff0008000a2010 x12: 0000000000000000
[ 7.540206] x11: ffff000805176bb0 x10: ffff000805176b58 x9 : ffff0008000a2010
[ 7.547346] x8 : ffff800082be3710 x7 : 0000000000000000 x6 : ffff00080283a460
[ 7.554501] x5 : 000000000080007f x4 : 0000000000000000 x3 : 0000000000000000
[ 7.561642] x2 : ffff000806c4d280 x1 : 0000000000000000 x0 : 0000000000000008
[ 7.568773] Call trace:
[ 7.571217] device_link_put_kref+0x14/0x114
[ 7.575490] device_link_del+0x30/0x48
[ 7.579237] tidss_detach_pm_domains.part.0+0x4c/0xa8 [tidss]
[ 7.585005] tidss_probe+0x160/0x364 [tidss]
[ 7.589290] platform_probe+0x68/0xc4
[ 7.592954] really_probe+0xbc/0x29c
[ 7.596534] __driver_probe_device+0x78/0x12c
[ 7.600891] driver_probe_device+0xd8/0x15c
[ 7.605073] __driver_attach+0x90/0x19c
[ 7.608909] bus_for_each_dev+0x7c/0xe0
[ 7.612743] driver_attach+0x24/0x30
[ 7.616312] bus_add_driver+0xe4/0x208
[ 7.620053] driver_register+0x5c/0x124
[ 7.623882] __platform_driver_register+0x24/0x30
[ 7.628575] tidss_platform_driver_init+0x28/0x1000 [tidss]
[ 7.634154] do_one_initcall+0x80/0x1c8
[ 7.637982] do_init_module+0x58/0x1fc
[ 7.641725] load_module+0x1bcc/0x1d8c
[ 7.645466] init_module_from_file+0x88/0xcc
[ 7.649727] __arm64_sys_finit_module+0x148/0x324
[ 7.654422] invoke_syscall+0x48/0x10c
[ 7.658164] el0_svc_common.constprop.0+0xc0/0xe0
[ 7.662859] do_el0_svc+0x1c/0x28
[ 7.666166] el0_svc+0x28/0x98
[ 7.669215] el0t_64_sync_handler+0x120/0x12c
[ 7.673562] el0t_64_sync+0x190/0x194
[ 7.677218] Code: a9be7bfd 910003fd a90153f3 aa0003f3 (b9432401)
[ 7.683297] ---[ end trace 0000000000000000 ]---
Starting Telnet Server...
[ OK ] Started Serial Getty on ttyS2.
BR、
DongCAN