This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] PROCESSOR-SDK-AM62X:SDL DCC R5

Guru**** 2587365 points
Other Parts Discussed in Thread: SK-AM62

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1555986/processor-sdk-am62x-sdl-dcc-r5

器件型号:PROCESSOR-SDK-AM62X
主题中讨论的其他器件:SK-AM62

工具/软件:

MCU SDK 版本:mcu_plus_sdk_am62x_10_01_00_33

测试 EVM:SK-AM62

CCS 版本:12.8.1

我从 C:\ti\mcu_plus_sdk_am62x_10_01_00_33\examples\sdl\dcc\dcc_modes\am62x-sk\r5fss0-0_freertos\导入了示例

然后、我编译了 R5 工程并将生成的  appimage.hs_fs 复制到以下路径中。

--file=sbl_prebuilt/am62x-sk/WZ_Debug/dcc_am62x-sk_r5fss0-0_freertos_ti-arm-clang.appimage.hs_fs -operation=flash -flash-offset=0xA00000

我使用下面的文件刷写测试示例。

e2e.ti.com/.../default_5F00_sbl_5F00_ospi_5F00_hs_5F00_fs_2D00_r5.cfg

下面是来自 SBL UART 的 UART 日志

SYSFW Firmware Version 10.1.8--v10.01.08 (Fiery Fox)
SYSFW Firmware revision 0xa
SYSFW ABI revision 4.0

[BOOTLOADER_PROFILE] Boot Media       : FLASH 
[BOOTLOADER_PROFILE] Boot Media Clock : 166.667 MHz 
[BOOTLOADER_PROFILE] Boot Image Size  : 175 KB 
[BOOTLOADER_PROFILE] Cores present    : 
m4f0-0
r5f0-0
[BOOTLOADER PROFILE] System_init                      :       5491us 
[BOOTLOADER PROFILE] Board_init                       :          0us 
[BOOTLOADER PROFILE] Drivers_open                     :        301us 
[BOOTLOADER PROFILE] Board_driversOpen                :       1260us 
[BOOTLOADER PROFILE] Sciclient Get Version            :      10202us 
[BOOTLOADER PROFILE] App_waitForMcuPbist              :       8663us 
[BOOTLOADER PROFILE] App_waitForMcuLbist              :       7689us 
[BOOTLOADER PROFILE] App_loadImages                   :       3327us 
[BOOTLOADER PROFILE] App_loadSelfcoreImage            :       4041us 
[BOOTLOADER_PROFILE] SBL Total Time Taken             :      40979us 

Image loading done, switching to application ...
Starting MCU-m4f and 2nd stage bootloader

SYSFW Firmware Version 10.1.8--v10.01.08 (Fiery Fox)
SYSFW Firmware revision 0xa
SYSFW ABI revision 4.0

[BOOTLOADER_PROFILE] Boot Media       : FLASH 
[BOOTLOADER_PROFILE] Boot Media Clock : 166.667 MHz 
[BOOTLOADER_PROFILE] Boot Image Size  : 408 KB 
[BOOTLOADER_PROFILE] Cores present    : 
hsm-m4f0-0
r5f0-0
a530-0
[BOOTLOADER PROFILE] System_init                      :       2789us 
[BOOTLOADER PROFILE] Board_init                       :          1us 
[BOOTLOADER PROFILE] Drivers_open                     :        386us 
[BOOTLOADER PROFILE] Board_driversOpen                :        139us 
[BOOTLOADER PROFILE] Sciclient Get Version            :      10225us 
[BOOTLOADER PROFILE] App_loadImages                   :       2690us 
[BOOTLOADER PROFILE] App_loadSelfcoreImage            :       5349us 
[BOOTLOADER PROFILE] App_loadA53Images                :       4116us 
[BOOTLOADER_PROFILE] SBL Total Time Taken             :      25698us 

Image loading done, switching to application ...
Starting RTOS/Baremetal applications
NOTICE:  BL31: v2.11.0(release):REL.MCUSDK.K3.10.01.00.33
NOTICE:  BL31: Built : 04:57:09, Dec 19 2024

下面是来自 DM UART 的 UART 日志

[15:15:23.569]收←◆Sciserver Testapp Built On: Dec 19 2024 04:51:59
Sciserver Version: v2024.12.0.0-REL.MCUSDK.K3.10.01.00.33+
RM_PM_HAL Version: v10.01.08
Starting Sciserver..... PASSED

 DCC Example Test Application

DCC_Test_init: Init WKUP ESM complete 


USECASE: 0
Source clock: HFOSC0 
Test clock: SYSCLK0

SDL DCC EXAMPLE TEST: Seed values calculation done.
SDL DCC EXAMPLE TEST: Enabling DCC and waiting for Error interrupt 

问题:如何运行此 DCC R5 示例?

我可以成功运行 DCC M4F C:\ti\mcu_plus_sdk_am62x_10_01_00_33\examples\sdl\dcc\dcc_modes\am62x-sk\m4fss0-0_nortos\

下面是日志。

但它无法在 DM 内核中成功运行   

[BLAZAR_Cortex_M4F_0] 
 DCC Example Test Application

DCC_Test_init: Init WKUP ESM complete 


USECASE: 0
Source clock: HFOSC0 
Test clock: SYSCLK0

SDL DCC EXAMPLE TEST: Seed values calculation done.
SDL DCC EXAMPLE TEST: Enabling DCC and waiting for Error interrupt 
SDL DCC EXAMPLE TEST: DCC Generated Error interrupt 
SDL DCC EXAMPLE TEST: Indicating clock drift/change 
UC-0 Completed Successfully

USECASE: 1
Source clock: HFOSC0 
Test clock: SYSCLK0

SDL DCC EXAMPLE TEST: Seed values calculation done.
SDL DCC EXAMPLE TEST: DCC Generated completion interrupt 
SDL DCC EXAMPLE TEST: No Clock Drift was observed 
UC-1 Completed Successfully

USECASE: 2
Source clock: HFOSC0 
Test clock: SYSCLK0

SDL DCC EXAMPLE TEST: Seed values calculation done.
SDL DCC EXAMPLE TEST: Enabling DCC and running for some time 
UC-2 Completed Successfully

USECASE: 3
Source clock: RC OSC 
Test clock: SYSCLK0

SDL DCC EXAMPLE TEST: Seed values calculation done.
SDL DCC EXAMPLE TEST: DCC Generated completion interrupt 
SDL DCC EXAMPLE TEST: No Clock Drift was observed 
UC-3 Completed Successfully

USECASE: 4
Source clock: RC OSC 
Test clock: SYSCLK0

SDL DCC EXAMPLE TEST: Seed values calculation done.
SDL DCC EXAMPLE TEST: Enabling DCC and waiting for Error interrupt 
SDL DCC EXAMPLE TEST: DCC Generated Error interrupt 
SDL DCC EXAMPLE TEST: Indicating clock drift/change 
UC-4 Completed Successfully

USECASE: 5
Source clock: RC OSC 
Test clock: SYSCLK0

SDL DCC EXAMPLE TEST: Seed values calculation done.
SDL DCC EXAMPLE TEST: Enabling DCC and waiting for Error interrupt 
SDL DCC EXAMPLE TEST: DCC Generated Error interrupt 
SDL DCC EXAMPLE TEST: Indicating clock drift/change 
UC-5 Completed Successfully

USECASE: 6
Source clock: RC OSC 
Test clock: SYSCLK0

SDL DCC EXAMPLE TEST: Seed values calculation done.
SDL DCC EXAMPLE TEST: Enabling DCC and waiting for Error interrupt 
SDL DCC EXAMPLE TEST: DCC Generated Error interrupt 
SDL DCC EXAMPLE TEST: Indicating clock drift/change 
UC-6 Completed Successfully

USECASE: 7
Source clock: HFOSC0 
Test clock: MAIN_SYSCLK0

SDL DCC EXAMPLE TEST: Seed values calculation done.
SDL DCC EXAMPLE TEST: Enabling DCC and waiting for Error interrupt 
SDL DCC EXAMPLE TEST: DCC Generated Error interrupt 
SDL DCC EXAMPLE TEST: Indicating clock drift/change 
UC-7 Completed Successfully

USECASE: 8
Source clock: RC OSC 
Test clock: MAIN_SYSCLK0

SDL DCC EXAMPLE TEST: Seed values calculation done.
SDL DCC EXAMPLE TEST: Enabling DCC and running for some time 
UC-8 Completed Successfully

USECASE: 9
Source clock: HFOSC0 
Test clock: FICLK

SDL DCC EXAMPLE TEST: Seed values calculation done.
SDL DCC EXAMPLE TEST: Enabling DCC and running for some time 
UC-9 Completed Successfully

USECASE: 10
Source clock: FICLK 
Test clock: MAIN_SYSCLK0

SDL DCC EXAMPLE TEST: Seed values calculation done.
SDL DCC EXAMPLE TEST: Enabling DCC and running for some time 
UC-10 Completed Successfully

 All tests have passed. 

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    请 TI 专家提供帮助吗?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好:

    10.1 MCU+SDK 中 R5 上的 DCC 示例似乎存在一些问题。 我遇到了一个类似的问题。  

    但是、此示例在最新的 11.1 SDK 中按预期运行。

    您是否可以尝试运行该示例并检查是否遇到了同一个问题?

    https://www.ti.com/tool/download/MCU-PLUS-SDK AM62X/11.01.00.16

    此致、

    Nihar Potturu

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    更新:增加 linker.cmd 文件中的 SVC 堆栈大小修复了问题。 这似乎是一些栈溢出问题、导致 R5F 内核进入预取中止状态。 是否可以增加 SVC 堆栈大小并检查这样是否解决了问题?

    此致、

    Nihar Potturu

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    这是什么意思?

    __SVC_STACK_SIZE = 0x0100;/*这是 R5 处于 SVC 模式时的栈大小*/

    我正在尝试将其增加到 __SVC_STACK_SIZE = 0x0200;/*这是 R5 处于 SVC 模式时的栈大小*/

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您的更新提示正确。

    将 __SVC_STACK_SIZE 从 0x100 更改为 0x200 后、会正常工作。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    但我检查了 mcu_plus_sdk_am62x_11_00_00_16 中的示例 dcc_am62x-sk_r5fss0-0_freertos_ti-arm-clang 。

     SVC_STACK_SIZE 为 0x100。  为什么这个示例可以工作?

    编译器是否会带来差异?

    我使用了 mcu_plus_sdk_am62x_11_00_00_16。 使用 CCS 20.1.1。

    或 mcu_plus_sdk_am62x_10_01_00_33。 Code Composer Studio 12.8.1。

    项目团队已决定使用 mcu_plus_sdk_am62x_10_01_00_33。  Code Composer Studio 12.8.1。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好:  

    DM 固件很可能出现此问题。 在处理某些 DM 请求时、堆栈必须溢出。 11.0 SDK 中的 DM 固件有一些更新、可以修复此问题。

    此致、

    Nihar Potturu