This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TDA4AL-Q1:在为 TDA4AL 上的 R5f 内核操作调试脚本时需要帮助

Guru**** 2668435 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1560782/tda4al-q1-need-help-in-acuring-debug-scripts-for-r5f-core-on-tda4al

器件型号:TDA4AL-Q1
主题中讨论的其他器件:TDA4VL

工具/软件:

Hello TI Team,

I’m an engineer at Aptiv currently working with the TDA4AL platform. We are using Lauterbach TRACE32 for debugging and need CMM scripts to support debugging of the R5F cores (both MCU and MAIN domains).

Could you please share the recommended CMM scripts or direct us to resources where we can obtain them? Specifically, we are looking for:
- Initialization and debug setup for R5F cores
- Support for bare-metal and FreeRTOS environments

We are using binaries built with the TI PDK and would appreciate any guidance on adapting the scripts to our setup.

Thank you for your support!
  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好:

    我附上了一些示例脚本、它们用于 TDA4VL 上的不同级别(裸机,RTOS、HLOS)。  密码为“TDA4VL"。“。  您可以包含 R5F 的连接脚本。

    e2e.ti.com/.../0652.cmm_2D00_tda4v_5F00_j721s2.7z

    此外、Lauterbach 在其发布版本中为 J721S2(也称为 TDA4VL)提供了示例裸机脚本:
    •  ./T32/demo/arm/hardware/j721s2
    如果您不熟悉 TRACE32、运行他们的演示脚本并与他们的支持互动可能是开始工作的最佳方式。
    此致、
    理查德·W·