This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TMS320C6748:使用 GPIO 测试项目构建错误#10010

Guru**** 2611705 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1565424/tms320c6748-build-error-10010-using-gpio-test-project

部件号:TMS320C6748
主题中讨论的其他器件:OMAPL138

工具/软件:

您好:

我想使用示例工程“GPIO_LedBlink_lcdkOMAPL138_c674xTestProject",“,但、但收到以下错误:


[0]****项目 GPIO_LedBlink_lcdkOMAPL138_c674xTestProject 的配置调试构建****
[1]“C:\ti\ccs2001\ccs\\utils\\bin\gmake“-k -j 12 all -O  
 
[2]编译目标:“GPIO_LedBlink_lcdkOMAPL138_c674xTestProject.out"</s>“
[3]调用:C6000 链接器
[4]“C:/ti/ti-cgt-c6000_8.5.0.LTS/bin/cl6x -mv6740 --define=SOC_OMAPL138 --define=LCDK_OMAPL138 --define=use_bios --define=lcdkOMAPL138 --define=C6748 -g ---link_cdsuppress=1111 --diag_suppress=827 --diag_diag_diag_display=824 ---diag_diag_/ti/ti-cgt-c6000_8.5.0.LTS/lib /ti/ti-cgt-c6000_8.5.0.LTS/include   
[5]<Linking>
[6]“configPkg/linker.cmd",“,第、第 34 行:错误#10264:L3_CBA_RAM 存储器范围与现有存储器范围 SHRAM 重叠
[7]错误#10010:链接期间遇到错误;未构建“GPIO_LedBlink_lcdkOMAPL138_c674xTestProject.out"</s>“
 
[8]>>编译失败
[9] gmake[1]:***[makefile:138:GPIO_LedBlink_lcdkOMAPL138_c674xTestProject.out]错误 1
[10]gmake:***[makefile:132:all]错误 2.
[11]*****构建完成****