This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] AM625:AM6254 GPU 无法找到 EGLConfig

Guru**** 2535150 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1564206/am625-am6254-gpu-cannot-find-eglconfig

器件型号:AM625


工具/软件:

您好 TI

我们要使用 AM6254 GPU、并在 TI 的 SDK 目录中找到 GPU 驱动程序源代码:install_path/ti-processor-sdk-linux-am62xx-evm-09.02.01.10/board-support/extra-drivers/ti-img-rogue-driver-23.3.6512818。 我编译了驱动程序源代码并获得了 pvrsrvkm.ko。 pvrsrvkm.ko 模块也已成功加载。 相关的打印日志如下所示:

[    2.837653] pvrsrvkm: loading out-of-tree module taints kernel.
[    2.850545] PVR_K:  325: Device: fd00000.gpu
[    2.850744] PVR_K:  325: Read BVNC 33.15.11.3 from HW device registers
[    2.850839] PVR_K:  325: RGX Device registered with BVNC 33.15.11.3
[    2.852054] [drm] Initialized pvr 23.3.6512818 20170530 for fd00000.gpu on minor 1

lsmod 命令的输出如下:

root@am62xx-evm:~# lsmod
    Tainted: G
pvrsrvkm 1163264 0 - Live 0xffff800000a40000 (O)
root@am62xx-evm:~#

rgx_triangle_test 命令的输出如下所示:

root@am62xx-evm:~# rgx_triangle_test
Connecting to first (0) default pvr device
Selected display mode: 1024x600@59
----------------------- Start -----------------------
Using display type: DRM/KMS
Window created with 2 buffers
Frame number 0
Frame number 100
Frame number 200
Frame number 300
Frame number 400
Frame number 500
Frame number 600
Frame number 700
Frame number 800
Frame number 900

Total time: 16882ms
Mean time per frame: 16899us
FPS: 59.2

root@am62xx-evm:~#

rgx_triangle_test 命令的演示效果如下所示:  

e2e.ti.com/.../mmexport1757558722033.mp4

我们的项目没有使用 Wayland/Houston 框架或 X11 框架。 eglinfo 指令的输出如下:

root@am62xx-evm:~# eglinfo
EGL client extensions string:
    EGL_EXT_client_extensions EGL_EXT_device_base
    EGL_EXT_device_enumeration EGL_EXT_device_query EGL_EXT_platform_base
    EGL_KHR_client_get_all_proc_addresses EGL_KHR_debug
    EGL_EXT_platform_device EGL_EXT_platform_wayland
    EGL_KHR_platform_wayland EGL_MESA_platform_gbm EGL_KHR_platform_gbm
    EGL_MESA_platform_surfaceless

GBM platform:
EGL API version: 1.5
EGL vendor string: Mesa Project
EGL version string: 1.5
EGL client APIs: OpenGL_ES
EGL extensions string:
    EGL_ANDROID_native_fence_sync EGL_EXT_buffer_age
    EGL_EXT_create_context_robustness EGL_EXT_image_dma_buf_import
    EGL_EXT_image_dma_buf_import_modifiers EGL_EXT_image_gl_colorspace
    EGL_EXT_yuv_surface EGL_IMG_context_priority EGL_KHR_cl_event2
    EGL_KHR_config_attribs EGL_KHR_create_context EGL_KHR_fence_sync
    EGL_KHR_get_all_proc_addresses EGL_KHR_gl_colorspace
    EGL_KHR_gl_renderbuffer_image EGL_KHR_gl_texture_2D_image
    EGL_KHR_gl_texture_3D_image EGL_KHR_gl_texture_cubemap_image
    EGL_KHR_image EGL_KHR_image_base EGL_KHR_image_pixmap
    EGL_KHR_no_config_context EGL_KHR_partial_update
    EGL_KHR_reusable_sync EGL_KHR_surfaceless_context
    EGL_EXT_pixel_format_float EGL_KHR_wait_sync
    EGL_MESA_configless_context EGL_MESA_drm_image
    EGL_MESA_image_dma_buf_export EGL_MESA_query_driver
    EGL_WL_bind_wayland_display EGL_IMG_cl_image
Configurations:
     bf lv colorbuffer dp st  ms    vis   cav bi  renderable  supported
  id sz  l  r  g  b  a th cl ns b    id   eat nd gl es es2 vg surfaces
---------------------------------------------------------------------
0x01 32  0  8  8  8  8  0  0  0 0 0x34325241--      a     y        win,pb
0x02 32  0  8  8  8  8  0  0  2 1 0x34325241--      a     y        win,pb
0x03 32  0  8  8  8  8  0  0  4 1 0x34325241--      a     y        win,pb
0x04 32  0  8  8  8  8 24  8  0 0 0x34325241--      a     y        win,pb
0x05 32  0  8  8  8  8 24  8  2 1 0x34325241--      a     y        win,pb
0x06 32  0  8  8  8  8 24  8  4 1 0x34325241--      a     y        win,pb
0x07 24  0  8  8  8  0  0  0  0 0 0x34325258--      y     y        win,pb
0x08 24  0  8  8  8  0  0  0  2 1 0x34325258--      y     y        win,pb
0x09 24  0  8  8  8  0  0  0  4 1 0x34325258--      y     y        win,pb
0x0a 24  0  8  8  8  0 24  8  0 0 0x34325258--      y     y        win,pb
0x0b 24  0  8  8  8  0 24  8  2 1 0x34325258--      y     y        win,pb
0x0c 24  0  8  8  8  0 24  8  4 1 0x34325258--      y     y        win,pb
0x0d 16  0  5  6  5  0  0  0  0 0 0x36314752--      y     y        win,pb
0x0e 16  0  5  6  5  0  0  0  2 1 0x36314752--      y     y        win,pb
0x0f 16  0  5  6  5  0  0  0  4 1 0x36314752--      y     y        win,pb
0x10 16  0  5  6  5  0 24  8  0 0 0x36314752--      y     y        win,pb
0x11 16  0  5  6  5  0 24  8  2 1 0x36314752--      y     y        win,pb
0x12 16  0  5  6  5  0 24  8  4 1 0x36314752--      y     y        win,pb

Wayland platform:
error: XDG_RUNTIME_DIR not set in the environment.
error: XDG_RUNTIME_DIR not set in the environment.
eglinfo: eglInitialize failed

Device platform:
eglinfo: eglInitialize failed

root@am62xx-evm:~#


但是当我们使用 kmscube 命令时、发生以下错误、错误消息是找不到 EGL 配置、但我们已经移植了依赖库、如 EGL 和 OpenGL。 在执行 kmscube 命令之前和之后、cat/sys/kernel/debug/pvr/status 中显示的内容也不同。

root@am62xx-evm:~# cat /sys/kernel/debug/pvr/status
Driver Status:   OK

Device ID: 0:128
Firmware Status: OK
Server Errors:   0
WGP Error Count: 0
TRP Error Count: 0
APM Event Count: 0
root@am62xx-evm:~# kmscube -D /dev/dri/card0
[   41.577338] PVR_K:  357: RGX Firmware image 'rgx.fw.33.15.11.3' loaded
[   41.583422] PVR_K:  357: Shader binary image 'rgx.sh.33.15.11.3' loaded
Using display 0x102fbc80 with EGL version 1.5
===================================
EGL information:
  version: "1.5"
  vendor: "Mesa Project"
  client extensions: "EGL_EXT_client_extensions EGL_EXT_device_base EGL_EXT_device_enumeration EGL_EXT_device_query EGL_EXT_pl                                                                      atform_base EGL_KHR_client_get_all_proc_addresses EGL_KHR_debug EGL_EXT_platform_device EGL_EXT_platform_wayland EGL_KHR_platf                                                                      orm_wayland EGL_MESA_platform_gbm EGL_KHR_platform_gbm EGL_MESA_platform_surfaceless"
  display extensions: "EGL_ANDROID_native_fence_sync EGL_EXT_buffer_age EGL_EXT_create_context_robustness EGL_EXT_image_dma_bu                                                                      f_import EGL_EXT_image_dma_buf_import_modifiers EGL_EXT_image_gl_colorspace EGL_EXT_yuv_surface EGL_IMG_context_priority EGL_K                                                                      HR_cl_event2 EGL_KHR_config_attribs EGL_KHR_create_context EGL_KHR_fence_sync EGL_KHR_get_all_proc_addresses EGL_KHR_gl_colors                                                                      pace EGL_KHR_gl_renderbuffer_image EGL_KHR_gl_texture_2D_image EGL_KHR_gl_texture_3D_image EGL_KHR_gl_texture_cubemap_image EG                                                                      L_KHR_image EGL_KHR_image_base EGL_KHR_image_pixmap EGL_KHR_no_config_context EGL_KHR_partial_update EGL_KHR_reusable_sync EGL                                                                      _KHR_surfaceless_context EGL_EXT_pixel_format_float EGL_KHR_wait_sync EGL_MESA_configless_context EGL_MESA_drm_image EGL_MESA_                                                                      image_dma_buf_export EGL_MESA_query_driver EGL_WL_bind_wayland_display EGL_IMG_cl_image "
===================================
No EGL configs with appropriate attributes.
failed to choose config
failed to initialize EGL
root@am62xx-evm:~# cat /sys/kernel/debug/pvr/status
Driver Status:   OK

Device ID: 0:128
Firmware Status: OK
Server Errors:   0
HWR Event Count: 0
CRR Event Count: 0
SLR Event Count: 0
WGP Error Count: 0
TRP Error Count: 0
FWF Event Count: 0
APM Event Count: 1
GPU Utilisation: 0%
                    VM0
2D    Utilisation:   0%
GEOM  Utilisation:   0%
3D    Utilisation:   0%
CDM   Utilisation:   0%
root@am62xx-evm:~#

配置 Qt 环境变量后、我们的应用程序还将报告一个错误、指出“无法找到 EGL 配置“:

After I configure the Qt environment variables, our application will also report an error saying 'cannot find egl configs':

我想问 TI、错误无法找到 EGL 配置的原因是什么、它是否与我不使用显示框架 (Wayland/West) 有关? cat/sys/kernel/debug/pvr/status 查看的内容中是否与 GPU 驱动程序加载失败有关? 请让 TI 专家帮我了解一下、谢谢!