请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号: TDA2EG-17
主题中讨论的其他器件: TDA2
尊敬的专家:
我尝试构建 TDA2 软件环境。
- 主机: Ubuntu 20.04.6 LTS
- SDK:ti-processor-sdk-linux-automotive-dra7x-evm-6.00.00.03
- Doucument :作为附件
- PROCESSOR_SDK_SDK Linux_Automotive_Software_Developers_Guide_-_SDK Texas_Instruments_Wiki.pdf
- EVB : XC5777X
Python 版本如下所示。
gibbs@gibbs-HP-ZBook-15-G5:~$ pyenv versions
system
3.7.6
3.8.12
* 3.14.0 (set by /home/gibbs/.pyenv/version)
执行“.0000.0000.flue"时“时/bin/fetch-sources.sh、会出现如下所示的错误。
gibbs@gibbs-HP-ZBook-15-G5:~/work/dra7x/ti-processor-sdk-linux-automotive-dra7xx-evm-6.00.00.03$ ./bin/fetch-sources.sh
Syncing: 12% (1/8), done in 1.124s
fatal: unable to connect to arago-project.org:
arago-project.org[0: 192.163.14.205]: errno=Connection timed out
oe-layersetup:
fatal: unable to connect to arago-project.org:
arago-project.org[0: 192.163.14.205]: errno=Connection timed out
oe-layersetup: sleeping 4.0 seconds before retrying
fatal: unable to connect to arago-project.org:
arago-project.org[0: 192.163.14.205]: errno=Connection timed out
Syncing: 100% (8/8) 4:27 | 1 job | 4:26 oe-layersetup @ yocto-layerserror: Unable to fully sync the tree
error: Downloading network changes failed.
Failing repos (network):
yocto-layers
Try re-running with "-j1 --fail-fast" to exit at the first error.
================================================================================
Repo command failed due to the following `SyncError` errors:
GitCommandError: 'fetch --quiet --progress arago --prune --recurse-submodules=no --tags +refs/heads/*:refs/remotes/arago/* +refs/tags/*:refs/tags/*' on oe-layersetup failed
stdout: fatal: unable to connect to arago-project.org:
skipping yocto-layers/
skipping yocto-layers/
gibbs@gibbs-HP-ZBook-15-G5:~/work/dra7x/ti-processor-sdk-linux-automotive-dra7xx-evm-6.00.00.03$
SDK 上下文如下所示、
我是否知道如何解决这个提取失败的 问题? 有什么建议吗?
谢谢你。
Gibbs