This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] AM623:ESM 错误

Guru**** 2999690 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1625308/am623-esm-error

器件型号: AM623

系统正常启动并进入终端控制台后、它将运行一段时间、并在运行期间自动重新启动。 芯片模型为 am62x、SDK 版本为 10.01.10.04。 重新启动的原因是什么? 可以读取哪些寄存器来进一步解决该问题?
读取寄存器 0x431A178h、有以下输出日志:

1  [system reboot time: 1970-01-01 00:00:02] POR Reset, Register_value: 0x00000000. Note: The ZLG and FORLINX core boards can't distinguish between an external watchdog reset and a power-on reset.
2  [system reboot time: 1970-01-01 08:00:01] WARM Reset, Register_value: 0x00010000.
3  [system reboot time: 2026-03-10 01:27:59] POR Reset, Register_value: 0x00000000. Note: The ZLG and FORLINX core boards can't distinguish between an external watchdog reset and a power-on reset.
4  [system reboot time: 2026-03-10 01:34:13] WARM Reset, Register_value: 0x00010000.
5  [system reboot time: 2026-03-10 16:50:43] POR Reset, Register_value: 0x00000000. Note: The ZLG and FORLINX core boards can't distinguish between an external watchdog reset and a power-on reset.
6  [system reboot time: 2026-03-10 18:12:09] WARM Reset, Register_value: 0x00010000.
7  [system reboot time: 2026-03-10 18:19:23] WARM Reset, Register_value: 0x00010000.
8  [system reboot time: 2026-03-10 18:43:16] WARM Reset, Register_value: 0x00010000.
9  [system reboot time: 2026-03-10 22:08:56] WARM Reset, Register_value: 0x00010000.
10 [system reboot time: 2026-03-10 22:12:03] WARM Reset, Register_value: 0x00010000.
11 [system reboot time: 2026-03-10 22:28:24] WARM Reset, Register_value: 0x00010000.
12 [system reboot time: 2026-03-10 22:49:20] WARM Reset, Register_value: 0x00010000.
13 [system reboot time: 2026-03-10 22:55:18] WARM Reset, Register_value: 0x00010000.
14 [system reboot time: 2026-03-10 23:35:19] POR Reset, Register_value: 0x00000000. Note: The ZLG and FORLINX core boards can't distinguish between an external watchdog reset and a power-on reset.
15 [system reboot time: 2026-03-11 00:14:57] POR Reset, Register_value: 0x00000000. Note: The ZLG and FORLINX core boards can't distinguish between an external watchdog reset and a power-on reset.
16 [system reboot time: 2026-03-11 00:54:59] OTHER Reset, Register_value: 0xC0000000.

 

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、

    系统正常启动并进入终端控制台后、它将运行一段时间、并在操作过程中自动重新启动。 [/报价]

    这是 TI EVM 还是您的定制电路板? 电路板使用哪种电源。 当电源电压过低导致 SoC 无法正常工作时、我们也会出现类似的问题。  

    此外、您可以在 MCU 或 A53 内核中启用 WDG 模块和 ESM 模块。 您能否分享以下寄存器的值:

    0x4518170

    0x43018170

    此致、

    Nihar Potturu