Other Parts Discussed in Thread: AM62P
部件号: AM62P
您好、专家、
我们的定制板上有一个 AM62P。 在 CPSW 端口 2 上、我们通过 RMII 从 Microchip 的 LAN9354 连接了一个外部以太网交换机。 它通过 MDIO 进行管理。 下图描述了我们的设置:

如果我省略 DSA 驱动程序、该开关在 U-Boot 和 Linux 中都能正常工作。 然后、它将作为具有两个端口的普通非托管交换机运行。
当我在 DTS 中添加 DSA 驱动程序片段时、芯片似乎被正确探测、但我在两个用户端口上没有连接。
探测本身似乎有点不稳。 有些引导不会成功并返回到非托管模式。 所有数据线和时钟线均已重新连接以实现布线长度匹配。
以下是一些相关片段:
DTS:
&cpsw3g {
status = "okay";
pinctrl-names = "default";
pinctrl-0 = <&main_rgmii1_pins_default>,
<&main_rgmii2_pins_default>;
};
&cpsw_port1 {
status = "disabled";
};
&cpsw_port2 {
status = "okay";
phy-mode = "rmii";
fixed-link {
speed = <100>;
full-duplex;
};
};
&cpsw3g_mdio {
status = "okay";
pinctrl-names = "default";
pinctrl-0 = <&main_mdio1_pins_default>;
lan9354_switch: switch@1 {
compatible = "microchip,lan9354-mdio";
reg = <1>;
reset-gpios = <&main_gpio0 17 GPIO_ACTIVE_LOW>; /* GPIO0_91 */
reset-duration = <1000>;
ports {
#address-cells = <1>;
#size-cells = <0>;
port@0 {
reg = <0>;
label = "cpu";
ethernet = <&cpsw_port2>;
phy-mode = "rmii";
fixed-link {
speed = <100>;
full-duplex;
};
};
port@1 {
reg = <1>;
label = "lan1";
};
port@2 {
reg = <2>;
label = "lan2";
};
};
};
};
引导日志 dmesg:
root@AS-B-3-261750009:~# dmesg | grep -i lan
[ 0.146339] usbcore: registered new interface driver lan78xx
[ 0.160256] 8021q: 802.1Q VLAN Support v1.8
[ 1.378937] LAN9303_MDIO 8000f00.mdio:01: Found LAN9354 rev. 1
[ 1.394316] LAN9303_MDIO 8000f00.mdio:01: configuring for fixed/rmii link mode
[ 1.396514] LAN9303_MDIO 8000f00.mdio:01: Link is Up - 100Mbps/Full - flow control off
[ 1.398273] LAN9303_MDIO 8000f00.mdio:01 lan1 (uninitialized): PHY [dsa-0.0:01] driver [Generic PHY] (irq=POLL)
[ 1.401181] LAN9303_MDIO 8000f00.mdio:01 lan2 (uninitialized): PHY [dsa-0.0:02] driver [Generic PHY] (irq=POLL)
[ 1.401810] LAN9303_MDIO 8000f00.mdio:01: LAN9303 MDIO driver loaded successfully
[ 3.600363] LAN9303_MDIO 8000f00.mdio:01 ethernet1: renamed from lan1
[ 3.603653] LAN9303_MDIO 8000f00.mdio:01 ethernet2: renamed from lan2
[ 8.142677] 8021q: adding VLAN 0 to HW filter on device ethernet3
[ 8.146455] am65-cpsw-nuss 8000000.ethernet: Adding vlan 1 to vlan filter
[ 8.150146] LAN9303_MDIO 8000f00.mdio:01 ethernet1: configuring for phy/gmii link mode
[ 8.155020] LAN9303_MDIO 8000f00.mdio:01 ethernet1: Link is Up - 100Mbps/Full - flow control rx/tx
接口:
root@AS-B-3-261750009:~# ip a
1: lo: <LOOPBACK,UP,LOWER_UP> mtu 65536 qdisc noqueue qlen 1000
link/loopback 00:00:00:00:00:00 brd 00:00:00:00:00:00
inet 127.0.0.1/8 scope host lo
valid_lft forever preferred_lft forever
inet6 ::1/128 scope host noprefixroute
valid_lft forever preferred_lft forever
2: ethernet3: <BROADCAST,MULTICAST,UP,LOWER_UP> mtu 1504 qdisc mq qlen 1000
link/ether aa:a3:80:99:b7:66 brd ff:ff:ff:ff:ff:ff
inet6 fe80::a8a3:80ff:fe99:b766/64 scope link
valid_lft forever preferred_lft forever
3: ethernet1@ethernet3: <BROADCAST,MULTICAST,UP,LOWER_UP> mtu 1500 qdisc noqueue qlen 1000
link/ether aa:a3:80:99:b7:66 brd ff:ff:ff:ff:ff:ff
inet6 fe80::a8a3:80ff:fe99:b766/64 scope link
valid_lft forever preferred_lft forever
4: ethernet2@ethernet3: <BROADCAST,MULTICAST> mtu 1500 qdisc noop qlen 1000
link/ether aa:a3:80:99:b7:66 brd ff:ff:ff:ff:ff:ff
5: g_ether0: <NO-CARRIER,BROADCAST,MULTICAST,UP> mtu 1500 qdisc pfifo_fast qlen 1000
link/ether 62:d9:66:af:f6:5c brd ff:ff:ff:ff:ff:ff
inet6 fe80::2:6175:9/64 scope link tentative
valid_lft forever preferred_lft forever
6: g_ether1: <BROADCAST,MULTICAST,UP,LOWER_UP> mtu 1500 qdisc pfifo_fast qlen 1000
link/ether 2a:1a:1e:d6:3b:c9 brd ff:ff:ff:ff:ff:ff
inet6 fe80::2:6175:9/64 scope link
valid_lft forever preferred_lft forever
inet6 fe80::281a:1eff:fed6:3bc9/64 scope link
valid_lft forever preferred_lft forever
7: br0: <BROADCAST,MULTICAST> mtu 1500 qdisc noop qlen 1000
link/ether de:ef:90:2b:e1:d3 brd ff:ff:ff:ff:ff:ff
尝试配置 Ethernet1:
root@AS-B-3-261750009:~# ip addr add 10.142.3.9/22 dev ethernet1
root@AS-B-3-261750009:~# ip link set ethernet1 up
root@AS-B-3-261750009:~# ip route add default via 10.142.0.1
root@AS-B-3-261750009:~# ping -c 4 10.142.0.1
PING 10.142.0.1 (10.142.0.1): 56 data bytes
--- 10.142.0.1 ping statistics ---
4 packets transmitted, 0 packets received, 100% packet loss
像往常一样,感谢所有的帮助,我可以得到。
此致、
/BO