请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:AM5729 “线程”中讨论的其它部件:BeagleBone, PCM5102A, test
我希望能够在我的 BeagleBone AI (AM5729)中记录来自 TIDA-01454 CMB 的信息,因此我遵循 本指南 时有一些不同,因为它是 BeagleBone AI,而不是 BeagleBone Black。 我成功地添加和修改 了 pcm5102a.c 编解码器,因此在使用 arecord-l 命令时,声卡已注册并显示。 我还配置了具有 I2C 的 CMB,因此蓝色 LED 亮起。 但是,当我尝试录制测试文件时,我收到以下错误:
ebian@beaglebone:/var/lib/cloud9$ arecord --device="hw:1,0" -d 20 -f S16_LE test.wav Recording WAVE 'test.wav' : Signed 16 bit Little Endian, Rate 8000 Hz, Mono arecord: pcm_read:2145: read error: Input/output error
我认为这可能是 ALSA 配置问题或 DTS 文件的问题(因为我无法使用指南中使用的文件),所以我保留这两个文件以防需要它们。 但这可能是任何其他问题。
请提前感谢您的参与。
米克尔
asound.conf:
pcm.onboard{ type hw card 0 } ctl.onboard { type hw card 0 } ### Dsnoop splited channels pcm.onboard_capture_left { type dsnoop ipc_key 32 slave { pcm "onboard" channels 2 rate 48000 format S32_LE } bindings.0 0 } pcm.onboard_playback_left { type dmix ipc_key 33 slave { pcm "onboard" channels 2 } bindings.0 0 } pcm.onboard_capture_right { type dsnoop ipc_key 32 slave { pcm "onboard" channels 2 rate 48000 format S32_LE } bindings.0 1 } pcm.onboard_playback_right { type dmix ipc_key 33 slave { pcm "onboard" channels 2 } bindings.0 1 } ### PLUGS ## ### used with darkice ### device = plug:plug_onboard_left pcm.plug_onboard_capture_left{ type plug slave.pcm "onboard_capture_left" } pcm.plug_onboard_playback_left{ type plug slave.pcm "onboard_playback_left" } pcm.!default { type asym playback.pcm "plug_onboard_playback_left" capture.pcm "plug_onboard_capture_left" }
DTS 文件:
#include "am5729-beagleboneai.dts" // make it easy to determine which dtb you're currently running on // (via /proc/device-tree/chosen/) / { chosen { base_dtb = "am5729-beagleboneai-custom.dts"; base_dtb_timestamp = __TIMESTAMP__; }; }; // eventually these should be available in a header #define P9_14 (0x3400 + 4 * 107) #define P9_16 (0x3400 + 4 * 108) #define P9_19a (0x3400 + 4 * 16) #define P9_19b (0x3400 + 4 * 95) #define P9_20a (0x3400 + 4 * 17) #define P9_20b (0x3400 + 4 * 94) #define P9_12 (0x3400 + 4 * 171) #define P9_27b (0x3400 + 4 * 172) #define P9_18b (0x3400 + 4 * 173) // /{ pcm5102a: pcm5102a { #sound-dai-cells = <0>; compatible = "ti,pcm5102a"; status = "okay"; }; sound {compatible = "simple-audio-card"; simple-audio-card,format = "i2s"; simple-audio-card,name = "PCM5102a"; simple-audio-card,bitclock-master = <&sound1_master>; simple-audio-card,frame-master = <&sound1_master>; simple-audio-card,bitclock-inversion; simple-audio-card,cpu { sound-dai = <&mcasp1>; }; sound1_master: simple-audio-card,codec { #sound-dai-cells = <0>; sound-dai = <&pcm5102a>; }; }; }; // enable i2c-3 on P9.19 (scl) + P9.20 (sda) &i2c4 { status = "okay"; clock-frequency = <400000>; pinctrl-names = "default"; pinctrl-0 = <&i2c4_pins>; }; &mcasp1 { #sound-dai-cells = <0>; status = "okay"; pinctrl-names = "default"; pinctrl-0 = <&mcasp1_pins>; op-mode = <0>; /* MCASP_IIS_MODE */ tdm-slots = <2>; num-serializer = <4>; /* 16 serializers */ serial-dir = < /* 1 TX 2 RX 0 unused */ 2 0 0 0 >; rx-num-evt = <1>; tx-num-evt = <1>; }; &dra7_pmx_core { i2c4_pins: i2c4 { pinctrl-single,pins = < DRA7XX_CORE_IOPAD( P9_19a, PIN_INPUT_PULLUP | MUX_MODE7 ) // scl DRA7XX_CORE_IOPAD( P9_19b, PIN_INPUT_PULLUP | MUX_MODE14 ) // (shared pin) DRA7XX_CORE_IOPAD( P9_20a, PIN_INPUT_PULLUP | MUX_MODE7 ) // sda DRA7XX_CORE_IOPAD( P9_20b, PIN_INPUT_PULLUP | MUX_MODE14 ) // (shared pin) >; }; mcasp1_pins: mcasp1_pins { pinctrl-single,pins = < DRA7XX_CORE_IOPAD(P9_12, PIN_INPUT_PULLDOWN | MUX_MODE0) // 12 0 mcasp1_aclkr BIT CLOCK BCLK DRA7XX_CORE_IOPAD(P9_27b, PIN_INPUT | MUX_MODE0) // 27b 0 mcasp1_fsr FRAME SYNC LRCLK DRA7XX_CORE_IOPAD(P9_18b, PIN_INPUT | MUX_MODE0) // 18b 0 mcasp1_axr0 I2S INPUT DATA >; }; }; // enable pwm-2 on P9.14 (out-A) + P9.16 (out-B) &epwmss2 { status = "okay"; }; &ehrpwm2 { status = "okay"; pinctrl-names = "default"; pinctrl-0 = <&ehrpwm2_pins>; }; &dra7_pmx_core { ehrpwm2_pins: ehrpwm2 { pinctrl-single,pins = < DRA7XX_CORE_IOPAD( P9_14, PIN_OUTPUT_PULLDOWN | MUX_MODE10 ) // out A DRA7XX_CORE_IOPAD( P9_16, PIN_OUTPUT_PULLDOWN | MUX_MODE10 ) // out B >; }; }; // Here's the obnoxious part: since u-boot doesn't have same pin defaults yet, all pins not // explicitly setup above should be overridden here. This will eventually no longer be needed. &cape_pins_default { pinctrl-single,pins = < DRA7XX_CORE_IOPAD( 0x372C, PIN_INPUT_PULLDOWN | MUX_MODE15 ) // P9.11a (no gpio) DRA7XX_CORE_IOPAD( 0x3620, PIN_INPUT | MUX_MODE14 ) // P9.11b //DRA7XX_CORE_IOPAD( 0x36AC, PIN_INPUT_PULLDOWN | MUX_MODE14 ) // P9.12 DRA7XX_CORE_IOPAD( 0x3730, PIN_INPUT_PULLDOWN | MUX_MODE15 ) // P9.13 (no gpio) // DRA7XX_CORE_IOPAD( 0x35AC, PIN_INPUT_PULLDOWN | MUX_MODE14 ) // P9.14 DRA7XX_CORE_IOPAD( 0x3514, PIN_INPUT_PULLDOWN | MUX_MODE14 ) // P9.15 // DRA7XX_CORE_IOPAD( 0x35B0, PIN_INPUT_PULLDOWN | MUX_MODE14 ) // P9.16 DRA7XX_CORE_IOPAD( 0x37CC, PIN_INPUT_PULLDOWN | MUX_MODE14 ) // P9.17a DRA7XX_CORE_IOPAD( 0x36B8, PIN_INPUT | MUX_MODE14 ) // P9.17b DRA7XX_CORE_IOPAD( 0x37C8, PIN_INPUT_PULLDOWN | MUX_MODE14 ) // P9.18a //DRA7XX_CORE_IOPAD( 0x36B4, PIN_INPUT | MUX_MODE14 ) // P9.18b // DRA7XX_CORE_IOPAD( 0x3440, PIN_INPUT_PULLUP | MUX_MODE14 ) // P9.19a // DRA7XX_CORE_IOPAD( 0x357C, PIN_INPUT | MUX_MODE14 ) // P9.19b // DRA7XX_CORE_IOPAD( 0x3444, PIN_INPUT_PULLUP | MUX_MODE14 ) // P9.20a // DRA7XX_CORE_IOPAD( 0x3578, PIN_INPUT | MUX_MODE14 ) // P9.20b DRA7XX_CORE_IOPAD( 0x34F0, PIN_INPUT_PULLDOWN | MUX_MODE14 ) // P9.21a DRA7XX_CORE_IOPAD( 0x37C4, PIN_INPUT | MUX_MODE14 ) // P9.21b DRA7XX_CORE_IOPAD( 0x369C, PIN_INPUT_PULLDOWN | MUX_MODE14 ) // P9.22a DRA7XX_CORE_IOPAD( 0x37C0, PIN_INPUT | MUX_MODE14 ) // P9.22b DRA7XX_CORE_IOPAD( 0x37B4, PIN_INPUT_PULLUP | MUX_MODE14 ) // P9.23 DRA7XX_CORE_IOPAD( 0x368C, PIN_INPUT_PULLUP | MUX_MODE14 ) // P9.24 DRA7XX_CORE_IOPAD( 0x3694, PIN_INPUT_PULLDOWN | MUX_MODE14 ) // P9.25 DRA7XX_CORE_IOPAD( 0x3688, PIN_INPUT_PULLUP | MUX_MODE14 ) // P9.26a DRA7XX_CORE_IOPAD( 0x3544, PIN_INPUT | MUX_MODE14 ) // P9.26b DRA7XX_CORE_IOPAD( 0x35A0, PIN_INPUT_PULLDOWN | MUX_MODE14 ) // P9.27a //DRA7XX_CORE_IOPAD( 0x36B0, PIN_INPUT | MUX_MODE14 ) // P9.27b DRA7XX_CORE_IOPAD( 0x36E0, PIN_INPUT_PULLDOWN | MUX_MODE14 ) // P9.28 DRA7XX_CORE_IOPAD( 0x36D8, PIN_INPUT_PULLDOWN | MUX_MODE14 ) // P9.29a DRA7XX_CORE_IOPAD( 0x36A8, PIN_INPUT | MUX_MODE14 ) // P9.29b DRA7XX_CORE_IOPAD( 0x36DC, PIN_INPUT_PULLDOWN | MUX_MODE14 ) // P9.30 DRA7XX_CORE_IOPAD( 0x36D4, PIN_INPUT_PULLDOWN | MUX_MODE14 ) // P9.31a DRA7XX_CORE_IOPAD( 0x36A4, PIN_INPUT | MUX_MODE14 ) // P9.31b DRA7XX_CORE_IOPAD( 0x36A0, PIN_INPUT_PULLDOWN | MUX_MODE14 ) // P9.41a DRA7XX_CORE_IOPAD( 0x3580, PIN_INPUT | MUX_MODE14 ) // P9.41b DRA7XX_CORE_IOPAD( 0x36E4, PIN_INPUT_PULLDOWN | MUX_MODE14 ) // P9.42a DRA7XX_CORE_IOPAD( 0x359C, PIN_INPUT | MUX_MODE14 ) // P9.42b DRA7XX_CORE_IOPAD( 0x379C, PIN_INPUT_PULLUP | MUX_MODE14 ) // P8.3 DRA7XX_CORE_IOPAD( 0x37A0, PIN_INPUT_PULLUP | MUX_MODE14 ) // P8.4 DRA7XX_CORE_IOPAD( 0x378C, PIN_INPUT_PULLUP | MUX_MODE14 ) // P8.5 DRA7XX_CORE_IOPAD( 0x3790, PIN_INPUT_PULLUP | MUX_MODE14 ) // P8.6 DRA7XX_CORE_IOPAD( 0x36EC, PIN_INPUT_PULLDOWN | MUX_MODE14 ) // P8.7 DRA7XX_CORE_IOPAD( 0x36F0, PIN_INPUT_PULLDOWN | MUX_MODE14 ) // P8.8 DRA7XX_CORE_IOPAD( 0x3698, PIN_INPUT_PULLDOWN | MUX_MODE14 ) // P8.9 DRA7XX_CORE_IOPAD( 0x36E8, PIN_INPUT_PULLDOWN | MUX_MODE14 ) // P8.10 DRA7XX_CORE_IOPAD( 0x3510, PIN_INPUT_PULLDOWN | MUX_MODE14 ) // P8.11 DRA7XX_CORE_IOPAD( 0x350C, PIN_INPUT_PULLDOWN | MUX_MODE14 ) // P8.12 DRA7XX_CORE_IOPAD( 0x3590, PIN_INPUT_PULLDOWN | MUX_MODE14 ) // P8.13 DRA7XX_CORE_IOPAD( 0x3598, PIN_INPUT_PULLDOWN | MUX_MODE14 ) // P8.14 DRA7XX_CORE_IOPAD( 0x3570, PIN_INPUT_PULLDOWN | MUX_MODE14 ) // P8.15a DRA7XX_CORE_IOPAD( 0x35B4, PIN_INPUT | MUX_MODE14 ) // P8.15b DRA7XX_CORE_IOPAD( 0x35BC, PIN_INPUT_PULLDOWN | MUX_MODE14 ) // P8.16 DRA7XX_CORE_IOPAD( 0x3624, PIN_INPUT_PULLDOWN | MUX_MODE14 ) // P8.17 DRA7XX_CORE_IOPAD( 0x3588, PIN_INPUT_PULLDOWN | MUX_MODE14 ) // P8.18 DRA7XX_CORE_IOPAD( 0x358C, PIN_INPUT_PULLDOWN | MUX_MODE14 ) // P8.19 DRA7XX_CORE_IOPAD( 0x3780, PIN_INPUT_PULLUP | MUX_MODE14 ) // P8.20 DRA7XX_CORE_IOPAD( 0x377C, PIN_INPUT_PULLUP | MUX_MODE14 ) // P8.21 DRA7XX_CORE_IOPAD( 0x3798, PIN_INPUT_PULLUP | MUX_MODE14 ) // P8.22 DRA7XX_CORE_IOPAD( 0x3794, PIN_INPUT_PULLUP | MUX_MODE14 ) // P8.23 DRA7XX_CORE_IOPAD( 0x3788, PIN_INPUT_PULLUP | MUX_MODE14 ) // P8.24 DRA7XX_CORE_IOPAD( 0x3784, PIN_INPUT_PULLUP | MUX_MODE14 ) // P8.25 DRA7XX_CORE_IOPAD( 0x35B8, PIN_INPUT_PULLDOWN | MUX_MODE14 ) // P8.26 DRA7XX_CORE_IOPAD( 0x35D8, PIN_INPUT_PULLDOWN | MUX_MODE14 ) // P8.27a DRA7XX_CORE_IOPAD( 0x3628, PIN_INPUT | MUX_MODE14 ) // P8.27b DRA7XX_CORE_IOPAD( 0x35C8, PIN_INPUT_PULLDOWN | MUX_MODE14 ) // P8.28a DRA7XX_CORE_IOPAD( 0x362C, PIN_INPUT | MUX_MODE14 ) // P8.28b DRA7XX_CORE_IOPAD( 0x35D4, PIN_INPUT_PULLDOWN | MUX_MODE14 ) // P8.29a DRA7XX_CORE_IOPAD( 0x3630, PIN_INPUT | MUX_MODE14 ) // P8.29b DRA7XX_CORE_IOPAD( 0x35CC, PIN_INPUT_PULLDOWN | MUX_MODE14 ) // P8.30a DRA7XX_CORE_IOPAD( 0x3634, PIN_INPUT | MUX_MODE14 ) // P8.30b DRA7XX_CORE_IOPAD( 0x3614, PIN_INPUT_PULLDOWN | MUX_MODE14 ) // P8.31a DRA7XX_CORE_IOPAD( 0x373C, PIN_INPUT_PULLDOWN | MUX_MODE15 ) // P8.31b (no gpio) DRA7XX_CORE_IOPAD( 0x3618, PIN_INPUT_PULLDOWN | MUX_MODE14 ) // P8.32a DRA7XX_CORE_IOPAD( 0x3740, PIN_INPUT_PULLDOWN | MUX_MODE15 ) // P8.32b (no gpio) DRA7XX_CORE_IOPAD( 0x3610, PIN_INPUT_PULLDOWN | MUX_MODE14 ) // P8.33a DRA7XX_CORE_IOPAD( 0x34E8, PIN_INPUT | MUX_MODE14 ) // P8.33b DRA7XX_CORE_IOPAD( 0x3608, PIN_INPUT_PULLDOWN | MUX_MODE14 ) // P8.34a DRA7XX_CORE_IOPAD( 0x3564, PIN_INPUT | MUX_MODE14 ) // P8.34b DRA7XX_CORE_IOPAD( 0x360C, PIN_INPUT_PULLDOWN | MUX_MODE14 ) // P8.35a DRA7XX_CORE_IOPAD( 0x34E4, PIN_INPUT | MUX_MODE14 ) // P8.35b DRA7XX_CORE_IOPAD( 0x3604, PIN_INPUT_PULLDOWN | MUX_MODE14 ) // P8.36a DRA7XX_CORE_IOPAD( 0x3568, PIN_INPUT | MUX_MODE14 ) // P8.36b DRA7XX_CORE_IOPAD( 0x35FC, PIN_INPUT_PULLDOWN | MUX_MODE14 ) // P8.37a DRA7XX_CORE_IOPAD( 0x3738, PIN_INPUT_PULLDOWN | MUX_MODE15 ) // P8.37b (no gpio) DRA7XX_CORE_IOPAD( 0x3600, PIN_INPUT_PULLDOWN | MUX_MODE14 ) // P8.38a DRA7XX_CORE_IOPAD( 0x3734, PIN_INPUT_PULLDOWN | MUX_MODE15 ) // P8.38b (no gpio) DRA7XX_CORE_IOPAD( 0x35F4, PIN_INPUT_PULLDOWN | MUX_MODE14 ) // P8.39 DRA7XX_CORE_IOPAD( 0x35F8, PIN_INPUT_PULLDOWN | MUX_MODE14 ) // P8.40 DRA7XX_CORE_IOPAD( 0x35EC, PIN_INPUT_PULLDOWN | MUX_MODE14 ) // P8.41 DRA7XX_CORE_IOPAD( 0x35F0, PIN_INPUT_PULLDOWN | MUX_MODE14 ) // P8.42 DRA7XX_CORE_IOPAD( 0x35E4, PIN_INPUT_PULLDOWN | MUX_MODE14 ) // P8.43 DRA7XX_CORE_IOPAD( 0x35E8, PIN_INPUT_PULLDOWN | MUX_MODE14 ) // P8.44 DRA7XX_CORE_IOPAD( 0x35DC, PIN_INPUT_PULLDOWN | MUX_MODE14 ) // P8.45a DRA7XX_CORE_IOPAD( 0x361C, PIN_INPUT | MUX_MODE14 ) // P8.45b DRA7XX_CORE_IOPAD( 0x35E0, PIN_INPUT_PULLDOWN | MUX_MODE14 ) // P8.46a DRA7XX_CORE_IOPAD( 0x3638, PIN_INPUT | MUX_MODE14 ) // P8.46b >; };