This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TMS320DM8168:嵌入式Linux中的AVS控制

Guru**** 2805935 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1104059/tms320dm8168-avs-control-in-embedded-linux

部件号:TMS320DM8168

您好,

我无法在Wiki中找到AVS相关文档。 我想在嵌入式Linux中启用AVS,用于自定义DM8168卡。 请共享文档,在嵌入式Linux中进行必要的更改,以使AVS能够解决与-40°C至85°C的工作温度相关的问题(如果没有风扇,则仅使用散热片散热)。

提前感谢您,

此致,

KumaraswamyHollaV