This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] PROCESSOR-SDK-AM64X:AM6442 ICSSG1连接到2个 PHY

Guru**** 2553450 points
Other Parts Discussed in Thread: DP83869HM

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1116655/processor-sdk-am64x-am6442-icssg1-connected-to-2-phys

器件型号:PROCESSOR-SDK-AM64X
主题中讨论的其他器件:DP83869HM

我有一个带 AM64X 处理器的定制硬件。

我的软件是 Linux 内核5.10.41。

我有2个 DP83869HM PHY 连接到 ICSSG1-pru1和 ICSSG1-pru0

我正在使用  08.04.00.003中的 am65x-sr2-固件:   

am65x-sr2-pru0-prueth-Fw.elf   am65x-sr2-rtu1-prueth-Fw.elf
am65x-sr2-pru1-prueth-Fw.elf  am65x-sr2-txpru0-prueth-Fw.elf
am65x-sr2-rtu0-prueth-Fw.elf  am65x-sr2-txpru1-prueth-Fw.elf

我可以检测 MDIO 总线上2个 PHY 的链路 、但无法通过 MII 总线(RGMII)发送/接收数据。

我想器件树中的某些内容未正确定义、或者我使用了错误的固件。

当我尝试 ping 外部时、TX 计数器会增加、但 RX 计数器保持为0。

在另一台计算机上使用 tcpdump、我验证了硬件中的数据实际上没有发送。

设备树:

// SPDX-License-Identifier: GPL-2.0
/*
 * Copyright (C) 2020-2021 Texas Instruments Incorporated - https://www.ti.com/
 */

/dts-v1/;

#include <dt-bindings/phy/phy.h>
#include <dt-bindings/mux/ti-serdes.h>
#include <dt-bindings/leds/common.h>
#include <dt-bindings/gpio/gpio.h>
#include <dt-bindings/net/ti-dp83869.h>
#include "k3-am642.dtsi"

/ {
	compatible =  "ti,am642-evm", "ti,am642";
	model = "Texas Instruments AM642 SolidRun Board";

	chosen {
		stdout-path = "serial2:115200n8";
		bootargs = "console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000";
	};

	aliases {
		ethernet2 = &icssg1_emac0;
		ethernet3 = &icssg1_emac1;
	};

	memory@80000000 {
		device_type = "memory";
		/* 1G RAM */
                reg = <0x0 0x80000000 0 0x40000000>;

	};

	reserved-memory {
		#address-cells = <2>;
		#size-cells = <2>;
		ranges;

		secure_ddr: optee@9e800000 {
			reg = <0x00 0x9e800000 0x00 0x01800000>; /* for OP-TEE */
			alignment = <0x1000>;
			no-map;
		};

		main_r5fss0_core0_dma_memory_region: r5f-dma-memory@a0000000 {
			compatible = "shared-dma-pool";
			reg = <0x00 0xa0000000 0x00 0x100000>;
			no-map;
		};

		main_r5fss0_core0_memory_region: r5f-memory@a0100000 {
			compatible = "shared-dma-pool";
			reg = <0x00 0xa0100000 0x00 0xf00000>;
			no-map;
		};

		main_r5fss0_core1_dma_memory_region: r5f-dma-memory@a1000000 {
			compatible = "shared-dma-pool";
			reg = <0x00 0xa1000000 0x00 0x100000>;
			no-map;
		};

		main_r5fss0_core1_memory_region: r5f-memory@a1100000 {
			compatible = "shared-dma-pool";
			reg = <0x00 0xa1100000 0x00 0xf00000>;
			no-map;
		};

		main_r5fss1_core0_dma_memory_region: r5f-dma-memory@a2000000 {
			compatible = "shared-dma-pool";
			reg = <0x00 0xa2000000 0x00 0x100000>;
			no-map;
		};

		main_r5fss1_core0_memory_region: r5f-memory@a2100000 {
			compatible = "shared-dma-pool";
			reg = <0x00 0xa2100000 0x00 0xf00000>;
			no-map;
		};

		main_r5fss1_core1_dma_memory_region: r5f-dma-memory@a3000000 {
			compatible = "shared-dma-pool";
			reg = <0x00 0xa3000000 0x00 0x100000>;
			no-map;
		};

		main_r5fss1_core1_memory_region: r5f-memory@a3100000 {
			compatible = "shared-dma-pool";
			reg = <0x00 0xa3100000 0x00 0xf00000>;
			no-map;
		};

		rtos_ipc_memory_region: ipc-memories@a5000000 {
			reg = <0x00 0xa5000000 0x00 0x00800000>;
			alignment = <0x1000>;
			no-map;
		};
	};

	evm_12v0: fixedregulator-evm12v0 {
		/* main DC jack */
		compatible = "regulator-fixed";
		regulator-name = "evm_12v0";
		regulator-min-microvolt = <12000000>;
		regulator-max-microvolt = <12000000>;
		regulator-always-on;
		regulator-boot-on;
	};

	vsys_5v0: fixedregulator-vsys5v0 {
		/* output of LM5140 */
		compatible = "regulator-fixed";
		regulator-name = "vsys_5v0";
		regulator-min-microvolt = <5000000>;
		regulator-max-microvolt = <5000000>;
		vin-supply = <&evm_12v0>;
		regulator-always-on;
		regulator-boot-on;
	};

	vsys_3v3: fixedregulator-vsys3v3 {
		/* output of LM5140 */
		compatible = "regulator-fixed";
		regulator-name = "vsys_3v3";
		regulator-min-microvolt = <3300000>;
		regulator-max-microvolt = <3300000>;
		vin-supply = <&evm_12v0>;
		regulator-always-on;
		regulator-boot-on;
	};

	vdd_mmc1: fixed-regulator-sd {
		/* TPS2051BD */
		compatible = "regulator-fixed";
		regulator-name = "vdd_mmc1";
		regulator-min-microvolt = <3300000>;
		regulator-max-microvolt = <3300000>;
		regulator-boot-on;
		enable-active-high;
		vin-supply = <&vsys_3v3>;
		gpio = <&exp1 6 GPIO_ACTIVE_HIGH>;
	};

	vddb: fixedregulator-vddb {
		compatible = "regulator-fixed";
		regulator-name = "vddb_3v3_display";
		regulator-min-microvolt = <3300000>;
		regulator-max-microvolt = <3300000>;
		vin-supply = <&vsys_3v3>;
		regulator-always-on;
		regulator-boot-on;
	};

	leds {
		compatible = "gpio-leds";

		led-0 {
			label = "am64-evm:red:heartbeat";
			gpios = <&exp1 16 GPIO_ACTIVE_HIGH>;
			linux,default-trigger = "heartbeat";
			function = LED_FUNCTION_HEARTBEAT;
			default-state = "off";
		};
	};
	
    mdio_mux: mux-controller {
        compatible = "gpio-mux";
        #mux-control-cells = <0>;

        mux-gpios = <&exp1 12 GPIO_ACTIVE_HIGH>;
    };


	transceiver1: can-phy0 {
		compatible = "ti,tcan1042";
		#phy-cells = <0>;
		max-bitrate = <5000000>;
		standby-gpios = <&exp1 8 GPIO_ACTIVE_HIGH>;
	};

	transceiver2: can-phy1 {
		compatible = "ti,tcan1042";
		#phy-cells = <0>;
		max-bitrate = <5000000>;
		standby-gpios = <&exp1 9 GPIO_ACTIVE_HIGH>;
	};
	
    davinci_mdio: mdio@4a101000 {
         compatible = "ti,davinci_mdio";
         #address-cells = <1>;
         #size-cells = <0>;
         reg = <0x4a101000 0x1000>;
         bus_freq = <1000000>;
    };

	icssg1_eth: icssg1-eth {
        status = "okay";
		compatible = "ti,am642-icssg-prueth";
		pinctrl-names = "default";
		pinctrl-0 = <&icssg1_rgmii1_pins_default &icssg1_rgmii2_pins_default>;


		sram = <&oc_sram>;
		ti,prus = <&pru1_0>, <&rtu1_0>, <&tx_pru1_0>, <&pru1_1>, <&rtu1_1>, <&tx_pru1_1>;
		firmware-name = "ti-pruss/am65x-sr2-pru0-prueth-fw.elf",
				"ti-pruss/am65x-sr2-rtu0-prueth-fw.elf",
				"ti-pruss/am65x-sr2-txpru0-prueth-fw.elf",
				"ti-pruss/am65x-sr2-pru1-prueth-fw.elf",
				"ti-pruss/am65x-sr2-rtu1-prueth-fw.elf",
				"ti-pruss/am65x-sr2-txpru1-prueth-fw.elf";

		ti,pruss-gp-mux-sel = <2>,	/* MII mode */
				      <2>,
				      <2>,
				      <2>,	/* MII mode */
				      <2>,
				      <2>;

		mii-g-rt = <&icssg1_mii_g_rt>;
        mii-rt = <&icssg1_mii_rt>;
        iep = <&icssg1_iep0>,  <&icssg1_iep1>;
        
        interrupt-parent = <&icssg1_intc>;
        interrupts = <24 0 2>, <25 1 3>;
        interrupt-names = "tx_ts0", "tx_ts1";
        
		dmas = <&main_pktdma 0xc200 0>, /* egress slice 0 */
		       <&main_pktdma 0xc201 0>, /* egress slice 0 */
		       <&main_pktdma 0xc202 0>, /* egress slice 0 */
		       <&main_pktdma 0xc203 0>, /* egress slice 0 */
		       <&main_pktdma 0xc204 0>, /* egress slice 1 */
		       <&main_pktdma 0xc205 0>, /* egress slice 1 */
		       <&main_pktdma 0xc206 0>, /* egress slice 1 */
		       <&main_pktdma 0xc207 0>, /* egress slice 1 */
		       <&main_pktdma 0x4200 0>, /* ingress slice 0 */
		       <&main_pktdma 0x4201 0>, /* ingress slice 1 */
		       <&main_pktdma 0x4202 0>, /* mgmnt rsp slice 0 */
		       <&main_pktdma 0x4203 0>; /* mgmnt rsp slice 1 */
		dma-names = "tx0-0", "tx0-1", "tx0-2", "tx0-3",
			    "tx1-0", "tx1-1", "tx1-2", "tx1-3",
			    "rx0", "rx1","rxmgm0", "rxmgm1";
            

		icssg1_emac0: ethernet-mii0 {
            status = "okay";
			phy-handle = <&icssg1_phy1>;
			phy-mode = "rgmii-rxid";
			syscon-rgmii-delay = <&main_conf 0x4110>;
			/* Filled in by bootloader */
			local-mac-address = [12 34 53 12 55 67];
		};

		icssg1_emac1: ethernet-mii1 {
            status = "okay";
			phy-handle = <&icssg1_phy2>;
			phy-mode = "rgmii-rxid";
			syscon-rgmii-delay = <&main_conf 0x4114>;
			/* Filled in by bootloader */
			local-mac-address = [12 34 53 12 55 58];
		};
	};

};

&oc_sram {
	main_r5fss0_core0_sram: r5f-sram@40000 {
		reg = <0x40000 0x40000>;
	};

	main_r5fss0_core1_sram: r5f-sram@80000 {
		reg = <0x80000 0x40000>;
	};

	main_r5fss1_core0_sram: r5f-sram@c0000 {
		reg = <0xc0000 0x40000>;
	};

	main_r5fss1_core1_sram: r5f-sram@100000 {
		reg = <0x100000 0x40000>;
	};
};

&main_r5fss0_core0 {
	mboxes = <&mailbox0_cluster2 &mbox_main_r5fss0_core0>;
	memory-region = <&main_r5fss0_core0_dma_memory_region>,
			<&main_r5fss0_core0_memory_region>;
	sram = <&main_r5fss0_core0_sram>;
};

&main_r5fss0_core1 {
	mboxes = <&mailbox0_cluster2 &mbox_main_r5fss0_core1>;
	memory-region = <&main_r5fss0_core1_dma_memory_region>,
			<&main_r5fss0_core1_memory_region>;
	sram = <&main_r5fss0_core1_sram>;
};

&main_r5fss1_core0 {
	mboxes = <&mailbox0_cluster4 &mbox_main_r5fss1_core0>;
	memory-region = <&main_r5fss1_core0_dma_memory_region>,
			<&main_r5fss1_core0_memory_region>;
	sram = <&main_r5fss1_core0_sram>;
};

&main_r5fss1_core1 {
	mboxes = <&mailbox0_cluster4 &mbox_main_r5fss1_core1>;
	memory-region = <&main_r5fss1_core1_dma_memory_region>,
			<&main_r5fss1_core1_memory_region>;
	sram = <&main_r5fss1_core1_sram>;
};

&main_pmx0 {
	main_mmc1_pins_default: main-mmc1-pins-default {
		pinctrl-single,pins = <
			AM64X_IOPAD(0x0294, PIN_INPUT_PULLUP, 0) /* (J19) MMC1_CMD */
			AM64X_IOPAD(0x028c, PIN_INPUT_PULLDOWN, 0) /* (L20) MMC1_CLK */
			AM64X_IOPAD(0x0288, PIN_INPUT_PULLUP, 0) /* (K21) MMC1_DAT0 */
			AM64X_IOPAD(0x0284, PIN_INPUT_PULLUP, 0) /* (L21) MMC1_DAT1 */
			AM64X_IOPAD(0x0280, PIN_INPUT_PULLUP, 0) /* (K19) MMC1_DAT2 */
			AM64X_IOPAD(0x027c, PIN_INPUT_PULLUP, 0) /* (K18) MMC1_DAT3 */
			AM64X_IOPAD(0x029c, PIN_INPUT, 0) /* (C20) MMC1_SDWP */
			AM64X_IOPAD(0x0290, PIN_INPUT, 0) /* MMC1_CLKLB */
		>;
	};

	main_uart0_pins_default: main-uart0-pins-default {
		pinctrl-single,pins = <
			AM64X_IOPAD(0x0238, PIN_INPUT, 0) /* (B16) UART0_CTSn */
			AM64X_IOPAD(0x023c, PIN_OUTPUT, 0) /* (A16) UART0_RTSn */
			AM64X_IOPAD(0x0230, PIN_INPUT, 0) /* (D15) UART0_RXD */
			AM64X_IOPAD(0x0234, PIN_OUTPUT, 0) /* (C16) UART0_TXD */
		>;
	};

	main_spi0_pins_default: main-spi0-pins-default {
		pinctrl-single,pins = <
			AM64X_IOPAD(0x0210, PIN_INPUT, 0) /* (D13) SPI0_CLK */
			AM64X_IOPAD(0x0208, PIN_OUTPUT, 0) /* (D12) SPI0_CS0 */
			AM64X_IOPAD(0x0214, PIN_OUTPUT, 0) /* (A13) SPI0_D0 */
			AM64X_IOPAD(0x0218, PIN_INPUT, 0) /* (A14) SPI0_D1 */
		>;
	};

	i2c0_pins: i2c0-pins {
		pinctrl-single,pins = <
			AM64X_IOPAD(0x0260, PIN_INPUT_PULLUP, 0) /* (A18) I2C0_SCL */
			AM64X_IOPAD(0x0264, PIN_INPUT_PULLUP, 0) /* (B18) I2C0_SDA */
		>;
	};

	main_i2c1_pins_default: main-i2c1-pins-default {
		pinctrl-single,pins = <
			AM64X_IOPAD(0x0268, PIN_INPUT_PULLUP, 0) /* (C18) I2C1_SCL */
			AM64X_IOPAD(0x026c, PIN_INPUT_PULLUP, 0) /* (B19) I2C1_SDA */
		>;
	};
	mdio1_pins_default: mdio1-pins-default {
		pinctrl-single,pins = <
			AM64X_IOPAD(0x01fc, PIN_OUTPUT, 4) /* (R2) PRG0_PRU1_GPO19.MDIO0_MDC */
			AM64X_IOPAD(0x01f8, PIN_INPUT, 4) /* (P5) PRG0_PRU1_GPO18.MDIO0_MDIO */
		>;
	};
    
	rgmii1_pins_default: rgmii1-pins-default {
		pinctrl-single,pins = <
			AM64X_IOPAD(0x01cc, PIN_INPUT, 4) /* (W5) PRG0_PRU1_GPO7.RGMII1_RD0 */
			AM64X_IOPAD(0x01d4, PIN_INPUT, 4) /* (Y5) PRG0_PRU1_GPO9.RGMII1_RD1 */
			AM64X_IOPAD(0x01d8, PIN_INPUT, 4) /* (V6) PRG0_PRU1_GPO10.RGMII1_RD2 */
			AM64X_IOPAD(0x01f4, PIN_INPUT, 4) /* (V5) PRG0_PRU1_GPO17.RGMII1_RD3 */
			AM64X_IOPAD(0x0188, PIN_INPUT, 4) /* (AA5) PRG0_PRU0_GPO10.RGMII1_RXC */
			AM64X_IOPAD(0x0184, PIN_INPUT, 4) /* (W6) PRG0_PRU0_GPO9.RGMII1_RX_CTL */
			AM64X_IOPAD(0x0124, PIN_OUTPUT, 4) /* (V15) PRG1_PRU1_GPO7.RGMII1_TD0 */
			AM64X_IOPAD(0x012c, PIN_OUTPUT, 4) /* (V14) PRG1_PRU1_GPO9.RGMII1_TD1 */
			AM64X_IOPAD(0x0130, PIN_OUTPUT, 4) /* (W14) PRG1_PRU1_GPO10.RGMII1_TD2 */
			AM64X_IOPAD(0x014c, PIN_OUTPUT, 4) /* (AA14) PRG1_PRU1_GPO17.RGMII1_TD3 */
			AM64X_IOPAD(0x00e0, PIN_OUTPUT, 4) /* (U14) PRG1_PRU0_GPO10.RGMII1_TXC */
			AM64X_IOPAD(0x00dc, PIN_OUTPUT, 4) /* (U15) PRG1_PRU0_GPO9.RGMII1_TX_CTL */
		>;
	};

	main_usb0_pins_default: main-usb0-pins-default {
		pinctrl-single,pins = <
			AM64X_IOPAD(0x02a8, PIN_OUTPUT, 0) /* (E19) USB0_DRVVBUS */
		>;
	};

	ospi0_pins_default: ospi0-pins-default {
		pinctrl-single,pins = <
			AM64X_IOPAD(0x0000, PIN_OUTPUT, 0) /* (N20) OSPI0_CLK */
			AM64X_IOPAD(0x002c, PIN_OUTPUT, 0) /* (L19) OSPI0_CSn0 */
			AM64X_IOPAD(0x000c, PIN_INPUT, 0) /* (M19) OSPI0_D0 */
			AM64X_IOPAD(0x0010, PIN_INPUT, 0) /* (M18) OSPI0_D1 */
			AM64X_IOPAD(0x0014, PIN_INPUT, 0) /* (M20) OSPI0_D2 */
			AM64X_IOPAD(0x0018, PIN_INPUT, 0) /* (M21) OSPI0_D3 */
			AM64X_IOPAD(0x001c, PIN_INPUT, 0) /* (P21) OSPI0_D4 */
			AM64X_IOPAD(0x0020, PIN_INPUT, 0) /* (P20) OSPI0_D5 */
			AM64X_IOPAD(0x0024, PIN_INPUT, 0) /* (N18) OSPI0_D6 */
			AM64X_IOPAD(0x0028, PIN_INPUT, 0) /* (M17) OSPI0_D7 */
			AM64X_IOPAD(0x0008, PIN_INPUT, 0) /* (N19) OSPI0_DQS */
		>;
	};

	main_mcan0_pins_default: main-mcan0-pins-default {
		pinctrl-single,pins = <
			AM64X_IOPAD(0x0254, PIN_INPUT, 0) /* (B17) MCAN0_RX */
			AM64X_IOPAD(0x0250, PIN_OUTPUT, 0) /* (A17) MCAN0_TX */
		>;
	};

	main_mcan1_pins_default: main-mcan1-pins-default {
		pinctrl-single,pins = <
			AM64X_IOPAD(0x025c, PIN_INPUT, 0) /* (D17) MCAN1_RX */
			AM64X_IOPAD(0x0258, PIN_OUTPUT, 0) /* (C17) MCAN1_TX */
		>;
	};
    
	icssg1_mdio1_pins_default: icssg1-mdio1-pins-default {
		pinctrl-single,pins = <
			AM64X_IOPAD(0x015c, PIN_OUTPUT, 0) /* (Y6) PRG1_MDIO0_MDC */
			AM64X_IOPAD(0x0158, PIN_INPUT, 0) /* (AA6) PRG1_MDIO0_MDIO */
		>;
	};

	icssg1_rgmii1_pins_default: icssg1-rgmii1-pins-default {
		pinctrl-single,pins = <
            /***************ICSSG1 PRU0 ETH3******************/
			AM64X_IOPAD(0x00b8, PIN_INPUT, 2) /* (Y7) PRG1_PRU0_GPO0.PRG1_RGMII1_RD0 */
			AM64X_IOPAD(0x00bc, PIN_INPUT, 2) /* (U8) PRG1_PRU0_GPO1.PRG1_RGMII1_RD1 */
			AM64X_IOPAD(0x00c0, PIN_INPUT, 2) /* (W8) PRG1_PRU0_GPO2.PRG1_RGMII1_RD2 */
			AM64X_IOPAD(0x00c4, PIN_INPUT, 2) /* (V8) PRG1_PRU0_GPO3.PRG1_RGMII1_RD3 */
			AM64X_IOPAD(0x00d0, PIN_INPUT, 2) /* (AA7) PRG1_PRU0_GPO6.PRG1_RGMII1_RXC */
			AM64X_IOPAD(0x00c8, PIN_INPUT, 2) /* (Y8) PRG1_PRU0_GPO4.PRG1_RGMII1_RX_CTL */
			AM64X_IOPAD(0x00e4, PIN_OUTPUT, 2) /* (AA8) PRG1_PRU0_GPO11.PRG1_RGMII1_TD0 */
			AM64X_IOPAD(0x00e8, PIN_OUTPUT, 2) /* (U9) PRG1_PRU0_GPO12.PRG1_RGMII1_TD1 */
			AM64X_IOPAD(0x00ec, PIN_OUTPUT, 2) /* (W9) PRG1_PRU0_GPO13.PRG1_RGMII1_TD2 */
			AM64X_IOPAD(0x00f0, PIN_OUTPUT, 2) /* (AA9) PRG1_PRU0_GPO14.PRG1_RGMII1_TD3 */
			AM64X_IOPAD(0x00f8, PIN_OUTPUT | PIN_INPUT, 2) /* (V9) PRG1_PRU0_GPO16.PRG1_RGMII1_TXC */
			AM64X_IOPAD(0x00f4, PIN_OUTPUT, 2) /* (Y9) PRG1_PRU0_GPO15.PRG1_RGMII1_TX_CTL */
			
		>;
	};
		icssg1_rgmii2_pins_default: icssg1-rgmii2-pins-default {
		pinctrl-single,pins = <

			/***************ICSSG1 PRU1 ETH2******************/
            AM64X_IOPAD(0x0108, PIN_INPUT, 2) /* (W11) PRG1_PRU1_GPO0.RGMII2_RD0 */
			AM64X_IOPAD(0x010c, PIN_INPUT, 2) /* (V11) PRG1_PRU1_GPO1.RGMII2_RD1 */
			AM64X_IOPAD(0x0110, PIN_INPUT, 2) /* (AA12) PRG1_PRU1_GPO2.RGMII2_RD2 */
			AM64X_IOPAD(0x0114, PIN_INPUT, 2) /* (Y12) PRG1_PRU1_GPO3.RGMII2_RD3 */
			AM64X_IOPAD(0x0120, PIN_INPUT, 2) /* (U11) PRG1_PRU1_GPO6.RGMII2_RXC */
			AM64X_IOPAD(0x0118, PIN_INPUT, 2) /* (W12) PRG1_PRU1_GPO4.RGMII2_RX_CTL */
			AM64X_IOPAD(0x0134, PIN_OUTPUT, 2) /* (AA10) PRG1_PRU1_GPO11.RGMII2_TD0 */
			AM64X_IOPAD(0x0138, PIN_OUTPUT, 2) /* (V10) PRG1_PRU1_GPO12.RGMII2_TD1 */
			AM64X_IOPAD(0x013c, PIN_OUTPUT, 2) /* (U10) PRG1_PRU1_GPO13.RGMII2_TD2 */
			AM64X_IOPAD(0x0140, PIN_OUTPUT, 2) /* (AA11) PRG1_PRU1_GPO14.RGMII2_TD3 */
			AM64X_IOPAD(0x0148, PIN_OUTPUT | PIN_INPUT, 2) /* (Y10) PRG1_PRU1_GPO16.RGMII2_TXC */
			AM64X_IOPAD(0x0144, PIN_OUTPUT, 2) /* (Y11) PRG1_PRU1_GPO15.RGMII2_TX_CTL */
			
		>;
	};


	main_ecap0_pins_default: main-ecap0-pins-default {
		pinctrl-single,pins = <
			AM64X_IOPAD(0x0270, PIN_INPUT, 0) /* (D18) ECAP0_IN_APWM_OUT */
		>;
	};
};

&wkup_pmx0 {
	mcu_uart1_pins_default: mcu-uart1-pins-default {
		pinctrl-single,pins = <
			AM64X_MCU_IOPAD(0x0038, PIN_INPUT, 0) /* (C9) MCU_UART1_RXD */
			AM64X_MCU_IOPAD(0x003c, PIN_OUTPUT, 0) /* (D9) MCU_UART1_TXD */
		>;
	};
};

&main_uart0 {
	pinctrl-names = "default";
	pinctrl-0 = <&main_uart0_pins_default>;
};

/* main_uart1 is reserved for firmware usage */
&main_uart1 {
	status = "reserved";
};

&main_uart2 {
	status = "disabled";
};

&main_uart3 {
	status = "disabled";
};

&main_uart4 {
	status = "disabled";
};

&main_uart5 {
	status = "disabled";
};

&main_uart6 {
	status = "disabled";
};

&mcu_uart0 {
	status = "disabled";
};

&mcu_uart1 {
	pinctrl-names = "default";
	pinctrl-0 = <&mcu_uart1_pins_default>;
};


&main_i2c0 {
	pinctrl-names = "default";
	pinctrl-0 = <&i2c0_pins>;
	clock-frequency = <400000>;
};


&main_i2c1 {
	pinctrl-names = "default";
	pinctrl-0 = <&main_i2c1_pins_default>;
	clock-frequency = <400000>;

	exp1: gpio@22 {
		compatible = "ti,tca6424";
		reg = <0x22>;
		gpio-controller;
		#gpio-cells = <2>;
		gpio-line-names = "GPIO_eMMC_RSTn", "CAN_MUX_SEL",
				  "GPIO_CPSW1_RST", "GPIO_RGMII1_RST",
				  "GPIO_RGMII2_RST", "GPIO_PCIe_RST_OUT",
				  "MMC1_SD_EN", "FSI_FET_SEL",
				  "MCAN0_STB_3V3", "MCAN1_STB_3V3",
				  "CPSW_FET_SEL", "CPSW_FET2_SEL",
				  "PRG1_RGMII2_FET_SEL", "TEST_GPIO2",
				  "GPIO_OLED_RESETn", "VPP_LDO_EN",
				  "TEST_LED1", "TP92", "TP90", "TP88",
				  "TP87", "TP86", "TP89", "TP91";
	};
};

&main_i2c2 {
	status = "disabled";
};


&main_i2c3 {
	status = "disabled";
};



/* mcu_gpio0 is reserved for mcu firmware usage */
&mcu_gpio0 {
	status = "reserved";
};

&mcu_i2c0 {
	status = "disabled";
};

&mcu_i2c1 {
	status = "disabled";
};

&mcu_spi0 {
	status = "disabled";
};

&mcu_spi1 {
	status = "disabled";
};

&main_spi0 {
	pinctrl-names = "default";
	pinctrl-0 = <&main_spi0_pins_default>;
	ti,pindir-d0-out-d1-in = <1>;
	eeprom@0 {
		compatible = "microchip,93lc46b";
		reg = <0>;
		spi-max-frequency = <1000000>;
		spi-cs-high;
		data-size = <16>;
	};
};

&sdhci0 {
	/* emmc */
	bus-width = <8>;
	non-removable;
	ti,driver-strength-ohm = <50>;
	disable-wp;
	no-1-8-v;
};

&sdhci1 {
	/* SD/MMC */
	pinctrl-names = "default";
	bus-width = <4>;
	pinctrl-0 = <&main_mmc1_pins_default>;
	cd-gpios = <&main_gpio1 77 1>;
	ti,driver-strength-ohm = <50>;
	disable-wp;
};

&usbss0 {
	ti,vbus-divider;
	ti,usb2-only;
};

&usb0 {
	dr_mode = "host";
	maximum-speed = "high-speed";
	pinctrl-names = "default";
	status = "okay";
	pinctrl-0 = <&main_usb0_pins_default>;
};

&cpsw3g {
	pinctrl-names = "default";
	pinctrl-0 = <&mdio1_pins_default
		     &rgmii1_pins_default >;

	cpts@3d000 {
		ti,pps = <7 1>;
	};
};

&cpsw_port1 {
	phy-mode = "rgmii-rxid";
	phy-handle = <&cpsw3g_phy0>;
	

	/*
	Parameter is defined in DTSI.
	Overwrite it with an empty entry, The MAC address is read from efuse during U-boot
	No need to do it again in kernel
	*/

	ti,syscon-efuse = <>;
};

&cpsw_port2 {
	status = "disabled";
};

&cpsw3g_mdio {
	cpsw3g_phy0: ethernet-phy@0 {
		reg = <0>;
		ti,op-mode = <DP83869_RGMII_COPPER_ETHERNET>;
	};
};



&icssg1_mdio {
    status = "okay";
	pinctrl-names = "default";
	pinctrl-0 = <&icssg1_mdio1_pins_default>;
    #address-cells = <1>;
    #size-cells = <0>;

	icssg1_phy1: ethernet-phy@f {
        reg = <0xf>;
        tx-fifo-depth = <DP83869_PHYCR_FIFO_DEPTH_4_B_NIB>;
        rx-fifo-depth = <DP83869_PHYCR_FIFO_DEPTH_4_B_NIB>;
		ti,op-mode = <DP83869_RGMII_COPPER_ETHERNET>;
        ti,max-output-impedance = "true";
        ti,clk-output-sel = <DP83869_CLK_O_SEL_CHN_A_RCLK>;
        rx-internal-delay-ps = <2000>;
        tx-internal-delay-ps = <2000>;		
	};
	
	icssg1_phy2: ethernet-phy@3 {
        reg = <3>;
        tx-fifo-depth = <DP83869_PHYCR_FIFO_DEPTH_4_B_NIB>;
        rx-fifo-depth = <DP83869_PHYCR_FIFO_DEPTH_4_B_NIB>;
		ti,op-mode = <DP83869_RGMII_COPPER_ETHERNET>;
        ti,max-output-impedance = "true";
        ti,clk-output-sel = <DP83869_CLK_O_SEL_CHN_A_RCLK>;
        rx-internal-delay-ps = <2000>;
        tx-internal-delay-ps = <2000>;	
	};
};

#define TS_OFFSET(pa, val)     (0x4+(pa)*4) (0x10000 | val)

&timesync_router {
	pinctrl-names = "default";
	pinctrl-0 = <&mcu_cpts_pps>;

	/* Example of the timesync routing */
	mcu_cpts_pps: mcu-cpts-pps {
		pinctrl-single,pins = <
				/* pps [cpts genf1] in22 -> out37 [cpts hw8_push] */
				TS_OFFSET(37, 22)
				/* pps [cpts genf1] in22 -> out25 [SYNC1_OUT pin] */
				TS_OFFSET(25, 22)
				>;
	};
};

&mailbox0_cluster2 {
	mbox_main_r5fss0_core0: mbox-main-r5fss0-core0 {
		ti,mbox-rx = <0 0 2>;
		ti,mbox-tx = <1 0 2>;
	};

	mbox_main_r5fss0_core1: mbox-main-r5fss0-core1 {
		ti,mbox-rx = <2 0 2>;
		ti,mbox-tx = <3 0 2>;
	};
};

&mailbox0_cluster3 {
	status = "disabled";
};

&mailbox0_cluster4 {
	mbox_main_r5fss1_core0: mbox-main-r5fss1-core0 {
		ti,mbox-rx = <0 0 2>;
		ti,mbox-tx = <1 0 2>;
	};

	mbox_main_r5fss1_core1: mbox-main-r5fss1-core1 {
		ti,mbox-rx = <2 0 2>;
		ti,mbox-tx = <3 0 2>;
	};
};

&mailbox0_cluster5 {
	status = "disabled";
};

&mailbox0_cluster6 {
	mbox_m4_0: mbox-m4-0 {
		ti,mbox-rx = <0 0 2>;
		ti,mbox-tx = <1 0 2>;
	};
};

&mailbox0_cluster7 {
	status = "disabled";
};

&serdes_ln_ctrl {
	idle-states = <AM64_SERDES0_LANE0_PCIE0>;
};

&serdes0 {
	serdes0_pcie_link: phy@0 {
		reg = <0>;
		cdns,num-lanes = <1>;
		#phy-cells = <0>;
		cdns,phy-type = <PHY_TYPE_PCIE>;
		resets = <&serdes_wiz0 1>;
	};
};

&pcie0_rc {
	reset-gpios = <&exp1 5 GPIO_ACTIVE_HIGH>;
	phys = <&serdes0_pcie_link>;
	phy-names = "pcie-phy";
	num-lanes = <1>;
};

&pcie0_ep {
	phys = <&serdes0_pcie_link>;
	phy-names = "pcie-phy";
	num-lanes = <1>;
	status = "disabled";
};

&tscadc0 {
	/* ADC is reserved for R5 usage */
	status = "reserved";
};

&ospi0 {
	pinctrl-names = "default";
	pinctrl-0 = <&ospi0_pins_default>;

	flash@0{
		compatible = "jedec,spi-nor";
		reg = <0x0>;
		spi-tx-bus-width = <8>;
		spi-rx-bus-width = <8>;
		spi-max-frequency = <25000000>;
		cdns,tshsl-ns = <60>;
		cdns,tsd2d-ns = <60>;
		cdns,tchsh-ns = <60>;
		cdns,tslch-ns = <60>;
		cdns,read-delay = <4>;
		cdns,phy-mode;
		#address-cells = <1>;
		#size-cells = <1>;
	};
};

&main_mcan0 {
	pinctrl-names = "default";
	pinctrl-0 = <&main_mcan0_pins_default>;
	phys = <&transceiver1>;
};

&main_mcan1 {
	pinctrl-names = "default";
	pinctrl-0 = <&main_mcan1_pins_default>;
	phys = <&transceiver2>;
};

&icssg0_mdio {
	status = "disabled";
};

&ecap0 {
	/* PWM is available on Pin 1 of header J12 */
	pinctrl-names = "default";
	pinctrl-0 = <&main_ecap0_pins_default>;
};

相关引导日志部件:

# ifconfig eth1 up
[   79.841549] remoteproc remoteproc10: powering up 300b4000.pru
[   79.851856] remoteproc remoteproc10: Booting fw image ti-pruss/am65x-sr2-pru0-prueth-fw.elf, size 37644
[   79.861316] remoteproc remoteproc10: unsupported resource 5
[   79.866920] remoteproc remoteproc10: remote processor 300b4000.pru is now up
[   79.874001] remoteproc remoteproc11: powering up 30084000.rtu
[   79.883143] remoteproc remoteproc11: Booting fw image ti-pruss/am65x-sr2-rtu0-prueth-fw.elf, size 30860
[   79.892609] remoteproc remoteproc11: remote processor 30084000.rtu is now up
[   79.899693] remoteproc remoteproc12: powering up 3008a000.txpru
[   79.908897] remoteproc remoteproc12: Booting fw image ti-pruss/am65x-sr2-txpru0-prueth-fw.elf, size 36948
[   79.918520] remoteproc remoteproc12: remote processor 3008a000.txpru is now up
[   79.927114] pps pps1: new PPS source ptp2
[   79.932895] TI DP83869 300b2400.mdio:0f: attached PHY driver [TI DP83869] (mii_bus:phy_addr=300b2400.mdio:0f, irq=POLL)
[   79.943998] net eth1: started

# dmesg | grep davinci
[    0.182966] davinci_mdio 4a10100000001000.mdio: failed to get device clock
[    0.182994] davinci_mdio: probe of 4a10100000001000.mdio failed with error -2
[    0.391513] davinci_mdio 300b2400.mdio: davinci mdio revision 1.7, bus freq 1000000
[    0.408862] davinci_mdio 300b2400.mdio: phy[3]: device 300b2400.mdio:03, driver TI DP83869
[    0.408886] davinci_mdio 300b2400.mdio: phy[15]: device 300b2400.mdio:0f, driver TI DP83869
[    2.339512] davinci_mdio 8000f00.mdio: davinci mdio revision 9.7, bus freq 1000000
[    2.356371] davinci_mdio 8000f00.mdio: phy[0]: device 8000f00.mdio:00, driver TI DP83869

# ethtool eth1
Settings for eth1:
        Supported ports: [ TP MII ]
        Supported link modes:   10baseT/Full
                                100baseT/Full
                                1000baseT/Full
                                1000baseX/Full
        Supported pause frame use: No
        Supports auto-negotiation: Yes
        Supported FEC modes: Not reported
        Advertised link modes:  10baseT/Full
                                100baseT/Full
                                1000baseT/Full
                                1000baseX/Full
        Advertised pause frame use: No
        Advertised auto-negotiation: Yes
        Advertised FEC modes: Not reported
        Link partner advertised link modes:  10baseT/Half 10baseT/Full
                                             100baseT/Half 100baseT/Full
                                             1000baseT/Full
        Link partner advertised pause frame use: No
        Link partner advertised auto-negotiation: Yes
        Link partner advertised FEC modes: Not reported
        Speed: 1000Mb/s
        Duplex: Full
        Port: Twisted Pair
        PHYAD: 15
        Transceiver: internal
        Auto-negotiation: on
        MDI-X: Unknown
        Current message level: 0x00007fff (32767)
                               drv probe link timer ifdown ifup rx_err tx_err tx_queued intr tx_done rx_status pktdata hw wol
        Link detected: yes

#  ethtool -S eth1
NIC statistics:
     rx_good_frames: 0
     rx_broadcast_frames: 0
     rx_multicast_frames: 0
     rx_crc_error_frames: 0
     rx_mii_error_frames: 0
     rx_odd_nibble_frames: 0
     rx_frame_max_size: 2000
     rx_max_size_error_frames: 0
     rx_frame_min_size: 64
     rx_min_size_error_frames: 16
     rx_overrun_frames: 0
     rx_class0_hits: 16
     rx_class1_hits: 0
     rx_class2_hits: 0
     rx_class3_hits: 0
     rx_class4_hits: 0
     rx_class5_hits: 0
     rx_class6_hits: 0
     rx_class7_hits: 0
     rx_class8_hits: 16
     rx_class9_hits: 16
     rx_class10_hits: 0
     rx_class11_hits: 0
     rx_class12_hits: 0
     rx_class13_hits: 0
     rx_class14_hits: 0
     rx_class15_hits: 0
     rx_smd_frags: 0
     rx_bucket1_size: 64
     rx_bucket2_size: 128
     rx_bucket3_size: 256
     rx_bucket4_size: 512
     rx_64B_frames: 0
     rx_bucket1_frames: 16
     rx_bucket2_frames: 0
     rx_bucket3_frames: 0
     rx_bucket4_frames: 0
     rx_bucket5_frames: 0
     rx_total_bytes: 0
     rx_tx_total_bytes: 0
     tx_good_frames: 0
     tx_broadcast_frames: 0
     tx_multicast_frames: 0
     tx_odd_nibble_frames: 0
     tx_underflow_errors: 0
     tx_frame_max_size: 2000
     tx_max_size_error_frames: 0
     tx_frame_min_size: 64
     tx_min_size_error_frames: 0
     tx_bucket1_size: 64
     tx_bucket2_size: 128
     tx_bucket3_size: 256
     tx_bucket4_size: 512
     tx_64B_frames: 0
     tx_bucket1_frames: 0
     tx_bucket2_frames: 0
     tx_bucket3_frames: 0
     tx_bucket4_frames: 0
     tx_bucket5_frames: 0
     tx_total_bytes: 0

完整引导日志  

U-Boot 2021.01-00014-gf70147e0-dirty (Jul 10 2022 - 18:31:56 +0000)

SoC:   AM64X SR1.0
Model: Texas Instruments AM642 SolidRun Board
DRAM:  1 GiB
MMC:   mmc@fa10000: 0, mmc@fa00000: 1
In:    serial@2800000
Out:   serial@2800000
Err:   serial@2800000
No MAC address 1 in EEPROM, using random MAC address.
No MAC address 2 in EEPROM, using random MAC address.
No MAC address 3 in EEPROM, using random MAC address.
Net:   eth0: ethernet@8000000
Hit any key to stop autoboot:  0
19950080 bytes read in 858 ms (22.2 MiB/s)
53852 bytes read in 5 ms (10.3 MiB/s)
## Flattened Device Tree blob at 88000000
   Booting using the fdt blob at 0x88000000
   Loading Device Tree to 000000008ffef000, end 000000008ffff25b ... OK

Starting kernel ...

[    0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
[    0.000000] Linux version 5.10.41-00013-gdc5f5efbc5e1-dirty (moaath@7beb34a846cf) (aarch64-none-linux-gnu-gcc (GNU Toolchain for the A-profile Architecture 9.2-2019.12 (arm-9.10)) 9.2.1 20191025, GNU ld (GNU Toolchain for the A-profile Architecture 9.2-2019.12 (arm-9.10)) 2.33.1.20191209) #95 SMP PREEMPT Sun Jul 10 18:32:12 UTC 2022
[    0.000000] Machine model: Texas Instruments AM642 SolidRun Board
[    0.000000] efi: UEFI not found.
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a0000000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node r5f-dma-memory@a0000000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a0100000, size 15 MiB
[    0.000000] OF: reserved mem: initialized node r5f-memory@a0100000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a1000000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node r5f-dma-memory@a1000000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a1100000, size 15 MiB
[    0.000000] OF: reserved mem: initialized node r5f-memory@a1100000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a2000000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node r5f-dma-memory@a2000000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a2100000, size 15 MiB
[    0.000000] OF: reserved mem: initialized node r5f-memory@a2100000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a3000000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node r5f-dma-memory@a3000000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a3100000, size 15 MiB
[    0.000000] OF: reserved mem: initialized node r5f-memory@a3100000, compatible id shared-dma-pool
[    0.000000] Zone ranges:
[    0.000000]   DMA      [mem 0x0000000080000000-0x00000000bfffffff]
[    0.000000]   DMA32    empty
[    0.000000]   Normal   empty
[    0.000000] Movable zone start for each node
[    0.000000] Early memory node ranges
[    0.000000]   node   0: [mem 0x0000000080000000-0x000000009e7fffff]
[    0.000000]   node   0: [mem 0x000000009e800000-0x00000000a3ffffff]
[    0.000000]   node   0: [mem 0x00000000a4000000-0x00000000a4ffffff]
[    0.000000]   node   0: [mem 0x00000000a5000000-0x00000000a57fffff]
[    0.000000]   node   0: [mem 0x00000000a5800000-0x00000000bfffffff]
[    0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000000bfffffff]
[    0.000000] cma: Reserved 24 MiB at 0x00000000bc800000
[    0.000000] psci: probing for conduit method from DT.
[    0.000000] psci: PSCIv1.1 detected in firmware.
[    0.000000] psci: Using standard PSCI v0.2 function IDs
[    0.000000] psci: Trusted OS migration not required
[    0.000000] psci: SMC Calling Convention v1.2
[    0.000000] percpu: Embedded 22 pages/cpu s49880 r8192 d32040 u90112
[    0.000000] Detected VIPT I-cache on CPU0
[    0.000000] CPU features: detected: ARM erratum 845719
[    0.000000] CPU features: detected: GIC system register CPU interface
[    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 258048
[    0.000000] Kernel command line: console=ttyS2,115200n8 root=/dev/mmcblk1p2 rw rootwait
[    0.000000] Dentry cache hash table entries: 131072 (order: 8, 1048576 bytes, linear)
[    0.000000] Inode-cache hash table entries: 65536 (order: 7, 524288 bytes, linear)
[    0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
[    0.000000] Memory: 885492K/1048576K available (11648K kernel code, 1178K rwdata, 4568K rodata, 1984K init, 436K bss, 138508K reserved, 24576K cma-reserved)
[    0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
[    0.000000] rcu: Preemptible hierarchical RCU implementation.
[    0.000000] rcu:     RCU event tracing is enabled.
[    0.000000] rcu:     RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=2.
[    0.000000]  Trampoline variant of Tasks RCU enabled.
[    0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[    0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2
[    0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[    0.000000] GICv3: GIC: Using split EOI/Deactivate mode
[    0.000000] GICv3: 256 SPIs implemented
[    0.000000] GICv3: 0 Extended SPIs implemented
[    0.000000] GICv3: Distributor has no Range Selector support
[    0.000000] GICv3: 16 PPIs implemented
[    0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000001840000
[    0.000000] ITS [mem 0x01820000-0x0182ffff]
[    0.000000] GIC: enabling workaround for ITS: Socionext Synquacer pre-ITS
[    0.000000] ITS@0x0000000001820000: Devices Table too large, reduce ids 20->19
[    0.000000] ITS@0x0000000001820000: allocated 524288 Devices @80800000 (flat, esz 8, psz 64K, shr 0)
[    0.000000] ITS: using cache flushing for cmd queue
[    0.000000] GICv3: using LPI property table @0x0000000080030000
[    0.000000] GIC: using cache flushing for LPI property table
[    0.000000] GICv3: CPU0: using allocated LPI pending table @0x0000000080040000
[    0.000000] random: get_random_bytes called from start_kernel+0x32c/0x4d4 with crng_init=0
[    0.000000] arch_timer: cp15 timer(s) running at 200.00MHz (phys).
[    0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x2e2049d3e8, max_idle_ns: 440795210634 ns
[    0.000005] sched_clock: 56 bits at 200MHz, resolution 5ns, wraps every 4398046511102ns
[    0.000323] Console: colour dummy device 80x25
[    0.000383] Calibrating delay loop (skipped), value calculated using timer frequency.. 400.00 BogoMIPS (lpj=800000)
[    0.000400] pid_max: default: 32768 minimum: 301
[    0.000510] LSM: Security Framework initializing
[    0.000579] Mount-cache hash table entries: 2048 (order: 2, 16384 bytes, linear)
[    0.000596] Mountpoint-cache hash table entries: 2048 (order: 2, 16384 bytes, linear)
[    0.002430] rcu: Hierarchical SRCU implementation.
[    0.002686] Platform MSI: msi-controller@1820000 domain created
[    0.002963] PCI/MSI: /bus@f4000/interrupt-controller@1800000/msi-controller@1820000 domain created
[    0.003077] EFI services will not be available.
[    0.003342] smp: Bringing up secondary CPUs ...
[    0.004012] Detected VIPT I-cache on CPU1
[    0.004056] GICv3: CPU1: found redistributor 1 region 0:0x0000000001860000
[    0.004071] GICv3: CPU1: using allocated LPI pending table @0x0000000080050000
[    0.004142] CPU1: Booted secondary processor 0x0000000001 [0x410fd034]
[    0.004275] smp: Brought up 1 node, 2 CPUs
[    0.004296] SMP: Total of 2 processors activated.
[    0.004306] CPU features: detected: 32-bit EL0 Support
[    0.004314] CPU features: detected: CRC32 instructions
[    0.012845] CPU: All CPU(s) started at EL2
[    0.012874] alternatives: patching kernel code
[    0.014138] devtmpfs: initialized
[    0.022276] KASLR disabled due to lack of seed
[    0.022518] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[    0.022539] futex hash table entries: 512 (order: 3, 32768 bytes, linear)
[    0.023659] pinctrl core: initialized pinctrl subsystem
[    0.024441] DMI not present or invalid.
[    0.025034] NET: Registered protocol family 16
[    0.026865] DMA: preallocated 128 KiB GFP_KERNEL pool for atomic allocations
[    0.027014] DMA: preallocated 128 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
[    0.027155] DMA: preallocated 128 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
[    0.027833] thermal_sys: Registered thermal governor 'step_wise'
[    0.027840] thermal_sys: Registered thermal governor 'power_allocator'
[    0.028346] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[    0.028453] ASID allocator initialised with 65536 entries
[    0.059208] HugeTLB registered 1.00 GiB page size, pre-allocated 0 pages
[    0.059232] HugeTLB registered 32.0 MiB page size, pre-allocated 0 pages
[    0.059240] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages
[    0.059248] HugeTLB registered 64.0 KiB page size, pre-allocated 0 pages
[    0.060509] cryptd: max_cpu_qlen set to 1000
[    0.063839] k3-chipinfo 43000014.chipid: Family:AM64X rev:SR1.0 JTAGID[0x0bb3802f] Detected
[    0.064631] vsys_5v0: supplied by evm_12v0
[    0.064986] vsys_3v3: supplied by evm_12v0
[    0.065378] vddb_3v3_display: supplied by vsys_3v3
[    0.066429] iommu: Default domain type: Translated
[    0.066852] SCSI subsystem initialized
[    0.067087] usbcore: registered new interface driver usbfs
[    0.067133] usbcore: registered new interface driver hub
[    0.067169] usbcore: registered new device driver usb
[    0.067772] mc: Linux media interface: v0.10
[    0.067814] videodev: Linux video capture interface: v2.00
[    0.067901] pps_core: LinuxPPS API ver. 1 registered
[    0.067908] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[    0.067926] PTP clock support registered
[    0.067965] EDAC MC: Ver: 3.0.0
[    0.068901] omap-mailbox 29020000.mailbox: omap mailbox rev 0x66fc9100
[    0.069131] omap-mailbox 29040000.mailbox: omap mailbox rev 0x66fc9100
[    0.069277] omap-mailbox 29060000.mailbox: omap mailbox rev 0x66fc9100
[    0.070117] FPGA manager framework
[    0.070235] Advanced Linux Sound Architecture Driver Initialized.
[    0.071385] clocksource: Switched to clocksource arch_sys_counter
[    0.071627] VFS: Disk quotas dquot_6.6.0
[    0.071686] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[    0.078124] NET: Registered protocol family 2
[    0.078325] IP idents hash table entries: 16384 (order: 5, 131072 bytes, linear)
[    0.079682] tcp_listen_portaddr_hash hash table entries: 512 (order: 1, 8192 bytes, linear)
[    0.079723] TCP established hash table entries: 8192 (order: 4, 65536 bytes, linear)
[    0.079795] TCP bind hash table entries: 8192 (order: 5, 131072 bytes, linear)
[    0.079923] TCP: Hash tables configured (established 8192 bind 8192)
[    0.080106] UDP hash table entries: 512 (order: 2, 16384 bytes, linear)
[    0.080140] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes, linear)
[    0.080309] NET: Registered protocol family 1
[    0.080972] RPC: Registered named UNIX socket transport module.
[    0.080989] RPC: Registered udp transport module.
[    0.080995] RPC: Registered tcp transport module.
[    0.081001] RPC: Registered tcp NFSv4.1 backchannel transport module.
[    0.081019] PCI: CLS 0 bytes, default 64
[    0.081866] hw perfevents: enabled with armv8_cortex_a53 PMU driver, 7 counters available
[    0.086117] Initialise system trusted keyrings
[    0.086378] workingset: timestamp_bits=46 max_order=18 bucket_order=0
[    0.091032] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[    0.091840] NFS: Registering the id_resolver key type
[    0.091885] Key type id_resolver registered
[    0.091893] Key type id_legacy registered
[    0.091970] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[    0.091978] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...
[    0.092221] 9p: Installing v9fs 9p2000 file system support
[    0.136038] Key type asymmetric registered
[    0.136066] Asymmetric key parser 'x509' registered
[    0.136153] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 243)
[    0.136163] io scheduler mq-deadline registered
[    0.136171] io scheduler kyber registered
[    0.138820] pinctrl-single 4084000.pinctrl: 32 pins, size 128
[    0.139323] pinctrl-single f4000.pinctrl: 180 pins, size 720
[    0.140581] pinctrl-single a40000.timesync-router: 512 pins, size 2048
[    0.150795] Serial: 8250/16550 driver, 10 ports, IRQ sharing enabled
[    0.167963] brd: module loaded
[    0.176295] loop: module loaded
[    0.177247] megasas: 07.714.04.00-rc1
[    0.180301] libphy: Fixed MDIO Bus: probed
[    0.182180] tun: Universal TUN/TAP device driver, 1.6
[    0.182971] igbvf: Intel(R) Gigabit Virtual Function Network Driver
[    0.182983] igbvf: Copyright (c) 2009 - 2012 Intel Corporation.
[    0.183061] sky2: driver version 1.30
[    0.183630] davinci_mdio 4a10100000001000.mdio: failed to get device clock
[    0.183658] davinci_mdio: probe of 4a10100000001000.mdio failed with error -2
[    0.185262] usbcore: registered new interface driver cdc_ether
[    0.185321] usbcore: registered new interface driver cdc_ncm
[    0.185355] usbcore: registered new interface driver cdc_mbim
[    0.185650] VFIO - User Level meta-driver version: 0.3
[    0.187622] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[    0.187643] ehci-pci: EHCI PCI platform driver
[    0.187707] ehci-platform: EHCI generic platform driver
[    0.187921] ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver
[    0.187969] ohci-pci: OHCI PCI platform driver
[    0.188015] ohci-platform: OHCI generic platform driver
[    0.188645] usbcore: registered new interface driver cdc_wdm
[    0.188977] usbcore: registered new interface driver uas
[    0.189035] usbcore: registered new interface driver usb-storage
[    0.189138] usbcore: registered new interface driver usbserial_generic
[    0.189166] usbserial: USB Serial support registered for generic
[    0.189196] usbcore: registered new interface driver ftdi_sio
[    0.189216] usbserial: USB Serial support registered for FTDI USB Serial Device
[    0.189247] usbcore: registered new interface driver option
[    0.189268] usbserial: USB Serial support registered for GSM modem (1-port)
[    0.189297] usbcore: registered new interface driver sierra
[    0.189318] usbserial: USB Serial support registered for Sierra USB modem
[    0.189353] usbcore: registered new interface driver usb_serial_simple
[    0.189377] usbserial: USB Serial support registered for carelink
[    0.189398] usbserial: USB Serial support registered for zio
[    0.189418] usbserial: USB Serial support registered for funsoft
[    0.189440] usbserial: USB Serial support registered for flashloader
[    0.189461] usbserial: USB Serial support registered for google
[    0.189482] usbserial: USB Serial support registered for libtransistor
[    0.189503] usbserial: USB Serial support registered for vivopay
[    0.189525] usbserial: USB Serial support registered for moto_modem
[    0.189546] usbserial: USB Serial support registered for motorola_tetra
[    0.189567] usbserial: USB Serial support registered for novatel_gps
[    0.189588] usbserial: USB Serial support registered for hp4x
[    0.189612] usbserial: USB Serial support registered for suunto
[    0.189634] usbserial: USB Serial support registered for siemens_mpi
[    0.189665] usbcore: registered new interface driver usb_ehset_test
[    0.190148] udc-core: couldn't find an available UDC - added [zero] to list of pending drivers
[    0.190157] udc-core: couldn't find an available UDC - added [g_audio] to list of pending drivers
[    0.190164] udc-core: couldn't find an available UDC - added [g_ether] to list of pending drivers
[    0.190859] i2c /dev entries driver
[    0.192229] sdhci: Secure Digital Host Controller Interface driver
[    0.192241] sdhci: Copyright(c) Pierre Ossman
[    0.192620] sdhci-pltfm: SDHCI platform and OF driver helper
[    0.193936] ledtrig-cpu: registered to indicate activity on CPUs
[    0.194423] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping ....
[    0.194594] usbcore: registered new interface driver usbhid
[    0.194601] usbhid: USB HID core driver
[    0.196936] optee: probing for conduit method.
[    0.196979] optee: revision 3.14 (e4ca953c)
[    0.197581] optee: initialized driver
[    0.200449] NET: Registered protocol family 17
[    0.200631] 9pnet: Installing 9P2000 support
[    0.200706] Key type dns_resolver registered
[    0.201017] Loading compiled-in X.509 certificates
[    0.220523] ti-sci 44043000.dmsc: ABI: 3.1 (firmware rev 0x0015 '21.5.0--v2021.05 (Terrific Llam')
[    0.255511] random: fast init done
[    0.260469] platform 78000000.r5f: configured R5F for remoteproc mode
[    0.260692] platform 78000000.r5f: assigned reserved memory node r5f-dma-memory@a0000000
[    0.261059] remoteproc remoteproc0: 78000000.r5f is available
[    0.261307] remoteproc remoteproc0: Direct firmware load for am64-main-r5f0_0-fw failed with error -2
[    0.261327] remoteproc remoteproc0: powering up 78000000.r5f
[    0.261369] remoteproc remoteproc0: Direct firmware load for am64-main-r5f0_0-fw failed with error -2
[    0.261379] remoteproc remoteproc0: request_firmware failed: -2
[    0.261494] platform 78200000.r5f: configured R5F for remoteproc mode
[    0.261681] platform 78200000.r5f: assigned reserved memory node r5f-dma-memory@a1000000
[    0.262016] remoteproc remoteproc1: 78200000.r5f is available
[    0.263144] remoteproc remoteproc1: Direct firmware load for am64-main-r5f0_1-fw failed with error -2
[    0.263169] remoteproc remoteproc1: powering up 78200000.r5f
[    0.263211] remoteproc remoteproc1: Direct firmware load for am64-main-r5f0_1-fw failed with error -2
[    0.263221] remoteproc remoteproc1: request_firmware failed: -2
[    0.266413] platform 78400000.r5f: configured R5F for remoteproc mode
[    0.266636] platform 78400000.r5f: assigned reserved memory node r5f-dma-memory@a2000000
[    0.267032] remoteproc remoteproc2: 78400000.r5f is available
[    0.267267] remoteproc remoteproc2: Direct firmware load for am64-main-r5f1_0-fw failed with error -2
[    0.267281] remoteproc remoteproc2: powering up 78400000.r5f
[    0.267323] remoteproc remoteproc2: Direct firmware load for am64-main-r5f1_0-fw failed with error -2
[    0.267334] remoteproc remoteproc2: request_firmware failed: -2
[    0.267514] platform 78600000.r5f: configured R5F for remoteproc mode
[    0.267716] platform 78600000.r5f: assigned reserved memory node r5f-dma-memory@a3000000
[    0.268072] remoteproc remoteproc3: 78600000.r5f is available
[    0.269324] remoteproc remoteproc3: Direct firmware load for am64-main-r5f1_1-fw failed with error -2
[    0.269350] remoteproc remoteproc3: powering up 78600000.r5f
[    0.269394] remoteproc remoteproc3: Direct firmware load for am64-main-r5f1_1-fw failed with error -2
[    0.269404] remoteproc remoteproc3: request_firmware failed: -2
[    0.272578] omap_i2c 20000000.i2c: bus 0 rev0.12 at 400 kHz
[    0.274759] pca953x 1-0022: supply vcc not found, using dummy regulator
[    0.274915] pca953x 1-0022: using AI
[    0.295436] pca953x 1-0022: failed writing register
[    0.295626] pca953x: probe of 1-0022 failed with error -121
[    0.295814] omap_i2c 20010000.i2c: bus 1 rev0.12 at 400 kHz
[    0.296298] ti-sci-intr bus@f4000:bus@4000000:interrupt-controller1: Interrupt Router 5 domain created
[    0.296468] ti-sci-intr bus@f4000:interrupt-controller0: Interrupt Router 3 domain created
[    0.296759] ti-sci-inta 48000000.interrupt-controller: Interrupt Aggregator domain 28 created
[    0.307810] j721e-pcie f102000.pcie: host bridge /bus@f4000/pcie@f102000 ranges:
[    0.307865] j721e-pcie f102000.pcie:       IO 0x0068001000..0x0068010fff -> 0x0068001000
[    0.307889] j721e-pcie f102000.pcie:      MEM 0x0068011000..0x006fffffff -> 0x0068011000
[    0.307912] j721e-pcie f102000.pcie:   IB MEM 0x0000000000..0x0fffffffff -> 0x0000000000
[    0.308947] ti-bcdma 485c0100.dma-controller: Number of rings: 68
[    0.310280] ti-bcdma 485c0100.dma-controller: Channels: 24 (bchan: 12, tchan: 6, rchan: 6)
[    0.312298] ti-pktdma 485c0000.dma-controller: Number of rings: 288
[    0.320052] ti-pktdma 485c0000.dma-controller: Channels: 44 (tchan: 29, rchan: 15)
[    0.330675] remoteproc remoteproc4: 30034000.pru is available
[    0.332017] remoteproc remoteproc5: 30004000.rtu is available
[    0.333205] remoteproc remoteproc6: 3000a000.txpru is available
[    0.334399] remoteproc remoteproc7: 30038000.pru is available
[    0.335672] remoteproc remoteproc8: 30006000.rtu is available
[    0.336867] remoteproc remoteproc9: 3000c000.txpru is available
[    0.345194] remoteproc remoteproc10: 300b4000.pru is available
[    0.346218] remoteproc remoteproc11: 30084000.rtu is available
[    0.347210] remoteproc remoteproc12: 3008a000.txpru is available
[    0.348331] remoteproc remoteproc13: 300b8000.pru is available
[    0.349298] remoteproc remoteproc14: 30086000.rtu is available
[    0.350274] remoteproc remoteproc15: 3008c000.txpru is available
[    0.391395] davinci_mdio 300b2400.mdio: davinci mdio revision 1.7, bus freq 1000000
[    0.391419] libphy: 300b2400.mdio: probed
[    0.408741] davinci_mdio 300b2400.mdio: phy[3]: device 300b2400.mdio:03, driver TI DP83869
[    0.408765] davinci_mdio 300b2400.mdio: phy[15]: device 300b2400.mdio:0f, driver TI DP83869
[    0.410296] 4a10000.serial: ttyS1 at MMIO 0x4a10000 (irq = 15, base_baud = 6000000) is a 8250
[    0.411974] 2800000.serial: ttyS2 at MMIO 0x2800000 (irq = 17, base_baud = 3000000) is a 8250
[    2.273656] printk: console [ttyS2] enabled
[    2.280751] spi-nor spi0.0: unrecognized JEDEC id bytes: ff ff ff ff ff ff
[    2.287702] spi-nor: probe of spi0.0 failed with error -2
[    2.339393] davinci_mdio 8000f00.mdio: davinci mdio revision 9.7, bus freq 1000000
[    2.346991] libphy: 8000f00.mdio: probed
[    2.356256] davinci_mdio 8000f00.mdio: phy[0]: device 8000f00.mdio:00, driver TI DP83869
[    2.364501] am65-cpsw-nuss 8000000.ethernet: initializing am65 cpsw nuss version 0x6BA00903, cpsw version 0x6BA80903 Ports: 3 quirks:00000002
[    2.378172] am65-cpsw-nuss 8000000.ethernet: set new flow-id-base 16
[    2.384883] am65-cpsw-nuss 8000000.ethernet: initialized cpsw ale version 1.4
[    2.392031] am65-cpsw-nuss 8000000.ethernet: ALE Table size 512
[    2.398628] pps pps0: new PPS source ptp0
[    2.403059] am65-cpsw-nuss 8000000.ethernet: CPTS ver 0x4e8a010c, freq:500000000, add_val:1 pps:1
[    2.413296] am65-cpsw-nuss 8000000.ethernet: devlink port type for port 2 set to Ethernet without a software interface reference, device type not supported by the kernel?
[    2.430597] am65-cpts 39000000.cpts: CPTS ver 0x4e8a010c, freq:500000000, add_val:1 pps:0
[    2.476842] icssg-prueth icssg1-eth: TI PRU ethernet driver initialized: dual EMAC mode
[    2.487972] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
[    2.493532] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 1
[    2.501533] xhci-hcd xhci-hcd.0.auto: hcc params 0x200073c9 hci version 0x100 quirks 0x0000002000010010
[    2.510975] xhci-hcd xhci-hcd.0.auto: irq 344, io mem 0x0f410000
[    2.518045] hub 1-0:1.0: USB hub found
[    2.521846] hub 1-0:1.0: 1 port detected
[    2.526092] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
[    2.531594] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 2
[    2.539266] xhci-hcd xhci-hcd.0.auto: Host supports USB 3.0 SuperSpeed
[    2.545873] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM.
[    2.554601] hub 2-0:1.0: USB hub found
[    2.558391] hub 2-0:1.0: 1 port detected
[    2.565814] sdhci-am654 fa00000.mmc: parsing dt failed (-517)
[    2.571783] mmc0: CQHCI version 5.10
[    2.584201] j721e-pcie f102000.pcie: host bridge /bus@f4000/pcie@f102000 ranges:
[    2.591705] j721e-pcie f102000.pcie:       IO 0x0068001000..0x0068010fff -> 0x0068001000
[    2.599827] j721e-pcie f102000.pcie:      MEM 0x0068011000..0x006fffffff -> 0x0068011000
[    2.607926] j721e-pcie f102000.pcie:   IB MEM 0x0000000000..0x0fffffffff -> 0x0000000000
[    2.618978] sdhci-am654 fa00000.mmc: Got CD GPIO
[    2.623927] j721e-pcie f102000.pcie: host bridge /bus@f4000/pcie@f102000 ranges:
[    2.623935] mmc1: CQHCI version 5.10
[    2.627458] mmc0: SDHCI controller on fa10000.mmc [fa10000.mmc] using ADMA 64-bit
[    2.631409] j721e-pcie f102000.pcie:       IO 0x0068001000..0x0068010fff -> 0x0068001000
[    2.650490] j721e-pcie f102000.pcie:      MEM 0x0068011000..0x006fffffff -> 0x0068011000
[    2.658600] j721e-pcie f102000.pcie:   IB MEM 0x0000000000..0x0fffffffff -> 0x0000000000
[    2.669310] j721e-pcie f102000.pcie: host bridge /bus@f4000/pcie@f102000 ranges:
[    2.672223] mmc1: SDHCI controller on fa00000.mmc [fa00000.mmc] using ADMA 64-bit
[    2.676797] j721e-pcie f102000.pcie:       IO 0x0068001000..0x0068010fff -> 0x0068001000
[    2.692325] j721e-pcie f102000.pcie:      MEM 0x0068011000..0x006fffffff -> 0x0068011000
[    2.700433] j721e-pcie f102000.pcie:   IB MEM 0x0000000000..0x0fffffffff -> 0x0000000000
[    2.711152] j721e-pcie f102000.pcie: host bridge /bus@f4000/pcie@f102000 ranges:
[    2.718608] j721e-pcie f102000.pcie:       IO 0x0068001000..0x0068010fff -> 0x0068001000
[    2.726709] j721e-pcie f102000.pcie:      MEM 0x0068011000..0x006fffffff -> 0x0068011000
[    2.734805] j721e-pcie f102000.pcie:   IB MEM 0x0000000000..0x0fffffffff -> 0x0000000000
[    2.735016] mmc1: new ultra high speed SDR104 SDHC card at address aaaa
[    2.744496] debugfs: Directory 'pd:114' with parent 'pm_genpd' already present!
[    2.750845] mmcblk1: mmc1:aaaa SC16G 14.8 GiB
[    2.761861] mmc0: Command Queue Engine enabled
[    2.766347] mmc0: new high speed MMC card at address 0001
[    2.773780] mmcblk0: mmc0:0001 8GTF4R 7.28 GiB
[    2.778547]  mmcblk1: p1 p2
[    2.782952] mmcblk0boot0: mmc0:0001 8GTF4R partition 1 4.00 MiB
[    2.789182] mmcblk0boot1: mmc0:0001 8GTF4R partition 2 4.00 MiB
[    2.796349] ALSA device list:
[    2.797792] j721e-pcie f102000.pcie: host bridge /bus@f4000/pcie@f102000 ranges:
[    2.799333]   No soundcards found.
[    2.806850] mmcblk0rpmb: mmc0:0001 8GTF4R partition 3 512 KiB, chardev (236:0)
[    2.817542] j721e-pcie f102000.pcie:       IO 0x0068001000..0x0068010fff -> 0x0068001000
[    2.825698] j721e-pcie f102000.pcie:      MEM 0x0068011000..0x006fffffff -> 0x0068011000
[    2.833807] j721e-pcie f102000.pcie:   IB MEM 0x0000000000..0x0fffffffff -> 0x0000000000
[    2.848828] j721e-pcie f102000.pcie: host bridge /bus@f4000/pcie@f102000 ranges:
[    2.856469] j721e-pcie f102000.pcie:       IO 0x0068001000..0x0068010fff -> 0x0068001000
[    2.864716] j721e-pcie f102000.pcie:      MEM 0x0068011000..0x006fffffff -> 0x0068011000
[    2.872911] j721e-pcie f102000.pcie:   IB MEM 0x0000000000..0x0fffffffff -> 0x0000000000
[    2.881094] usb 1-1: new high-speed USB device number 2 using xhci-hcd
[    2.894434] EXT4-fs (mmcblk1p2): mounted filesystem with ordered data mode. Opts: (null)
[    2.902626] VFS: Mounted root (ext4 filesystem) on device 179:2.
[    2.911205] devtmpfs: mounted
[    2.915731] Freeing unused kernel memory: 1984K
[    2.920393] Run /sbin/init as init process
[    3.009962] EXT4-fs (mmcblk1p2): re-mounted. Opts: (null)
[    3.041383] hub 1-1:1.0: USB hub found
[    3.045532] hub 1-1:1.0: 4 ports detected
[    3.054256] j721e-pcie f102000.pcie: host bridge /bus@f4000/pcie@f102000 ranges:
[    3.061875] j721e-pcie f102000.pcie:       IO 0x0068001000..0x0068010fff -> 0x0068001000
[    3.070180] j721e-pcie f102000.pcie:      MEM 0x0068011000..0x006fffffff -> 0x0068011000
[    3.078476] j721e-pcie f102000.pcie:   IB MEM 0x0000000000..0x0fffffffff -> 0x0000000000
Starting syslogd: OK
Starting klogd: OK
Running sysctl: OK
Initializing random number generator: OK
Saving random seed: [    3.246072] random: dd: uninitialized urandom read (512 bytes read)
OK
Starting system message bus: [    3.291728] random: dbus-uuidgen: uninitialized urandom read (12 bytes read)
[    3.298951] random: dbus-uuidgen: uninitialized urandom read (8 bytes read)
done
Starting network: OK

Welcome to Buildroot
buildroot login:

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    抱歉、由于回复延迟、您的问题被分配给了错误的员工。 今天稍后、我将尝试回圈并进行更仔细的研究。 如果您明天尚未收到响应、请对该主题执行 Ping 操作。

    此致、

    Nick

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Nick、

    我还没有收到任何回复。