This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TDA4VM:TDA4VM:分辨率为1080x1920的 DSI 不起作用

Guru**** 2542950 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1112916/tda4vm-tda4vm-dsi-with-1080x1920-resolution-dose-not-work

器件型号:TDA4VM
主题中讨论的其他器件:DRA829

各位专家:

我正在使用 DS90UB941AS 的 DRA829客户电路板、通过1080x1920面板连接到 UB948。

通过跟踪启动指南,我被吸入“DSI_DTYPE 报告错误”。

DSI_DTYPE 返回0x0。

这是 DSI (4通道):SDK 8.01的配置

vision_apps/apps/basic_demos/app_tirtos/common/app_init.c  

vision_apps/utils/dss/src/app_dss_defaults.c  

3.ti/drv/dss/src/drv/dctrl/DSS_dctrlDSI.c  

4、 vision_apps/platform/j721e/rtos/common/app_cfg_mcu2_0.h

undef enable_CSI2TX

#undef enable_dss_eDP

#define ENABLE_DSS_DSI

5. vision_apps/apps/dl_demos/app_tidL/app_common.h

6. vision_apps/apps/dl_demos/app_tidl/main.c

7. DS90UB941AS 配置:

uint8_t Ub941Ub925Config[][4] = {
#if 1
{0x16, 0x01, 0x02, 0x60},//Disable DSI
{0x16, 0x01, 0x08, 0x5},//Reset Reg
#endif
{0x16, 0x06, 0x00, 0x5},

{0x16, 0x1E, 0x01, 0x5},//Select port0
{0x16, 0x4F, 0x8C, 0x5},//DSI Continuous CLK/4 Lanes
{0x16, 0x5B, 0x0B, 0x5},//Dual mode "MUST"

{0x16, 0x03, 0x9A, 0x5},//I2C pass through
{0x2C, 0x1E, 0x30, 0x5},
{0x2C, 0x20, 0x03, 0x5},

0x16, 0x66, 0   , 0x5},
{0x16, 0x67, 0x0 , 0x5},
{0x16, 0x66, 1   , 0x5},
{0x16, 0x67, 0x0 , 0x5},
{0x16, 0x66, 2   , 0x5},
{0x16, 0x67, 0x0 , 0x5},
{0x16, 0x66, 3   , 0x5},
{0x16, 0x67, 0x16, 0x5},
{0x16, 0x66, 4   , 0x5},
{0x16, 0x67, 0xd8, 0x5},
{0x16, 0x66, 5   , 0x5},
{0x16, 0x67, 0x74, 0x5},
{0x16, 0x66, 6   , 0x5},
{0x16, 0x67, 0x7b, 0x5},
{0x16, 0x66, 7   , 0x5},
{0x16, 0x67, 0x38, 0x5},
{0x16, 0x66, 8   , 0x5},
{0x16, 0x67, 0x04, 0x5},
{0x16, 0x66, 9   , 0x5},
{0x16, 0x67, 0x78, 0x5},
{0x16, 0x66, 10  , 0x5},
{0x16, 0x67, 0x20, 0x5},
{0x16, 0x66, 11  , 0x5},
{0x16, 0x67, 0x0a, 0x5},
{0x16, 0x66, 12  , 0x5},
{0x16, 0x67, 0x50, 0x5},
{0x16, 0x66, 13  , 0x5},
{0x16, 0x67, 0x2a, 0x5},
{0x16, 0x66, 14  , 0x5},
{0x16, 0x67, 0x3 , 0x5},
{0x16, 0x66, 15  , 0x5},
{0x16, 0x67, 0x1e, 0x5},
{0x16, 0x66, 16  , 0x5},
{0x16, 0x67, 0xe , 0x5},
{0x16, 0x66, 17  , 0x5},
{0x16, 0x67, 0x21, 0x5},
{0x16, 0x66, 18  , 0x5},
{0x16, 0x67, 0x43, 0x5},
{0x16, 0x66, 19  , 0x5},
{0x16, 0x67, 0x65, 0x5},
{0x16, 0x66, 20  , 0x5},
{0x16, 0x67, 0x87, 0x5},
{0x16, 0x66, 21  , 0x5},
{0x16, 0x67, 0xa9, 0x5},
{0x16, 0x66, 22  , 0x5},
{0x16, 0x67, 0xcb, 0x5},
{0x16, 0x66, 23  , 0x5},
{0x16, 0x67, 0xed, 0x5},
{0x16, 0x66, 24  , 0x5},
{0x16, 0x67, 0xf , 0x5},
{0x16, 0x66, 25  , 0x5},
{0x16, 0x67, 0x0 , 0x5},
{0x16, 0x66, 26  , 0x5},
{0x16, 0x67, 0x04, 0x5},

#if 1
{0x16, 0x01, 0x00, 0x5},
#endif
#if 0
{0x16, 0x65, 0x68, 0x5},
{0x16, 0x64, 0x15, 0xF8},
#endif
};

8.输出:

root@j7-evm:/opt/vision_apps# [MCU2_0]      3.618258 s: CIO: Init ... Done !!!
[MCU2_0]      3.618335 s: ### CPU Frequency = 1000000000 Hz
[MCU2_0]      3.618379 s: APP: Init ... !!!
[MCU2_0]      3.618405 s: SCICLIENT: Init ... !!!
[MCU2_0]      3.618666 s: SCICLIENT: DMSC FW version [21.9.1--v2021.09a (Terrific Lla]
[MCU2_0]      3.618724 s: SCICLIENT: DMSC FW revision 0x15
[MCU2_0]      3.618780 s: SCICLIENT: DMSC FW ABI revision 3.1
[MCU2_0]      3.618821 s: SCICLIENT: Init ... Done !!!
[MCU2_0]      3.618851 s: UDMA: Init ... !!!
[MCU2_0]      3.620276 s: UDMA: Init ... Done !!!
[MCU2_0]      3.620347 s: MEM: Init ... !!!
[MCU2_0]      3.620397 s: MEM: Created heap (DDR_SHARED_MEM, id=0, flags=0x00000004) @ d9000000 of size 16777216 bytes !!!
[MCU2_0]      3.620480 s: MEM: Created heap (L3_MEM, id=1, flags=0x00000000) @ 3600000 of size 262144 bytes !!!
[MCU2_0]      3.620544 s: MEM: Init ... Done !!!
[MCU2_0]      3.620573 s: IPC: Init ... !!!
[MCU2_0]      3.620642 s: IPC: 6 CPUs participating in IPC !!!
[MCU2_0]      3.620689 s: IPC: Waiting for HLOS to be ready ... !!!
[MCU2_0]     17.746026 s: IPC: HLOS is ready !!!
[MCU2_0]     17.761773 s: IPC: Init ... Done !!!
[MCU2_0]     17.761843 s: APP: Syncing with 5 CPUs ... !!!
[MCU2_0]     17.927250 s: APP: Syncing with 5 CPUs ... Done !!!
[MCU2_0]     17.927488 s: REMOTE_SERVICE: Init ... !!!
[MCU2_0]     17.929049 s: REMOTE_SERVICE: Init ... Done !!!
[MCU2_0]     17.929123 s: FVID2: Init ... !!!
[MCU2_0]     17.929204 s: FVID2: Init ... Done !!!
[MCU2_0]     17.929256 s: DSS: Init ... !!!
[MCU2_0]     17.929287 s: DSS: Display type is DSI !!!
[MCU2_0]     17.929316 s: DSS: M2M Path is enabled !!!
[MCU2_0]     17.929345 s: DSS: SoC init ... !!!
[MCU2_0]     17.929373 s: SCICLIENT: Sciclient_pmSetModuleState module=152 state=2
[MCU2_0]     17.929551 s: SCICLIENT: Sciclient_pmSetModuleState success
[MCU2_0]     17.929596 s: SCICLIENT: Sciclient_pmSetModuleState module=150 state=2
[MCU2_0]     17.930095 s: SCICLIENT: Sciclient_pmSetModuleState success
[MCU2_0]     17.930138 s: SCICLIENT: Sciclient_pmSetModuleState module=296 state=2
[MCU2_0]     17.930530 s: SCICLIENT: Sciclient_pmSetModuleState success
[MCU2_0]     17.930572 s: SCICLIENT: Sciclient_pmSetModuleClkParent module=152 clk=9 parent=11
[MCU2_0]     17.931114 s: SCICLIENT: Sciclient_pmSetModuleClkParent success
[MCU2_0]     17.931157 s: SCICLIENT: Sciclient_pmSetModuleClkFreq module=152 clk=9 freq=146940000
[MCU2_0]     17.932472 s: SCICLIENT: Sciclient_pmSetModuleClkFreq success
[MCU2_0]     17.932514 s: SCICLIENT: Sciclient_pmModuleClkRequest module=152 clk=9 state=2 flag=0
[MCU2_0]     17.933070 s: SCICLIENT: Sciclient_pmModuleClkRequest success
[MCU2_0]     17.933111 s: DSS: SoC init ... Done !!!
[MCU2_0]     17.933142 s: DSS: Configuring SERDES ... !!!
[MCU2_0]     18.074743 s: 0x2c Success!!
[MCU2_0]     18.079738 s: 0x2c Success!!
[MCU2_0]     18.612735 s: I2c finish
[MCU2_0]     18.612940 s: [Michael] 0x16, 0x0 0x2c
[MCU2_0]     18.613139 s: [Michael] 0x16, 0x1 0x0
[MCU2_0]     18.613323 s: [Michael] 0x16, 0x2 0x0
[MCU2_0]     18.613507 s: [Michael] 0x16, 0x3 0x9a
[MCU2_0]     18.613691 s: [Michael] 0x16, 0x4 0x0
[MCU2_0]     18.613881 s: [Michael] 0x16, 0x5 0x0
[MCU2_0]     18.614070 s: [Michael] 0x16, 0x6 0x58
[MCU2_0]     18.614260 s: [Michael] 0x16, 0x7 0x0
[MCU2_0]     18.614444 s: [Michael] 0x16, 0x8 0x0
[MCU2_0]     18.614625 s: [Michael] 0x16, 0x9 0x1
[MCU2_0]     18.614812 s: [Michael] 0x16, 0xa 0x81
[MCU2_0]     18.615003 s: [Michael] 0x16, 0xb 0x0
[MCU2_0]     18.615185 s: [Michael] 0x16, 0xc 0x7
[MCU2_0]     18.615369 s: [Michael] 0x16, 0xd 0x30
[MCU2_0]     18.615554 s: [Michael] 0x16, 0xe 0x0
[MCU2_0]     18.615745 s: [Michael] 0x16, 0xf 0x0
[MCU2_0]     18.615930 s: [Michael] 0x16, 0x10 0x0
[MCU2_0]     18.616118 s: [Michael] 0x16, 0x11 0x0
[MCU2_0]     18.616303 s: [Michael] 0x16, 0x12 0x0
[MCU2_0]     18.616488 s: [Michael] 0x16, 0x13 0xcf
[MCU2_0]     18.616674 s: [Michael] 0x16, 0x14 0x0
[MCU2_0]     18.616860 s: [Michael] 0x16, 0x15 0x0
[MCU2_0]     18.617047 s: [Michael] 0x16, 0x16 0xfe
[MCU2_0]     18.617237 s: [Michael] 0x16, 0x17 0x1e
[MCU2_0]     18.617424 s: [Michael] 0x16, 0x18 0x7f
[MCU2_0]     18.617607 s: [Michael] 0x16, 0x19 0x7f
[MCU2_0]     18.617800 s: [Michael] 0x16, 0x1a 0x1
[MCU2_0]     18.617988 s: [Michael] 0x16, 0x1b 0x0
[MCU2_0]     18.618175 s: [Michael] 0x16, 0x1c 0x0
[MCU2_0]     18.618357 s: [Michael] 0x16, 0x1d 0x0
[MCU2_0]     18.618541 s: [Michael] 0x16, 0x1e 0x1
[MCU2_0]     18.618726 s: [Michael] 0x16, 0x1f 0x0
[MCU2_0]     18.618920 s: [Michael] 0x16, 0x20 0xb
[MCU2_0]     18.619109 s: [Michael] 0x16, 0x21 0x0
[MCU2_0]     18.619291 s: [Michael] 0x16, 0x22 0x25
[MCU2_0]     18.619475 s: [Michael] 0x16, 0x23 0x0
[MCU2_0]     18.619657 s: [Michael] 0x16, 0x24 0x0
[MCU2_0]     18.619846 s: [Michael] 0x16, 0x25 0x0
[MCU2_0]     18.620032 s: [Michael] 0x16, 0x26 0x0
[MCU2_0]     18.620219 s: [Michael] 0x16, 0x27 0x0
[MCU2_0]     18.620403 s: [Michael] 0x16, 0x28 0x1
[MCU2_0]     18.620586 s: [Michael] 0x16, 0x29 0x20
[MCU2_0]     18.620775 s: [Michael] 0x16, 0x2a 0x20
[MCU2_0]     18.620962 s: [Michael] 0x16, 0x2b 0xa0
[MCU2_0]     18.621149 s: [Michael] 0x16, 0x2c 0x0
[MCU2_0]     18.621332 s: [Michael] 0x16, 0x2d 0x0
[MCU2_0]     18.621517 s: [Michael] 0x16, 0x2e 0xa5
[MCU2_0]     18.621699 s: [Michael] 0x16, 0x2f 0x5a
[MCU2_0]     18.621890 s: [Michael] 0x16, 0x30 0x0
[MCU2_0]     18.622076 s: [Michael] 0x16, 0x31 0xb9
[MCU2_0]     18.622258 s: [Michael] 0x16, 0x32 0x0
[MCU2_0]     18.622439 s: [Michael] 0x16, 0x33 0x5
[MCU2_0]     18.622625 s: [Michael] 0x16, 0x34 0xc
[MCU2_0]     18.622821 s: [Michael] 0x16, 0x35 0x0
[MCU2_0]     18.623011 s: [Michael] 0x16, 0x36 0x0
[MCU2_0]     18.623197 s: [Michael] 0x16, 0x37 0x0
[MCU2_0]     18.623383 s: [Michael] 0x16, 0x38 0x0
[MCU2_0]     18.623569 s: [Michael] 0x16, 0x39 0x0
[MCU2_0]     18.623762 s: [Michael] 0x16, 0x3a 0x0
[MCU2_0]     18.623951 s: [Michael] 0x16, 0x3b 0x0
[MCU2_0]     18.624139 s: [Michael] 0x16, 0x3c 0x0
[MCU2_0]     18.624321 s: [Michael] 0x16, 0x3d 0x0
[MCU2_0]     18.624504 s: [Michael] 0x16, 0x3e 0xb0
[MCU2_0]     18.624686 s: [Michael] 0x16, 0x3f 0x2
[MCU2_0]     18.624875 s: [Michael] 0x16, 0x40 0x10
[MCU2_0]     18.625063 s: [Michael] 0x16, 0x41 0x94
[MCU2_0]     18.625246 s: [Michael] 0x16, 0x42 0x0
[MCU2_0]     18.625423 s: [Michael] 0x16, 0x43 0x0
[MCU2_0]     18.625605 s: [Michael] 0x16, 0x44 0x0
[MCU2_0]     18.625794 s: [Michael] 0x16, 0x45 0x0
[MCU2_0]     18.625982 s: [Michael] 0x16, 0x46 0x0
[MCU2_0]     18.626165 s: [Michael] 0x16, 0x47 0x0
[MCU2_0]     18.626351 s: [Michael] 0x16, 0x48 0x0
[MCU2_0]     18.626531 s: [Michael] 0x16, 0x49 0x0
[MCU2_0]     18.626717 s: [Michael] 0x16, 0x4a 0x0
[MCU2_0]     18.626912 s: [Michael] 0x16, 0x4b 0x0
[MCU2_0]     18.627095 s: [Michael] 0x16, 0x4c 0x0
[MCU2_0]     18.627279 s: [Michael] 0x16, 0x4d 0x0
[MCU2_0]     18.627463 s: [Michael] 0x16, 0x4e 0x0
[MCU2_0]     18.627644 s: [Michael] 0x16, 0x4f 0x8c
[MCU2_0]     18.627834 s: [Michael] 0x16, 0x50 0x16
[MCU2_0]     18.628023 s: [Michael] 0x16, 0x51 0x0
[MCU2_0]     18.628213 s: [Michael] 0x16, 0x52 0x0
[MCU2_0]     18.628399 s: [Michael] 0x16, 0x53 0x0
[MCU2_0]     18.628583 s: [Michael] 0x16, 0x54 0x2
[MCU2_0]     18.628769 s: [Michael] 0x16, 0x55 0x10
[MCU2_0]     18.628954 s: [Michael] 0x16, 0x56 0x0
[MCU2_0]     18.629143 s: [Michael] 0x16, 0x57 0x2
[MCU2_0]     18.629324 s: [Michael] 0x16, 0x58 0x0
[MCU2_0]     18.629509 s: [Michael] 0x16, 0x59 0x0
[MCU2_0]     18.629693 s: [Michael] 0x16, 0x5a 0x18
[MCU2_0]     18.629885 s: [Michael] 0x16, 0x5b 0xb
[MCU2_0]     18.630074 s: [Michael] 0x16, 0x5c 0x7
[MCU2_0]     18.630262 s: [Michael] 0x16, 0x5d 0x6
[MCU2_0]     18.630446 s: [Michael] 0x16, 0x5e 0x44
[MCU2_0]     18.630628 s: [Michael] 0x16, 0x5f 0x17
[MCU2_0]     18.630821 s: [Michael] 0x16, 0x60 0x22
[MCU2_0]     18.631007 s: [Michael] 0x16, 0x61 0x2
[MCU2_0]     18.631195 s: [Michael] 0x16, 0x62 0x0
[MCU2_0]     18.631378 s: [Michael] 0x16, 0x63 0x0
[MCU2_0]     18.631562 s: [Michael] 0x16, 0x64 0x15
[MCU2_0]     18.631755 s: [Michael] 0x16, 0x65 0x6c
[MCU2_0]     18.631945 s: [Michael] 0x16, 0x66 0x1a
[MCU2_0]     18.632134 s: [Michael] 0x16, 0x67 0x4
[MCU2_0]     18.632318 s: [Michael] 0x16, 0x68 0x0
[MCU2_0]     18.632506 s: [Michael] 0x16, 0x69 0x0
[MCU2_0]     18.632692 s: [Michael] 0x16, 0x6a 0x0
[MCU2_0]     18.632891 s: [Michael] 0x16, 0x6b 0x0
[MCU2_0]     18.633078 s: [Michael] 0x16, 0x6c 0x0
[MCU2_0]     18.633264 s: [Michael] 0x16, 0x6d 0x0
[MCU2_0]     18.633447 s: [Michael] 0x16, 0x6e 0x20
[MCU2_0]     18.633630 s: [Michael] 0x16, 0x6f 0x0
[MCU2_0]     18.633821 s: [Michael] 0x16, 0x70 0x0
[MCU2_0]     18.634006 s: [Michael] 0x16, 0x71 0x0
[MCU2_0]     18.634194 s: [Michael] 0x16, 0x72 0x0
[MCU2_0]     18.634378 s: [Michael] 0x16, 0x73 0x0
[MCU2_0]     18.634559 s: [Michael] 0x16, 0x74 0x0
[MCU2_0]     18.634750 s: [Michael] 0x16, 0x75 0x0
[MCU2_0]     18.634938 s: [Michael] 0x16, 0x76 0x0
[MCU2_0]     18.635124 s: [Michael] 0x16, 0x77 0x0
[MCU2_0]     18.635307 s: [Michael] 0x16, 0x78 0x0
[MCU2_0]     18.635494 s: [Michael] 0x16, 0x79 0x0
[MCU2_0]     18.635677 s: [Michael] 0x16, 0x7a 0x0
[MCU2_0]     18.635866 s: [Michael] 0x16, 0x7b 0x0
[MCU2_0]     18.636053 s: [Michael] 0x16, 0x7c 0x0
[MCU2_0]     18.636238 s: [Michael] 0x16, 0x7d 0x0
[MCU2_0]     18.636423 s: [Michael] 0x16, 0x7e 0x7f
[MCU2_0]     18.636604 s: [Michael] 0x16, 0x7f 0x0
[MCU2_0]     18.636640 s: DSS: SERDES Configuration... Done !!!
[MCU2_0]     18.639860 s: DSS: Init ... Done !!!
[MCU2_0]     18.639933 s: [Michael] prm.timings.width = 1080
[MCU2_0]     18.639976 s: [Michael] prm.timings.height = 1920
[MCU2_0]     18.640011 s: VHWA: VPAC Init ... !!!
[MCU2_0]     18.640037 s: SCICLIENT: Sciclient_pmSetModuleState module=290 state=2
[MCU2_0]     18.640225 s: SCICLIENT: Sciclient_pmSetModuleState success
[MCU2_0]     18.640271 s: VHWA: LDC Init ... !!!
[MCU2_0]     18.643867 s: VHWA: LDC Init ... Done !!!
[MCU2_0]     18.643934 s: VHWA: MSC Init ... !!!
[MCU2_0]     18.654637 s: VHWA: MSC Init ... Done !!!
[MCU2_0]     18.654701 s: VHWA: NF Init ... !!!
[MCU2_0]     18.656612 s: VHWA: NF Init ... Done !!!
[MCU2_0]     18.656679 s: VHWA: VISS Init ... !!!
[MCU2_0]     18.667769 s: VHWA: VISS Init ... Done !!!
[MCU2_0]     18.667839 s: VHWA: VPAC Init ... Done !!!
[MCU2_0]     18.667893 s:  VX_ZONE_INIT:Enabled
[MCU2_0]     18.667924 s:  VX_ZONE_ERROR:Enabled
[MCU2_0]     18.667952 s:  VX_ZONE_WARNING:Enabled
[MCU2_0]     18.669135 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:54] Added target IPU1-0
[MCU2_0]     18.669375 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:54] Added target VPAC_NF
[MCU2_0]     18.669606 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:54] Added target VPAC_LDC1
[MCU2_0]     18.669845 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:54] Added target VPAC_MSC1
[MCU2_0]     18.670077 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:54] Added target VPAC_MSC2
[MCU2_0]     18.670385 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:54] Added target VPAC_VISS1
[MCU2_0]     18.670652 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:54] Added target CAPTURE1
[MCU2_0]     18.670928 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:54] Added target CAPTURE2
[MCU2_0]     18.671189 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:54] Added target DISPLAY1
[MCU2_0]     18.671454 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:54] Added target DISPLAY2
[MCU2_0]     18.671685 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:54] Added target CSITX
[MCU2_0]     18.671971 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:54] Added target CAPTURE3
[MCU2_0]     18.672240 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:54] Added target CAPTURE4
[MCU2_0]     18.672509 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:54] Added target CAPTURE5
[MCU2_0]     18.672779 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:54] Added target CAPTURE6
[MCU2_0]     18.673086 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:54] Added target CAPTURE7
[MCU2_0]     18.673397 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:54] Added target CAPTURE8
[MCU2_0]     18.673645 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:54] Added target DSS_M2M1
[MCU2_0]     18.673891 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:54] Added target DSS_M2M2
[MCU2_0]     18.674126 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:54] Added target DSS_M2M3
[MCU2_0]     18.674357 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:54] Added target DSS_M2M4
[MCU2_0]     18.674415 s:  VX_ZONE_INIT:[tivxInitLocal:130] Initialization Done !!!
[MCU2_0]     18.674455 s: APP: OpenVX Target kernel init ... !!!
[MCU2_0]     18.689902 s: APP: OpenVX Target kernel init ... Done !!!
[MCU2_0]     18.689969 s: CSI2RX: Init ... !!!
[MCU2_0]     18.690001 s: SCICLIENT: Sciclient_pmSetModuleState module=25 state=2
[MCU2_0]     18.690146 s: SCICLIENT: Sciclient_pmSetModuleState success
[MCU2_0]     18.690196 s: SCICLIENT: Sciclient_pmSetModuleState module=26 state=2
[MCU2_0]     18.690355 s: SCICLIENT: Sciclient_pmSetModuleState success
[MCU2_0]     18.690396 s: SCICLIENT: Sciclient_pmSetModuleState module=27 state=2
[MCU2_0]     18.690539 s: SCICLIENT: Sciclient_pmSetModuleState success
[MCU2_0]     18.690579 s: SCICLIENT: Sciclient_pmSetModuleState module=147 state=2
[MCU2_0]     18.690684 s: SCICLIENT: Sciclient_pmSetModuleState success
[MCU2_0]     18.690723 s: SCICLIENT: Sciclient_pmSetModuleState module=148 state=2
[MCU2_0]     18.690836 s: SCICLIENT: Sciclient_pmSetModuleState success
[MCU2_0]     18.691631 s: CSI2RX: Init ... Done !!!
[MCU2_0]     18.691694 s: ISS: Init ... !!!
[MCU2_0]     18.691757 s: Michael: IssSensor_IMX390_Init()
[MCU2_0]     18.691797 s: Found sensor IMX390-UB953_D3 at location 0
[MCU2_0]     18.691845 s: Found sensor AR0233-UB953_MARS at location 1
[MCU2_0]     18.691888 s: Found sensor AR0820-UB953_LI at location 2
[MCU2_0]     18.691930 s: Found sensor UB9xxx_RAW12_TESTPATTERN at location 3
[MCU2_0]     18.691971 s: Found sensor UB96x_UYVY_TESTPATTERN at location 4
[MCU2_0]     18.692010 s: Found sensor GW_AR0233_UYVY at location 5
[MCU2_0]     18.692051 s: Michael: IssSensor_ISX019_Init()
[MCU2_0]     18.692080 s: Found sensor ISX019-UB913_oTo at location 6
[MCU2_0]     18.692119 s: IssSensor_Init ... Done !!!
[MCU2_0]     18.692212 s: vissRemoteServer_Init ... Done !!!
[MCU2_0]     18.692282 s: IttRemoteServer_Init ... Done !!!
[MCU2_0]     18.692319 s: UDMA Copy: Init ... !!!
[MCU2_0]     18.694238 s: UDMA Copy: Init ... Done !!!
[MCU2_0]     18.694345 s: APP: Init ... Done !!!
[MCU2_0]     18.694384 s: APP: Run ... !!!
[MCU2_0]     18.694412 s: IPC: Starting echo test ...
[MCU2_0]     18.696988 s: APP: Run ... Done !!!
[MCU2_0]     18.698582 s: IPC: Echo status: mpu1_0[x] mcu2_0[s] mcu2_1[.] C66X_1[P] C66X_2[.] C7X_1[.]
[MCU2_0]     18.698912 s: IPC: Echo status: mpu1_0[x] mcu2_0[s] mcu2_1[P] C66X_1[P] C66X_2[.] C7X_1[.]
[MCU2_0]     18.699031 s: IPC: Echo status: mpu1_0[x] mcu2_0[s] mcu2_1[P] C66X_1[P] C66X_2[P] C7X_1[.]
[MCU2_0]     18.699135 s: IPC: Echo status: mpu1_0[x] mcu2_0[s] mcu2_1[P] C66X_1[P] C66X_2[P] C7X_1[P]
[MCU2_1]      3.633229 s: CIO: Init ... Done !!!
[MCU2_1]      3.633298 s: ### CPU Frequency = 1000000000 Hz
[MCU2_1]      3.633342 s: APP: Init ... !!!
[MCU2_1]      3.633367 s: SCICLIENT: Init ... !!!
[MCU2_1]      3.633623 s: SCICLIENT: DMSC FW version [21.9.1--v2021.09a (Terrific Lla]
[MCU2_1]      3.633675 s: SCICLIENT: DMSC FW revision 0x15
[MCU2_1]      3.633710 s: SCICLIENT: DMSC FW ABI revision 3.1
[MCU2_1]      3.633747 s: SCICLIENT: Init ... Done !!!
[MCU2_1]      3.633793 s: UDMA: Init ... !!!
[MCU2_1]      3.635301 s: UDMA: Init ... Done !!!
[MCU2_1]      3.635367 s: MEM: Init ... !!!
[MCU2_1]      3.635414 s: MEM: Created heap (DDR_SHARED_MEM, id=0, flags=0x00000004) @ da000000 of size 16777216 bytes !!!
[MCU2_1]      3.635489 s: MEM: Created heap (L3_MEM, id=1, flags=0x00000001) @ 3640000 of size 262144 bytes !!!
[MCU2_1]      3.635550 s: MEM: Init ... Done !!!
[MCU2_1]      3.635576 s: IPC: Init ... !!!
[MCU2_1]      3.635638 s: IPC: 6 CPUs participating in IPC !!!
[MCU2_1]      3.635693 s: IPC: Waiting for HLOS to be ready ... !!!
[MCU2_1]     17.911420 s: IPC: HLOS is ready !!!
[MCU2_1]     17.927134 s: IPC: Init ... Done !!!
[MCU2_1]     17.927201 s: APP: Syncing with 5 CPUs ... !!!
[MCU2_1]     17.927248 s: APP: Syncing with 5 CPUs ... Done !!!
[MCU2_1]     17.927287 s: REMOTE_SERVICE: Init ... !!!
[MCU2_1]     17.929058 s: REMOTE_SERVICE: Init ... Done !!!
[MCU2_1]     17.929129 s: FVID2: Init ... !!!
[MCU2_1]     17.929205 s: FVID2: Init ... Done !!!
[MCU2_1]     17.929239 s: VHWA: DMPAC: Init ... !!!
[MCU2_1]     17.929266 s: SCICLIENT: Sciclient_pmSetModuleState module=48 state=2
[MCU2_1]     17.929452 s: SCICLIENT: Sciclient_pmSetModuleState success
[MCU2_1]     17.929496 s: SCICLIENT: Sciclient_pmSetModuleState module=305 state=2
[MCU2_1]     17.930013 s: SCICLIENT: Sciclient_pmSetModuleState success
[MCU2_1]     17.930055 s: VHWA: DOF Init ... !!!
[MCU2_1]     17.940173 s: VHWA: DOF Init ... Done !!!
[MCU2_1]     17.940239 s: VHWA: SDE Init ... !!!
[MCU2_1]     17.943139 s: VHWA: SDE Init ... Done !!!
[MCU2_1]     17.943199 s: VHWA: DMPAC: Init ... Done !!!
[MCU2_1]     17.943250 s:  VX_ZONE_INIT:Enabled
[MCU2_1]     17.943284 s:  VX_ZONE_ERROR:Enabled
[MCU2_1]     17.943312 s:  VX_ZONE_WARNING:Enabled
[MCU2_1]     17.944484 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:54] Added target DMPAC_SDE
[MCU2_1]     17.944723 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:54] Added target DMPAC_DOF
[MCU2_1]     17.944962 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:54] Added target IPU1-1
[MCU2_1]     17.945019 s:  VX_ZONE_INIT:[tivxInitLocal:130] Initialization Done !!!
[MCU2_1]     17.945058 s: APP: OpenVX Target kernel init ... !!!
[MCU2_1]     17.945343 s: APP: OpenVX Target kernel init ... Done !!!
[MCU2_1]     17.945384 s: UDMA Copy: Init ... !!!
[MCU2_1]     17.947305 s: UDMA Copy: Init ... Done !!!
[MCU2_1]     17.947377 s: APP: Init ... Done !!!
[MCU2_1]     17.947415 s: APP: Run ... !!!
[MCU2_1]     17.947441 s: IPC: Starting echo test ...
[MCU2_1]     17.949994 s: APP: Run ... Done !!!
[MCU2_1]     17.951418 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[s] C66X_1[P] C66X_2[.] C7X_1[.]
[MCU2_1]     17.951543 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[s] C66X_1[P] C66X_2[P] C7X_1[.]
[MCU2_1]     17.951642 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[s] C66X_1[P] C66X_2[P] C7X_1[P]
[MCU2_1]     18.698536 s: IPC: Echo status: mpu1_0[x] mcu2_0[P] mcu2_1[s] C66X_1[P] C66X_2[P] C7X_1[P]
[C6x_1 ]      3.703249 s: CIO: Init ... Done !!!
[C6x_1 ]      3.703278 s: ### CPU Frequency = 1350000000 Hz
[C6x_1 ]      3.703289 s: APP: Init ... !!!
[C6x_1 ]      3.703298 s: SCICLIENT: Init ... !!!
[C6x_1 ]      3.703553 s: SCICLIENT: DMSC FW version [21.9.1--v2021.09a (Terrific Lla]
[C6x_1 ]      3.703569 s: SCICLIENT: DMSC FW revision 0x15
[C6x_1 ]      3.703579 s: SCICLIENT: DMSC FW ABI revision 3.1
[C6x_1 ]      3.703590 s: SCICLIENT: Init ... Done !!!
[C6x_1 ]      3.703600 s: UDMA: Init ... !!!
[C6x_1 ]      3.705374 s: UDMA: Init ... Done !!!
[C6x_1 ]      3.705398 s: MEM: Init ... !!!
[C6x_1 ]      3.705413 s: MEM: Created heap (DDR_SHARED_MEM, id=0, flags=0x00000004) @ dc000000 of size 16777216 bytes !!!
[C6x_1 ]      3.705433 s: MEM: Created heap (L2_MEM, id=2, flags=0x00000001) @ 800000 of size 229376 bytes !!!
[C6x_1 ]      3.705450 s: MEM: Created heap (DDR_SCRATCH_MEM, id=4, flags=0x00000001) @ dd000000 of size 50331648 bytes !!!
[C6x_1 ]      3.705468 s: MEM: Init ... Done !!!
[C6x_1 ]      3.705477 s: IPC: Init ... !!!
[C6x_1 ]      3.705501 s: IPC: 6 CPUs participating in IPC !!!
[C6x_1 ]      3.705517 s: IPC: Waiting for HLOS to be ready ... !!!
[C6x_1 ]     12.004874 s: IPC: HLOS is ready !!!
[C6x_1 ]     12.009516 s: IPC: Init ... Done !!!
[C6x_1 ]     12.009547 s: APP: Syncing with 5 CPUs ... !!!
[C6x_1 ]     17.927248 s: APP: Syncing with 5 CPUs ... Done !!!
[C6x_1 ]     17.927260 s: REMOTE_SERVICE: Init ... !!!
[C6x_1 ]     17.927934 s: REMOTE_SERVICE: Init ... Done !!!
[C6x_1 ]     17.927976 s:  VX_ZONE_INIT:Enabled
[C6x_1 ]     17.927988 s:  VX_ZONE_ERROR:Enabled
[C6x_1 ]     17.927999 s:  VX_ZONE_WARNING:Enabled
[C6x_1 ]     17.928892 s:  VX_ZONE_INIT:[tivxInitLocal:130] Initialization Done !!!
[C6x_1 ]     17.928910 s: APP: OpenVX Target kernel init ... !!!
[C6x_1 ]     17.929346 s: APP: OpenVX Target kernel init ... Done !!!
[C6x_1 ]     17.929368 s: UDMA Copy: Init ... !!!
[C6x_1 ]     17.934153 s: UDMA Copy: Init ... Done !!!
[C6x_1 ]     17.934177 s: APP: Init ... Done !!!
[C6x_1 ]     17.934975 s: APP: Run ... !!!
[C6x_1 ]     17.934991 s: IPC: Starting echo test ...
[C6x_1 ]     17.936057 s: APP: Run ... Done !!!
[C6x_1 ]     17.936470 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[x] C66X_1[s] C66X_2[x] C7X_1[P]
[C6x_1 ]     17.936917 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[x] C66X_1[s] C66X_2[P] C7X_1[P]
[C6x_1 ]     17.951117 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[P] C66X_1[s] C66X_2[P] C7X_1[P]
[C6x_1 ]     18.698341 s: IPC: Echo status: mpu1_0[x] mcu2_0[P] mcu2_1[P] C66X_1[s] C66X_2[P] C7X_1[P]
[C6x_2 ]      3.794438 s: CIO: Init ... Done !!!
[C6x_2 ]      3.794468 s: ### CPU Frequency = 1350000000 Hz
[C6x_2 ]      3.794480 s: APP: Init ... !!!
[C6x_2 ]      3.794489 s: SCICLIENT: Init ... !!!
[C6x_2 ]      3.794740 s: SCICLIENT: DMSC FW version [21.9.1--v2021.09a (Terrific Lla]
[C6x_2 ]      3.794756 s: SCICLIENT: DMSC FW revision 0x15
[C6x_2 ]      3.794767 s: SCICLIENT: DMSC FW ABI revision 3.1
[C6x_2 ]      3.794778 s: SCICLIENT: Init ... Done !!!
[C6x_2 ]      3.794788 s: UDMA: Init ... !!!
[C6x_2 ]      3.796583 s: UDMA: Init ... Done !!!
[C6x_2 ]      3.796608 s: MEM: Init ... !!!
[C6x_2 ]      3.796623 s: MEM: Created heap (DDR_SHARED_MEM, id=0, flags=0x00000004) @ e0000000 of size 16777216 bytes !!!
[C6x_2 ]      3.796643 s: MEM: Created heap (L2_MEM, id=2, flags=0x00000001) @ 800000 of size 229376 bytes !!!
[C6x_2 ]      3.796660 s: MEM: Created heap (DDR_SCRATCH_MEM, id=4, flags=0x00000001) @ e1000000 of size 50331648 bytes !!!
[C6x_2 ]      3.796679 s: MEM: Init ... Done !!!
[C6x_2 ]      3.796688 s: IPC: Init ... !!!
[C6x_2 ]      3.796712 s: IPC: 6 CPUs participating in IPC !!!
[C6x_2 ]      3.796729 s: IPC: Waiting for HLOS to be ready ... !!!
[C6x_2 ]     12.212903 s: IPC: HLOS is ready !!!
[C6x_2 ]     12.217543 s: IPC: Init ... Done !!!
[C6x_2 ]     12.217574 s: APP: Syncing with 5 CPUs ... !!!
[C6x_2 ]     17.927248 s: APP: Syncing with 5 CPUs ... Done !!!
[C6x_2 ]     17.927261 s: REMOTE_SERVICE: Init ... !!!
[C6x_2 ]     17.927945 s: REMOTE_SERVICE: Init ... Done !!!
[C6x_2 ]     17.927987 s:  VX_ZONE_INIT:Enabled
[C6x_2 ]     17.927999 s:  VX_ZONE_ERROR:Enabled
[C6x_2 ]     17.928010 s:  VX_ZONE_WARNING:Enabled
[C6x_2 ]     17.928899 s:  VX_ZONE_INIT:[tivxInitLocal:130] Initialization Done !!!
[C6x_2 ]     17.928916 s: APP: OpenVX Target kernel init ... !!!
[C6x_2 ]     17.929355 s: APP: OpenVX Target kernel init ... Done !!!
[C6x_2 ]     17.929376 s: UDMA Copy: Init ... !!!
[C6x_2 ]     17.934475 s: UDMA Copy: Init ... Done !!!
[C6x_2 ]     17.934499 s: APP: Init ... Done !!!
[C6x_2 ]     17.935304 s: APP: Run ... !!!
[C6x_2 ]     17.935320 s: IPC: Starting echo test ...
[C6x_2 ]     17.936478 s: APP: Run ... Done !!!
[C6x_2 ]     17.936919 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[x] C66X_1[P] C66X_2[s] C7X_1[.]
[C6x_2 ]     17.936964 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[x] C66X_1[P] C66X_2[s] C7X_1[P]
[C6x_2 ]     17.951146 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[P] C66X_1[P] C66X_2[s] C7X_1[P]
[C6x_2 ]     18.698375 s: IPC: Echo status: mpu1_0[x] mcu2_0[P] mcu2_1[P] C66X_1[P] C66X_2[s] C7X_1[P]
[C7x_1 ]      4.012493 s: CIO: Init ... Done !!!
[C7x_1 ]      4.012508 s: ### CPU Frequency = 1000000000 Hz
[C7x_1 ]      4.012520 s: APP: Init ... !!!
[C7x_1 ]      4.012529 s: SCICLIENT: Init ... !!!
[C7x_1 ]      4.012746 s: SCICLIENT: DMSC FW version [21.9.1--v2021.09a (Terrific Lla]
[C7x_1 ]      4.012761 s: SCICLIENT: DMSC FW revision 0x15
[C7x_1 ]      4.012772 s: SCICLIENT: DMSC FW ABI revision 3.1
[C7x_1 ]      4.012783 s: SCICLIENT: Init ... Done !!!
[C7x_1 ]      4.012792 s: UDMA: Init ... !!!
[C7x_1 ]      4.013981 s: UDMA: Init ... Done !!!
[C7x_1 ]      4.013994 s: MEM: Init ... !!!
[C7x_1 ]      4.014005 s: MEM: Created heap (DDR_SHARED_MEM, id=0, flags=0x00000004) @ 100000000 of size 268435456 bytes !!!
[C7x_1 ]      4.014027 s: MEM: Created heap (L3_MEM, id=1, flags=0x00000001) @ 70020000 of size 8159232 bytes !!!
[C7x_1 ]      4.014045 s: MEM: Created heap (L2_MEM, id=2, flags=0x00000001) @ 64800000 of size 458752 bytes !!!
[C7x_1 ]      4.014063 s: MEM: Created heap (L1_MEM, id=3, flags=0x00000001) @ 64e00000 of size 16384 bytes !!!
[C7x_1 ]      4.014080 s: MEM: Created heap (DDR_SCRATCH_MEM, id=4, flags=0x00000001) @ e4000000 of size 402653184 bytes !!!
[C7x_1 ]      4.014100 s: MEM: Init ... Done !!!
[C7x_1 ]      4.014108 s: IPC: Init ... !!!
[C7x_1 ]      4.014123 s: IPC: 6 CPUs participating in IPC !!!
[C7x_1 ]      4.014138 s: IPC: Waiting for HLOS to be ready ... !!!
[C7x_1 ]     12.443410 s: IPC: HLOS is ready !!!
[C7x_1 ]     12.445532 s: IPC: Init ... Done !!!
[C7x_1 ]     12.445548 s: APP: Syncing with 5 CPUs ... !!!
[C7x_1 ]     17.927249 s: APP: Syncing with 5 CPUs ... Done !!!
[C7x_1 ]     17.927266 s: REMOTE_SERVICE: Init ... !!!
[C7x_1 ]     17.927446 s: REMOTE_SERVICE: Init ... Done !!!
[C7x_1 ]     17.927468 s:  VX_ZONE_INIT:Enabled
[C7x_1 ]     17.927480 s:  VX_ZONE_ERROR:Enabled
[C7x_1 ]     17.927490 s:  VX_ZONE_WARNING:Enabled
[C7x_1 ]     17.927652 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:59] Added target DSP_C7-1
[C7x_1 ]     17.927718 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:59] Added target DSP_C7-1_PRI_2
[C7x_1 ]     17.927785 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:59] Added target DSP_C7-1_PRI_3
[C7x_1 ]     17.927906 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:59] Added target DSP_C7-1_PRI_4
[C7x_1 ]     17.927977 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:59] Added target DSP_C7-1_PRI_5
[C7x_1 ]     17.928049 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:59] Added target DSP_C7-1_PRI_6
[C7x_1 ]     17.928154 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:59] Added target DSP_C7-1_PRI_7
[C7x_1 ]     17.928221 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:59] Added target DSP_C7-1_PRI_8
[C7x_1 ]     17.928243 s:  VX_ZONE_INIT:[tivxInitLocal:130] Initialization Done !!!
[C7x_1 ]     17.928256 s: APP: OpenVX Target kernel init ... !!!
[C7x_1 ]     17.928426 s: APP: OpenVX Target kernel init ... Done !!!
[C7x_1 ]     17.928441 s: APP: Init ... Done !!!
[C7x_1 ]     17.928451 s: APP: Run ... !!!
[C7x_1 ]     17.928460 s: IPC: Starting echo test ...
[C7x_1 ]     17.928627 s: APP: Run ... Done !!!
[C7x_1 ]     17.936458 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[x] C66X_1[P] C66X_2[x] C7X_1[s]
[C7x_1 ]     17.936918 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[x] C66X_1[P] C66X_2[P] C7X_1[s]
[C7x_1 ]     17.951162 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[P] C66X_1[P] C66X_2[P] C7X_1[s]
[C7x_1 ]     18.698431 s: IPC: Echo status: mpu1_0[x] mcu2_0[P] mcu2_1[P] C66X_1[P] C66X_2[P] C7X_1[s]

root@j7-evm:/opt/vision_apps# ./run_app_tidl.sh
APP: Init ... !!!
MEM: Init ... !!!
MEM: Initialized DMA HEAP (fd=4) !!!
MEM: Init ... Done !!!
IPC: Init ... !!!
IPC: Init ... Done !!!
REMOTE_SERVICE: Init ... !!!
REMOTE_SERVICE: Init ... Done !!!
   630.260356 s: GTC Frequency = 200 MHz
APP: Init ... Done !!!
   630.273850 s:  VX_ZONE_INIT:Enabled
   630.273890 s:  VX_ZONE_ERROR:Enabled
   630.273895 s:  VX_ZONE_WARNING:Enabled
   630.286275 s:  VX_ZONE_INIT:[tivxInitLocal:130] Initialization Done !!!
   630.286514 s:  VX_ZONE_INIT:[tivxHostInitLocal:86] Initialization Done for HOST !!!
network file: /opt/vision_apps/test_data/tivx/tidl_models/tidl_net_mobilenet_v1.bin
config  file: /opt/vision_apps/test_data/tivx/tidl_models/tidl_io_mobilenet_v1_1.bin
Iteration 0 of 1000000 ...


 =================================
 Demo : TIDL Object Classification
 =================================

 p: Print performance statistics

 x: Exit

 Enter Choice: p


Summary of CPU load,
====================

CPU: mpu1_0: TOTAL LOAD =   6.35 % ( HWI =   0. 0 %, SWI =   0. 0 % )
CPU: mcu2_0: TOTAL LOAD =   3. 0 % ( HWI =   0. 0 %, SWI =   0. 0 % )
CPU: mcu2_1: TOTAL LOAD =   3. 0 % ( HWI =   0. 0 %, SWI =   0. 0 % )
CPU:  c6x_1: TOTAL LOAD =   1. 0 % ( HWI =   0. 0 %, SWI =   0. 0 % )
CPU:  c6x_2: TOTAL LOAD =   0. 0 % ( HWI =   0. 0 %, SWI =   0. 0 % )
CPU:  c7x_1: TOTAL LOAD =   1. 0 % ( HWI =   0. 0 %, SWI =   0. 0 % )


HWA performance statistics,
===========================



DDR performance statistics,
===========================

DDR: READ  BW: AVG =    392 MB/s, PEAK =   6630 MB/s
DDR: WRITE BW: AVG =     34 MB/s, PEAK =   2808 MB/s
DDR: TOTAL BW: AVG =    426 MB/s, PEAK =   9438 MB/s


Detailed CPU performance/memory statistics,
===========================================

CPU: mcu2_0: TASK:           IPC_RX:   0. 0 %
CPU: mcu2_0: TASK:       REMOTE_SRV:   0. 0 %
CPU: mcu2_0: TASK:        LOAD_TEST:   0. 0 %
CPU: mcu2_0: TASK:       TIVX_CPU_0:   0. 0 %
CPU: mcu2_0: TASK:          TIVX_NF:   0. 0 %
CPU: mcu2_0: TASK:        TIVX_LDC1:   0. 0 %
CPU: mcu2_0: TASK:        TIVX_MSC1:   0. 0 %
CPU: mcu2_0: TASK:        TIVX_MSC2:   0. 0 %
CPU: mcu2_0: TASK:       TIVX_VISS1:   0. 0 %
CPU: mcu2_0: TASK:       TIVX_CAPT1:   0. 0 %
CPU: mcu2_0: TASK:       TIVX_CAPT2:   0. 0 %
CPU: mcu2_0: TASK:       TIVX_DISP1:   0. 3 %
CPU: mcu2_0: TASK:       TIVX_DISP2:   0. 0 %
CPU: mcu2_0: TASK:       TIVX_CSITX:   0. 0 %
CPU: mcu2_0: TASK:       TIVX_CAPT3:   0. 0 %
CPU: mcu2_0: TASK:       TIVX_CAPT4:   0. 0 %
CPU: mcu2_0: TASK:       TIVX_CAPT5:   0. 0 %
CPU: mcu2_0: TASK:       TIVX_CAPT6:   0. 0 %
CPU: mcu2_0: TASK:       TIVX_CAPT7:   0. 0 %
CPU: mcu2_0: TASK:       TIVX_CAPT8:   0. 0 %
CPU: mcu2_0: TASK:      TIVX_DISP_M:   0. 0 %
CPU: mcu2_0: TASK:      TIVX_DISP_M:   0. 0 %
CPU: mcu2_0: TASK:      TIVX_DISP_M:   0. 0 %
CPU: mcu2_0: TASK:      TIVX_DISP_M:   0. 0 %

CPU: mcu2_0: HEAP:   DDR_SHARED_MEM: size =   16777216 B, free =    4230912 B ( 25 % unused)
CPU: mcu2_0: HEAP:           L3_MEM: size =     262144 B, free =     261888 B ( 99 % unused)

CPU: mcu2_1: TASK:           IPC_RX:   0. 0 %
CPU: mcu2_1: TASK:       REMOTE_SRV:   0. 0 %
CPU: mcu2_1: TASK:        LOAD_TEST:   0. 0 %
CPU: mcu2_1: TASK:         TIVX_SDE:   0. 0 %
CPU: mcu2_1: TASK:         TIVX_DOF:   0. 0 %
CPU: mcu2_1: TASK:       TIVX_CPU_1:   0. 0 %
CPU: mcu2_1: TASK:      IPC_TEST_RX:   0. 0 %
CPU: mcu2_1: TASK:      IPC_TEST_TX:   0. 0 %
CPU: mcu2_1: TASK:      IPC_TEST_TX:   0. 0 %
CPU: mcu2_1: TASK:      IPC_TEST_TX:   0. 0 %
CPU: mcu2_1: TASK:      IPC_TEST_TX:   0. 0 %
CPU: mcu2_1: TASK:      IPC_TEST_TX:   0. 0 %

CPU: mcu2_1: HEAP:   DDR_SHARED_MEM: size =   16777216 B, free =   16773376 B ( 99 % unused)
CPU: mcu2_1: HEAP:           L3_MEM: size =     262144 B, free =     262144 B (100 % unused)

CPU:  c6x_1: TASK:           IPC_RX:   0. 0 %
CPU:  c6x_1: TASK:       REMOTE_SRV:   0. 0 %
CPU:  c6x_1: TASK:        LOAD_TEST:   0. 0 %
CPU:  c6x_1: TASK:         TIVX_CPU:   0. 0 %
CPU:  c6x_1: TASK:      IPC_TEST_RX:   0. 0 %
CPU:  c6x_1: TASK:      IPC_TEST_TX:   0. 0 %
CPU:  c6x_1: TASK:      IPC_TEST_TX:   0. 0 %
CPU:  c6x_1: TASK:      IPC_TEST_TX:   0. 0 %
CPU:  c6x_1: TASK:      IPC_TEST_TX:   0. 0 %
CPU:  c6x_1: TASK:      IPC_TEST_TX:   0. 0 %

CPU:  c6x_1: HEAP:   DDR_SHARED_MEM: size =   16777216 B, free =   16773376 B ( 99 % unused)
CPU:  c6x_1: HEAP:           L2_MEM: size =     229376 B, free =     229376 B (100 % unused)
CPU:  c6x_1: HEAP:  DDR_SCRATCH_MEM: size =   50331648 B, free =   50331648 B ( 14 % unused)

CPU:  c6x_2: TASK:           IPC_RX:   0. 0 %
CPU:  c6x_2: TASK:       REMOTE_SRV:   0. 0 %
CPU:  c6x_2: TASK:        LOAD_TEST:   0. 0 %
CPU:  c6x_2: TASK:         TIVX_CPU:   0. 0 %
CPU:  c6x_2: TASK:      IPC_TEST_RX:   0. 0 %
CPU:  c6x_2: TASK:      IPC_TEST_TX:   0. 0 %
CPU:  c6x_2: TASK:      IPC_TEST_TX:   0. 0 %
CPU:  c6x_2: TASK:      IPC_TEST_TX:   0. 0 %
CPU:  c6x_2: TASK:      IPC_TEST_TX:   0. 0 %
CPU:  c6x_2: TASK:      IPC_TEST_TX:   0. 0 %

CPU:  c6x_2: HEAP:   DDR_SHARED_MEM: size =   16777216 B, free =   16773376 B ( 99 % unused)
CPU:  c6x_2: HEAP:           L2_MEM: size =     229376 B, free =     229376 B (100 % unused)
CPU:  c6x_2: HEAP:  DDR_SCRATCH_MEM: size =   50331648 B, free =   50331648 B ( 14 % unused)

CPU:  c7x_1: TASK:           IPC_RX:   0. 0 %
CPU:  c7x_1: TASK:       REMOTE_SRV:   0. 0 %
CPU:  c7x_1: TASK:        LOAD_TEST:   0. 0 %
CPU:  c7x_1: TASK:      TIVX_CPU_PR:   0.22 %
CPU:  c7x_1: TASK:      TIVX_CPU_PR:   0. 0 %
CPU:  c7x_1: TASK:      TIVX_CPU_PR:   0. 0 %
CPU:  c7x_1: TASK:      TIVX_CPU_PR:   0. 0 %
CPU:  c7x_1: TASK:      TIVX_CPU_PR:   0. 0 %
CPU:  c7x_1: TASK:      TIVX_CPU_PR:   0. 0 %
CPU:  c7x_1: TASK:      TIVX_CPU_PR:   0. 0 %
CPU:  c7x_1: TASK:      TIVX_CPU_PR:   0. 0 %
CPU:  c7x_1: TASK:      IPC_TEST_RX:   0. 0 %
CPU:  c7x_1: TASK:      IPC_TEST_TX:   0. 0 %
CPU:  c7x_1: TASK:      IPC_TEST_TX:   0. 0 %
CPU:  c7x_1: TASK:      IPC_TEST_TX:   0. 0 %
CPU:  c7x_1: TASK:      IPC_TEST_TX:   0. 0 %
CPU:  c7x_1: TASK:      IPC_TEST_TX:   0. 0 %

CPU:  c7x_1: HEAP:   DDR_SHARED_MEM: size =  268435456 B, free =  243593728 B ( 10 % unused)
CPU:  c7x_1: HEAP:           L3_MEM: size =    8159232 B, free =          0 B (  0 % unused)
CPU:  c7x_1: HEAP:           L2_MEM: size =     458752 B, free =     458752 B (100 % unused)
CPU:  c7x_1: HEAP:           L1_MEM: size =      16384 B, free =          0 B (  0 % unused)
CPU:  c7x_1: HEAP:  DDR_SCRATCH_MEM: size =  402653184 B, free =  402646784 B (  3 % unused)


GRAPH:   app_tidl_graph (#nodes =   1, #executions =      2)
 NODE:       DSP_C7-1:                 TIDLNode: avg =   1969 usecs, min/max =   1350 /   2588 usecs, #executions =          2

GRAPH:          Display (#nodes =   1, #executions =      2)
 NODE:       DISPLAY1:              DisplayNode: avg = 125200 usecs, min/max = 119309 / 131091 usecs, #executions =          2
 
 PERF:           FILEIO: avg =  61711 usecs, min/max =  61203 /  62219 usecs, #executions =          2
 PERF:             DRAW: avg =  59367 usecs, min/max =  52065 /  66669 usecs, #executions =          2
 PERF:            TOTAL: avg = 252466 usecs, min/max = 249845 / 255088 usecs, #executions =          2

 PERF:            TOTAL:    3.96 FPS

FPS 为3.96。 看起来有些东西、但面板是黑色的。

请帮助我调试这种情况。

谢谢

Michael  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我今天测量的 DSI txclk 大约为440~443 MHz、但数据通道上没有。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Jay Sun、

    您只能在运行某些示例时获取数据。 因此、请仅在运行示例后检查数据通道。  

    您是否在调试模式下运行上述示例? 因为我看到大多数节点在非实时模式下的性能。 FileIO 花费61.8ms、消耗60ms、显示250ms。  这可能是图形性能非常低的原因。  

    您的电路板上是否有单摄像头或多摄像头示例? 然后、您可以尝试运行其中一个摄像头应用程序吗?  

    此致、

    Brijesh

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    是的、我在调试模式下运行示例。

    在运行 run_app_tidl.sh 时测量了 DSI txclk 和数据通道。

    我今天刚提出了多凸轮、明天就要试一下。  

    非常感谢你的帮助。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我运行分辨率为1080x1920的多摄像头示例、但面板上没有显示任何内容。

    马赛克输出00000000_1080x190.YUV

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Jay Sun、

    根据上面的时序信息、您似乎 在尝试以63fps (2080x1135x62.2)获得1080p 分辨率。 ~= 146.94MHz)、您能否确认这是否正确?  

    对于此分辨率和 fps、您需要至少885Mbps 的信道速度。 (2080x1135x62.23x24/4 ~= 881Mbps)。 但您似乎只是将通道带设置为390Mbps 至450Mbps (在 dphyTxRate 中、0xE << 5 | 0xE)。 您可以尝试将通道速度提高到 UB941中配置的速度吗?  

    此致、

    Brijesh

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我尝试使用 (水平) 1080 x (垂直) 1920 (60fps)点亮垂直屏幕。

      (1080+48+80+32) x (1920+3+42+10) X60 = 1240x1975x60 = 146.94Mhz

    (0xE << 5 | 0xE)用于870至950Mbps 之间的通道频带、我说得对吗?

    谢谢

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    很抱歉我把它弄混了。 是的、分辨率、像素时钟和通道速度似乎是正确的。

    请尝试使用较低的分辨率吗? 实际上、您能否检查 SDK 中支持的原始分辨率1280x800是否正常工作?  

    此致、

    Brijesh

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    数据通道信号在1280x800分辨率下看起来很好。

    推测、对于其余参数、我在1080x1920设置中将 dphyTxFbDiv 修改为0x16F。  

    即使 没有启用 PATGEN、启动后面板也会自动显示测试图形、并且我无法禁用它。  

    它是 示波器上的 DSI 数据通道信号。

    e2e.ti.com/.../20220629_5F00_185606_5F00_1.mp4

    在运行多摄像头示例时

    #FYI、ub941设置

    uint8_t Ub941Ub925Config[][4] = {
    #if 1
    {0x16, 0x01, 0x02, 0x60},//Disable DSI
    {0x16, 0x01, 0x08, 0x5},//Reset Reg
    #endif
    {0x16, 0x06, 0x00, 0x5},
    
    {0x16, 0x1E, 0x01, 0x5},//Select port0
    {0x16, 0x4F, 0x8C, 0x5},//DSI Continuous CLK/4 Lanes
    {0x16, 0x5B, 0x0B, 0x5},//Dual mode "MUST"
    
    {0x16, 0x03, 0x9A, 0x5},//I2C pass through
    {0x2C, 0x1E, 0x30, 0x5},
    {0x2C, 0x20, 0x03, 0x5},
    
    {0x16, 0x01, 0x00, 0x5},//enable DSI
    };

    谢谢

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
    [引用 userid="487798" URL"~/support/processors-group/processors/f/processors-forum/1112916/tda4vm-tda4vm-dSI-with -1080x1920-resolution-dote-not-work /4127229#4127229"]数据通道信号在1280x800[引用]的分辨率下看起来不错。

    这是很好的了解。

    [引用 userid="487798" URL"~/support/processors-group/processors/f/processors-forum/1112916/tda4vm-tda4vm-dSI-with -1080x1920分辨率-剂量-非工作/4127229#4127229"]

    推测、对于其余参数、我在1080x1920设置中将 dphyTxFbDiv 修改为0x16F。  

    即使 没有启用 PATGEN、启动后面板也会自动显示测试图形、并且我无法禁用它。  

    [/报价]

    不确定这些颜色图案的来源。 串行器或解串器中是否启用了某个功能? 是否可以检查两者的配置?

    但从 DSI 的角度来看、您似乎获得了一些有效的数据输出。 您可以尝试运行一些演示来检查输出吗?  

    此致、

    Brijesh

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    这是如此的毛。 我禁用  UB941 并复位 UB941和 UB948的所有寄存器、但启用 UB941后会显示颜色模式。

    这些颜色模式是否可能来自 DRA829?

    谢谢

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    顺便说一下、从 UB941寄存器返回的 DSI 数据类型为0x3E、这是正确的。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
    [引用 userid="487798" URL"~/support/processors-group/processors/f/processors-forum/1112916/tda4vm-tda4vm-dSI-with -1080x1920-resolution -dote-no-work /4128335#4128335"]这些颜色模式是否可能来自 DRA829?[引用]

    否、默认情况下、DSS 无法发送此颜色模式。 您正在运行一些示例吗? 这种模式是否可能来自摄像头输入? 如果您没有运行任何示例、您是否看到此模式? 您是否可以尝试在覆盖管理器中更改背景颜色并查看输出中是否有任何更改?

    [引用 userid="487798" URL"~/support/processors/group/processors/f/processors-forum/1112916/tda4vm-tda4vm-dsI-wing-1080x1920-resolution-dote-note-work /4128348#4128348"]顺便说一下、DSI 数据类型从 U941[引用的 U941]寄存器返回正确的 DSI 数据类型。

    这意味着 ub941正在正确识别输入流。

    此致、

    Brijesh

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    如果检测到时钟或数据类型等不匹配信号、则该测试模式来自面板控制器。

    现在、它在面板上有一些东西、但我无法对像素时钟进行更精细的调优、因为 DSI_PCLK_DIV 的范围相当有限。

    # ub941 reg dump、将0x19写入0x1f 并针对 pclk 返回0x9a=154MHz。

    #ub948 reg dump、将0x14写入0x1b 并为 pclk 返回0x93=147MHz。 它`s 接近目标 pclk (146.94MHz)。

    谢谢。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    这是一个视频计时示例。 现在一切都正常。

    顺便说一下、我指的是另一个线程、该线程说的是使用上限值进行 FbDiv 计算、但它仅适用于地面值。

    感谢您的支持。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    感谢 Jay Sun 关闭此机票。