This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TDA4VM:MCAN 实例 MCAN7和 MCAN9

Guru**** 1796780 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1102503/tda4vm-mcan-instances-mcan7-and-mcan9

器件型号:TDA4VM

我正在尝试在 MCU2_1主内核1) MCAN 7实例2) MCAN9实例上运行两个任务。

两个实例使用相同的参数进行初始化、然后等待清除中断以接收新的接收消息

当我先从 Canoe 发送 MCAN7消息、然后它运行正常、然后我尝试发送 MCAN9消息、MCAN 9会给出一些接收器错误、或者当我先从 Canoe 发送 MCAN9消息、然后它运行正常、然后我尝试发送 MCAN7消息、然后 MCAN 7会给出 一些接收器错误

/* ========================================================================== */
/*                 Header file inclusion                                      */
/* ========================================================================== */
#include <canReceive.h>
// #include <ti/kernel/freertos/FreeRTOS-LTS/FreeRTOS-Kernel/include/FreeRTOS.h>
// #include <ti/kernel/freertos/FreeRTOS-LTS/FreeRTOS-Kernel/include/semphr.h>
//#include <ti/osal/MutexP.h>


/* ========================================================================== */
/*                                Macros                                      */
/* ========================================================================== */
#define APP_ENABLE_UART_PRINT                    (0U)
#define APP_MCAN_STD_ID_FILT_START_ADDR          (0U)
#define APP_MCAN_STD_ID_FILTER_NUM               (1U)
#define APP_MCAN_EXT_ID_FILT_START_ADDR          (48U)
#define APP_MCAN_EXT_ID_FILTER_NUM               (1U)
#define APP_MCAN_TX_EVENT_START_ADDR             (100U)
#define APP_MCAN_TX_EVENT_SIZE                   (5U)
#define APP_MCAN_TX_BUFF_START_ADDR              (148U)
#define APP_MCAN_TX_BUFF_SIZE                    (5U)
#define APP_MCAN_TX_FIFO_SIZE                    (5U)
#define APP_MCAN_FIFO_0_START_ADDR               (548U)
#define APP_MCAN_FIFO_0_NUM                      (64U)
#define APP_MCAN_FIFO_1_START_ADDR               (748U)
#define APP_MCAN_FIFO_1_NUM                      (64U)
#define APP_MCAN_RX_BUFF_START_ADDR              (948U)
#define APP_MCAN_EXT_ID_AND_MASK                 (0x1FFFFFFFU)
#define MCAN_PSR_BO_BUS_OFF                      (1U)
#define CAN_FD_OP_ENABLE                         (0x1U)
#define BAUD_RATE_SWITCH_ENABLE                  (0x1U)
#define TRANSMIT_PAUSE_DISABLED                  (0x0U)
#define EDGE_FILTRING_DISABLED                   (0x0U)
#define PROTOCOL_EXCEP_HANDLE_ENABLE             (0x0U)
#define AUTOMATIC_RETRANSMISSION_DISABLED        (0x1U)
#define WAKEUP_REQUEST_ENABLE                    (0x1U)
#define AUTO_WAKEUP_ENABLE                       (0x1U)
#define EMULATION_ENABLE                         (0x1U)
#define EMULATION_FAST_ACK_DISABLED              (0x0U)
#define CLK_STOP_FAST_ACK_DISABLED               (0x0U)
#define START_VAL_MESG_RAM_WATCHDOG_CNTR         (0xFFU)
#define TRANS_DELAY_COMPENS_FILTER_WINDOW_LENGTH (0xAU)
#define TRANS_DELAY_COMPENS_OFFSET               (0x6U)
#define TRANS_DELAY_COMPENS_ENABLE               (0x1U)
#define BUS_MONITORING_MODE_DISABLED             (0x0U)
#define NORMAL_CAN_OPERATION                     (0x0U)
#define TIMESTAMP_CNTR_PRESCALER                 (0xFU)
#define TIMESTAMP_SOURCE_SELECTTION              (0x0U)
#define TIMEOUT_CNTR_DISABLED                    (0x0U)
#define START_VAL_TIMEOUT_DOWN_CNTR              (0xFFFFU)
#define REJECT_REMOTE_FRAME_STD_ENABLE           (0x1U) 
#define REJECT_REMOTE_FRAME_EXT_ENABLE           (0x1U)
#define REJECT_NONMATCHING_FRAME_EXT             (0x2U)
#define REJECT_NONMATCHING_FRAME_STD             (0x2U)
#define EXT_FILTER_TYPE_CLASSIC                  (0x2U)
#define EFEC_STORE_IN_RX_FIFO1                   (0x2U)
#define EFID1_RECEIVE_ALL_ID_FILTER_VAL          (0x0U)
#define EFID2_RECEIVE_ALL_ID_MASK_VAL            (0x0U)
#define STD_FILTER_TYPE_CLASSIC                  (0x2U)
#define SFEC_STORE_IN_RX_FIFO1                   (0x2U)
#define SFID1_RECEIVE_ALL_ID_FILTER_VAL          (0x0U)
#define SFID2_RECEIVE_ALL_ID_MASK_VAL            (0x0U)
#define NOMINAL_BR_PRESCALER                     (0x3U)
#define NOMINAL_TIMESEG1_BEFORE_SAMPLE_PNT       (0x1EU)
#define NOMINAL_TIMESEG2_AFTER_SAMPLE_PNT        (0x7U)
#define NOMINAL_SYNC_JUMP_WIDTH                  (0x8U)
#define DATA_BR_PRESCALER                        (0x3U)
#define DATA_TIMESEG1_BEFORE_SAMPLE_PNT          (0x6U)
#define DATA_TIMESEG2_AFTER_SAMPLE_PNT           (0x1U)
#define DATA_SYNC_JUMP_WIDTH                     (0x2U)
#define DEDICATED_TX_BUF_0                       (0U)
#define TX_FIFO_OPERATION                        (0U)
#define TX_EVENT_FIFO_WATERMARK_INTR_3           (3U)
#define RX_EVENT_FIFO_0_WATERMARK_INTR_3         (3U)
#define RX_FIFO_0_BLOCKING_MODE                  (0U)
#define RX_EVENT_FIFO_1_WATERMARK_INTR_3         (3U)
#define RX_FIFO_1_BLOCKING_MODE                  (0U)

//main domain r5 core
#define APP_MAIN_MCAN_7_INT0                (CSLR_R5FSS1_CORE0_INTR_MCAN7_MCANSS_MCAN_LVL_INT_0)
#define APP_MAIN_MCAN_7_INT1                (CSLR_R5FSS1_CORE0_INTR_MCAN7_MCANSS_MCAN_LVL_INT_1)
#define APP_MAIN_MCAN_7_TS_INT              (CSLR_R5FSS1_CORE0_INTR_MCAN7_MCANSS_EXT_TS_ROLLOVER_LVL_INT_0)
#define APP_MAIN_MCAN_9_INT0                (CSLR_R5FSS1_CORE0_INTR_MCAN9_MCANSS_MCAN_LVL_INT_0)
#define APP_MAIN_MCAN_9_INT1                (CSLR_R5FSS1_CORE0_INTR_MCAN9_MCANSS_MCAN_LVL_INT_1)
#define APP_MAIN_MCAN_9_TS_INT              (CSLR_R5FSS1_CORE0_INTR_MCAN9_MCANSS_EXT_TS_ROLLOVER_LVL_INT_0)

/* Print buffer character limit for prints- UART or CCS Console */
#define APP_PRINT_BUFFER_SIZE           (200U)
#define J721E_GPIO_GESI_CAN_STB_PIN     (0x003C)

/* ========================================================================== */
/*                            Global Variables                                */
/* ========================================================================== */

/* Data length Code(DLC) with respect to Data */
uint32_t          gMcanAppdataSize[16] ={
    0, 1, 2, 3, 4, 5, 6, 7, 8, 12, 16, 20, 24, 32, 48, 64
    };

/* CAN TX interrupt flag*/
volatile uint32_t gMcanIsrIntr0Flag = 1U;
/* CAN RX interrupt flag*/
volatile uint32_t gMcan7IsrIntr1Flag = 1U, gMcan9IsrIntr1Flag = 1U;
/* RX interrupt Status*/
volatile uint32_t gRxIntr1Status0    = 0U, gRxIntr1Status1    = 0U;;
/*Hold the CAN instance address */
//uint32_t gMcanModAddr[2];
/* Array of memory base address of CAN instances*/
static uint32_t gMcanMods[] =
    {
        CSL_MCAN7_MSGMEM_RAM_BASE,
        CSL_MCAN9_MSGMEM_RAM_BASE};

/* GPIO Driver board specific pin configuration structure */
GPIO_PinConfig gpioPinConfigs[] = {
    /* Output pin : CAN STB */
    J721E_GPIO_GESI_CAN_STB_PIN | GPIO_CFG_OUTPUT,
};

/* GPIO Driver call back functions */
GPIO_CallbackFxn gpioCallbackFunctions[] = {
    NULL};

/* GPIO Driver configuration structure */
GPIO_v0_Config GPIO_v0_config = {
    gpioPinConfigs,
    gpioCallbackFunctions,
    sizeof(gpioPinConfigs) / sizeof(GPIO_PinConfig),
    sizeof(gpioCallbackFunctions) / sizeof(GPIO_CallbackFxn),
    0,
};


  


/* ========================================================================== */
/*                 Global Function Declarations                             */
/* ========================================================================== */

extern Board_STATUS Board_moduleClockEnable(uint32_t moduleId);

/*******************************************************************************
 * Function Name		: canInstInit
 *
 * Description		    : Initialization of CAN parameter
 *
 * Arguments	        : None
 *
 * Return Values		: None
 *

 ******************************************************************************/
void canInstInit(uint8_t addressIdx)
{  

    int32_t configStatus = CSL_PASS;
    uint32_t mcanInstAddr;

    /* Do Pad Config for MCAN */
    padConfig_prcmEnable();

    /* MCAN Instance Base address selected */
    mcanInstAddr = gMcanMods[addressIdx];

    /* CrossBar Configuration */
    configStatus = mcanRegisterIsr(mcanInstAddr);
    if (CSL_PASS == configStatus)
    {
        consolePrintf("MCAN Register ISR Done..\n");
    }
    /* MCAN CAN Bittime, RX TX BUffer/FIFO, Global Filter Configuration */
    configStatus = mcanConfig(mcanInstAddr);

    if (CSL_PASS == configStatus)
    {
        consolePrintf("MCAN Configuration Done..\n");
    }

    /* Select Interrupt Line */
    MCAN_selectIntrLine(mcanInstAddr,
                        MCAN_INTR_MASK_ALL,
                        MCAN_INTR_LINE_NUM_1);

}

/*******************************************************************************
 * Function Name		: padConfig_prcmEnable
 *
 * Description		    : Pad configuration , Pin Mux configuration
 *
 * Arguments	        : None
 *
 * Return Values		: None

 ******************************************************************************/
void padConfig_prcmEnable()
{
    Board_STATUS boardStatus;

    /* MCAN 7 Module clocl Enable*/
    Board_moduleClockEnable(TISCI_DEV_MCAN7);
    /* MCAN 9 Module clocl Enable*/
    Board_moduleClockEnable(TISCI_DEV_MCAN9);
    /* Pin mux for CAN STB used in GESI board */
    *(volatile unsigned int *)(0x0011c0f4) = 0x20007;
        /* Pinmux for MAIN_MCAN7 */
    *(volatile unsigned int *)(0x0011c074) = 0x60006;
    *(volatile unsigned int *)(0x0011c078) = 0x60006;
    /* Pinmux for MAIN_MCAN9 */
    *(volatile unsigned int *)(0x0011c0cc) = 0x60006;
    *(volatile unsigned int *)(0x0011c0d0) = 0x60006;

    /* GPIO initialization */
    GPIO_init();
    appLogPrintf("GPIO_init Done \n");

    /* Enable CAN transceivers by setting the STB pins */
    /* Enable the TCAN on GESI board.
     * Main Domain MCAN instances 4,5,6,7,9,11.
     */
    GPIO_write(0, GPIO_PIN_LOW);
}

/*******************************************************************************
 * Function Name		: mcanConfig
 *
 * Description		    : This function will configure MCAN module ,CAN frame format,
 *                        bit time, operation mode, memory config
 *
 * Arguments	        : None
 *
 * Return Values		: configuration status
 *******************************************************************************/
static int32_t mcanConfig(uint32_t mcanInstAddr)
{

    uint32_t                   fdoe;
    int32_t                    configStatus = CSL_PASS;
    MCAN_RevisionId            revId;
    MCAN_InitParams            initParams;
    MCAN_ConfigParams          configParams;
    MCAN_MsgRAMConfigParams    msgRAMConfigParams;
    MCAN_StdMsgIDFilterElement stdFiltelem;
    MCAN_ExtMsgIDFilterElement extFiltelem;
    MCAN_BitTimingParams       bitTimes;

    /* Initialize MCAN Init params */
    initParams.fdMode          = CAN_FD_OP_ENABLE;
    initParams.brsEnable       = BAUD_RATE_SWITCH_ENABLE;
    initParams.txpEnable       = TRANSMIT_PAUSE_DISABLED;
    initParams.efbi            = EDGE_FILTRING_DISABLED;
    initParams.pxhddisable     = PROTOCOL_EXCEP_HANDLE_ENABLE;
    initParams.darEnable       = AUTOMATIC_RETRANSMISSION_DISABLED;
    initParams.wkupReqEnable   = WAKEUP_REQUEST_ENABLE;
    initParams.autoWkupEnable  = AUTO_WAKEUP_ENABLE;
    initParams.emulationEnable = EMULATION_ENABLE;
    initParams.emulationFAck   = EMULATION_FAST_ACK_DISABLED;
    initParams.clkStopFAck     = CLK_STOP_FAST_ACK_DISABLED;
    initParams.wdcPreload      = START_VAL_MESG_RAM_WATCHDOG_CNTR;
    initParams.tdcEnable       = TRANS_DELAY_COMPENS_ENABLE;
    initParams.tdcConfig.tdcf  = TRANS_DELAY_COMPENS_FILTER_WINDOW_LENGTH;
    initParams.tdcConfig.tdco  = TRANS_DELAY_COMPENS_OFFSET;

    /* Initialize MCAN Config params */
    configParams.monEnable         = BUS_MONITORING_MODE_DISABLED;
    configParams.asmEnable         = NORMAL_CAN_OPERATION;
    configParams.tsPrescalar       = TIMESTAMP_CNTR_PRESCALER;
    configParams.tsSelect          = TIMESTAMP_SOURCE_SELECTTION;
    configParams.timeoutSelect     = MCAN_TIMEOUT_SELECT_CONT;
    configParams.timeoutPreload    = START_VAL_TIMEOUT_DOWN_CNTR;
    configParams.timeoutCntEnable  = TIMEOUT_CNTR_DISABLED;
    configParams.filterConfig.rrfs = REJECT_REMOTE_FRAME_STD_ENABLE;
    configParams.filterConfig.rrfe = REJECT_REMOTE_FRAME_EXT_ENABLE;
    configParams.filterConfig.anfe = REJECT_NONMATCHING_FRAME_EXT;
    configParams.filterConfig.anfs = REJECT_NONMATCHING_FRAME_STD;
    
    /* Initialize Message RAM Sections Configuration Parameters */
    msgRAMConfigParams.flssa                = APP_MCAN_STD_ID_FILT_START_ADDR;
    msgRAMConfigParams.lss                  = APP_MCAN_STD_ID_FILTER_NUM;
    msgRAMConfigParams.flesa                = APP_MCAN_EXT_ID_FILT_START_ADDR;
    msgRAMConfigParams.lse                  = APP_MCAN_EXT_ID_FILTER_NUM;

    msgRAMConfigParams.txStartAddr          = APP_MCAN_TX_BUFF_START_ADDR;
    msgRAMConfigParams.txBufNum             = DEDICATED_TX_BUF_0;
    msgRAMConfigParams.txFIFOSize           = APP_MCAN_TX_FIFO_SIZE;
    msgRAMConfigParams.txBufMode            = TX_FIFO_OPERATION;
    msgRAMConfigParams.txBufElemSize        = MCAN_ELEM_SIZE_64BYTES;
    msgRAMConfigParams.txEventFIFOStartAddr = APP_MCAN_TX_EVENT_START_ADDR;
    msgRAMConfigParams.txEventFIFOSize      = APP_MCAN_TX_BUFF_SIZE;
    msgRAMConfigParams.txEventFIFOWaterMark = TX_EVENT_FIFO_WATERMARK_INTR_3;

    msgRAMConfigParams.rxFIFO0startAddr     = APP_MCAN_FIFO_0_START_ADDR;
    msgRAMConfigParams.rxFIFO0size          = APP_MCAN_FIFO_0_NUM;
    msgRAMConfigParams.rxFIFO0waterMark     = RX_EVENT_FIFO_0_WATERMARK_INTR_3;
    msgRAMConfigParams.rxFIFO0OpMode        = RX_FIFO_0_BLOCKING_MODE;
    msgRAMConfigParams.rxFIFO1startAddr     = APP_MCAN_FIFO_1_START_ADDR;
    msgRAMConfigParams.rxFIFO1size          = APP_MCAN_FIFO_1_NUM;
    msgRAMConfigParams.rxFIFO1waterMark     = RX_EVENT_FIFO_1_WATERMARK_INTR_3;
    msgRAMConfigParams.rxFIFO1OpMode        = RX_FIFO_1_BLOCKING_MODE;
    msgRAMConfigParams.rxBufStartAddr       = APP_MCAN_RX_BUFF_START_ADDR;
    msgRAMConfigParams.rxBufElemSize        = MCAN_ELEM_SIZE_64BYTES;
    msgRAMConfigParams.rxFIFO0ElemSize      = MCAN_ELEM_SIZE_64BYTES;
    msgRAMConfigParams.rxFIFO1ElemSize      = MCAN_ELEM_SIZE_64BYTES;

    /* Initialize filter on IDs for incoming CAN frames */
    // change in configParams.filterConfig.anfs/anfe for accept/reject non matching frames 
    /* SFID2 = mask(0) to receive all IDs */
    stdFiltelem.sfid2 = SFID2_RECEIVE_ALL_ID_MASK_VAL;
    /* SFID1 = filter(0) to receive all IDs */
    stdFiltelem.sfid1 = SFID1_RECEIVE_ALL_ID_FILTER_VAL;
    /* Store in Rx FIFO 1 if filter matches */
    stdFiltelem.sfec  = SFEC_STORE_IN_RX_FIFO1; 
    /* EFID1 = filter, EFID2 = mask */
    stdFiltelem.sft   = STD_FILTER_TYPE_CLASSIC;

    /* EFID2 = mask(0) to receive all IDs */
    extFiltelem.efid2 = EFID2_RECEIVE_ALL_ID_MASK_VAL;
    /* EFID1 = filter(0) to receive all IDs */
    extFiltelem.efid1 = EFID1_RECEIVE_ALL_ID_FILTER_VAL;  
    /* Store in Rx FIFO 1 if filter matches */ 
    extFiltelem.efec  = EFEC_STORE_IN_RX_FIFO1;
    /* EFID1 = filter, EFID2 = mask */
    extFiltelem.eft   = EXT_FILTER_TYPE_CLASSIC;

    //500kbps nominal bit rate
    bitTimes.nomRatePrescalar   = NOMINAL_BR_PRESCALER;
    bitTimes.nomTimeSeg1        = NOMINAL_TIMESEG1_BEFORE_SAMPLE_PNT;
    bitTimes.nomTimeSeg2        = NOMINAL_TIMESEG2_AFTER_SAMPLE_PNT;
    bitTimes.nomSynchJumpWidth  = NOMINAL_SYNC_JUMP_WIDTH;

    //2Mbps data bit rate
    bitTimes.dataRatePrescalar  = DATA_BR_PRESCALER;
    bitTimes.dataTimeSeg1       = DATA_TIMESEG1_BEFORE_SAMPLE_PNT;
    bitTimes.dataTimeSeg2       = DATA_TIMESEG2_AFTER_SAMPLE_PNT;
    bitTimes.dataSynchJumpWidth = DATA_SYNC_JUMP_WIDTH;

    /* Get MCANSS Revision ID */
    MCAN_getRevisionId(mcanInstAddr, &revId);
    consolePrintf("gMcanMods:0x%x\n", mcanInstAddr);
    consolePrintf("MCANSS Revision ID:\n");
    consolePrintf("scheme:0x%x\n", revId.scheme);
    consolePrintf("Business Unit:0x%x\n", revId.bu);
    consolePrintf("Module ID:0x%x\n", revId.modId);
    consolePrintf("RTL Revision:0x%x\n", revId.rtlRev);
    consolePrintf("Major Revision:0x%x\n", revId.major);
    consolePrintf("Custom Revision:0x%x\n", revId.custom);
    consolePrintf("Minor Revision:0x%x\n", revId.minor); 

    /* Enable Auto wakeup */
    fdoe = MCAN_isFDOpEnable(mcanInstAddr);
    if ((uint32_t)TRUE == fdoe)
    {
        consolePrintf("CAN-FD operation is enabled through E-Fuse.\n");
    }
    else
    {
        consolePrintf("CAN-FD operation is disabled through E-Fuse.\n");
    }

    /* wait for memory initialization to happen */
    while (FALSE == MCAN_isMemInitDone(mcanInstAddr))
    {}
                 
    /* Put MCAN in SW initialization mode */
    MCAN_setOpMode(mcanInstAddr, MCAN_OPERATION_MODE_SW_INIT);
    while (MCAN_OPERATION_MODE_SW_INIT != MCAN_getOpMode(mcanInstAddr))
    {}

    /* Initialize MCAN module */
    MCAN_init(mcanInstAddr, &initParams);
    /* Configure MCAN module */
    MCAN_config(mcanInstAddr, &configParams);
    /* Configure Bit timings */
    MCAN_setBitTime(mcanInstAddr, &bitTimes);
    /* Set Extended ID Mask */
    MCAN_setExtIDAndMask(mcanInstAddr, APP_MCAN_EXT_ID_AND_MASK);
    /* Configure Message RAM Sections */
    MCAN_msgRAMConfig(mcanInstAddr, &msgRAMConfigParams);
    /* Configure Standard ID filter element */
    MCAN_addStdMsgIDFilter(mcanInstAddr, 0U, &stdFiltelem);
    /* Configure Extended ID filter element */
    MCAN_addExtMsgIDFilter(mcanInstAddr, 0U, &extFiltelem);

    /* Take MCAN out of the SW initialization mode */
    MCAN_setOpMode(mcanInstAddr, MCAN_OPERATION_MODE_NORMAL);
    while (MCAN_OPERATION_MODE_NORMAL != MCAN_getOpMode(mcanInstAddr))
    {}

    return configStatus;
}

/*******************************************************************************
 * Function Name		: mcanRegisterInterrupt
 *
 * Description		    : Enable CPU Interrrupts and Register ISR
 *
 *
 * Arguments	        : inttrupt vector num, Function address
 *                        void f(uintptr_t) implicitaly converted to void (*f)(uintptr_t)
 *
 * Return Values		: configStatus

 ******************************************************************************/
static int32_t mcanRegisterInterrupt(uint32_t intNum, void f(uintptr_t))
{
    int32_t configStatus = STW_SOK;
    OsalRegisterIntrParams_t    intrPrms;
    OsalInterruptRetCode_e      osalRetVal;
    HwiP_Handle                 hwiHandle = NULL;

    /* Enable CPU Interrupts and register ISR*/
    Osal_RegisterInterrupt_initParams(&intrPrms);
    /* Populate the interrupt parameters */
    intrPrms.corepacConfig.arg              = (uintptr_t) NULL;
    intrPrms.corepacConfig.isrRoutine       = f;
    intrPrms.corepacConfig.priority         = 0U;
    intrPrms.corepacConfig.corepacEventNum  = 0U;
    intrPrms.corepacConfig.intVecNum        = intNum;

    /* Register interrupts */
    osalRetVal = Osal_RegisterInterrupt(&intrPrms, &hwiHandle);
    if(OSAL_INT_SUCCESS != osalRetVal)
    {
        configStatus = CSL_EFAIL;
    }
    return configStatus;
}

/*******************************************************************************
 * Function Name		: mcanTSIntrISR
 *
 * Description		    : This is Interrupt Service Routine for MCAN TimeStamp interrupt
 *
 * Arguments	        : ptr
 *
 * Return Values		: None

 ******************************************************************************/

static void mcanTSIntrISR(uintptr_t arg)
{
    consolePrintf("Time Stamp overflow happened.\n");
}

/*******************************************************************************
 * Function Name		: mcanRegisterIsr
 *
 * Description		    : This API will register MCAN ISR
 *
 * Arguments	        : CAN instance(Bus) address
 *
 * Return Values		: Config Status

 ******************************************************************************/
static int32_t mcanRegisterIsr(uint32_t mcanInstAddr)
{
    int32_t configStatus = STW_SOK,configStatus1 = STW_SOK, configStatus2 = STW_SOK;

    /* Main MCAN Inst 9 */
    if(mcanInstAddr == CSL_MCAN9_MSGMEM_RAM_BASE)
    {
        consolePrintf("CrossBar/Interrupt Configuration for MCAN9.\n");
    configStatus2 = mcanRegisterInterrupt(APP_MAIN_MCAN_9_INT0, &mcanIntr0ISR_tx);
    configStatus2 += mcanRegisterInterrupt(APP_MAIN_MCAN_9_INT1, &mcanIntr1ISR_rx);
    configStatus2 += mcanRegisterInterrupt(APP_MAIN_MCAN_9_TS_INT, &mcanTSIntrISR);

    if (STW_SOK != configStatus2)
    {
        consolePrintf("CrossBar/Interrupt Configuration failed.\n");
    }
    else
    {
        consolePrintf("CrossBar/Interrupt Configuration done.\n");
    }
    return configStatus2;

    }
    else if(mcanInstAddr == CSL_MCAN7_MSGMEM_RAM_BASE)
    {
   /* Main MCAN Inst 9 */
   consolePrintf("CrossBar/Interrupt Configuration for MCAN7.\n");
    configStatus1 = mcanRegisterInterrupt(APP_MAIN_MCAN_7_INT0, &mcanIntr0ISR_tx);
    configStatus1 += mcanRegisterInterrupt(APP_MAIN_MCAN_7_INT1, &mcanIntr1ISR_rx);
    configStatus1 += mcanRegisterInterrupt(APP_MAIN_MCAN_7_TS_INT, &mcanTSIntrISR);

    if (STW_SOK != configStatus1)
    {
        consolePrintf("CrossBar/Interrupt Configuration failed.\n");
    }
    else
    {
        consolePrintf("CrossBar/Interrupt Configuration done.\n");
    }
    return configStatus1;    
    }

return configStatus;

}

/*******************************************************************************
 * Function Name		: canReceiveMsgs
 *
 * Description		    : Read Data from CAN BUS and store into local buffer rxMsg
 *
 * Arguments	        : local buffer to store received can frame
 *
 * Return Values		: Status

 ******************************************************************************/

int32_t canReceiveMsgs(MCAN_RxBufElement *rxMsg, uint8_t addressIdx)
{
    static uint32_t   rxFifo1Idx0  = 0U,rxFifo1Idx1  = 0U;
    int32_t              rxProcessStatus = CSL_PASS;
    MCAN_RxNewDataStatus newDataStatus;
    MCAN_ErrCntStatus    errCounter;
    MCAN_ProtocolStatus protStatus;
    MCAN_RxFIFOStatus fifoStatus0,fifoStatus1;
    volatile uint32_t mcanInstAddr0, mcanInstAddr1;
    MCAN_HighPriorityMsgInfo hpm;


if(addressIdx == 0)
{
    mcanInstAddr0 = gMcanMods[0];
    /* Enable Interrupts for RX */
    MCAN_enableIntr(mcanInstAddr0, MCAN_INTR_MASK_ALL, (uint32_t)TRUE);
    MCAN_enableIntr(mcanInstAddr0,
                    MCAN_INTR_SRC_RES_ADDR_ACCESS, (uint32_t)FALSE);

    /* Enable Interrupt Line */
    MCAN_enableIntrLine(mcanInstAddr0,
                        MCAN_INTR_LINE_NUM_1,
                        1U);
}
else
{
    mcanInstAddr1 = gMcanMods[1];
    /* Enable Interrupts for RX */
    MCAN_enableIntr(mcanInstAddr1, MCAN_INTR_MASK_ALL, (uint32_t)TRUE);
    MCAN_enableIntr(mcanInstAddr1,
                    MCAN_INTR_SRC_RES_ADDR_ACCESS, (uint32_t)FALSE);

    /* Enable Interrupt Line */
    MCAN_enableIntrLine(mcanInstAddr1,
                        MCAN_INTR_LINE_NUM_1,
                        1U);    
}
    // waiting for interrupt to be cleared by ISR for MCAN9
    consolePrintf(" wait for interrupt to be cleared by ISR\n");
        while (gMcan7IsrIntr1Flag && gMcan9IsrIntr1Flag)
        {}
    consolePrintf("gMcan9IsrIntr1Flag..%d\n",gMcan9IsrIntr1Flag);
    consolePrintf("gMcan7IsrIntr1Flag..%d\n",gMcan7IsrIntr1Flag);

   // if(mcanInstAddr == CSL_MCAN9_MSGMEM_RAM_BASE)
    if(gMcan9IsrIntr1Flag == 0)
    {
            gMcan9IsrIntr1Flag = 1U;

        /* Checking for Errors */
        MCAN_getErrCounters(mcanInstAddr1, &errCounter);
        consolePrintf("MCAN9 Error Counter ..recErrCnt =%d  canErrLogCnt =%d\n",errCounter.recErrCnt,errCounter.canErrLogCnt );
        MCAN_getHighPriorityMsgStatus(mcanInstAddr1, &hpm);
        consolePrintf("MCAN9 MCAN_getHighPriorityMsgStatus ..filterIdx =%d  filterList =%d\n",hpm.filterIdx,hpm.filterList );

        if ((0U == errCounter.recErrCnt) &&
            (0U == errCounter.canErrLogCnt))
        {
            MCAN_getNewDataStatus(mcanInstAddr1, &newDataStatus);
            MCAN_clearNewDataStatus(mcanInstAddr1, &newDataStatus);

            fifoStatus1.num = (uint32_t)MCAN_RX_FIFO_NUM_1;
            MCAN_getRxFIFOStatus(mcanInstAddr1, &fifoStatus1);
            //rxFifo1Idx1 = fifoStatus1.getIdx;
            consolePrintf("MCAN9 FIFO index num..%d\n",fifoStatus1.getIdx);
            consolePrintf("MCAN9 FIFO fillLvl..%d\n",fifoStatus1.fillLvl);

            MCAN_readMsgRam(mcanInstAddr1,
                        MCAN_MEM_TYPE_FIFO,
                        fifoStatus1.getIdx,
                        fifoStatus1.num,
                        rxMsg);
    
            // read out(drain) message from RXFIFO1
            MCAN_writeRxFIFOAck(mcanInstAddr1, fifoStatus1.num, fifoStatus1.getIdx);

            MCAN_getProtocolStatus(mcanInstAddr1, &protStatus);
            if (MCAN_PSR_BO_BUS_OFF == protStatus.busOffStatus)
            {
                consolePrintf("MCAN9 BUSOFF Error..\n");
            }
            // increment FIFO Index to store new message at RXFIFO1[rxFifo1Idx]

            consolePrintf("MCAN9 Rx Message Received\n");
        }
        else
        {
            consolePrintf("MCAN9 CSL_EFAIL\n");

            rxProcessStatus = CSL_EFAIL;
        }
    }
 //   if(mcanInstAddr == CSL_MCAN7_MSGMEM_RAM_BASE)
    else if(gMcan7IsrIntr1Flag == 0)
    {
        gMcan7IsrIntr1Flag = 1U;
         /* Checking for Errors */
        MCAN_getErrCounters(mcanInstAddr0, &errCounter);
        consolePrintf("MCAN7 Error Counter ..recErrCnt =%d  canErrLogCnt =%d\n",errCounter.recErrCnt,errCounter.canErrLogCnt );
        MCAN_getHighPriorityMsgStatus(mcanInstAddr1, &hpm);
        consolePrintf("MCAN9 MCAN_getHighPriorityMsgStatus ..filterIdx =%d  filterList =%d\n",hpm.filterIdx,hpm.filterList );

        if ((0U == errCounter.recErrCnt) &&
            (0U == errCounter.canErrLogCnt))
        {
            MCAN_getNewDataStatus(mcanInstAddr0, &newDataStatus);
            MCAN_clearNewDataStatus(mcanInstAddr0, &newDataStatus);

            fifoStatus0.num = (uint32_t)MCAN_RX_FIFO_NUM_1;
            MCAN_getRxFIFOStatus(mcanInstAddr0, &fifoStatus0);
           // rxFifo1Idx0 = fifoStatus0.getIdx;
            consolePrintf("MCAN7 FIFO index num..%d\n",fifoStatus0.getIdx);
            consolePrintf("MCAN7 FIFO fillLvl..%d\n",fifoStatus0.fillLvl);

            MCAN_readMsgRam(mcanInstAddr0,
                        MCAN_MEM_TYPE_FIFO,
                        fifoStatus0.getIdx,
                        fifoStatus0.num,
                        rxMsg);
    
            // read out(drain) message from RXFIFO1
            MCAN_writeRxFIFOAck(mcanInstAddr0, fifoStatus0.num, fifoStatus0.getIdx);

            MCAN_getProtocolStatus(mcanInstAddr0, &protStatus);
            if (MCAN_PSR_BO_BUS_OFF == protStatus.busOffStatus)
            {
                consolePrintf("MCAN7 BUSOFF Error..\n");
            }
            // increment FIFO Index to store new message at RXFIFO1[rxFifo1Idx]

            consolePrintf("MCAN7 Rx Message Received\n");
        }
        else
        {
            consolePrintf("MCAN7 CSL_EFAIL\n");

            rxProcessStatus = CSL_EFAIL;
        }
    }


    return rxProcessStatus;

}

/*******************************************************************************
 * Function Name		: mcanIntr0ISR_tx
 *
 * Description		    : This is Interrupt Service Routine for MCAN interrupt 0
 *                        and is invoked when CAN message transmission is completed
 * 
 * Arguments	        : Ptr
 *
 * Return Values		: None

 ******************************************************************************/

static void mcanIntr0ISR_tx(uintptr_t arg)
{
    uint32_t intrStatus;

    intrStatus = MCAN_getIntrStatus(gMcanMods[0]);
    MCAN_clearIntrStatus(gMcanMods[0], intrStatus);

    consolePrintf("\nInside MCAN Tx ISR. Intr Status : 0x%x", intrStatus);

    if (MCAN_INTR_SRC_TRANS_COMPLETE ==
        (intrStatus & MCAN_INTR_SRC_TRANS_COMPLETE))
    {
        gMcanIsrIntr0Flag = 0U;
        consolePrintf("\nTx flag cleared");
    }
}

/*******************************************************************************
 * Function Name		: mcanIntr1ISR_rx
 *
 * Description		    : This is Interrupt Service Routine for MCAN interrupt 1
 *                        and is invoked when CAN message received
 * 
 * Arguments	        : Ptr
 *
 * Return Values		: None

 ******************************************************************************/

static void mcanIntr1ISR_rx(uintptr_t arg)
{

    gRxIntr1Status0 = MCAN_getIntrStatus(gMcanMods[0]);
    MCAN_clearIntrStatus(gMcanMods[0], gRxIntr1Status0);
    consolePrintf("MCAN 7 Rx interrupt status= %d\n",gRxIntr1Status0);

    if ((MCAN_INTR_SRC_RX_FIFO1_NEW_MSG == (gRxIntr1Status0 & MCAN_INTR_SRC_RX_FIFO1_NEW_MSG)) 
    || (MCAN_INTR_SRC_RX_FIFO1_WATERMARK == (gRxIntr1Status0 & MCAN_INTR_SRC_RX_FIFO1_WATERMARK)) 
    || (MCAN_INTR_SRC_RX_FIFO1_FULL == (gRxIntr1Status0 & MCAN_INTR_SRC_RX_FIFO1_FULL))
    || (MCAN_INTR_SRC_RX_FIFO1_MSG_LOST == (gRxIntr1Status0 & MCAN_INTR_SRC_RX_FIFO1_MSG_LOST)))
    {
        consolePrintf("Rx MCAN7 interrupt flag cleared\n");
        gMcan7IsrIntr1Flag = 0U;
    }

    gRxIntr1Status1 = MCAN_getIntrStatus(gMcanMods[1]);
    MCAN_clearIntrStatus(gMcanMods[1], gRxIntr1Status1);
    consolePrintf("MCAN 9 Rx interrupt status= %d\n",gRxIntr1Status1);

    if ((MCAN_INTR_SRC_RX_FIFO1_NEW_MSG == (gRxIntr1Status1 & MCAN_INTR_SRC_RX_FIFO1_NEW_MSG)) 
    || (MCAN_INTR_SRC_RX_FIFO1_WATERMARK == (gRxIntr1Status1 & MCAN_INTR_SRC_RX_FIFO1_WATERMARK)) 
    || (MCAN_INTR_SRC_RX_FIFO1_FULL == (gRxIntr1Status1 & MCAN_INTR_SRC_RX_FIFO1_FULL))
    || (MCAN_INTR_SRC_RX_FIFO1_MSG_LOST == (gRxIntr1Status1 & MCAN_INTR_SRC_RX_FIFO1_MSG_LOST)))
    {
        consolePrintf("Rx MCAN9 interrupt flag cleared\n");

        gMcan9IsrIntr1Flag = 0U;
    }
}
/*******************************************************************************
 * Function Name		: consolePrintf
 *
 * Description		    : This is function for printing data on console.
 *
 * Arguments	        : String
 *

*****************************************************************************/
void consolePrintf(const char *pcString, ...)
{
    static char printBuffer[APP_PRINT_BUFFER_SIZE];
    va_list arguments;

    /* Start the varargs processing. */
    va_start(arguments, pcString);
    vsnprintf(printBuffer, sizeof(printBuffer), pcString, arguments);
    printf(printBuffer);
    /* End the varargs processing. */
    va_end(arguments);
}

/*******************************************************************************
 * Function Name		: mcanPrintRxMsg
 *
 * Description		    : This is function for printing Rx data on console.
 *
 * Arguments	        : Rx CAN buffer
 *
 * Return Values		: None

 ******************************************************************************/
void mcanPrintRxMsg(const MCAN_RxBufElement *rxMsg)
{
    uint32_t loopCnt;

    consolePrintf("\nMessage ID(hex): 0x%x", rxMsg->id);
    consolePrintf("\nMessage Remote Transmission Request: 0x%x", rxMsg->rtr);
    consolePrintf("\nMessage Extended Frame ID(0:11Bit ID/1:29bit ID): 0x%x",
                      rxMsg->xtd);
    consolePrintf("\nMessage Error State Indicator(0:Error Active/1:Error Passive): 0x%x",
                      rxMsg->esi);
    consolePrintf("\nMessage TimeStamp: 0x%x", rxMsg->rxts);
    consolePrintf("\nMessage Data Length Code: 0x%x", rxMsg->dlc);
    consolePrintf("\nMessage BRS: 0x%x", rxMsg->brs);
    consolePrintf("\nMessage CAN FD format: 0x%x", rxMsg->fdf);
    consolePrintf("\nMessage Filter Index: 0x%x", rxMsg->fidx);
    consolePrintf("\nMessage Accept Non-matching Frame: 0x%x", rxMsg->anmf);
    for (loopCnt = 0U; loopCnt < gMcanAppdataSize[rxMsg->dlc]; loopCnt++)
    {
        consolePrintf("\nMessage DataByte%d", loopCnt);
        consolePrintf(": 0x%x", rxMsg->data[loopCnt]);
    }
}

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Sandeep、

    您很可能不会为其中一个 CAN 实例启用中断。

    您在16上获得中断状态、这意味着 MCAN_IR 寄存器中的第4位已置位。 第4位对应于 RF1N、即"Rx FIFO 1新消息"、因此您将收到新消息、但仅是 ISR 未被触发。

    请检查调用 canReceiveMsgs()的逻辑,以及在 addressIdx 中传递什么内容。 这将解决您的问题。

    此致

    Karan

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Karan、

    addressIdx 是 gMcanMods[]数组和 canReceiveMsgs()的索引号此函数调用在两个任务中循环继续。

    如下所示。

     

    静态 appMain1 (*arg0*arg1)
      MCAN_TxBufElement txMsg;
      MCAN_RxBufElement rxMsg;
      int32_t rxStatus;
      TaskP_SLEEP (1000);
      consolePrintf ("\nTask1已创建。。。。");
      canInstInit (0);
      consolePrintf ("\nMCAN init done in appmain1..");
      TaskP_SLEEP (10);
      while (1)
      {
        rxStatus = canReceiveMsgs (&rxMsg、0);
        if (rxStatus == CSL_PASS)
        {
          consolePrintf ("\n########################################## ");
          consolePrintf ("\n 接收 MCAN7上的最后一条消息,并具有以下详细信息:");
           mcanPrintRxMsg (&rxMsg);
          //*将数据存储在 J1939缓冲器中*/
          j1939ListenForMessages (&rxMsg);
        }


        // 10mil 延迟
        TaskP_SLEEP (100);
      }

      appDeInit()
      

    静态 appMain2 (*arg0*arg1)
      MCAN_TxBufElement txMsg;
      MCAN_RxBufElement rxMsg;
      int32_t rxStatus;

      consolePrintf ("\nTask2已创建。。。。");
      canInstInit(1)
      consolePrintf ("\nMCAN init done in appmain2..");
      TaskP_SLEEP (10);
      while (1)
      {
        rxStatus = canReceiveMsgs (&rxMsg、1);
        if (rxStatus == CSL_PASS)
        {
          consolePrintf ("\n########################################## ");
          consolePrintf ("\n 接收 MCAN9上的最后一条消息,并具有以下详细信息:");
          mcanPrintRxMsg (&rxMsg);
            //将数据存储在 J1939缓冲器中
          j1939ListenForMessages (&rxMsg);
        }


        // 10mil 延迟
        TaskP_SLEEP (100);
      }

      appDeInit()