This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] AM5708:PCIe 双通道 PHY 和 USB3 PHY

Guru**** 1129470 points
Other Parts Discussed in Thread: AM5708
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1044059/am5708-pcie-x2-lane-phy-and-usb3-phy

器件型号:AM5708

您好、TI

   

在开发 AM5708的过程中,我有一些问题,希望得到解答。

在 am5708 PCIe x2通道模式下、我需要在 USB1中使用 USB3 phy、这是我从手册中获得的知识

2.当 am5708使用 USB1的 USB2 phy1 (USB_dm \ USB_DP)来实现 USB 功能时、能否使用 PCIe x2通道模式? 配置是否需要修改 dra7.dtsi 文件?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    大家好、有人在这里更新了吗?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    于  

    是的、当 PCIe 使用 SERDES 时、您可以在 USB 2.0模式下使用 USB1端口。 您将需要修改 dtsi 文件以确保两个 SERDES 都分配给 PCIe、USB1端口仅具有 USB2.0 PHY。  

    此致

    Jian

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    你好、Jian

     您能给我一个修改示例吗?

      我删除了 USB3 phy、内核痛 c

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    于  

    您能否向我发送您当前的 DTS 文件、我将尝试查看并提出建议。 我目前没有安装 AM57 SDK。 但可以查看您的、看看是否有明显的东西。  

    Jian

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好,Jian

     这是我的 dtsi 文件

    /*
     * Copyright (C) 2013 Texas Instruments Incorporated - http://www.ti.com/
     *
     * This program is free software; you can redistribute it and/or modify
     * it under the terms of the GNU General Public License version 2 as
     * published by the Free Software Foundation.
     * Based on "omap4.dtsi"
     */
    
    #include <dt-bindings/interrupt-controller/arm-gic.h>
    #include <dt-bindings/pinctrl/dra.h>
    
    #define MAX_SOURCES 400
    
    / {
    	#address-cells = <2>;
    	#size-cells = <2>;
    
    	compatible = "ti,dra7xx";
    	interrupt-parent = <&crossbar_mpu>;
    	chosen { };
    
    	aliases {
    		i2c0 = &i2c1;
    		i2c1 = &i2c2;
    		i2c2 = &i2c3;
    		i2c3 = &i2c4;
    		i2c4 = &i2c5;
    		serial0 = &uart1;
    		serial1 = &uart2;
    		serial2 = &uart3;
    		serial3 = &uart4;
    		serial4 = &uart5;
    		serial5 = &uart6;
    		serial6 = &uart7;
    		serial7 = &uart8;
    		serial8 = &uart9;
    		serial9 = &uart10;
    		ethernet0 = &cpsw_emac0;
    		ethernet1 = &cpsw_emac1;
    		d_can0 = &dcan1;
    		d_can1 = &dcan2;
    		spi0 = &qspi;
    	};
    
    	timer {
    		compatible = "arm,armv7-timer";
    		interrupts = <GIC_PPI 13 (GIC_CPU_MASK_SIMPLE(2) | IRQ_TYPE_LEVEL_LOW)>,
    			     <GIC_PPI 14 (GIC_CPU_MASK_SIMPLE(2) | IRQ_TYPE_LEVEL_LOW)>,
    			     <GIC_PPI 11 (GIC_CPU_MASK_SIMPLE(2) | IRQ_TYPE_LEVEL_LOW)>,
    			     <GIC_PPI 10 (GIC_CPU_MASK_SIMPLE(2) | IRQ_TYPE_LEVEL_LOW)>;
    		interrupt-parent = <&gic>;
    	};
    
    	gic: interrupt-controller@48211000 {
    		compatible = "arm,cortex-a15-gic";
    		interrupt-controller;
    		#interrupt-cells = <3>;
    		reg = <0x0 0x48211000 0x0 0x1000>,
    		      <0x0 0x48212000 0x0 0x1000>,
    		      <0x0 0x48214000 0x0 0x2000>,
    		      <0x0 0x48216000 0x0 0x2000>;
    		interrupts = <GIC_PPI 9 (GIC_CPU_MASK_SIMPLE(2) | IRQ_TYPE_LEVEL_HIGH)>;
    		interrupt-parent = <&gic>;
    	};
    
    	wakeupgen: interrupt-controller@48281000 {
    		compatible = "ti,omap5-wugen-mpu", "ti,omap4-wugen-mpu";
    		interrupt-controller;
    		#interrupt-cells = <3>;
    		reg = <0x0 0x48281000 0x0 0x1000>;
    		interrupt-parent = <&gic>;
    	};
    
    	cpus {
    		#address-cells = <1>;
    		#size-cells = <0>;
    
    		cpu0: cpu@0 {
    			device_type = "cpu";
    			compatible = "arm,cortex-a15";
    			reg = <0>;
    
    			operating-points-v2 = <&cpu0_opp_table>;
    
    			clocks = <&dpll_mpu_ck>;
    			clock-names = "cpu";
    
    			clock-latency = <300000>; /* From omap-cpufreq driver */
    
    			/* cooling options */
    			cooling-min-level = <0>;
    			cooling-max-level = <2>;
    			#cooling-cells = <2>; /* min followed by max */
    
    			vbb-supply = <&abb_mpu>;
    		};
    	};
    
    	cpu0_opp_table: opp_table0 {
    		compatible = "operating-points-v2-ti-cpu";
    		ti,syscon-efuse = <&scm_wkup 0x20c 0xf80000 19>;
    		ti,syscon-rev = <&scm_wkup 0x204>;
    
    		opp_nom@1000000000 {
    			opp-hz = /bits/ 64 <1000000000>;
    			opp-microvolt = <1060000 850000 1150000>,
    					<1060000 850000 1150000>;
    			opp-supported-hw = <0xFF 0x01>;
    			opp-suspend;
    		};
    
    		opp_od@1176000000 {
    			opp-hz = /bits/ 64 <1176000000>;
    			opp-microvolt = <1160000 885000 1160000>,
    					<1160000 885000 1160000>;
    
    			opp-supported-hw = <0xFF 0x02>;
    		};
    
    		opp_high@1500000000 {
    			opp-hz = /bits/ 64 <1500000000>;
    			opp-microvolt = <1210000 950000 1250000>,
    					<1210000 950000 1250000>;
    			opp-supported-hw = <0xFF 0x04>;
    		};
    	};
    
    	/*
    	 * The soc node represents the soc top level view. It is used for IPs
    	 * that are not memory mapped in the MPU view or for the MPU itself.
    	 */
    	soc {
    		compatible = "ti,omap-infra";
    		mpu {
    			compatible = "ti,omap5-mpu";
    			ti,hwmods = "mpu";
    		};
    	};
    
    	/*
    	 * XXX: Use a flat representation of the SOC interconnect.
    	 * The real OMAP interconnect network is quite complex.
    	 * Since it will not bring real advantage to represent that in DT for
    	 * the moment, just use a fake OCP bus entry to represent the whole bus
    	 * hierarchy.
    	 */
    	ocp {
    		compatible = "ti,dra7-l3-noc", "simple-bus";
    		#address-cells = <1>;
    		#size-cells = <1>;
    		ranges = <0x0 0x0 0x0 0xc0000000>;
    		ti,hwmods = "l3_main_1", "l3_main_2";
    		reg = <0x0 0x44000000 0x0 0x1000000>,
    		      <0x0 0x45000000 0x0 0x1000>;
    		interrupts-extended = <&crossbar_mpu GIC_SPI 4 IRQ_TYPE_LEVEL_HIGH>,
    				      <&wakeupgen GIC_SPI 10 IRQ_TYPE_LEVEL_HIGH>;
    
    		l4_cfg: l4@4a000000 {
    			compatible = "ti,dra7-l4-cfg", "simple-bus";
    			#address-cells = <1>;
    			#size-cells = <1>;
    			ranges = <0 0x4a000000 0x22c000>;
    
    			scm: scm@2000 {
    				compatible = "ti,dra7-scm-core", "simple-bus";
    				reg = <0x2000 0x2000>;
    				#address-cells = <1>;
    				#size-cells = <1>;
    				ranges = <0 0x2000 0x2000>;
    
    				scm_conf: scm_conf@0 {
    					compatible = "syscon", "simple-bus";
    					reg = <0x0 0x1400>;
    					#address-cells = <1>;
    					#size-cells = <1>;
    					ranges = <0 0x0 0x1400>;
    
    					pbias_regulator: pbias_regulator@e00 {
    						compatible = "ti,pbias-dra7", "ti,pbias-omap";
    						reg = <0xe00 0x4>;
    						syscon = <&scm_conf>;
    						pbias_mmc_reg: pbias_mmc_omap5 {
    							regulator-name = "pbias_mmc_omap5";
    							regulator-min-microvolt = <1800000>;
    							regulator-max-microvolt = <3300000>;
    						};
    					};
    
    					scm_conf_clocks: clocks {
    						#address-cells = <1>;
    						#size-cells = <0>;
    					};
    				};
    
    				dra7_pmx_core: pinmux@1400 {
    					compatible = "ti,dra7-padconf",
    						     "pinctrl-single";
    					reg = <0x1400 0x0468>;
    					#address-cells = <1>;
    					#size-cells = <0>;
    					#pinctrl-cells = <1>;
    					#interrupt-cells = <1>;
    					interrupt-controller;
    					pinctrl-single,register-width = <32>;
    					pinctrl-single,function-mask = <0x3fffffff>;
    				};
    
    				scm_conf1: scm_conf@1c04 {
    					compatible = "syscon";
    					reg = <0x1c04 0x0020>;
    				};
    
    				scm_conf_pcie: scm_conf@1c24 {
    					compatible = "syscon";
    					reg = <0x1c24 0x0024>;
    				};
    
    				sdma_xbar: dma-router@b78 {
    					compatible = "ti,dra7-dma-crossbar";
    					reg = <0xb78 0xfc>;
    					#dma-cells = <1>;
    					dma-requests = <205>;
    					ti,dma-safe-map = <0>;
    					dma-masters = <&sdma>;
    				};
    
    				edma_xbar: dma-router@c78 {
    					compatible = "ti,dra7-dma-crossbar";
    					reg = <0xc78 0x7c>;
    					#dma-cells = <2>;
    					dma-requests = <204>;
    					ti,dma-safe-map = <0>;
    					dma-masters = <&edma>;
    				};
    			};
    
    			cm_core_aon: cm_core_aon@5000 {
    				compatible = "ti,dra7-cm-core-aon";
    				reg = <0x5000 0x2000>;
    
    				cm_core_aon_clocks: clocks {
    					#address-cells = <1>;
    					#size-cells = <0>;
    				};
    
    				cm_core_aon_clockdomains: clockdomains {
    				};
    			};
    
    			cm_core: cm_core@8000 {
    				compatible = "ti,dra7-cm-core";
    				reg = <0x8000 0x3000>;
    
    				cm_core_clocks: clocks {
    					#address-cells = <1>;
    					#size-cells = <0>;
    				};
    
    				cm_core_clockdomains: clockdomains {
    				};
    			};
    		};
    
    		l4_wkup: l4@4ae00000 {
    			compatible = "ti,dra7-l4-wkup", "simple-bus";
    			#address-cells = <1>;
    			#size-cells = <1>;
    			ranges = <0 0x4ae00000 0x3f000>;
    
    			counter32k: counter@4000 {
    				compatible = "ti,omap-counter32k";
    				reg = <0x4000 0x40>;
    				ti,hwmods = "counter_32k";
    			};
    
    			prm: prm@6000 {
    				compatible = "ti,dra7-prm";
    				reg = <0x6000 0x3000>;
    				interrupts = <GIC_SPI 6 IRQ_TYPE_LEVEL_HIGH>;
    
    				prm_clocks: clocks {
    					#address-cells = <1>;
    					#size-cells = <0>;
    				};
    
    				prm_clockdomains: clockdomains {
    				};
    			};
    
    			scm_wkup: scm_conf@c000 {
    				compatible = "syscon";
    				reg = <0xc000 0x1000>;
    			};
    		};
    
    		axi@0 {
    			compatible = "simple-bus";
    			#size-cells = <1>;
    			#address-cells = <1>;
    			ranges = <0x51000000 0x51000000 0x3000
    				  0x0	     0x20000000 0x10000000>;
    			/**
    			 * To enable PCI endpoint mode, disable the pcie1_rc
    			 * node and enable pcie1_ep mode.
    			 */
    			pcie1_rc: pcie@51000000 {
    				reg = <0x51000000 0x2000>, <0x51002000 0x14c>, <0x1000 0x2000>;
    				reg-names = "rc_dbics", "ti_conf", "config";
    				interrupts = <0 232 0x4>, <0 233 0x4>;
    				#address-cells = <3>;
    				#size-cells = <2>;
    				device_type = "pci";
    				ranges = <0x81000000 0 0          0x03000 0 0x00010000
    					  0x82000000 0 0x20013000 0x13000 0 0xffed000>;
    				#interrupt-cells = <1>;
    				num-lanes = <1>;
    				linux,pci-domain = <0>;
    				ti,hwmods = "pcie1";
    				phys = <&pcie1_phy>;
    				phy-names = "pcie-phy0";
    				syscon-lane-conf = <&scm_conf 0x558>;
    				syscon-lane-sel = <&scm_conf_pcie 0x18>;
    				interrupt-map-mask = <0 0 0 7>;
    				interrupt-map = <0 0 0 1 &pcie1_intc 1>,
    						<0 0 0 2 &pcie1_intc 2>,
    						<0 0 0 3 &pcie1_intc 3>,
    						<0 0 0 4 &pcie1_intc 4>;
    				status = "disabled";
    				pcie1_intc: interrupt-controller {
    					interrupt-controller;
    					#address-cells = <0>;
    					#interrupt-cells = <1>;
    				};
    			};
    
    			pcie1_ep: pcie_ep@51000000 {
    				reg = <0x51000000 0x28>, <0x51002000 0x14c>, <0x51001000 0x28>, <0x1000 0x10000000>;
    				reg-names = "ep_dbics", "ti_conf", "ep_dbics2", "addr_space";
    				interrupts = <0 232 0x4>;
    				num-lanes = <1>;
    				num-ib-windows = <4>;
    				num-ob-windows = <16>;
    				ti,hwmods = "pcie1";
    				phys = <&pcie1_phy>;
    				phy-names = "pcie-phy0";
    				syscon-legacy-mode = <&scm_conf1 0x14 2>;
    				status = "disabled";
    			};
    		};
    
    		axi@1 {
    			compatible = "simple-bus";
    			#size-cells = <1>;
    			#address-cells = <1>;
    			ranges = <0x51800000 0x51800000 0x3000
    				  0x0	     0x30000000 0x10000000>;
    			status = "disabled";
    			pcie2_rc: pcie@51800000 {
    				reg = <0x51800000 0x2000>, <0x51802000 0x14c>, <0x1000 0x2000>;
    				reg-names = "rc_dbics", "ti_conf", "config";
    				interrupts = <0 355 0x4>, <0 356 0x4>;
    				#address-cells = <3>;
    				#size-cells = <2>;
    				device_type = "pci";
    				ranges = <0x81000000 0 0          0x03000 0 0x00010000
    					  0x82000000 0 0x30013000 0x13000 0 0xffed000>;
    				#interrupt-cells = <1>;
    				num-lanes = <1>;
    				linux,pci-domain = <1>;
    				ti,hwmods = "pcie2";
    				phys = <&pcie2_phy>;
    				phy-names = "pcie-phy0";
    				interrupt-map-mask = <0 0 0 7>;
    				interrupt-map = <0 0 0 1 &pcie2_intc 1>,
    						<0 0 0 2 &pcie2_intc 2>,
    						<0 0 0 3 &pcie2_intc 3>,
    						<0 0 0 4 &pcie2_intc 4>;
    				pcie2_intc: interrupt-controller {
    					interrupt-controller;
    					#address-cells = <0>;
    					#interrupt-cells = <1>;
    				};
    			};
    		};
    
    		ocmcram1: ocmcram@40300000 {
    			compatible = "mmio-sram";
    			reg = <0x40300000 0x80000>;
    			ranges = <0x0 0x40300000 0x80000>;
    			#address-cells = <1>;
    			#size-cells = <1>;
    			/*
    			 * This is a placeholder for an optional reserved
    			 * region for use by secure software. The size
    			 * of this region is not known until runtime so it
    			 * is set as zero to either be updated to reserve
    			 * space or left unchanged to leave all SRAM for use.
    			 * On HS parts that that require the reserved region
    			 * either the bootloader can update the size to
    			 * the required amount or the node can be overridden
    			 * from the board dts file for the secure platform.
    			 */
    			sram-hs@0 {
    				compatible = "ti,secure-ram";
    				reg = <0x0 0x0>;
    			};
    		};
    
    		/*
    		 * NOTE: ocmcram2 and ocmcram3 are not available on all
    		 * DRA7xx and AM57xx variants. Confirm availability in
    		 * the data manual for the exact part number in use
    		 * before enabling these nodes in the board dts file.
    		 */
    		ocmcram2: ocmcram@40400000 {
    			status = "disabled";
    			compatible = "mmio-sram";
    			reg = <0x40400000 0x100000>;
    			ranges = <0x0 0x40400000 0x100000>;
    			#address-cells = <1>;
    			#size-cells = <1>;
    		};
    
    		ocmcram3: ocmcram@40500000 {
    			status = "disabled";
    			compatible = "mmio-sram";
    			reg = <0x40500000 0x100000>;
    			ranges = <0x0 0x40500000 0x100000>;
    			#address-cells = <1>;
    			#size-cells = <1>;
    		};
    
    		bandgap: bandgap@4a0021e0 {
    			reg = <0x4a0021e0 0xc
    				0x4a00232c 0xc
    				0x4a002380 0x2c
    				0x4a0023C0 0x3c
    				0x4a002564 0x8
    				0x4a002574 0x50>;
    				compatible = "ti,dra752-bandgap";
    				interrupts = <GIC_SPI 121 IRQ_TYPE_LEVEL_HIGH>;
    				#thermal-sensor-cells = <1>;
    		};
    
    		dsp1_system: dsp_system@40d00000 {
    			compatible = "syscon";
    			reg = <0x40d00000 0x100>;
    		};
    
    		dra7_iodelay_core: padconf@4844a000 {
    			compatible = "ti,dra7-iodelay";
    			reg = <0x4844a000 0x0d1c>;
    			#address-cells = <1>;
    			#size-cells = <0>;
    			#pinctrl-cells = <2>;
    		};
    
    		sdma: dma-controller@4a056000 {
    			compatible = "ti,omap4430-sdma";
    			reg = <0x4a056000 0x1000>;
    			interrupts = <GIC_SPI 7 IRQ_TYPE_LEVEL_HIGH>,
    				     <GIC_SPI 8 IRQ_TYPE_LEVEL_HIGH>,
    				     <GIC_SPI 9 IRQ_TYPE_LEVEL_HIGH>,
    				     <GIC_SPI 10 IRQ_TYPE_LEVEL_HIGH>;
    			#dma-cells = <1>;
    			dma-channels = <32>;
    			dma-requests = <127>;
    		};
    
    		edma: edma@43300000 {
    			compatible = "ti,edma3-tpcc";
    			ti,hwmods = "tpcc";
    			reg = <0x43300000 0x100000>;
    			reg-names = "edma3_cc";
    			interrupts = <GIC_SPI 361 IRQ_TYPE_LEVEL_HIGH>,
    				     <GIC_SPI 360 IRQ_TYPE_LEVEL_HIGH>,
    				     <GIC_SPI 359 IRQ_TYPE_LEVEL_HIGH>;
    			interrupt-names = "edma3_ccint", "edma3_mperr",
    					  "edma3_ccerrint";
    			dma-requests = <64>;
    			#dma-cells = <2>;
    
    			ti,tptcs = <&edma_tptc0 7>, <&edma_tptc1 0>;
    
    			/*
    			 * memcpy is disabled, can be enabled with:
    			 * ti,edma-memcpy-channels = <20 21>;
    			 * for example. Note that these channels need to be
    			 * masked in the xbar as well.
    			 */
    		};
    
    		edma_tptc0: tptc@43400000 {
    			compatible = "ti,edma3-tptc";
    			ti,hwmods = "tptc0";
    			reg =	<0x43400000 0x100000>;
    			interrupts = <GIC_SPI 370 IRQ_TYPE_LEVEL_HIGH>;
    			interrupt-names = "edma3_tcerrint";
    		};
    
    		edma_tptc1: tptc@43500000 {
    			compatible = "ti,edma3-tptc";
    			ti,hwmods = "tptc1";
    			reg =	<0x43500000 0x100000>;
    			interrupts = <GIC_SPI 371 IRQ_TYPE_LEVEL_HIGH>;
    			interrupt-names = "edma3_tcerrint";
    		};
    
    		gpio1: gpio@4ae10000 {
    			compatible = "ti,omap4-gpio";
    			reg = <0x4ae10000 0x200>;
    			interrupts = <GIC_SPI 24 IRQ_TYPE_LEVEL_HIGH>;
    			ti,hwmods = "gpio1";
    			gpio-controller;
    			#gpio-cells = <2>;
    			interrupt-controller;
    			#interrupt-cells = <2>;
    		};
    
    		gpio2: gpio@48055000 {
    			compatible = "ti,omap4-gpio";
    			reg = <0x48055000 0x200>;
    			interrupts = <GIC_SPI 25 IRQ_TYPE_LEVEL_HIGH>;
    			ti,hwmods = "gpio2";
    			gpio-controller;
    			#gpio-cells = <2>;
    			interrupt-controller;
    			#interrupt-cells = <2>;
    		};
    
    		gpio3: gpio@48057000 {
    			compatible = "ti,omap4-gpio";
    			reg = <0x48057000 0x200>;
    			interrupts = <GIC_SPI 26 IRQ_TYPE_LEVEL_HIGH>;
    			ti,hwmods = "gpio3";
    			gpio-controller;
    			#gpio-cells = <2>;
    			interrupt-controller;
    			#interrupt-cells = <2>;
    		};
    
    		gpio4: gpio@48059000 {
    			compatible = "ti,omap4-gpio";
    			reg = <0x48059000 0x200>;
    			interrupts = <GIC_SPI 27 IRQ_TYPE_LEVEL_HIGH>;
    			ti,hwmods = "gpio4";
    			gpio-controller;
    			#gpio-cells = <2>;
    			interrupt-controller;
    			#interrupt-cells = <2>;
    		};
    
    		gpio5: gpio@4805b000 {
    			compatible = "ti,omap4-gpio";
    			reg = <0x4805b000 0x200>;
    			interrupts = <GIC_SPI 28 IRQ_TYPE_LEVEL_HIGH>;
    			ti,hwmods = "gpio5";
    			gpio-controller;
    			#gpio-cells = <2>;
    			interrupt-controller;
    			#interrupt-cells = <2>;
    		};
    
    		gpio6: gpio@4805d000 {
    			compatible = "ti,omap4-gpio";
    			reg = <0x4805d000 0x200>;
    			interrupts = <GIC_SPI 29 IRQ_TYPE_LEVEL_HIGH>;
    			ti,hwmods = "gpio6";
    			gpio-controller;
    			#gpio-cells = <2>;
    			interrupt-controller;
    			#interrupt-cells = <2>;
    		};
    
    		gpio7: gpio@48051000 {
    			compatible = "ti,omap4-gpio";
    			reg = <0x48051000 0x200>;
    			interrupts = <GIC_SPI 30 IRQ_TYPE_LEVEL_HIGH>;
    			ti,hwmods = "gpio7";
    			gpio-controller;
    			#gpio-cells = <2>;
    			interrupt-controller;
    			#interrupt-cells = <2>;
    		};
    
    		gpio8: gpio@48053000 {
    			compatible = "ti,omap4-gpio";
    			reg = <0x48053000 0x200>;
    			interrupts = <GIC_SPI 116 IRQ_TYPE_LEVEL_HIGH>;
    			ti,hwmods = "gpio8";
    			gpio-controller;
    			#gpio-cells = <2>;
    			interrupt-controller;
    			#interrupt-cells = <2>;
    		};
    
    		uart1: serial@4806a000 {
    			compatible = "ti,dra742-uart", "ti,omap4-uart";
    			reg = <0x4806a000 0x100>;
    			interrupts-extended = <&crossbar_mpu GIC_SPI 67 IRQ_TYPE_LEVEL_HIGH>;
    			ti,hwmods = "uart1";
    			clock-frequency = <48000000>;
    			status = "disabled";
    			dmas = <&sdma_xbar 49>, <&sdma_xbar 50>;
    			dma-names = "tx", "rx";
    		};
    
    		uart2: serial@4806c000 {
    			compatible = "ti,dra742-uart", "ti,omap4-uart";
    			reg = <0x4806c000 0x100>;
    			interrupts = <GIC_SPI 68 IRQ_TYPE_LEVEL_HIGH>;
    			ti,hwmods = "uart2";
    			clock-frequency = <48000000>;
    			status = "disabled";
    			dmas = <&sdma_xbar 51>, <&sdma_xbar 52>;
    			dma-names = "tx", "rx";
    		};
    
    		uart3: serial@48020000 {
    			compatible = "ti,dra742-uart", "ti,omap4-uart";
    			reg = <0x48020000 0x100>;
    			interrupts = <GIC_SPI 69 IRQ_TYPE_LEVEL_HIGH>;
    			ti,hwmods = "uart3";
    			clock-frequency = <48000000>;
    			status = "disabled";
    			dmas = <&sdma_xbar 53>, <&sdma_xbar 54>;
    			dma-names = "tx", "rx";
    		};
    
    		uart4: serial@4806e000 {
    			compatible = "ti,dra742-uart", "ti,omap4-uart";
    			reg = <0x4806e000 0x100>;
    			interrupts = <GIC_SPI 65 IRQ_TYPE_LEVEL_HIGH>;
    			ti,hwmods = "uart4";
    			clock-frequency = <48000000>;
                            status = "disabled";
    			dmas = <&sdma_xbar 55>, <&sdma_xbar 56>;
    			dma-names = "tx", "rx";
    		};
    
    		uart5: serial@48066000 {
    			compatible = "ti,dra742-uart", "ti,omap4-uart";
    			reg = <0x48066000 0x100>;
    			interrupts = <GIC_SPI 100 IRQ_TYPE_LEVEL_HIGH>;
    			ti,hwmods = "uart5";
    			clock-frequency = <48000000>;
    			status = "disabled";
    			dmas = <&sdma_xbar 63>, <&sdma_xbar 64>;
    			dma-names = "tx", "rx";
    		};
    
    		uart6: serial@48068000 {
    			compatible = "ti,dra742-uart", "ti,omap4-uart";
    			reg = <0x48068000 0x100>;
    			interrupts = <GIC_SPI 101 IRQ_TYPE_LEVEL_HIGH>;
    			ti,hwmods = "uart6";
    			clock-frequency = <48000000>;
    			status = "disabled";
    			dmas = <&sdma_xbar 79>, <&sdma_xbar 80>;
    			dma-names = "tx", "rx";
    		};
    
    		uart7: serial@48420000 {
    			compatible = "ti,dra742-uart", "ti,omap4-uart";
    			reg = <0x48420000 0x100>;
    			interrupts = <GIC_SPI 218 IRQ_TYPE_LEVEL_HIGH>;
    			ti,hwmods = "uart7";
    			clock-frequency = <48000000>;
    			status = "disabled";
    		};
    
    		uart8: serial@48422000 {
    			compatible = "ti,dra742-uart", "ti,omap4-uart";
    			reg = <0x48422000 0x100>;
    			interrupts = <GIC_SPI 219 IRQ_TYPE_LEVEL_HIGH>;
    			ti,hwmods = "uart8";
    			clock-frequency = <48000000>;
    			status = "disabled";
    		};
    
    		uart9: serial@48424000 {
    			compatible = "ti,dra742-uart", "ti,omap4-uart";
    			reg = <0x48424000 0x100>;
    			interrupts = <GIC_SPI 220 IRQ_TYPE_LEVEL_HIGH>;
    			ti,hwmods = "uart9";
    			clock-frequency = <48000000>;
    			status = "disabled";
    		};
    
    		uart10: serial@4ae2b000 {
    			compatible = "ti,dra742-uart", "ti,omap4-uart";
    			reg = <0x4ae2b000 0x100>;
    			interrupts = <GIC_SPI 221 IRQ_TYPE_LEVEL_HIGH>;
    			ti,hwmods = "uart10";
    			clock-frequency = <48000000>;
    			status = "disabled";
    		};
    
    		mailbox1: mailbox@4a0f4000 {
    			compatible = "ti,omap4-mailbox";
    			reg = <0x4a0f4000 0x200>;
    			interrupts = <GIC_SPI 21 IRQ_TYPE_LEVEL_HIGH>,
    				     <GIC_SPI 135 IRQ_TYPE_LEVEL_HIGH>,
    				     <GIC_SPI 134 IRQ_TYPE_LEVEL_HIGH>;
    			ti,hwmods = "mailbox1";
    			#mbox-cells = <1>;
    			ti,mbox-num-users = <3>;
    			ti,mbox-num-fifos = <8>;
    			status = "disabled";
    		};
    
    		mailbox2: mailbox@4883a000 {
    			compatible = "ti,omap4-mailbox";
    			reg = <0x4883a000 0x200>;
    			interrupts = <GIC_SPI 237 IRQ_TYPE_LEVEL_HIGH>,
    				     <GIC_SPI 238 IRQ_TYPE_LEVEL_HIGH>,
    				     <GIC_SPI 239 IRQ_TYPE_LEVEL_HIGH>,
    				     <GIC_SPI 240 IRQ_TYPE_LEVEL_HIGH>;
    			ti,hwmods = "mailbox2";
    			#mbox-cells = <1>;
    			ti,mbox-num-users = <4>;
    			ti,mbox-num-fifos = <12>;
    			status = "disabled";
    		};
    
    		mailbox3: mailbox@4883c000 {
    			compatible = "ti,omap4-mailbox";
    			reg = <0x4883c000 0x200>;
    			interrupts = <GIC_SPI 241 IRQ_TYPE_LEVEL_HIGH>,
    				     <GIC_SPI 242 IRQ_TYPE_LEVEL_HIGH>,
    				     <GIC_SPI 243 IRQ_TYPE_LEVEL_HIGH>,
    				     <GIC_SPI 244 IRQ_TYPE_LEVEL_HIGH>;
    			ti,hwmods = "mailbox3";
    			#mbox-cells = <1>;
    			ti,mbox-num-users = <4>;
    			ti,mbox-num-fifos = <12>;
    			status = "disabled";
    		};
    
    		mailbox4: mailbox@4883e000 {
    			compatible = "ti,omap4-mailbox";
    			reg = <0x4883e000 0x200>;
    			interrupts = <GIC_SPI 245 IRQ_TYPE_LEVEL_HIGH>,
    				     <GIC_SPI 246 IRQ_TYPE_LEVEL_HIGH>,
    				     <GIC_SPI 247 IRQ_TYPE_LEVEL_HIGH>,
    				     <GIC_SPI 248 IRQ_TYPE_LEVEL_HIGH>;
    			ti,hwmods = "mailbox4";
    			#mbox-cells = <1>;
    			ti,mbox-num-users = <4>;
    			ti,mbox-num-fifos = <12>;
    			status = "disabled";
    		};
    
    		mailbox5: mailbox@48840000 {
    			compatible = "ti,omap4-mailbox";
    			reg = <0x48840000 0x200>;
    			interrupts = <GIC_SPI 249 IRQ_TYPE_LEVEL_HIGH>,
    				     <GIC_SPI 250 IRQ_TYPE_LEVEL_HIGH>,
    				     <GIC_SPI 251 IRQ_TYPE_LEVEL_HIGH>,
    				     <GIC_SPI 252 IRQ_TYPE_LEVEL_HIGH>;
    			ti,hwmods = "mailbox5";
    			#mbox-cells = <1>;
    			ti,mbox-num-users = <4>;
    			ti,mbox-num-fifos = <12>;
    			status = "disabled";
    		};
    
    		mailbox6: mailbox@48842000 {
    			compatible = "ti,omap4-mailbox";
    			reg = <0x48842000 0x200>;
    			interrupts = <GIC_SPI 253 IRQ_TYPE_LEVEL_HIGH>,
    				     <GIC_SPI 254 IRQ_TYPE_LEVEL_HIGH>,
    				     <GIC_SPI 255 IRQ_TYPE_LEVEL_HIGH>,
    				     <GIC_SPI 256 IRQ_TYPE_LEVEL_HIGH>;
    			ti,hwmods = "mailbox6";
    			#mbox-cells = <1>;
    			ti,mbox-num-users = <4>;
    			ti,mbox-num-fifos = <12>;
    			status = "disabled";
    		};
    
    		mailbox7: mailbox@48844000 {
    			compatible = "ti,omap4-mailbox";
    			reg = <0x48844000 0x200>;
    			interrupts = <GIC_SPI 257 IRQ_TYPE_LEVEL_HIGH>,
    				     <GIC_SPI 258 IRQ_TYPE_LEVEL_HIGH>,
    				     <GIC_SPI 259 IRQ_TYPE_LEVEL_HIGH>,
    				     <GIC_SPI 260 IRQ_TYPE_LEVEL_HIGH>;
    			ti,hwmods = "mailbox7";
    			#mbox-cells = <1>;
    			ti,mbox-num-users = <4>;
    			ti,mbox-num-fifos = <12>;
    			status = "disabled";
    		};
    
    		mailbox8: mailbox@48846000 {
    			compatible = "ti,omap4-mailbox";
    			reg = <0x48846000 0x200>;
    			interrupts = <GIC_SPI 261 IRQ_TYPE_LEVEL_HIGH>,
    				     <GIC_SPI 262 IRQ_TYPE_LEVEL_HIGH>,
    				     <GIC_SPI 263 IRQ_TYPE_LEVEL_HIGH>,
    				     <GIC_SPI 264 IRQ_TYPE_LEVEL_HIGH>;
    			ti,hwmods = "mailbox8";
    			#mbox-cells = <1>;
    			ti,mbox-num-users = <4>;
    			ti,mbox-num-fifos = <12>;
    			status = "disabled";
    		};
    
    		mailbox9: mailbox@4885e000 {
    			compatible = "ti,omap4-mailbox";
    			reg = <0x4885e000 0x200>;
    			interrupts = <GIC_SPI 265 IRQ_TYPE_LEVEL_HIGH>,
    				     <GIC_SPI 266 IRQ_TYPE_LEVEL_HIGH>,
    				     <GIC_SPI 267 IRQ_TYPE_LEVEL_HIGH>,
    				     <GIC_SPI 268 IRQ_TYPE_LEVEL_HIGH>;
    			ti,hwmods = "mailbox9";
    			#mbox-cells = <1>;
    			ti,mbox-num-users = <4>;
    			ti,mbox-num-fifos = <12>;
    			status = "disabled";
    		};
    
    		mailbox10: mailbox@48860000 {
    			compatible = "ti,omap4-mailbox";
    			reg = <0x48860000 0x200>;
    			interrupts = <GIC_SPI 269 IRQ_TYPE_LEVEL_HIGH>,
    				     <GIC_SPI 270 IRQ_TYPE_LEVEL_HIGH>,
    				     <GIC_SPI 271 IRQ_TYPE_LEVEL_HIGH>,
    				     <GIC_SPI 272 IRQ_TYPE_LEVEL_HIGH>;
    			ti,hwmods = "mailbox10";
    			#mbox-cells = <1>;
    			ti,mbox-num-users = <4>;
    			ti,mbox-num-fifos = <12>;
    			status = "disabled";
    		};
    
    		mailbox11: mailbox@48862000 {
    			compatible = "ti,omap4-mailbox";
    			reg = <0x48862000 0x200>;
    			interrupts = <GIC_SPI 273 IRQ_TYPE_LEVEL_HIGH>,
    				     <GIC_SPI 274 IRQ_TYPE_LEVEL_HIGH>,
    				     <GIC_SPI 275 IRQ_TYPE_LEVEL_HIGH>,
    				     <GIC_SPI 276 IRQ_TYPE_LEVEL_HIGH>;
    			ti,hwmods = "mailbox11";
    			#mbox-cells = <1>;
    			ti,mbox-num-users = <4>;
    			ti,mbox-num-fifos = <12>;
    			status = "disabled";
    		};
    
    		mailbox12: mailbox@48864000 {
    			compatible = "ti,omap4-mailbox";
    			reg = <0x48864000 0x200>;
    			interrupts = <GIC_SPI 277 IRQ_TYPE_LEVEL_HIGH>,
    				     <GIC_SPI 278 IRQ_TYPE_LEVEL_HIGH>,
    				     <GIC_SPI 279 IRQ_TYPE_LEVEL_HIGH>,
    				     <GIC_SPI 280 IRQ_TYPE_LEVEL_HIGH>;
    			ti,hwmods = "mailbox12";
    			#mbox-cells = <1>;
    			ti,mbox-num-users = <4>;
    			ti,mbox-num-fifos = <12>;
    			status = "disabled";
    		};
    
    		mailbox13: mailbox@48802000 {
    			compatible = "ti,omap4-mailbox";
    			reg = <0x48802000 0x200>;
    			interrupts = <GIC_SPI 379 IRQ_TYPE_LEVEL_HIGH>,
    				     <GIC_SPI 380 IRQ_TYPE_LEVEL_HIGH>,
    				     <GIC_SPI 381 IRQ_TYPE_LEVEL_HIGH>,
    				     <GIC_SPI 382 IRQ_TYPE_LEVEL_HIGH>;
    			ti,hwmods = "mailbox13";
    			#mbox-cells = <1>;
    			ti,mbox-num-users = <4>;
    			ti,mbox-num-fifos = <12>;
    			status = "disabled";
    		};
    
    		timer1: timer@4ae18000 {
    			compatible = "ti,omap5430-timer";
    			reg = <0x4ae18000 0x80>;
    			interrupts = <GIC_SPI 32 IRQ_TYPE_LEVEL_HIGH>;
    			ti,hwmods = "timer1";
    			ti,timer-alwon;
    		};
    
    		timer2: timer@48032000 {
    			compatible = "ti,omap5430-timer";
    			reg = <0x48032000 0x80>;
    			interrupts = <GIC_SPI 33 IRQ_TYPE_LEVEL_HIGH>;
    			ti,hwmods = "timer2";
    		};
    
    		timer3: timer@48034000 {
    			compatible = "ti,omap5430-timer";
    			reg = <0x48034000 0x80>;
    			interrupts = <GIC_SPI 34 IRQ_TYPE_LEVEL_HIGH>;
    			ti,hwmods = "timer3";
    		};
    
    		timer4: timer@48036000 {
    			compatible = "ti,omap5430-timer";
    			reg = <0x48036000 0x80>;
    			interrupts = <GIC_SPI 35 IRQ_TYPE_LEVEL_HIGH>;
    			ti,hwmods = "timer4";
    		};
    
    		timer5: timer@48820000 {
    			compatible = "ti,omap5430-timer";
    			reg = <0x48820000 0x80>;
    			interrupts = <GIC_SPI 36 IRQ_TYPE_LEVEL_HIGH>;
    			ti,hwmods = "timer5";
    		};
    
    		timer6: timer@48822000 {
    			compatible = "ti,omap5430-timer";
    			reg = <0x48822000 0x80>;
    			interrupts = <GIC_SPI 37 IRQ_TYPE_LEVEL_HIGH>;
    			ti,hwmods = "timer6";
    		};
    
    		timer7: timer@48824000 {
    			compatible = "ti,omap5430-timer";
    			reg = <0x48824000 0x80>;
    			interrupts = <GIC_SPI 38 IRQ_TYPE_LEVEL_HIGH>;
    			ti,hwmods = "timer7";
    		};
    
    		timer8: timer@48826000 {
    			compatible = "ti,omap5430-timer";
    			reg = <0x48826000 0x80>;
    			interrupts = <GIC_SPI 39 IRQ_TYPE_LEVEL_HIGH>;
    			ti,hwmods = "timer8";
    		};
    
    		timer9: timer@4803e000 {
    			compatible = "ti,omap5430-timer";
    			reg = <0x4803e000 0x80>;
    			interrupts = <GIC_SPI 40 IRQ_TYPE_LEVEL_HIGH>;
    			ti,hwmods = "timer9";
    		};
    
    		timer10: timer@48086000 {
    			compatible = "ti,omap5430-timer";
    			reg = <0x48086000 0x80>;
    			interrupts = <GIC_SPI 41 IRQ_TYPE_LEVEL_HIGH>;
    			ti,hwmods = "timer10";
    		};
    
    		timer11: timer@48088000 {
    			compatible = "ti,omap5430-timer";
    			reg = <0x48088000 0x80>;
    			interrupts = <GIC_SPI 42 IRQ_TYPE_LEVEL_HIGH>;
    			ti,hwmods = "timer11";
    		};
    
    		timer12: timer@4ae20000 {
    			compatible = "ti,omap5430-timer";
    			reg = <0x4ae20000 0x80>;
    			interrupts = <GIC_SPI 90 IRQ_TYPE_LEVEL_HIGH>;
    			ti,hwmods = "timer12";
    			ti,timer-alwon;
    			ti,timer-secure;
    		};
    
    		timer13: timer@48828000 {
    			compatible = "ti,omap5430-timer";
    			reg = <0x48828000 0x80>;
    			interrupts = <GIC_SPI 339 IRQ_TYPE_LEVEL_HIGH>;
    			ti,hwmods = "timer13";
    		};
    
    		timer14: timer@4882a000 {
    			compatible = "ti,omap5430-timer";
    			reg = <0x4882a000 0x80>;
    			interrupts = <GIC_SPI 340 IRQ_TYPE_LEVEL_HIGH>;
    			ti,hwmods = "timer14";
    		};
    
    		timer15: timer@4882c000 {
    			compatible = "ti,omap5430-timer";
    			reg = <0x4882c000 0x80>;
    			interrupts = <GIC_SPI 341 IRQ_TYPE_LEVEL_HIGH>;
    			ti,hwmods = "timer15";
    		};
    
    		timer16: timer@4882e000 {
    			compatible = "ti,omap5430-timer";
    			reg = <0x4882e000 0x80>;
    			interrupts = <GIC_SPI 342 IRQ_TYPE_LEVEL_HIGH>;
    			ti,hwmods = "timer16";
    		};
    
    		wdt2: wdt@4ae14000 {
    			compatible = "ti,omap3-wdt";
    			reg = <0x4ae14000 0x80>;
    			interrupts = <GIC_SPI 75 IRQ_TYPE_LEVEL_HIGH>;
    			ti,hwmods = "wd_timer2";
    		};
    
    		hwspinlock: spinlock@4a0f6000 {
    			compatible = "ti,omap4-hwspinlock";
    			reg = <0x4a0f6000 0x1000>;
    			ti,hwmods = "spinlock";
    			#hwlock-cells = <1>;
    		};
    
    		dmm@4e000000 {
    			compatible = "ti,dra7-dmm", "ti,omap5-dmm";
    			reg = <0x4e000000 0x800>;
    			interrupts = <GIC_SPI 108 IRQ_TYPE_LEVEL_HIGH>;
    			ti,hwmods = "dmm";
    		};
    
    		ipu1: ipu@58820000 {
    			compatible = "ti,dra7-ipu";
    			reg = <0x58820000 0x10000>;
    			reg-names = "l2ram";
    			ti,hwmods = "ipu1";
    			iommus = <&mmu_ipu1>;
    			ti,rproc-standby-info = <0x4a005520>;
    			status = "disabled";
    		};
    
    		ipu2: ipu@55020000 {
    			compatible = "ti,dra7-ipu";
    			reg = <0x55020000 0x10000>;
    			reg-names = "l2ram";
    			ti,hwmods = "ipu2";
    			iommus = <&mmu_ipu2>;
    			ti,rproc-standby-info = <0x4a008920>;
    			status = "disabled";
    		};
    
    		dsp1: dsp@40800000 {
    			compatible = "ti,dra7-dsp";
    			reg = <0x40800000 0x48000>,
    			      <0x40e00000 0x8000>,
    			      <0x40f00000 0x8000>;
    			reg-names = "l2ram", "l1pram", "l1dram";
    			ti,hwmods = "dsp1";
    			syscon-bootreg = <&scm_conf 0x55c>;
    			iommus = <&mmu0_dsp1>, <&mmu1_dsp1>;
    			ti,rproc-standby-info = <0x4a005420>;
    			status = "disabled";
    		};
    
    		i2c1: i2c@48070000 {
    			compatible = "ti,omap4-i2c";
    			reg = <0x48070000 0x100>;
    			interrupts = <GIC_SPI 51 IRQ_TYPE_LEVEL_HIGH>;
    			#address-cells = <1>;
    			#size-cells = <0>;
    			ti,hwmods = "i2c1";
    			status = "disabled";
    		};
    
    		i2c2: i2c@48072000 {
    			compatible = "ti,omap4-i2c";
    			reg = <0x48072000 0x100>;
    			interrupts = <GIC_SPI 52 IRQ_TYPE_LEVEL_HIGH>;
    			#address-cells = <1>;
    			#size-cells = <0>;
    			ti,hwmods = "i2c2";
    			status = "disabled";
    		};
    
    		i2c3: i2c@48060000 {
    			compatible = "ti,omap4-i2c";
    			reg = <0x48060000 0x100>;
    			interrupts = <GIC_SPI 56 IRQ_TYPE_LEVEL_HIGH>;
    			#address-cells = <1>;
    			#size-cells = <0>;
    			ti,hwmods = "i2c3";
    			status = "disabled";
    		};
    
    		i2c4: i2c@4807a000 {
    			compatible = "ti,omap4-i2c";
    			reg = <0x4807a000 0x100>;
    			interrupts = <GIC_SPI 57 IRQ_TYPE_LEVEL_HIGH>;
    			#address-cells = <1>;
    			#size-cells = <0>;
    			ti,hwmods = "i2c4";
    			status = "disabled";
    		};
    
    		i2c5: i2c@4807c000 {
    			compatible = "ti,omap4-i2c";
    			reg = <0x4807c000 0x100>;
    			interrupts = <GIC_SPI 55 IRQ_TYPE_LEVEL_HIGH>;
    			#address-cells = <1>;
    			#size-cells = <0>;
    			ti,hwmods = "i2c5";
    			status = "disabled";
    		};
    
    		mmc1: mmc@4809c000 {
    			compatible = "ti,dra7-hsmmc", "ti,omap4-hsmmc";
    			reg = <0x4809c000 0x400>;
    			interrupts = <GIC_SPI 78 IRQ_TYPE_LEVEL_HIGH>;
    			ti,hwmods = "mmc1";
    			ti,dual-volt;
    			ti,needs-special-reset;
    			dmas = <&sdma_xbar 61>, <&sdma_xbar 62>;
    			dma-names = "tx", "rx";
    			status = "disabled";
    			pbias-supply = <&pbias_mmc_reg>;
    			max-frequency = <192000000>;
    			sd-uhs-sdr104;
    			sd-uhs-sdr50;
    			sd-uhs-ddr50;
    			sd-uhs-sdr25;
    			sd-uhs-sdr12;
    		};
    
    		mmc2: mmc@480b4000 {
    			compatible = "ti,dra7-hsmmc", "ti,omap4-hsmmc";
    			reg = <0x480b4000 0x400>;
    			interrupts = <GIC_SPI 81 IRQ_TYPE_LEVEL_HIGH>;
    			ti,hwmods = "mmc2";
    			ti,needs-special-reset;
    			dmas = <&sdma_xbar 47>, <&sdma_xbar 48>;
    			dma-names = "tx", "rx";
    			status = "disabled";
    			max-frequency = <192000000>;
    			sd-uhs-sdr25;
    			sd-uhs-sdr12;
    			mmc-hs200-1_8v;
    			mmc-ddr-1_8v;
    		};
    
    		mmc3: mmc@480ad000 {
    			compatible = "ti,dra7-hsmmc", "ti,omap4-hsmmc";
    			reg = <0x480ad000 0x400>;
    			interrupts = <GIC_SPI 89 IRQ_TYPE_LEVEL_HIGH>;
    			ti,hwmods = "mmc3";
    			ti,needs-special-reset;
    			dmas = <&sdma_xbar 77>, <&sdma_xbar 78>;
    			dma-names = "tx", "rx";
    			status = "disabled";
    			/* Errata i887 limits max-frequency of MMC3 to 64 MHz */
    			max-frequency = <64000000>;
    			sd-uhs-sdr12;
    			sd-uhs-sdr25;
    			sd-uhs-sdr50;
    		};
    
    		mmc4: mmc@480d1000 {
    			compatible = "ti,dra7-hsmmc", "ti,omap4-hsmmc";
    			reg = <0x480d1000 0x400>;
    			interrupts = <GIC_SPI 91 IRQ_TYPE_LEVEL_HIGH>;
    			ti,hwmods = "mmc4";
    			ti,needs-special-reset;
    			dmas = <&sdma_xbar 57>, <&sdma_xbar 58>;
    			dma-names = "tx", "rx";
    			status = "disabled";
    			max-frequency = <192000000>;
    			sd-uhs-sdr12;
    			sd-uhs-sdr25;
    		};
    
    		mmu0_dsp1: mmu@40d01000 {
    			compatible = "ti,dra7-dsp-iommu";
    			reg = <0x40d01000 0x100>;
    			interrupts = <GIC_SPI 23 IRQ_TYPE_LEVEL_HIGH>;
    			ti,hwmods = "mmu0_dsp1";
    			#iommu-cells = <0>;
    			ti,syscon-mmuconfig = <&dsp1_system 0x0>;
    			status = "disabled";
    		};
    
    		mmu1_dsp1: mmu@40d02000 {
    			compatible = "ti,dra7-dsp-iommu";
    			reg = <0x40d02000 0x100>;
    			interrupts = <GIC_SPI 145 IRQ_TYPE_LEVEL_HIGH>;
    			ti,hwmods = "mmu1_dsp1";
    			#iommu-cells = <0>;
    			ti,syscon-mmuconfig = <&dsp1_system 0x1>;
    			status = "disabled";
    		};
    
    		mmu_ipu1: mmu@58882000 {
    			compatible = "ti,dra7-iommu";
    			reg = <0x58882000 0x100>;
    			interrupts = <GIC_SPI 395 IRQ_TYPE_LEVEL_HIGH>;
    			ti,hwmods = "mmu_ipu1";
    			#iommu-cells = <0>;
    			ti,iommu-bus-err-back;
    			status = "disabled";
    		};
    
    		mmu_ipu2: mmu@55082000 {
    			compatible = "ti,dra7-iommu";
    			reg = <0x55082000 0x100>;
    			interrupts = <GIC_SPI 396 IRQ_TYPE_LEVEL_HIGH>;
    			ti,hwmods = "mmu_ipu2";
    			#iommu-cells = <0>;
    			ti,iommu-bus-err-back;
    			status = "disabled";
    		};
    
    		pruss_soc_bus1: pruss_soc_bus@4b226000 {
    			compatible = "ti,am5728-pruss-soc-bus";
    			reg = <0x4b226000 0x2000>;
    			ti,hwmods = "pruss1";
    			#address-cells = <1>;
    			#size-cells = <1>;
    			ranges;
    			status = "disabled";
    
    			pruss1: pruss@4b200000 {
    				compatible = "ti,am5728-pruss";
    				reg = <0x4b200000 0x2000>,
    				      <0x4b202000 0x2000>,
    				      <0x4b210000 0x8000>,
    				      <0x4b226000 0x2000>,
    				      <0x4b22e000 0x31c>,
    				      <0x4b232000 0x58>;
    				reg-names = "dram0", "dram1", "shrdram2", "cfg",
    					    "iep", "mii_rt";
    				#address-cells = <1>;
    				#size-cells = <1>;
    				ranges;
    				status = "disabled";
    
    				pruss1_intc: intc@4b220000 {
    					compatible = "ti,am5728-pruss-intc";
    					reg = <0x4b220000 0x2000>;
    					reg-names = "intc";
    					interrupts =
    					     <GIC_SPI 186 IRQ_TYPE_LEVEL_HIGH>,
    					     <GIC_SPI 187 IRQ_TYPE_LEVEL_HIGH>,
    					     <GIC_SPI 188 IRQ_TYPE_LEVEL_HIGH>,
    					     <GIC_SPI 189 IRQ_TYPE_LEVEL_HIGH>,
    					     <GIC_SPI 190 IRQ_TYPE_LEVEL_HIGH>,
    					     <GIC_SPI 191 IRQ_TYPE_LEVEL_HIGH>,
    					     <GIC_SPI 192 IRQ_TYPE_LEVEL_HIGH>,
    					     <GIC_SPI 193 IRQ_TYPE_LEVEL_HIGH>;
    					interrupt-names = "host2", "host3",
    							  "host4", "host5",
    							  "host6", "host7",
    							  "host8", "host9";
    					interrupt-controller;
    					#interrupt-cells = <1>;
    				};
    
    				pru1_0: pru@4b234000 {
    					compatible = "ti,am5728-pru";
    					reg = <0x4b234000 0x3000>,
    					      <0x4b222000 0x400>,
    					      <0x4b222400 0x100>;
    					reg-names = "iram", "control", "debug";
    					label = "pru0";
    					status = "disabled";
    				};
    
    				pru1_1: pru@4b238000 {
    					compatible = "ti,am5728-pru";
    					reg = <0x4b238000 0x3000>,
    					      <0x4b224000 0x400>,
    					      <0x4b224400 0x100>;
    					reg-names = "iram", "control", "debug";
    					label = "pru1";
    					status = "disabled";
    				};
    
    				pruss1_mdio: mdio@4b232400 {
    					compatible = "ti,davinci_mdio";
    					#address-cells = <1>;
    					#size-cells = <0>;
    					clocks = <&dpll_gmac_h13x2_ck>;
    					clock-names = "fck";
    					bus_freq = <1000000>;
    					reg = <0x4b232400 0x90>;
    					status = "disabled";
    				};
    			};
    		};
    
    		pruss_soc_bus2: pruss_soc_bus@4b2a6000 {
    			compatible = "ti,am5728-pruss-soc-bus";
    			reg = <0x4b2a6000 0x2000>;
    			ti,hwmods = "pruss2";
    			#address-cells = <1>;
    			#size-cells = <1>;
    			ranges;
    			status = "disabled";
    
    			pruss2: pruss@4b280000 {
    				compatible = "ti,am5728-pruss";
    				reg = <0x4b280000 0x2000>,
    				      <0x4b282000 0x2000>,
    				      <0x4b290000 0x8000>,
    				      <0x4b2a6000 0x2000>,
    				      <0x4b2ae000 0x31c>,
    				      <0x4b2b2000 0x58>;
    				reg-names = "dram0", "dram1", "shrdram2", "cfg",
    					    "iep", "mii_rt";
    				#address-cells = <1>;
    				#size-cells = <1>;
    				ranges;
    				status = "disabled";
    
    				pruss2_intc: intc@4b2a0000 {
    					compatible = "ti,am5728-pruss-intc";
    					reg = <0x4b2a0000 0x2000>;
    					reg-names = "intc";
    					interrupts =
    					     <GIC_SPI 196 IRQ_TYPE_LEVEL_HIGH>,
    					     <GIC_SPI 197 IRQ_TYPE_LEVEL_HIGH>,
    					     <GIC_SPI 198 IRQ_TYPE_LEVEL_HIGH>,
    					     <GIC_SPI 199 IRQ_TYPE_LEVEL_HIGH>,
    					     <GIC_SPI 200 IRQ_TYPE_LEVEL_HIGH>,
    					     <GIC_SPI 201 IRQ_TYPE_LEVEL_HIGH>,
    					     <GIC_SPI 202 IRQ_TYPE_LEVEL_HIGH>,
    					     <GIC_SPI 203 IRQ_TYPE_LEVEL_HIGH>;
    					interrupt-names = "host2", "host3",
    							  "host4", "host5",
    							  "host6", "host7",
    							  "host8", "host9";
    					interrupt-controller;
    					#interrupt-cells = <1>;
    				};
    
    				pru2_0: pru@4b2b4000 {
    					compatible = "ti,am5728-pru";
    					reg = <0x4b2b4000 0x3000>,
    					      <0x4b2a2000 0x400>,
    					      <0x4b2a2400 0x100>;
    					reg-names = "iram", "control", "debug";
    					label = "pru0";
    					status = "disabled";
    				};
    
    				pru2_1: pru@4b2b8000 {
    					compatible = "ti,am5728-pru";
    					reg = <0x4b2b8000 0x3000>,
    					      <0x4b2a4000 0x400>,
    					      <0x4b2a4400 0x100>;
    					reg-names = "iram", "control", "debug";
    					label = "pru1";
    					status = "disabled";
    				};
    
    				pruss2_mdio: mdio@4b2b2400 {
    					compatible = "ti,davinci_mdio";
    					#address-cells = <1>;
    					#size-cells = <0>;
    					clocks = <&dpll_gmac_h13x2_ck>;
    					clock-names = "fck";
    					bus_freq = <1000000>;
    					reg = <0x4b2b2400 0x90>;
    					status = "disabled";
    				};
    			};
    		};
    
    		abb_mpu: regulator-abb-mpu {
    			compatible = "ti,abb-v3";
    			regulator-name = "abb_mpu";
    			#address-cells = <0>;
    			#size-cells = <0>;
    			clocks = <&sys_clkin1>;
    			ti,settling-time = <50>;
    			ti,clock-cycles = <16>;
    
    			reg = <0x4ae07ddc 0x4>, <0x4ae07de0 0x4>,
    			      <0x4ae06014 0x4>, <0x4a003b20 0xc>,
    			      <0x4ae0c158 0x4>;
    			reg-names = "setup-address", "control-address",
    				    "int-address", "efuse-address",
    				    "ldo-address";
    			ti,tranxdone-status-mask = <0x80>;
    			/* LDOVBBMPU_FBB_MUX_CTRL */
    			ti,ldovbb-override-mask = <0x400>;
    			/* LDOVBBMPU_FBB_VSET_OUT */
    			ti,ldovbb-vset-mask = <0x1F>;
    
    			/*
    			 * NOTE: only FBB mode used but actual vset will
    			 * determine final biasing
    			 */
    			ti,abb_info = <
    			/*uV		ABB	efuse	rbb_m fbb_m	vset_m*/
    			1060000		0	0x0	0 0x02000000 0x01F00000
    			1160000		0	0x4	0 0x02000000 0x01F00000
    			1210000		0	0x8	0 0x02000000 0x01F00000
    			>;
    		};
    
    		abb_ivahd: regulator-abb-ivahd {
    			compatible = "ti,abb-v3";
    			regulator-name = "abb_ivahd";
    			#address-cells = <0>;
    			#size-cells = <0>;
    			clocks = <&sys_clkin1>;
    			ti,settling-time = <50>;
    			ti,clock-cycles = <16>;
    
    			reg = <0x4ae07e34 0x4>, <0x4ae07e24 0x4>,
    			      <0x4ae06010 0x4>, <0x4a0025cc 0xc>,
    			      <0x4a002470 0x4>;
    			reg-names = "setup-address", "control-address",
    				    "int-address", "efuse-address",
    				    "ldo-address";
    			ti,tranxdone-status-mask = <0x40000000>;
    			/* LDOVBBIVA_FBB_MUX_CTRL */
    			ti,ldovbb-override-mask = <0x400>;
    			/* LDOVBBIVA_FBB_VSET_OUT */
    			ti,ldovbb-vset-mask = <0x1F>;
    
    			/*
    			 * NOTE: only FBB mode used but actual vset will
    			 * determine final biasing
    			 */
    			ti,abb_info = <
    			/*uV		ABB	efuse	rbb_m fbb_m	vset_m*/
    			1055000		0	0x0	0 0x02000000 0x01F00000
    			1150000		0	0x4	0 0x02000000 0x01F00000
    			1250000		0	0x8	0 0x02000000 0x01F00000
    			>;
    		};
    
    		abb_dspeve: regulator-abb-dspeve {
    			compatible = "ti,abb-v3";
    			regulator-name = "abb_dspeve";
    			#address-cells = <0>;
    			#size-cells = <0>;
    			clocks = <&sys_clkin1>;
    			ti,settling-time = <50>;
    			ti,clock-cycles = <16>;
    
    			reg = <0x4ae07e30 0x4>, <0x4ae07e20 0x4>,
    			      <0x4ae06010 0x4>, <0x4a0025e0 0xc>,
    			      <0x4a00246c 0x4>;
    			reg-names = "setup-address", "control-address",
    				    "int-address", "efuse-address",
    				    "ldo-address";
    			ti,tranxdone-status-mask = <0x20000000>;
    			/* LDOVBBDSPEVE_FBB_MUX_CTRL */
    			ti,ldovbb-override-mask = <0x400>;
    			/* LDOVBBDSPEVE_FBB_VSET_OUT */
    			ti,ldovbb-vset-mask = <0x1F>;
    
    			/*
    			 * NOTE: only FBB mode used but actual vset will
    			 * determine final biasing
    			 */
    			ti,abb_info = <
    			/*uV		ABB	efuse	rbb_m fbb_m	vset_m*/
    			1055000		0	0x0	0 0x02000000 0x01F00000
    			1150000		0	0x4	0 0x02000000 0x01F00000
    			1250000		0	0x8	0 0x02000000 0x01F00000
    			>;
    		};
    
    		abb_gpu: regulator-abb-gpu {
    			compatible = "ti,abb-v3";
    			regulator-name = "abb_gpu";
    			#address-cells = <0>;
    			#size-cells = <0>;
    			clocks = <&sys_clkin1>;
    			ti,settling-time = <50>;
    			ti,clock-cycles = <16>;
    
    			reg = <0x4ae07de4 0x4>, <0x4ae07de8 0x4>,
    			      <0x4ae06010 0x4>, <0x4a003b08 0xc>,
    			      <0x4ae0c154 0x4>;
    			reg-names = "setup-address", "control-address",
    				    "int-address", "efuse-address",
    				    "ldo-address";
    			ti,tranxdone-status-mask = <0x10000000>;
    			/* LDOVBBGPU_FBB_MUX_CTRL */
    			ti,ldovbb-override-mask = <0x400>;
    			/* LDOVBBGPU_FBB_VSET_OUT */
    			ti,ldovbb-vset-mask = <0x1F>;
    
    			/*
    			 * NOTE: only FBB mode used but actual vset will
    			 * determine final biasing
    			 */
    			ti,abb_info = <
    			/*uV		ABB	efuse	rbb_m fbb_m	vset_m*/
    			1090000		0	0x0	0 0x02000000 0x01F00000
    			1210000		0	0x4	0 0x02000000 0x01F00000
    			1280000		0	0x8	0 0x02000000 0x01F00000
    			>;
    		};
    
    		mcspi1: spi@48098000 {
    			compatible = "ti,omap4-mcspi";
    			reg = <0x48098000 0x200>;
    			interrupts = <GIC_SPI 60 IRQ_TYPE_LEVEL_HIGH>;
    			#address-cells = <1>;
    			#size-cells = <0>;
    			ti,hwmods = "mcspi1";
    			ti,spi-num-cs = <4>;
    			dmas = <&sdma_xbar 35>,
    			       <&sdma_xbar 36>,
    			       <&sdma_xbar 37>,
    			       <&sdma_xbar 38>,
    			       <&sdma_xbar 39>,
    			       <&sdma_xbar 40>,
    			       <&sdma_xbar 41>,
    			       <&sdma_xbar 42>;
    			dma-names = "tx0", "rx0", "tx1", "rx1",
    				    "tx2", "rx2", "tx3", "rx3";
    			status = "disabled";
    		};
    
    		mcspi2: spi@4809a000 {
    			compatible = "ti,omap4-mcspi";
    			reg = <0x4809a000 0x200>;
    			interrupts = <GIC_SPI 61 IRQ_TYPE_LEVEL_HIGH>;
    			#address-cells = <1>;
    			#size-cells = <0>;
    			ti,hwmods = "mcspi2";
    			ti,spi-num-cs = <2>;
    			dmas = <&sdma_xbar 43>,
    			       <&sdma_xbar 44>,
    			       <&sdma_xbar 45>,
    			       <&sdma_xbar 46>;
    			dma-names = "tx0", "rx0", "tx1", "rx1";
    			status = "disabled";
    		};
    
    		mcspi3: spi@480b8000 {
    			compatible = "ti,omap4-mcspi";
    			reg = <0x480b8000 0x200>;
    			interrupts = <GIC_SPI 86 IRQ_TYPE_LEVEL_HIGH>;
    			#address-cells = <1>;
    			#size-cells = <0>;
    			ti,hwmods = "mcspi3";
    			ti,spi-num-cs = <2>;
    			dmas = <&sdma_xbar 15>, <&sdma_xbar 16>;
    			dma-names = "tx0", "rx0";
    			status = "disabled";
    		};
    
    		mcspi4: spi@480ba000 {
    			compatible = "ti,omap4-mcspi";
    			reg = <0x480ba000 0x200>;
    			interrupts = <GIC_SPI 43 IRQ_TYPE_LEVEL_HIGH>;
    			#address-cells = <1>;
    			#size-cells = <0>;
    			ti,hwmods = "mcspi4";
    			ti,spi-num-cs = <1>;
    			dmas = <&sdma_xbar 70>, <&sdma_xbar 71>;
    			dma-names = "tx0", "rx0";
    			status = "disabled";
    		};
    
    		qspi: qspi@4b300000 {
    			compatible = "ti,dra7xxx-qspi";
    			reg = <0x4b300000 0x100>,
    			      <0x5c000000 0x4000000>;
    			reg-names = "qspi_base", "qspi_mmap";
    			syscon-chipselects = <&scm_conf 0x558>;
    			#address-cells = <1>;
    			#size-cells = <0>;
    			ti,hwmods = "qspi";
    			clocks = <&qspi_gfclk_div>;
    			clock-names = "fck";
    			num-cs = <4>;
    			interrupts = <GIC_SPI 343 IRQ_TYPE_LEVEL_HIGH>;
    			status = "disabled";
    		};
    
    		/* OCP2SCP3 */
    		ocp2scp@4a090000 {
    			compatible = "ti,omap-ocp2scp";
    			#address-cells = <1>;
    			#size-cells = <1>;
    			ranges;
    			reg = <0x4a090000 0x20>;
    			ti,hwmods = "ocp2scp3";
    			sata_phy: phy@4A096000 {
    				compatible = "ti,phy-pipe3-sata";
    				reg = <0x4A096000 0x80>, /* phy_rx */
    				      <0x4A096400 0x64>, /* phy_tx */
    				      <0x4A096800 0x40>; /* pll_ctrl */
    				reg-names = "phy_rx", "phy_tx", "pll_ctrl";
    				syscon-phy-power = <&scm_conf 0x374>;
    				clocks = <&sys_clkin1>, <&sata_ref_clk>;
    				clock-names = "sysclk", "refclk";
    				syscon-pllreset = <&scm_conf 0x3fc>;
    				#phy-cells = <0>;
    			};
    
    			pcie1_phy: pciephy@4a094000 {
    				compatible = "ti,phy-pipe3-pcie";
    				reg = <0x4a094000 0x80>, /* phy_rx */
    				      <0x4a094400 0x64>; /* phy_tx */
    				reg-names = "phy_rx", "phy_tx";
    				syscon-phy-power = <&scm_conf_pcie 0x1c>;
    				syscon-pcs = <&scm_conf_pcie 0x10>;
    				clocks = <&dpll_pcie_ref_ck>,
    					 <&dpll_pcie_ref_m2ldo_ck>,
    					 <&optfclk_pciephy1_32khz>,
    					 <&optfclk_pciephy1_clk>,
    					 <&optfclk_pciephy1_div_clk>,
    					 <&optfclk_pciephy_div>,
    					 <&sys_clkin1>;
    				clock-names = "dpll_ref", "dpll_ref_m2",
    					      "wkupclk", "refclk",
    					      "div-clk", "phy-div", "sysclk";
    				#phy-cells = <0>;
    			};
    
    			pcie2_phy: pciephy@4a095000 {
    				compatible = "ti,phy-pipe3-pcie";
    				reg = <0x4a095000 0x80>, /* phy_rx */
    				      <0x4a095400 0x64>; /* phy_tx */
    				reg-names = "phy_rx", "phy_tx";
    				syscon-phy-power = <&scm_conf_pcie 0x20>;
    				syscon-pcs = <&scm_conf_pcie 0x10>;
    				clocks = <&dpll_pcie_ref_ck>,
    					 <&dpll_pcie_ref_m2ldo_ck>,
    					 <&optfclk_pciephy2_32khz>,
    					 <&optfclk_pciephy2_clk>,
    					 <&optfclk_pciephy2_div_clk>,
    					 <&optfclk_pciephy_div>,
    					 <&sys_clkin1>;
    				clock-names = "dpll_ref", "dpll_ref_m2",
    					      "wkupclk", "refclk",
    					      "div-clk", "phy-div", "sysclk";
    				#phy-cells = <0>;
    				status = "disabled";
    			};
    		};
    
    		sata: sata@4a141100 {
    			compatible = "snps,dwc-ahci";
    			reg = <0x4a140000 0x1100>, <0x4a141100 0x7>;
    			interrupts = <GIC_SPI 49 IRQ_TYPE_LEVEL_HIGH>;
    			phys = <&sata_phy>;
    			phy-names = "sata-phy";
    			clocks = <&sata_ref_clk>;
    			ti,hwmods = "sata";
    			ports-implemented = <0x1>;
    		};
    
    		rtc: rtc@48838000 {
    			compatible = "ti,am3352-rtc";
    			reg = <0x48838000 0x100>;
    			interrupts = <GIC_SPI 217 IRQ_TYPE_LEVEL_HIGH>,
    				     <GIC_SPI 217 IRQ_TYPE_LEVEL_HIGH>;
    			ti,hwmods = "rtcss";
    			clocks = <&sys_32k_ck>;
    		};
    
    		/* OCP2SCP1 */
    		ocp2scp@4a080000 {
    			compatible = "ti,omap-ocp2scp";
    			#address-cells = <1>;
    			#size-cells = <1>;
    			ranges;
    			reg = <0x4a080000 0x20>;
    			ti,hwmods = "ocp2scp1";
    
    			usb2_phy1: phy@4a084000 {
    				compatible = "ti,dra7x-usb2", "ti,omap-usb2";
    				reg = <0x4a084000 0x400>;
    				syscon-phy-power = <&scm_conf 0x300>;
    				clocks = <&usb_phy1_always_on_clk32k>,
    					 <&usb_otg_ss1_refclk960m>;
    				clock-names =	"wkupclk",
    						"refclk";
    				#phy-cells = <0>;
    			};
    
    			usb2_phy2: phy@4a085000 {
    				compatible = "ti,dra7x-usb2-phy2",
    					     "ti,omap-usb2";
    				reg = <0x4a085000 0x400>;
    				syscon-phy-power = <&scm_conf 0xe74>;
    				clocks = <&usb_phy2_always_on_clk32k>,
    					 <&usb_otg_ss2_refclk960m>;
    				clock-names =	"wkupclk",
    						"refclk";
    				#phy-cells = <0>;
    			};
    
    			usb3_phy1: phy@4a084400 {
    				compatible = "ti,omap-usb3";
    				reg = <0x4a084400 0x80>,
    				      <0x4a084800 0x64>,
    				      <0x4a084c00 0x40>;
    				reg-names = "phy_rx", "phy_tx", "pll_ctrl";
    				syscon-phy-power = <&scm_conf 0x370>;
    				clocks = <&usb_phy3_always_on_clk32k>,
    					 <&sys_clkin1>,
    					 <&usb_otg_ss1_refclk960m>;
    				clock-names =	"wkupclk",
    						"sysclk",
    						"refclk";
    				#phy-cells = <0>;
    			};
    		};
    
    		omap_dwc3_1: omap_dwc3_1@48880000 {
    			compatible = "ti,dwc3";
    			ti,hwmods = "usb_otg_ss1";
    			reg = <0x48880000 0x10000>;
    			interrupts = <GIC_SPI 72 IRQ_TYPE_LEVEL_HIGH>;
    			#address-cells = <1>;
    			#size-cells = <1>;
    			utmi-mode = <2>;
    			ranges;
    			usb1: usb@48890000 {
    				compatible = "snps,dwc3";
    				reg = <0x48890000 0x17000>;
    				interrupts = <GIC_SPI 71 IRQ_TYPE_LEVEL_HIGH>,
    					     <GIC_SPI 71 IRQ_TYPE_LEVEL_HIGH>,
    					     <GIC_SPI 72 IRQ_TYPE_LEVEL_HIGH>;
    				interrupt-names = "peripheral",
    						  "host",
    						  "otg";
    				//phys = <&usb2_phy1>, <&usb3_phy1>;
    				phys = <&usb2_phy1>;
    				//phy-names = "usb2-phy", "usb3-phy";
    				phy-names = "usb2-phy";
    				//maximum-speed = "super-speed";
    				maximum-speed = "high-speed";
    				dr_mode = "otg";
    				snps,dis_u3_susphy_quirk;
    				snps,dis_u2_susphy_quirk;
    				snps,devctrl_halt_quirk;
    			};
    		};
    
    		omap_dwc3_2: omap_dwc3_2@488c0000 {
    			compatible = "ti,dwc3";
    			ti,hwmods = "usb_otg_ss2";
    			reg = <0x488c0000 0x10000>;
    			interrupts = <GIC_SPI 87 IRQ_TYPE_LEVEL_HIGH>;
    			#address-cells = <1>;
    			#size-cells = <1>;
    			utmi-mode = <2>;
    			ranges;
    			usb2: usb@488d0000 {
    				compatible = "snps,dwc3";
    				reg = <0x488d0000 0x17000>;
    				interrupts = <GIC_SPI 73 IRQ_TYPE_LEVEL_HIGH>,
    					     <GIC_SPI 73 IRQ_TYPE_LEVEL_HIGH>,
    					     <GIC_SPI 87 IRQ_TYPE_LEVEL_HIGH>;
    				interrupt-names = "peripheral",
    						  "host",
    						  "otg";
    				phys = <&usb2_phy2>;
    				phy-names = "usb2-phy";
    				maximum-speed = "high-speed";
    				dr_mode = "otg";
    				snps,dis_u3_susphy_quirk;
    				snps,dis_u2_susphy_quirk;
    				snps,devctrl_halt_quirk;
    			};
    		};
    
    		/* IRQ for DWC3_3 and DWC3_4 need IRQ crossbar */
    		omap_dwc3_3: omap_dwc3_3@48900000 {
    			compatible = "ti,dwc3";
    			ti,hwmods = "usb_otg_ss3";
    			reg = <0x48900000 0x10000>;
    			interrupts = <GIC_SPI 344 IRQ_TYPE_LEVEL_HIGH>;
    			#address-cells = <1>;
    			#size-cells = <1>;
    			utmi-mode = <2>;
    			ranges;
    			status = "disabled";
    			usb3: usb@48910000 {
    				compatible = "snps,dwc3";
    				reg = <0x48910000 0x17000>;
    				interrupts = <GIC_SPI 88 IRQ_TYPE_LEVEL_HIGH>,
    					     <GIC_SPI 88 IRQ_TYPE_LEVEL_HIGH>,
    					     <GIC_SPI 344 IRQ_TYPE_LEVEL_HIGH>;
    				interrupt-names = "peripheral",
    						  "host",
    						  "otg";
    				maximum-speed = "high-speed";
    				dr_mode = "otg";
    				snps,dis_u3_susphy_quirk;
    				snps,dis_u2_susphy_quirk;
    			};
    		};
    
    		elm: elm@48078000 {
    			compatible = "ti,am3352-elm";
    			reg = <0x48078000 0xfc0>;      /* device IO registers */
    			interrupts = <GIC_SPI 1 IRQ_TYPE_LEVEL_HIGH>;
    			ti,hwmods = "elm";
    			status = "disabled";
    		};
    
    		gpmc: gpmc@50000000 {
    			compatible = "ti,am3352-gpmc";
    			ti,hwmods = "gpmc";
    			reg = <0x50000000 0x37c>;      /* device IO registers */
    			interrupts = <GIC_SPI 15 IRQ_TYPE_LEVEL_HIGH>;
    			dmas = <&edma_xbar 4 0>;
    			dma-names = "rxtx";
    			gpmc,num-cs = <8>;
    			gpmc,num-waitpins = <2>;
    			#address-cells = <2>;
    			#size-cells = <1>;
    			interrupt-controller;
    			#interrupt-cells = <2>;
    			gpio-controller;
    			#gpio-cells = <2>;
    			status = "disabled";
    		};
    
    		atl: atl@4843c000 {
    			compatible = "ti,dra7-atl";
    			reg = <0x4843c000 0x3ff>;
    			ti,hwmods = "atl";
    			ti,provided-clocks = <&atl_clkin0_ck>, <&atl_clkin1_ck>,
    					     <&atl_clkin2_ck>, <&atl_clkin3_ck>;
    			clocks = <&atl_gfclk_mux>;
    			clock-names = "fck";
    			status = "disabled";
    		};
    
    		mcasp1: mcasp@48460000 {
    			compatible = "ti,dra7-mcasp-audio";
    			ti,hwmods = "mcasp1";
    			reg = <0x48460000 0x2000>,
    			      <0x45800000 0x1000>;
    			reg-names = "mpu","dat";
    			interrupts = <GIC_SPI 104 IRQ_TYPE_LEVEL_HIGH>,
    				     <GIC_SPI 103 IRQ_TYPE_LEVEL_HIGH>;
    			interrupt-names = "tx", "rx";
    			dmas = <&edma_xbar 129 1>, <&edma_xbar 128 1>;
    			dma-names = "tx", "rx";
    			clocks = <&mcasp1_aux_gfclk_mux>, <&mcasp1_ahclkx_mux>,
    				 <&mcasp1_ahclkr_mux>;
    			clock-names = "fck", "ahclkx", "ahclkr";
    			status = "disabled";
    		};
    
    		mcasp2: mcasp@48464000 {
    			compatible = "ti,dra7-mcasp-audio";
    			ti,hwmods = "mcasp2";
    			reg = <0x48464000 0x2000>,
    			      <0x45c00000 0x1000>;
    			reg-names = "mpu","dat";
    			interrupts = <GIC_SPI 149 IRQ_TYPE_LEVEL_HIGH>,
    				     <GIC_SPI 148 IRQ_TYPE_LEVEL_HIGH>;
    			interrupt-names = "tx", "rx";
    			dmas = <&edma_xbar 131 1>, <&edma_xbar 130 1>;
    			dma-names = "tx", "rx";
    			clocks = <&mcasp2_aux_gfclk_mux>, <&mcasp2_ahclkx_mux>,
    				 <&mcasp2_ahclkr_mux>;
    			clock-names = "fck", "ahclkx", "ahclkr";
    			status = "disabled";
    		};
    
    		mcasp3: mcasp@48468000 {
    			compatible = "ti,dra7-mcasp-audio";
    			ti,hwmods = "mcasp3";
    			reg = <0x48468000 0x2000>,
    			      <0x46000000 0x1000>;
    			reg-names = "mpu","dat";
    			interrupts = <GIC_SPI 151 IRQ_TYPE_LEVEL_HIGH>,
    				     <GIC_SPI 150 IRQ_TYPE_LEVEL_HIGH>;
    			interrupt-names = "tx", "rx";
    			dmas = <&edma_xbar 133 1>, <&edma_xbar 132 1>;
    			dma-names = "tx", "rx";
    			clocks = <&mcasp3_aux_gfclk_mux>, <&mcasp3_ahclkx_mux>;
    			clock-names = "fck", "ahclkx";
    			status = "disabled";
    		};
    
    		mcasp4: mcasp@4846c000 {
    			compatible = "ti,dra7-mcasp-audio";
    			ti,hwmods = "mcasp4";
    			reg = <0x4846c000 0x2000>,
    			      <0x48436000 0x1000>;
    			reg-names = "mpu","dat";
    			interrupts = <GIC_SPI 153 IRQ_TYPE_LEVEL_HIGH>,
    				     <GIC_SPI 152 IRQ_TYPE_LEVEL_HIGH>;
    			interrupt-names = "tx", "rx";
    			dmas = <&edma_xbar 135 1>, <&edma_xbar 134 1>;
    			dma-names = "tx", "rx";
    			clocks = <&mcasp4_aux_gfclk_mux>, <&mcasp4_ahclkx_mux>;
    			clock-names = "fck", "ahclkx";
    			status = "disabled";
    		};
    
    		mcasp5: mcasp@48470000 {
    			compatible = "ti,dra7-mcasp-audio";
    			ti,hwmods = "mcasp5";
    			reg = <0x48470000 0x2000>,
    			      <0x4843a000 0x1000>;
    			reg-names = "mpu","dat";
    			interrupts = <GIC_SPI 155 IRQ_TYPE_LEVEL_HIGH>,
    				     <GIC_SPI 154 IRQ_TYPE_LEVEL_HIGH>;
    			interrupt-names = "tx", "rx";
    			dmas = <&edma_xbar 137 1>, <&edma_xbar 136 1>;
    			dma-names = "tx", "rx";
    			clocks = <&mcasp5_aux_gfclk_mux>, <&mcasp5_ahclkx_mux>;
    			clock-names = "fck", "ahclkx";
    			status = "disabled";
    		};
    
    		mcasp6: mcasp@48474000 {
    			compatible = "ti,dra7-mcasp-audio";
    			ti,hwmods = "mcasp6";
    			reg = <0x48474000 0x2000>,
    			      <0x4844c000 0x1000>;
    			reg-names = "mpu","dat";
    			interrupts = <GIC_SPI 157 IRQ_TYPE_LEVEL_HIGH>,
    				     <GIC_SPI 156 IRQ_TYPE_LEVEL_HIGH>;
    			interrupt-names = "tx", "rx";
    			dmas = <&edma_xbar 139 1>, <&edma_xbar 138 1>;
    			dma-names = "tx", "rx";
    			clocks = <&mcasp6_aux_gfclk_mux>, <&mcasp6_ahclkx_mux>;
    			clock-names = "fck", "ahclkx";
    			status = "disabled";
    		};
    
    		mcasp7: mcasp@48478000 {
    			compatible = "ti,dra7-mcasp-audio";
    			ti,hwmods = "mcasp7";
    			reg = <0x48478000 0x2000>,
    			      <0x48450000 0x1000>;
    			reg-names = "mpu","dat";
    			interrupts = <GIC_SPI 159 IRQ_TYPE_LEVEL_HIGH>,
    				     <GIC_SPI 158 IRQ_TYPE_LEVEL_HIGH>;
    			interrupt-names = "tx", "rx";
    			dmas = <&edma_xbar 141 1>, <&edma_xbar 140 1>;
    			dma-names = "tx", "rx";
    			clocks = <&mcasp7_aux_gfclk_mux>, <&mcasp7_ahclkx_mux>;
    			clock-names = "fck", "ahclkx";
    			status = "disabled";
    		};
    
    		mcasp8: mcasp@4847c000 {
    			compatible = "ti,dra7-mcasp-audio";
    			ti,hwmods = "mcasp8";
    			reg = <0x4847c000 0x2000>,
    			      <0x48454000 0x1000>;
    			reg-names = "mpu","dat";
    			interrupts = <GIC_SPI 161 IRQ_TYPE_LEVEL_HIGH>,
    				     <GIC_SPI 160 IRQ_TYPE_LEVEL_HIGH>;
    			interrupt-names = "tx", "rx";
    			dmas = <&edma_xbar 143 1>, <&edma_xbar 142 1>;
    			dma-names = "tx", "rx";
    			clocks = <&mcasp8_aux_gfclk_mux>, <&mcasp8_ahclkx_mux>;
    			clock-names = "fck", "ahclkx";
    			status = "disabled";
    		};
    
    		crossbar_mpu: crossbar@4a002a48 {
    			compatible = "ti,irq-crossbar";
    			reg = <0x4a002a48 0x130>;
    			interrupt-controller;
    			interrupt-parent = <&wakeupgen>;
    			#interrupt-cells = <3>;
    			ti,max-irqs = <160>;
    			ti,max-crossbar-sources = <MAX_SOURCES>;
    			ti,reg-size = <2>;
    			ti,irqs-reserved = <0 1 2 3 5 6 131 132>;
    			ti,irqs-skip = <10 133 139 140>;
    			ti,irqs-safe-map = <0>;
    		};
    
    		mac: ethernet@48484000 {
    			compatible = "ti,dra7-cpsw","ti,cpsw";
    			ti,hwmods = "gmac";
    			clocks = <&gmac_main_clk>, <&gmac_rft_clk_mux>;
    			clock-names = "fck", "cpts";
    			cpdma_channels = <8>;
    			ale_entries = <1024>;
    			bd_ram_size = <0x2000>;
    			mac_control = <0x20>;
    			slaves = <2>;
    			active_slave = <0>;
    			cpts_clock_mult = <0x784CFE14>;
    			cpts_clock_shift = <29>;
    			reg = <0x48484000 0x1000
    			       0x48485200 0x2E00>;
    			#address-cells = <1>;
    			#size-cells = <1>;
    
    			/*
    			 * Do not allow gating of cpsw clock as workaround
    			 * for errata i877. Keeping internal clock disabled
    			 * causes the device switching characteristics
    			 * to degrade over time and eventually fail to meet
    			 * the data manual delay time/skew specs.
    			 */
    			ti,no-idle;
    
    			/*
    			 * rx_thresh_pend
    			 * rx_pend
    			 * tx_pend
    			 * misc_pend
    			 */
    			interrupts = <GIC_SPI 334 IRQ_TYPE_LEVEL_HIGH>,
    				     <GIC_SPI 335 IRQ_TYPE_LEVEL_HIGH>,
    				     <GIC_SPI 336 IRQ_TYPE_LEVEL_HIGH>,
    				     <GIC_SPI 337 IRQ_TYPE_LEVEL_HIGH>;
    			ranges;
    			syscon = <&scm_conf>;
    			status = "disabled";
    
    			davinci_mdio: mdio@48485000 {
    				compatible = "ti,cpsw-mdio","ti,davinci_mdio";
    				#address-cells = <1>;
    				#size-cells = <0>;
    				ti,hwmods = "davinci_mdio";
    				bus_freq = <1000000>;
    				reg = <0x48485000 0x100>;
    			};
    
    			cpsw_emac0: slave@48480200 {
    				/* Filled in by U-Boot */
    				mac-address = [ 00 00 00 00 00 00 ];
    			};
    
    			cpsw_emac1: slave@48480300 {
    				/* Filled in by U-Boot */
    				mac-address = [ 00 00 00 00 00 00 ];
    			};
    
    			phy_sel: cpsw-phy-sel@4a002554 {
    				compatible = "ti,dra7xx-cpsw-phy-sel";
    				reg= <0x4a002554 0x4>;
    				reg-names = "gmii-sel";
    			};
    		};
    
    		dcan1: can@481cc000 {
    			compatible = "ti,dra7-d_can";
    			ti,hwmods = "dcan1";
    			reg = <0x4ae3c000 0x2000>;
    			syscon-raminit = <&scm_conf 0x558 0>;
    			interrupts = <GIC_SPI 222 IRQ_TYPE_LEVEL_HIGH>;
    			clocks = <&dcan1_sys_clk_mux>;
    			status = "disabled";
    		};
    
    		dcan2: can@481d0000 {
    			compatible = "ti,dra7-d_can";
    			ti,hwmods = "dcan2";
    			reg = <0x48480000 0x2000>;
    			syscon-raminit = <&scm_conf 0x558 1>;
    			interrupts = <GIC_SPI 225 IRQ_TYPE_LEVEL_HIGH>;
    			clocks = <&sys_clkin1>;
    			status = "disabled";
    		};
    
    		gpu: gpu@56000000 {
    			compatible = "ti,dra7-sgx544", "img,sgx544";
    			reg = <0x56000000 0x10000>;
    			reg-names = "gpu_ocp_base";
    			interrupts = <GIC_SPI 16 IRQ_TYPE_LEVEL_HIGH>;
    			ti,hwmods = "gpu";
    			clocks = <&l3_iclk_div>, <&gpu_core_gclk_mux>,
    				<&gpu_hyd_gclk_mux>;
    			clock-names = "iclk", "fclk1", "fclk2";
    		};
    
    		bb2d: bb2d@59000000 {
    			compatible = "ti,dra7-bb2d";
    			reg = <0x59000000 0x0700>;
    			interrupts = <GIC_SPI 120 IRQ_TYPE_LEVEL_HIGH>;
    			ti,hwmods = "bb2d";
    			clocks = <&dpll_core_h24x2_ck>;
    			clock-names = "fclk";
    			status = "disabled";
    		};
    
    		dss: dss@58000000 {
    			compatible = "ti,dra7-dss";
    			/* 'reg' defined in dra72x.dtsi and dra74x.dtsi */
    			/* 'clocks' defined in dra72x.dtsi and dra74x.dtsi */
    			status = "disabled";
    			ti,hwmods = "dss_core";
    			/* CTRL_CORE_DSS_PLL_CONTROL */
    			syscon-pll-ctrl = <&scm_conf 0x538>;
    			#address-cells = <1>;
    			#size-cells = <1>;
    			ranges;
    
    			dispc: dispc@58001000 {
    				compatible = "ti,dra7-dispc";
    				reg = <0x58001000 0x1000>;
    				interrupts = <GIC_SPI 20 IRQ_TYPE_LEVEL_HIGH>;
    				ti,hwmods = "dss_dispc";
    				clocks = <&dss_dss_clk>;
    				clock-names = "fck";
    				/* CTRL_CORE_SMA_SW_1 */
    				syscon-pol = <&scm_conf 0x534>;
    			};
    
    			hdmi: encoder@58060000 {
    				compatible = "ti,dra7-hdmi";
    				reg = <0x58040000 0x200>,
    				      <0x58040200 0x80>,
    				      <0x58040300 0x80>,
    				      <0x58060000 0x19000>;
    				reg-names = "wp", "pll", "phy", "core";
    				interrupts = <GIC_SPI 96 IRQ_TYPE_LEVEL_HIGH>;
    				status = "disabled";
    				ti,hwmods = "dss_hdmi";
    				clocks = <&dss_48mhz_clk>, <&dss_hdmi_clk>;
    				clock-names = "fck", "sys_clk";
    				dmas = <&sdma_xbar 76>;
    				dma-names = "audio_tx";
    			};
    		};
    
    		epwmss0: epwmss@4843e000 {
    			compatible = "ti,dra746-pwmss", "ti,am33xx-pwmss";
    			reg = <0x4843e000 0x30>;
    			ti,hwmods = "epwmss0";
    			#address-cells = <1>;
    			#size-cells = <1>;
    			status = "disabled";
    			ranges;
    
    			ehrpwm0: pwm@4843e200 {
    				compatible = "ti,dra746-ehrpwm",
    					     "ti,am3352-ehrpwm";
    				#pwm-cells = <3>;
    				reg = <0x4843e200 0x80>;
    				clocks = <&ehrpwm0_tbclk>, <&l4_root_clk_div>;
    				clock-names = "tbclk", "fck";
    				status = "disabled";
    			};
    
    			ecap0: ecap@4843e100 {
    				compatible = "ti,dra746-ecap",
    					     "ti,am3352-ecap";
    				#pwm-cells = <3>;
    				reg = <0x4843e100 0x80>;
    				clocks = <&l4_root_clk_div>;
    				clock-names = "fck";
    				status = "disabled";
    			};
    		};
    
    		epwmss1: epwmss@48440000 {
    			compatible = "ti,dra746-pwmss", "ti,am33xx-pwmss";
    			reg = <0x48440000 0x30>;
    			ti,hwmods = "epwmss1";
    			#address-cells = <1>;
    			#size-cells = <1>;
    			status = "disabled";
    			ranges;
    
    			ehrpwm1: pwm@48440200 {
    				compatible = "ti,dra746-ehrpwm",
    					     "ti,am3352-ehrpwm";
    				#pwm-cells = <3>;
    				reg = <0x48440200 0x80>;
    				clocks = <&ehrpwm1_tbclk>, <&l4_root_clk_div>;
    				clock-names = "tbclk", "fck";
    				status = "disabled";
    			};
    
    			ecap1: ecap@48440100 {
    				compatible = "ti,dra746-ecap",
    					     "ti,am3352-ecap";
    				#pwm-cells = <3>;
    				reg = <0x48440100 0x80>;
    				clocks = <&l4_root_clk_div>;
    				clock-names = "fck";
    				status = "disabled";
    			};
    		};
    
    		epwmss2: epwmss@48442000 {
    			compatible = "ti,dra746-pwmss", "ti,am33xx-pwmss";
    			reg = <0x48442000 0x30>;
    			ti,hwmods = "epwmss2";
    			#address-cells = <1>;
    			#size-cells = <1>;
    			status = "disabled";
    			ranges;
    
    			ehrpwm2: pwm@48442200 {
    				compatible = "ti,dra746-ehrpwm",
    					     "ti,am3352-ehrpwm";
    				#pwm-cells = <3>;
    				reg = <0x48442200 0x80>;
    				clocks = <&ehrpwm2_tbclk>, <&l4_root_clk_div>;
    				clock-names = "tbclk", "fck";
    				status = "disabled";
    			};
    
    			ecap2: ecap@48442100 {
    				compatible = "ti,dra746-ecap",
    					     "ti,am3352-ecap";
    				#pwm-cells = <3>;
    				reg = <0x48442100 0x80>;
    				clocks = <&l4_root_clk_div>;
    				clock-names = "fck";
    				status = "disabled";
    			};
    		};
    
    		aes1: aes@4b500000 {
    			compatible = "ti,omap4-aes";
    			ti,hwmods = "aes1";
    			reg = <0x4b500000 0xa0>;
    			interrupts = <GIC_SPI 80 IRQ_TYPE_LEVEL_HIGH>;
    			dmas = <&edma_xbar 111 0>, <&edma_xbar 110 0>;
    			dma-names = "tx", "rx";
    			clocks = <&l3_iclk_div>;
    			clock-names = "fck";
    		};
    
    		aes2: aes@4b700000 {
    			compatible = "ti,omap4-aes";
    			ti,hwmods = "aes2";
    			reg = <0x4b700000 0xa0>;
    			interrupts = <GIC_SPI 59 IRQ_TYPE_LEVEL_HIGH>;
    			dmas = <&edma_xbar 114 0>, <&edma_xbar 113 0>;
    			dma-names = "tx", "rx";
    			clocks = <&l3_iclk_div>;
    			clock-names = "fck";
    		};
    
    		des: des@480a5000 {
    			compatible = "ti,omap4-des";
    			ti,hwmods = "des";
    			reg = <0x480a5000 0xa0>;
    			interrupts = <GIC_SPI 77 IRQ_TYPE_LEVEL_HIGH>;
    			dmas = <&sdma_xbar 117>, <&sdma_xbar 116>;
    			dma-names = "tx", "rx";
    			clocks = <&l3_iclk_div>;
    			clock-names = "fck";
    		};
    
    		sham: sham@53100000 {
    			compatible = "ti,omap5-sham";
    			ti,hwmods = "sham";
    			reg = <0x4b101000 0x300>;
    			interrupts = <GIC_SPI 46 IRQ_TYPE_LEVEL_HIGH>;
    			dmas = <&edma_xbar 119 0>;
    			dma-names = "rx";
    			clocks = <&l3_iclk_div>;
    			clock-names = "fck";
    		};
    
    		rng: rng@48090000 {
    			compatible = "ti,omap4-rng";
    			ti,hwmods = "rng";
    			reg = <0x48090000 0x2000>;
    			interrupts = <GIC_SPI 47 IRQ_TYPE_LEVEL_HIGH>;
    			clocks = <&l3_iclk_div>;
    			clock-names = "fck";
    		};
    
    		opp_supply_mpu: opp-supply@4a003b20 {
    			compatible = "ti,omap5-opp-supply";
    			reg = <0x4a003b20 0xc>;
    			ti,efuse-settings = <
    			/* uV   offset */
    			1060000 0x0
    			1160000 0x4
    			1210000 0x8
    			>;
    			ti,absolute-max-voltage-uv = <1500000>;
    		};
    
    		vpe {
    			compatible = "ti,vpe";
    			ti,hwmods = "vpe";
    			clocks = <&dpll_core_h23x2_ck>;
    			clock-names = "fck";
    			reg = <0x489d0000 0x120>,
    			      <0x489d0300 0x20>,
    			      <0x489d0400 0x20>,
    			      <0x489d0500 0x20>,
    			      <0x489d0600 0x3c>,
    			      <0x489d0700 0x80>,
    			      <0x489d5700 0x18>,
    			      <0x489dd000 0x400>;
    			reg-names = "vpe_top",
    				    "vpe_chr_us0",
    				    "vpe_chr_us1",
    				    "vpe_chr_us2",
    				    "vpe_dei",
    				    "sc",
    				    "csc",
    				    "vpdma";
    			interrupts = <GIC_SPI 354 IRQ_TYPE_LEVEL_HIGH>;
    			#address-cells = <1>;
    			#size-cells = <0>;
    		};
    
    		vip1: vip@0x48970000 {
    			compatible = "ti,vip1";
    			reg = <0x48970000 0x114>,
    			      <0x48975500 0xD8>,
    			      <0x48975700 0x18>,
    			      <0x48975800 0x80>,
    			      <0x48975a00 0xD8>,
    			      <0x48975c00 0x18>,
    			      <0x48975d00 0x80>,
    			      <0x4897d000 0x400>;
    			reg-names = "vip",
    				    "parser0",
    				    "csc0",
    				    "sc0",
    				    "parser1",
    				    "csc1",
    				    "sc1",
    				    "vpdma";
    			ti,hwmods = "vip1";
    			interrupts = <GIC_SPI 351 IRQ_TYPE_LEVEL_HIGH>,
    				     <GIC_SPI 392 IRQ_TYPE_LEVEL_HIGH>;
    			/* CTRL_CORE_SMA_SW_1 */
    			syscon-pol = <&scm_conf 0x534>;
    			#address-cells = <1>;
    			#size-cells = <0>;
    			status = "disabled";
    			vin1a: port@0 {
    				#address-cells = <1>;
    				#size-cells = <0>;
    				reg = <0>;
    				status = "disabled";
    			};
    			vin2a: port@1 {
    				#address-cells = <1>;
    				#size-cells = <0>;
    				reg = <1>;
    				status = "disabled";
    			};
    			vin1b: port@2 {
    				#address-cells = <1>;
    				#size-cells = <0>;
    				reg = <2>;
    				status = "disabled";
    			};
    			vin2b: port@3 {
    				#address-cells = <1>;
    				#size-cells = <0>;
    				reg = <3>;
    				status = "disabled";
    			};
    		};
    	};
    
    	thermal_zones: thermal-zones {
    		#include "omap4-cpu-thermal.dtsi"
    		#include "omap5-gpu-thermal.dtsi"
    		#include "omap5-core-thermal.dtsi"
    		#include "dra7-dspeve-thermal.dtsi"
    		#include "dra7-iva-thermal.dtsi"
    	};
    
    };
    
    &cpu_thermal {
    	polling-delay = <500>; /* milliseconds */
    };
    
    &cpu_crit {
    	temperature = <120000>; /* milli Celsius */
    };
    
    &core_crit {
    	temperature = <120000>; /* milli Celsius */
    };
    
    &gpu_crit {
    	temperature = <120000>; /* milli Celsius */
    };
    
    &dspeve_crit {
    	temperature = <120000>; /* milli Celsius */
    };
    
    &iva_crit {
    	temperature = <120000>; /* milli Celsius */
    };
    
    /include/ "dra7xx-clocks.dtsi"