This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TDA4VM:vxGraphParameterEnqueeReadyRef 的 CSIRX 问题

Guru**** 2540720 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1047240/tda4vm-csirx-problem-with-vxgraphparameterenqueuereadyref

器件型号:TDA4VM

您好,专家

我正在使用 single_cam demo 从 ISP 处理器(OAX4000)获取 mipi 信号。OAX4000已经通过 CSIRX1感应 mipi。

我进行了一些更改、但当代码运行到函数 vxGraphParameteEnqueueReadyRef 时、代码会被占用。 我检查了代码、认为设置正常。

MIPI: 4通道、1472Mbps/通道、VC0:YUV422-8、3840X2170@30fps

sensor_drv 中的设置如下所示:

 static IssSensor_CreateParams  oax4000CreatePrms = {
    SENSOR_OV_OAX4000_M96717,     /*sensor name*/
    0x1,                             /*i2cInstId*/
    {0x36, 0, 0, 0, 0, 0, 0, 0},   /*i2cAddrSensor*/
    {0x42, 0, 0, 0, 0, 0, 0, 0},      /*i2cAddrSer*/
    /*IssSensor_Info*/
    {
        {
            OAX4000_OUT_WIDTH,               /*width*/
            OAX4000_OUT_HEIGHT,              /*height*/
            1,                              /*num_exposures*/
            vx_false_e,                     /*line_interleaved*/
            {
                {VX_DF_IMAGE_UYVY, 7},    /*dataFormat and MSB [0]*/
            },
            0,                              /*meta_height_before*/
            0,                              /*meta_height_after*/
        },
        ISS_SENSOR_OAX4000_FEATURES,     /*features*/
        ALGORITHMS_ISS_AEWB_MODE_NONE,  /*aewbMode*/
        30,                             /*fps*/
        4,                              /*numDataLanes*/
        {1, 2, 3, 4},                   /*dataLanesMap*/
        {0, 0, 0, 0},                   /*dataLanesPolarity*/
        683,                            /*CSI Clock*/
    },
    1,                                  /*numChan*/
    4000,                                /*dccId*/
};

static IssSensorFxns           oax4000SensorFxns = {
    OAX4000_Probe,
    OAX4000_Config,
    OAX4000_StreamOn,
    OAX4000_StreamOff,
    OAX4000_PowerOn,
    OAX4000_PowerOff,
    OAX4000_GetExpParams,
    OAX4000_SetAeParams,
    OAX4000_GetDccParams,
    OAX4000_InitAewbConfig,
    OAX4000_GetIspConfig,
    OAX4000_ReadWriteReg,
    OAX4000_GetExpPrgFxn,
    OAX4000_deinit,
    OAX4000_GetWBPrgFxn,
    OAX4000_SetAwbParams
};

static IssSensorIntfParams     oax4000SensorIntfPrms = {
    0,                                /*isMultiChannel*/
    4,                              /*numCSI2Lanes*/
    1,                              /*inCsi2VirtualChanNum*/
    1,                /* isCplxCfgValid */
     {
        {0, 1}, /* Clock Lane */
        {0, 2}, /* data1Lane */
        {0, 3}, /* data2Lane */
        {0, 4}, /* data3Lane*/
        {0, 5}, /* data4Lane */
    },
    683,                 /* csi2PhyClk */
    0,             /*sensorBroadcast*/
    0,             /*enableFsin*/
};

此外、我在 single_cam 演示中的函数 app_create_graph 中进行了一些更改:

	printf("########################## OAX4000 !!!!!!\r\n");
	local_capture_config.instId[0] = 1;
	local_capture_config.chInstMap[0] = 1U;
	local_capture_config.instCfg[0].laneBandSpeed = TIVX_CAPTURE_LANE_BAND_SPEED_1350_TO_1500_MBPS; 
	local_capture_config.chVcNum[0]   = 0;

演示日志为:

root@j7-evm:~# /opt/vision_apps/vx_app_single_cam.out 
APP: Init ... !!!
MEM: Init ... !!!
MEM: Initialized DMA HEAP (fd=4) !!!
MEM: Init ... Done !!!
IPC: Init ... !!!
IPC: Init ... Done !!!
REMOTE_SERVICE: Init ... !!!
REMOTE_SERVICE: Init ... Done !!!
   171.282926 s: GTC Frequency = 200 MHz
APP: Init ... Done !!!
   171.286469 s:  VX_ZONE_INIT:Enabled
   171.286495 s:  VX_ZONE_ERROR:Enabled
   171.286503 s:  VX_ZONE_WARNING:Enabled
   171.292925 s:  VX_ZONE_INIT:[tivxInit:71] Initialization Done !!!
   171.293097 s:  VX_ZONE_INIT:[tivxHostInit:48] Initialization Done for HOST !!!

 Single Camera Demo - (c) Texas Instruments 2019
 ========================================================

 Usage,
  /opt/vision_apps/vx_app_single_cam.out --cfg <config file>

Defaulting to interactive mode 
IttCtrl_registerHandler: command echo registered at location 0 
IttCtrl_registerHandler: command iss_read_2a_params registered at location 1 
IttCtrl_registerHandler: command iss_write_2a_params registered at location 2 
IttCtrl_registerHandler: command iss_raw_save registered at location 3 
IttCtrl_registerHandler: command iss_yuv_save registered at location 4 
IttCtrl_registerHandler: command iss_read_sensor_reg registered at location 5 
IttCtrl_registerHandler: command iss_write_sensor_reg registered at location 6 
IttCtrl_registerHandler: command dev_ctrl registered at location 7 
IttCtrl_registerHandler: command iss_send_dcc_file registered at location 8 
 NETWORK: Opened at IP Addr = 0.0.0.0, socket port=5000!!!
   171.293959 s: ISS: Enumerating sensors ... !!!
   171.294362 s: ISS: Enumerating sensors ... found 0 : IMX390-UB953_D3
   171.294372 s: ISS: Enumerating sensors ... found 1 : AR0233-UB953_MARS
   171.294380 s: ISS: Enumerating sensors ... found 2 : AR0820-UB953_LI
   171.294387 s: ISS: Enumerating sensors ... found 3 : UB9xxx_RAW12_TESTPATTERN
   171.294395 s: ISS: Enumerating sensors ... found 4 : UB96x_UYVY_TESTPATTERN
   171.294403 s: ISS: Enumerating sensors ... found 5 : GW_AR0233_UYVY
   171.294410 s: ISS: Enumerating sensors ... found 6 : OAX4000-MAX96717
Select camera port index 0-7 : [MCU2_0]    171.294050 s: ImageSensor_RemoteServiceHandler: IM_SENSOR_CMD_CREATE 
[MCU2_0]    171.294114 s: Sensor at index 0 = IMX390-UB953_D3 
[MCU2_0]    171.294146 s: Sensor at index 1 = AR0233-UB953_MARS 
[MCU2_0]    171.294172 s: Sensor at index 2 = AR0820-UB953_LI 
[MCU2_0]    171.294195 s: Sensor at index 3 = UB9xxx_RAW12_TESTPATTERN 
[MCU2_0]    171.294220 s: Sensor at index 4 = UB96x_UYVY_TESTPATTERN 
[MCU2_0]    171.294245 s: Sensor at index 5 = GW_AR0233_UYVY 
[MCU2_0]    171.294283 s: Sensor at index 6 = OAX4000-MAX96717 
6
0x7 registered sensor drivers
a : IMX390-UB953_D3 
b : AR0233-UB953_MARS 
c : AR0820-UB953_LI 
d : UB9xxx_RAW12_TESTPATTERN 
e : UB96x_UYVY_TESTPATTERN 
f : GW_AR0233_UYVY 
g : OAX4000-MAX96717 
Select a sensor above or press '0' to autodetect the sensor : Invalid selection 
. Try again 
0x7 registered sensor drivers
a : IMX390-UB953_D3 
b : AR0233-UB953_MARS 
c : AR0820-UB953_LI 
d : UB9xxx_RAW12_TESTPATTERN 
e : UB96x_UYVY_TESTPATTERN 
f : GW_AR0233_UYVY 
g : OAX4000-MAX96717 
Select a sensor above or press '0' to autodetect the sensor : g
Sensor selected : OAX4000-MAX96717
LDC Selection Yes(1)/No(0) : LDC Selection Yes(1)/No(0) : 0
Querying OAX4000-MAX96717 
   179.690395 s: ISS: Querying sensor [OAX4000-MAX96717] ... !!!
   179.690642 s: ISS: Querying sensor [OAX4000-MAX96717] ... Done !!!
YUV Input selected. VISS and AEWB nodes will be bypassed. 
   179.690655 s: ISS: Initializing sensor [OAX4000-MAX96717], doing IM_SENSOR_CMD_PWRON ... !!!
[MCU2_0]    179.690496 s: ImageSensor_RemoteServiceHandler: IM_SENSOR_CMD_QUERY 
[MCU2_0]    179.690555 s: Received Query for OAX4000-MAX96717 
[MCU2_0]    179.690713 s: ImageSensor_RemoteServiceHandler: IM_SENSOR_CMD_PWRON 
   179.690950 s: ISS: Initializing sensor [OAX4000-MAX96717], doing IM_SENSOR_CMD_CONFIG ... !!!
   179.691217 s: ISS: Initializing sensor [OAX4000-MAX96717] ... Done !!!
############# width:3840 height:2170 
########################## OAX4000 !!!!!!
disable LDC
Scaler is disabled


 ==========================
 Demo : Single Camera w/ 2A
 ==========================

 p: Print performance statistics

 s: Save Sensor RAW, VISS Output and H3A output images to File System

 e: Export performance statistics

 u: Update DCC from File System


 x: Exit

 Enter Choice: 
Unsupported command 



 ==========================
 Demo : Single Camera w/ 2A
 ==========================

 p: Print performance statistics

 s: Save Sensor RAW, VISS Output and H3A output images to File System

 e: Export performance statistics

 u: Update DCC from File System


 x: Exit

 Enter Choice:    179.696380 s: ISS: Starting sensor [OAX4000-MAX96717] ... !!!
   179.696748 s: ISS: Starting sensor [OAX4000-MAX96717] ... !!!
[MCU2_0]    179.690790 s: IM_SENSOR_CMD_PWRON : channel_mask = 0x1 sensor_name:OAX4000-MAX96717
[MCU2_0]    179.690852 s: fpd i2cInst:0 Addr:0x0 status;-1
[MCU2_0]    179.690888 s: sensor powron status:0
[MCU2_0]    179.691024 s: ImageSensor_RemoteServiceHandler: IM_SENSOR_CMD_CONFIG 
[MCU2_0]    179.691061 s: Application requested features = 0x0 
[MCU2_0]  
[MCU2_0]    179.691115 s: Configuring camera # 0 
[MCU2_0]    179.691154 s: IM_SENSOR_CMD_CONFIG returning status = 0 
[MCU2_0]    179.696495 s: ImageSensor_RemoteServiceHandler: IM_SENSOR_CMD_STREAM_ON 
[MCU2_0]    179.696582 s: IM_SENSOR_CMD_STREAM_ON:  channel_mask = 0x1
[MCU2_0]    179.696619 s: IssSensor_Start chId:0
[MCU2_0]    179.696664 s: OAX4000 StreamOn !!!!!!!!!
p


Summary of CPU load,
====================

CPU: mpu1_0: TOTAL LOAD =  15. 6 % ( HWI =   0. 4 %, SWI =   0. 4 % )
CPU: mcu2_0: TOTAL LOAD =   2.53 % ( HWI =   0.47 %, SWI =   0. 9 % )
CPU: mcu2_1: TOTAL LOAD =   0. 9 % ( HWI =   0. 6 %, SWI =   0. 1 % )
CPU:  c6x_1: TOTAL LOAD =   0.47 % ( HWI =   0.28 %, SWI =   0.17 % )
CPU:  c6x_2: TOTAL LOAD =   0.47 % ( HWI =   0.28 %, SWI =   0.17 % )
CPU:  c7x_1: TOTAL LOAD =   0. 7 % ( HWI =   0. 3 %, SWI =   0. 2 % )


HWA performance statistics,
===========================



DDR performance statistics,
===========================

DDR: READ  BW: AVG =     11 MB/s, PEAK =    300 MB/s
DDR: WRITE BW: AVG =      5 MB/s, PEAK =    200 MB/s
DDR: TOTAL BW: AVG =     16 MB/s, PEAK =    500 MB/s


Detailed CPU performance/memory statistics,
===========================================

CPU: mcu2_0: TASK:           IPC_RX:   0. 0 %
CPU: mcu2_0: TASK:       REMOTE_SRV:   0. 0 %
CPU: mcu2_0: TASK:        LOAD_TEST:   0. 0 %
CPU: mcu2_0: TASK:         TIVX_CPU:   0. 0 %
CPU: mcu2_0: TASK:          TIVX_NF:   0. 0 %
CPU: mcu2_0: TASK:        TIVX_LDC1:   0. 0 %
CPU: mcu2_0: TASK:        TIVX_MSC1:   0. 0 %
CPU: mcu2_0: TASK:        TIVX_MSC2:   0. 0 %
CPU: mcu2_0: TASK:       TIVX_VISS1:   0. 0 %
CPU: mcu2_0: TASK:       TIVX_CAPT1:   0. 0 %
CPU: mcu2_0: TASK:       TIVX_CAPT2:   0. 0 %
CPU: mcu2_0: TASK:       TIVX_DISP1:   0. 0 %
CPU: mcu2_0: TASK:       TIVX_DISP2:   0. 0 %
CPU: mcu2_0: TASK:       TIVX_CSITX:   0. 0 %
CPU: mcu2_0: TASK:       TIVX_CAPT3:   0. 0 %
CPU: mcu2_0: TASK:       TIVX_CAPT4:   0. 0 %

CPU: mcu2_0: HEAP:   DDR_SHARED_MEM: size =   16777216 B, free =   16712448 B ( 99 % unused)
CPU: mcu2_0: HEAP:           L3_MEM: size =     131072 B, free =     131072 B (100 % unused)
CPU: mcu2_0: HEAP:  DDR_NON_CACHE_M: size =   16777216 B, free =   16777216 B (100 % unused)

CPU: mcu2_1: TASK:           IPC_RX:   0. 0 %
CPU: mcu2_1: TASK:       REMOTE_SRV:   0. 0 %
CPU: mcu2_1: TASK:        LOAD_TEST:   0. 0 %
CPU: mcu2_1: TASK:         TIVX_SDE:   0. 0 %
CPU: mcu2_1: TASK:         TIVX_DOF:   0. 0 %
CPU: mcu2_1: TASK:       TIVX_VDEC1:   0. 0 %
CPU: mcu2_1: TASK:       TIVX_VDEC2:   0. 0 %
CPU: mcu2_1: TASK:       TIVX_VENC1:   0. 0 %
CPU: mcu2_1: TASK:       TIVX_VENC2:   0. 0 %
CPU: mcu2_1: TASK:      IPC_TEST_RX:   0. 0 %
CPU: mcu2_1: TASK:      IPC_TEST_TX:   0. 0 %
CPU: mcu2_1: TASK:      IPC_TEST_TX:   0. 0 %
CPU: mcu2_1: TASK:      IPC_TEST_TX:   0. 0 %
CPU: mcu2_1: TASK:      IPC_TEST_TX:   0. 0 %
CPU: mcu2_1: TASK:      IPC_TEST_TX:   0. 0 %

CPU: mcu2_1: HEAP:   DDR_SHARED_MEM: size =   16777216 B, free =   16774912 B ( 99 % unused)
CPU: mcu2_1: HEAP:           L3_MEM: size =     131072 B, free =     131072 B (100 % unused)
CPU: mcu2_1: HEAP:  DDR_NON_CACHE_M: size =  117440512 B, free =   97542144 B (  9 % unused)

CPU:  c6x_1: TASK:           IPC_RX:   0. 0 %
CPU:  c6x_1: TASK:       REMOTE_SRV:   0. 0 %
CPU:  c6x_1: TASK:        LOAD_TEST:   0. 0 %
CPU:  c6x_1: TASK:         TIVX_CPU:   0. 0 %
CPU:  c6x_1: TASK:      IPC_TEST_RX:   0. 0 %
CPU:  c6x_1: TASK:      IPC_TEST_TX:   0. 0 %
CPU:  c6x_1: TASK:      IPC_TEST_TX:   0. 0 %
CPU:  c6x_1: TASK:      IPC_TEST_TX:   0. 0 %
CPU:  c6x_1: TASK:      IPC_TEST_TX:   0. 0 %
CPU:  c6x_1: TASK:      IPC_TEST_TX:   0. 0 %

CPU:  c6x_1: HEAP:   DDR_SHARED_MEM: size =   16777216 B, free =   16774912 B ( 99 % unused)
CPU:  c6x_1: HEAP:           L2_MEM: size =     229376 B, free =     229376 B (100 % unused)
CPU:  c6x_1: HEAP:  DDR_SCRATCH_MEM: size =   50331648 B, free =   50331648 B ( 14 % unused)

CPU:  c6x_2: TASK:           IPC_RX:   0. 0 %
CPU:  c6x_2: TASK:       REMOTE_SRV:   0. 0 %
CPU:  c6x_2: TASK:        LOAD_TEST:   0. 0 %
CPU:  c6x_2: TASK:         TIVX_CPU:   0. 0 %
CPU:  c6x_2: TASK:      IPC_TEST_RX:   0. 0 %
CPU:  c6x_2: TASK:      IPC_TEST_TX:   0. 0 %
CPU:  c6x_2: TASK:      IPC_TEST_TX:   0. 0 %
CPU:  c6x_2: TASK:      IPC_TEST_TX:   0. 0 %
CPU:  c6x_2: TASK:      IPC_TEST_TX:   0. 0 %
CPU:  c6x_2: TASK:      IPC_TEST_TX:   0. 0 %

CPU:  c6x_2: HEAP:   DDR_SHARED_MEM: size =   16777216 B, free =   16774912 B ( 99 % unused)
CPU:  c6x_2: HEAP:           L2_MEM: size =     229376 B, free =     229376 B (100 % unused)
CPU:  c6x_2: HEAP:  DDR_SCRATCH_MEM: size =   50331648 B, free =   50331648 B ( 14 % unused)

CPU:  c7x_1: TASK:           IPC_RX:   0. 0 %
CPU:  c7x_1: TASK:       REMOTE_SRV:   0. 0 %
CPU:  c7x_1: TASK:        LOAD_TEST:   0. 0 %
CPU:  c7x_1: TASK:         TIVX_CPU:   0. 0 %
CPU:  c7x_1: TASK:      IPC_TEST_RX:   0. 0 %
CPU:  c7x_1: TASK:      IPC_TEST_TX:   0. 0 %
CPU:  c7x_1: TASK:      IPC_TEST_TX:   0. 0 %
CPU:  c7x_1: TASK:      IPC_TEST_TX:   0. 0 %
CPU:  c7x_1: TASK:      IPC_TEST_TX:   0. 0 %
CPU:  c7x_1: TASK:      IPC_TEST_TX:   0. 0 %

CPU:  c7x_1: HEAP:   DDR_SHARED_MEM: size = 1073741824 B, free = 1073741824 B (  0 % unused)
CPU:  c7x_1: HEAP:           L3_MEM: size =    8159232 B, free =    8159232 B (100 % unused)
CPU:  c7x_1: HEAP:           L2_MEM: size =     491520 B, free =     491520 B (100 % unused)
CPU:  c7x_1: HEAP:           L1_MEM: size =      16384 B, free =      16384 B (100 % unused)
CPU:  c7x_1: HEAP:  DDR_SCRATCH_MEM: size =  100663296 B, free =  100663296 B ( 14 % unused)


GRAPH:         graph_85 (#nodes =   2, #executions =      0)
 NODE:   CAPTURE2:                  node_96: avg =      0 usecs, min/max = 18446744073709551 /      0 usecs, #executions =          0
 NODE:   DISPLAY1:                  node_97: avg =      0 usecs, min/max = 18446744073709551 /      0 usecs, #executions =          0

 PERF:            TOTAL: avg =      0 usecs, min/max = 4294967295 /      0 usecs, #executions =          0

 PERF:            TOTAL:    0. 0 FPS

CSIRX 似乎没有接收到信号、但我不知道为什么、所有更改看起来都是正确的

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我已经解决了这个问题

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您能帮助我们了解哪些改变使其正常工作吗? 是否需要在驱动程序/设置/配置中进行任何更改?

    此致、

    Brijesh

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Brijesh、

    实际上、我没有完全解决这个问题

    我使用了 Fvid2接口 并 成功获得了图像、 这对我来说已经足够了。另一方面、我认为 CSIRX 驱动程序工作正常、因此给传感器 drv 剂量。 在 single_cam 演示中、可能有问题。您对此有什么想法吗? 谢谢。

    此致、

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    赵好、

     您使用的是哪个 SDK 版本? 在早期 SDK 版本中、假设通道速度为1.5Gbps。 您需要更改代码以更新其他通道速度。  

    此致、

    Brijesh

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好 、Brijesh、

    SDK Ver 7.3中、我更新了通道速度、但仍然无法正常工作。在什么情况下会将 vxGraphParameterEnqueueReadyRef 占用?

    此致,

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    赵好、

    vxGraphParameterEnqueeReadyRef API 不应卡住。 通常情况下、由于捕获不起作用、我已经看到 DequeDoneRef 卡滞。 但是 EnqueueReadyRef 只是为节点提供新的缓冲区。

    您确定它是 EnqueueReadyRef 吗?

    此致、

    Brijesh

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好  Brijesh,

    [报价 userid="80721" URL"~/support/processors-group/processors/f/processors-forum/1047240/tda4vm-csirx-problem-with-vxgraphparameterenqueuereadyref/3875685 #3875685"]您确定它是 EnqueueReadyRef 吗?

    是的,我确定。 我在 函数 app_run_graph 中进行了一些调试打印。  

    [引用 userid="80721" URL"~/support/processors-group/processors/f/processors-forum/1047240/tda4vm-csirx-problem-with-vxgraphparameterenqueuereadyref/3875685 #3875685"] EnqueueReadyRef 仅为节点提供新的缓冲区。

    我将检查我所做的所有更改、以查看这些更改是否会解决问题。

    谢谢。

    此致、

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Brijesh、

    我仍然不知道 为什么 EnqueueReadyRef 被占用。 我 使用 fvid2接口获得了正确的图像。 因此、这意味着 CSIRX 是正确的、传感器驱动器也是正确的。

    图像大小为4K@30 YUV。 因此、在单个凸轮演示中、VISS&LDC 状态为禁用(LDC&VISS 不支持 YUV)、 只剩下捕获节点和显示节点。 由于分频器不工作,显示节点也不应工作。 基于这些、只能使用捕获节点、我可能通过命令"SAVE"获取映像。 但它被吸入函数  EnqueueReadyRef 。

    1.如何确认捕获节点工作正常?

    2.我 是否正确操作了 single_cam? (可能只有捕获节点工作)

    我只想先获取图像。 在我获得正确的图像后、将添加着色空间和定标器。

    希望您能回答。

    谢谢。

     

    此致、

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    赵好、

    在共享代码中、捕获输出分辨率是多少? 您提到捕获是 YUV422格式、LDC 使能标志设置为 false。 在代码中、我看到以下情况、这意味着如果捕获分辨率不是显示分辨率、它将启用标量、但 标量不支持 YUV422格式。 能否确保在图形中禁用标量? 因此捕获输出应直接连接到显示屏。

    否则((image_width!= obj->display_params.outWidth)||(image_height!= obj->display_params.outHeight))

      obj->scaler_enable = vx_tru_e;

    哪个排队参考呼叫被卡住? 它是否位于下方? 此外,代码中是否启用了测试模式(obj->test_mode)?  

    app_printf ("11111111 vxGraphParameterEnqueueReadyRef\n");
    status = vxGraphParameterEnqueueReadyRef (obj->graph, 0、(vx_reference*)&(obj->cap_frames[buf_id])、1);
    app_printf ("2222222222 vxGraphParameterEnqueeReadyRef\n");

    您能否检查是否在以下代码中正确分配了所有对象数组?

    for (buf_id=0;buf_id num_cap_buf;buf_id++)

      if (status == vx_Success)
      {
        obj->cap_frames[buf_id]= vxCreateObjectArray (obj->context、(vx_reference) capt_yuV_image、num_caption_frames);
        status = vxGetStatus (((vx_reference) obj->cap_frames[buf_id]);
      }

    此致、

    Brijesh

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Brijesh、

    感谢您的回复。

    1。

    [引用 userid="80721" URL"~/support/processors-group/processors/f/processors-forum/1047240/tda4vm-csirx-problem-with-vxgraphparameterenqueuereadyref/3884398 #3884398"]

    能否确保在图形中禁用标量? 因此捕获输出应直接连接到显示屏。

    否则((image_width!= obj->display_params.outWidth)||(image_height!= obj->display_params.outHeight))

      obj->scaler_enable = vx_tru_e;

    [/报价]

    禁用定标器。 由于 obj->cat_yuV_image 不是 NULL、因此 scaler_enable = vx_false_e

    if (NULL!= obj->capt_yuV_image)

    /*MSC 不支持 YUV422输入*/
    obj->scaler_enable = vx_false;

    否则((image_width!= obj->display_params.outWidth)||(image_height!= obj->display_params.outHeight))

    obj->scaler_enable = vx_tru_e;

    2.

    [引用 userid="80721" URL"~/support/processors-group/processors/f/processors-forum/1047240/tda4vm-csirx-problem-with-vxgraphparameterenqueuereadyref/3884398 #3884398">您是否还在代码中启用了测试模式(obj->test_mode)?  [/报价]

    测试模式被禁用。

    3.

    [报价 userid="80721" URL"~/support/processors-group/processors/f/processors-forum/1047240/tda4vm-csirx-problem-with-vxgraphparameterenqueuereadyref/3884398 #3884398"]是否还可以检查是否在以下代码中正确分配了所有对象数组?

    Allocate 的状态为0。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    以下是日志:

    e2e.ti.com/.../1817.log.txt

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我还在 tivxCaptureProcess,中添加了一些打印内容,但程序从未出现,看起来 captureProcess 从未运行。 所以 fvid2没有启动并且排队

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Brijesh、

    好消息、我们现在可以成功获取映像。此问题是由于 TIvxCaptureProcess 未运行。 我们编辑了 Linux 内核中的 mm.c 来修复总线错误问题、但此更改以某种方式影响了进程的运行。我将启动有关总线错误问题的新线程。此问题将关闭。感谢您的帮助。

    此致、