This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] DRA821U:DRA821:CPSW5G 在 SDK8.0中不起作用

Guru**** 2555630 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1045832/dra821u-dra821-cpsw5g-does-not-work-in-sdk8-0

器件型号:DRA821U

您好 TI!

在 TI EVM 板中 、默认编译并下载 sdk8.0后、cpsw5g 不会链接。
接口'eth1'可见、但 ping 不起作用。
看起来 Phy 驱动程序没有注册。

以太网固件加载到目标中。
root@j7200-EVM:~# ls /lib/firmware/ethfw
app_remotesmifcfg_server_strip.xer5f

1) 1)是否有可在日志中检查的日志?
2) 2)是否有可在 Linux 提示符下检查的命令?
3) 3)如果未加载 cpsw5g 的固件、则修复点在哪里?

下面是内核日志。 我可以寻求帮助吗?
谢谢你。

U-Boot SPL 2021.01 (Oct 19 2021 - 08:47:23 +0900)
Model: Texas Instruments K3 J7200 SoC
Board: J7200X-PM2-SOM rev E6
SYSFW ABI: 3.1 (firmware rev 0x0015 '21.5.0--v2021.05 (Terrific Llam')
Trying to boot from MMC1
init_env from device 17 not supported!
Starting ATF on ARM64 core...

NOTICE:  BL31: v2.5(release):08.00.00.004-dirty
NOTICE:  BL31: Built : 07:25:50, Aug  7 2021

U-Boot SPL 2021.01 (Oct 19 2021 - 08:47:07 +0900)
Model: Texas Instruments K3 J7200 SoC
Board: J7200X-PM2-SOM rev E6
SYSFW ABI: 3.1 (firmware rev 0x0015 '21.5.0--v2021.05 (Terrific Llam')
Detected: J7X-BASE-CPB rev E3
Detected: J7X-GESI-EXP rev E3
Detected: J7X-VSC8514-ETH rev E2
Trying to boot from MMC1


U-Boot 2021.01 (Oct 19 2021 - 08:47:07 +0900)

SoC:   J7200 SR1.0
Model: Texas Instruments K3 J7200 SoC
Board: J7200X-PM2-SOM rev E6
DRAM:  4 GiB
Flash: 0 Bytes
MMC:   sdhci@4f80000: 0, sdhci@4fb0000: 1
Loading Environment from MMC... OK
In:    serial@2800000
Out:   serial@2800000
Err:   serial@2800000
Detected: J7X-BASE-CPB rev E3
Detected: J7X-GESI-EXP rev E3
Detected: J7X-VSC8514-ETH rev E2
Net:   am65_cpsw_nuss_slave ethernet@46000000: K3 CPSW: nuss_ver: 0x6BA02102 cpsw_ver: 0x6BA82102 ale_ver: 0x00293904 Ports:1 mdio_freq:1000000
eth0: ethernet@46000000
Hit any key to stop autoboot:  0
switch to partitions #0, OK
mmc0(part 0) is current device
SD/MMC found on device 0
fs_devread read outside partition 6992
Failed to load 'boot.scr'
** Unrecognized filesystem type **
19137024 bytes read in 56 ms (325.9 MiB/s)
45267 bytes read in 2 ms (21.6 MiB/s)
## Flattened Device Tree blob at 88000000
   Booting using the fdt blob at 0x88000000
   Loading Device Tree to 000000008fef1000, end 000000008fffffff ... OK

Starting kernel ...

[    0.000000] Booting Linux on physical CPU 0x0000000000 [0x411fd080]
[    0.000000] Linux version 5.10.41-g4c2eade9f7 (dongsukkim@auto-dev131) (aarch64-none-linux-gnu-gcc (GNU Toolchain for the A-profile Architecture 9.2-2019.12 (arm-9.10)) 9.2.1 20191025, GNU ld (GNU Toolchain for the A-profile Architecture 9.2-2019.12 (arm-9.10)) 2.33.1.20191209) #1 SMP PREEMPT Mon Oct 18 16:54:00 KST 2021
[    0.000000] Machine model: Texas Instruments K3 J7200 SoC
[    0.000000] earlycon: ns16550a0 at MMIO32 0x0000000002800000 (options '')
[    0.000000] printk: bootconsole [ns16550a0] enabled
[    0.000000] efi: UEFI not found.
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a0000000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node r5f-dma-memory@a0000000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a0100000, size 15 MiB
[    0.000000] OF: reserved mem: initialized node r5f-memory@a0100000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a1000000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node r5f-dma-memory@a1000000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a1100000, size 15 MiB
[    0.000000] OF: reserved mem: initialized node r5f-memory@a1100000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a2000000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node r5f-dma-memory@a2000000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a2100000, size 15 MiB
[    0.000000] OF: reserved mem: initialized node r5f-memory@a2100000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a3000000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node r5f-dma-memory@a3000000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a3100000, size 15 MiB
[    0.000000] OF: reserved mem: initialized node r5f-memory@a3100000, compatible id shared-dma-pool
[    0.000000] Zone ranges:
[    0.000000]   DMA      [mem 0x0000000080000000-0x00000000ffffffff]
[    0.000000]   DMA32    empty
[    0.000000]   Normal   [mem 0x0000000100000000-0x00000008ffffffff]
[    0.000000] Movable zone start for each node
[    0.000000] Early memory node ranges
[    0.000000]   node   0: [mem 0x0000000080000000-0x000000009e7fffff]
[    0.000000]   node   0: [mem 0x000000009e800000-0x00000000a47fffff]
[    0.000000]   node   0: [mem 0x00000000a4800000-0x00000000ffffffff]
[    0.000000]   node   0: [mem 0x0000000880000000-0x00000008ffffffff]
[    0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000008ffffffff]
[    0.000000] cma: Reserved 512 MiB at 0x00000000e0000000
[    0.000000] psci: probing for conduit method from DT.
[    0.000000] psci: PSCIv1.1 detected in firmware.
[    0.000000] psci: Using standard PSCI v0.2 function IDs
[    0.000000] psci: Trusted OS migration not required
[    0.000000] psci: SMC Calling Convention v1.2
[    0.000000] percpu: Embedded 2 pages/cpu s49880 r8192 d73000 u131072
[    0.000000] Detected PIPT I-cache on CPU0
[    0.000000] CPU features: detected: GIC system register CPU interface
[    0.000000] CPU features: detected: EL2 vector hardening
[    0.000000] CPU features: detected: ARM errata 1165522, 1319367, or 1530923
[    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 65472
[    0.000000] Kernel command line: console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000 mtdparts=47040000.spi.0:1m(ospi.tiboot3),2m(ospi.tispl),4m(ospi.u-boot),256k(ospi.env),256k(ospi.env.backup),57088k@8m(ospi.rootfs),256k(ospi.phypattern);47034000.hyperbus:1m(hbmc.tiboot3),2m(hbmc.tispl),4m(hbmc.u-boot),256k(hbmc.env),-@8m(hbmc.rootfs) root=PARTUUID=708b7f8e-b653-f04c-a041-3abacf3dd9b1 rw rootfstype=ext4 rootwait
[    0.000000] Dentry cache hash table entries: 524288 (order: 6, 4194304 bytes, linear)
[    0.000000] Inode-cache hash table entries: 262144 (order: 5, 2097152 bytes, linear)
[    0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
[    0.000000] software IO TLB: mapped [mem 0x00000000dc000000-0x00000000e0000000] (64MB)
[    0.000000] Memory: 3474688K/4194304K available (10816K kernel code, 1344K rwdata, 4288K rodata, 1856K init, 758K bss, 195328K reserved, 524288K cma-reserved)
[    0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
[    0.000000] rcu: Preemptible hierarchical RCU implementation.
[    0.000000] rcu:     RCU event tracing is enabled.
[    0.000000] rcu:     RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=2.
[    0.000000]  Trampoline variant of Tasks RCU enabled.
[    0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[    0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2
[    0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[    0.000000] GICv3: GIC: Using split EOI/Deactivate mode
[    0.000000] GICv3: 960 SPIs implemented
[    0.000000] GICv3: 0 Extended SPIs implemented
[    0.000000] GICv3: Distributor has no Range Selector support
[    0.000000] GICv3: 16 PPIs implemented
[    0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000001900000
[    0.000000] ITS [mem 0x01820000-0x0182ffff]
[    0.000000] GIC: enabling workaround for ITS: Socionext Synquacer pre-ITS
[    0.000000] ITS@0x0000000001820000: allocated 1048576 Devices @880800000 (flat, esz 8, psz 64K, shr 0)
[    0.000000] ITS: using cache flushing for cmd queue
[    0.000000] GICv3: using LPI property table @0x00000008800b0000
[    0.000000] GIC: using cache flushing for LPI property table
[    0.000000] GICv3: CPU0: using allocated LPI pending table @0x00000008800c0000
[    0.000000] random: get_random_bytes called from start_kernel+0x32c/0x4d4 with crng_init=0
[    0.000000] arch_timer: cp15 timer(s) running at 200.00MHz (phys).
[    0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x2e2049d3e8, max_idle_ns: 440795210634 ns
[    0.000002] sched_clock: 56 bits at 200MHz, resolution 5ns, wraps every 4398046511102ns
[    0.008289] Console: colour dummy device 80x25
[    0.012851] Calibrating delay loop (skipped), value calculated using timer frequency.. 400.00 BogoMIPS (lpj=800000)
[    0.023522] pid_max: default: 32768 minimum: 301
[    0.028270] LSM: Security Framework initializing
[    0.033021] Mount-cache hash table entries: 8192 (order: 0, 65536 bytes, linear)
[    0.040598] Mountpoint-cache hash table entries: 8192 (order: 0, 65536 bytes, linear)
[    0.050154] rcu: Hierarchical SRCU implementation.
[    0.055336] Platform MSI: msi-controller@1820000 domain created
[    0.061516] PCI/MSI: /bus@100000/interrupt-controller@1800000/msi-controller@1820000 domain created
[    0.070802] EFI services will not be available.
[    0.075637] smp: Bringing up secondary CPUs ...
[    0.080994] Detected PIPT I-cache on CPU1
[    0.081019] GICv3: CPU1: found redistributor 1 region 0:0x0000000001920000
[    0.081032] GICv3: CPU1: using allocated LPI pending table @0x00000008800d0000
[    0.081072] CPU1: Booted secondary processor 0x0000000001 [0x411fd080]
[    0.081157] smp: Brought up 1 node, 2 CPUs
[    0.110517] SMP: Total of 2 processors activated.
[    0.115324] CPU features: detected: 32-bit EL0 Support
[    0.120581] CPU features: detected: CRC32 instructions
[    0.134155] CPU: All CPU(s) started at EL2
[    0.138362] alternatives: patching kernel code
[    0.143516] devtmpfs: initialized
[    0.149757] KASLR disabled due to lack of seed
[    0.154488] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[    0.164462] futex hash table entries: 512 (order: -1, 32768 bytes, linear)
[    0.172261] pinctrl core: initialized pinctrl subsystem
[    0.177898] DMI not present or invalid.
[    0.182197] NET: Registered protocol family 16
[    0.189992] DMA: preallocated 512 KiB GFP_KERNEL pool for atomic allocations
[    0.197373] DMA: preallocated 512 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
[    0.205430] DMA: preallocated 512 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
[    0.213800] thermal_sys: Registered thermal governor 'step_wise'
[    0.213804] thermal_sys: Registered thermal governor 'power_allocator'
[    0.220186] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[    0.233852] ASID allocator initialised with 65536 entries
[    0.250541] HugeTLB registered 16.0 GiB page size, pre-allocated 0 pages
[    0.257401] HugeTLB registered 512 MiB page size, pre-allocated 0 pages
[    0.264160] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages
[    0.273713] cryptd: max_cpu_qlen set to 1000
[    0.281193] k3-chipinfo 43000014.chipid: Family:J7200 rev:SR1.0 JTAGID[0x0bb6d02f] Detected
[    0.290137] vsys_3v3: supplied by evm_12v0
[    0.294495] vsys_5v0: supplied by evm_12v0
[    0.299154] iommu: Default domain type: Translated
[    0.304366] SCSI subsystem initialized
[    0.308555] mc: Linux media interface: v0.10
[    0.312942] videodev: Linux video capture interface: v2.00
[    0.318582] pps_core: LinuxPPS API ver. 1 registered
[    0.323654] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[    0.332994] PTP clock support registered
[    0.337015] EDAC MC: Ver: 3.0.0
[    0.340900] FPGA manager framework
[    0.344447] Advanced Linux Sound Architecture Driver Initialized.
[    0.351210] clocksource: Switched to clocksource arch_sys_counter
[    0.357680] VFS: Disk quotas dquot_6.6.0
[    0.361759] VFS: Dquot-cache hash table entries: 8192 (order 0, 65536 bytes)
[    0.371972] NET: Registered protocol family 2
[    0.376748] IP idents hash table entries: 65536 (order: 3, 524288 bytes, linear)
[    0.385638] tcp_listen_portaddr_hash hash table entries: 4096 (order: 0, 65536 bytes, linear)
[    0.394463] TCP established hash table entries: 32768 (order: 2, 262144 bytes, linear)
[    0.402677] TCP bind hash table entries: 32768 (order: 3, 524288 bytes, linear)
[    0.410646] TCP: Hash tables configured (established 32768 bind 32768)
[    0.417499] UDP hash table entries: 2048 (order: 0, 65536 bytes, linear)
[    0.424407] UDP-Lite hash table entries: 2048 (order: 0, 65536 bytes, linear)
[    0.431846] NET: Registered protocol family 1
[    0.436760] RPC: Registered named UNIX socket transport module.
[    0.442825] RPC: Registered udp transport module.
[    0.447631] RPC: Registered tcp transport module.
[    0.452436] RPC: Registered tcp NFSv4.1 backchannel transport module.
[    0.459021] PCI: CLS 0 bytes, default 64
[    0.463412] hw perfevents: enabled with armv8_cortex_a72 PMU driver, 7 counters available
[    0.475460] Initialise system trusted keyrings
[    0.480152] workingset: timestamp_bits=46 max_order=16 bucket_order=0
[    0.488690] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[    0.495032] NFS: Registering the id_resolver key type
[    0.500224] Key type id_resolver registered
[    0.504498] Key type id_legacy registered
[    0.508633] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[    0.515485] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...
[    0.523166] 9p: Installing v9fs 9p2000 file system support
[    0.547952] Key type asymmetric registered
[    0.552150] Asymmetric key parser 'x509' registered
[    0.557161] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 243)
[    0.564722] io scheduler mq-deadline registered
[    0.569348] io scheduler kyber registered
[    0.574514] pinctrl-single 4301c000.pinctrl: 94 pins, size 376
[    0.580756] pinctrl-single 11c000.pinctrl: 173 pins, size 692
[    0.588991] k3-ringacc 2b800000.ringacc: Failed to get MSI domain
[    0.595321] k3-ringacc 3c000000.ringacc: Failed to get MSI domain
[    0.603185] Serial: 8250/16550 driver, 10 ports, IRQ sharing enabled
[    0.617301] brd: module loaded
[    0.624974] loop: module loaded
[    0.628619] megasas: 07.714.04.00-rc1
[    0.633540] libphy: Fixed MDIO Bus: probed
[    0.638270] tun: Universal TUN/TAP device driver, 1.6
[    0.643741] igbvf: Intel(R) Gigabit Virtual Function Network Driver
[    0.650157] igbvf: Copyright (c) 2009 - 2012 Intel Corporation.
[    0.656236] sky2: driver version 1.30
[    0.660556] VFIO - User Level meta-driver version: 0.3
[    0.666336] i2c /dev entries driver
[    0.670448] sdhci: Secure Digital Host Controller Interface driver
[    0.676785] sdhci: Copyright(c) Pierre Ossman
[    0.681410] sdhci-pltfm: SDHCI platform and OF driver helper
[    0.687686] ledtrig-cpu: registered to indicate activity on CPUs
[    0.694066] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping ....
[    0.701319] optee: probing for conduit method.
[    0.705895] optee: revision 3.12 (3d47a131)
[    0.706230] optee: initialized driver
[    0.715603] NET: Registered protocol family 17
[    0.720238] 9pnet: Installing 9P2000 support
[    0.724644] Key type dns_resolver registered
[    0.729115] Loading compiled-in X.509 certificates
[    0.738926] k3-ringacc 2b800000.ringacc: Failed to get MSI domain
[    0.745367] k3-ringacc 3c000000.ringacc: Failed to get MSI domain
[    0.753307] ti-sci 44083000.dmsc: ABI: 3.1 (firmware rev 0x0015 '21.5.0--v2021.05 (Terrific Llam')
[    0.777795] omap_i2c 40b00000.i2c: bus 0 rev0.12 at 100 kHz
[    0.784067] omap_i2c 40b10000.i2c: bus 1 rev0.12 at 100 kHz
[    0.790338] omap_i2c 42120000.i2c: bus 2 rev0.12 at 100 kHz
[    0.796789] pca953x 3-0021: supply vcc not found, using dummy regulator
[    0.803644] pca953x 3-0021: using no AI
[    0.831759] pca953x 3-0020: supply vcc not found, using dummy regulator
[    0.838598] pca953x 3-0020: using no AI
[    0.843197] pca953x 3-0022: supply vcc not found, using dummy regulator
[    0.850039] pca953x 3-0022: using AI
[    0.854135] random: fast init done
[    0.857898] omap_i2c 2000000.i2c: bus 3 rev0.12 at 400 kHz
[    0.864281] pca953x 4-0020: supply vcc not found, using dummy regulator
[    0.871170] pca953x 4-0020: using no AI
[    0.895615] omap_i2c 2010000.i2c: bus 4 rev0.12 at 400 kHz
[    0.901871] omap_i2c 2020000.i2c: bus 5 rev0.12 at 100 kHz
[    0.908052] omap_i2c 2030000.i2c: bus 6 rev0.12 at 100 kHz
[    0.914233] omap_i2c 2040000.i2c: bus 7 rev0.12 at 100 kHz
[    0.920440] omap_i2c 2050000.i2c: bus 8 rev0.12 at 100 kHz
[    0.926604] omap_i2c 2060000.i2c: bus 9 rev0.12 at 100 kHz
[    0.932799] ti-sci-intr bus@100000:bus@28380000:interrupt-controller2: Interrupt Router 137 domain created
[    0.942812] ti-sci-intr bus@100000:interrupt-controller0: Interrupt Router 131 domain created
[    0.951637] ti-sci-intr bus@100000:bus@30000000:interrupt-controller1: Interrupt Router 213 domain created
[    0.961664] ti-sci-inta 33d00000.msi-controller: Interrupt Aggregator domain 209 created
[    0.971494] j721e-pcie 2910000.pcie: host bridge /bus@100000/pcie@2910000 ranges:
[    0.979184] j721e-pcie 2910000.pcie:       IO 0x0018001000..0x0018010fff -> 0x0018001000
[    0.987464] j721e-pcie 2910000.pcie:      MEM 0x0018011000..0x001fffffff -> 0x0018011000
[    0.995747] j721e-pcie 2910000.pcie:   IB MEM 0x0000000000..0xffffffffffff -> 0x0000000000
[    2.011813] j721e-pcie 2910000.pcie: PCI host bridge to bus 0000:00
[    2.018256] pci_bus 0000:00: root bus resource [bus 00-0f]
[    2.023868] pci_bus 0000:00: root bus resource [io  0x0000-0xffff] (bus address [0x18001000-0x18010fff])
[    2.033560] pci_bus 0000:00: root bus resource [mem 0x18011000-0x1fffffff]
[    2.040613] pci 0000:00:00.0: [104c:b00f] type 01 class 0x060400
[    2.046833] pci 0000:00:00.0: supports D1
[    2.050930] pci 0000:00:00.0: PME# supported from D0 D1 D3hot
[    2.057648] pci 0000:00:00.0: bridge configuration invalid ([bus 00-00]), reconfiguring
[    2.066571] pci_bus 0000:01: busn_res: [bus 01-0f] end is updated to 01
[    2.073349] pci 0000:00:00.0: PCI bridge to [bus 01]
[    2.078682] pcieport 0000:00:00.0: PME: Signaling with IRQ 36
[    2.085841] k3-ringacc 2b800000.ringacc: Ring Accelerator probed rings:286, gp-rings[96,32] sci-dev-id:235
[    2.095759] k3-ringacc 2b800000.ringacc: dma-ring-reset-quirk: disabled
[    2.102523] k3-ringacc 2b800000.ringacc: RA Proxy rev. 66349100, num_proxies:64
[    2.112215] k3-ringacc 3c000000.ringacc: Ring Accelerator probed rings:1024, gp-rings[120,200] sci-dev-id:211
[    2.122384] k3-ringacc 3c000000.ringacc: dma-ring-reset-quirk: disabled
[    2.129145] k3-ringacc 3c000000.ringacc: RA Proxy rev. 66349100, num_proxies:64
[    2.137174] 40a00000.serial: ttyS1 at MMIO 0x40a00000 (irq = 15, base_baud = 6000000) is a 8250
[    2.146751] 2800000.serial: ttyS2 at MMIO 0x2800000 (irq = 22, base_baud = 3000000) is a 8250
[    2.155515] printk: console [ttyS2] enabled
[    2.155515] printk: console [ttyS2] enabled
[    2.163954] printk: bootconsole [ns16550a0] disabled
[    2.163954] printk: bootconsole [ns16550a0] disabled
[    2.174600] 2810000.serial: ttyS3 at MMIO 0x2810000 (irq = 23, base_baud = 3000000) is a 8250
[    2.351217] davinci_mdio 46000f00.mdio: davinci mdio revision 9.7, bus freq 20000
[    2.358700] libphy: 46000f00.mdio: probed
[    2.386914] davinci_mdio 46000f00.mdio: phy[0]: device 46000f00.mdio:00, driver TI DP83867
[    2.395256] am65-cpsw-nuss 46000000.ethernet: initializing am65 cpsw nuss version 0x6BA02102, cpsw version 0x6BA82102 Ports: 2 quirks:00000000
[    2.410630] am65-cpts 310d0000.cpts: CPTS ver 0x4e8a010b, freq:200000000, add_val:4 pps:0
[    2.419699] mmc0: CQHCI version 5.10
[    2.427703] vdd_mmc1: supplied by vsys_3v3
[    2.432456] omap-mailbox 31f80000.mailbox: omap mailbox rev 0x66fc8900
[    2.439378] omap-mailbox 31f81000.mailbox: omap mailbox rev 0x66fc8900
[    2.446537] ti-udma 285c0000.dma-controller: Channels: 26 (tchan: 13, rchan: 13, gp-rflow: 8)
[    2.456538] ti-udma 31150000.dma-controller: Channels: 50 (tchan: 25, rchan: 25, gp-rflow: 8)
[    2.464478] mmc0: SDHCI controller on 4f80000.mmc [4f80000.mmc] using ADMA 64-bit
[    2.474915] spi-nor spi0.0: s28hs512t (65536 Kbytes)
[    2.479895] 7 cmdlinepart partitions found on MTD device 47040000.spi.0
[    2.486500] Creating 7 MTD partitions on "47040000.spi.0":
[    2.491974] 0x000000000000-0x000000100000 : "ospi.tiboot3"
[    2.498148] 0x000000100000-0x000000300000 : "ospi.tispl"
[    2.504154] 0x000000300000-0x000000700000 : "ospi.u-boot"
[    2.510182] 0x000000700000-0x000000740000 : "ospi.env"
[    2.516021] 0x000000740000-0x000000780000 : "ospi.env.backup"
[    2.522481] 0x000000800000-0x000003fc0000 : "ospi.rootfs"
[    2.528581] 0x000003fc0000-0x000004000000 : "ospi.phypattern"
[    2.560184] mmc0: Command Queue Engine enabled
[    2.564647] mmc0: new HS400 MMC card at address 0001
[    2.570015] mmcblk0: mmc0:0001 S0J56X 14.8 GiB
[    2.574745] mmcblk0boot0: mmc0:0001 S0J56X partition 1 31.5 MiB
[    2.580873] mmcblk0boot1: mmc0:0001 S0J56X partition 2 31.5 MiB
[    2.586913] mmcblk0rpmb: mmc0:0001 S0J56X partition 3 4.00 MiB, chardev (237:0)
[    2.596140]  mmcblk0: p1 p2
[    2.707225] davinci_mdio 46000f00.mdio: davinci mdio revision 9.7, bus freq 20000
[    2.714708] libphy: 46000f00.mdio: probed
[    2.742506] davinci_mdio 46000f00.mdio: phy[0]: device 46000f00.mdio:00, driver TI DP83867
[    2.750838] am65-cpsw-nuss 46000000.ethernet: initializing am65 cpsw nuss version 0x6BA02102, cpsw version 0x6BA82102 Ports: 2 quirks:00000000
[    2.764400] am65-cpsw-nuss 46000000.ethernet: set new flow-id-base 48
[    2.771411] am65-cpsw-nuss 46000000.ethernet: initialized cpsw ale version 1.4
[    2.778644] am65-cpsw-nuss 46000000.ethernet: ALE Table size 64
[    2.785028] am65-cpsw-nuss 46000000.ethernet: CPTS ver 0x4e8a010b, freq:500000000, add_val:1 pps:0
[    2.795137] debugfs: Directory 'pd:240' with parent 'pm_genpd' already present!
[    2.795604] mmc1: CQHCI version 5.10
[    2.808651] ALSA device list:
[    2.811626]   No soundcards found.
[    4.321018] sdhci-am654 4fb0000.mmc: Power on failed
[    4.356650] mmc1: SDHCI controller on 4fb0000.mmc [4fb0000.mmc] using ADMA 64-bit
[    4.494843] EXT4-fs (mmcblk0p2): recovery complete
[    4.500758] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
[    4.508881] VFS: Mounted root (ext4 filesystem) on device 179:2.
[    4.516055] devtmpfs: mounted
[    4.520241] Freeing unused kernel memory: 1856K
[    4.524822] Run /sbin/init as init process
[    4.573615] systemd[1]: System time before build time, advancing clock.
[    4.600514] NET: Registered protocol family 10
[    4.605511] Segment Routing with IPv6
[    4.616467] systemd[1]: systemd 244.5+ running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR -SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN2 -IDN -PCRE2 default-hierarchy=hybrid)
[    4.638323] systemd[1]: Detected architecture arm64.

Welcome to Arago 2020.09!

[    4.679765] systemd[1]: Set hostname to <j7200-evm>.
[    4.848979] systemd[1]: /lib/systemd/system/docker.socket:6: ListenStream= references a path below legacy directory /var/run/, updating /var/run/docker.sock → /run/docker.sock; please update the unit file accordingly.
[    4.915884] random: systemd: uninitialized urandom read (16 bytes read)
[    4.922629] systemd[1]: system-getty.slice: unit configures an IP firewall, but the local system does not support BPF/cgroup firewalling.
[    4.934971] systemd[1]: (This warning is only shown for the first unit using IP firewalling.)
[    4.945354] systemd[1]: Created slice system-getty.slice.
[  OK  ] Created slice system-getty.slice.
[    4.967331] random: systemd: uninitialized urandom read (16 bytes read)
[    4.974856] systemd[1]: Created slice system-serial\x2dgetty.slice.
[  OK  ] Created slice system-serial\x2dgetty.slice.
[    4.995329] random: systemd: uninitialized urandom read (16 bytes read)
[    5.002898] systemd[1]: Created slice system-syslog\x2dng.slice.
[  OK  ] Created slice system-syslog\x2dng.slice.
[    5.024243] systemd[1]: Created slice User and Session Slice.
[  OK  ] Created slice User and Session Slice.
[    5.047503] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
[  OK  ] Started Dispatch Password …ts to Console Directory Watch.
[    5.071447] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
[  OK  ] Started Forward Password R…uests to Wall Directory Watch.
[    5.095408] systemd[1]: Reached target Paths.
[  OK  ] Reached target Paths.
[    5.111339] systemd[1]: Reached target Remote File Systems.
[  OK  ] Reached target Remote File Systems.
[    5.131333] systemd[1]: Reached target Slices.
[  OK  ] Reached target Slices.
[    5.147339] systemd[1]: Reached target Swap.
[  OK  ] Reached target Swap.
[    5.166224] systemd[1]: Listening on RPCbind Server Activation Socket.
[  OK  ] Listening on RPCbind Server Activation Socket.
[    5.187354] systemd[1]: Reached target RPC Port Mapper.
[  OK  ] Reached target RPC Port Mapper.
[    5.209518] systemd[1]: Listening on Process Core Dump Socket.
[  OK  ] Listening on Process Core Dump Socket.
[    5.231507] systemd[1]: Listening on initctl Compatibility Named Pipe.
[  OK  ] Listening on initctl Compatibility Named Pipe.
[    5.259501] systemd[1]: Condition check resulted in Journal Audit Socket being skipped.
[    5.267926] systemd[1]: Listening on Journal Socket (/dev/log).
[  OK  ] Listening on Journal Socket (/dev/log).
[    5.291672] systemd[1]: Listening on Journal Socket.
[  OK  ] Listening on Journal Socket.
[    5.307704] systemd[1]: Listening on Network Service Netlink Socket.
[  OK  ] Listening on Network Service Netlink Socket.
[    5.331661] systemd[1]: Listening on udev Control Socket.
[  OK  ] Listening on udev Control Socket.
[    5.351523] systemd[1]: Listening on udev Kernel Socket.
[  OK  ] Listening on udev Kernel Socket.
[    5.374716] systemd[1]: Mounting Huge Pages File System...
         Mounting Huge Pages File System...
[    5.395151] systemd[1]: Mounting POSIX Message Queue File System...
         Mounting POSIX Message Queue File System...
[    5.422640] systemd[1]: Mounting Kernel Debug File System...
         Mounting Kernel Debug File System...
[    5.449247] systemd[1]: Mounting Temporary Directory (/tmp)...
         Mounting Temporary Directory (/tmp)...
[    5.471490] systemd[1]: Starting Create list of static device nodes for the current kernel...
         Starting Create list of st…odes for the current kernel...
[    5.504121] systemd[1]: Started Hardware RNG Entropy Gatherer Daemon.
[  OK  ] Started Hardware RNG Entropy Gatherer Daemon.
[    5.530828] systemd[1]: Starting RPC Bind...
         Starting RPC Bind...
[    5.547465] systemd[1]: Condition check resulted in File System Check on Root Device being skipped.
[    5.572087] systemd[1]: Starting Journal Service...
         Starting Journal Service...
[    5.596425] systemd[1]: Starting Load Kernel Modules...
         Starting Load Kernel Modules...
[    5.612628] cryptodev: loading out-of-tree module taints kernel.
[    5.626327] systemd[1]: Starting Remount Root and Kernel File Systems...
         Starting Remount Root and Kernel File Systems cryptodev: driver 1.10 loaded.
[0m...
[    5.666013] systemd[1]: Starting udev Coldplug all Devices...
         Starting udev Coldplug all Devices...
[    5.694129] systemd[1]: Started RPC Bind.
[  OK  ] Started RPC Bind.
[    5.716636] systemd[1]: Started Journal Service.
[  OK  ] Started Journal Service.[    5.723976] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)

[  OK  ] Mounted Huge Pages File System.
[  OK  ] Mounted POSIX Message Queue File System.
[  OK  ] Mounted Kernel Debug File System.
[  OK  ] Mounted Temporary Directory (/tmp).
[  OK  ] Started Create list of sta… nodes for the current kernel.
[  OK  ] Started Load Kernel Modules.
[  OK  ] Started Remount Root and Kernel File Systems.
         Mounting Kernel Configuration File System...
         Starting Flush Journal to Persistent Storage...
[    5.901676] systemd-journald[154]: Received client request to flush runtime journal.
         Starting Apply Kernel Variables...
         Starting Create Static Device Nodes in /dev...
[  OK  ] Mounted Kernel Configuration File System.
[  OK  ] Started Flush Journal to Persistent Storage.
[  OK  ] Started Apply Kernel Variables.
[  OK  ] Started Create Static Device Nodes in /dev.
[  OK  ] Reached target Local File Systems (Pre).
         Mounting /media/ram...
         Mounting /var/volatile...
         Starting udev Kernel Device Manager...
[  OK  ] Mounted /media/ram.
[  OK  ] Mounted /var/volatile.
         Starting Load/Save Random Seed...
[  OK  ] Reached target Local File Systems.
         Starting Create Volatile Files and Directories...
[  OK  ] Started udev Kernel Device Manager.
[  OK  ] Started udev Coldplug all Devices.
[  OK  ] Started Create Volatile Files and Directories.
         Starting Network Time Synchronization...
         Starting Update UTMP about System Boot/Shutdown...
[  OK  ] Started Update UTMP about System Boot/Shutdown.
[  OK  ] Started Network Time Synchronization.
[  OK  ] Reached target System Initialization.
[  OK  ] Started Daily Cleanup of Temporary Directories.
[  OK  ] Reached target System Time Set.
[  OK  ] Reached target System Time Synchronized.
[  OK  ] Started Daily rotation of log files.
[  OK  ] Reached target Timers.
[  OK  ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket.
[  OK  ] Listening on D-Bus System Message Bus Socket.
         Starting Docker Socket for the API.
[  OK  ] Listening on dropbear.socket.
         Starting Reboot and dump vmcore via kexec...
[  OK  ] Listening on Docker Socket for the API.
[  OK  ] Started Reboot and dump vmcore via kexec.
[  OK  ] Reached target Sockets.
[  OK  ] Reached target Basic System.
[  OK  ] Started Job spooling tools.
[  OK  ] Started Periodic Command Scheduler.
[  OK  ] Started D-Bus System Message Bus.
         Starting Ethernet Bridge Filtering Tables...
         Starting Print notice about GPLv3 packages...
         Starting IPv6 Packet Filtering Framework...
         Starting IPv4 Packet Filtering Framework...
[  OK  ] Started irqbalance daemon.
         Starting Telephony service...
         Starting System Logger Daemon "default" instance...
         Starting Login Service...
         Starting telnetd.service...
[  OK  ] Started Ethernet Bridge Filtering Tables.
[  OK  ] Started IPv4 Packet Filtering Framework.
[  OK  ] Started IPv6 Packet Filtering Framework.
[  OK  ] Reached target Network (Pre).
         Starting Network Service...
[  OK  ] Started telnetd.service.
         Starting syslog.service...
[  OK  ] Started Telephony service.
[    6.978654] Bluetooth: Core ver 2.22
[    6.982353] NET: Registered protocol family 31
[    6.991248] Bluetooth: HCI device and connection manager initialized
[    7.002078] Bluetooth: HCI socket layer initialized
[    7.007009] Bluetooth: L2CAP socket layer initialized
[    7.014456] Bluetooth: SCO socket layer initialized
[  OK  ] Started Network Service.
         Starting Wait for Network to be Configured...
         Starting Network Name Resolution...
[  OK  ] Started Login Service.
[  OK  ] Started Network Name Resolution.
[  OK  ] Reached target Network.
[  OK  ] Reached target Host and Network Name Lookups.
         Starting Avahi mDNS/DNS-SD Stack...
         Starting Enable and configure wl18xx bluetooth stack...
[  OK  ] Started NFS status monitor for NFSv2/3 locking..
         Starting Simple Network Ma…ent Protocol (SNMP) Daemon....
         Starting Permit User Sessions...
[  OK  ] Started Vsftpd ftp daemon.
[  OK  ] Started Avahi mDNS/DNS-SD Stack.
[  OK  ] Started Enable and configure wl18xx bluetooth stack.
[  OK  ] Started Permit User Sessions.
[  OK  ] Started Getty on tty1.
[  OK  ] Started Serial Getty on ttyS2.
[  OK  ] Started Serial Getty on ttyS3.
[  OK  ] Reached target Login Prompts.
         Starting Synchronize System and HW clocks...
[FAILED] Failed to start Synchronize System and HW clocks.
See 'systemctl status sync-clocks.service' for details.
[    8.111260] random: crng init done
[    8.114663] random: 7 urandom warning(s) missed due to ratelimiting
[  OK  ] Started Load/Save Random Seed.
[  OK  ] Started System Logger Daemon "default" instance.
[  OK  ] Started syslog.service.
[  OK  ] Started Simple Network Man…ement Protocol (SNMP) Daemon..
[    8.639301] ti-udma 285c0000.dma-controller: chan1: is running!
[    9.027366] platform 41000000.r5f: R5F core may have been powered on by a different host, programmed state (0) != actual state (1)
[    9.273444] platform 41000000.r5f: configured R5F for IPC-only mode
***************************************************************
***************************************************************
NOTICE: This file system contains the following GPLv3 packages:
        autoconf
        bash-dev
        bash
        bc
        binutils
        cifs-utils
        coreutils-stdbuf
        coreutils
        cpio
        cpp-symlinks
        cpp
        dosfsto[    9.378157] platform 41000000.r5f: assigned reserved memory node r5f-dma-memory@a0000000
ols
        elfutils
        g++-symlinks
        g++
        gawk
        gcc-symlinks
        gcc
        gdb
        gdbserver
        gettext
        gstreamer1.0-libav-dev
        gstreamer1.0-libav
        gzip
        less
        libasm1
        libbfd
        libdw1
        libelf1
        libgdbm-compat4
        libgdbm-dev
        libgdbm6
        libgettextlib
        libgettextsrc
        libgmp-dev
        libgmp10
        libgmpxx4
        libidn2-0
        libidn2-dev
        libmpc3
        libmpfr6
        libreadline-dev
        libreadline8
        libunistring-dev
        libunistring2
        m4-dev
        m4
        make
        nettle-dev
        nettle
        parted
        python3-rfc3987
        python3-strict-rfc3339
        tar
        which
        zeromq

If you do not wish to distribute GPLv3 components please remove
the above packages prior to distribution.  This can be done using
the opkg remove command.  i.e.:
    opkg remove <package>
Where <package> is the name printed in the list above

NOTE: If the package is a dependency of another package you
      will be notified of the dependent packages.  You should
      use the --force-removal-of-dependent-packages option to
      also remove the dependent packages as well
***************************************************************
***************************************************************
[    9.496119] TI DP83867 46000f00.mdio:00: attached PHY driver [TI DP83867] (mii_bus:phy_addr=46000f00.mdio:00, irq=POLL)
[  OK  ] Started Print notice about GPLv3 packages.
[    9.590423] am65-cpsw-nuss 46000000.ethernet eth0: Link is Down
[    9.742952] remoteproc remoteproc0: 41000000.r5f is available
[    9.811378] remoteproc remoteproc0: attaching to 41000000.r5f
[    9.917192] platform 41000000.r5f: R5F core initialized in IPC-only mode
[   10.090853]  remoteproc0#vdev0buffer: assigned reserved memory node r5f-dma-memory@a0000000
[   10.284417] virtio_rpmsg_bus virtio0: rpmsg host is online
[   10.298558] virtio_rpmsg_bus virtio0: creating channel ti.ipc4.ping-pong addr 0xd
[   10.306160] virtio_rpmsg_bus virtio0: creating channel rpmsg_chrdev addr 0xe
[   10.423832]  remoteproc0#vdev0buffer: registered virtio0 (type 7)
[   10.528311] remoteproc remoteproc0: remote processor 41000000.r5f is now attached
[   10.701350] platform 5c00000.r5f: configured R5F for remoteproc mode
[   10.828331] platform 5c00000.r5f: assigned reserved memory node r5f-dma-memory@a2000000
[   10.975434] remoteproc remoteproc1: 5c00000.r5f is available
[   11.103762] remoteproc remoteproc1: powering up 5c00000.r5f
[   11.109361] remoteproc remoteproc1: Booting fw image j7200-main-r5f0_0-fw, size 707720
[   11.125362] platform 5d00000.r5f: configured R5F for remoteproc mode
[   11.133036]  remoteproc1#vdev0buffer: assigned reserved memory node r5f-dma-memory@a2000000
[   11.147574] virtio_rpmsg_bus virtio1: rpmsg host is online
[   11.153137]  remoteproc1#vdev0buffer: registered virtio1 (type 7)
[   11.163238] remoteproc remoteproc1: remote processor 5c00000.r5f is now up
[   11.216964] virtio_rpmsg_bus virtio1: creating channel ti.ethfw.notifyservice addr 0x1e
[   11.226518] virtio_rpmsg_bus virtio1: creating channel rpmsg-kdrv addr 0x1a
[   11.239699] rpmsg-kdrv-eth-switch rpmsg-kdrv-2-mpu_1_0_ethswitch-device-0: Device info: permissions: 07FFFFFF uart_id: 3
[   11.255242] rpmsg-kdrv-eth-switch rpmsg-kdrv-2-mpu_1_0_ethswitch-device-0: FW ver 0.1 (rev 1) 18/Oct/2021 SHA:908db8ce
[   11.274718] j721e-cpsw-virt-mac main_r5fss_cpsw5g_virt_mac0: virt_cpsw_nuss mac loaded
[   11.286120] j721e-cpsw-virt-mac main_r5fss_cpsw5g_virt_mac0: rdev_features:00000003 rdev_mtu:1522 flow_id:84 tx_psil_dst_id:4A00
[   11.303243] j721e-cpsw-virt-mac main_r5fss_cpsw5g_virt_mac0: local_mac_addr:00:00:00:00:00:00 rdev_mac_addr:70:ff:76:1d:92:c1
[   11.353314] platform 5d00000.r5f: assigned reserved memory node r5f-dma-memory@a3000000
[   11.496043] remoteproc remoteproc2: 5d00000.r5f is available
[   11.601270] remoteproc remoteproc2: powering up 5d00000.r5f
[   11.607251] remoteproc remoteproc2: Booting fw image j7200-main-r5f0_1-fw, size 65652
[   11.623997]  remoteproc2#vdev0buffer: assigned reserved memory node r5f-dma-memory@a3000000
[   11.635570] virtio_rpmsg_bus virtio2: rpmsg host is online
[   11.644229] virtio_rpmsg_bus virtio2: creating channel ti.ipc4.ping-pong addr 0xd
[   11.645448]  remoteproc2#vdev0buffer: registered virtio2 (type 7)
[   11.651809] virtio_rpmsg_bus virtio2: creating channel rpmsg_chrdev addr 0xe
[   11.664637] remoteproc remoteproc2: remote processor 5d00000.r5f is now up
[  OK  ] Listening on Load/Save RF …itch Status /dev/rfkill Watch.
[  OK  ] Created slice system-systemd\x2dfsck.slice.
[   12.166517] usbcore: registered new interface driver usbfs
[   12.231073] omap_rng 40910000.rng: Random Number Generator ver. 241b34c
[   12.257782] usbcore: registered new interface driver hub
[   12.306256] usbcore: registered new device driver usb
[   12.469621] j721e-cpsw-virt-mac main_r5fss_cpsw5g_virt_mac0: virt_cpsw_nuss mac started
[  OK  ] Reached target Hardware activated USB gadget.
[  OK  ] Found device /dev/mmcblk0p1.
         Starting File System Check on /dev/mmcblk0p1...
[FAILED] Failed to start File System Check on /dev/mmcblk0p1.
See 'systemctl status systemd-fsck@dev-mmcblk0p1.service' for details.
[DEPEND] Dependency failed for /run/media/mmcblk0p1.

 _____                    _____           _         _
|  _  |___ ___ ___ ___   |  _  |___ ___  |_|___ ___| |_
|     |  _| .'| . | . |  |   __|  _| . | | | -_|  _|  _|
|__|__|_| |__,|_  |___|  |__|  |_| |___|_| |___|___|_|
              |___|                    |___|

Arago Project http://arago-project.org j7200-evm ttyS2

Arago 2020.09 j7200-evm ttyS2

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    当我搜索 e2e 时、我知道可以使用下面的命令查看以太网固件日志、因此我附加下面的日志。
    CAT /sys/kernel/debug/remoteproc/remoteproc */trace0

    root@j7200-evm:~# cat /sys/kernel/debug/remoteproc/remoteproc*/trace0
    Starting Sciserver..... PASSED
    IPC_echo_test (core : mcu1_0) .....
    IPC Driver Revision: 01.00.00.01
    mcu1_0 <--> mcu2_1, Ping- 10000, pong - 10000 completed
    =======================================================
    CPSW Ethernet Firmware
    =======================================================
    CPSW_5G Test on MAIN NAVSS
    PHY 0 is alive
    PHY 3 is alive
    PHY 23 is alive
    
    ETHFW Version : 0.01.01
    ETHFW Build Date: Jul 13, 2021
    ETHFW Build Time: 15:43:32
    ETHFW Commit SHA: 4cb38131
    
    Starting lwIP, local interface IP is dhcp-enabled
    Host MAC address: 70:ff:76:1d:92:c2
    [LWIPIF_LWIP] NETIF INIT SUCCESS
    Added interface 'ti1', IP is 0.0.0.0
    IPC_echo_test (core : mcu2_0) .....
    Remote demo device (core : mcu2_0) .....
    [IPC] TX Virtio creation failure: 0
    [IPC] Ipc_lateVirtioCreate: Failed to create VirtIO for procId..
    EthApp_initIpcTask: Ipc_lateVirtioCreate failed: -1
    Function:CpswProxyServer_attachExtHandlerCb,HostId:0,CpswType:5
    Function:CpswProxyServer_registerMacHandlerCb,HostId:0,Handle:a287c00c,CoreKey:38acb7e6, MacAddress:70:ff:76:1d:92:c1, FlowIdx:84, FlowIdxOffset:0
    Cpsw_ioctlInternal: CPSW: Registered MAC address.ALE entry:8, Policer Entry:1IPC_echo_test (core : mcu2_1) .....
    IPC Driver Revision: 01.00.00.01
    mcu2_1 <--> mcu1_0, Ping- 10000, pong - 10000 completed

    设置 IP 后、ping 在 PC (192.168.0.2)上不起作用。

    root@j7200-evm:~# ifconfig eth1 192.168.0.3 netmask 255.255.255.0 up
    root@j7200-evm:~# ifconfig
    docker0: flags=4099<UP,BROADCAST,MULTICAST>  mtu 1500  metric 1
            inet 172.17.0.1  netmask 255.255.0.0  broadcast 172.17.255.255
            ether 02:42:44:12:01:04  txqueuelen 0  (Ethernet)
            RX packets 0  bytes 0 (0.0 B)
            RX errors 0  dropped 0  overruns 0  frame 0
            TX packets 0  bytes 0 (0.0 B)
            TX errors 0  dropped 0 overruns 0  carrier 0  collisions 0
    
    eth0: flags=4099<UP,BROADCAST,MULTICAST>  mtu 1500  metric 1
            ether f4:84:4c:f8:68:1e  txqueuelen 1000  (Ethernet)
            RX packets 0  bytes 0 (0.0 B)
            RX errors 0  dropped 0  overruns 0  frame 0
            TX packets 0  bytes 0 (0.0 B)
            TX errors 0  dropped 0 overruns 0  carrier 0  collisions 0
    
    eth1: flags=4163<UP,BROADCAST,RUNNING,MULTICAST>  mtu 1500  metric 1
            inet 192.168.0.3  netmask 255.255.255.0  broadcast 192.168.0.255
            inet6 fe80::72ff:76ff:fe1d:92c1  prefixlen 64  scopeid 0x20<link>
            ether 70:ff:76:1d:92:c1  txqueuelen 1000  (Ethernet)
            RX packets 0  bytes 0 (0.0 B)
            RX errors 0  dropped 0  overruns 0  frame 0
            TX packets 43  bytes 7760 (7.5 KiB)
            TX errors 0  dropped 0 overruns 0  carrier 0  collisions 0
    
    lo: flags=73<UP,LOOPBACK,RUNNING>  mtu 65536  metric 1
            inet 127.0.0.1  netmask 255.0.0.0
            inet6 ::1  prefixlen 128  scopeid 0x10<host>
            loop  txqueuelen 1000  (Local Loopback)
            RX packets 82  bytes 6220 (6.0 KiB)
            RX errors 0  dropped 0  overruns 0  frame 0
            TX packets 82  bytes 6220 (6.0 KiB)
            TX errors 0  dropped 0 overruns 0  carrier 0  collisions 0
    
    root@j7200-evm:~# ping -I eth1 192.168.0.2
    PING 192.168.0.2 (192.168.0.2): 56 data bytes
    ^C
    --- 192.168.0.2 ping statistics ---
    4 packets transmitted, 0 packets received, 100% packet loss

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 DongSeuk:

    请查看以下 e2e。

    https://e2e.ti.com/support/processors-group/processors/f/processors-forum/999836/dra821u-why-therda821u-ethernet-is-not-working-in-sdk7-3-default-image/3694447?tisearch=e2e-sitesearch&keymatch=dra821%2520AND%2520eth1#3694447

    A72无法接收广播消息(SDK 8.1中将添加支持)、因此当您首先从 PC ping 时、它将失败、因为 A72不会响应 PC 的 ARP 请求。

    但是、当您从 A72 ping EVM 时、A72的 MAC 地址将进入 PC 的 ARP 表、下次从 PC ping 时、它将使用 ARP 表中的条目。

    此外、当您离开 PC 几分钟时、ARP 缓存将被清除、因此问题将返回。

    谢谢、此致、

    SI