This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
参考
执行以下步骤以运行 IPC_TEST。
1。
cd $/ ti-processor-sdk-rtos-j721e-evm-07_03_00_07/pdk_jacinto_07_03_00_29/packages/ti/build
make -s -j build_profile=release Board=j721e_evm core=mcu1_0 ex02_BIOS_multicore_echo_test
make -s -j build_profile=release Board=j721e_evm core=MCU2_0 ex02_BIOS_multicore_echo 测试
make -s -j build_profile=release Board=j721e_evm core=MCU2_1 ex02_BIOS_multicore_echo_test
make -s -j build_profile=release Board=j721e_evm core=c66xdsp_1 ex02_BIOS_multicore_echo 测试
make -s -j build_profile=release Board=j721e_evm core=c66xdsp_2 ex02_BIOS_multicore_echo 测试
make -s -j build_profile=release Board=j721e_evm core=c7x_1 ex02_BIOS_multicore_echo 测试
2.
cd $/ ti-processor-sdk-rtos-j721e-evm-07_03_00_07/pdk_jacinto_07_03_00_29/packages/ti/binary
CP ex02_BIOS_multicore_echo_test_c7x_1_release.xe71 /media/tda4/rootfs/lib/firmware/j7-c71_0-fw
CP ex02_BIOS_multicore_echo_test_c66xdsp_2_release.xe66 /media/tda4/rootfs/lib/firmware/j7-c66_1-fw
CP ex02_BIOS_multicore_echo_test_c66xdsp_1_release.xe66 /media/tda4/rootfs/lib/firmware/j7-c66_0-fw
CP ex02_BIOS_multicore_echo_test_MCU2_1_release.xer5f /media/tda4/rootfs/lib/firmware/j7-main-r5f0_1-fw
CP ex02_BIOS_multicore_echo_test_MCU2_0_release.xer5f /media/tda4/rootfs/lib/firmware/j7-main-r5f0_0-fw
3.运行 EVM, 运行‘IPC_TEST -v’
U-Boot SPL 2020.01-g2781231a33 (Apr 10 2021 - 01:08:23 +0000) SYSFW ABI: 3.1 (firmware rev 0x0015 '21.1.1--v2021.01a (Terrific Lla') Trying to boot from MMC2 Loading Environment from MMC... *** Warning - No MMC card found, using default environment Starting ATF on ARM64 core... NOTICE: BL31: v2.4(release):07.03.00.005-dirty NOTICE: BL31: Built : 00:15:40, Apr 10 2021 U-Boot SPL 2020.01-g2781231a33 (Apr 10 2021 - 00:17:14 +0000) SYSFW ABI: 3.1 (firmware rev 0x0015 '21.1.1--v2021.01a (Terrific Lla') Detected: J7X-BASE-CPB rev E3 Detected: J7X-VSC8514-ETH rev E2 Trying to boot from MMC2 U-Boot 2020.01-g2781231a33 (Apr 10 2021 - 00:17:14 +0000) SoC: J721E SR1.0 Model: Texas Instruments K3 J721E SoC Board: J721EX-PM2-SOM rev E7 DRAM: 4 GiB not found for dev hbmc-mux Flash: 0 Bytes MMC: sdhci@4f80000: 0, sdhci@4fb0000: 1 Loading Environment from MMC... OK In: serial@2800000 Out: serial@2800000 Err: serial@2800000 Detected: J7X-BASE-CPB rev E3 Detected: J7X-VSC8514-ETH rev E2 Net: K3 CPSW: nuss_ver: 0x6BA00101 cpsw_ver: 0x6BA80100 ale_ver: 0x00293904 Ports:1 mdio_freq:1000000 Warning: ethernet@46000000 using MAC address from ROM eth0: ethernet@46000000 Hit any key to stop autoboot: 0 switch to partitions #0, OK mmc1 is current device SD/MMC found on device 1 526 bytes read in 3 ms (170.9 KiB/s) Loaded env from uEnv.txt Importing environment from mmc1 ... Running uenvcmd ... Core 1 is already in use. No rproc commands work Core 2 is already in use. No rproc commands work 4286448 bytes read in 91 ms (44.9 MiB/s) Load Remote Processor 2 with data@addr=0x82000000 4286448 bytes: Success! 4286420 bytes read in 91 ms (44.9 MiB/s) Load Remote Processor 3 with data@addr=0x82000000 4286420 bytes: Success! 5444692 bytes read in 116 ms (44.8 MiB/s) Load Remote Processor 6 with data@addr=0x82000000 5444692 bytes: Success! 5444708 bytes read in 115 ms (45.2 MiB/s) Load Remote Processor 7 with data@addr=0x82000000 5444708 bytes: Success! 11479872 bytes read in 37 ms (295.9 MiB/s) Load Remote Processor 8 with data@addr=0x82000000 11479872 bytes: Success! 8176868 bytes read in 173 ms (45.1 MiB/s) ## Starting application at 0x80080000 ... MMU: 16-bit ASID 44-bit PA TCR_EL1=b5183519 cpu0: MPIDR=80000000 cpu0: MIDR=411fd080 Cortex-A72 r1p0 cpu0: CWG=4 ERG=4 Dminline=4 Iminline=4 PIPT cpu0: CLIDR=a200023 LoUU=1 LoC=2 LoUIS=1 cpu0: L1 Icache 48K linesz=64 set/way=256/3 cpu0: L1 Dcache 32K linesz=64 set/way=256/2 cpu0: L2 Unified 1024K linesz=64 set/way=1024/16 Display set to R5 Loading IFS...decompressing...done cpu1: MPIDR=80000001 cpu1: MIDR=411fd080 Cortex-A72 r1p0 cpu1: CWG=4 ERG=4 Dminline=4 Iminline=4 PIPT cpu1: CLIDR=a200023 LoUU=1 LoC=2 LoUIS=1 cpu1: L1 Icache 48K linesz=64 set/way=256/3 cpu1: L1 Dcache 32K linesz=64 set/way=256/2 cpu1: L2 Unified 1024K linesz=64 set/way=1024/16 System page at phys:0000000080011000 user:ffffff8040254000 kern:ffffff8040251000 Starting next program at vffffff8060086e10 All ClockCycles offsets within tolerance Welcome to QNX Neutrino 7.1.0 on the TI J721E EVM Board!! Starting random service ... start serial driver Starting MMC/SD memory card driver... eMMC Starting MMC/SD memory card driver... SD Starting XHCI driver on USB3SS0 and USB3SS1 Path=0 - am65x target=0 lun=0 Direct-Access(0) - SDMMC: S0J56X Rev: 1.0 Setting environment variables... done.. Mounting the sd .. Looking for user script to run: /ti_fs/scripts/user.sh Running user script... user.sh called... Setting additional environment variables... Starting tisci-mgr.. Starting shmemallocator.. Starting tiipc-mgr.. Mailbox_plugInterrupt: interrupt Number 489, arg 0x4C48B018 Mailbox_plugInterrupt: interrupt Number 490, arg 0x4C48B1B8 Mailbox_plugInterrupt: interrupt Number 491, arg 0x4C48B358 Mailbox_plugInterrupt: interrupt Number 492, arg 0x4C48B4F8 Mailbox_plugInterrupt: interrupt Number 493, arg 0x4C48B698 Process 57360 (tiipc-mgr) terminated SIGSEGV code=1 fltno=11 ip=000000384c43f798(/ti_fs/tibin/tiipc-mgr@lose+0x0000000000003438) mapaddr=000000000000f798. ref=0000005230448bf0 Memory fault (core dumped) Starting tiudma-mgr.. Start screen.. screen started with dss_on_r5 configuration.. done... J7EVM@QNX:/# ipc_test -v IPC_echo_test (core : ) ..... responderFxn will stay active. Please use ctrl-c to exit the test when finished. RecvTask: Failed to create endpoint SendTask 1: Failed to create message endpoint SendTask 2: Failed to create message endpoint SendTask 3: Failed to create message endpoint SendTask 4: Failed to create message endpoint SendTask 5: Failed to create message endpoint SendTask 6: Failed to create message endpoint SendTask 7: Failed to create message endpoint SendTask 8: Failed to create message endpoint SendTask 9: Failed to create message endpoint
从日志中、IPC_TEST 不起作用。然后我修改了$/ti-processor-sdk-rtos-j721e-evm-07_03_00_07/pdk_jacinto_07_03_00_29/packages/ti/drv/ipc/examples/common/src/ipc_setup.h
/*为每个器件设置起始地址*/
#ifdef SOC_AM65XX
#define VING_BASE_ADDRESS 0xA2000000U
定义了#Elif (SOC_J7200)
#define VING_BASE_ADDRESS 0xA4000000U
定义了#Elif (SOC_AM64X)
#define VING_BASE_ADDRESS 0xA5000000U
其他
//#define VING_BASE_ADDRESS 0xAA000000U
#define VING_BASE_ADDRESS 0xB0000000U
#endif
运行 EVM。
U-Boot SPL 2020.01-g2781231a33 (Apr 10 2021 - 01:08:23 +0000) SYSFW ABI: 3.1 (firmware rev 0x0015 '21.1.1--v2021.01a (Terrific Lla') Trying to boot from MMC2 Loading Environment from MMC... *** Warning - No MMC card found, using default environment Starting ATF on ARM64 core... NOTICE: BL31: v2.4(release):07.03.00.005-dirty NOTICE: BL31: Built : 00:15:40, Apr 10 2021 U-Boot SPL 2020.01-g2781231a33 (Apr 10 2021 - 00:17:14 +0000) SYSFW ABI: 3.1 (firmware rev 0x0015 '21.1.1--v2021.01a (Terrific Lla') Detected: J7X-BASE-CPB rev E3 Detected: J7X-VSC8514-ETH rev E2 Trying to boot from MMC2 U-Boot 2020.01-g2781231a33 (Apr 10 2021 - 00:17:14 +0000) SoC: J721E SR1.0 Model: Texas Instruments K3 J721E SoC Board: J721EX-PM2-SOM rev E7 DRAM: 4 GiB not found for dev hbmc-mux Flash: 0 Bytes MMC: sdhci@4f80000: 0, sdhci@4fb0000: 1 Loading Environment from MMC... OK In: serial@2800000 Out: serial@2800000 Err: serial@2800000 Detected: J7X-BASE-CPB rev E3 Detected: J7X-VSC8514-ETH rev E2 Net: K3 CPSW: nuss_ver: 0x6BA00101 cpsw_ver: 0x6BA80100 ale_ver: 0x00293904 Ports:1 mdio_freq:1000000 Warning: ethernet@46000000 using MAC address from ROM eth0: ethernet@46000000 Hit any key to stop autoboot: 0 switch to partitions #0, OK mmc1 is current device SD/MMC found on device 1 526 bytes read in 3 ms (170.9 KiB/s) Loaded env from uEnv.txt Importing environment from mmc1 ... Running uenvcmd ... Core 1 is already in use. No rproc commands work Core 2 is already in use. No rproc commands work 4286448 bytes read in 91 ms (44.9 MiB/s) Load Remote Processor 2 with data@addr=0x82000000 4286448 bytes: Success! 4286420 bytes read in 91 ms (44.9 MiB/s) Load Remote Processor 3 with data@addr=0x82000000 4286420 bytes: Success! 5444692 bytes read in 115 ms (45.2 MiB/s) Load Remote Processor 6 with data@addr=0x82000000 5444692 bytes: Success! 5444708 bytes read in 116 ms (44.8 MiB/s) Load Remote Processor 7 with data@addr=0x82000000 5444708 bytes: Success! 11479872 bytes read in 37 ms (295.9 MiB/s) Load Remote Processor 8 with data@addr=0x82000000 11479872 bytes: Success! 8176868 bytes read in 173 ms (45.1 MiB/s) ## Starting application at 0x80080000 ... MMU: 16-bit ASID 44-bit PA TCR_EL1=b5183519 cpu0: MPIDR=80000000 cpu0: MIDR=411fd080 Cortex-A72 r1p0 cpu0: CWG=4 ERG=4 Dminline=4 Iminline=4 PIPT cpu0: CLIDR=a200023 LoUU=1 LoC=2 LoUIS=1 cpu0: L1 Icache 48K linesz=64 set/way=256/3 cpu0: L1 Dcache 32K linesz=64 set/way=256/2 cpu0: L2 Unified 1024K linesz=64 set/way=1024/16 Display set to R5 Loading IFS...decompressing...done cpu1: MPIDR=80000001 cpu1: MIDR=411fd080 Cortex-A72 r1p0 cpu1: CWG=4 ERG=4 Dminline=4 Iminline=4 PIPT cpu1: CLIDR=a200023 LoUU=1 LoC=2 LoUIS=1 cpu1: L1 Icache 48K linesz=64 set/way=256/3 cpu1: L1 Dcache 32K linesz=64 set/way=256/2 cpu1: L2 Unified 1024K linesz=64 set/way=1024/16 System page at phys:0000000080011000 user:ffffff8040254000 kern:ffffff8040251000 Starting next program at vffffff8060086e10 All ClockCycles offsets within tolerance Welcome to QNX Neutrino 7.1.0 on the TI J721E EVM Board!! Starting random service ... start serial driver Starting MMC/SD memory card driver... eMMC Starting MMC/SD memory card driver... SD Starting XHCI driver on USB3SS0 and USB3SS1 Path=0 - am65x target=0 lun=0 Direct-Access(0) - SDMMC: S0J56X Rev: 1.0 Setting environment variables... done.. Mounting the sd .. Looking for user script to run: /ti_fs/scripts/user.sh Running user script... user.sh called... Setting additional environment variables... Starting tisci-mgr.. Starting shmemallocator.. Starting tiipc-mgr.. Mailbox_plugInterrupt: interrupt Number 489, arg 0x88A71018 Mailbox_plugInterrupt: interrupt Number 490, arg 0x88A711B8 Mailbox_plugInterrupt: interrupt Number 491, arg 0x88A71358 Mailbox_plugInterrupt: interrupt Number 492, arg 0x88A714F8 Mailbox_plugInterrupt: interrupt Number 493, arg 0x88A71698 Starting TI IPC Resmgr Starting tiudma-mgr.. Start screen.. screen started with dss_on_r5 configuration.. done... J7EVM@QNX:/# ipc_test -v IPC_echo_test (core : mpu1_0) ..... responderFxn will stay active. Please use ctrl-c to exit the test when finished. SendTask3: Sending "ping 0" from mpu1_0 to mcu2_0... SendTask9: Sending "ping 0" from mpu1_0 to C7X_1... SendTask4: Sending "ping 0" from mpu1_0 to mcu2_1... SendTask7: Sending "ping 0" from mpu1_0 to C66X_1... SendTask8: Sending "ping 0" from mpu1_0 to C66X_2... SendTask9: RPMessage_recv failed with code -1 SendTask9: Received "ping 0" len 7 from C7X_1 endPt 13 SendTask4: RPMessage_recv failed with code -1 SendTask9: Sending "ping 1" from mpu1_0 to C7X_1... SendTask4: Received "ping 0" len 7 from mcu2_1 endPt 13 SendTask4: Sending "ping 1" from mpu1_0 to mcu2_1... SendTask7: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask8: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask9: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask4: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask7: RPMessage_recv failed with code -1 SendTask7: Received "ping 0" len 7 from C66X_1 endPt 13 SendTask8: RPMessage_recv failed with code -1 SendTask7: Sending "ping 1" from mpu1_0 to C66X_1... SendTask9: RPMessage_recv failed with code -1 SendTask8: Received "ping 0" len 7 from C66X_2 endPt 13 SendTask4: RPMessage_recv failed with code -1 SendTask7: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask9: Received "ping 1" len 7 from C7X_1 endPt 13 SendTask8: Sending "ping 1" from mpu1_0 to C66X_2... SendTask4: Received "ping 1" len 7 from mcu2_1 endPt 13 SendTask7: RPMessage_recv failed with code -1 SendTask9: Sending "ping 2" from mpu1_0 to C7X_1... SendTask8: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask4: Sending "ping 2" from mpu1_0 to mcu2_1... SendTask7: Received "ping 1" len 7 from C66X_1 endPt 13 SendTask9: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask8: RPMessage_recv failed with code -1 SendTask4: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask7: Sending "ping 2" from mpu1_0 to C66X_1... SendTask9: RPMessage_recv failed with code -1 SendTask8: Received "ping 1" len 7 from C66X_2 endPt 13 SendTask4: RPMessage_recv failed with code -1 SendTask7: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask9: Received "ping 2" len 7 from C7X_1 endPt 13 Process 57360 (tiipc-mgr) terminated SIGSEGV code=1 fltno=11 ip=0000002588a22e60(/ti_fs/tibin/tiipc-mgr@lose+0x0000000000000b00) mapaddr=000000000000ce60. ref=0000002bf5bf04f0 SendTask8: Sending "ping 2" from mpu1_0 to C66X_2... SendTask4: Received "ping 2" len 7 from mcu2_1 endPt 13 SendTask7: RPMessage_recv failed with code -1 SendTask9: Sending "ping 3" from mpu1_0 to C7X_1... SendTask3: RPMessage_recv failed with code -1 SendTask4: Sending "ping 3" from mpu1_0 to mcu2_1... SendTask7: Received "ping 2" len 7 from C66X_1 endPt 13 SendTask1: Sending "ping 0" from mpu1_0 to mcu1_0... SendTask2: Sending "ping 0" from mpu1_0 to mcu1_1... SendTask3: Received "ping 0" len 7 from mcu2_0 endPt 13 SendTask6: Sending "ping 0" from mpu1_0 to mcu3_1... SendTask5: Sending "ping 0" from mpu1_0 to mcu3_0... SendTask7: Sending "ping 3" from mpu1_0 to C66X_1... SendTask8: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask9: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask4: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask3: Sending "ping 1" from mpu1_0 to mcu2_0... SendTask1: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask2: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask6: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask5: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask7: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask8: RPMessage_recv failed with code -1 SendTask9: RPMessage_recv failed with code -1 SendTask4: RPMessage_recv failed with code -1 SendTask3: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask1: RPMessage_recv failed with code -1 SendTask2: RPMessage_recv failed with code -1 SendTask6: RPMessage_recv failed with code -1 SendTask5: RPMessage_recv failed with code -1 SendTask8: Received "ping 2" len 7 from C66X_2 endPt 13 SendTask7: RPMessage_recv failed with code -1 SendTask9: Received "ping 3" len 7 from C7X_1 endPt 13 SendTask4: Received "ping 3" len 7 from mcu2_1 endPt 13 SendTask3: RPMessage_recv failed with code -1 SendTask1: Received "ping 0" len 7 from mcu1_0 endPt 13 SendTask2: Received "ping 0" len 7 from mcu1_1 endPt 13 SendTask6: Received "ping 0" len 7 from mcu3_1 endPt 13 SendTask5: Received "ping 0" len 7 from mcu3_0 endPt 13 SendTask8: Sending "ping 3" from mpu1_0 to C66X_2... SendTask7: Received "ping 3" len 7 from C66X_1 endPt 13 SendTask9: Sending "ping 4" from mpu1_0 to C7X_1... SendTask4: Sending "ping 4" from mpu1_0 to mcu2_1... SendTask3: Received "ping 1" len 7 from mcu2_0 endPt 13 SendTask1: Sending "ping 1" from mpu1_0 to mcu1_0... SendTask2: Sending "ping 1" from mpu1_0 to mcu1_1... SendTask6: Sending "ping 1" from mpu1_0 to mcu3_1... SendTask5: Sending "ping 1" from mpu1_0 to mcu3_0... SendTask8: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask7: Sending "ping 4" from mpu1_0 to C66X_1... SendTask9: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask4: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask3: Sending "ping 2" from mpu1_0 to mcu2_0... SendTask1: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask2: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask6: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask5: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask8: RPMessage_recv failed with code -1 SendTask7: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask9: RPMessage_recv failed with code -1 SendTask4: RPMessage_recv failed with code -1 SendTask3: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask1: RPMessage_recv failed with code -1 SendTask2: RPMessage_recv failed with code -1 SendTask6: RPMessage_recv failed with code -1 SendTask5: RPMessage_recv failed with code -1 SendTask8: Received "ping 3" len 7 from C66X_2 endPt 13 SendTask7: RPMessage_recv failed with code -1 SendTask9: Received "ping 4" len 7 from C7X_1 endPt 13 SendTask4: Received "ping 4" len 7 from mcu2_1 endPt 13 SendTask3: RPMessage_recv failed with code -1 SendTask1: Received "ping 1" len 7 from mcu1_0 endPt 13 SendTask2: Received "ping 1" len 7 from mcu1_1 endPt 13 SendTask6: Received "ping 1" len 7 from mcu3_1 endPt 13 SendTask5: Received "ping 1" len 7 from mcu3_0 endPt 13 SendTask8: Sending "ping 4" from mpu1_0 to C66X_2... SendTask7: Received "ping 4" len 7 from C66X_1 endPt 13 SendTask9: Sending "ping 5" from mpu1_0 to C7X_1... SendTask4: Sending "ping 5" from mpu1_0 to mcu2_1... SendTask3: Received "ping 2" len 7 from mcu2_0 endPt 13 SendTask1: Sending "ping 2" from mpu1_0 to mcu1_0... SendTask2: Sending "ping 2" from mpu1_0 to mcu1_1... SendTask6: Sending "ping 2" from mpu1_0 to mcu3_1... SendTask5: Sending "ping 2" from mpu1_0 to mcu3_0... SendTask8: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask7: Sending "ping 5" from mpu1_0 to C66X_1... SendTask9: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask4: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask3: Sending "ping 3" from mpu1_0 to mcu2_0... SendTask1: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask2: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask6: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask5: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask8: RPMessage_recv failed with code -1 SendTask7: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask9: RPMessage_recv failed with code -1 SendTask4: RPMessage_recv failed with code -1 SendTask3: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask1: RPMessage_recv failed with code -1 SendTask2: RPMessage_recv failed with code -1 SendTask6: RPMessage_recv failed with code -1 SendTask5: RPMessage_recv failed with code -1 SendTask8: Received "ping 4" len 7 from C66X_2 endPt 13 SendTask7: RPMessage_recv failed with code -1 SendTask9: Received "ping 5" len 7 from C7X_1 endPt 13 SendTask4: Received "ping 5" len 7 from mcu2_1 endPt 13 SendTask3: RPMessage_recv failed with code -1 SendTask1: Received "ping 2" len 7 from mcu1_0 endPt 13 SendTask2: Received "ping 2" len 7 from mcu1_1 endPt 13 SendTask6: Received "ping 2" len 7 from mcu3_1 endPt 13 SendTask5: Received "ping 2" len 7 from mcu3_0 endPt 13 SendTask8: Sending "ping 5" from mpu1_0 to C66X_2... SendTask7: Received "ping 5" len 7 from C66X_1 endPt 13 SendTask9: Sending "ping 6" from mpu1_0 to C7X_1... SendTask4: Sending "ping 6" from mpu1_0 to mcu2_1... SendTask3: Received "ping 3" len 7 from mcu2_0 endPt 13 SendTask1: Sending "ping 3" from mpu1_0 to mcu1_0... SendTask2: Sending "ping 3" from mpu1_0 to mcu1_1... SendTask6: Sending "ping 3" from mpu1_0 to mcu3_1... SendTask5: Sending "ping 3" from mpu1_0 to mcu3_0... SendTask8: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask7: Sending "ping 6" from mpu1_0 to C66X_1... SendTask9: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask4: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask3: Sending "ping 4" from mpu1_0 to mcu2_0... SendTask1: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask2: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask6: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask5: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask8: RPMessage_recv failed with code -1 SendTask7: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask9: RPMessage_recv failed with code -1 SendTask4: RPMessage_recv failed with code -1 SendTask3: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask1: RPMessage_recv failed with code -1 SendTask2: RPMessage_recv failed with code -1 SendTask6: RPMessage_recv failed with code -1 SendTask5: RPMessage_recv failed with code -1 SendTask8: Received "ping 5" len 7 from C66X_2 endPt 13 SendTask7: RPMessage_recv failed with code -1 SendTask9: Received "ping 6" len 7 from C7X_1 endPt 13 SendTask4: Received "ping 6" len 7 from mcu2_1 endPt 13 SendTask3: RPMessage_recv failed with code -1 SendTask1: Received "ping 3" len 7 from mcu1_0 endPt 13 SendTask2: Received "ping 3" len 7 from mcu1_1 endPt 13 SendTask6: Received "ping 3" len 7 from mcu3_1 endPt 13 SendTask5: Received "ping 3" len 7 from mcu3_0 endPt 13 SendTask8: Sending "ping 6" from mpu1_0 to C66X_2... SendTask7: Received "ping 6" len 7 from C66X_1 endPt 13 SendTask9: Sending "ping 7" from mpu1_0 to C7X_1... SendTask4: Sending "ping 7" from mpu1_0 to mcu2_1... SendTask3: Received "ping 4" len 7 from mcu2_0 endPt 13 SendTask1: Sending "ping 4" from mpu1_0 to mcu1_0... SendTask2: Sending "ping 4" from mpu1_0 to mcu1_1... SendTask6: Sending "ping 4" from mpu1_0 to mcu3_1... SendTask5: Sending "ping 4" from mpu1_0 to mcu3_0... SendTask8: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask7: Sending "ping 7" from mpu1_0 to C66X_1... SendTask9: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask4: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask3: Sending "ping 5" from mpu1_0 to mcu2_0... SendTask1: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask2: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask6: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask5: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask8: RPMessage_recv failed with code -1 SendTask7: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask9: RPMessage_recv failed with code -1 SendTask4: RPMessage_recv failed with code -1 SendTask3: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask1: RPMessage_recv failed with code -1 SendTask2: RPMessage_recv failed with code -1 SendTask6: RPMessage_recv failed with code -1 SendTask5: RPMessage_recv failed with code -1 SendTask8: Received "ping 6" len 7 from C66X_2 endPt 13 SendTask7: RPMessage_recv failed with code -1 SendTask9: Received "ping 7" len 7 from C7X_1 endPt 13 SendTask4: Received "ping 7" len 7 from mcu2_1 endPt 13 SendTask3: RPMessage_recv failed with code -1 SendTask1: Received "ping 4" len 7 from mcu1_0 endPt 13 SendTask2: Received "ping 4" len 7 from mcu1_1 endPt 13 SendTask6: Received "ping 4" len 7 from mcu3_1 endPt 13 SendTask5: Received "ping 4" len 7 from mcu3_0 endPt 13 SendTask8: Sending "ping 7" from mpu1_0 to C66X_2... SendTask7: Received "ping 7" len 7 from C66X_1 endPt 13 SendTask9: Sending "ping 8" from mpu1_0 to C7X_1... SendTask4: Sending "ping 8" from mpu1_0 to mcu2_1... SendTask3: Received "ping 5" len 7 from mcu2_0 endPt 13 SendTask1: Sending "ping 5" from mpu1_0 to mcu1_0... SendTask2: Sending "ping 5" from mpu1_0 to mcu1_1... SendTask6: Sending "ping 5" from mpu1_0 to mcu3_1... SendTask5: Sending "ping 5" from mpu1_0 to mcu3_0... SendTask8: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask7: Sending "ping 8" from mpu1_0 to C66X_1... SendTask9: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask4: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask3: Sending "ping 6" from mpu1_0 to mcu2_0... SendTask1: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask2: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask6: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask5: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask8: RPMessage_recv failed with code -1 SendTask7: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask9: RPMessage_recv failed with code -1 SendTask4: RPMessage_recv failed with code -1 SendTask3: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask1: RPMessage_recv failed with code -1 SendTask2: RPMessage_recv failed with code -1 SendTask6: RPMessage_recv failed with code -1 SendTask5: RPMessage_recv failed with code -1 SendTask8: Received "ping 7" len 7 from C66X_2 endPt 13 SendTask7: RPMessage_recv failed with code -1 SendTask9: Received "ping 8" len 7 from C7X_1 endPt 13 SendTask4: Received "ping 8" len 7 from mcu2_1 endPt 13 SendTask3: RPMessage_recv failed with code -1 SendTask1: Received "ping 5" len 7 from mcu1_0 endPt 13 SendTask2: Received "ping 5" len 7 from mcu1_1 endPt 13 SendTask6: Received "ping 5" len 7 from mcu3_1 endPt 13 SendTask5: Received "ping 5" len 7 from mcu3_0 endPt 13 SendTask8: Sending "ping 8" from mpu1_0 to C66X_2... SendTask7: Received "ping 8" len 7 from C66X_1 endPt 13 SendTask9: Sending "ping 9" from mpu1_0 to C7X_1... SendTask4: Sending "ping 9" from mpu1_0 to mcu2_1... SendTask3: Received "ping 6" len 7 from mcu2_0 endPt 13 SendTask1: Sending "ping 6" from mpu1_0 to mcu1_0... SendTask2: Sending "ping 6" from mpu1_0 to mcu1_1... SendTask6: Sending "ping 6" from mpu1_0 to mcu3_1... SendTask5: Sending "ping 6" from mpu1_0 to mcu3_0... SendTask8: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask7: Sending "ping 9" from mpu1_0 to C66X_1... SendTask9: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask4: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask3: Sending "ping 7" from mpu1_0 to mcu2_0... SendTask1: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask2: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask6: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask5: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask8: RPMessage_recv failed with code -1 SendTask7: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask9: RPMessage_recv failed with code -1 SendTask4: RPMessage_recv failed with code -1 SendTask3: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask1: RPMessage_recv failed with code -1 SendTask2: RPMessage_recv failed with code -1 SendTask6: RPMessage_recv failed with code -1 SendTask5: RPMessage_recv failed with code -1 SendTask8: Received "ping 8" len 7 from C66X_2 endPt 13 SendTask7: RPMessage_recv failed with code -1 SendTask9: Received "ping 9" len 7 from C7X_1 endPt 13 SendTask4: Received "ping 9" len 7 from mcu2_1 endPt 13 SendTask3: RPMessage_recv failed with code -1 SendTask1: Received "ping 6" len 7 from mcu1_0 endPt 13 SendTask2: Received "ping 6" len 7 from mcu1_1 endPt 13 SendTask6: Received "ping 6" len 7 from mcu3_1 endPt 13 SendTask5: Received "ping 6" len 7 from mcu3_0 endPt 13 SendTask8: Sending "ping 9" from mpu1_0 to C66X_2... SendTask7: Received "ping 9" len 7 from C66X_1 endPt 13 SendTask9: mpu1_0 <--> C7X_1, Ping- 10, pong - 10 completed SendTask4: mpu1_0 <--> mcu2_1, Ping- 10, pong - 10 completed SendTask3: Received "ping 7" len 7 from mcu2_0 endPt 13 SendTask1: Sending "ping 7" from mpu1_0 to mcu1_0... SendTask2: Sending "ping 7" from mpu1_0 to mcu1_1... SendTask6: Sending "ping 7" from mpu1_0 to mcu3_1... SendTask5: Sending "ping 7" from mpu1_0 to mcu3_0... SendTask8: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask7: mpu1_0 <--> C66X_1, Ping- 10, pong - 10 completed SendTask3: Sending "ping 8" from mpu1_0 to mcu2_0... SendTask1: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask2: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask6: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask5: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask8: RPMessage_recv failed with code -1 SendTask3: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask1: RPMessage_recv failed with code -1 SendTask2: RPMessage_recv failed with code -1 SendTask6: RPMessage_recv failed with code -1 SendTask5: RPMessage_recv failed with code -1 SendTask8: Received "ping 9" len 7 from C66X_2 endPt 13 SendTask3: RPMessage_recv failed with code -1 SendTask1: Received "ping 7" len 7 from mcu1_0 endPt 13 SendTask2: Received "ping 7" len 7 from mcu1_1 endPt 13 SendTask6: Received "ping 7" len 7 from mcu3_1 endPt 13 SendTask5: Received "ping 7" len 7 from mcu3_0 endPt 13 SendTask8: mpu1_0 <--> C66X_2, Ping- 10, pong - 10 completed SendTask3: Received "ping 8" len 7 from mcu2_0 endPt 13 SendTask1: Sending "ping 8" from mpu1_0 to mcu1_0... SendTask2: Sending "ping 8" from mpu1_0 to mcu1_1... SendTask6: Sending "ping 8" from mpu1_0 to mcu3_1... SendTask5: Sending "ping 8" from mpu1_0 to mcu3_0... SendTask3: Sending "ping 9" from mpu1_0 to mcu2_0... SendTask1: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask2: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask6: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask5: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask3: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask1: RPMessage_recv failed with code -1 SendTask2: RPMessage_recv failed with code -1 SendTask6: RPMessage_recv failed with code -1 SendTask5: RPMessage_recv failed with code -1 SendTask3: RPMessage_recv failed with code -1 SendTask1: Received "ping 8" len 7 from mcu1_0 endPt 13 SendTask2: Received "ping 8" len 7 from mcu1_1 endPt 13 SendTask6: Received "ping 8" len 7 from mcu3_1 endPt 13 SendTask5: Received "ping 8" len 7 from mcu3_0 endPt 13 SendTask3: Received "ping 9" len 7 from mcu2_0 endPt 13 SendTask1: Sending "ping 9" from mpu1_0 to mcu1_0... SendTask2: Sending "ping 9" from mpu1_0 to mcu1_1... SendTask6: Sending "ping 9" from mpu1_0 to mcu3_1... SendTask5: Sending "ping 9" from mpu1_0 to mcu3_0... SendTask3: mpu1_0 <--> mcu2_0, Ping- 10, pong - 10 completed SendTask1: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask2: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask6: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask5: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask1: RPMessage_recv failed with code -1 SendTask2: RPMessage_recv failed with code -1 SendTask6: RPMessage_recv failed with code -1 SendTask5: RPMessage_recv failed with code -1 SendTask1: Received "ping 9" len 7 from mcu1_0 endPt 13 SendTask2: Received "ping 9" len 7 from mcu1_1 endPt 13 SendTask6: Received "ping 9" len 7 from mcu3_1 endPt 13 SendTask5: Received "ping 9" len 7 from mcu3_0 endPt 13 SendTask1: mpu1_0 <--> mcu1_0, Ping- 10, pong - 10 completed SendTask2: mpu1_0 <--> mcu1_1, Ping- 10, pong - 10 completed SendTask6: mpu1_0 <--> mcu3_1, Ping- 10, pong - 10 completed SendTask5: mpu1_0 <--> mcu3_0, Ping- 10, pong - 10 completed
1。 如何解决这个问题?
2。 表单日志、MPU 和(mcu3_0、mcu3_1、mcu1_0、mcu1_1)之间的 IPC 函 数可以正常工作、但在/media/tda4/rootfs/lib/firmware 中没有相关固件。 为什么是这样?
然后我继续
TDA4VM:QNX 环境中的 IPC 失败-处理器论坛-处理器- TI E2E 支持论坛
仍然失败。
U-Boot SPL 2020.01-g2781231a33 (Apr 10 2021 - 01:08:23 +0000) SYSFW ABI: 3.1 (firmware rev 0x0015 '21.1.1--v2021.01a (Terrific Lla') Trying to boot from MMC2 Loading Environment from MMC... *** Warning - No MMC card found, using default environment Starting ATF on ARM64 core... NOTICE: BL31: v2.4(release):07.03.00.005-dirty NOTICE: BL31: Built : 00:15:40, Apr 10 2021 U-Boot SPL 2020.01-g2781231a33 (Apr 10 2021 - 00:17:14 +0000) SYSFW ABI: 3.1 (firmware rev 0x0015 '21.1.1--v2021.01a (Terrific Lla') Detected: J7X-BASE-CPB rev E3 Detected: J7X-VSC8514-ETH rev E2 Trying to boot from MMC2 U-Boot 2020.01-g2781231a33 (Apr 10 2021 - 00:17:14 +0000) SoC: J721E SR1.0 Model: Texas Instruments K3 J721E SoC Board: J721EX-PM2-SOM rev E7 DRAM: 4 GiB not found for dev hbmc-mux Flash: 0 Bytes MMC: sdhci@4f80000: 0, sdhci@4fb0000: 1 Loading Environment from MMC... OK In: serial@2800000 Out: serial@2800000 Err: serial@2800000 Detected: J7X-BASE-CPB rev E3 Detected: J7X-VSC8514-ETH rev E2 Net: K3 CPSW: nuss_ver: 0x6BA00101 cpsw_ver: 0x6BA80100 ale_ver: 0x00293904 Ports:1 mdio_freq:1000000 Warning: ethernet@46000000 using MAC address from ROM eth0: ethernet@46000000 Hit any key to stop autoboot: 0 switch to partitions #0, OK mmc1 is current device SD/MMC found on device 1 526 bytes read in 3 ms (170.9 KiB/s) Loaded env from uEnv.txt Importing environment from mmc1 ... Running uenvcmd ... Core 1 is already in use. No rproc commands work Core 2 is already in use. No rproc commands work 4286416 bytes read in 92 ms (44.4 MiB/s) Load Remote Processor 2 with data@addr=0x82000000 4286416 bytes: Success! 4286388 bytes read in 92 ms (44.4 MiB/s) Load Remote Processor 3 with data@addr=0x82000000 4286388 bytes: Success! 4286388 bytes read in 91 ms (44.9 MiB/s) Load Remote Processor 4 with data@addr=0x82000000 4286388 bytes: Success! 4286388 bytes read in 92 ms (44.4 MiB/s) Load Remote Processor 5 with data@addr=0x82000000 4286388 bytes: Success! 5444692 bytes read in 115 ms (45.2 MiB/s) Load Remote Processor 6 with data@addr=0x82000000 5444692 bytes: Success! 5444708 bytes read in 116 ms (44.8 MiB/s) Load Remote Processor 7 with data@addr=0x82000000 5444708 bytes: Success! 11479872 bytes read in 36 ms (304.1 MiB/s) Load Remote Processor 8 with data@addr=0x82000000 11479872 bytes: Success! 8176868 bytes read in 173 ms (45.1 MiB/s) ## Starting application at 0x80080000 ... MMU: 16-bit ASID 44-bit PA TCR_EL1=b5183519 cpu0: MPIDR=80000000 cpu0: MIDR=411fd080 Cortex-A72 r1p0 cpu0: CWG=4 ERG=4 Dminline=4 Iminline=4 PIPT cpu0: CLIDR=a200023 LoUU=1 LoC=2 LoUIS=1 cpu0: L1 Icache 48K linesz=64 set/way=256/3 cpu0: L1 Dcache 32K linesz=64 set/way=256/2 cpu0: L2 Unified 1024K linesz=64 set/way=1024/16 Display set to R5 Loading IFS...decompressing...done cpu1: MPIDR=80000001 cpu1: MIDR=411fd080 Cortex-A72 r1p0 cpu1: CWG=4 ERG=4 Dminline=4 Iminline=4 PIPT cpu1: CLIDR=a200023 LoUU=1 LoC=2 LoUIS=1 cpu1: L1 Icache 48K linesz=64 set/way=256/3 cpu1: L1 Dcache 32K linesz=64 set/way=256/2 cpu1: L2 Unified 1024K linesz=64 set/way=1024/16 System page at phys:0000000080011000 user:ffffff8040254000 kern:ffffff8040251000 Starting next program at vffffff8060086e10 All ClockCycles offsets within tolerance Welcome to QNX Neutrino 7.1.0 on the TI J721E EVM Board!! Starting random service ... start serial driver Starting MMC/SD memory card driver... eMMC Starting MMC/SD memory card driver... SD Starting XHCI driver on USB3SS0 and USB3SS1 Path=0 - am65x target=0 lun=0 Direct-Access(0) - SDMMC: S0J56X Rev: 1.0 Setting environment variables... done.. Mounting the sd .. Looking for user script to run: /ti_fs/scripts/user.sh Running user script... user.sh called... Setting additional environment variables... Starting tisci-mgr.. Starting shmemallocator.. Starting tiipc-mgr.. Mailbox_plugInterrupt: interrupt Number 489, arg 0x6F942018 Mailbox_plugInterrupt: interrupt Number 490, arg 0x6F9421B8 Mailbox_plugInterrupt: interrupt Number 491, arg 0x6F942358 Mailbox_plugInterrupt: interrupt Number 492, arg 0x6F9424F8 Mailbox_plugInterrupt: interrupt Number 493, arg 0x6F942698 Starting TI IPC Resmgr Starting tiudma-mgr.. Start screen.. screen started with dss_on_r5 configuration.. done... J7EVM@QNX:/# J7EVM@QNX:/# J7EVM@QNX:/# ipc_test -v IPC_echo_test (core : mpu1_0) ..... responderFxn will stay active. Please use ctrl-c to exit the test when finished. SendTask3: Sending "ping 0" from mpu1_0 to mcu2_0... SendTask6: Sending "ping 0" from mpu1_0 to mcu3_1... SendTask9: Sending "ping 0" from mpu1_0 to C7X_1... SendTask4: Sending "ping 0" from mpu1_0 to mcu2_1... SendTask5: Sending "ping 0" from mpu1_0 to mcu3_0... SendTask7: Sending "ping 0" from mpu1_0 to C66X_1... SendTask8: Sending "ping 0" from mpu1_0 to C66X_2... Process 57360 (tiipc-mgr) terminated SIGSEGV code=1 fltno=11 ip=0000005c6f8f3e60(/ti_fs/tibin/tiipc-mgr@lose+0x0000000000000b00) mapaddr=000000000000ce60. ref=00000063deaddcf0 SendTask8: RPMessage_recv failed with code -1 SendTask8: Received "ping 0" len 7 from C66X_2 endPt 13 SendTask7: RPMessage_recv failed with code -1 SendTask8: Sending "ping 1" from mpu1_0 to C66X_2... SendTask5: RPMessage_recv failed with code -1 SendTask7: Received "ping 0" len 7 from C66X_1 endPt 13 SendTask4: RPMessage_recv failed with code -1 SendTask9: RPMessage_recv failed with code -1 SendTask5: Received "ping 0" len 7 from mcu3_0 endPt 13 SendTask6: RPMessage_recv failed with code -1 SendTask7: Sending "ping 1" from mpu1_0 to C66X_1... SendTask3: RPMessage_recv failed with code -1 SendTask4: Received "ping 0" len 7 from mcu2_1 endPt 13 SendTask9: Received "ping 0" len 7 from C7X_1 endPt 13 SendTask1: Sending "ping 0" from mpu1_0 to mcu1_0... SendTask5: Sending "ping 1" from mpu1_0 to mcu3_0... SendTask2: Sending "ping 0" from mpu1_0 to mcu1_1... SendTask6: Received "ping 0" len 7 from mcu3_1 endPt 13 SendTask8: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask7: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask3: Received "ping 0" len 7 from mcu2_0 endPt 13 SendTask4: Sending "ping 1" from mpu1_0 to mcu2_1... SendTask9: Sending "ping 1" from mpu1_0 to C7X_1... SendTask1: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask5: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask2: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask6: Sending "ping 1" from mpu1_0 to mcu3_1... SendTask8: RPMessage_recv failed with code -1 SendTask7: RPMessage_recv failed with code -1 SendTask3: Sending "ping 1" from mpu1_0 to mcu2_0... SendTask4: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask9: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask1: RPMessage_recv failed with code -1 SendTask5: RPMessage_recv failed with code -1 SendTask2: RPMessage_recv failed with code -1 SendTask6: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask8: Received "ping 1" len 7 from C66X_2 endPt 13 SendTask7: Received "ping 1" len 7 from C66X_1 endPt 13 SendTask3: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask4: RPMessage_recv failed with code -1 SendTask9: RPMessage_recv failed with code -1 SendTask1: Received "ping 0" len 7 from mcu1_0 endPt 13 SendTask5: Received "ping 1" len 7 from mcu3_0 endPt 13 SendTask2: Received "ping 0" len 7 from mcu1_1 endPt 13 SendTask6: RPMessage_recv failed with code -1 SendTask8: Sending "ping 2" from mpu1_0 to C66X_2... SendTask7: Sending "ping 2" from mpu1_0 to C66X_1... SendTask3: RPMessage_recv failed with code -1 SendTask4: Received "ping 1" len 7 from mcu2_1 endPt 13 SendTask9: Received "ping 1" len 7 from C7X_1 endPt 13 SendTask1: Sending "ping 1" from mpu1_0 to mcu1_0... SendTask5: Sending "ping 2" from mpu1_0 to mcu3_0... SendTask2: Sending "ping 1" from mpu1_0 to mcu1_1... SendTask6: Received "ping 1" len 7 from mcu3_1 endPt 13 SendTask8: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask7: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask3: Received "ping 1" len 7 from mcu2_0 endPt 13 SendTask4: Sending "ping 2" from mpu1_0 to mcu2_1... SendTask9: Sending "ping 2" from mpu1_0 to C7X_1... SendTask1: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask5: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask2: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask6: Sending "ping 2" from mpu1_0 to mcu3_1... SendTask8: RPMessage_recv failed with code -1 SendTask7: RPMessage_recv failed with code -1 SendTask3: Sending "ping 2" from mpu1_0 to mcu2_0... SendTask4: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask9: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask1: RPMessage_recv failed with code -1 SendTask5: RPMessage_recv failed with code -1 SendTask2: RPMessage_recv failed with code -1 SendTask6: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask8: Received "ping 2" len 7 from C66X_2 endPt 13 SendTask7: Received "ping 2" len 7 from C66X_1 endPt 13 SendTask3: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask4: RPMessage_recv failed with code -1 SendTask9: RPMessage_recv failed with code -1 SendTask1: Received "ping 1" len 7 from mcu1_0 endPt 13 SendTask5: Received "ping 2" len 7 from mcu3_0 endPt 13 SendTask2: Received "ping 1" len 7 from mcu1_1 endPt 13 SendTask6: RPMessage_recv failed with code -1 SendTask8: Sending "ping 3" from mpu1_0 to C66X_2... SendTask7: Sending "ping 3" from mpu1_0 to C66X_1... SendTask3: RPMessage_recv failed with code -1 SendTask4: Received "ping 2" len 7 from mcu2_1 endPt 13 SendTask9: Received "ping 2" len 7 from C7X_1 endPt 13 SendTask1: Sending "ping 2" from mpu1_0 to mcu1_0... SendTask5: Sending "ping 3" from mpu1_0 to mcu3_0... SendTask2: Sending "ping 2" from mpu1_0 to mcu1_1... SendTask6: Received "ping 2" len 7 from mcu3_1 endPt 13 SendTask8: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask7: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask3: Received "ping 2" len 7 from mcu2_0 endPt 13 SendTask4: Sending "ping 3" from mpu1_0 to mcu2_1... SendTask9: Sending "ping 3" from mpu1_0 to C7X_1... SendTask1: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask5: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask2: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask6: Sending "ping 3" from mpu1_0 to mcu3_1... SendTask8: RPMessage_recv failed with code -1 SendTask7: RPMessage_recv failed with code -1 SendTask3: Sending "ping 3" from mpu1_0 to mcu2_0... SendTask4: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask9: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask1: RPMessage_recv failed with code -1 SendTask5: RPMessage_recv failed with code -1 SendTask2: RPMessage_recv failed with code -1 SendTask6: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask8: Received "ping 3" len 7 from C66X_2 endPt 13 SendTask7: Received "ping 3" len 7 from C66X_1 endPt 13 SendTask3: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask4: RPMessage_recv failed with code -1 SendTask9: RPMessage_recv failed with code -1 SendTask1: Received "ping 2" len 7 from mcu1_0 endPt 13 SendTask5: Received "ping 3" len 7 from mcu3_0 endPt 13 SendTask2: Received "ping 2" len 7 from mcu1_1 endPt 13 SendTask6: RPMessage_recv failed with code -1 SendTask8: Sending "ping 4" from mpu1_0 to C66X_2... SendTask7: Sending "ping 4" from mpu1_0 to C66X_1... SendTask3: RPMessage_recv failed with code -1 SendTask4: Received "ping 3" len 7 from mcu2_1 endPt 13 SendTask9: Received "ping 3" len 7 from C7X_1 endPt 13 SendTask1: Sending "ping 3" from mpu1_0 to mcu1_0... SendTask5: Sending "ping 4" from mpu1_0 to mcu3_0... SendTask2: Sending "ping 3" from mpu1_0 to mcu1_1... SendTask6: Received "ping 3" len 7 from mcu3_1 endPt 13 SendTask8: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask7: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask3: Received "ping 3" len 7 from mcu2_0 endPt 13 SendTask4: Sending "ping 4" from mpu1_0 to mcu2_1... SendTask9: Sending "ping 4" from mpu1_0 to C7X_1... SendTask1: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask5: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask2: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask6: Sending "ping 4" from mpu1_0 to mcu3_1... SendTask8: RPMessage_recv failed with code -1 SendTask7: RPMessage_recv failed with code -1 SendTask3: Sending "ping 4" from mpu1_0 to mcu2_0... SendTask4: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask9: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask1: RPMessage_recv failed with code -1 SendTask5: RPMessage_recv failed with code -1 SendTask2: RPMessage_recv failed with code -1 SendTask6: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask8: Received "ping 4" len 7 from C66X_2 endPt 13 SendTask7: Received "ping 4" len 7 from C66X_1 endPt 13 SendTask3: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask4: RPMessage_recv failed with code -1 SendTask9: RPMessage_recv failed with code -1 SendTask1: Received "ping 3" len 7 from mcu1_0 endPt 13 SendTask5: Received "ping 4" len 7 from mcu3_0 endPt 13 SendTask2: Received "ping 3" len 7 from mcu1_1 endPt 13 SendTask6: RPMessage_recv failed with code -1 SendTask8: Sending "ping 5" from mpu1_0 to C66X_2... SendTask7: Sending "ping 5" from mpu1_0 to C66X_1... SendTask3: RPMessage_recv failed with code -1 SendTask4: Received "ping 4" len 7 from mcu2_1 endPt 13 SendTask9: Received "ping 4" len 7 from C7X_1 endPt 13 SendTask1: Sending "ping 4" from mpu1_0 to mcu1_0... SendTask5: Sending "ping 5" from mpu1_0 to mcu3_0... SendTask2: Sending "ping 4" from mpu1_0 to mcu1_1... SendTask6: Received "ping 4" len 7 from mcu3_1 endPt 13 SendTask8: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask7: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask3: Received "ping 4" len 7 from mcu2_0 endPt 13 SendTask4: Sending "ping 5" from mpu1_0 to mcu2_1... SendTask9: Sending "ping 5" from mpu1_0 to C7X_1... SendTask1: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask5: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask2: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask6: Sending "ping 5" from mpu1_0 to mcu3_1... SendTask8: RPMessage_recv failed with code -1 SendTask7: RPMessage_recv failed with code -1 SendTask3: Sending "ping 5" from mpu1_0 to mcu2_0... SendTask4: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask9: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask1: RPMessage_recv failed with code -1 SendTask5: RPMessage_recv failed with code -1 SendTask2: RPMessage_recv failed with code -1 SendTask6: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask8: Received "ping 5" len 7 from C66X_2 endPt 13 SendTask7: Received "ping 5" len 7 from C66X_1 endPt 13 SendTask3: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask4: RPMessage_recv failed with code -1 SendTask9: RPMessage_recv failed with code -1 SendTask1: Received "ping 4" len 7 from mcu1_0 endPt 13 SendTask5: Received "ping 5" len 7 from mcu3_0 endPt 13 SendTask2: Received "ping 4" len 7 from mcu1_1 endPt 13 SendTask6: RPMessage_recv failed with code -1 SendTask8: Sending "ping 6" from mpu1_0 to C66X_2... SendTask7: Sending "ping 6" from mpu1_0 to C66X_1... SendTask3: RPMessage_recv failed with code -1 SendTask4: Received "ping 5" len 7 from mcu2_1 endPt 13 SendTask9: Received "ping 5" len 7 from C7X_1 endPt 13 SendTask1: Sending "ping 5" from mpu1_0 to mcu1_0... SendTask5: Sending "ping 6" from mpu1_0 to mcu3_0... SendTask2: Sending "ping 5" from mpu1_0 to mcu1_1... SendTask6: Received "ping 5" len 7 from mcu3_1 endPt 13 SendTask8: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask7: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask3: Received "ping 5" len 7 from mcu2_0 endPt 13 SendTask4: Sending "ping 6" from mpu1_0 to mcu2_1... SendTask9: Sending "ping 6" from mpu1_0 to C7X_1... SendTask1: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask5: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask2: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask6: Sending "ping 6" from mpu1_0 to mcu3_1... SendTask8: RPMessage_recv failed with code -1 SendTask7: RPMessage_recv failed with code -1 SendTask3: Sending "ping 6" from mpu1_0 to mcu2_0... SendTask4: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask9: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask1: RPMessage_recv failed with code -1 SendTask5: RPMessage_recv failed with code -1 SendTask2: RPMessage_recv failed with code -1 SendTask6: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask8: Received "ping 6" len 7 from C66X_2 endPt 13 SendTask7: Received "ping 6" len 7 from C66X_1 endPt 13 SendTask3: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask4: RPMessage_recv failed with code -1 SendTask9: RPMessage_recv failed with code -1 SendTask1: Received "ping 5" len 7 from mcu1_0 endPt 13 SendTask5: Received "ping 6" len 7 from mcu3_0 endPt 13 SendTask2: Received "ping 5" len 7 from mcu1_1 endPt 13 SendTask6: RPMessage_recv failed with code -1 SendTask8: Sending "ping 7" from mpu1_0 to C66X_2... SendTask7: Sending "ping 7" from mpu1_0 to C66X_1... SendTask3: RPMessage_recv failed with code -1 SendTask4: Received "ping 6" len 7 from mcu2_1 endPt 13 SendTask9: Received "ping 6" len 7 from C7X_1 endPt 13 SendTask1: Sending "ping 6" from mpu1_0 to mcu1_0... SendTask5: Sending "ping 7" from mpu1_0 to mcu3_0... SendTask2: Sending "ping 6" from mpu1_0 to mcu1_1... SendTask6: Received "ping 6" len 7 from mcu3_1 endPt 13 SendTask8: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask7: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask3: Received "ping 6" len 7 from mcu2_0 endPt 13 SendTask4: Sending "ping 7" from mpu1_0 to mcu2_1... SendTask9: Sending "ping 7" from mpu1_0 to C7X_1... SendTask1: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask5: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask2: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask6: Sending "ping 7" from mpu1_0 to mcu3_1... SendTask8: RPMessage_recv failed with code -1 SendTask7: RPMessage_recv failed with code -1 SendTask3: Sending "ping 7" from mpu1_0 to mcu2_0... SendTask4: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask9: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask1: RPMessage_recv failed with code -1 SendTask5: RPMessage_recv failed with code -1 SendTask2: RPMessage_recv failed with code -1 SendTask6: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask8: Received "ping 7" len 7 from C66X_2 endPt 13 SendTask7: Received "ping 7" len 7 from C66X_1 endPt 13 SendTask3: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask4: RPMessage_recv failed with code -1 SendTask9: RPMessage_recv failed with code -1 SendTask1: Received "ping 6" len 7 from mcu1_0 endPt 13 SendTask5: Received "ping 7" len 7 from mcu3_0 endPt 13 SendTask2: Received "ping 6" len 7 from mcu1_1 endPt 13 SendTask6: RPMessage_recv failed with code -1 SendTask8: Sending "ping 8" from mpu1_0 to C66X_2... SendTask7: Sending "ping 8" from mpu1_0 to C66X_1... SendTask3: RPMessage_recv failed with code -1 SendTask4: Received "ping 7" len 7 from mcu2_1 endPt 13 SendTask9: Received "ping 7" len 7 from C7X_1 endPt 13 SendTask1: Sending "ping 7" from mpu1_0 to mcu1_0... SendTask5: Sending "ping 8" from mpu1_0 to mcu3_0... SendTask2: Sending "ping 7" from mpu1_0 to mcu1_1... SendTask6: Received "ping 7" len 7 from mcu3_1 endPt 13 SendTask8: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask7: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask3: Received "ping 7" len 7 from mcu2_0 endPt 13 SendTask4: Sending "ping 8" from mpu1_0 to mcu2_1... SendTask9: Sending "ping 8" from mpu1_0 to C7X_1... SendTask1: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask5: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask2: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask6: Sending "ping 8" from mpu1_0 to mcu3_1... SendTask8: RPMessage_recv failed with code -1 SendTask7: RPMessage_recv failed with code -1 SendTask3: Sending "ping 8" from mpu1_0 to mcu2_0... SendTask4: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask9: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask1: RPMessage_recv failed with code -1 SendTask5: RPMessage_recv failed with code -1 SendTask2: RPMessage_recv failed with code -1 SendTask6: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask8: Received "ping 8" len 7 from C66X_2 endPt 13 SendTask7: Received "ping 8" len 7 from C66X_1 endPt 13 SendTask3: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask4: RPMessage_recv failed with code -1 SendTask9: RPMessage_recv failed with code -1 SendTask1: Received "ping 7" len 7 from mcu1_0 endPt 13 SendTask5: Received "ping 8" len 7 from mcu3_0 endPt 13 SendTask2: Received "ping 7" len 7 from mcu1_1 endPt 13 SendTask6: RPMessage_recv failed with code -1 SendTask8: Sending "ping 9" from mpu1_0 to C66X_2... SendTask7: Sending "ping 9" from mpu1_0 to C66X_1... SendTask3: RPMessage_recv failed with code -1 SendTask4: Received "ping 8" len 7 from mcu2_1 endPt 13 SendTask9: Received "ping 8" len 7 from C7X_1 endPt 13 SendTask1: Sending "ping 8" from mpu1_0 to mcu1_0... SendTask5: Sending "ping 9" from mpu1_0 to mcu3_0... SendTask2: Sending "ping 8" from mpu1_0 to mcu1_1... SendTask6: Received "ping 8" len 7 from mcu3_1 endPt 13 SendTask8: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask7: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask3: Received "ping 8" len 7 from mcu2_0 endPt 13 SendTask4: Sending "ping 9" from mpu1_0 to mcu2_1... SendTask9: Sending "ping 9" from mpu1_0 to C7X_1... SendTask1: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask5: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask2: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask6: Sending "ping 9" from mpu1_0 to mcu3_1... SendTask8: RPMessage_recv failed with code -1 SendTask7: RPMessage_recv failed with code -1 SendTask3: Sending "ping 9" from mpu1_0 to mcu2_0... SendTask4: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask9: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask1: RPMessage_recv failed with code -1 SendTask5: RPMessage_recv failed with code -1 SendTask2: RPMessage_recv failed with code -1 SendTask6: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask8: Received "ping 9" len 7 from C66X_2 endPt 13 SendTask7: Received "ping 9" len 7 from C66X_1 endPt 13 SendTask3: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask4: RPMessage_recv failed with code -1 SendTask9: RPMessage_recv failed with code -1 SendTask1: Received "ping 8" len 7 from mcu1_0 endPt 13 SendTask5: Received "ping 9" len 7 from mcu3_0 endPt 13 SendTask2: Received "ping 8" len 7 from mcu1_1 endPt 13 SendTask6: RPMessage_recv failed with code -1 SendTask8: mpu1_0 <--> C66X_2, Ping- 10, pong - 10 completed SendTask7: mpu1_0 <--> C66X_1, Ping- 10, pong - 10 completed SendTask3: RPMessage_recv failed with code -1 SendTask4: Received "ping 9" len 7 from mcu2_1 endPt 13 SendTask9: Received "ping 9" len 7 from C7X_1 endPt 13 SendTask1: Sending "ping 9" from mpu1_0 to mcu1_0... SendTask5: mpu1_0 <--> mcu3_0, Ping- 10, pong - 10 completed SendTask2: Sending "ping 9" from mpu1_0 to mcu1_1... SendTask6: Received "ping 9" len 7 from mcu3_1 endPt 13 SendTask3: Received "ping 9" len 7 from mcu2_0 endPt 13 SendTask4: mpu1_0 <--> mcu2_1, Ping- 10, pong - 10 completed SendTask9: mpu1_0 <--> C7X_1, Ping- 10, pong - 10 completed SendTask1: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask2: rpmsg_senderFxn: RPMessage_send failed status -1 SendTask6: mpu1_0 <--> mcu3_1, Ping- 10, pong - 10 completed SendTask3: mpu1_0 <--> mcu2_0, Ping- 10, pong - 10 completed SendTask1: RPMessage_recv failed with code -1 SendTask2: RPMessage_recv failed with code -1 SendTask1: Received "ping 9" len 7 from mcu1_0 endPt 13 SendTask2: Received "ping 9" len 7 from mcu1_1 endPt 13 SendTask1: mpu1_0 <--> mcu1_0, Ping- 10, pong - 10 completed SendTask2: mpu1_0 <--> mcu1_1, Ping- 10, pong - 10 completed
然后、我在 版本7.02 (RTOS+QNX)中验证 IPC_TEST。 它的工作原理。
U-Boot SPL 2020.01-g2781231a33 (Apr 10 2021 - 01:08:23 +0000) SYSFW ABI: 3.1 (firmware rev 0x0015 '21.1.1--v2021.01a (Terrific Lla') Trying to boot from MMC2 Loading Environment from MMC... *** Warning - No MMC card found, using default environment Starting ATF on ARM64 core... NOTICE: BL31: v2.4(release):07.03.00.005-dirty NOTICE: BL31: Built : 00:15:40, Apr 10 2021 U-Boot SPL 2020.01-g2781231a33 (Apr 10 2021 - 00:17:14 +0000) SYSFW ABI: 3.1 (firmware rev 0x0015 '21.1.1--v2021.01a (Terrific Lla') Detected: J7X-BASE-CPB rev E3 Detected: J7X-VSC8514-ETH rev E2 Trying to boot from MMC2 U-Boot 2020.01-g2781231a33 (Apr 10 2021 - 00:17:14 +0000) SoC: J721E SR1.0 Model: Texas Instruments K3 J721E SoC Board: J721EX-PM2-SOM rev E7 DRAM: 4 GiB not found for dev hbmc-mux Flash: 0 Bytes MMC: sdhci@4f80000: 0, sdhci@4fb0000: 1 Loading Environment from MMC... OK In: serial@2800000 Out: serial@2800000 Err: serial@2800000 Detected: J7X-BASE-CPB rev E3 Detected: J7X-VSC8514-ETH rev E2 Net: K3 CPSW: nuss_ver: 0x6BA00101 cpsw_ver: 0x6BA80100 ale_ver: 0x00293904 Ports:1 mdio_freq:1000000 Warning: ethernet@46000000 using MAC address from ROM eth0: ethernet@46000000 Hit any key to stop autoboot: 0 switch to partitions #0, OK mmc1 is current device SD/MMC found on device 1 530 bytes read in 3 ms (171.9 KiB/s) Loaded env from uEnv.txt Importing environment from mmc1 ... Running uenvcmd ... Core 1 is already in use. No rproc commands work Core 2 is already in use. No rproc commands work 4274368 bytes read in 90 ms (45.3 MiB/s) Load Remote Processor 2 with data@addr=0x82000000 4274368 bytes: Success! 4274352 bytes read in 90 ms (45.3 MiB/s) Load Remote Processor 3 with data@addr=0x82000000 4274352 bytes: Success! 4274348 bytes read in 91 ms (44.8 MiB/s) Load Remote Processor 4 with data@addr=0x82000000 4274348 bytes: Success! 4274352 bytes read in 91 ms (44.8 MiB/s) Load Remote Processor 5 with data@addr=0x82000000 4274352 bytes: Success! 5433728 bytes read in 116 ms (44.7 MiB/s) Load Remote Processor 6 with data@addr=0x82000000 5433728 bytes: Success! 5433740 bytes read in 114 ms (45.5 MiB/s) Load Remote Processor 7 with data@addr=0x82000000 5433740 bytes: Success! 11460416 bytes read in 36 ms (303.6 MiB/s) Load Remote Processor 8 with data@addr=0x82000000 11460416 bytes: Success! 8176360 bytes read in 173 ms (45.1 MiB/s) ## Starting application at 0x80080000 ... MMU: 16-bit ASID 44-bit PA TCR_EL1=b5183519 cpu0: MPIDR=80000000 cpu0: MIDR=411fd080 Cortex-A72 r1p0 cpu0: CWG=4 ERG=4 Dminline=4 Iminline=4 PIPT cpu0: CLIDR=a200023 LoUU=1 LoC=2 LoUIS=1 cpu0: L1 Icache 48K linesz=64 set/way=256/3 cpu0: L1 Dcache 32K linesz=64 set/way=256/2 cpu0: L2 Unified 1024K linesz=64 set/way=1024/16 Display set to R5 Loading IFS...decompressing...done cpu1: MPIDR=80000001 cpu1: MIDR=411fd080 Cortex-A72 r1p0 cpu1: CWG=4 ERG=4 Dminline=4 Iminline=4 PIPT cpu1: CLIDR=a200023 LoUU=1 LoC=2 LoUIS=1 cpu1: L1 Icache 48K linesz=64 set/way=256/3 cpu1: L1 Dcache 32K linesz=64 set/way=256/2 cpu1: L2 Unified 1024K linesz=64 set/way=1024/16 System page at phys:0000000080011000 user:ffffff8040254000 kern:ffffff8040251000 Starting next program at vffffff8060086e10 All ClockCycles offsets within tolerance Welcome to QNX Neutrino 7.1.0 on the TI J721E EVM Board!! Starting random service ... start serial driver Starting MMC/SD memory card driver... eMMC Starting MMC/SD memory card driver... SD Starting XHCI driver on USB3SS0 and USB3SS1 Path=0 - am65x target=0 lun=0 Direct-Access(0) - SDMMC: S0J56X Rev: 1.0 Setting environment variables... done.. Looking for user script to run: /ti_fs/scripts/user.sh Running user script... user.sh called... Setting additional environment variables... Starting tisci-mgr.. Starting shmemallocator.. Starting tiipc-mgr.. Mailbox_plugInterrupt: interrupt Number 489, arg 0xF0B05EA0 Mailbox_plugInterrupt: interrupt Number 490, arg 0xF0B06040 Mailbox_plugInterrupt: interrupt Number 491, arg 0xF0B061E0 Mailbox_plugInterrupt: interrupt Number 492, arg 0xF0B06380 Mailbox_plugInterrupt: interrupt Number 493, arg 0xF0B06520 Starting TI IPC Resmgr Starting tiudma-mgr.. Start screen.. screen started with dss_on_r5 configuration.. done... J7EVM@QNX:/# ipc_test IPC_echo_test (core : mpu1_0) ..... responderFxn will stay active. Please use ctrl-c to exit the test when finished. SendTask9: mpu1_0 <--> C7X_1, Ping- 10, pong - 10 completed SendTask7: mpu1_0 <--> C66X_1, Ping- 10, pong - 10 completed SendTask8: mpu1_0 <--> C66X_2, Ping- 10, pong - 10 completed SendTask6: mpu1_0 <--> mcu3_1, Ping- 10, pong - 10 completed SendTask4: mpu1_0 <--> mcu2_1, Ping- 10, pong - 10 completed SendTask5: mpu1_0 <--> mcu3_0, Ping- 10, pong - 10 completed SendTask3: mpu1_0 <--> mcu2_0, Ping- 10, pong - 10 completed
但 MPU 和 mcu1之间没有 SendTask。 如何解决这个问题?
您好!
关于 在 PSDK 7.3上运行的 IPC_TEST、请参阅以下链接上的默认安装说明、无需修改代码:
(+)[常见问题解答] TDA4VM:PSDK QNX 7.2/PSDK QNX 7.3上的 IPC_Test -处理器论坛-处理器- TI E2E 支持论坛
关于 MPU 到 MCU1的通信、由于 MCU1映像已在运行、 因此未加载"IPC echo test"固件映像。 将更新此主题、并提供解决此问题的建议步骤。
KB
您好 KB:
感谢你的答复。
根据 IPC_TEST 示例、已知 7.02或7.03版中未实现 MPU 到 MCU1的通信。此外、系统存储器映射与之前的版本不同。
发件人线程:
TDA4VM:在构建 MCU1_0后,运行 Vision Apps Demos for Display,出现 IPC 错误。 -处理器论坛-处理器- TI E2E 支持论坛
已知 Vision Apps 为启用 IPC 的 MCU1_0生成的固件映像在7.03版中无法正常工作。
那么、如何证明 MCU1_0和 MPU IPC 通信?
2 .MPU 到 MCU1 IPC 通信是我们项目中需要开发的一项紧急任务。 我们尝试使用 cddipc 来满足此要求 、但失败了。
要在项目中使用 cddipc 进行参考,必须成功进行 IPC 通信。
我想知道 cddipc 模块是否是 MPU 到 MCU1 IPC 通信的可用方式?
3.如果 cddipc 不起作用,根据 TI 的建议,如何 实现 MPU 到 MCU1 IPC 的通信?
您好!
该问题与在 MCU1上运行的固件映像有关。 要使 IPC 测试成功、MCU1固件映像需要:
根据之前的响应、TI 将 使用解决方法的建议步骤更新此主题。
此致、
KB
您好!
参考 PSDK QNX 7.1的常见问题解答:
(+)[常见问题解答] PROCESSOR-SDK-DRA8X-TDA4X:如何在 PSDKQA7.0上使用 IPC 示例应用回波测试-处理器论坛-处理器- TI E2E 支持论坛
其中的日志显示 mcu1_0响应 IPC 回波测试:
"SendTask1:mpu1_0 <->mcu1_0、乒声10、pong -10已完成"
此致、
KB
您好 KB:
感谢你的答复。
关注您的主题:
(+)[常见问题解答] TDA4VM:PSDK QNX 7.2/PSDK QNX 7.3上的 IPC_Test -处理器论坛-处理器- TI E2E 支持论坛
我得到的结果与您相同。
您好!
补丁 PSDK_QNX_07_03_03_patch 可从 PROCESSOR-SDK-QNX-J721E_07.03.00.02 | TI.com 获取、该补丁包含自述文件和说明。
应用 PSDK_QNX_07_03_03_patch 并遵循自述文件说明后 、预期 IPC_echo 测试的 MCU1_0通信将正常运行。
此致、
KB