您好!
我正在使用 SDK 8.2下的 J7200 cpsw5g Linux 本机驱动程序和 J721E cpsw2g 测试以太网功能。
以下是我的客户电路板配置:
摄像头---- J721E cpsw2g -- J7200 cpsw5g 充当开关-- J721E cpsw2g -- J721E 显示摄像头流
20分钟后、链路断开、 物理层错误、 按如下方式进行记录
(1) J7200 PHY 错误
[ 1348.301156] davinci_mdio c000f00.mdio: timed out waiting for user access [ 1348.307976] ------------[ cut here ]------------ [ 1348.312593] WARNING: CPU: 0 PID: 104 at drivers/net/phy/phy.c:958 phy_error+0x14/0x60 [ 1348.320400] Modules linked in: xt_conntrack xt_MASQUERADE xt_addrtype iptable_filter iptable_nat nf_nat nf_conntrack nf_defrag_ipv6 nf_defrag_ipv4 libcrc32c ip_tables x_tables overlay xfrm_user xfrm_algo md5 ecb aes_neon_bs aes_neon_blk des_generic libdes cbc bridge stp llc bluetooth ecdh_generic ecc rfkill rpmsg_char omap_rng rng_core crct10dif_ce ti_k3_r5_remoteproc virtio_rpmsg_bus sa2ul sha512_generic authenc rti_wdt sch_fq_codel rpmsg_kdrv_switch cryptodev(O) ipv6 [ 1348.361909] CPU: 0 PID: 104 Comm: kworker/u4:2 Tainted: G O 5.10.100-g7a7a3af903 #3 [ 1348.370844] Hardware name: Texas Instruments K3 J7200 SoC (DT) [ 1348.376663] Workqueue: events_power_efficient phy_state_machine [ 1348.382567] pstate: 60000005 (nZCv daif -PAN -UAO -TCO BTYPE=--) [ 1348.388556] pc : phy_error+0x14/0x60 [ 1348.392118] lr : phy_state_machine+0x88/0x218 [ 1348.396457] sp : ffff8000130cfd30 [ 1348.399758] x29: ffff8000130cfd30 x28: ffff800011151000 [ 1348.405055] x27: ffff000800050070 x26: ffff000800050020 [ 1348.410351] x25: 0000000000000000 x24: 00000000ffffff92 [ 1348.415648] x23: ffff0008027f04e8 x22: ffff000800356200 [ 1348.420944] x21: ffff0008027f0000 x20: 0000000000000005 [ 1348.426239] x19: ffff0008027f0000 x18: 0000000000000010 [ 1348.431536] x17: 0000000000000000 x16: 0000000000000000 [ 1348.436832] x15: ffff000800356730 x14: 0000000000000343 [ 1348.442128] x13: 0000000000000000 x12: 0000000000000044 [ 1348.447424] x11: 0000000000000000 x10: 00000000000009a0 [ 1348.452721] x9 : 0000000000000366 x8 : ffff00087facb0c0 [ 1348.458017] x7 : ffff0008001654c0 x6 : 0000000000000003 [ 1348.463313] x5 : 0000000000000000 x4 : 0000000000000000 [ 1348.468609] x3 : ffff0008027f04e8 x2 : 0000000000000000 [ 1348.473904] x1 : ffff000800356200 x0 : ffff0008027f0000 [ 1348.479201] Call trace: [ 1348.481637] phy_error+0x14/0x60 [ 1348.484851] phy_state_machine+0x88/0x218 [ 1348.488849] process_one_work+0x1a0/0x328 [ 1348.492845] worker_thread+0x4c/0x420 [ 1348.496495] kthread+0x140/0x160 [ 1348.499710] ret_from_fork+0x10/0x34 [ 1348.503272] ---[ end trace c5674e92eabd970e ]---
(2) J721E PHY 错误
[12957.256255] am65-cpsw-nuss 46000000.ethernet eth0: Link is Down [12965.448175] ------------[ cut here ]------------ [12965.452798] WARNING: CPU: 0 PID: 2714 at drivers/net/phy/phy.c:958 phy_error+0x14/0x60 [12965.460692] Modules linked in: xt_conntrack xt_MASQUERADE xt_addrtype iptable_filter iptable_nat nf_nat nf_conntrack nf_defrag_ipv6 nf_defrag_ipv4 libcrc32c ip_tables x_tables bridge stp llc overlay xfrm_user xfrm_algo md5 ecb aes_neon_bs aes_neon_blk des_generic libdes cbc sch_mqprio act_skbedit cls_u32 sch_ingress bluetooth ecdh_generic ecc rfkill rpmsg_char ti_am335x_adc kfifo_buf omap_rng rng_core pru_rproc icss_iep irq_pruss_intc crct10dif_ce ti_j721e_cpsw_virt_mac ti_am335x_tscadc ti_k3_r5_remoteproc pruss vxe_enc vxd_dec pvrsrvkm(O) sa2ul videobuf2_dma_contig videobuf2_dma_sg v4l2_mem2mem ti_k3_dsp_remoteproc sha512_generic authenc videobuf2_memops videobuf2_v4l2 videobuf2_common virtio_rpmsg_bus rti_wdt sch_fq_codel v4l2loopback rpmsg_kdrv_switch cryptodev(O) ipv6 [12965.529015] CPU: 0 PID: 2714 Comm: kworker/u4:2 Tainted: G O 5.10.100-g7a7a3af903 #2 [12965.538036] Hardware name: Texas Instruments K3 J721E SoC (DT) [12965.543854] Workqueue: events_power_efficient phy_state_machine [12965.549758] pstate: 60000005 (nZCv daif -PAN -UAO -TCO BTYPE=--) [12965.555746] pc : phy_error+0x14/0x60 [12965.559306] lr : phy_state_machine+0x88/0x218 [12965.563646] sp : ffff80012762fd30 [12965.566947] x29: ffff80012762fd30 x28: ffff800011151000 [12965.572243] x27: ffff80012e02fcc8 x26: ffff00082869a3c8 [12965.577539] x25: 0000000000000000 x24: 00000000fffffffb [12965.582835] x23: ffff0008241d8ce8 x22: ffff000824c59a00 [12965.588131] x21: ffff0008241d8800 x20: 0000000000000005 [12965.593427] x19: ffff0008241d8800 x18: 0000000000000000 [12965.598722] x17: 0000000000000000 x16: 0000000000000000 [12965.604018] x15: 0000ffff826fe430 x14: 00000000000003f5 [12965.609314] x13: 0000000000000000 x12: 0000000000000001 [12965.614611] x11: 0000000000000000 x10: 00000000000009a0 [12965.619907] x9 : ffff80012762fad0 x8 : ffff000824c5a400 [12965.625202] x7 : ffff00087fa6b140 x6 : 0000025c10f36475 [12965.630497] x5 : 00ffffffffffffff x4 : 0000000000000000 [12965.635793] x3 : ffff0008241d8ce8 x2 : 0000000000000000 [12965.641089] x1 : ffff000824c59a00 x0 : ffff0008241d8800 [12965.646386] Call trace: [12965.648821] phy_error+0x14/0x60 [12965.652036] phy_state_machine+0x88/0x218 [12965.656036] process_one_work+0x1a0/0x328 [12965.660030] worker_thread+0x4c/0x420 [12965.663678] kthread+0x140/0x160 [12965.666894] ret_from_fork+0x10/0x34 [12965.670455] ---[ end trace 91d0ddd4b6b6af5c ]---
[ 8414.315558] davinci_mdio c000f00.mdio: timed out waiting for user access [ 8414.322282] ------------[ cut here ]------------ [ 8414.326895] WARNING: CPU: 1 PID: 1409 at drivers/net/phy/phy.c:958 phy_error+0x14/0x60 [ 8414.334789] Modules linked in: xt_conntrack xt_MASQUERADE xt_addrtype iptable_filter iptabl e_nat nf_nat nf_conntrack nf_defrag_ipv6 nf_defrag_ipv4 libcrc32c ip_tables x_tables overlay x frm_user xfrm_algo md5 ecb aes_neon_bs aes_neon_blk des_generic libdes cbc act_skbedit cls_u32 sch_ingress sch_taprio bridge stp llc bluetooth ecdh_generic ecc rfkill rpmsg_char omap_rng r ng_core crct10dif_ce sa2ul sha512_generic authenc ti_k3_r5_remoteproc virtio_rpmsg_bus rti_wdt sch_fq_codel rpmsg_kdrv_switch cryptodev(O) ipv6 [ 8414.380033] CPU: 1 PID: 1409 Comm: kworker/u4:2 Tainted: G O 5.10.100-g7a7a3 af903 #3 [ 8414.389055] Hardware name: Texas Instruments K3 J7200 SoC (DT) [ 8414.394878] Workqueue: events_power_efficient phy_state_machine [ 8414.400782] pstate: 60000005 (nZCv daif -PAN -UAO -TCO BTYPE=--) [ 8414.406771] pc : phy_error+0x14/0x60 [ 8414.410334] lr : phy_state_machine+0x88/0x218 [ 8414.414674] sp : ffff8000194efd30 [ 8414.417975] x29: ffff8000194efd30 x28: ffff800011151000 [ 8414.423271] x27: ffff80001222fcc8 x26: ffff000803a8ad48 [ 8414.428567] x25: 0000000000000000 x24: 00000000ffffff92 [ 8414.433862] x23: ffff0008023144e8 x22: ffff000801227e00 [ 8414.439158] x21: ffff000802314000 x20: 0000000000000004 [ 8414.444455] x19: ffff000802314000 x18: 0000000000000010 [ 8414.449751] x17: 0000000000000000 x16: 0000000000000000 [ 8414.455047] x15: ffff000801228330 x14: 00000000000001d7 [ 8414.460343] x13: ffff000801228330 x12: 00000000ffffffea [ 8414.465639] x11: ffff8000111da3e0 x10: ffff8000111c23a0 [ 8414.470936] x9 : ffff8000111c23f8 x8 : 0000000000017fe8 [ 8414.476232] x7 : c0000000ffffefff x6 : 0000018817072da5 [ 8414.481528] x5 : 00ffffffffffffff x4 : 0000000000000000 [ 8414.486824] x3 : ffff0008023144e8 x2 : 0000000000000000 [ 8414.492120] x1 : ffff000801227e00 x0 : ffff000802314000 [ 8414.497416] Call trace: [ 8414.499853] phy_error+0x14/0x60 [ 8414.503069] phy_state_machine+0x88/0x218 [ 8414.507066] process_one_work+0x1a0/0x328 [ 8414.511062] worker_thread+0x4c/0x420 [ 8414.514711] kthread+0x140/0x160 [ 8414.517926] ret_from_fork+0x10/0x34 [ 8414.521487] ---[ end trace d905449417dbb081 ]---
对此有什么想法吗?
BR
Jay