This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] AM6442:AM64x 和 AM65x、eth0不能在引导时使用静态 IP 提供

Guru**** 2560390 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1027383/am6442-am64x-and-am65x-eth0-doesn-t-come-up-at-boot-with-static-ip

器件型号:AM6442

尊敬的 TI 团队:

在 AM64x EVM 和 AM65x EVM 上、我注意到如果我为 eth0分配静态 IP 地址(通过更改/etc/network/interfaces 并重新引导)、则 eth0在引导时不会分配静态 IP。 网卡仍然未配置、但可以通过两次发出"ifdown eth0 && ifup eth0"来修复(一次似乎没有执行)。

请参阅下面的 AM64x EVM 控制台日志、其中显示 eth0已关闭、直到我连续发出 ifdown/ifup 两次:

 _____                    _____           _         _
|  _  |___ ___ ___ ___   |  _  |___ ___  |_|___ ___| |_
|     |  _| .'| . | . |  |   __|  _| . | | | -_|  _|  _|
|__|__|_| |__,|_  |___|  |__|  |_| |___|_| |___|___|_|
              |___|                    |___|

Arago Project http://arago-project.org am64xx-evm ttyS2

Arago 2020.09 am64xx-evm ttyS2

[   16.478620] omap_rng 40910000.rng: Random Number Generator ver. 241b34c
[   16.611492] icssg-prueth icssg1-eth: TI PRU ethernet driver initialized: single EMAC mode
[   17.427651] usbcore: registered new interface driver usbfs
[   17.478077] usbcore: registered new interface driver hub
[   17.515878] usbcore: registered new device driver usb
[   17.936466] remoteproc remoteproc10: powering up 300b4000.pru
[   17.950552] remoteproc remoteproc10: Booting fw image ti-pruss/am65x-sr2-pru0-prueth-fw.elf, size 36316
[   17.965024] remoteproc remoteproc10: unsupported resource 5
[   17.976961] remoteproc remoteproc10: remote processor 300b4000.pru is now up
[   17.989697] remoteproc remoteproc11: powering up 30084000.rtu
[   18.005061] remoteproc remoteproc11: Booting fw image ti-pruss/am65x-sr2-rtu0-prueth-fw.elf, size 29944
[   18.033018] remoteproc remoteproc11: remote processor 30084000.rtu is now up
[   18.052946] remoteproc remoteproc12: powering up 3008a000.txpru
[   18.068431] remoteproc remoteproc12: Booting fw image ti-pruss/am65x-sr2-txpru0-prueth-fw.elf, size 35916
[   18.085055] remoteproc remoteproc12: remote processor 3008a000.txpru is now up
[   18.102406] pps pps1: new PPS source ptp2
[   18.122100] TI DP83869 300b2400.mdio:0f: attached PHY driver [TI DP83869] (mii_bus:phy_addr=300b2400.mdio:0f, irq=POLL)
[   18.141192] net eth2: started

am64xx-evm login: root
Password:
root@am64xx-evm:~# ifconfig
eth0: flags=4163<UP,BROADCAST,RUNNING,MULTICAST>  mtu 1500  metric 1
        inet6 fe80::f684:4cff:fef9:7d1a  prefixlen 64  scopeid 0x20<link>
        ether f4:84:4c:f9:7d:1a  txqueuelen 1000  (Ethernet)
        RX packets 86  bytes 7878 (7.6 KiB)
        RX errors 0  dropped 0  overruns 0  frame 0
        TX packets 25  bytes 4186 (4.0 KiB)
        TX errors 0  dropped 0 overruns 0  carrier 0  collisions 0

eth1: flags=4099<UP,BROADCAST,MULTICAST>  mtu 1500  metric 1
        ether 70:ff:76:1e:29:1a  txqueuelen 1000  (Ethernet)
        RX packets 0  bytes 0 (0.0 B)
        RX errors 0  dropped 0  overruns 0  frame 0
        TX packets 0  bytes 0 (0.0 B)
        TX errors 0  dropped 0 overruns 0  carrier 0  collisions 0

eth2: flags=4099<UP,BROADCAST,MULTICAST>  mtu 1500  metric 1
        ether 70:ff:76:1e:29:1b  txqueuelen 1000  (Ethernet)
        RX packets 0  bytes 0 (0.0 B)
        RX errors 0  dropped 0  overruns 0  frame 0
        TX packets 0  bytes 0 (0.0 B)
        TX errors 0  dropped 0 overruns 0  carrier 0  collisions 0

lo: flags=73<UP,LOOPBACK,RUNNING>  mtu 65536  metric 1
        inet 127.0.0.1  netmask 255.0.0.0
        inet6 ::1  prefixlen 128  scopeid 0x10<host>
        loop  txqueuelen 1000  (Local Loopback)
        RX packets 82  bytes 6220 (6.0 KiB)
        RX errors 0  dropped 0  overruns 0  frame 0
        TX packets 82  bytes 6220 (6.0 KiB)
        TX errors 0  dropped 0 overruns 0  carrier 0  collisions 0

root@am64xx-evm:~# ping 192.168.10.1
PING 192.168.10.1 (192.168.10.1): 56 data bytes
ping: sendto: Network is unreachable
root@am64xx-evm:~# ifdown eth0 && ifup eth0 && ifdown eth0 && ifup eth0
ifdown: interface eth0 not configured
[   64.606611] am65-cpsw-nuss 8000000.ethernet eth0: Link is Down
[   64.702978] TI DP83867 8000f00.mdio:00: attached PHY driver [TI DP83867] (mii_bus:phy_addr=8000f00.mdio:00, irq=POLL)
[   64.716307] am65-cpsw-nuss 8000000.ethernet eth0: Link is Down
root@am64xx-evm:~# [   67.802461] am65-cpsw-nuss 8000000.ethernet eth0: Link is Up - 1Gbps/Full - flow control off
[   67.810979] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready

root@am64xx-evm:~# ping 192.168.10.1
PING 192.168.10.1 (192.168.10.1): 56 data bytes
64 bytes from 192.168.10.1: seq=0 ttl=128 time=1.609 ms
64 bytes from 192.168.10.1: seq=1 ttl=128 time=1.423 ms
64 bytes from 192.168.10.1: seq=2 ttl=128 time=1.411 ms
64 bytes from 192.168.10.1: seq=3 ttl=128 time=1.179 ms
^C
--- 192.168.10.1 ping statistics ---
4 packets transmitted, 4 packets received, 0% packet loss
round-trip min/avg/max = 1.179/1.405/1.609 ms
root@am64xx-evm:~# ifconfig
eth0: flags=4163<UP,BROADCAST,RUNNING,MULTICAST>  mtu 1500  metric 1
        inet 192.168.10.2  netmask 255.255.0.0  broadcast 192.168.255.255
        inet6 fe80::f684:4cff:fef9:7d1a  prefixlen 64  scopeid 0x20<link>
        ether f4:84:4c:f9:7d:1a  txqueuelen 1000  (Ethernet)
        RX packets 268  bytes 28611 (27.9 KiB)
        RX errors 0  dropped 0  overruns 0  frame 0
        TX packets 75  bytes 11457 (11.1 KiB)
        TX errors 0  dropped 0 overruns 0  carrier 0  collisions 0

eth1: flags=4099<UP,BROADCAST,MULTICAST>  mtu 1500  metric 1
        ether 70:ff:76:1e:29:1a  txqueuelen 1000  (Ethernet)
        RX packets 0  bytes 0 (0.0 B)
        RX errors 0  dropped 0  overruns 0  frame 0
        TX packets 0  bytes 0 (0.0 B)
        TX errors 0  dropped 0 overruns 0  carrier 0  collisions 0

eth2: flags=4099<UP,BROADCAST,MULTICAST>  mtu 1500  metric 1
        ether 70:ff:76:1e:29:1b  txqueuelen 1000  (Ethernet)
        RX packets 0  bytes 0 (0.0 B)
        RX errors 0  dropped 0  overruns 0  frame 0
        TX packets 0  bytes 0 (0.0 B)
        TX errors 0  dropped 0 overruns 0  carrier 0  collisions 0

lo: flags=73<UP,LOOPBACK,RUNNING>  mtu 65536  metric 1
        inet 127.0.0.1  netmask 255.0.0.0
        inet6 ::1  prefixlen 128  scopeid 0x10<host>
        loop  txqueuelen 1000  (Local Loopback)
        RX packets 82  bytes 6220 (6.0 KiB)
        RX errors 0  dropped 0  overruns 0  frame 0
        TX packets 82  bytes 6220 (6.0 KiB)
        TX errors 0  dropped 0 overruns 0  carrier 0  collisions 0