This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TDA4VM:7.03版 RTOS+QNX 中发生远程服务测试失败

Guru**** 2539500 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1024493/tda4vm-remote-service-test-fail-occured-in-version-7-03-rtos-qnx

器件型号:TDA4VM

 应用 PSDK_QNX_07_03_03_patch 后、  

修改文件:

在   vision_apps/vision_apps_build_flags.mak 中   

BUIL_CPU_MPU1?=是
BUIL_CPU_MCU1_0?=是
BUIL_CPU_MCU2_0?=是
BUIL_CPU_MCU2_1?=是
BUIL_CPU_MCU3_0?=否
Build_CPU_MCU3_1?=否
build_cpu_c6x_1?=是
build_cpu_c6x_2?=是
build_cpu_c7x_1?=是

在  vision_apps/apps/basic_demos/app_tirtos/common/app_cfg.h 中

#define ENABLE_IPC_MPU1_0
#define ENABLE_IPC_MCU1_0
//#define ENABLE_IPC_MCU1_1
#define ENABLE_IPC_MCU2_0
#define ENABLE_IPC_MCU2_1
//#define ENABLE_IPC_MCU3_0
//#define ENABLE_IPC_MCU3_1
#define ENABLE_IPC_C6X_1
#define ENABLE_IPC_C6X_2
#define ENABLE_IPC_C7x_1

运行 EVM。

运行 vx_app_arm_ipc.out。   

U-Boot SPL 2020.01-g2781231a33 (Apr 10 2021 - 01:08:23 +0000)
SYSFW ABI: 3.1 (firmware rev 0x0015 '21.1.1--v2021.01a (Terrific Lla')
Trying to boot from MMC2
Loading Environment from MMC... *** Warning - No MMC card found, using default environment

Starting ATF on ARM64 core...

NOTICE:  BL31: v2.4(release):07.03.00.005-dirty
NOTICE:  BL31: Built : 00:15:40, Apr 10 2021

U-Boot SPL 2020.01-dirty (Aug 04 2021 - 15:21:39 +0800)
SYSFW ABI: 3.1 (firmware rev 0x0015 '21.1.1--v2021.01a (Terrific Lla')
Detected: J7X-BASE-CPB rev E3
Detected: J7X-VSC8514-ETH rev E2
Trying to boot from MMC2


U-Boot 2020.01-dirty (Aug 04 2021 - 14:54:55 +0800)

SoC:   J721E SR1.0
Model: Texas Instruments K3 J721E SoC
Board: J721EX-PM2-SOM rev E7
DRAM:  4 GiB
not found for dev hbmc-mux
Flash: 0 Bytes
MMC:   sdhci@4f80000: 0, sdhci@4fb0000: 1
Loading Environment from MMC... *** Warning - bad CRC, using default environment

In:    serial@2800000
Out:   serial@2800000
Err:   serial@2800000
Detected: J7X-BASE-CPB rev E3
Detected: J7X-VSC8514-ETH rev E2
Net:   K3 CPSW: nuss_ver: 0x6BA00101 cpsw_ver: 0x6BA80100 ale_ver: 0x00293904 Ports:1 mdio_freq:1000000

Warning: ethernet@46000000 using MAC address from ROM
eth0: ethernet@46000000
Hit any key to stop autoboot:  0
switch to partitions #0, OK
mmc1 is current device
SD/MMC found on device 1
526 bytes read in 3 ms (170.9 KiB/s)
Loaded env from uEnv.txt
Importing environment from mmc1 ...
Running uenvcmd ...
Core 1 is already in use. No rproc commands work
Core 2 is already in use. No rproc commands work
5265720 bytes read in 111 ms (45.2 MiB/s)
Load Remote Processor 2 with data@addr=0x82000000 5265720 bytes: Success!
1968096 bytes read in 43 ms (43.6 MiB/s)
Load Remote Processor 3 with data@addr=0x82000000 1968096 bytes: Success!
1579120 bytes read in 33 ms (45.6 MiB/s)
Load Remote Processor 6 with data@addr=0x82000000 1579120 bytes: Success!
1579120 bytes read in 34 ms (44.3 MiB/s)
Load Remote Processor 7 with data@addr=0x82000000 1579120 bytes: Success!
10268600 bytes read in 90 ms (108.8 MiB/s)
Load Remote Processor 8 with data@addr=0x82000000 10268600 bytes: Success!
8176892 bytes read in 173 ms (45.1 MiB/s)
## Starting application at 0x80080000 ...
MMU: 16-bit ASID 44-bit PA TCR_EL1=b5183519
cpu0: MPIDR=80000000
cpu0: MIDR=411fd080 Cortex-A72 r1p0
cpu0: CWG=4 ERG=4 Dminline=4 Iminline=4 PIPT
cpu0: CLIDR=a200023 LoUU=1 LoC=2 LoUIS=1
cpu0: L1 Icache 48K linesz=64 set/way=256/3
cpu0: L1 Dcache 32K linesz=64 set/way=256/2
cpu0: L2 Unified 1024K linesz=64 set/way=1024/16
Display set to R5
Loading IFS...decompressing...done
cpu1: MPIDR=80000001
cpu1: MIDR=411fd080 Cortex-A72 r1p0
cpu1: CWG=4 ERG=4 Dminline=4 Iminline=4 PIPT
cpu1: CLIDR=a200023 LoUU=1 LoC=2 LoUIS=1
cpu1: L1 Icache 48K linesz=64 set/way=256/3
cpu1: L1 Dcache 32K linesz=64 set/way=256/2
cpu1: L2 Unified 1024K linesz=64 set/way=1024/16

System page at phys:0000000080011000 user:ffffff8040254000 kern:ffffff8040251000
Starting next program at vffffff8060086e10
All ClockCycles offsets within tolerance
Welcome to QNX Neutrino 7.1.0 on the TI J721E EVM Board!!
Starting random service ...
start serial driver
Starting MMC/SD memory card driver... eMMC
Starting MMC/SD memory card driver... SD
Starting XHCI driver on USB3SS0 and USB3SS1
Path=0 - am65x
 target=0 lun=0     Direct-Access(0) - SDMMC: S0J56X Rev: 1.0
Setting environment variables...
done..
Mounting the sd ..
Looking for user script to run: /ti_fs/scripts/user.sh
Running user script...
user.sh called...
Setting additional environment variables...
Starting tisci-mgr..
Starting shmemallocator..
Starting tiipc-mgr..
Mailbox_plugInterrupt: interrupt Number 489, arg 0xAE3D9328
Mailbox_plugInterrupt: interrupt Number 490, arg 0xAE3D94C8
Mailbox_plugInterrupt: interrupt Number 491, arg 0xAE3D9668
Mailbox_plugInterrupt: interrupt Number 492, arg 0xAE3D9808
Mailbox_plugInterrupt: interrupt Number 493, arg 0xAE3D99A8
Starting TI IPC Resmgr
Starting tiudma-mgr..
Start screen..
screen started with dss_on_r5 configuration..
done...
J7EVM@QNX:/#
J7EVM@QNX:/#
J7EVM@QNX:/# cd ti_fs/vision_apps/
J7EVM@QNX:/ti_fs/vision_apps# ./vx_app_arm_ipc.out
APP: Init QNX ... !!!
Sciclient_qnxVirtToPhyFxn:Error from mem_offset
Sciclient_qnxVirtToPhyFxn:Error from mem_offset
appIpcInit: IPC: Init QNX ... !!!
appIpcInit: IPC: Init ... Done !!!
  3876.607099 s: REMOTE_SERVICE: Init ... !!!
  3876.607216 s: REMOTE_SERVICE: Init ... Done !!!
  3876.607245 s: GTC Frequency = 200 MHz
APP: Init ... Done !!!
  3876.607269 s:  VX_ZONE_INIT:Enabled
  3876.607283 s:  VX_ZONE_ERROR:Enabled
  3876.607295 s:  VX_ZONE_WARNING:Enabled
  3876.607484 s:  VX_ZONE_INIT:[tivxInit:71] Initialization Done !!!
  3876.607519 s:  VX_ZONE_INIT:[tivxHostInit:48] Initialization Done for HOST !!!
  3876.607794 s: IPC: RX: mcu1_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0000
  3876.607991 s: IPC: RX: mcu1_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0001
  3876.608042 s: IPC: RX: mcu1_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0002
  3876.608087 s: IPC: RX: mcu1_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0003
  3876.608133 s: IPC: RX: mcu1_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0004
  3876.608240 s: IPC: RX: mcu1_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0005
  3876.608294 s: IPC: RX: mcu1_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0006
  3876.608342 s: IPC: RX: mcu1_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0007
  3876.608383 s: IPC: RX: mcu1_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0008
  3876.608439 s: IPC: RX: mcu2_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0000
  3876.608623 s: IPC: RX: mcu1_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0009
  3876.608705 s: IPC: RX: mcu2_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0001
  3876.608792 s: IPC: RX: mcu2_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0002
  3876.608865 s: IPC: RX: mcu2_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0003
  3876.608931 s: IPC: RX: mcu2_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0004
  3876.609008 s: IPC: RX: mcu1_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead000a
  3876.609081 s: IPC: RX: mcu1_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead000b
  3876.609152 s: IPC: RX: mcu1_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead000c
  3876.609228 s: IPC: RX: mcu1_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead000d
  3876.609286 s: IPC: RX: mcu1_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead000e
APP IPC: Waiting for all messages to get echoed from remote core...
  3876.744502 s: IPC: RX: mcu1_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead000f
  3876.744534 s: IPC: RX: mcu2_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0005
  3876.744565 s: IPC: RX: mcu2_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0006
  3876.744595 s: IPC: RX: mcu2_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0007
  3876.744624 s: IPC: RX: mcu2_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0008
  3876.744654 s: IPC: RX: mcu2_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0009
  3876.744684 s: IPC: RX: mcu2_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead000a
  3876.744713 s: IPC: RX: mcu2_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead000b
  3876.744746 s: IPC: RX: mcu2_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead000c
  3876.744775 s: IPC: RX: mcu2_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead000d
  3876.744804 s: IPC: RX: mcu2_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0000
  3876.744835 s: IPC: RX: mcu2_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead000e
  3876.744864 s: IPC: RX: mcu2_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead000f
  3876.744894 s: IPC: RX: mcu2_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0001
  3876.744924 s: IPC: RX: mcu2_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0002
  3876.744953 s: IPC: RX: mcu2_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0003
  3876.744982 s: IPC: RX: mcu2_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0004
  3876.745012 s: IPC: RX: mcu2_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0005
  3876.879517 s: IPC: RX: mcu2_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0006
  3876.879548 s: IPC: RX: mcu2_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0007
  3876.879577 s: IPC: RX: mcu2_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0008
  3876.879607 s: IPC: RX: C66X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0000
  3876.879637 s: IPC: RX: mcu2_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0009
  3876.879666 s: IPC: RX: mcu2_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead000a
  3876.879696 s: IPC: RX: mcu2_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead000b
  3876.879728 s: IPC: RX: mcu2_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead000c
  3876.879757 s: IPC: RX: mcu2_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead000d
  3876.879788 s: IPC: RX: C66X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0001
  3876.879817 s: IPC: RX: mcu2_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead000e
  3876.879847 s: IPC: RX: mcu2_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead000f
  3876.879876 s: IPC: RX: C66X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0002
  3876.879906 s: IPC: RX: C66X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0003
  3876.879936 s: IPC: RX: C66X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0004
  3876.879965 s: IPC: RX: C66X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0005
  3876.879994 s: IPC: RX: C66X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0006
  3876.880024 s: IPC: RX: C66X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0007
  3876.880054 s: IPC: RX: C66X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0008
  3877.014543 s: IPC: RX: C66X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0009
  3877.014573 s: IPC: RX: C66X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead000a
  3877.014603 s: IPC: RX: C66X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead000b
  3877.014633 s: IPC: RX: C66X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead000c
  3877.014662 s: IPC: RX: C66X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead000d
  3877.014691 s: IPC: RX: C66X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead000e
  3877.014723 s: IPC: RX: C66X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead000f
  3877.014753 s: IPC: RX: C66X_2 (port 13) -> mpu1_0 (port 101) msg = 0xdead0000
  3877.014782 s: IPC: RX: C66X_2 (port 13) -> mpu1_0 (port 101) msg = 0xdead0001
  3877.014813 s: IPC: RX: C66X_2 (port 13) -> mpu1_0 (port 101) msg = 0xdead0002
  3877.014842 s: IPC: RX: C66X_2 (port 13) -> mpu1_0 (port 101) msg = 0xdead0003
  3877.014871 s: IPC: RX: C66X_2 (port 13) -> mpu1_0 (port 101) msg = 0xdead0004
  3877.014901 s: IPC: RX: C66X_2 (port 13) -> mpu1_0 (port 101) msg = 0xdead0005
  3877.014931 s: IPC: RX: C66X_2 (port 13) -> mpu1_0 (port 101) msg = 0xdead0006
  3877.014961 s: IPC: RX: C66X_2 (port 13) -> mpu1_0 (port 101) msg = 0xdead0007
  3877.014990 s: IPC: RX: C66X_2 (port 13) -> mpu1_0 (port 101) msg = 0xdead0008
  3877.015019 s: IPC: RX: C66X_2 (port 13) -> mpu1_0 (port 101) msg = 0xdead0009
  3877.015049 s: IPC: RX: C66X_2 (port 13) -> mpu1_0 (port 101) msg = 0xdead000a
  3877.015079 s: IPC: RX: C66X_2 (port 13) -> mpu1_0 (port 101) msg = 0xdead000b
  3877.149569 s: IPC: RX: C66X_2 (port 13) -> mpu1_0 (port 101) msg = 0xdead000c
  3877.149599 s: IPC: RX: C66X_2 (port 13) -> mpu1_0 (port 101) msg = 0xdead000d
  3877.149629 s: IPC: RX: C66X_2 (port 13) -> mpu1_0 (port 101) msg = 0xdead000e
  3877.149659 s: IPC: RX: C66X_2 (port 13) -> mpu1_0 (port 101) msg = 0xdead000f
  3877.149688 s: IPC: RX: C7X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0000
  3877.149719 s: IPC: RX: C7X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0001
  3877.149750 s: IPC: RX: C7X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0002
  3877.149780 s: IPC: RX: C7X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0003
  3877.149809 s: IPC: RX: C7X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0004
  3877.149839 s: IPC: RX: C7X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0005
  3877.149869 s: IPC: RX: C7X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0006
  3877.149898 s: IPC: RX: C7X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0007
  3877.149928 s: IPC: RX: C7X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0008
  3877.149958 s: IPC: RX: C7X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0009
  3877.149988 s: IPC: RX: C7X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead000a
  3877.150017 s: IPC: RX: C7X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead000b
  3877.150046 s: IPC: RX: C7X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead000c
  3877.150076 s: IPC: RX: C7X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead000d
  3877.150105 s: IPC: RX: C7X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead000e
  3877.284596 s: IPC: RX: C7X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead000f
  3877.284626 s: IPC: RX: mcu1_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0000
  3877.284656 s: IPC: RX: mcu1_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0001
  3877.284686 s: IPC: RX: mcu1_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0002
  3877.284715 s: IPC: RX: mcu1_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0003
  3877.284747 s: IPC: RX: mcu1_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0004
  3877.284777 s: IPC: RX: mcu1_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0005
  3877.284806 s: IPC: RX: mcu1_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0006
  3877.284836 s: IPC: RX: mcu2_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0000
  3877.284866 s: IPC: RX: mcu1_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0007
  3877.284895 s: IPC: RX: mcu2_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0001
  3877.284924 s: IPC: RX: mcu1_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0008
  3877.284955 s: IPC: RX: mcu2_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0002
  3877.284984 s: IPC: RX: mcu1_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0009
  3877.285014 s: IPC: RX: mcu2_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0003
  3877.285043 s: IPC: RX: mcu1_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead000a
  3877.285073 s: IPC: RX: mcu1_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead000b
  3877.285103 s: IPC: RX: mcu1_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead000c
  3877.285132 s: IPC: RX: mcu1_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead000d
  3877.419622 s: IPC: RX: mcu1_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead000e
  3877.419653 s: IPC: RX: mcu1_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead000f
  3877.419682 s: IPC: RX: mcu2_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0004
  3877.419712 s: IPC: RX: mcu2_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0005
  3877.419744 s: IPC: RX: mcu2_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0006
  3877.419773 s: IPC: RX: mcu2_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0007
  3877.419803 s: IPC: RX: mcu2_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0008
  3877.419832 s: IPC: RX: mcu2_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0009
  3877.419862 s: IPC: RX: mcu2_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0000
  3877.419892 s: IPC: RX: mcu2_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0001
  3877.419921 s: IPC: RX: mcu2_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead000a
  3877.419950 s: IPC: RX: mcu2_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead000b
  3877.419980 s: IPC: RX: mcu2_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0002
  3877.420010 s: IPC: RX: mcu2_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead000c
  3877.420040 s: IPC: RX: mcu2_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead000d
  3877.420069 s: IPC: RX: mcu2_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead000e
  3877.420098 s: IPC: RX: mcu2_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0003
  3877.420128 s: IPC: RX: mcu2_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead000f
  3877.420158 s: IPC: RX: mcu2_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0004
  3877.554649 s: IPC: RX: mcu2_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0005
  3877.554679 s: IPC: RX: mcu2_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0006
  3877.554708 s: IPC: RX: mcu2_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0007
  3877.554741 s: IPC: RX: mcu2_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0008
  3877.554770 s: IPC: RX: mcu2_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0009
  3877.554800 s: IPC: RX: C66X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0000
  3877.554830 s: IPC: RX: mcu2_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead000a
  3877.554859 s: IPC: RX: C66X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0001
  3877.554888 s: IPC: RX: mcu2_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead000b
  3877.554918 s: IPC: RX: mcu2_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead000c
  3877.554948 s: IPC: RX: mcu2_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead000d
  3877.554977 s: IPC: RX: mcu2_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead000e
  3877.555007 s: IPC: RX: mcu2_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead000f
  3877.555036 s: IPC: RX: C66X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0002
  3877.555066 s: IPC: RX: C66X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0003
  3877.555096 s: IPC: RX: C66X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0004
  3877.555125 s: IPC: RX: C66X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0005
  3877.555155 s: IPC: RX: C66X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0006
  3877.555184 s: IPC: RX: C66X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0007
  3877.689677 s: IPC: RX: C66X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0008
  3877.689707 s: IPC: RX: C66X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0009
  3877.689764 s: IPC: RX: C66X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead000a
  3877.689806 s: IPC: RX: C66X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead000b
  3877.689838 s: IPC: RX: C66X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead000c
  3877.689868 s: IPC: RX: C66X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead000d
  3877.689897 s: IPC: RX: C66X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead000e
  3877.689927 s: IPC: RX: C66X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead000f
  3877.689956 s: IPC: RX: C66X_2 (port 13) -> mpu1_0 (port 101) msg = 0xdead0000
  3877.689986 s: IPC: RX: C66X_2 (port 13) -> mpu1_0 (port 101) msg = 0xdead0001
  3877.690016 s: IPC: RX: C66X_2 (port 13) -> mpu1_0 (port 101) msg = 0xdead0002
  3877.690045 s: IPC: RX: C66X_2 (port 13) -> mpu1_0 (port 101) msg = 0xdead0003
  3877.690074 s: IPC: RX: C66X_2 (port 13) -> mpu1_0 (port 101) msg = 0xdead0004
  3877.690104 s: IPC: RX: C66X_2 (port 13) -> mpu1_0 (port 101) msg = 0xdead0005
  3877.690134 s: IPC: RX: C66X_2 (port 13) -> mpu1_0 (port 101) msg = 0xdead0006
  3877.690163 s: IPC: RX: C66X_2 (port 13) -> mpu1_0 (port 101) msg = 0xdead0007
  3877.690193 s: IPC: RX: C66X_2 (port 13) -> mpu1_0 (port 101) msg = 0xdead0008
  3877.690222 s: IPC: RX: C66X_2 (port 13) -> mpu1_0 (port 101) msg = 0xdead0009
  3877.690252 s: IPC: RX: C66X_2 (port 13) -> mpu1_0 (port 101) msg = 0xdead000a
  3877.824791 s: IPC: RX: C66X_2 (port 13) -> mpu1_0 (port 101) msg = 0xdead000b
  3877.824821 s: IPC: RX: C66X_2 (port 13) -> mpu1_0 (port 101) msg = 0xdead000c
  3877.824851 s: IPC: RX: C66X_2 (port 13) -> mpu1_0 (port 101) msg = 0xdead000d
  3877.824881 s: IPC: RX: C66X_2 (port 13) -> mpu1_0 (port 101) msg = 0xdead000e
  3877.824910 s: IPC: RX: C66X_2 (port 13) -> mpu1_0 (port 101) msg = 0xdead000f
  3877.824939 s: IPC: RX: C7X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0000
  3877.824969 s: IPC: RX: C7X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0001
  3877.824999 s: IPC: RX: C7X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0002
  3877.825028 s: IPC: RX: C7X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0003
  3877.825059 s: IPC: RX: C7X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0004
  3877.825088 s: IPC: RX: C7X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0005
  3877.825118 s: IPC: RX: C7X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0006
  3877.825148 s: IPC: RX: C7X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0007
  3877.825177 s: IPC: RX: C7X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0008
  3877.825207 s: IPC: RX: C7X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0009
  3877.825237 s: IPC: RX: C7X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead000a
  3877.825266 s: IPC: RX: C7X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead000b
  3877.825296 s: IPC: RX: C7X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead000c
  3877.825325 s: IPC: RX: C7X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead000d
  3877.959816 s: IPC: RX: C7X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead000e
  3877.959846 s: IPC: RX: C7X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead000f
  3877.959876 s: IPC: RX: mcu1_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0000
  3877.959906 s: IPC: RX: mcu1_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0001
  3877.959936 s: IPC: RX: mcu1_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0002
  3877.959965 s: IPC: RX: mcu1_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0003
  3877.959995 s: IPC: RX: mcu1_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0004
  3877.960024 s: IPC: RX: mcu1_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0005
  3877.960053 s: IPC: RX: mcu2_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0000
  3877.960084 s: IPC: RX: mcu1_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0006
  3877.960113 s: IPC: RX: mcu1_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0007
  3877.960142 s: IPC: RX: mcu1_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0008
  3877.960172 s: IPC: RX: mcu1_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0009
  3877.960202 s: IPC: RX: mcu2_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0001
  3877.960231 s: IPC: RX: mcu1_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead000a
  3877.960261 s: IPC: RX: mcu2_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0002
  3877.960290 s: IPC: RX: mcu2_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0003
  3877.960320 s: IPC: RX: mcu1_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead000b
  3877.960349 s: IPC: RX: mcu1_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead000c
  3878.094842 s: IPC: RX: mcu1_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead000d
  3878.094872 s: IPC: RX: mcu1_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead000e
  3878.094902 s: IPC: RX: mcu1_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead000f
  3878.094932 s: IPC: RX: mcu2_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0004
  3878.094961 s: IPC: RX: mcu2_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0005
  3878.094991 s: IPC: RX: mcu2_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0006
  3878.095021 s: IPC: RX: mcu2_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0007
  3878.095050 s: IPC: RX: mcu2_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0008
  3878.095079 s: IPC: RX: mcu2_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0009
  3878.095109 s: IPC: RX: mcu2_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead000a
  3878.095139 s: IPC: RX: mcu2_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead000b
  3878.095168 s: IPC: RX: mcu2_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead000c
  3878.095198 s: IPC: RX: mcu2_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead000d
  3878.095227 s: IPC: RX: mcu2_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0000
  3878.095257 s: IPC: RX: mcu2_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead000e
  3878.095287 s: IPC: RX: mcu2_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead000f
  3878.095316 s: IPC: RX: mcu2_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0001
  3878.095345 s: IPC: RX: mcu2_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0002
  3878.095376 s: IPC: RX: mcu2_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0003
  3878.229869 s: IPC: RX: C66X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0000
  3878.229899 s: IPC: RX: mcu2_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0004
  3878.229928 s: IPC: RX: mcu2_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0005
  3878.229959 s: IPC: RX: mcu2_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0006
  3878.229988 s: IPC: RX: mcu2_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0007
  3878.230017 s: IPC: RX: mcu2_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0008
  3878.230047 s: IPC: RX: C66X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0001
  3878.230077 s: IPC: RX: mcu2_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0009
  3878.230106 s: IPC: RX: mcu2_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead000a
  3878.230136 s: IPC: RX: mcu2_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead000b
  3878.230165 s: IPC: RX: mcu2_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead000c
  3878.230195 s: IPC: RX: mcu2_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead000d
  3878.230225 s: IPC: RX: mcu2_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead000e
  3878.230254 s: IPC: RX: C66X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0002
  3878.230283 s: IPC: RX: mcu2_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead000f
  3878.230313 s: IPC: RX: C66X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0003
  3878.230342 s: IPC: RX: C66X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0004
  3878.230372 s: IPC: RX: C66X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0005
  3878.230402 s: IPC: RX: C66X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0006
  3878.364896 s: IPC: RX: C66X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0007
  3878.364926 s: IPC: RX: C66X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0008
  3878.364955 s: IPC: RX: C66X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0009
  3878.364985 s: IPC: RX: C66X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead000a
  3878.365014 s: IPC: RX: C66X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead000b
  3878.365044 s: IPC: RX: C66X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead000c
  3878.365074 s: IPC: RX: C66X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead000d
  3878.365103 s: IPC: RX: C66X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead000e
  3878.365132 s: IPC: RX: C66X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead000f
  3878.365162 s: IPC: RX: C66X_2 (port 13) -> mpu1_0 (port 101) msg = 0xdead0000
  3878.365192 s: IPC: RX: C66X_2 (port 13) -> mpu1_0 (port 101) msg = 0xdead0001
  3878.365221 s: IPC: RX: C66X_2 (port 13) -> mpu1_0 (port 101) msg = 0xdead0002
  3878.365251 s: IPC: RX: C66X_2 (port 13) -> mpu1_0 (port 101) msg = 0xdead0003
  3878.365280 s: IPC: RX: C66X_2 (port 13) -> mpu1_0 (port 101) msg = 0xdead0004
  3878.365310 s: IPC: RX: C66X_2 (port 13) -> mpu1_0 (port 101) msg = 0xdead0005
  3878.365340 s: IPC: RX: C66X_2 (port 13) -> mpu1_0 (port 101) msg = 0xdead0006
  3878.365370 s: IPC: RX: C66X_2 (port 13) -> mpu1_0 (port 101) msg = 0xdead0007
  3878.365399 s: IPC: RX: C66X_2 (port 13) -> mpu1_0 (port 101) msg = 0xdead0008
  3878.365429 s: IPC: RX: C66X_2 (port 13) -> mpu1_0 (port 101) msg = 0xdead0009
  3878.499922 s: IPC: RX: C66X_2 (port 13) -> mpu1_0 (port 101) msg = 0xdead000a
  3878.499952 s: IPC: RX: C66X_2 (port 13) -> mpu1_0 (port 101) msg = 0xdead000b
  3878.499982 s: IPC: RX: C66X_2 (port 13) -> mpu1_0 (port 101) msg = 0xdead000c
  3878.500012 s: IPC: RX: C66X_2 (port 13) -> mpu1_0 (port 101) msg = 0xdead000d
  3878.500041 s: IPC: RX: C66X_2 (port 13) -> mpu1_0 (port 101) msg = 0xdead000e
  3878.500070 s: IPC: RX: C66X_2 (port 13) -> mpu1_0 (port 101) msg = 0xdead000f
  3878.500100 s: IPC: RX: C7X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0000
  3878.500130 s: IPC: RX: C7X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0001
  3878.500159 s: IPC: RX: C7X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0002
  3878.500189 s: IPC: RX: C7X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0003
  3878.500219 s: IPC: RX: C7X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0004
  3878.500248 s: IPC: RX: C7X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0005
  3878.500278 s: IPC: RX: C7X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0006
  3878.500308 s: IPC: RX: C7X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0007
  3878.500337 s: IPC: RX: C7X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0008
  3878.500367 s: IPC: RX: C7X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0009
  3878.500397 s: IPC: RX: C7X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead000a
  3878.500427 s: IPC: RX: C7X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead000b
  3878.500456 s: IPC: RX: C7X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead000c
  3878.500486 s: IPC: RX: C7X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead000d
  3878.635036 s: IPC: RX: C7X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead000e
  3878.635066 s: IPC: RX: C7X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead000f
  3878.635095 s: IPC: RX: mcu1_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0000
  3878.635126 s: IPC: RX: mcu1_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0001
  3878.635155 s: IPC: RX: mcu1_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0002
  3878.635184 s: IPC: RX: mcu1_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0003
  3878.635214 s: IPC: RX: mcu1_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0004
  3878.635244 s: IPC: RX: mcu2_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0000
  3878.635273 s: IPC: RX: mcu1_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0005
  3878.635303 s: IPC: RX: mcu2_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0001
  3878.635332 s: IPC: RX: mcu1_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0006
  3878.635362 s: IPC: RX: mcu2_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0002
  3878.635392 s: IPC: RX: mcu1_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0007
  3878.635421 s: IPC: RX: mcu1_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0008
  3878.635450 s: IPC: RX: mcu1_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0009
  3878.635480 s: IPC: RX: mcu1_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead000a
  3878.635509 s: IPC: RX: mcu1_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead000b
  3878.635539 s: IPC: RX: mcu1_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead000c
  3878.635569 s: IPC: RX: mcu1_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead000d
  3878.770063 s: IPC: RX: mcu1_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead000e
  3878.770092 s: IPC: RX: mcu1_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead000f
  3878.770122 s: IPC: RX: mcu2_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0003
  3878.770152 s: IPC: RX: mcu2_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0004
  3878.770181 s: IPC: RX: mcu2_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0005
  3878.770210 s: IPC: RX: mcu2_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0006
  3878.770240 s: IPC: RX: mcu2_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0007
  3878.770270 s: IPC: RX: mcu2_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0008
  3878.770299 s: IPC: RX: mcu2_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead0009
  3878.770329 s: IPC: RX: mcu2_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead000a
  3878.770358 s: IPC: RX: mcu2_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead000b
  3878.770388 s: IPC: RX: mcu2_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0000
  3878.770418 s: IPC: RX: mcu2_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0001
  3878.770447 s: IPC: RX: mcu2_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead000c
  3878.770476 s: IPC: RX: mcu2_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead000d
  3878.770506 s: IPC: RX: mcu2_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead000e
  3878.770536 s: IPC: RX: mcu2_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0002
  3878.770565 s: IPC: RX: mcu2_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0003
  3878.770595 s: IPC: RX: mcu2_0 (port 13) -> mpu1_0 (port 101) msg = 0xdead000f
  3878.905089 s: IPC: RX: mcu2_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0004
  3878.905119 s: IPC: RX: C66X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0000
  3878.905148 s: IPC: RX: mcu2_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0005
  3878.905178 s: IPC: RX: C66X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0001
  3878.905208 s: IPC: RX: mcu2_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0006
  3878.905237 s: IPC: RX: mcu2_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0007
  3878.905267 s: IPC: RX: mcu2_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0008
  3878.905296 s: IPC: RX: mcu2_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0009
  3878.905325 s: IPC: RX: mcu2_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead000a
  3878.905356 s: IPC: RX: mcu2_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead000b
  3878.905385 s: IPC: RX: mcu2_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead000c
  3878.905414 s: IPC: RX: mcu2_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead000d
  3878.905444 s: IPC: RX: mcu2_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead000e
  3878.905473 s: IPC: RX: C66X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0002
  3878.905502 s: IPC: RX: mcu2_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead000f
  3878.905533 s: IPC: RX: C66X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0003
  3878.905562 s: IPC: RX: C66X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0004
  3878.905591 s: IPC: RX: C66X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0005
  3878.905621 s: IPC: RX: C66X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0006
  3879.040116 s: IPC: RX: C66X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0007
  3879.040146 s: IPC: RX: C66X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0008
  3879.040175 s: IPC: RX: C66X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0009
  3879.040205 s: IPC: RX: C66X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead000a
  3879.040235 s: IPC: RX: C66X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead000b
  3879.040264 s: IPC: RX: C66X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead000c
  3879.040294 s: IPC: RX: C66X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead000d
  3879.040323 s: IPC: RX: C66X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead000e
  3879.040353 s: IPC: RX: C66X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead000f
  3879.040383 s: IPC: RX: C66X_2 (port 13) -> mpu1_0 (port 101) msg = 0xdead0000
  3879.040412 s: IPC: RX: C66X_2 (port 13) -> mpu1_0 (port 101) msg = 0xdead0001
  3879.040441 s: IPC: RX: C66X_2 (port 13) -> mpu1_0 (port 101) msg = 0xdead0002
  3879.040472 s: IPC: RX: C66X_2 (port 13) -> mpu1_0 (port 101) msg = 0xdead0003
  3879.040501 s: IPC: RX: C66X_2 (port 13) -> mpu1_0 (port 101) msg = 0xdead0004
  3879.040530 s: IPC: RX: C66X_2 (port 13) -> mpu1_0 (port 101) msg = 0xdead0005
  3879.040560 s: IPC: RX: C66X_2 (port 13) -> mpu1_0 (port 101) msg = 0xdead0006
  3879.040590 s: IPC: RX: C66X_2 (port 13) -> mpu1_0 (port 101) msg = 0xdead0007
  3879.040619 s: IPC: RX: C66X_2 (port 13) -> mpu1_0 (port 101) msg = 0xdead0008
  3879.040649 s: IPC: RX: C66X_2 (port 13) -> mpu1_0 (port 101) msg = 0xdead0009
  3879.175142 s: IPC: RX: C66X_2 (port 13) -> mpu1_0 (port 101) msg = 0xdead000a
  3879.175172 s: IPC: RX: C66X_2 (port 13) -> mpu1_0 (port 101) msg = 0xdead000b
  3879.175202 s: IPC: RX: C66X_2 (port 13) -> mpu1_0 (port 101) msg = 0xdead000c
  3879.175232 s: IPC: RX: C66X_2 (port 13) -> mpu1_0 (port 101) msg = 0xdead000d
  3879.175261 s: IPC: RX: C66X_2 (port 13) -> mpu1_0 (port 101) msg = 0xdead000e
  3879.175290 s: IPC: RX: C66X_2 (port 13) -> mpu1_0 (port 101) msg = 0xdead000f
  3879.175321 s: IPC: RX: C7X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0000
  3879.175350 s: IPC: RX: C7X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0001
  3879.175380 s: IPC: RX: C7X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0002
  3879.175410 s: IPC: RX: C7X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0003
  3879.175439 s: IPC: RX: C7X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0004
  3879.175469 s: IPC: RX: C7X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0005
  3879.175499 s: IPC: RX: C7X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0006
  3879.175529 s: IPC: RX: C7X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0007
  3879.175558 s: IPC: RX: C7X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0008
  3879.175588 s: IPC: RX: C7X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead0009
  3879.175618 s: IPC: RX: C7X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead000a
  3879.175648 s: IPC: RX: C7X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead000b
  3879.175677 s: IPC: RX: C7X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead000c
  3879.310169 s: IPC: RX: C7X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead000d
  3879.310199 s: IPC: RX: C7X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead000e
  3879.310229 s: IPC: RX: C7X_1 (port 13) -> mpu1_0 (port 101) msg = 0xdead000f
APP IPC: Waiting for all messages to get echoed ... Done.
APP IPC: Running remote service test ...
  3886.744787 s: REMOTE_SERVICE_TEST: Running test for CPU mcu1_0 !!!
  3886.745385 s: REMOTE_SERVICE_TEST: Test passed !!!
  3886.745591 s: REMOTE_SERVICE_TEST: Running test @ 0xb8000000 of 1024 bytes size for CPU mcu1_0 !!!
  3886.745712 s: REMOTE_SERVICE_TEST: Test failed @ iteration 0 !!!
  3886.745732 s: REMOTE_SERVICE_TEST: Running timer test of 10000 msecs for CPU mcu1_0 !!!
  3896.745544 s: REMOTE_SERVICE_TEST: Running timer test of 10000 msecs for CPU mcu1_0 ... DONE !!!
  3896.745618 s: REMOTE_SERVICE_TEST: Running test for CPU mcu2_0 !!!
  3896.746227 s: REMOTE_SERVICE_TEST: Test passed !!!
  3896.746294 s: REMOTE_SERVICE_TEST: Running test @ 0xb8000000 of 1024 bytes size for CPU mcu2_0 !!!
  3896.746398 s: REMOTE_SERVICE_TEST: Test failed @ iteration 0 !!!
  3896.746417 s: REMOTE_SERVICE_TEST: Running timer test of 10000 msecs for CPU mcu2_0 !!!
  3906.745879 s: REMOTE_SERVICE_TEST: Running timer test of 10000 msecs for CPU mcu2_0 ... DONE !!!
  3906.745954 s: REMOTE_SERVICE_TEST: Running test for CPU mcu2_1 !!!
  3906.746566 s: REMOTE_SERVICE_TEST: Test passed !!!
  3906.746632 s: REMOTE_SERVICE_TEST: Running test @ 0xb8000000 of 1024 bytes size for CPU mcu2_1 !!!
  3906.746745 s: REMOTE_SERVICE_TEST: Test failed @ iteration 0 !!!
  3906.746763 s: REMOTE_SERVICE_TEST: Running timer test of 10000 msecs for CPU mcu2_1 !!!
  3916.746841 s: REMOTE_SERVICE_TEST: Running timer test of 10000 msecs for CPU mcu2_1 ... DONE !!!
  3916.746915 s: REMOTE_SERVICE_TEST: Running test for CPU C66X_1 !!!
  3916.747354 s: REMOTE_SERVICE_TEST: Test passed !!!
  3916.747416 s: REMOTE_SERVICE_TEST: Running test @ 0xb8000000 of 1024 bytes size for CPU C66X_1 !!!
  3916.747508 s: REMOTE_SERVICE_TEST: Test failed @ iteration 0 !!!
  3916.747527 s: REMOTE_SERVICE_TEST: Running timer test of 10000 msecs for CPU C66X_1 !!!
  3926.747239 s: REMOTE_SERVICE_TEST: Running timer test of 10000 msecs for CPU C66X_1 ... DONE !!!
  3926.747313 s: REMOTE_SERVICE_TEST: Running test for CPU C66X_2 !!!
  3926.747747 s: REMOTE_SERVICE_TEST: Test passed !!!
  3926.747808 s: REMOTE_SERVICE_TEST: Running test @ 0xb8000000 of 1024 bytes size for CPU C66X_2 !!!
  3926.747901 s: REMOTE_SERVICE_TEST: Test failed @ iteration 0 !!!
  3926.747920 s: REMOTE_SERVICE_TEST: Running timer test of 10000 msecs for CPU C66X_2 !!!
  3936.747240 s: REMOTE_SERVICE_TEST: Running timer test of 10000 msecs for CPU C66X_2 ... DONE !!!
  3936.747313 s: REMOTE_SERVICE_TEST: Running test for CPU C7X_1 !!!
  3936.747704 s: REMOTE_SERVICE_TEST: Test passed !!!
  3936.747766 s: REMOTE_SERVICE_TEST: Running test @ 0xb8000000 of 1024 bytes size for CPU C7X_1 !!!
  3936.747852 s: REMOTE_SERVICE_TEST: Test failed @ iteration 0 !!!
  3936.747871 s: REMOTE_SERVICE_TEST: Running timer test of 10000 msecs for CPU C7X_1 !!!
  3946.747805 s: REMOTE_SERVICE_TEST: Running timer test of 10000 msecs for CPU C7X_1 ... DONE !!!
APP IPC: Running remote service test ... Done.
  3946.747890 s:  VX_ZONE_INIT:[tivxHostDeInit:56] De-Initialization Done for HOST !!!
  3946.755739 s:  VX_ZONE_INIT:[tivxDeInit:111] De-Initialization Done !!!
APP: Deinit ... !!!
  3946.755766 s: REMOTE_SERVICE: Deinit ... !!!
  3946.755816 s: REMOTE_SERVICE: Deinit ... Done !!!
IPC: Deinit ... !!!
IPC: Deinit ... Done !!!
APP: Deinit ... Done !!!
APP IPC: Done !!!
J7EVM@QNX:/ti_fs/vision_apps#

发现"remote_service_test:test failed @ iteration 0!!!"。

如果未定义 ENABLE_IPC_MCU1_0、 则远程服务测试工作正常。  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

     PSDK_QNX_07_03_03_patch 允许 IPC 示例应用(IPC_TEST)运行、包括 MCU1_0。  

    对于您的目标生产用例、您是否希望使用 Vision Apps 框架生成图像、并且 Vision Apps 远程服务将在 MCU1_0上运行?

    谢谢、

    KB