Thread 中讨论的其他器件:SYSBIOS
工具/软件:TI-RTOS
您好!
我尝试了几次安装 CCS、tirtos 和 wolfsl 的尝试、但都失败了。 第一次尝试时、我安装了 CCS 的最新版本(7.0)、tivacware、tirtos 2.16.01.14和 wolfsl 3.10。 按照以下网址上的 wolfsl 构建说明进行操作: http://processors.wiki.ti.com/index.php/Using_wolfSSL_with_TI-RTOS#Targets
按照 wiki 中的指示设置 wolfsl\tirtos\products.mak。 在 Windows cmd shell 中使用 gmake (我正在使用 Win7笔记本电脑)启动编译。 在控制台输出大量之后、出现错误(我没有记下)。 我 搜索了 TI 论坛、发现~2个月前有人讨论过同样的错误。 响应者说、wolfsl 尚未通过 CCS 测试、而是要切换到 wolfsl 3.9.6。
我下载了该文件、并在 wiki 上重复了这些步骤。 出现以下错误:
Gmake: *** No rule to make target ‘uf’ stop.
(note that the u has an ^ character above it in the console output).
在论坛上逛了几个小时后、决定尝试从 CCS 7切换到6.2。
Installed into C:\ti\ccs620. Moved wolfssi from ccs7 over to c:\ti\ccsv6\ folder.
After getting this to run, dug into the TM4C129ED_UG, p. 23 states tirtos v2.14.00.10 or later will work with the demo board IoT app, with any wolfssl ver from 3.6.6 onwards. However, in the CCS Resource Explorer, only shows TI-RTOS for Tivac ver v2.16.00.08. So which should I use? Lets try downloading the one that CCS 6.2 is pointing to, into c:\ti\ccs620. Downloaded from here:
http://software-dl.ti.com/dsps/dsps_public_sw/sdo_sb/targetcontent/tirtos/index.html
However, there is a note on the above page to download/install via CCS AppCenter. Opened App Cntr and searched tirtos – was directed to go into Resource Explorer. There is a tirtos for tivaC there – used the download arrow icon on the right of the page – started download/installed. Said it was saving to desktop – got installed into C:\ti\tirex-content. Why/how I have no clue.
After install, a window popped up regarding dependencies - directing to select xdctools-3.32.00.06.
Note that there is already a xdctools-3.32.01.22_core in the ccs620 folder. Select OK – started another download.
Installed to C:\ti\tirex-content. Another window opened asking to install new products, tirtos and xdctools.
After it did its install, asked to restart CCS.
Try leaving wolfssl where I have it now, in c:\ti\ccs620
After edit of products.mak in C:\ti\ccs620\wolfssl\tirtos, from this folder, run build:
..\..\..\tirex-content\xdctools_3_32_00_06_core\gmake.exe –f wolfssl.mak all
Resulted in same error as before: Gmake: *** No rule to make target ‘uf’ stop.
不知道该怎么做、我已经用尽 了我在论坛上可以想到的所有搜索。 希望有人能帮忙吗?
谢谢你。