This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好!
我的客户现在使用 AM5728。
他们想知道具有3D 加速器的 AM5728的帧速率。
MPU:600MHz
GPU:124MHz
DDR:400 MHz
显示大小:VGA
在这种情况下、帧速率如何?
除了" Processor_SDK_Linux_Kernel_Performance_Guide"(http://processors.wiki.ti.com/index.php/Processor_SDK_Linux_Kernel_Performance_Guide#Performance_.28Fps.29 )之外,我找不到任何3D 加速器的性能数据。
感谢您的快速回复。
此致、
Michi