This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] Linux/AM5728:Ubuntu 16.04中 input-utils-1.0-r0的 d_compile 故障

Guru**** 2611805 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/602876/linux-am5728-do_compile-failure-of-input-utils-1-0-r0-in-ubuntu-16-04

器件型号:AM5728

工具/软件:Linux

在 Ubuntu 16.04环境中编译 SDK 时出现故障。

注意:make -j 32 destdir=/data/bsp/PHYTEC_BSPs/yocto_ti/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/input-utils/1.0-r0/image strip=
| make.config:1:***空变量名。 停下。
|错误:OE_runmake 失败

祝福,