This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] AM4378:PVR_K:HWRecoveryResetSGX:触发 SGX 硬件恢复

Guru**** 1475205 points
Other Parts Discussed in Thread: AM4378
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1174931/am4378-pvr_k-hwrecoveryresetsgx-sgx-hardware-recovery-triggered

器件型号:AM4378

CPU:AM4378

SDK:07.03.00.005

内核:5.4.106

SGX:ti-SGX-DDK-KM-1.17.4948957

内核日志:

[    0.000000] Booting Linux on physical CPU 0x0
[    0.000000] Linux version 5.4.106+ (root@monitor1804) (gcc version 9.2.1 20191025 (GNU Toolchain for the A-profile Architecture 9.2-2019.12 (arm-9.10))) #1 PREEMPT Mon Nov 7 04:20:23 UTC 2022
[    0.000000] CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d
[    0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[    0.000000] OF: fdt: Machine model: EDAN MPM AM43xx
[    0.000000] Memory policy: Data cache writeback
[    0.000000] efi: Getting EFI parameters from FDT:
[    0.000000] efi: UEFI not found.
[    0.000000] cma: Reserved 48 MiB at 0x9d000000
[    0.000000] On node 0 totalpages: 131072
[    0.000000]   Normal zone: 1152 pages used for memmap
[    0.000000]   Normal zone: 0 pages reserved
[    0.000000]   Normal zone: 131072 pages, LIFO batch:31
[    0.000000] CPU: All CPU(s) started in SVC mode.
[    0.000000] AM437x ES1.2 (sgx neon)
[    0.000000] pcpu-alloc: s0 r0 d32768 u32768 alloc=1*32768
[    0.000000] pcpu-alloc: [0] 0
[    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 129920
[    0.000000] Kernel command line: console=null board_name=RespArray root=PARTUUID=b0e7b6cb-03 rw rootfstype=ext4 rootwait
[    0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes, linear)
[    0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes, linear)
[    0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
[    0.000000] Memory: 456900K/524288K available (8192K kernel code, 266K rwdata, 2728K rodata, 1024K init, 250K bss, 18236K reserved, 49152K cma-reserved, 0K highmem)
[    0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
[    0.000000] rcu: Preemptible hierarchical RCU implementation.
[    0.000000]  Tasks RCU enabled.
[    0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 10 jiffies.
[    0.000000] NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16
[    0.000000] L2C: platform modifies aux control register: 0x0e030000 -> 0x3e430000
[    0.000000] L2C: DT/platform modifies aux control register: 0x0e030000 -> 0x3e430000
[    0.000000] L2C-310 enabling early BRESP for Cortex-A9
[    0.000000] OMAP L2C310: ROM does not support power control setting
[    0.000000] L2C-310 dynamic clock gating disabled, standby mode disabled
[    0.000000] L2C-310 cache controller enabled, 16 ways, 256 kB
[    0.000000] L2C-310: CACHE_ID 0x410000c9, AUX_CTRL 0x4e430000
[    0.000000] random: get_random_bytes called from start_kernel+0x2b8/0x478 with crng_init=0
[    0.000000] OMAP clockevent source: timer2 at 24000000 Hz
[    0.000016] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 89478484971ns
[    0.000035] clocksource: timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 79635851949 ns
[    0.000046] OMAP clocksource: timer1 at 24000000 Hz
[    0.000515] clocksource: 32k_counter: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 58327039986419 ns
[    0.000524] OMAP clocksource: 32k_counter at 32768 Hz
[    0.001127] Console: colour dummy device 80x30
[    0.001210] Calibrating delay loop... 1993.93 BogoMIPS (lpj=9969664)
[    0.060185] pid_max: default: 32768 minimum: 301
[    0.060349] LSM: Security Framework initializing
[    0.060393] TOMOYO Linux initialized
[    0.060486] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes, linear)
[    0.060508] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes, linear)
[    0.061656] CPU: Testing write buffer coherency: ok
[    0.061745] CPU0: Spectre v2: using BPIALL workaround
[    0.063041] Setting up static identity map for 0x80100000 - 0x80100060
[    0.063225] rcu: Hierarchical SRCU implementation.
[    0.063337] EFI services will not be available.
[    0.063875] devtmpfs: initialized
[    0.077068] VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
[    0.077617] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[    0.077647] futex hash table entries: 256 (order: -1, 3072 bytes, linear)
[    0.081809] pinctrl core: initialized pinctrl subsystem
[    0.082776] DMI not present or invalid.
[    0.083399] NET: Registered protocol family 16
[    0.085899] DMA: preallocated 256 KiB pool for atomic coherent allocations
[    0.108513] cpuidle: using governor ladder
[    0.108552] cpuidle: using governor menu
[    0.110678] omap_l3_noc 44000000.ocp: L3 debug error: target 8 mod:0 (unclearable)
[    0.110768] omap_l3_noc 44000000.ocp: L3 application error: target 8 mod:0 (unclearable)
[    0.128557] No ATAGs?
[    0.128589] hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
[    0.128609] hw-breakpoint: maximum watchpoint size is 4 bytes.
[    0.146450] debugfs: Directory '49000000.edma' with parent 'dmaengine' already present!
[    0.146492] edma 49000000.edma: TI EDMA DMA engine driver
[    0.147288] reg-fixed-voltage fixedregulator-v3_3d: GPIO lookup for consumer (null)
[    0.147297] reg-fixed-voltage fixedregulator-v3_3d: using device tree for GPIO lookup
[    0.147318] of_get_named_gpiod_flags: can't parse 'gpios' property of node '/fixedregulator-v3_3d[0]'
[    0.147331] of_get_named_gpiod_flags: can't parse 'gpio' property of node '/fixedregulator-v3_3d[0]'
[    0.147342] reg-fixed-voltage fixedregulator-v3_3d: using lookup tables for GPIO lookup
[    0.147351] reg-fixed-voltage fixedregulator-v3_3d: No GPIO consumer (null) found
[    0.147974] iommu: Default domain type: Translated
[    0.150680] SCSI subsystem initialized
[    0.150977] usbcore: registered new interface driver usbfs
[    0.151026] usbcore: registered new interface driver hub
[    0.151088] usbcore: registered new device driver usb
[    0.151662] pps_core: LinuxPPS API ver. 1 registered
[    0.151671] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[    0.151698] PTP clock support registered
[    0.151742] EDAC MC: Ver: 3.0.0
[    0.153222] Advanced Linux Sound Architecture Driver Initialized.
[    0.154718] clocksource: Switched to clocksource timer1
[    0.163295] thermal_sys: Registered thermal governor 'fair_share'
[    0.163304] thermal_sys: Registered thermal governor 'bang_bang'
[    0.163322] thermal_sys: Registered thermal governor 'step_wise'
[    0.163327] thermal_sys: Registered thermal governor 'user_space'
[    0.163332] thermal_sys: Registered thermal governor 'power_allocator'
[    0.164093] NET: Registered protocol family 2
[    0.165122] tcp_listen_portaddr_hash hash table entries: 512 (order: 0, 4096 bytes, linear)
[    0.165161] TCP established hash table entries: 4096 (order: 2, 16384 bytes, linear)
[    0.165225] TCP bind hash table entries: 4096 (order: 2, 16384 bytes, linear)
[    0.165289] TCP: Hash tables configured (established 4096 bind 4096)
[    0.165498] UDP hash table entries: 256 (order: 0, 4096 bytes, linear)
[    0.165522] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes, linear)
[    0.165709] NET: Registered protocol family 1
[    0.166492] RPC: Registered named UNIX socket transport module.
[    0.166505] RPC: Registered udp transport module.
[    0.166510] RPC: Registered tcp transport module.
[    0.166515] RPC: Registered tcp NFSv4.1 backchannel transport module.
[    0.166534] PCI: CLS 0 bytes, default 64
[    0.168587] Initialise system trusted keyrings
[    0.169050] workingset: timestamp_bits=14 max_order=17 bucket_order=3
[    0.174162] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[    0.175408] NFS: Registering the id_resolver key type
[    0.175460] Key type id_resolver registered
[    0.175466] Key type id_legacy registered
[    0.175524] ntfs: driver 2.1.32 [Flags: R/O].
[    0.176387] Key type asymmetric registered
[    0.176401] Asymmetric key parser 'x509' registered
[    0.176465] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 245)
[    0.176476] io scheduler mq-deadline registered
[    0.176483] io scheduler kyber registered
[    0.181316] gpio gpiochip0: (gpio-0-31): added GPIO chardev (254:0)
[    0.181416] gpiochip_setup_dev: registered GPIOs 0 to 31 on device: gpiochip0 (gpio-0-31)
[    0.181478] OMAP GPIO hardware version 0.1
[    0.191434] ti-sysc 4804c000.target-module: dts flag should be at module level for ti,no-reset-on-init
[    0.192243] gpio gpiochip1: Persistence not supported for GPIO 0
[    0.192257] GPIO line 32 (rstb0) hogged as output/low
[    0.192276] gpio gpiochip1: Persistence not supported for GPIO 1
[    0.192280] GPIO line 33 (pwd0) hogged as output/low
[    0.192602] gpio gpiochip1: (gpio-32-63): added GPIO chardev (254:1)
[    0.192705] gpiochip_setup_dev: registered GPIOs 32 to 63 on device: gpiochip1 (gpio-32-63)
[    0.195239] omap-mailbox 480c8000.mailbox: omap mailbox rev 0x400
[    0.200826] gpio gpiochip2: (gpio-64-95): added GPIO chardev (254:2)
[    0.200961] gpiochip_setup_dev: registered GPIOs 64 to 95 on device: gpiochip2 (gpio-64-95)
[    0.202493] gpio gpiochip3: (gpio-96-127): added GPIO chardev (254:3)
[    0.202579] gpiochip_setup_dev: registered GPIOs 96 to 127 on device: gpiochip3 (gpio-96-127)
[    0.206556] ti-sysc 48320000.target-module: dts flag should be at module level for ti,no-reset-on-init
[    0.207396] gpio gpiochip4: Persistence not supported for GPIO 0
[    0.207412] GPIO line 128 (ctrl1v35) hogged as output/low
[    0.207703] gpio gpiochip4: (gpio-128-159): added GPIO chardev (254:4)
[    0.207807] gpiochip_setup_dev: registered GPIOs 128 to 159 on device: gpiochip4 (gpio-128-159)
[    0.208094] ti-sysc 48322000.target-module: dts flag should be at module level for ti,no-reset-on-init
[    0.208939] gpio gpiochip5: Persistence not supported for GPIO 1
[    0.208951] GPIO line 161 (lcden) hogged as output/high
[    0.209216] gpio gpiochip5: (gpio-160-191): added GPIO chardev (254:5)
[    0.209294] gpiochip_setup_dev: registered GPIOs 160 to 191 on device: gpiochip5 (gpio-160-191)
[    0.219542] pinctrl-single 44e10800.pinmux: 199 pins, size 796
[    0.223957] pwm-backlight backlight: GPIO lookup for consumer enable
[    0.223969] pwm-backlight backlight: using device tree for GPIO lookup
[    0.223994] of_get_named_gpiod_flags: can't parse 'enable-gpios' property of node '/backlight[0]'
[    0.224006] of_get_named_gpiod_flags: can't parse 'enable-gpio' property of node '/backlight[0]'
[    0.224018] pwm-backlight backlight: using lookup tables for GPIO lookup
[    0.224026] pwm-backlight backlight: No GPIO consumer enable found
[    0.224049] pwm-backlight backlight: backlight supply power not found, using dummy regulator
[    0.228947] Serial: 8250/16550 driver, 10 ports, IRQ sharing enabled
[    0.232834] omap8250 44e09000.serial: No clock speed specified: using default: 48000000
[    0.233433] 44e09000.serial: ttyS0 at MMIO 0x44e09000 (irq = 66, base_baud = 3000000) is a 8250
[    0.234211] omap8250 48022000.serial: No clock speed specified: using default: 48000000
[    0.234692] 48022000.serial: ttyS1 at MMIO 0x48022000 (irq = 70, base_baud = 3000000) is a 8250
[    0.235535] omap8250 481a6000.serial: No clock speed specified: using default: 48000000
[    0.236022] 481a6000.serial: ttyS3 at MMIO 0x481a6000 (irq = 80, base_baud = 3000000) is a 8250
[    0.236673] omap8250 481a8000.serial: No clock speed specified: using default: 48000000
[    0.237119] 481a8000.serial: ttyS4 at MMIO 0x481a8000 (irq = 81, base_baud = 3000000) is a 8250
[    0.239771] omap_rng 48310000.rng: Random Number Generator ver. 20
[    0.241163] omapdss_dss 4832a000.dss: 4832a000.dss supply vdda_video not found, using dummy regulator
[    0.245014] random: fast init done
[    0.245364] random: crng init done
[    0.247947] panel-simple display: display supply power not found, using dummy regulator
[    0.248070] panel-simple display: GPIO lookup for consumer enable
[    0.248076] panel-simple display: using device tree for GPIO lookup
[    0.248124] of_get_named_gpiod_flags: parsed 'enable-gpios' property of node '/display[0]' - status (0)
[    0.248218] gpio gpiochip0: Persistence not supported for GPIO 6
[    0.255354] brd: module loaded
[    0.268964] loop: module loaded
[    0.272805] mdio_bus fixed-0: GPIO lookup for consumer reset
[    0.272819] mdio_bus fixed-0: using lookup tables for GPIO lookup
[    0.272826] mdio_bus fixed-0: No GPIO consumer reset found
[    0.272847] libphy: Fixed MDIO Bus: probed
[    0.275535] mdio_bus 4a101000.mdio: GPIO lookup for consumer reset
[    0.275548] mdio_bus 4a101000.mdio: using device tree for GPIO lookup
[    0.275571] of_get_named_gpiod_flags: can't parse 'reset-gpios' property of node '/ocp@44000000/interconnect@4a000000/segment@0/target-module@100000/ethernet@0/mdio@1000[0]'
[    0.275585] of_get_named_gpiod_flags: can't parse 'reset-gpio' property of node '/ocp@44000000/interconnect@4a000000/segment@0/target-module@100000/ethernet@0/mdio@1000[0]'
[    0.275597] mdio_bus 4a101000.mdio: using lookup tables for GPIO lookup
[    0.275604] mdio_bus 4a101000.mdio: No GPIO consumer reset found
[    0.334731] davinci_mdio 4a101000.mdio: davinci mdio revision 1.6, bus freq 1000000
[    0.334749] libphy: 4a101000.mdio: probed
[    0.335743] mdio_bus 4a101000.mdio:00: GPIO lookup for consumer reset
[    0.335751] mdio_bus 4a101000.mdio:00: using device tree for GPIO lookup
[    0.335775] of_get_named_gpiod_flags: can't parse 'reset-gpios' property of node '/ocp@44000000/interconnect@4a000000/segment@0/target-module@100000/ethernet@0/mdio@1000/ethernet-phy@0[0]'
[    0.335788] of_get_named_gpiod_flags: can't parse 'reset-gpio' property of node '/ocp@44000000/interconnect@4a000000/segment@0/target-module@100000/ethernet@0/mdio@1000/ethernet-phy@0[0]'
[    0.335796] mdio_bus 4a101000.mdio:00: using lookup tables for GPIO lookup
[    0.335803] mdio_bus 4a101000.mdio:00: No GPIO consumer reset found
[    0.336301] davinci_mdio 4a101000.mdio: phy[0]: device 4a101000.mdio:00, driver SMSC LAN8710/LAN8720
[    0.336484] cpsw 4a100000.ethernet: initialized cpsw ale version 1.4
[    0.336494] cpsw 4a100000.ethernet: ALE Table size 1024
[    0.336618] cpsw 4a100000.ethernet: cpts: overflow check period 500 (jiffies)
[    0.336711] cpsw 4a100000.ethernet: Detected MACID = f8:33:31:7d:9a:a3
[    0.338165] usbcore: registered new interface driver usb-storage
[    0.338230] i2c /dev entries driver
[    0.340559] cpuidle: enable-method property 'ti,am4372' found operations
[    0.341243] sdhci: Secure Digital Host Controller Interface driver
[    0.341250] sdhci: Copyright(c) Pierre Ossman
[    0.342526] omap_hsmmc 48060000.mmc: GPIO lookup for consumer cd
[    0.342535] omap_hsmmc 48060000.mmc: using device tree for GPIO lookup
[    0.342561] of_get_named_gpiod_flags: can't parse 'cd-gpios' property of node '/ocp@44000000/interconnect@48000000/segment@0/target-module@60000/mmc@0[0]'
[    0.342576] of_get_named_gpiod_flags: can't parse 'cd-gpio' property of node '/ocp@44000000/interconnect@48000000/segment@0/target-module@60000/mmc@0[0]'
[    0.342586] omap_hsmmc 48060000.mmc: using lookup tables for GPIO lookup
[    0.342593] omap_hsmmc 48060000.mmc: No GPIO consumer cd found
[    0.342601] omap_hsmmc 48060000.mmc: GPIO lookup for consumer wp
[    0.342605] omap_hsmmc 48060000.mmc: using device tree for GPIO lookup
[    0.342617] of_get_named_gpiod_flags: can't parse 'wp-gpios' property of node '/ocp@44000000/interconnect@48000000/segment@0/target-module@60000/mmc@0[0]'
[    0.342628] of_get_named_gpiod_flags: can't parse 'wp-gpio' property of node '/ocp@44000000/interconnect@48000000/segment@0/target-module@60000/mmc@0[0]'
[    0.342634] omap_hsmmc 48060000.mmc: using lookup tables for GPIO lookup
[    0.342639] omap_hsmmc 48060000.mmc: No GPIO consumer wp found
[    0.355448] omap_hsmmc 47810000.mmc: GPIO lookup for consumer cd
[    0.355459] omap_hsmmc 47810000.mmc: using device tree for GPIO lookup
[    0.355500] of_get_named_gpiod_flags: parsed 'cd-gpios' property of node '/ocp@44000000/target-module@47810000/mmc@0[0]' - status (0)
[    0.355525] gpio gpiochip1: Persistence not supported for GPIO 3
[    0.355540] omap_gpio 4804c000.gpio: Could not set line 3 debounce to 200000 microseconds (-22)
[    0.355551] omap_hsmmc 47810000.mmc: Got CD GPIO
[    0.355560] omap_hsmmc 47810000.mmc: GPIO lookup for consumer wp
[    0.355564] omap_hsmmc 47810000.mmc: using device tree for GPIO lookup
[    0.355578] of_get_named_gpiod_flags: can't parse 'wp-gpios' property of node '/ocp@44000000/target-module@47810000/mmc@0[0]'
[    0.355590] of_get_named_gpiod_flags: can't parse 'wp-gpio' property of node '/ocp@44000000/target-module@47810000/mmc@0[0]'
[    0.355599] omap_hsmmc 47810000.mmc: using lookup tables for GPIO lookup
[    0.355604] omap_hsmmc 47810000.mmc: No GPIO consumer wp found
[    0.382376] sdhci-pltfm: SDHCI platform and OF driver helper
[    0.383627] of_get_named_gpiod_flags: parsed 'gpios' property of node '/leds/led0[0]' - status (0)
[    0.383656] gpio gpiochip4: Persistence not supported for GPIO 17
[    0.383660] no flags found for gpios
[    0.383856] of_get_named_gpiod_flags: parsed 'gpios' property of node '/leds/led1[0]' - status (0)
[    0.383870] gpio gpiochip1: Persistence not supported for GPIO 24
[    0.383873] no flags found for gpios
[    0.383975] of_get_named_gpiod_flags: parsed 'gpios' property of node '/leds/led2[0]' - status (0)
[    0.383985] gpio gpiochip1: Persistence not supported for GPIO 4
[    0.383988] no flags found for gpios
[    0.384069] of_get_named_gpiod_flags: parsed 'gpios' property of node '/leds/led3[0]' - status (0)
[    0.384079] gpio gpiochip4: Persistence not supported for GPIO 10
[    0.384081] no flags found for gpios
[    0.385752] spi_ims spi1.0: GPIO lookup for consumer hwver0
[    0.385762] spi_ims spi1.0: using device tree for GPIO lookup
[    0.385801] of_get_named_gpiod_flags: parsed 'hwver0-gpios' property of node '/ocp@44000000/interconnect@48000000/segment@100000/target-module@a2000/spi@0/mainboard@0[0]' - status (0)
[    0.385887] gpio gpiochip3: Persistence not supported for GPIO 16
[    0.385899] spi_ims spi1.0: GPIO lookup for consumer hwver1
[    0.385904] spi_ims spi1.0: using device tree for GPIO lookup
[    0.385926] of_get_named_gpiod_flags: parsed 'hwver1-gpios' property of node '/ocp@44000000/interconnect@48000000/segment@100000/target-module@a2000/spi@0/mainboard@0[0]' - status (0)
[    0.385936] gpio gpiochip3: Persistence not supported for GPIO 15
[    0.385942] spi_ims spi1.0: GPIO lookup for consumer hwver2
[    0.385946] spi_ims spi1.0: using device tree for GPIO lookup
[    0.385964] of_get_named_gpiod_flags: parsed 'hwver2-gpios' property of node '/ocp@44000000/interconnect@48000000/segment@100000/target-module@a2000/spi@0/mainboard@0[0]' - status (0)
[    0.385971] gpio gpiochip3: Persistence not supported for GPIO 14
[    0.385977] spi_ims spi1.0: GPIO lookup for consumer send
[    0.385981] spi_ims spi1.0: using device tree for GPIO lookup
[    0.386003] of_get_named_gpiod_flags: parsed 'send-gpios' property of node '/ocp@44000000/interconnect@48000000/segment@100000/target-module@a2000/spi@0/mainboard@0[0]' - status (0)
[    0.386012] gpio gpiochip5: Persistence not supported for GPIO 7
[    0.386019] spi_ims spi1.0: GPIO lookup for consumer status
[    0.386023] spi_ims spi1.0: using device tree for GPIO lookup
[    0.386043] of_get_named_gpiod_flags: parsed 'status-gpios' property of node '/ocp@44000000/interconnect@48000000/segment@100000/target-module@a2000/spi@0/mainboard@0[0]' - status (0)
[    0.386050] gpio gpiochip4: Persistence not supported for GPIO 7
[    0.386059] spi_ims spi1.0: GPIO lookup for consumer watchdog
[    0.386063] spi_ims spi1.0: using device tree for GPIO lookup
[    0.386080] of_get_named_gpiod_flags: parsed 'watchdog-gpios' property of node '/ocp@44000000/interconnect@48000000/segment@100000/target-module@a2000/spi@0/mainboard@0[0]' - status (0)
[    0.386087] gpio gpiochip4: Persistence not supported for GPIO 8
[    0.386180] spi_ims spi1.0: start talking to iMx.RT1052
[    0.386459] v8kbd_init(line 626):
[    0.386462] succeed
[    0.389937] davinci-mcasp 4803c000.mcasp: IRQ common not found
[    0.391734] NET: Registered protocol family 10
[    0.393155] Segment Routing with IPv6
[    0.393268] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
[    0.394017] NET: Registered protocol family 17
[    0.394440] Key type dns_resolver registered
[    0.394615] omap_voltage_late_init: Voltage driver support not added
[    0.395523] Loading compiled-in X.509 certificates
[    0.405811] index=1,h=11,l=6f
[    0.425381] index=1176,h=11,l=69
[    0.445429] index=116f,h=11,l=76
[    0.449375] omap_i2c 44e0b000.i2c: bus 0 rev0.12 at 100 kHz
[    0.476539] rtc-pcf8563 1-0051: char device (252:0)
[    0.476567] rtc-pcf8563 1-0051: registered as rtc0
[    0.477880] tlv320aic31xx-codec 1-0018: GPIO lookup for consumer reset
[    0.477890] tlv320aic31xx-codec 1-0018: using device tree for GPIO lookup
[    0.477959] of_get_named_gpiod_flags: parsed 'reset-gpios' property of node '/ocp@44000000/interconnect@48000000/segment@0/target-module@2a000/i2c@0/tlv320dac3100@18[0]' - status (0)
[    0.477984] gpio gpiochip4: Persistence not supported for GPIO 3
[    0.478126] tlv320aic31xx-codec 1-0018: 1-0018 supply SPRVDD not found, using dummy regulator
[    0.478185] tlv320aic31xx-codec 1-0018: 1-0018 supply SPLVDD not found, using dummy regulator
[    0.480247] omap_i2c 4802a000.i2c: bus 1 rev0.12 at 400 kHz
[    0.482065] sii9022x 2-003b: GPIO lookup for consumer reset
[    0.482076] sii9022x 2-003b: using device tree for GPIO lookup
[    0.482119] of_get_named_gpiod_flags: parsed 'reset-gpios' property of node '/ocp@44000000/interconnect@48000000/segment@100000/target-module@9c000/i2c@0/sii9022@3b[0]' - status (0)
[    0.482141] gpio gpiochip1: Persistence not supported for GPIO 2
[    0.505721] sii9022x 2-003b: Sii902x: init
[    0.505960] omap_i2c 4819c000.i2c: bus 2 rev0.12 at 400 kHz
[    0.509387] omapdss_dss 4832a000.dss: 4832a000.dss supply vdda_video not found, using dummy regulator
[    0.509610] DSS: OMAP DSS rev 2.0
[    0.510761] omapdss_dss 4832a000.dss: bound 4832a400.dispc (ops dispc_component_ops)
[    0.511335] omapdrm omapdrm.0: DMM not available, disable DMM support
[    0.511716] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[    0.511725] [drm] No driver support for vblank timestamp query.
[    0.529879] omapdrm omapdrm.0: fb0: omapdrmdrmfb frame buffer device
[    0.530738] [drm] Initialized omapdrm 1.0.0 20110917 for omapdrm.0 on minor 0
[    0.532959] omap_hsmmc 48060000.mmc: GPIO lookup for consumer cd
[    0.532971] omap_hsmmc 48060000.mmc: using device tree for GPIO lookup
[    0.532998] of_get_named_gpiod_flags: can't parse 'cd-gpios' property of node '/ocp@44000000/interconnect@48000000/segment@0/target-module@60000/mmc@0[0]'
[    0.533012] of_get_named_gpiod_flags: can't parse 'cd-gpio' property of node '/ocp@44000000/interconnect@48000000/segment@0/target-module@60000/mmc@0[0]'
[    0.533022] omap_hsmmc 48060000.mmc: using lookup tables for GPIO lookup
[    0.533029] omap_hsmmc 48060000.mmc: No GPIO consumer cd found
[    0.533038] omap_hsmmc 48060000.mmc: GPIO lookup for consumer wp
[    0.533042] omap_hsmmc 48060000.mmc: using device tree for GPIO lookup
[    0.533053] of_get_named_gpiod_flags: can't parse 'wp-gpios' property of node '/ocp@44000000/interconnect@48000000/segment@0/target-module@60000/mmc@0[0]'
[    0.533064] of_get_named_gpiod_flags: can't parse 'wp-gpio' property of node '/ocp@44000000/interconnect@48000000/segment@0/target-module@60000/mmc@0[0]'
[    0.533070] omap_hsmmc 48060000.mmc: using lookup tables for GPIO lookup
[    0.533075] omap_hsmmc 48060000.mmc: No GPIO consumer wp found
[    0.558668] of_get_named_gpiod_flags: can't parse 'simple-audio-card,hp-det-gpio' property of node '/sound[0]'
[    0.558689] of_get_named_gpiod_flags: can't parse 'simple-audio-card,mic-det-gpio' property of node '/sound[0]'
[    0.560793] asoc-simple-card sound: tlv320dac31xx-hifi <-> 4803c000.mcasp mapping ok
[    0.560847] asoc-simple-card sound: ASoC: no DMI vendor name!
[    0.565055] input: MPM Am43xx Audio Headphone as /devices/platform/sound/sound/card0/input0
[    0.566523] rtc-pcf8563 1-0051: setting system clock to 2022-11-10T01:33:43 UTC (1668044023)
[    0.568051] ALSA device list:
[    0.568073]   #0: MPM Am43xx Audio
[    0.568178] Warning: unable to open an initial console.
[    0.568616] Waiting for root device PARTUUID=b0e7b6cb-03...
[    0.617650] mmc1: new high speed MMC card at address 0001
[    0.619022] mmcblk1: mmc1:0001 Q2J54A 3.59 GiB
[    0.619725] mmcblk1boot0: mmc1:0001 Q2J54A partition 1 16.0 MiB
[    0.620430] mmcblk1boot1: mmc1:0001 Q2J54A partition 2 16.0 MiB
[    0.620836] mmcblk1rpmb: mmc1:0001 Q2J54A partition 3 512 KiB, chardev (244:0)
[    0.624467]  mmcblk1: p1 p2 p3 p4
[    0.682385] EXT4-fs (mmcblk1p3): mounted filesystem with ordered data mode. Opts: (null)
[    0.682511] VFS: Mounted root (ext4 filesystem) on device 179:3.
[    0.683735] devtmpfs: mounted
[    0.687922] Freeing unused kernel memory: 1024K
[    0.688065] Run /sbin/init as init process
[    0.705481] Not activating Mandatory Access Control as /sbin/tomoyo-init does not exist.
[    0.908070] systemd[1]: systemd 244.5+ running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR -SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN2 -IDN -PCRE2 default-hierarchy=hybrid)
[    0.908722] systemd[1]: Detected architecture arm.
[    0.919239] systemd[1]: Set hostname to <am437x-evm>.
[    1.598043] systemd[1]: user.slice: unit configures an IP firewall, but the local system does not support BPF/cgroup firewalling.
[    1.598094] systemd[1]: (This warning is only shown for the first unit using IP firewalling.)
[    1.601228] systemd[1]: Created slice User and Session Slice.
[    1.602184] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
[    1.602642] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
[    1.602938] systemd[1]: Reached target Login Prompts.
[    1.603242] systemd[1]: Reached target Paths.
[    1.603427] systemd[1]: Reached target Slices.
[    1.603610] systemd[1]: Reached target Swap.
[    1.617839] systemd[1]: Listening on Process Core Dump Socket.
[    1.618708] systemd[1]: Listening on initctl Compatibility Named Pipe.
[    1.640539] systemd[1]: Condition check resulted in Journal Audit Socket being skipped.
[    1.641919] systemd[1]: Listening on Journal Socket (/dev/log).
[    1.643157] systemd[1]: Listening on Journal Socket.
[    1.644591] systemd[1]: Listening on Network Service Netlink Socket.
[    1.646811] systemd[1]: Listening on udev Control Socket.
[    1.647889] systemd[1]: Listening on udev Kernel Socket.
[    1.648811] systemd[1]: Condition check resulted in Huge Pages File System being skipped.
[    1.657630] systemd[1]: Mounting POSIX Message Queue File System...
[    1.676475] systemd[1]: Mounting Kernel Debug File System...
[    1.702854] systemd[1]: Mounting Temporary Directory (/tmp)...
[    1.704007] systemd[1]: Condition check resulted in Create list of static device nodes for the current kernel being skipped.
[    1.737193] systemd[1]: Started LVGL Logo Boot Screen.
[    1.754322] systemd[1]: Starting Synchronize System and HW clocks...
[    1.760353] systemd[1]: Condition check resulted in File System Check on Root Device being skipped.
[    1.790611] systemd[1]: Starting Journal Service...
[    1.823508] systemd[1]: Condition check resulted in Load Kernel Modules being skipped.
[    1.825357] systemd[1]: Condition check resulted in FUSE Control File System being skipped.
[    1.868419] systemd[1]: Mounting Kernel Configuration File System...
[    1.945548] poweron_type:0
[    1.945569] poweron_type:0
[    1.945574] poweron_type:0
[    1.945577] poweron_type:0
[    1.956511] systemd[1]: Starting Remount Root and Kernel File Systems...
[    2.025611] poweron_type:0
[    2.029102] systemd[1]: Starting Apply Kernel Variables...
[    2.122606] systemd[1]: Starting udev Coldplug all Devices...
[    2.188395] EXT4-fs (mmcblk1p3): re-mounted. Opts: (null)
[    2.283589] systemd[1]: Mounted POSIX Message Queue File System.
[    2.304055] systemd[1]: Mounted Kernel Debug File System.
[    2.316124] systemd[1]: Mounted Temporary Directory (/tmp).
[    2.347327] systemd[1]: logo-start.service: Succeeded.
[    2.376391] systemd[1]: Mounted Kernel Configuration File System.
[    2.400608] systemd[1]: Started Remount Root and Kernel File Systems.
[    2.428738] systemd[1]: Started Apply Kernel Variables.
[    2.444179] systemd[1]: Condition check resulted in Rebuild Hardware Database being skipped.
[    2.448089] systemd[1]: Condition check resulted in Create System Users being skipped.
[    2.493353] systemd[1]: Starting Create Static Device Nodes in /dev...
[    2.554448] systemd[1]: sync-clocks.service: Succeeded.
[    2.574040] systemd[1]: Started Synchronize System and HW clocks.
[    2.668899] systemd[1]: Started Create Static Device Nodes in /dev.
[    2.669996] systemd[1]: Reached target Local File Systems (Pre).
[    2.699414] systemd[1]: Mounting /media/ram...
[    2.746911] systemd[1]: Mounting /var/volatile...
[    2.781007] systemd[1]: Starting udev Kernel Device Manager...
[    2.823748] systemd[1]: Mounted /media/ram.
[    2.846248] systemd[1]: Mounted /var/volatile.
[    2.847471] systemd[1]: Condition check resulted in Bind mount volatile /var/cache being skipped.
[    2.847719] systemd[1]: Condition check resulted in Bind mount volatile /var/lib being skipped.
[    2.877918] systemd[1]: Starting Load/Save Random Seed...
[    2.878507] systemd[1]: Condition check resulted in Bind mount volatile /var/spool being skipped.
[    2.878840] systemd[1]: Condition check resulted in Bind mount volatile /srv being skipped.
[    2.879048] systemd[1]: Reached target Local File Systems.
[    2.879503] systemd[1]: Condition check resulted in Rebuild Dynamic Linker Cache being skipped.
[    2.880010] systemd[1]: Condition check resulted in Commit a transient machine-id on disk being skipped.
[    2.978316] systemd[1]: Started Load/Save Random Seed.
[    3.117957] systemd[1]: Started Journal Service.
[    3.165024] Mvid=46bb
[    3.255658] systemd-journald[86]: Received client request to flush runtime journal.
[    4.332943] lcd res_x = 1920, res_y = 1080
[    4.332950] v8kbd_connect
[    4.333508] serio: Serial port ttyS1
[    4.345117] connect succeed
[    4.345419] input: EDAN V8 Serial Touchscreen as /devices/virtual/input/input2
[    4.345867] register touch device succeed
[    4.346011] input: EDAN V8 Serial Keyboard as /devices/virtual/input/input1
[    4.346206] register keyboard device succeed
[    4.637395] EXT4-fs (mmcblk1p2): mounted filesystem with ordered data mode. Opts: (null)
[    4.637460] ext4 filesystem being mounted at /etc/nx supports timestamps until 2038 (0x7fffffff)
[    4.756126] pvrsrvkm: loading out-of-tree module taints kernel.
[    4.762347] remoteproc remoteproc0: wkup_m3 is available
[    4.899942] [drm] Initialized pvr 1.17.4948957 20110701 for 56000000.gpu on minor 1
[    4.987574] EXT4-fs (mmcblk1p4): mounted filesystem with ordered data mode. Opts: (null)
[    5.176194] omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 10 sec
[    5.436382] remoteproc remoteproc0: powering up wkup_m3
[    5.447280] remoteproc remoteproc0: Booting fw image am335x-pm-firmware.elf, size 243196
[    5.448174] remoteproc remoteproc0: remote processor wkup_m3 is now up
[    5.448287] wkup_m3_ipc 44e11324.wkup_m3_ipc: CM3 Firmware Version = 0x192
[    6.410037] PVR_K: UM DDK-(4948957) and KM DDK-(4948957) match. [ OK ]
[    8.271059] omap-sham 53100000.sham: hw accel on OMAP rev 0.0
[    8.304659] omap-aes 53501000.aes: OMAP AES hw accel rev: 0.1
[    8.315904] omap-des 53701000.des: OMAP DES hw accel rev: 0.33
[    8.345496] omap-des 53701000.des: will run requests pump with realtime priority
[    8.357108] omap-aes 53501000.aes: will run requests pump with realtime priority
[    8.883564] cpsw 4a100000.ethernet: initializing cpsw version 1.15 (0)
[    9.025942] SMSC LAN8710/LAN8720 4a101000.mdio:00: attached PHY driver [SMSC LAN8710/LAN8720] (mii_bus:phy_addr=4a101000.mdio:00, irq=POLL)
[    9.924196] dwc3 48390000.usb: Failed to get clk 'ref': -2
[    9.980841] dwc3 483d0000.usb: Failed to get clk 'ref': -2
[   10.214440] remoteproc remoteproc1: 54434000.pru is available
[   10.214617] pru-rproc 54434000.pru: PRU rproc node /ocp@44000000/target-module@54400000/pruss@0/pru@34000 probed successfully
[   10.222293] remoteproc remoteproc2: 54438000.pru is available
[   10.222502] pru-rproc 54438000.pru: PRU rproc node /ocp@44000000/target-module@54400000/pruss@0/pru@38000 probed successfully
[   10.243839] remoteproc remoteproc3: 54474000.pru is available
[   10.243975] pru-rproc 54474000.pru: PRU rproc node /ocp@44000000/target-module@54400000/pruss@40000/pru@74000 probed successfully
[   10.262902] remoteproc remoteproc4: 54478000.pru is available
[   10.263091] pru-rproc 54478000.pru: PRU rproc node /ocp@44000000/target-module@54400000/pruss@40000/pru@78000 probed successfully
[   10.544168] xhci-hcd xhci-hcd.3.auto: xHCI Host Controller
[   10.544291] xhci-hcd xhci-hcd.3.auto: new USB bus registered, assigned bus number 1
[   10.557184] xhci-hcd xhci-hcd.3.auto: hcc params 0x0238f06d hci version 0x100 quirks 0x0000000002010010
[   10.557278] xhci-hcd xhci-hcd.3.auto: irq 100, io mem 0x48390000
[   10.563512] hub 1-0:1.0: USB hub found
[   10.564693] hub 1-0:1.0: 1 port detected
[   10.583811] xhci-hcd xhci-hcd.3.auto: xHCI Host Controller
[   10.583965] xhci-hcd xhci-hcd.3.auto: new USB bus registered, assigned bus number 2
[   10.584000] xhci-hcd xhci-hcd.3.auto: Host supports USB 3.0 SuperSpeed
[   10.584149] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM.
[   10.594950] hub 2-0:1.0: USB hub found
[   10.595061] hub 2-0:1.0: 1 port detected
[   10.601732] xhci-hcd xhci-hcd.4.auto: xHCI Host Controller
[   10.601791] xhci-hcd xhci-hcd.4.auto: new USB bus registered, assigned bus number 3
[   10.609883] xhci-hcd xhci-hcd.4.auto: hcc params 0x0238f06d hci version 0x100 quirks 0x0000000002010010
[   10.609976] xhci-hcd xhci-hcd.4.auto: irq 101, io mem 0x483d0000
[   10.618536] hub 3-0:1.0: USB hub found
[   10.618634] hub 3-0:1.0: 1 port detected
[   10.624472] xhci-hcd xhci-hcd.4.auto: xHCI Host Controller
[   10.625566] xhci-hcd xhci-hcd.4.auto: new USB bus registered, assigned bus number 4
[   10.625617] xhci-hcd xhci-hcd.4.auto: Host supports USB 3.0 SuperSpeed
[   10.626485] usb usb4: We don't know the algorithms for LPM for this host, disabling LPM.
[   10.637408] hub 4-0:1.0: USB hub found
[   10.637497] hub 4-0:1.0: 1 port detected
[   10.945035] usb 1-1: new high-speed USB device number 2 using xhci-hcd
[   10.985006] usb 3-1: new high-speed USB device number 2 using xhci-hcd
[   11.085561] index=141c,h=0,l=0
[   11.085590] index=1,h=14,l=1c
[   11.202433] hub 3-1:1.0: USB hub found
[   11.203184] hub 3-1:1.0: 4 ports detected
[   13.453219] cfg80211: Loading compiled-in X.509 certificates for regulatory database
[   13.507487] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
[   14.315193] wlan_aes_cmac: module license 'unspecified' taints kernel.
[   14.315220] Disabling lock debugging due to kernel taint
[   14.736002] onebox_usb_probe: driver initialization ...
[   14.737077] onebox_usb_probe: Product ID : 0x9113 Vendor ID : 0x1618
[   14.737091] onebox_usb_probe: 9113 MODULE IS CONNECTED
[   14.737266] common_hal_init: hung_task_timeout_secs is disabled
[   14.750152] will be ignored
[   15.360884] MAC Address     : 80 c9 55 1a b6 70
[   15.360911] MFG SW Version  : 4.4
               Onboard Antenna : 0
               Module Type     : 0 Non-HPM
[   15.360918] Bootloader Ver  : 18
               Band Support    : Dual Band
               Country domain  : 0
[   15.375761] usbcore: registered new interface driver Onebox-USB
[   16.509659] core_net80211_attach: macaddr 80:c9:55:1a:b6:70
[   16.510184] [onebox_update_country][1776] : Updating Country to 00 from WR!!!
[   17.007529] created vap: wlan0
[   17.127576] Bgscan: In onebox_ioctl and 1715
[   17.167285] Resetting the Adapter settings
[   31.204879] evm_v3_3d: disabling
[10377.642455] PVR_K: HWRecoveryResetSGX: SGX Hardware Recovery triggered
[10377.642487] PVR_K: SGX debug (SGX_DDK sgxddk 1.17@4948957)
[10377.642509] PVR_K:(Error): SGX Register Base Address (Linear):   0x2173c69c
[10377.642519] PVR_K:(Error): SGX Register Base Address (Physical): 0x56000000
[10377.642527] PVR_K: Running SGXREG Debug Scripts:
[10377.642535] PVR_K: (P0)
[10377.642544] PVR_K:   (SGXREG) 0x00000000 : 0x00222220
[10377.642553] PVR_K:   (SGXREG) 0x00000004 : 0x00110110
[10377.642560] PVR_K:   (SGXREG) 0x00000118 : 0x00000008
[10377.642569] PVR_K:   (SGXREG) 0x0000012C : 0x00000000
[10377.642576] PVR_K:   (SGXREG) 0x000004E0 : 0x013AEE60
[10377.642584] PVR_K:   (SGXREG) 0x000004E4 : 0x0001101F
[10377.642591] PVR_K:   (SGXREG) 0x00000658 : 0x00000000
[10377.642599] PVR_K:   (SGXREG) 0x00000A74 : 0x09BF8200
[10377.642607] PVR_K:   (SGXREG) 0x00000C04 : 0x00000000
[10377.642615] PVR_K:   (SGXREG) 0x00000C08 : 0x00000000
[10377.642622] PVR_K:   (SGXREG) 0x00000E04 : 0x00000000
[10377.642630] PVR_K:   (SGXREG) 0x00000624 : 0x000016E4
[10377.642638] PVR_K:   (SGXREG) 0x00000628 : 0x000118D1
[10377.642646] PVR_K:   (SGXREG) 0x00000630 : 0x00000007
[10377.642653] PVR_K:   (SGXREG) 0x00000734 : 0x00000000
[10377.642661] PVR_K:   (SGXREG) 0x00000AA4 : 0xAAAAAAAB
[10377.642732] PVR_K:   (SGXREG) 0x00000AA8 : 0xAAAAAAAA
[10377.642741] PVR_K:   (SGXREG) 0x00000B08 : 0x0001023F
[10377.642749] PVR_K:   (SGXREG) 0x00000B14 : 0x000177B9
[10377.642757] PVR_K:   (SGXREG) 0x00000B0C : 0x00012969
[10377.642765] PVR_K:   (SGXREG) 0x00000B18 : 0x0001963C
[10377.642772] PVR_K:   (SGXREG) 0x00000B10 : 0x0001250E
[10377.642780] PVR_K:   (SGXREG) 0x00000B1C : 0x00010000
[10377.642787] PVR_K: SGX Register Dump:
[10377.642796] PVR_K: (P0) EUR_CR_CORE_ID:          01120000
[10377.642804] PVR_K: (P0) EUR_CR_CORE_REVISION:    00010205
[10377.642812] PVR_K: (P0) EUR_CR_EVENT_STATUS:     00000000
[10377.642820] PVR_K: (P0) EUR_CR_EVENT_STATUS2:    00000008
[10377.642829] PVR_K: (P0) EUR_CR_BIF_CTRL:         00000000
[10377.642837] PVR_K: (P0) EUR_CR_BIF_INT_STAT:     00000000
[10377.642845] PVR_K: (P0) EUR_CR_BIF_FAULT:        00000000
[10377.642852] PVR_K: (P0) EUR_CR_BIF_MEM_REQ_STAT: 00000000
[10377.642861] PVR_K: (P0) EUR_CR_CLKGATECTL:       00222220
[10377.642869] PVR_K: (P0) EUR_CR_PDS_PC_BASE:      0030686C
[10377.642876] PVR_K:  Host Ctl flags= 00000006
[10377.642884] PVR_K: SGX Host control:
[10377.642894] PVR_K:   (HC-0) 0x00000001 0x00000000 0x00000000 0x00000001
[10377.642903] PVR_K:   (HC-10) 0x00000001 0x00000000 0x00000014 0x00030D40
[10377.642912] PVR_K:   (HC-20) 0x00000000 0x00000001 0x00000001 0x00000000
[10377.642922] PVR_K:   (HC-30) 0x00000000 0x009E4026 0xEE811670 0x00000000
[10377.642931] PVR_K:   (HC-40) 0x00000000 0x00000000 0x00229B49 0xDBB6218C
[10377.642938] PVR_K: SGX TA/3D control:
[10377.642948] PVR_K:   (T3C-0) 0x0F003000 0x0F003140 0x0F002000 0x00000000
[10377.642957] PVR_K:   (T3C-10) 0x00000000 0x00000000 0x00000002 0x00000000
[10377.642966] PVR_K:   (T3C-20) 0x00000000 0x00000000 0x00000000 0x00000000
[10377.642975] PVR_K:   (T3C-30) 0x00000000 0x00000000 0x00000000 0x00000000
[10377.642984] PVR_K:   (T3C-40) 0x00000000 0x00000000 0x00000000 0x00000000
[10377.642993] PVR_K:   (T3C-50) 0x00000000 0x00000000 0x00000000 0x00000000
[10377.643001] PVR_K:   (T3C-60) 0x00000000 0x00000000 0x00000000 0x00000000
[10377.643010] PVR_K:   (T3C-70) 0x00000000 0x00000000 0x00000000 0x00000000
[10377.643019] PVR_K:   (T3C-80) 0x00000000 0x00000000 0x0F09D640 0x0F000000
[10377.643028] PVR_K:   (T3C-90) 0x9A916000 0x0F091280 0x00000000 0x0F09E840
[10377.643037] PVR_K:   (T3C-A0) 0x0F00AEA0 0x0F09D640 0x0F09E840 0x00000000
[10377.643046] PVR_K:   (T3C-B0) 0x00000000 0x00000000 0x00000000 0x00000000
[10377.643055] PVR_K:   (T3C-C0) 0x00000000 0x00000000 0x000350C7 0x000350C7
[10377.643064] PVR_K:   (T3C-D0) 0x0F000000 0x8000B000 0x8004B000 0x0F004000
[10377.643074] PVR_K:   (T3C-E0) 0x0F00A420 0x0F00A740 0x0F08B000 0x0F08B000
[10377.643082] PVR_K:   (T3C-F0) 0x00000000 0x00000107 0x00000107 0x00000000
[10377.643092] PVR_K:   (T3C-100) 0x00000001 0x00000002 0x00000000 0x00000000
[10377.643101] PVR_K:   (T3C-110) 0xEE0C12A2 0x00000000 0x00000000 0x00000000
[10377.643110] PVR_K:   (T3C-120) 0x0F00AEA0 0x0F091280 0x00000000 0xDBB6212C
[10377.643119] PVR_K: SGX Kernel CCB WO:0x1B RO:0x1B
[10377.643127] PVR_K: Active syncs
[10377.643171] PVR_K:   SyncInfo 13:
[10377.643182] PVR_K:           Write ops (0x0d80120c): P/C = 72430/72429 (0x00011aee/0x00011aed)
[10377.643192] PVR_K:           Read ops (0x0d801214): P/C = 0/0 (0x00000000/0x00000000)
[10377.643202] PVR_K:           Read ops 2 (0x0d80121c): P/C = 0/0 (0x00000000/0x00000000)
[10377.643223] PVR_K:   SyncInfo 2:
[10377.643233] PVR_K:           Write ops (0x0d801054): P/C = 170/170 (0x000000aa/0x000000aa)
[10377.643242] PVR_K:           Read ops (0x0d80105c): P/C = 217295/217294 (0x000350cf/0x000350ce)
[10377.643252] PVR_K:           Read ops 2 (0x0d801064): P/C = 0/0 (0x00000000/0x00000000)
[10377.643261] PVR_K:   SyncInfo 0:
[10377.643270] PVR_K:           Write ops (0x0d801004): P/C = 217295/217294 (0x000350cf/0x000350ce)
[10377.643280] PVR_K:           Read ops (0x0d80100c): P/C = 0/0 (0x00000000/0x00000000)
[10377.643289] PVR_K:           Read ops 2 (0x0d801014): P/C = 0/0 (0x00000000/0x00000000)
[10551.052486] PVR_K: HWRecoveryResetSGX: SGX Hardware Recovery triggered
[10551.052519] PVR_K: SGX debug (SGX_DDK sgxddk 1.17@4948957)
[10551.052540] PVR_K:(Error): SGX Register Base Address (Linear):   0x2173c69c
[10551.052550] PVR_K:(Error): SGX Register Base Address (Physical): 0x56000000
[10551.052559] PVR_K: Running SGXREG Debug Scripts:
[10551.052567] PVR_K: (P0)
[10551.052576] PVR_K:   (SGXREG) 0x00000000 : 0x00222220
[10551.052584] PVR_K:   (SGXREG) 0x00000004 : 0x00110110
[10551.052592] PVR_K:   (SGXREG) 0x00000118 : 0x00000008
[10551.052600] PVR_K:   (SGXREG) 0x0000012C : 0x00000000
[10551.052607] PVR_K:   (SGXREG) 0x000004E0 : 0x01091EF0
[10551.052615] PVR_K:   (SGXREG) 0x000004E4 : 0x0003140F
[10551.052622] PVR_K:   (SGXREG) 0x00000658 : 0x00000000
[10551.052630] PVR_K:   (SGXREG) 0x00000A74 : 0x09BF8200
[10551.052638] PVR_K:   (SGXREG) 0x00000C04 : 0x00000000
[10551.052645] PVR_K:   (SGXREG) 0x00000C08 : 0x00000000
[10551.052653] PVR_K:   (SGXREG) 0x00000E04 : 0x00000000
[10551.052661] PVR_K:   (SGXREG) 0x00000624 : 0x000016E4
[10551.052669] PVR_K:   (SGXREG) 0x00000628 : 0x000118D1
[10551.052676] PVR_K:   (SGXREG) 0x00000630 : 0x00000007
[10551.052684] PVR_K:   (SGXREG) 0x00000734 : 0x00000000
[10551.052691] PVR_K:   (SGXREG) 0x00000AA4 : 0xAAAAAAAB
[10551.052699] PVR_K:   (SGXREG) 0x00000AA8 : 0xAAAAAAAA
[10551.052707] PVR_K:   (SGXREG) 0x00000B08 : 0x00013A28
[10551.052715] PVR_K:   (SGXREG) 0x00000B14 : 0x00017802
[10551.052722] PVR_K:   (SGXREG) 0x00000B0C : 0x0001BB34
[10551.052730] PVR_K:   (SGXREG) 0x00000B18 : 0x0001BB8D
[10551.052738] PVR_K:   (SGXREG) 0x00000B10 : 0x000108F1
[10551.052745] PVR_K:   (SGXREG) 0x00000B1C : 0x00010000
[10551.052752] PVR_K: SGX Register Dump:
[10551.052761] PVR_K: (P0) EUR_CR_CORE_ID:          01120000
[10551.052769] PVR_K: (P0) EUR_CR_CORE_REVISION:    00010205
[10551.052777] PVR_K: (P0) EUR_CR_EVENT_STATUS:     00000000
[10551.052785] PVR_K: (P0) EUR_CR_EVENT_STATUS2:    00000008
[10551.052793] PVR_K: (P0) EUR_CR_BIF_CTRL:         00000000
[10551.052802] PVR_K: (P0) EUR_CR_BIF_INT_STAT:     00000000
[10551.052810] PVR_K: (P0) EUR_CR_BIF_FAULT:        00000000
[10551.052818] PVR_K: (P0) EUR_CR_BIF_MEM_REQ_STAT: 00000000
[10551.052826] PVR_K: (P0) EUR_CR_CLKGATECTL:       00222220
[10551.052834] PVR_K: (P0) EUR_CR_PDS_PC_BASE:      0030686C
[10551.052842] PVR_K:  Host Ctl flags= 00000006
[10551.052850] PVR_K: SGX Host control:
[10551.052860] PVR_K:   (HC-0) 0x00000001 0x00000000 0x00000000 0x00000001
[10551.052870] PVR_K:   (HC-10) 0x00000002 0x00000000 0x00000014 0x00030D40
[10551.052879] PVR_K:   (HC-20) 0x00000000 0x00000001 0x00000001 0x00000000
[10551.052888] PVR_K:   (HC-30) 0x00000000 0x00A0E583 0x58AC6E30 0x00000000
[10551.052897] PVR_K:   (HC-40) 0x00000000 0x00000000 0x00232F1A 0xDBB6218C
[10551.052905] PVR_K: SGX TA/3D control:
[10551.052914] PVR_K:   (T3C-0) 0x0F003000 0x0F003140 0x0F002000 0x00000000
[10551.052923] PVR_K:   (T3C-10) 0x00000000 0x00000000 0x00000002 0x00000000
[10551.052932] PVR_K:   (T3C-20) 0x00000000 0x00000000 0x00000000 0x00000000
[10551.052941] PVR_K:   (T3C-30) 0x00000000 0x00000000 0x00000000 0x00000000
[10551.052950] PVR_K:   (T3C-40) 0x00000000 0x00000000 0x00000000 0x00000000
[10551.052959] PVR_K:   (T3C-50) 0x00000000 0x00000000 0x00000000 0x00000000
[10551.052967] PVR_K:   (T3C-60) 0x00000000 0x00000000 0x00000000 0x00000000
[10551.052976] PVR_K:   (T3C-70) 0x00000000 0x00000000 0x00000000 0x00000000
[10551.052985] PVR_K:   (T3C-80) 0x00000000 0x00000000 0x0F09D640 0x0F000000
[10551.052994] PVR_K:   (T3C-90) 0x9A916000 0x0F092400 0x00000000 0x0F09E840
[10551.053004] PVR_K:   (T3C-A0) 0x0F00AEA0 0x0F09D640 0x0F09E840 0x00000000
[10551.053012] PVR_K:   (T3C-B0) 0x00000000 0x00000000 0x00000000 0x00000000
[10551.053021] PVR_K:   (T3C-C0) 0x00000000 0x00000000 0x00035F01 0x00035F01
[10551.053031] PVR_K:   (T3C-D0) 0x0F000000 0x8000B000 0x8004B000 0x0F004000
[10551.053040] PVR_K:   (T3C-E0) 0x0F00A420 0x0F00A740 0x0F08B000 0x0F08B000
[10551.053049] PVR_K:   (T3C-F0) 0x00000000 0x00000107 0x00000107 0x00000000
[10551.053058] PVR_K:   (T3C-100) 0x00000001 0x00000003 0x00000000 0x00000000
[10551.053067] PVR_K:   (T3C-110) 0xA2965929 0x00000000 0x00000000 0x00000000
[10551.053077] PVR_K:   (T3C-120) 0x0F00AEA0 0x0F092400 0x00000000 0xDBB6212C
[10551.053113] PVR_K: SGX Kernel CCB WO:0x4 RO:0x4
[10551.053121] PVR_K: Active syncs
[10551.053166] PVR_K:   SyncInfo 13:
[10551.053177] PVR_K:           Write ops (0x0d80120c): P/C = 73644/73643 (0x00011fac/0x00011fab)
[10551.053187] PVR_K:           Read ops (0x0d801214): P/C = 0/0 (0x00000000/0x00000000)
[10551.053197] PVR_K:           Read ops 2 (0x0d80121c): P/C = 0/0 (0x00000000/0x00000000)
[10551.053218] PVR_K:   SyncInfo 2:
[10551.053227] PVR_K:           Write ops (0x0d801054): P/C = 170/170 (0x000000aa/0x000000aa)
[10551.053237] PVR_K:           Read ops (0x0d80105c): P/C = 220937/220936 (0x00035f09/0x00035f08)
[10551.053246] PVR_K:           Read ops 2 (0x0d801064): P/C = 0/0 (0x00000000/0x00000000)
[10551.053255] PVR_K:   SyncInfo 0:
[10551.053265] PVR_K:           Write ops (0x0d801004): P/C = 220937/220936 (0x00035f09/0x00035f08)
[10551.053274] PVR_K:           Read ops (0x0d80100c): P/C = 0/0 (0x00000000/0x00000000)
[10551.053284] PVR_K:           Read ops 2 (0x0d801014): P/C = 0/0 (0x00000000/0x00000000)
[34775.845625] tlv320aic31xx-codec 1-0018: Unknown DAC interrupt flags: 0x00000003
[72418.885551] tlv320aic31xx-codec 1-0018: Unknown DAC interrupt flags: 0x00000003
[76493.756917] PVR_K: HWRecoveryResetSGX: SGX Hardware Recovery triggered
[76493.756950] PVR_K: SGX debug (SGX_DDK sgxddk 1.17@4948957)
[76493.756972] PVR_K:(Error): SGX Register Base Address (Linear):   0x2173c69c
[76493.756982] PVR_K:(Error): SGX Register Base Address (Physical): 0x56000000
[76493.756989] PVR_K: Running SGXREG Debug Scripts:
[76493.756997] PVR_K: (P0)
[76493.757007] PVR_K:   (SGXREG) 0x00000000 : 0x00222220
[76493.757015] PVR_K:   (SGXREG) 0x00000004 : 0x00110110
[76493.757022] PVR_K:   (SGXREG) 0x00000118 : 0x00000008
[76493.757031] PVR_K:   (SGXREG) 0x0000012C : 0x00000000
[76493.757039] PVR_K:   (SGXREG) 0x000004E0 : 0x00EA31F0
[76493.757047] PVR_K:   (SGXREG) 0x000004E4 : 0x00012C1B
[76493.757054] PVR_K:   (SGXREG) 0x00000658 : 0x00000000
[76493.757062] PVR_K:   (SGXREG) 0x00000A74 : 0x09BF8200
[76493.757070] PVR_K:   (SGXREG) 0x00000C04 : 0x00000000
[76493.757078] PVR_K:   (SGXREG) 0x00000C08 : 0x00000000
[76493.757085] PVR_K:   (SGXREG) 0x00000E04 : 0x00000000
[76493.757093] PVR_K:   (SGXREG) 0x00000624 : 0x000016E4
[76493.757101] PVR_K:   (SGXREG) 0x00000628 : 0x000118D1
[76493.757109] PVR_K:   (SGXREG) 0x00000630 : 0x00000007
[76493.757116] PVR_K:   (SGXREG) 0x00000734 : 0x00000000
[76493.757124] PVR_K:   (SGXREG) 0x00000AA4 : 0xAAAAAAAB
[76493.757132] PVR_K:   (SGXREG) 0x00000AA8 : 0xAAAAAAAA
[76493.757139] PVR_K:   (SGXREG) 0x00000B08 : 0x0001E56C
[76493.757147] PVR_K:   (SGXREG) 0x00000B14 : 0x0001E9F4
[76493.757155] PVR_K:   (SGXREG) 0x00000B0C : 0x0001CE5D
[76493.757163] PVR_K:   (SGXREG) 0x00000B18 : 0x00017E39
[76493.757170] PVR_K:   (SGXREG) 0x00000B10 : 0x0001524C
[76493.757178] PVR_K:   (SGXREG) 0x00000B1C : 0x00010000
[76493.757184] PVR_K: SGX Register Dump:
[76493.757193] PVR_K: (P0) EUR_CR_CORE_ID:          01120000
[76493.757202] PVR_K: (P0) EUR_CR_CORE_REVISION:    00010205
[76493.757209] PVR_K: (P0) EUR_CR_EVENT_STATUS:     00000000
[76493.757217] PVR_K: (P0) EUR_CR_EVENT_STATUS2:    00000008
[76493.757225] PVR_K: (P0) EUR_CR_BIF_CTRL:         00000000
[76493.757234] PVR_K: (P0) EUR_CR_BIF_INT_STAT:     00000000
[76493.757242] PVR_K: (P0) EUR_CR_BIF_FAULT:        00000000
[76493.757250] PVR_K: (P0) EUR_CR_BIF_MEM_REQ_STAT: 00000000
[76493.757258] PVR_K: (P0) EUR_CR_CLKGATECTL:       00222220
[76493.757266] PVR_K: (P0) EUR_CR_PDS_PC_BASE:      0030686C
[76493.757274] PVR_K:  Host Ctl flags= 00000006
[76493.757282] PVR_K: SGX Host control:
[76493.757292] PVR_K:   (HC-0) 0x00000001 0x00000000 0x00000000 0x00000001
[76493.757301] PVR_K:   (HC-10) 0x00000003 0x00000000 0x00000014 0x00030D40
[76493.757310] PVR_K:   (HC-20) 0x00000000 0x00000001 0x00000001 0x00000000
[76493.757320] PVR_K:   (HC-30) 0x00000000 0x048F18E8 0x63027500 0x00000000
[76493.757329] PVR_K:   (HC-40) 0x00000000 0x00000000 0x00FFA249 0xDBB6218C
[76493.757336] PVR_K: SGX TA/3D control:
[76493.757346] PVR_K:   (T3C-0) 0x0F003000 0x0F003140 0x0F002000 0x00000000
[76493.757355] PVR_K:   (T3C-10) 0x00000000 0x00000000 0x00000002 0x00000000
[76493.757364] PVR_K:   (T3C-20) 0x00000000 0x00000000 0x00000000 0x00000000
[76493.757373] PVR_K:   (T3C-30) 0x00000000 0x00000000 0x00000000 0x00000000
[76493.757382] PVR_K:   (T3C-40) 0x00000000 0x00000000 0x00000000 0x00000000
[76493.757390] PVR_K:   (T3C-50) 0x00000000 0x00000000 0x00000000 0x00000000
[76493.757399] PVR_K:   (T3C-60) 0x00000000 0x00000000 0x00000000 0x00000000
[76493.757408] PVR_K:   (T3C-70) 0x00000000 0x00000000 0x00000000 0x00000000
[76493.757417] PVR_K:   (T3C-80) 0x00000000 0x00000000 0x0F09D640 0x0F000000
[76493.757426] PVR_K:   (T3C-90) 0x9A916000 0x0F08CE80 0x00000000 0x0F09E840
[76493.757436] PVR_K:   (T3C-A0) 0x0F00AEA0 0x0F09D640 0x0F09E840 0x00000000
[76493.757444] PVR_K:   (T3C-B0) 0x00000000 0x00000000 0x00000000 0x00000000
[76493.757454] PVR_K:   (T3C-C0) 0x00000000 0x00000000 0x00187FD7 0x00187FD7
[76493.757463] PVR_K:   (T3C-D0) 0x0F000000 0x8000B000 0x8004B000 0x0F004000
[76493.757472] PVR_K:   (T3C-E0) 0x0F00A420 0x0F00A740 0x0F08B000 0x0F08B000
[76493.757481] PVR_K:   (T3C-F0) 0x00000000 0x00000107 0x00000107 0x00000000
[76493.757490] PVR_K:   (T3C-100) 0x00000001 0x00000003 0x00000000 0x00000000
[76493.757499] PVR_K:   (T3C-110) 0xB3D83876 0x00000000 0x00000000 0x00000000
[76493.757509] PVR_K:   (T3C-120) 0x0F00AEA0 0x0F08CE80 0x00000000 0xDBB6212C
[76493.757517] PVR_K: SGX Kernel CCB WO:0x4A RO:0x4A
[76493.757525] PVR_K: Active syncs
[76493.757569] PVR_K:   SyncInfo 13:
[76493.757580] PVR_K:           Write ops (0x0d80120c): P/C = 535198/535197 (0x00082a9e/0x00082a9d)
[76493.757590] PVR_K:           Read ops (0x0d801214): P/C = 0/0 (0x00000000/0x00000000)
[76493.757600] PVR_K:           Read ops 2 (0x0d80121c): P/C = 0/0 (0x00000000/0x00000000)
[76493.757621] PVR_K:   SyncInfo 2:
[76493.757630] PVR_K:           Write ops (0x0d801054): P/C = 170/170 (0x000000aa/0x000000aa)
[76493.757640] PVR_K:           Read ops (0x0d80105c): P/C = 1605599/1605598 (0x00187fdf/0x00187fde)
[76493.757650] PVR_K:           Read ops 2 (0x0d801064): P/C = 0/0 (0x00000000/0x00000000)
[76493.757658] PVR_K:   SyncInfo 0:
[76493.757668] PVR_K:           Write ops (0x0d801004): P/C = 1605599/1605598 (0x00187fdf/0x00187fde)
[76493.757677] PVR_K:           Read ops (0x0d80100c): P/C = 0/0 (0x00000000/0x00000000)
[76493.757686] PVR_K:           Read ops 2 (0x0d801014): P/C = 0/0 (0x00000000/0x00000000)

我的应用程序在出现问题时运行了将近三个小时,我的程序是基于 EGLFS 的 QT 应用程序。

我已经研究了与论坛有关的问题,但没有一个问题得到解决。

TI 团队建议什么?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    我们不再支持 SGX 驱动程序、以下是可用选项:
    我们可以向您提供源代码、并让您的本地 FAE 联系我们。
    2.与第三方合作、该第三方可帮助进行 GPU 驱动程序调试。

    此致、
    Krunal