This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] Linux/TMS320DM8168:MCFW 演示不适用于 A8和 DSP 之间的 syslink

Guru**** 2979400 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/676517/linux-tms320dm8168-mcfw-demo-not-work-for-the-syslink-between-a8-and-dsp

器件型号:TMS320DM8168

工具/软件:Linux

[主机] MCFW_IPCFRAMES:Loopback _ipcFramesSendFxn:已输入... 0:系统:正在进行系统通用初始化!!!
0:系统:正在进行 IPC 初始化!!
13:系统:CPU [DSP] syslink p*** nameserver_add:找到重复的条目!
在文件/home/vefone/dm8148/sdk/ti-ezsdk_dm814x-evm_5_05_02_00/component-sources/syslink_2_20_02_20/packages/ti/syslink/utils/hlos/knl/Linux/../../../../../../ti/syslink/utils/hlos/knl/NameServer.c 中的行号:1055处出现错误[0xfffffffe]
ROC ID 是[0]!!*** HeapMemMP_create:无法添加到名称服务器!
在文件/home/vefone/dm8148/sdk/ti-ezsdk_dm814x-evm_5_05_02_00/component-sources/syslink_2_20_02_20/packages/ti/syslink/utils/hlos/knl/Linux/../../../../../../ti/syslink/ipc/hlos/knl/HeapMemMP.c 中的第2241行出现错误[0xffffff]
!!
13:系统:*** HeapMemMP_create:_HeapMemMP_create 在 HeapMemMP_create 中失败!
在文件/home/vefone/dm8148/sdk/ti-ezsdk_dm814x-evm_5_05_02_00/component-sources/syslink_2_20_02_20/packages/ti/syslink/utils/hlos/knl/Linux/../../../../../../ti/syslink/ipc/hlos/knl/HeapMemMP.c 中第613行出现错误[0xffffff]
CPU [VIDEE-M3] SAssertion at Line no: 379 in /home/vefone/dm8148/sdk/ti-ezsdk_dm814x-evm_5_05_02_00/component-sources/syslink_2_20_02_20/packages/ti/syslink/utils/hlos/knl/Linux/../../../../../../ti/syslink/ipc/hlos/knl/Linux/HeapMemMPDrv.c:(cargs.args.create.handle != NULL):failed
yslink proc ID 是[1]!!!
13:系统:CPU [VPSS-M3] syslink proc ID 是[2]!!!
13:系统:CPU [host] syslink proc ID 是[3]!!!
13:系统:创建 MSGQ 堆[IPC_MSGQ_MSG_HIP_3]...
断言(system_ipc_msgq.c|System_ipcMsgQHeapCreate|141)