This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] 66AK2E05:66AK2E05:如何将 GbE 接口配置为开关。

Guru**** 2551910 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1180567/66ak2e05-66ak2e05-how-to-configure-gbe-interfaces-as-switch

器件型号:66AK2E05

您好!

我正在尝试配置 Keystone  TI 通用平台以太网交换机(CPSW)。 是的  使用具有默认内核-器件树的 EVMK2E 开发板

按照 https://software-dl.ti.com/processor-sdk-linux/esd/docs/06_03_00_106/linux/Foundational_Components/Kernel/Kernel_Drivers/Network/CPSW.html 中的说明 、我设法构建了一个支持 TI CPSW 交换机802.1Q VLAN 支持的新内核

Load address: 0x88000000
Loading: ######
done
Bytes transferred = 27071 (69bf hex)
## Flattened Device Tree blob at 88000000
   Booting using the fdt blob at 0x88000000
   Loading Ramdisk to 8fff0000, end 8ffffe48 ... OK
   Loading Device Tree to 8ffe6000, end 8ffef9be ... OK

Starting kernel ...

[    0.000000] Booting Linux on physical CPU 0x0
[    0.000000] Linux version 4.19.94+ (ide@tmssrv) (gcc version 8.4.0 (Buildroot 2020.11.1)) #1 S
MP PREEMPT Mon Dec 5 16:34:44 EET 2022
[    0.000000] CPU: ARMv7 Processor [412fc0f4] revision 4 (ARMv7), cr=30c5387d
[    0.000000] CPU: div instructions available: patching division code
[    0.000000] CPU: PIPT / VIPT nonaliasing data cache, PIPT instruction cache
[    0.000000] OF: fdt: Machine model: Texas Instruments Keystone 2 Edison EVM
[    0.000000] Memory policy: Data cache writealloc
[    0.000000] Switching physical address space to 0x800000000
[    0.000000] Reserved memory: created CMA memory pool at 0x000000081f800000, size 8 MiB
[    0.000000] OF: reserved mem: initialized node dsp-common-memory@81f800000, compatible id shar
ed-dma-pool
[    0.000000] cma: Reserved 16 MiB at 0x000000087ec00000
[    0.000000] psci: probing for conduit method from DT.
[    0.000000] psci: Using PSCI v0.1 Function IDs from DT
[    0.000000] random: get_random_bytes called from start_kernel+0xa4/0x4a0 with crng_init=0
[    0.000000] percpu: Embedded 15 pages/cpu s32588 r8192 d20660 u61440
[    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 982016
[    0.000000] Kernel command line: console=ttyS0,115200n8 rootwait=1 mtdparts=spi0.0:1m(u-boot-s
pl)ro,-(misc) rootfstype=nfs root=/dev/nfs rw nfsroot=/srv/nfsCCM,v3,tcp,rsize=4096,wsize=4096 ip
=10.10.10.171:10.10.10.196:10.10.10.1:255.255.255.0:k2e-evm-2:eth0:off:10.10.10.1 nfsrootdebug
[    0.000000] log_buf_len individual max cpu contribution: 4096 bytes
[    0.000000] log_buf_len total cpu_extra contributions: 12288 bytes
[    0.000000] log_buf_len min size: 16384 bytes
[    0.000000] log_buf_len: 32768 bytes
[    0.000000] early log buf free: 14268(87%)
[    0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
[    0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
[    0.000000] Memory: 3860992K/3932160K available (8192K kernel code, 448K rwdata, 2348K rodata,
 2048K init, 197K bss, 46592K reserved, 24576K cma-reserved, 3391488K highmem)
[    0.000000] Virtual kernel memory layout:
[    0.000000]     vector  : 0xffff0000 - 0xffff1000   (   4 kB)
[    0.000000]     fixmap  : 0xffc00000 - 0xfff00000   (3072 kB)
[    0.000000]     vmalloc : 0xe0800000 - 0xff800000   ( 496 MB)
[    0.000000]     lowmem  : 0xc0000000 - 0xe0000000   ( 512 MB)
[    0.000000]     pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)
[    0.000000]     modules : 0xbf000000 - 0xbfe00000   (  14 MB)
[    0.000000]       .text : 0x(ptrval) - 0x(ptrval)   (10208 kB)
[    0.000000]       .init : 0x(ptrval) - 0x(ptrval)   (2048 kB)
[    0.000000]       .data : 0x(ptrval) - 0x(ptrval)   ( 449 kB)
[    0.000000]        .bss : 0x(ptrval) - 0x(ptrval)   ( 198 kB)
[    0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
[    0.000000] rcu: Preemptible hierarchical RCU implementation.
[    0.000000]  Tasks RCU enabled.
[    0.000000] NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16
[    0.000000] GIC: Using split EOI/Deactivate mode
[    0.000000] arch_timer: cp15 timer(s) running at 233.33MHz (phys).
[    0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x6ba0ac50b7, ma
x_idle_ns: 881590427583 ns
[    0.000003] sched_clock: 56 bits at 233MHz, resolution 4ns, wraps every 4398046511102ns
[    0.000012] Switching to timer-based delay loop, resolution 4ns
[    0.000125] keystone timer clock @233333333 Hz
[    0.000248] Console: colour dummy device 80x30
[    0.000270] Calibrating delay loop (skipped), value calculated using timer frequency.. 466.66 
BogoMIPS (lpj=2333333)
[    0.000280] pid_max: default: 4096 minimum: 301
[    0.000357] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)
[    0.000366] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)
[    0.000687] CPU: Testing write buffer coherency: ok
[    0.000707] CPU0: Spectre v2: firmware did not set auxiliary control register IBE bit, system 
vulnerable
[    0.000867] /cpus/cpu@0 missing clock-frequency property
[    0.000884] /cpus/cpu@1 missing clock-frequency property
[    0.000901] /cpus/cpu@2 missing clock-frequency property
[    0.000918] /cpus/cpu@3 missing clock-frequency property
[    0.000926] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
[    0.060025] Setting up static identity map for 0x80200000 - 0x80200138
[    0.080025] rcu: Hierarchical SRCU implementation.
[    0.120059] smp: Bringing up secondary CPUs ...
[    0.204334] CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
[    0.204340] CPU1: Spectre v2: firmware did not set auxiliary control register IBE bit, system 
vulnerable
[    0.284412] CPU2: thread -1, cpu 2, socket 0, mpidr 80000002
[    0.284417] CPU2: Spectre v2: firmware did not set auxiliary control register IBE bit, system 
vulnerable
[    0.364487] CPU3: thread -1, cpu 3, socket 0, mpidr 80000003
[    0.364492] CPU3: Spectre v2: firmware did not set auxiliary control register IBE bit, system 
vulnerable
[    0.364608] smp: Brought up 1 node, 4 CPUs
[    0.364617] SMP: Total of 4 processors activated (1866.66 BogoMIPS).
[    0.364623] CPU: All CPU(s) started in HYP mode.
[    0.364629] CPU: Virtualization extensions available.
[    0.364976] devtmpfs: initialized
[    0.368273] VFP support v0.3: implementor 41 architecture 4 part 30 variant f rev 0
[    0.368531] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 191126
04462750000 ns
[    0.368542] futex hash table entries: 16 (order: -2, 1024 bytes)
[    0.368840] pinctrl core: initialized pinctrl subsystem
[    0.369218] NET: Registered protocol family 16
[    0.369922] DMA: preallocated 256 KiB pool for atomic coherent allocations
[    0.370938] hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.
[    0.370946] hw-breakpoint: maximum watchpoint size is 8 bytes.
[    0.386615] vgaarb: loaded
[    0.386860] SCSI subsystem initialized
[    0.387192] usbcore: registered new interface driver usbfs
[    0.387263] usbcore: registered new interface driver hub
[    0.387345] usbcore: registered new device driver usb
[    0.389414] clocksource: Switched to clocksource arch_sys_counter
[    0.426861] NET: Registered protocol family 2
[    0.427196] tcp_listen_portaddr_hash hash table entries: 512 (order: 0, 6144 bytes)
[    0.427215] TCP established hash table entries: 4096 (order: 2, 16384 bytes)
[    0.427242] TCP bind hash table entries: 4096 (order: 3, 32768 bytes)
[    0.427290] TCP: Hash tables configured (established 4096 bind 4096)
[    0.427343] UDP hash table entries: 256 (order: 1, 8192 bytes)
[    0.427359] UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)
[    0.427451] NET: Registered protocol family 1
[    0.427695] RPC: Registered named UNIX socket transport module.
[    0.427702] RPC: Registered udp transport module.
[    0.427708] RPC: Registered tcp transport module.
[    0.427714] RPC: Registered tcp NFSv4.1 backchannel transport module.
[    0.427821] Unpacking initramfs...
[    0.431208] Freeing initrd memory: 64K
[    0.431419] hw perfevents: no interrupt-affinity property for /pmu, guessing.
[    0.431631] hw perfevents: enabled with armv7_cortex_a15 PMU driver, 7 counters available
[    0.432163] platform alarmtimer: set dma_pfn_offset00780000
[    0.433360] workingset: timestamp_bits=30 max_order=20 bucket_order=0
[    0.440516] Installing knfsd (copyright (C) 1996 okir@monad.swb.de).
[    0.440674] ntfs: driver 2.1.32 [Flags: R/O].
[    0.440973] jffs2: version 2.2. (NAND) ?? 2001-2006 Red Hat, Inc.
[    0.443480] NET: Registered protocol family 38
[    0.443516] bounce: pool size: 64 pages
[    0.443578] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 252)
[    0.443587] io scheduler noop registered
[    0.443593] io scheduler deadline registered
[    0.443614] io scheduler cfq registered (default)
[    0.443621] io scheduler mq-deadline registered
[    0.443627] io scheduler kyber registered
[    0.443866] keystone_irq 26202a0.keystone_irq: irqchip registered, nr_irqs 28
[    0.445615] keystone-pcie 21020000.pcie: host bridge /soc@0/pcie@21020000 ranges:
[    0.445641] keystone-pcie 21020000.pcie:    IO 0x60000000..0x600fffff -> 0x00000000
[    0.445656] keystone-pcie 21020000.pcie:   MEM 0x60100000..0x6fffffff -> 0x60100000
[    1.439421] keystone-pcie 21020000.pcie: Phy link never came up
[    1.439540] keystone-pcie 21020000.pcie: PCI host bridge to bus 0000:00
[    1.439551] pci_bus 0000:00: root bus resource [bus 00-ff]
[    1.439559] pci_bus 0000:00: root bus resource [io  0x0000-0xfffff]
[    1.439567] pci_bus 0000:00: root bus resource [mem 0x60100000-0x6fffffff]
[    1.440884] PCI: bus0: Fast back to back transfers disabled
[    1.442022] PCI: bus1: Fast back to back transfers enabled
[    1.442050] pci 0000:00:00.0: PCI bridge to [bus 01-ff]
[    1.442975] keystone-navigator-qmss soc@0:qmss@2a40000: qmgr start queue 0, number of queues 8
192
[    1.443080] keystone-navigator-qmss soc@0:qmss@2a40000: added qmgr start queue 0, num of queue
s 8192, reg_peek (ptrval), reg_status (ptrval), reg_config (ptrval), reg_region (ptrval), reg_pus
h (ptrval), reg_pop (ptrval)
[    1.443200] keystone-navigator-qmss soc@0:qmss@2a40000: firmware file ks2_qmss_pdsp_acc48.bin 
downloaded for PDSP
[    1.445406] keystone-navigator-dma soc@0:knav_dmas@0: DMA dma_gbe registered 149 logical chann
els, flows 128, tx chans: 21, rx chans: 91
[    1.493732] Serial: 8250/16550 driver, 4 ports, IRQ sharing disabled
[    1.493786] platform serial8250: set dma_pfn_offset00780000
[    1.495298] console [ttyS0] disabled
[    1.495338] 2530c00.serial: ttyS0 at MMIO 0x2530c00 (irq = 27, base_baud = 14583333) is a TI D
A8xx/66AK2x
[    2.359484] console [ttyS0] enabled
[    2.363635] 2531000.serial: ttyS1 at MMIO 0x2531000 (irq = 28, base_baud = 14583333) is a TI D
A8xx/66AK2x
[    2.379107] loop: module loaded
[    2.383141] at24 0-0050: 131072 byte 24c1024 EEPROM, writable, 1 bytes/write
[    2.391302] spi_davinci 21000400.spi: DMA is not supported (-19)
[    2.398034] m25p80 spi0.0: n25q128a11 (16384 Kbytes)
[    2.403031] 2 cmdlinepart partitions found on MTD device spi0.0
[    2.408962] Creating 2 MTD partitions on "spi0.0":
[    2.413776] 0x000000000000-0x000000100000 : "u-boot-spl"
[    2.419808] 0x000000100000-0x000001000000 : "misc"
[    2.425223] spi_davinci 21000400.spi: Controller at 0x(ptrval)
[    2.431284] spi_davinci 21000600.spi: DMA is not supported (-19)
[    2.437565] spi_davinci 21000600.spi: Controller at 0x(ptrval)
[    2.443627] spi_davinci 21000800.spi: DMA is not supported (-19)
[    2.449922] spi_davinci 21000800.spi: Controller at 0x(ptrval)
[    2.455985] platform Fixed MDIO bus.0: set dma_pfn_offset00780000
[    2.462264] libphy: Fixed MDIO Bus: probed
[    2.519426] davinci_mdio 24200f00.mdio: davinci mdio revision 1.7, bus freq 2500000
[    2.527100] libphy: 24200f00.mdio: probed
[    2.532491] davinci_mdio 24200f00.mdio: phy[0]: device 24200f00.mdio:00, driver Marvell 88E151
0
[    2.541226] davinci_mdio 24200f00.mdio: phy[1]: device 24200f00.mdio:01, driver Marvell 88E151
0
[    5.562972] netcp-1.0 2620110.netcp: initialized cpsw ale version 1.4
[    5.569438] netcp-1.0 2620110.netcp: ALE Table size 8192
[    5.575655] netcp-1.0 2620110.netcp: module(netcp-xgbe) not used for device
[    5.582745] keystone-usbphy 2620738.usb_phy: 2620738.usb_phy supply vcc not found, using dummy
 regulator
[    5.592298] keystone-usbphy 2620738.usb_phy: Linked as a consumer to regulator.0
[    5.599838] keystone-usbphy 2620750.usb_phy: 2620750.usb_phy supply vcc not found, using dummy
 regulator
[    5.609373] keystone-usbphy 2620750.usb_phy: Linked as a consumer to regulator.0
[    5.617660] dwc3 2690000.dwc3: Failed to get clk 'ref': -2
[    5.623368] platform xhci-hcd.0.auto: set dma_pfn_offset00780000
[    5.629914] dwc3 25010000.dwc3: Failed to get clk 'ref': -2
[    5.635527] dwc3 25010000.dwc3: Configuration mismatch. dr_mode forced to host
[    5.642865] platform xhci-hcd.1.auto: set dma_pfn_offset00780000
[    5.649910] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
[    5.655535] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 1
[    5.663397] xhci-hcd xhci-hcd.0.auto: hcc params 0x0298f06d hci version 0x100 quirks 0x0000000
002010010
[    5.672833] xhci-hcd xhci-hcd.0.auto: irq 35, io mem 0x02690000
[    5.679005] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 4.19
[    5.687302] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[    5.694551] usb usb1: Product: xHCI Host Controller
[    5.699447] usb usb1: Manufacturer: Linux 4.19.94+ xhci-hcd
[    5.705029] usb usb1: SerialNumber: xhci-hcd.0.auto
[    5.710261] hub 1-0:1.0: USB hub found
[    5.714035] hub 1-0:1.0: 1 port detected
[    5.718227] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
[    5.723862] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 2
[    5.731553] xhci-hcd xhci-hcd.0.auto: Host supports USB 3.0 SuperSpeed
[    5.738136] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM.
[    5.746334] usb usb2: New USB device found, idVendor=1d6b, idProduct=0003, bcdDevice= 4.19
[    5.754628] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[    5.761876] usb usb2: Product: xHCI Host Controller
[    5.766763] usb usb2: Manufacturer: Linux 4.19.94+ xhci-hcd
[    5.772355] usb usb2: SerialNumber: xhci-hcd.0.auto
[    5.777559] hub 2-0:1.0: USB hub found
[    5.781351] hub 2-0:1.0: 1 port detected
[    5.785623] xhci-hcd xhci-hcd.1.auto: xHCI Host Controller
[    5.791258] xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus number 3
[    5.799099] xhci-hcd xhci-hcd.1.auto: hcc params 0x0298f06d hci version 0x100 quirks 0x0000000
002010010
[    5.808534] xhci-hcd xhci-hcd.1.auto: irq 69, io mem 0x25010000
[    5.814699] usb usb3: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 4.19
[    5.823064] usb usb3: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[    5.830315] usb usb3: Product: xHCI Host Controller
[    5.835201] usb usb3: Manufacturer: Linux 4.19.94+ xhci-hcd
[    5.840795] usb usb3: SerialNumber: xhci-hcd.1.auto
[    5.846005] hub 3-0:1.0: USB hub found
[    5.849791] hub 3-0:1.0: 1 port detected
[    5.853974] xhci-hcd xhci-hcd.1.auto: xHCI Host Controller
[    5.859600] xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus number 4
[    5.867278] xhci-hcd xhci-hcd.1.auto: Host supports USB 3.0 SuperSpeed
[    5.873873] usb usb4: We don't know the algorithms for LPM for this host, disabling LPM.
[    5.882075] usb usb4: New USB device found, idVendor=1d6b, idProduct=0003, bcdDevice= 4.19
[    5.890442] usb usb4: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[    5.897680] usb usb4: Product: xHCI Host Controller
[    5.902578] usb usb4: Manufacturer: Linux 4.19.94+ xhci-hcd
[    5.908161] usb usb4: SerialNumber: xhci-hcd.1.auto
[    5.913373] hub 4-0:1.0: USB hub found
[    5.917146] hub 4-0:1.0: 1 port detected
[    5.921537] usbcore: registered new interface driver usb-storage
[    5.927711] i2c /dev entries driver
[    5.932298] davinci-wdt 22f0080.wdt: heartbeat 60 sec
[    5.938086] sdhci: Secure Digital Host Controller Interface driver
[    5.944292] sdhci: Copyright(c) Pierre Ossman
[    5.948792] sdhci-pltfm: SDHCI platform and OF driver helper
[    5.954763] ledtrig-cpu: registered to indicate activity on CPUs
[    5.961435] usbcore: registered new interface driver usbhid
[    5.967018] usbhid: USB HID core driver
[    5.971670] nand: device found, Manufacturer ID: 0x2c, Chip ID: 0xac
[    5.978038] nand: Micron MT29F4G08ABBDAH4
[    5.982066] nand: 512 MiB, SLC, erase size: 128 KiB, page size: 2048, OOB size: 64
[    5.989934] Bad block table found at page 262080, version 0x01
[    5.996236] Bad block table found at page 262016, version 0x01
[    6.002375] 3 fixed-partitions partitions found on MTD device 30000000.nand
[    6.009350] Creating 3 MTD partitions on "30000000.nand":
[    6.014774] 0x000000000000-0x000000100000 : "u-boot"
[    6.020399] 0x000000100000-0x000000180000 : "params"
[    6.025957] 0x000000180000-0x000020000000 : "ubifs"
[    6.034677] davinci_nand 30000000.nand: controller rev. 2.5
[    6.040567] platform oprofile-perf.0: set dma_pfn_offset00780000
[    6.046903] oprofile: using timer interrupt.
[    6.051809] ipip: IPv4 and MPLS over IPv4 tunneling driver
[    6.057655] gre: GRE over IPv4 demultiplexor driver
[    6.062555] ip_gre: GRE over IPv4 tunneling driver
[    6.068470] ipt_CLUSTERIP: ClusterIP Version 0.8 loaded successfully
[    6.074904] Initializing XFRM netlink socket
[    6.079417] (NULL net_device): Link is Down
[    6.083609] (NULL net_device): Link is Down
[    6.087797] (NULL net_device): Link is Down
[    6.091994] (NULL net_device): Link is Down
[    6.096183] (NULL net_device): Link is Down
[    6.100380] (NULL net_device): Link is Down
[    6.105112] NET: Registered protocol family 10
[    6.110451] Segment Routing with IPv6
[    6.114174] NET: Registered protocol family 17
[    6.118634] NET: Registered protocol family 15
[    6.123099] 8021q: 802.1Q VLAN Support v1.8
[    6.127322] sctp: Hash tables configured (bind 512/512)
[    6.132886] Registering SWP/SWPB emulation handler
[    6.262006] netcp-1.0 2620110.netcp eth0: Link is Down
[    6.283144] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
[    6.289003] 8021q: adding VLAN 0 to HW filter on device eth0
[    8.490471] netcp-1.0 2620110.netcp eth0: Link is Up - 100Mbps/Full - flow control rx/tx
[    8.509431] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
[    8.549472] IP-Config: Complete:
[    8.552707]      device=eth0, hwaddr=b4:99:4c:09:60:58, ipaddr=10.10.10.171, mask=255.255.255.
0, gw=10.10.10.1
[    8.562770]      host=k2e-evm-2, domain=, nis-domain=(none)
[    8.568354]      bootserver=10.10.10.196, rootserver=10.10.10.196, rootpath=
[    8.568356]      nameserver0=10.10.10.1
[    8.607514] VFS: Mounted root (nfs filesystem) on device 0:14.
[    8.614003] devtmpfs: mounted
[    8.617918] Freeing unused kernel memory: 2048K
[    8.622573] Run /sbin/init as init process
[    8.640641] random: fast init done
Starting rsyslogd: OK
Running sysctl: OK
Populating /dev using udev: done
Initializing random number generator: OK
Saving random seed: OK
Starting rngd: OK
Starting system message bus: done
Starting NetworkManager ... done.
Starting dropbear sshd: OK
Starting DHCP server: FAIL
Starting domain name daemon: OK


CCM READY!

当我尝试使用 ethtool 启用内部起搏时,我得到以下错误:

eth0      Link encap:Ethernet  HWaddr B4:99:4C:09:60:58  
          inet addr:10.10.10.171  Bcast:10.10.10.255  Mask:255.255.255.0
          UP BROADCAST RUNNING MULTICAST  MTU:1500  Metric:1
          RX packets:21241 errors:0 dropped:0 overruns:0 frame:0
          TX packets:16892 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:1000 
          RX bytes:26824035 (25.5 MiB)  TX bytes:2207426 (2.1 MiB)

eth125    Link encap:Ethernet  HWaddr 02:18:31:7E:3E:00  
          UP BROADCAST MULTICAST  MTU:1500  Metric:1
          RX packets:0 errors:0 dropped:0 overruns:0 frame:0
          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:1000 
          RX bytes:0 (0.0 B)  TX bytes:0 (0.0 B)

lo        Link encap:Local Loopback  
          inet addr:127.0.0.1  Mask:255.0.0.0
          UP LOOPBACK RUNNING  MTU:65536  Metric:1
          RX packets:2 errors:0 dropped:0 overruns:0 frame:0
          TX packets:2 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:1000 
          RX bytes:58 (58.0 B)  TX bytes:58 (58.0 B)

root@ccm:~# ./ethtool -C eth0 rx-usecs 50
Cannot get device coalesce settings: Operation not supported

我还在使用  Switch Config Commands 示例工具时遇到了一个问题。

Scanning dependencies of target cpsw-ioctl
[100%] Building C object cpsw-ioctl/CMakeFiles/cpsw-ioctl.dir/src/cpsw-ioctl.c.o
cpsw-ioctl/src/cpsw-ioctl.c: In function ‘main’:
cpsw-ioctl/src/cpsw-ioctl.c:73:23: error: ‘SIOCSWITCHCONFIG’ undeclared (first use in this function); did you mean ‘TIOCSERCONFIG’?
     if (ioctl(sockfd, SIOCSWITCHCONFIG, &ifr) < 0) {
                       ^~~~~~~~~~~~~~~~
                       TIOCSERCONFIG
cpsw-ioctl/src/cpsw-ioctl.c:73:23: note: each undeclared identifier is reported only once for each function it appears in

  1.    在 menuconfig 中启用时是否充分支持 TI CPSW 交换机和802.1Q VLAN、或者我需要做更多的事情来启用交换机?
  2. 是否需要更改默认器件树? 有什么我可以使用的例子吗?
  3. 是否有任何可以使用的开关配置命令工具?

如果您需要任何进一步的信息、请告诉我。

此致、

Konstantinos。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Konstantinos,

    Rajarajan 正在处理您的查询。

    他会尽快提出建议。

    感谢您的耐心等待。

    此致

    Shankari G

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Konstantinos:

    感谢您的耐心等待、

    当我尝试使用 ethtool 启用内部起搏时,我得到以下错误:

    [/报价]

    默认情况下不执行"中断定步"。 Linux CPSW 驱动程序中的实现可视为参考"drivers/net/Ethernet/ti/cpsw.c"。  请注意、 由于15.e2e.ti.com/.../0513.sprz360i.pdf 页上的器件勘误表"Advisory 1.0.9"、CPSW 中断不直接支持中断节奏

    K2E 的默认配置如下所示:"${SDK 文件夹}/board-support/linux-4.19.94-{COMMITID}/arch/arm/config/tisdk_k2e-evm_defconfig "

    CONFIG_TI_CPSW_ALE=y

    但是、我们可以添加 CPSW 配置、

    CONFIG_TI_CPSW_PHY_SEL=y
    CONFIG_TI_CPSW_ALE=y
    CONFIG_TI_CPSW=y

    并发出以下命令

    //export the compiler path
    export PATH=<sdk path>/linux-devkit/sysroots/x86_64-arago-linux/usr/bin:$PATH
    
    //copy def config to .config file
    make ARCH=arm CROSS_COMPILE=arm-linux-gnueabihf- tisdk_k2e-evm_defconfig
    
    //compile using .config file into zImage
    make ARCH=arm CROSS_COMPILE=arm-linux-gnueabihf- zImage
    
    

    加载 zImage 后、提供以下命令、以验证驱动程序中是否包含 CPSW 配置。

    zcat /proc/config.gz | grep CPSW

    只有这样、"ethtool"才能调用"${SDK 文件夹}/board-support/linux-4.19.94-{COMMITID}/drivers/net/ethernet/ti/cpsw.c "中的"cpsw_set_coalesce ()"。

    我认为 K2E 的 NIC 不会禁用"Interrupt Pacing"。 我将尝试并行执行这些步骤并进行更新。 请进行这些更改并提供您的反馈。

    谢谢。

    Rajarajan U

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Rajarajan:

    我遵照了您的建议、现在全部"CONFIG_TI_CPSW_..." 一个实数特征。

    我尝试过 zcat /proc/config.gz | grep CPSW

    并获得:

    CONFIG_TI_CPSW_PHY_SEL=y
    CONFIG_TI_CPSW_ALE=y
    CONFIG_TI_CPSW=y

     

    遗憾的是 ethtool 仍然 无法正常工作。

    有什么我失踪了吗?  

    谢谢!

    Konstantinos Ilias.

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Konstantinos:

    我将查看我的 EVM 并提供更新。

    谢谢

    Rajarajan U

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Rajarajan 先生、您有任何更新吗?  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Konstantinos:

    我还没有完成另一项任务,我将在2-3天后继续研究这一问题。

    谢谢。

    Rajarajan U

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Rajarajan 先生

    我还面临配置的 ioctl 部分的问题。

    我设法编译它,使它工作,但我得到 操作不受支持 每次都要尝试  ioctl (sockfd、SIOCSWTCHCONFIG、&IFR) ;命令  

    您对此也有任何意见吗,您是否需要进一步的信息?  

    我在下面添加了代码。

    #include <stdio.h>
    #include <stdlib.h>
    #include <unistd.h>
    #include <string.h>
    #include <sys/types.h>
    #include <sys/socket.h>
    #include <arpa/inet.h>
    #include <netinet/in.h>
    #include <netdb.h>
    #include <sys/ioctl.h>
    #include <net/if.h>
    
    #include <stdio.h>
    #include <asm/sockios.h>
    #include <net/if.h>
    #include <string.h>
    #include <linux/sockios.h>
    #include <errno.h>
    
    #include "net_switch_config.h"
    
    
    
    int main(void)
    {
        struct net_switch_config cmd_struct;
        struct ifreq ifr;
        int sockfd;
        int16_t retVal =-100;
    
        strncpy(ifr.ifr_name, "eth0", IFNAMSIZ);
    
        ifr.ifr_data = (char*)&cmd_struct;
    
        if ((sockfd = socket(AF_INET, SOCK_DGRAM, 0)) < 0) {
            printf("[IDE:]Can't open the socket\n");
            return -1;
        }
        else{
            printf("[IDE:]socket openeed sucesfully \n");
        }
    
        memset(&cmd_struct, 0, sizeof(struct net_switch_config));
    
        //...//initialise cmd_struct with switch commands
    
        cmd_struct.cmd = CONFIG_SWITCH_GET_PORT_CONFIG;
    
        ifr.ifr_data = (char*)&cmd_struct;
    
        retVal = ioctl(sockfd, SIOCSWITCHCONFIG, &ifr);
    
        if (retVal < 0) {
            printf("Command CONFIG_SWITCH_GET_PORT_CONFIG port =0 failed\n");
    
            perror("retVal");
    
            close(sockfd);
    
            return -1;
        }
        else{
            printf("Command CONFIG_SWITCH_GET_PORT_CONFIG port =0 Succeeded\n");
        }
    
        printf("command success\n");
        close(sockfd);
        return 0;
    }
    
    

    我期待您的回复。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Konstantinos:

    我将查看" ioctl "行动,然后回到你的身边。

    谢谢。

    Rajarajan U

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Konstantinos:

    我认为这可能是内核中的一个错误、在以下 Git 页面中报告了该错误:

    git.ti.com/.../

    此修复程序已包含在 ti-linux 内核5.10中、SDK Linux 附带的内核版本为"4.19.94"。 请尝试此版本的内核并提供您的更新。

    我设法编译它,使它工作,但我得到 操作不受支持 每次都要尝试  ioctl (sockfd、SIOCSWTCHCONFIG、&IFR) ;命令  

    [/报价]

    我相信是因为内核问题," ioctl "无法允许设备控制 以太网端口。

    谢谢。

    Rajarajan U

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Rajarajan 先生

    感谢您的回复,我已经做了一个测试从内核5.10到4.19移植一些文件,但它没有修复我的问题,我将尝试内核5.10并给你一个反馈.  

    现在我最大的问题与器件树有关。  

    我没有找到任何使用器件树将 netcp 配置为开关的示例。

    keystone-k2e-netcp.dtsi

    // SPDX-License-Identifier: GPL-2.0
    /*
     * Device Tree Source for Keystone 2 Edison Netcp driver
     *
     * Copyright (C) 2015-2017 Texas Instruments Incorporated - http://www.ti.com/
     */
    
    qmss: qmss@2a40000 {
    	compatible = "ti,keystone-navigator-qmss";
    	dma-coherent;
    	#address-cells = <1>;
    	#size-cells = <1>;
    	clocks = <&chipclk13>;
    	ranges;
    	queue-range	= <0 0x2000>;
    	linkram0	= <0x100000 0x4000>;
    	linkram1	= <0 0x10000>;
    
    	qmgrs {
    		#address-cells = <1>;
    		#size-cells = <1>;
    		ranges;
    		qmgr0 {
    			managed-queues = <0 0x2000>;
    			reg = <0x2a40000 0x20000>,
    			      <0x2a06000 0x400>,
    			      <0x2a02000 0x1000>,
    			      <0x2a03000 0x1000>,
    			      <0x23a80000 0x20000>,
    			      <0x2a80000 0x20000>;
    			reg-names = "peek", "status", "config",
    				    "region", "push", "pop";
    		};
    	};
    	queue-pools {
    		qpend {
    			qpend-0 {
    				qrange = <658 8>;
    				interrupts =<0 40 0xf04 0 41 0xf04 0 42 0xf04
    					     0 43 0xf04 0 44 0xf04 0 45 0xf04
    					     0 46 0xf04 0 47 0xf04>;
    			};
    			qpend-1 {
    				qrange = <528 16>;
    				interrupts = <0 48 0xf04 0 49 0xf04 0 50 0xf04
    					      0 51 0xf04 0 52 0xf04 0 53 0xf04
    					      0 54 0xf04 0 55 0xf04 0 56 0xf04
    					      0 57 0xf04 0 58 0xf04 0 59 0xf04
    					      0 60 0xf04 0 61 0xf04 0 62 0xf04
    					      0 63 0xf04>;
    				qalloc-by-id;
    			};
    			qpend-2 {
    				qrange = <544 16>;
    				interrupts = <0 64 0xf04 0 65 0xf04 0 66 0xf04
    					      0 59 0xf04 0 68 0xf04 0 69 0xf04
    					      0 70 0xf04 0 71 0xf04 0 72 0xf04
    					      0 73 0xf04 0 74 0xf04 0 75 0xf04
    					      0 76 0xf04 0 77 0xf04 0 78 0xf04
    					      0 79 0xf04>;
    			};
    		};
    		general-purpose {
    			gp-0 {
    				qrange = <4000 64>;
    			};
    			netcp-tx {
    				qrange = <896 128>;
    				qalloc-by-id;
    			};
    		};
    		accumulator {
    			acc-low-0 {
    				qrange = <480 32>;
    				accumulator = <0 47 16 2 50>;
    				interrupts = <0 226 0xf01>;
    				multi-queue;
    				qalloc-by-id;
    			};
    		};
    	};
    
    	descriptor-regions {
    		#address-cells = <1>;
    		#size-cells = <1>;
    		ranges;
    		region-12 {
    			id = <12>;
    			region-spec = <8192 128>;	/* num_desc desc_size */
    			link-index = <0x4000>;
    		};
    	};
    
    	pdsps {
    		#address-cells = <1>;
    		#size-cells = <1>;
    		ranges;
    		pdsp0@2a10000 {
    			reg = <0x2a10000 0x1000    /*iram */
    			       0x2a0f000 0x100     /*reg*/
    			       0x2a0c000 0x3c8	   /*intd */
    			       0x2a20000 0x4000>;  /*cmd*/
    			id = <0>;
    		};
    	};
    }; /* qmss */
    
    knav_dmas: knav_dmas@0 {
    	compatible = "ti,keystone-navigator-dma";
    	clocks = <&papllclk>;
    	#address-cells = <1>;
    	#size-cells = <1>;
    	ranges;
    	ti,navigator-cloud-address = <0x23a80000 0x23a90000
    				 0x23a80000 0x23a90000>;
    
    	dma_gbe: dma_gbe@0 {
    		reg = <0x24186000 0x100>,
    			  <0x24187000 0x2a0>,
    			  <0x24188000 0xb60>,
    			  <0x24186100 0x80>,
    			  <0x24189000 0x1000>;
    		reg-names = "global", "txchan", "rxchan",
    				"txsched", "rxflow";
    		ti,enable-all;
    	};
    };
    
    gbe_subsys: subsys@24200000 {
    	compatible = "syscon";
    	reg = <0x24200000 0x100>;
    };
    
    gbe_serdes0: phy@232a000 {
    	compatible		= "ti,keystone-serdes-gbe";
    	reg			= <0x0232a000 0x2000>;
    	status			= "disabled";
    	link-rate-kbps		= <1250000>;
    	num-lanes		= <4>;
    	#address-cells	= <1>;
    	#size-cells	= <0>;
    
    	serdes0_lane0: lane@0 {
    		#phy-cells	= <0>;
    		reg		= <0>;
    		status		= "ok";
    		control-rate	= <2>;
    		rx-start	= <7 5>;
    		rx-force	= <1 1>;
    		tx-coeff	= <0 0 0 12 4>;
    	};
    	serdes0_lane1: lane@1 {
    		#phy-cells	= <0>;
    		reg		= <1>;
    		status		= "ok";
    		control-rate	= <2>;
    		rx-start	= <7 5>;
    		rx-force	= <1 1>;
    		tx-coeff	= <0 0 0 12 4>;
    	};
    	serdes0_lane2: lane@2 {
    		#phy-cells	= <0>;
    		reg		= <2>;
    		status		= "disabled";
    		control-rate	= <2>;
    		rx-start	= <7 5>;
    		rx-force	= <1 1>;
    		tx-coeff	= <0 0 0 12 4>;
    	};
    	serdes0_lane3: lane@3 {
    		#phy-cells	= <0>;
    		reg		= <3>;
    		status		= "disabled";
    		control-rate	= <2>;
    		rx-start	= <7 5>;
    		rx-force	= <1 1>;
    		tx-coeff	= <0 0 0 12 4>;
    	};
    };
    
    gbe_serdes1: phy@2324000 {
    	compatible		= "ti,keystone-serdes-gbe";
    	reg			= <0x02324000 0x2000>;
    	status			= "disabled";
    	link-rate-kbps		= <1250000>;
    	num-lanes		= <4>;
    	#address-cells	= <1>;
    	#size-cells	= <0>;
    
    	serdes1_lane0: lane@0 {
    		#phy-cells	= <0>;
    		reg		= <0>;
    		status		= "disabled";
    		control-rate	= <2>;
    		rx-start	= <7 5>;
    		rx-force	= <1 1>;
    		tx-coeff	= <0 0 0 12 4>;
    	};
    	serdes1_lane1: lane@1 {
    		#phy-cells	= <0>;
    		reg		= <1>;
    		status		= "disabled";
    		control-rate	= <2>;
    		rx-start	= <7 5>;
    		rx-force	= <1 1>;
    		tx-coeff	= <0 0 0 12 4>;
    	};
    	serdes1_lane2: lane@2 {
    		#phy-cells	= <0>;
    		reg		= <2>;
    		status		= "disabled";
    		control-rate	= <2>;
    		rx-start	= <7 5>;
    		rx-force	= <1 1>;
    		tx-coeff	= <0 0 0 12 4>;
    	};
    	serdes1_lane3: lane@3 {
    		#phy-cells	= <0>;
    		reg		= <3>;
    		status		= "disabled";
    		control-rate	= <2>;
    		rx-start	= <7 5>;
    		rx-force	= <1 1>;
    		tx-coeff	= <0 0 0 12 4>;
    	};
    };
    
    netcp: netcp@24000000 {
    	reg = <0x2620110 0x8>;
    	reg-names = "efuse";
    	compatible = "ti,cpsw", "ti,netcp-1.0";
    	#address-cells = <1>;
    	#size-cells = <1>;
    
    	/* NetCP address range */
    	ranges = <0 0x24000000 0x1000000>;
    
    	clocks = <&clkpa>, <&clkcpgmac>, <&chipclk12>;
    	/*clock-names = "pa_clk", "ethss_clk", "cpts";*/
    	clock-names = "fck", "ethss_clk", "cpts";
    
    	dma-coherent;
    
    	ti,navigator-dmas = <&dma_gbe 0>,
    			<&dma_gbe 8>,
    			<&dma_gbe 0>;
    	ti,navigator-dma-names = "netrx0", "netrx1", "nettx";
    
    	slaves = <2>;
    	active_slave = <0>;
    	cpdma_channels = <8>;
    	ale_entries = <1024>;	
    	mac_control = <0x20>;
    	bd_ram_size = <0x2000>;
    
    	netcp-devices {
    		#address-cells = <1>;
    		#size-cells = <1>;
    		ranges;
    		gbe@200000 { /* ETHSS */
    			label = "netcp-gbe";
    			/*compatible = "ti,netcp-gbe-9", "ti,cpsw";*/
    			compatible = "ti,netcp-xgbe";
    			syscon-subsys = <&gbe_subsys>;
    			reg = <0x200100 0x800>, <0x220000 0x20000>;
    			tx-queue = <896>;
    			tx-channel = "nettx";
    
    			interfaces {
    				gbe0: interface-0 {
    					phys		= <&serdes0_lane0>;
    					slave-port	= <0>;
    					link-interface	= <1>;
    					phy-handle	= <&ethphy0>;
    				};
    				gbe1: interface-1 {
    					phys		= <&serdes0_lane1>;
    					slave-port	= <1>;
    					link-interface	= <1>;
    					phy-handle	= <&ethphy1>;
    				};
    			};
    
    			secondary-slave-ports {
    				port-2 {
    					phys = <&serdes0_lane2>;
    					slave-port = <2>;
    					link-interface	= <2>;
    				};
    				port-3 {
    					phys = <&serdes0_lane3>;
    					slave-port = <3>;
    					link-interface	= <2>;
    				};
    				port-4 {
    					phys = <&serdes1_lane0>;
    					slave-port = <4>;
    					link-interface	= <2>;
    				};
    				port-5 {
    					phys = <&serdes1_lane1>;
    					slave-port = <5>;
    					link-interface	= <2>;
    				};
    				port-6 {
    					phys = <&serdes1_lane2>;
    					slave-port = <6>;
    					link-interface	= <2>;
    				};
    				port-7 {
    					phys = <&serdes1_lane3>;
    					slave-port = <7>;
    					link-interface	= <2>;
    				};
    			};
    		};
    	};
    
    	netcp-interfaces {
    		interface-0 {
    			rx-channel = "netrx0";
    			rx-pool = <1024 12>;
    			tx-pool = <1024 12>;
    			rx-queue-depth = <128 128 0 0>;
    			rx-buffer-size = <1518 4096 0 0>;
    			rx-queue = <528>;
    			tx-completion-queue = <530>;
    			efuse-mac = <1>;
    			netcp-gbe = <&gbe0>;
    
    		};
    		interface-1 {
    			rx-channel = "netrx1";
    			rx-pool = <1024 12>;
    			tx-pool = <1024 12>;
    			rx-queue-depth = <128 128 0 0>;
    			rx-buffer-size = <1518 4096 0 0>;
    			rx-queue = <529>;
    			tx-completion-queue = <531>;
    			efuse-mac = <0>;
    			local-mac-address = [02 18 31 7e 3e 00];
    			netcp-gbe = <&gbe1>;
    		};
    	};
    };
    
    sa_subsys: subsys@24080000 {
    	#address-cells = <1>;
    	#size-cells = <1>;
    	compatible = "simple-bus";
    	ranges = <0 0x24080000 0x40000>;
    
    	sa_config: subsys@0 {
    		compatible = "syscon";
    		reg = <0x0 0x100>;
    	};
    
    	rng@24000 {
    		compatible = "ti,keystone-rng";
    		reg = <0x24000 0x1000>;
    		ti,syscon-sa-cfg = <&sa_config>;
    		clocks = <&clksa>;
    		clock-names = "fck";
    	};
    };
    
    

    内核日志

    U-Boot SPL 2019.01-g333c3e72d3 (Apr 19 2020 - 06:29:23 +0000)
    Trying to boot from SPI
    
    
    U-Boot 2019.01-g333c3e72d3 (Apr 19 2020 - 06:29:23 +0000)
    
    CPU: 66AK2Ex SR1.0
    Model: Texas Instruments Keystone 2 Edison EVM
    DRAM:  DDR3A Speed will be configured for 1600 Operation.
    Detected SO-DIMM [18KSF51272HZ-1G6K2]
    DDR3 speed 1600
    DRAM: 4 GiB
    
    Clear entire DDR3 memory to enable ECC
    2 GiB
    NAND:  512 MiB
    Loading Environment from NAND... OK
    Net:   eth0: netcp@24000000
    Warning: netcp@slave-1 (eth1) using random MAC address - 5a:91:34:bb:df:83
    , eth1: netcp@slave-1
    Warning: netcp@slave-2 (eth2) using random MAC address - 92:41:d8:ec:c1:81
    , eth2: netcp@slave-2
    Warning: netcp@slave-3 (eth3) using random MAC address - 3e:06:ee:16:60:ba
    , eth3: netcp@slave-3
    Warning: netcp@slave-4 (eth4) using random MAC address - 7e:d5:42:83:ab:59
    , eth4: netcp@slave-4
    Warning: netcp@slave-5 (eth5) using random MAC address - 5e:9e:59:0f:b2:09
    , eth5: netcp@slave-5
    Warning: netcp@slave-6 (eth6) using random MAC address - 9e:46:9c:22:20:07
    , eth6: netcp@slave-6
    Warning: netcp@slave-7 (eth7) using random MAC address - fe:0f:05:a8:23:74
    , eth7: netcp@slave-7
    Hit any key to stop autoboot:  0 
    
    netcp@24000000 Waiting for SGMII auto negotiation to complete. done
    Using netcp@24000000 device
    File transfer via NFS from server 10.10.10.196; our IP address is 10.10.10.171
    Filename '/srv/nfsCCM/boot/skern-k2e.bin'.
    Load address: 0x87000000
    Loading: #######
    done
    Bytes transferred = 32832 (8040 hex)
    K2_BM_15.07-53-ge1f885ab6dc5 SoC:k2e built:12:42:37, Jul  2 2020
                                                                    
    ## installed monitor @ 0xc1f0000, freq [233333333], status 203358208
    
    netcp@24000000 Waiting for SGMII auto negotiation to complete. done
    Using netcp@24000000 device
    File transfer via NFS from server 10.10.10.196; our IP address is 10.10.10.171
    Filename '/srv/nfsCCM/boot/zImage'.
    Load address: 0x82000000
    Loading: #################################################################
             #################################################################
             #################################################################
             #################################################################
             #################################################################
             #################################################################
             #################################################################
             #################################################################
             #################################################################
             #################################################################
             #################################################################
             #################################################################
             #################################################################
             ########################################################
    done
    Bytes transferred = 4612608 (466200 hex)
    
    netcp@24000000 Waiting for SGMII auto negotiation to complete. done
    Using netcp@24000000 device
    File transfer via NFS from server 10.10.10.196; our IP address is 10.10.10.171
    Filename '/srv/nfsCCM/boot/k2-fw-initrd.cpio.gz'.
    Load address: 0x88080000
    Loading: #############
    done
    Bytes transferred = 65096 (fe48 hex)
    
    netcp@24000000 Waiting for SGMII auto negotiation to complete. done
    Using netcp@24000000 device
    File transfer via NFS from server 10.10.10.196; our IP address is 10.10.10.171
    Filename '/srv/nfsCCM/boot/keystone-k2e-evm.dtb'.
    Load address: 0x88000000
    Loading: ######
    done
    Bytes transferred = 27242 (6a6a hex)
    ## Flattened Device Tree blob at 88000000
       Booting using the fdt blob at 0x88000000
       Loading Ramdisk to 8fff0000, end 8ffffe48 ... OK
       Loading Device Tree to 8ffe6000, end 8ffefa69 ... OK
    
    Starting kernel ...
    
    [    0.000000] Booting Linux on physical CPU 0x0
    [    0.000000] Linux version 4.19.94+ (ide@tmssrv) (gcc version 8.4.0 (Buildroot 2020.11.1)) #1 SMP PRE
    EMPT Wed Feb 1 14:44:27 EET 2023
    [    0.000000] CPU: ARMv7 Processor [412fc0f4] revision 4 (ARMv7), cr=30c5387d
    [    0.000000] CPU: div instructions available: patching division code
    [    0.000000] CPU: PIPT / VIPT nonaliasing data cache, PIPT instruction cache
    [    0.000000] OF: fdt: Machine model: Texas Instruments Keystone 2 Edison EVM
    [    0.000000] Memory policy: Data cache writealloc
    [    0.000000] Switching physical address space to 0x800000000
    [    0.000000] efi: Getting EFI parameters from FDT:
    [    0.000000] efi: UEFI not found.
    [    0.000000] Reserved memory: created CMA memory pool at 0x000000081f800000, size 8 MiB
    [    0.000000] OF: reserved mem: initialized node dsp-common-memory@81f800000, compatible id shared-dma
    -pool
    [    0.000000] cma: Reserved 24 MiB at 0x000000087e400000
    [    0.000000] psci: probing for conduit method from DT.
    [    0.000000] psci: Using PSCI v0.1 Function IDs from DT
    [    0.000000] random: get_random_bytes called from start_kernel+0xb4/0x470 with crng_init=0
    [    0.000000] percpu: Embedded 15 pages/cpu s32396 r8192 d20852 u61440
    [    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 981888
    [    0.000000] Kernel command line: console=ttyS0,115200n8 rootwait=1 mtdparts=spi0.0:1m(u-boot-spl)ro,
    -(misc) rootfstype=nfs root=/dev/nfs rw nfsroot=/srv/nfsCCM,v3,tcp,rsize=4096,wsize=4096 ip=10.10.10.17
    1:10.10.10.196:10.10.10.1:255.255.255.0:k2e-evm-2:eth0:off:10.10.10.1 nfsrootdebug
    [    0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
    [    0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
    [    0.000000] Memory: 3846996K/3932160K available (10240K kernel code, 324K rwdata, 3000K rodata, 2048
    K init, 267K bss, 52396K reserved, 32768K cma-reserved, 3383296K highmem)
    [    0.000000] Virtual kernel memory layout:
    [    0.000000]     vector  : 0xffff0000 - 0xffff1000   (   4 kB)
    [    0.000000]     fixmap  : 0xffc00000 - 0xfff00000   (3072 kB)
    [    0.000000]     vmalloc : 0xe0800000 - 0xff800000   ( 496 MB)
    [    0.000000]     lowmem  : 0xc0000000 - 0xe0000000   ( 512 MB)
    [    0.000000]     pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)
    [    0.000000]     modules : 0xbf000000 - 0xbfe00000   (  14 MB)
    [    0.000000]       .text : 0x(ptrval) - 0x(ptrval)   (12256 kB)
    [    0.000000]       .init : 0x(ptrval) - 0x(ptrval)   (2048 kB)
    [    0.000000]       .data : 0x(ptrval) - 0x(ptrval)   ( 325 kB)
    [    0.000000]        .bss : 0x(ptrval) - 0x(ptrval)   ( 268 kB)
    [    0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
    [    0.000000] rcu: Preemptible hierarchical RCU implementation.
    [    0.000000] rcu:     RCU restricting CPUs from NR_CPUS=8 to nr_cpu_ids=4.
    [    0.000000]  Tasks RCU enabled.
    [    0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
    [    0.000000] NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16
    [    0.000000] GIC: Using split EOI/Deactivate mode
    [    0.000000] arch_timer: cp15 timer(s) running at 233.33MHz (phys).
    [    0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x6ba0ac50b7, max_idle
    _ns: 881590427583 ns
    [    0.000004] sched_clock: 56 bits at 233MHz, resolution 4ns, wraps every 4398046511102ns
    [    0.000013] Switching to timer-based delay loop, resolution 4ns
    [    0.000145] keystone timer clock @233333333 Hz
    [    0.000277] Console: colour dummy device 80x30
    [    0.000314] Calibrating delay loop (skipped), value calculated using timer frequency.. 466.66 BogoMI
    PS (lpj=2333333)
    [    0.000324] pid_max: default: 32768 minimum: 301
    [    0.000418] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)
    [    0.000427] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)
    [    0.000891] CPU: Testing write buffer coherency: ok
    [    0.000914] CPU0: Spectre v2: firmware did not set auxiliary control register IBE bit, system vulner
    able
    [    0.001106] /cpus/cpu@0 missing clock-frequency property
    [    0.001127] /cpus/cpu@1 missing clock-frequency property
    [    0.001146] /cpus/cpu@2 missing clock-frequency property
    [    0.001166] /cpus/cpu@3 missing clock-frequency property
    [    0.001175] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
    [    0.060033] Setting up static identity map for 0x80200000 - 0x80200138
    [    0.080038] rcu: Hierarchical SRCU implementation.
    [    0.100179] EFI services will not be available.
    [    0.120079] smp: Bringing up secondary CPUs ...
    [    0.204371] CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
    [    0.204376] CPU1: Spectre v2: firmware did not set auxiliary control register IBE bit, system vulner
    able
    [    0.284465] CPU2: thread -1, cpu 2, socket 0, mpidr 80000002
    [    0.284470] CPU2: Spectre v2: firmware did not set auxiliary control register IBE bit, system vulner
    able
    [    0.364564] CPU3: thread -1, cpu 3, socket 0, mpidr 80000003
    [    0.364569] CPU3: Spectre v2: firmware did not set auxiliary control register IBE bit, system vulner
    able
    [    0.364698] smp: Brought up 1 node, 4 CPUs
    [    0.364708] SMP: Total of 4 processors activated (1866.66 BogoMIPS).
    [    0.364715] CPU: All CPU(s) started in HYP mode.
    [    0.364721] CPU: Virtualization extensions available.
    [    0.365142] devtmpfs: initialized
    [    0.369253] VFP support v0.3: implementor 41 architecture 4 part 30 variant f rev 0
    [    0.369459] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 191126044627
    50000 ns
    [    0.369473] futex hash table entries: 1024 (order: 4, 65536 bytes)
    [    0.369937] pinctrl core: initialized pinctrl subsystem
    [    0.370286] DMI not present or invalid.
    [    0.370507] NET: Registered protocol family 16
    [    0.371352] DMA: preallocated 256 KiB pool for atomic coherent allocations
    [    0.372032] cpuidle: using governor ladder
    [    0.372060] cpuidle: using governor menu
    [    0.372189] No ATAGs?
    [    0.372274] hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.
    [    0.372284] hw-breakpoint: maximum watchpoint size is 8 bytes.
    [    0.386703] SCSI subsystem initialized
    [    0.387597] media: Linux media interface: v0.10
    [    0.387629] videodev: Linux video capture interface: v2.00
    [    0.387681] pps_core: LinuxPPS API ver. 1 registered
    [    0.387688] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
    [    0.387704] PTP clock support registered
    [    0.387726] EDAC MC: Ver: 3.0.0
    [    0.388370] Advanced Linux Sound Architecture Driver Initialized.
    [    0.388952] clocksource: Switched to clocksource arch_sys_counter
    [    0.394623] NET: Registered protocol family 2
    [    0.394998] tcp_listen_portaddr_hash hash table entries: 512 (order: 0, 6144 bytes)
    [    0.395019] TCP established hash table entries: 4096 (order: 2, 16384 bytes)
    [    0.395047] TCP bind hash table entries: 4096 (order: 3, 32768 bytes)
    [    0.395095] TCP: Hash tables configured (established 4096 bind 4096)
    [    0.395151] UDP hash table entries: 256 (order: 1, 8192 bytes)
    [    0.395168] UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)
    [    0.395307] NET: Registered protocol family 1
    [    0.395595] RPC: Registered named UNIX socket transport module.
    [    0.395603] RPC: Registered udp transport module.
    [    0.395609] RPC: Registered tcp transport module.
    [    0.395615] RPC: Registered tcp NFSv4.1 backchannel transport module.
    [    0.395744] Trying to unpack rootfs image as initramfs...
    [    0.399367] Freeing initrd memory: 64K
    [    0.399591] hw perfevents: no interrupt-affinity property for /pmu, guessing.
    [    0.399822] hw perfevents: enabled with armv7_cortex_a15 PMU driver, 7 counters available
    [    0.400178] platform alarmtimer: set dma_pfn_offset00780000
    [    0.400657] Initialise system trusted keyrings
    [    0.400756] workingset: timestamp_bits=14 max_order=20 bucket_order=6
    [    0.404681] squashfs: version 4.0 (2009/01/31) Phillip Lougher
    [    0.405034] NFS: Registering the id_resolver key type
    [    0.405049] Key type id_resolver registered
    [    0.405055] Key type id_legacy registered
    [    0.405083] ntfs: driver 2.1.32 [Flags: R/O].
    [    0.406336] Key type asymmetric registered
    [    0.406345] Asymmetric key parser 'x509' registered
    [    0.406378] bounce: pool size: 64 pages
    [    0.406402] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 245)
    [    0.406409] io scheduler noop registered
    [    0.406416] io scheduler deadline registered
    [    0.406493] io scheduler cfq registered (default)
    [    0.406501] io scheduler mq-deadline registered
    [    0.406508] io scheduler kyber registered
    [    0.406780] keystone_irq 26202a0.keystone_irq: irqchip registered, nr_irqs 28
    [    0.407296] ti,keystone-serdes 2326000.phy: init fw ks2_pcie_serdes.bin: version 3.3.0.2c
    [    0.408024] ti,keystone-serdes 232a000.phy: init fw ks2_gbe_serdes.bin: version 3.3.0.2c
    [    0.410521] keystone-pcie 21020000.pcie: host bridge /soc@0/pcie@21020000 ranges:
    [    0.410547] keystone-pcie 21020000.pcie:    IO 0x60000000..0x600fffff -> 0x00000000
    [    0.410565] keystone-pcie 21020000.pcie:   MEM 0x60100000..0x6fffffff -> 0x60100000
    [    0.511079] keystone-pcie 21020000.pcie: Link up
    [    0.511175] keystone-pcie 21020000.pcie: PCI host bridge to bus 0000:00
    [    0.511185] pci_bus 0000:00: root bus resource [bus 00-ff]
    [    0.511194] pci_bus 0000:00: root bus resource [io  0x0000-0xfffff]
    [    0.511202] pci_bus 0000:00: root bus resource [mem 0x60100000-0x6fffffff]
    [    0.512615] PCI: bus0: Fast back to back transfers disabled
    [    0.512857] pci 0000:01:00.0: Enabling fixed DMA alias to 00.1
    [    0.540164] PCI: bus1: Fast back to back transfers disabled
    [    0.540195] pci 0000:00:00.0: BAR 8: assigned [mem 0x60100000-0x601fffff]
    [    0.540206] pci 0000:00:00.0: BAR 9: assigned [mem 0x60200000-0x602fffff pref]
    [    0.540214] pci 0000:00:00.0: BAR 7: assigned [io  0x1000-0x1fff]
    [    0.540226] pci 0000:01:00.0: BAR 6: assigned [mem 0x60200000-0x6020ffff pref]
    [    0.540235] pci 0000:01:00.0: BAR 5: assigned [mem 0x60100000-0x601001ff]
    [    0.540247] pci 0000:01:00.0: BAR 4: assigned [io  0x1000-0x100f]
    [    0.540258] pci 0000:01:00.0: BAR 0: assigned [io  0x1010-0x1017]
    [    0.540270] pci 0000:01:00.0: BAR 2: assigned [io  0x1018-0x101f]
    [    0.540282] pci 0000:01:00.0: BAR 1: assigned [io  0x1020-0x1023]
    [    0.540293] pci 0000:01:00.0: BAR 3: assigned [io  0x1024-0x1027]
    [    0.540305] pci 0000:00:00.0: PCI bridge to [bus 01-ff]
    [    0.540313] pci 0000:00:00.0:   bridge window [io  0x1000-0x1fff]
    [    0.540322] pci 0000:00:00.0:   bridge window [mem 0x60100000-0x601fffff]
    [    0.540331] pci 0000:00:00.0:   bridge window [mem 0x60200000-0x602fffff pref]
    [    0.540443] pcieport 0000:00:00.0: limiting MRRS to 256
    [    0.540598] pcieport 0000:00:00.0: Signaling PME with IRQ 80
    [    0.540712] pcieport 0000:00:00.0: AER enabled with IRQ 80
    [    0.541695] keystone-navigator-qmss soc@0:qmss@2a40000: qmgr start queue 0, number of queues 8192
    [    0.541812] keystone-navigator-qmss soc@0:qmss@2a40000: added qmgr start queue 0, num of queues 8192
    , reg_peek (ptrval), reg_status (ptrval), reg_config (ptrval), reg_region (ptrval), reg_push (ptrval), 
    reg_pop (ptrval)
    [    0.541950] keystone-navigator-qmss soc@0:qmss@2a40000: firmware file ks2_qmss_pdsp_acc48.bin downlo
    aded for PDSP
    [    0.544384] keystone-navigator-dma soc@0:knav_dmas@0: DMA dma_gbe registered 149 logical channels, f
    lows 128, tx chans: 21, rx chans: 91
    [    0.578252] Serial: 8250/16550 driver, 10 ports, IRQ sharing enabled
    [    0.578305] platform serial8250: set dma_pfn_offset00780000
    [    0.580873] console [ttyS0] disabled
    [    0.580916] 2530c00.serial: ttyS0 at MMIO 0x2530c00 (irq = 27, base_baud = 14583333) is a TI DA8xx/6
    6AK2x
    [    1.619469] console [ttyS0] enabled
    [    1.623653] 2531000.serial: ttyS1 at MMIO 0x2531000 (irq = 28, base_baud = 14583333) is a TI DA8xx/6
    6AK2x
    [    1.642070] brd: module loaded
    [    1.650750] loop: module loaded
    [    1.655439] spi_davinci 21000400.spi: DMA is not supported (-19)
    [    1.662167] m25p80 spi0.0: n25q128a11 (16384 Kbytes)
    [    1.667148] 2 cmdlinepart partitions found on MTD device spi0.0
    [    1.673098] Creating 2 MTD partitions on "spi0.0":
    [    1.677902] 0x000000000000-0x000000100000 : "u-boot-spl"
    [    1.683787] 0x000000100000-0x000001000000 : "misc"
    [    1.689134] spi_davinci 21000400.spi: Controller at 0x(ptrval)
    [    1.695214] spi_davinci 21000600.spi: DMA is not supported (-19)
    [    1.701522] spi_davinci 21000600.spi: Controller at 0x(ptrval)
    [    1.707609] spi_davinci 21000800.spi: DMA is not supported (-19)
    [    1.713910] spi_davinci 21000800.spi: Controller at 0x(ptrval)
    [    1.720007] platform Fixed MDIO bus.0: set dma_pfn_offset00780000
    [    1.726263] libphy: Fixed MDIO Bus: probed
    [    1.788976] davinci_mdio 24200f00.mdio: davinci mdio revision 1.7, bus freq 2500000
    [    1.796650] libphy: 24200f00.mdio: probed
    [    1.802329] davinci_mdio 24200f00.mdio: phy[0]: device 24200f00.mdio:00, driver Marvell 88E1510
    [    1.811066] davinci_mdio 24200f00.mdio: phy[1]: device 24200f00.mdio:01, driver Marvell 88E1510
    [    1.820085] cpsw 2620110.netcp: Random MACID = 32:fd:6d:f8:03:56
    [    1.826125] cpsw 2620110.netcp: invalid resource
    [    1.830795] cpsw: probe of 2620110.netcp failed with error -22
    [    1.837037] netcp-1.0 2620110.netcp: initialized cpsw ale version 1.4
    [    1.843507] netcp-1.0 2620110.netcp: ALE Table size 8192
    [    1.848848] netcp-1.0 2620110.netcp: cpts: overflow check period 300 (jiffies)
    [    1.856109] netcp-1.0 2620110.netcp: CPTS: ref_clk_freq:700000000 calc_mult:3067833783 calc_shift:31
     error:0 nsec/sec
    [    1.867420] netcp-1.0 2620110.netcp: module(netcp-xgbe) not used for device
    [    1.874657] i2c /dev entries driver
    [    1.880065] sdhci: Secure Digital Host Controller Interface driver
    [    1.886257] sdhci: Copyright(c) Pierre Ossman
    [    1.890823] sdhci-pltfm: SDHCI platform and OF driver helper
    [    1.896988] ledtrig-cpu: registered to indicate activity on CPUs
    [    1.904486] nand: device found, Manufacturer ID: 0x2c, Chip ID: 0xac
    [    1.910871] nand: Micron MT29F4G08ABBDAH4
    [    1.914888] nand: 512 MiB, SLC, erase size: 128 KiB, page size: 2048, OOB size: 64
    [    1.922752] Bad block table found at page 262080, version 0x01
    [    1.929068] Bad block table found at page 262016, version 0x01
    [    1.935206] 3 fixed-partitions partitions found on MTD device 30000000.nand
    [    1.942196] Creating 3 MTD partitions on "30000000.nand":
    [    1.947607] 0x000000000000-0x000000100000 : "u-boot"
    [    1.953169] 0x000000100000-0x000000180000 : "params"
    [    1.958674] 0x000000180000-0x000020000000 : "ubifs"
    [    1.967226] davinci_nand 30000000.nand: controller rev. 2.5
    [    1.973286] platform snd-soc-dummy: set dma_pfn_offset00780000
    [    1.979971] NET: Registered protocol family 10
    [    1.985140] Segment Routing with IPv6
    [    1.988850] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
    [    1.995168] NET: Registered protocol family 17
    [    1.999731] Key type dns_resolver registered
    [    2.004149] Registering SWP/SWPB emulation handler
    [    2.009318] Loading compiled-in X.509 certificates
    [    2.017429] hctosys: unable to open rtc device (rtc0)
    [    2.141549] netcp-1.0 2620110.netcp eth0: Link is Down
    [    2.162898] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
    [    4.330043] netcp-1.0 2620110.netcp eth0: Link is Up - 100Mbps/Full - flow control rx/tx
    [    4.348982] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
    [    4.389033] IP-Config: Complete:
    [    4.392269]      device=eth0, hwaddr=b4:99:4c:09:60:58, ipaddr=10.10.10.171, mask=255.255.255.0, gw=
    10.10.10.1
    [    4.402310]      host=k2e-evm-2, domain=, nis-domain=(none)
    [    4.407895]      bootserver=10.10.10.196, rootserver=10.10.10.196, rootpath=
    [    4.407897]      nameserver0=10.10.10.1
    [    4.428106] ALSA device list:
    [    4.431093]   No soundcards found.
    [    4.456229] VFS: Mounted root (nfs filesystem) on device 0:14.
    [    4.462811] devtmpfs: mounted
    [    4.466737] Freeing unused kernel memory: 2048K
    [    4.471410] Run /sbin/init as init process
    [    4.489223] random: fast init done
    Starting rsyslogd: OK
    Running sysctl: OK
    Populating /dev using udev: done
    Initializing random number generator: OK
    Saving random seed: OK
    Starting rngd: OK
    Starting system message bus: done
    Starting network: ip: RTNETLINK answers: File exists
    FAIL
    Starting NetworkManager ... done.
    Starting dropbear sshd: OK
    Starting cron ... done.
    atd: created missing .SEQ file (atjobs will be lost on reboot)
    Starting atd: OK
    eth125
    ip: RTNETLINK answers: Operation not supported
    ip: RTNETLINK answers: Operation not supported
    ip: can't find device 'brLAN'
    ip: SIOCGIFFLAGS: No such device
    ip: SIOCGIFFLAGS: No such device
    ip: can't find device 'brLAN'
    Starting mosquitto: OK
    Starting DHCP server: FAIL
    Starting HPA's tftpd: done
    
    CCM READY!
    ccm.tmn1.lan login: 

    我的 netcp 设备树是否正确?  

    我为什么会得到

    cpsw:2620110.netcp 资源无效

    cpsw: 2620110.netcp 的探测器失败,错误-22

    谢谢你。

    Konstantinos

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Konstantinos:

    将分析您的器件树并发布我的响应。

    谢谢。

    Rajarajan U

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Konstantinos:

    我相信您一直在 Linux 上工作、在 TI-RTOS 内核上开发了一个 CPPI 工作示例项目、其使用与 CPSW 驱动程序相同的配置。

    若要验证配置、请查看代码以供参考。

    CPSW 配置位于以下文件中:ti\pdk_k2e_4_0_16\packages/ti\drv\cppi\device\k2e\src

    TI-RTOS SDK 链接

    https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1040858/faq-66ak2e05-how-to-generate-the-ccs-pdk-examples-for-k2e

    我正在进行 Netcp 驱动程序配置。 我会尽快回复。

    谢谢

    Rajarajan U

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Konstantinos:

    我已经浏览了 CPSW 开关文档、

    https://software-dl.ti.com/processor-sdk-linux/esd/docs/06_03_00_106/linux/Foundational_Components/Kernel/Kernel_Drivers/Network/CPSW.html

    请仔细研究一下。

    谢谢。

    Rajarajan U

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Rajarajan 先生

    我知道这份文档、这是我在上面开始的第一份文档。  

    另一方面、在 tisdk Linux kerne I 上、我找到了 描述端口绑定过程的"./Documentation/devicetree/bindings/net/keystone-netcp.txt "。

     

    我按照这些指令(更改 k2e 的寄存器)尝试了器件树配置、但未能在评估板中实现端口绑定。

     

    我的目标是将 k2e netcp 的所有8个端口配置为非网管交换机。

     

    我的问题是:

    • 如何修改设备树?  
    • 我是否需要任何进一步的配置(器件树除外)?
    • 用户空间中是否需要 ethtool 或其他工具?  

     

    你能给我一些关于它的帮助吗?

    此致、

    Konstantinos。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Konstantinos:

    我对设备树了解不多、但 对 内核专家进行了亲密接触。

    请查看 netcp 的参考设备树。

    https://kernel.googlesource.com/pub/scm/linux/kernel/git/next/linux-next/+/refs/heads/akpm-base/Documentation/devicetree/bindings/net/keystone-netcp.txt

    谢谢。

    Rajarajan U

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Rajaran:

    我是 Konstantinos 的 FAE。 我想知道 您是否能够在团队中询问我们是否对器件树有任何了解?

    此致、

    但以理

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    大家好!  

    我设法使其几乎用作正常开关。

    步骤:

    1) 1)在 menuconfig 中、我添加了与 CPSW 相关的值、并且802…… 模块。

    2) 2)我使用的器件树如中所示

    文档 "./Documentation/devicetree/bindings/net/keystone-netcp.txt "。

    3)然后我运行以下命令。

    1. echo "port0_unicast_flood=1">/sys/class/net/eth0/device/ale_control
    2. echo "BYPASS=0">/sys/class/net/eth0/device/ale_control
    3. echo "NO_PORT_VLAN=1">/sys/class/net/eth0/device/ale_control

    当前情况:

    +-------------------------------+			|-----------------------|
    |	K2e EVM                     |  			|Server					|
    |								|	   |----|ip 10.10.10.191		|
    |		 |----------------------|      |    |mask 255.255.255.0		|
    |		 |	eth0				| 	   |	|-----------------------|
    |		 |	ip 10.10.10.171		|------+      
    |		 |	mask 255.255.255.0	| 	
    |		 |----------------------|   
    |		                  		|   
    |		 |----------------------| 			|-----------------------|
    |		 |	eth1				|   		|laptop					|
    |		 | 						|-----------|ip 10.10.10.200		|
    |		 |----------------------|   		|mask 255.255.255.0		|
    +-------------------------------+			|-----------------------|

    • Server(10.10.10.191) ping Laptop(10.10.10.200)和 Laptop ping Server
    • Server(10.10.10.191) ping K2eEVM(10.10.10.171)和 K2eEVM ping Server
    • K2eEVM (10.10.10.171)无法 ping 通 Laptop (10.10.10.200)、Laptop 无法 ping 通 K2eEVM   

    我该如何解决此问题??

    我是否需要在 ALE_CONTROL 中回显更多内容?

    如果您需要任何进一步的信息、请告诉我。

    此致、

    Konstantinos