This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] 66AK2H06:适用于端口3和端口4的 CPSW 配置寄存器复位值(0x060606)和数据包 DMA 通道

Guru**** 2554750 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1232870/66ak2h06-cpsw-configuration-register-reset-value-0x06060606-and-packet-dma-channels-for-port-3-and-port-4

器件型号:66AK2H06

您好!

KeyStone 器件用户指南(SPRUGZ6)中的网络协处理器显示 CPSW 配置寄存器(CPSW_CFG_REG)的复位值为0x00000606、该值已链接到数据包 DMA 通道22和23。
66AK2Hxx 有4个以太网端口。 我想知道复位值是否为0x060606、另外两个端口的数据包 DMA 通道是什么? 24,25 ? 或者可以是20和21?

此致、
马西莫