This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] J721EXSOMXEVM:闪存问题

Guru**** 2558250 points
Other Parts Discussed in Thread: J721EXSOMXEVM

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1236625/j721exsomxevm-flash-issue

器件型号:J721EXSOMXEVM

大家好、

已参考 此文档 在 PC 端烧录 J721EXSOMXEVM 系统、但失败了。  在将系统刷写到 USB 闪存驱动器 SDK 时出现问题、日志如下所示:  

(base) ubuntu@ubuntu-QiTianM430-N000:~/work/TDA4$ sudo dpkg-reconfigure dash
Removing 'diversion of /bin/sh to /bin/sh.distrib by dash'
Adding 'diversion of /bin/sh to /bin/sh.distrib by bash'
Removing 'diversion of /usr/share/man/man1/sh.1.gz to /usr/share/man/man1/sh.distrib.1.gz by dash'
Adding 'diversion of /usr/share/man/man1/sh.1.gz to /usr/share/man/man1/sh.distrib.1.gz by bash'
(base) ubuntu@ubuntu-QiTianM430-N000:~/work/TDA4$ sudo /home/ubuntu/work/TDA4/ti-processor-sdk-linux-j7-evm-08_06_01_02/bin/mksdboot.sh --device /dev/sdb1 --sdk /home/ubuntu/work/TDA4/ti-processor-sdk-linux-j7-evm-08_06_01_02
-- Main device is: /dev/nvme0n1p4
************************************************************
*         THIS WILL DELETE ALL THE DATA ON /dev/sdb1         *
*                                                          *
*         WARNING! Make sure your computer does not go     *
*                  in to idle mode while this script is    *
*                  running. The script will complete,      *
*                  but your SD card may be corrupted.      *
*                                                          *
*         Press <ENTER> to confirm....                     *
************************************************************

unmounting device '/dev/sdb1'
1024+0 records in
1024+0 records out
1048576 bytes (1.0 MB, 1.0 MiB) copied, 0.0866819 s, 12.1 MB/s

Welcome to fdisk (util-linux 2.37.2).
Changes will remain in memory only, until you decide to write them.
Be careful before using the write command.

Device does not contain a recognized partition table.
Created a new DOS disklabel with disk identifier 0xac8f2b89.

Command (m for help): Partition type
   p   primary (0 primary, 0 extended, 4 free)
   e   extended (container for logical partitions)
Select (default p): Partition number (1-4, default 1): First sector (2048-29032682, default 2048): Last sector, +/-sectors or +/-size{K,M,G,T,P} (2048-29032682, default 29032682):
Created a new partition 1 of type 'Linux' and of size 62 MiB.

Command (m for help): Partition type
   p   primary (1 primary, 0 extended, 3 free)
   e   extended (container for logical partitions)
Select (default p): Partition number (2-4, default 2): First sector (129024-29032682, default 129024): Last sector, +/-sectors or +/-size{K,M,G,T,P} (129024-29032682, default 29032682):
Created a new partition 2 of type 'Linux' and of size 13.8 GiB.

Command (m for help): Partition number (1,2, default 2): Hex code or alias (type L to list all):
Changed type of partition 'Linux' to 'W95 FAT32 (LBA)'.

Command (m for help): Partition number (1,2, default 2):
The bootable flag on partition 1 is enabled now.

Command (m for help): The partition table has been altered.
Calling ioctl() to re-read partition table.
Re-reading the partition table failed.: Invalid argument

The kernel still uses the old table. The new table will be used at the next reboot or after you run partprobe(8) or partx(8).

unmounting device '/dev/sdb1'
Formatting /dev/sdb1 ...
Cant find boot partition in /dev
mke2fs 1.46.5 (30-Dec-2021)
The file /dev/sdb1p2 does not exist and no size was specified.
Partitioning and formatting completed!
Copying filesystem on /dev/sdb1p1, /dev/sdb1p2
mount: /tmp/sdk/655483/boot: mount point does not exist.

ERROR: executing mount /dev/sdb1p1 /tmp/sdk/655483/boot

您能帮助检查这个问题吗? 谢谢。

此致、

切里

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Cherry:

    [报价用户 id="496057" url="~/support/processors-group/processors/f/processors-forum/1236625/j721exsomxevm-flash-issue "]

    已参考 此文档 在 PC 端烧录 J721EXSOMXEVM 系统、但失败了。  在将系统刷写到 USB 闪存驱动器 SDK 时出现问题、日志如下所示:  

    [/报价]

    该脚本用于 SD 引导模式、而不是 USB   

    此致
    迪瓦卡尔