This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] AM625:RNG 不工作

Guru**** 1472595 points
Other Parts Discussed in Thread: AM625
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1231230/am625-rng-not-working

器件型号:AM625

您好!

在基于 TI AM625的电路板上启用 RNG 无法工作、并导致一些错误:

这是我在 DTS 中发生的变化、

diff --git a/arch/arm64/boot/dts/ti/k3-am62-main.dtsi b/arch/arm64/boot/dts/ti/k3-am62-main.dtsi
index 510775e9a88f..3343d6ed196e 100644
--- a/arch/arm64/boot/dts/ti/k3-am62-main.dtsi
+++ b/arch/arm64/boot/dts/ti/k3-am62-main.dtsi
@@ -172,35 +172,35 @@ k3_clks: clock-controller {
 
                k3_reset: reset-controller {
                        compatible = "ti,sci-reset";
                        #reset-cells = <2>;
                };
        };
 
        crypto: crypto@40900000 {
                compatible = "ti,am62-sa3ul";
                reg = <0x00 0x40900000 0x00 0x1200>;
-               power-domains = <&k3_pds 70 TI_SCI_PD_SHARED>;
+//             power-domains = <&k3_pds 70 TI_SCI_PD_SHARED>;
                #address-cells = <2>;
                #size-cells = <2>;
                ranges = <0x00 0x40900000 0x00 0x40900000 0x00 0x30000>;
 
                dmas = <&main_pktdma 0xf501 0>, <&main_pktdma 0x7506 0>,
                                <&main_pktdma 0x7507 0>;
                dma-names = "tx", "rx1", "rx2";
 
                rng: rng@40910000 {
                        compatible = "inside-secure,safexcel-eip76";
                        reg = <0x00 0x40910000 0x00 0x7d>;
                        interrupts = <GIC_SPI 129 IRQ_TYPE_LEVEL_HIGH>;
                        clocks = <&k3_clks 70 0>;
-                       status = "disabled";
+//                     status = "disabled";
                };
        };
 
        mcrc: mcrc@30300000 {
                compatible = "ti,mcrc";
                reg = <0x00 0x30300000 0x00 0x1000>;
                clocks = <&k3_clks 116 0>;
                power-domains = <&k3_pds 116 TI_SCI_PD_EXCLUSIVE>;
        };
 

此处显示错误

[    7.828950] omap_rng 40910000.rng: Unable to enable the clk: -19
[    7.832257] remoteproc remoteproc3: 30078000.pru is available
[    7.835390] ------------[ cut here ]------------
[    7.845468] clk:70:0 already disabled
[    7.849228] WARNING: CPU: 0 PID: 223 at drivers/clk/clk.c:969 clk_core_disable+0xb0/0xb8
[    7.857323] Modules linked in: omap_rng(+) pru_rproc rng_core snd_soc_simple_card crct10dif_ce snd_soc_simple_card_utils dwc3_am62 extcon_usb_gpio ti_k3_r5_remoteproc virtio_rpmsg_bus r
ti_wdt j721e_csi2rx videobuf2_dma_contig ti_k3_m4_remoteproc videobuf2_memops sa2ul videobuf2_v4l2 sha512_generic mcrc authenc videobuf2_common cdns_dphy pruss m_can_platform m_can can_dev
 snd_soc_nau8822 ina2xx lm75 sch_fq_codel libcomposite udc_core usb_common fuse ipv6
[    7.897531] CPU: 0 PID: 223 Comm: systemd-udevd Not tainted 5.10.168-00097-g8f7291dacb2c #15
[    7.905965] Hardware name: Toradex Verdin AM62 on Verdin Development Board (DT)
[    7.913275] pstate: 60000085 (nZCv daIf -PAN -UAO -TCO BTYPE=--)
[    7.919283] pc : clk_core_disable+0xb0/0xb8
[    7.923461] lr : clk_core_disable+0xb0/0xb8
[    7.927635] sp : ffff80001161b8c0
[    7.930941] x29: ffff80001161b8c0 x28: 0000000000000100 
[    7.936246] x27: ffff8000100f7c08 x26: 0000000000000003 
[    7.941549] x25: ffff8000111a4138 x24: 0000000000000056 
[    7.946854] x23: ffff0000003d1800 x22: ffff0000003d1810 
[    7.952157] x21: ffff000003952a80 x20: ffff000000f19900 
[    7.957461] x19: ffff000000f19900 x18: 0000000000000010 
[    7.962765] x17: 0000000000000000 x16: 0000000000000000 
[    7.968068] x15: ffff000000eecc90 x14: 0000000000000172 
[    7.973371] x13: ffff000000eecc90 x12: 00000000ffffffea 
[    7.978674] x11: ffff800011160770 x10: ffff800011148730 
[    7.983977] x9 : ffff800011148788 x8 : 0000000000017fe8 
[    7.989281] x7 : c0000000ffffefff x6 : 0000000000000001 
[    7.994583] x5 : ffff00003fd7cab8 x4 : 0000000000000000 
[    7.999887] x3 : 0000000000000027 x2 : 0000000000000023 
[    8.005190] x1 : 0000000000000000 x0 : 0000000000000000 
[    8.010494] Call trace:
[    8.012936]  clk_core_disable+0xb0/0xb8
[    8.016763]  clk_core_disable_lock+0x24/0x40
[    8.021024]  clk_disable+0x20/0x30
[    8.024428]  omap_rng_probe+0x28c/0x378 [omap_rng]
[    8.029214]  platform_drv_probe+0x54/0xa8
[    8.033214]  really_probe+0xf0/0x500
[    8.036782]  driver_probe_device+0xf4/0x160
[    8.040954]  device_driver_attach+0x74/0x80
[    8.045127]  __driver_attach+0xc8/0x188
[    8.048957]  bus_for_each_dev+0x70/0xc8
[    8.052784]  driver_attach+0x24/0x30
[    8.056352]  bus_add_driver+0x144/0x230
[    8.060180]  driver_register+0x64/0x120
[    8.064006]  __platform_driver_register+0x48/0x58
[    8.068704]  omap_rng_driver_init+0x24/0x1000 [omap_rng]
[    8.074007]  do_one_initcall+0x54/0x1b8
[    8.077836]  do_init_module+0x44/0x1f0
[    8.081576]  load_module+0x21d0/0x2830
[    8.085315]  __do_sys_finit_module+0xbc/0x128
[    8.089663]  __arm64_sys_finit_module+0x20/0x30
[    8.094187]  el0_svc_common.constprop.0+0x78/0x1c8
[    8.098968]  do_el0_svc+0x24/0xa0
[    8.102278]  el0_svc+0x14/0x20
[    8.105325]  el0_sync_handler+0xb0/0xb8
[    8.109151]  el0_sync+0x180/0x1c0
[    8.112459] ---[ end trace ad859cb918a80adb ]---
[    8.117804] ------------[ cut here ]------------
[    8.122684] clk:70:0 already unprepared
[    8.128317] WARNING: CPU: 0 PID: 223 at drivers/clk/clk.c:828 clk_core_unprepare+0xf0/0x110
[    8.136720] Modules linked in: irq_pruss_intc omap_rng(+) pru_rproc rng_core snd_soc_simple_card crct10dif_ce snd_soc_simple_card_utils dwc3_am62 extcon_usb_gpio ti_k3_r5_remoteproc vir
tio_rpmsg_bus rti_wdt j721e_csi2rx videobuf2_dma_contig ti_k3_m4_remoteproc videobuf2_memops sa2ul videobuf2_v4l2 sha512_generic mcrc authenc videobuf2_common cdns_dphy pruss m_can_platfor
m m_can can_dev snd_soc_nau8822 ina2xx lm75 sch_fq_codel libcomposite udc_core usb_common fuse ipv6
[    8.178247] CPU: 0 PID: 223 Comm: systemd-udevd Tainted: G        W         5.10.168-00097-g8f7291dacb2c #15
[    8.188062] Hardware name: Toradex Verdin AM62 on Verdin Development Board (DT)
[    8.195363] pstate: 60000005 (nZCv daif -PAN -UAO -TCO BTYPE=--)
[    8.201370] pc : clk_core_unprepare+0xf0/0x110
[    8.205807] lr : clk_core_unprepare+0xf0/0x110
[    8.210241] sp : ffff80001161b8d0
[    8.213545] x29: ffff80001161b8d0 x28: 0000000000000100 
[    8.218851] x27: ffff8000100f7c08 x26: 0000000000000003 
[    8.224155] x25: ffff8000111a4138 x24: 0000000000000056 
[    8.229457] x23: ffff0000003d1800 x22: ffff0000003d1810 
[    8.234760] x21: ffff000003952a80 x20: ffff000002ad7600 
[    8.240063] x19: ffff000000f19900 x18: fffffe0000062e80 
[    8.245367] x17: 0000000000000000 x16: 0000000000000000 
[    8.250670] x15: 0000b41871b1ac84 x14: 000000000000019d 
[    8.255973] x13: 000000000000019d x12: 0000000000000000 
[    8.261276] x11: 0000000000000001 x10: 00000000000009f0 
[    8.266580] x9 : ffff80001161b600 x8 : ffff000000eed190 
[    8.271884] x7 : ffff00000351b200 x6 : 00000000000003db 
[    8.277188] x5 : 0000000000000000 x4 : ffff00003fd7cab8 
[    8.282491] x3 : ffff00003fd839f8 x2 : ffff00003fd7cab8 
[    8.287794] x1 : 0000000000000000 x0 : 0000000000000000 
[    8.293099] Call trace:
[    8.295542]  clk_core_unprepare+0xf0/0x110
[    8.299633]  clk_unprepare+0x2c/0x48
[    8.303210]  omap_rng_probe+0x294/0x378 [omap_rng]
[    8.307998]  platform_drv_probe+0x54/0xa8
[    8.311998]  really_probe+0xf0/0x500
[    8.315565]  driver_probe_device+0xf4/0x160
[    8.319738]  device_driver_attach+0x74/0x80
[    8.323913]  __driver_attach+0xc8/0x188
[    8.327744]  bus_for_each_dev+0x70/0xc8
[    8.331571]  driver_attach+0x24/0x30
[    8.335138]  bus_add_driver+0x144/0x230
[    8.338965]  driver_register+0x64/0x120
[    8.342793]  __platform_driver_register+0x48/0x58
[    8.347489]  omap_rng_driver_init+0x24/0x1000 [omap_rng]
[    8.352793]  do_one_initcall+0x54/0x1b8
[    8.356623]  do_init_module+0x44/0x1f0
[    8.360362]  load_module+0x21d0/0x2830
[    8.364102]  __do_sys_finit_module+0xbc/0x128
[    8.368449]  __arm64_sys_finit_module+0x20/0x30
[    8.372973]  el0_svc_common.constprop.0+0x78/0x1c8
[    8.377754]  do_el0_svc+0x24/0xa0
[    8.381064]  el0_svc+0x14/0x20
[    8.384109]  el0_sync_handler+0xb0/0xb8
[    8.387936]  el0_sync+0x180/0x1c0
[    8.391245] ---[ end trace ad859cb918a80adc ]---
[    8.397322] omap_rng 40910000.rng: initialization failed.

x rngd.service - Hardware RNG Entropy Gatherer Daemon
     Loaded: loaded (/lib/systemd/system/rngd.service; enabled; vendor preset: enabled)
     Active: failed (Result: exit-code) since Sat 2023-05-20 08:22:07 UTC; 11min ago
    Process: 542 ExecStart=/usr/sbin/rngd -f $EXTRA_ARGS (code=exited, status=1/FAILURE)
   Main PID: 542 (code=exited, status=1/FAILURE)

May 20 08:22:07 verdin-am62-14917616 systemd[1]: Started Hardware RNG Entropy Gatherer Daemon.
May 20 08:22:07 verdin-am62-14917616 rngd[542]: Initializing available sources
May 20 08:22:07 verdin-am62-14917616 rngd[542]: [hwrng ]: Initialization Failed
May 20 08:22:07 verdin-am62-14917616 rngd[542]: [rndr  ]: No HW SUPPORT
May 20 08:22:07 verdin-am62-14917616 rngd[542]: [rndr  ]: Initialization Failed
May 20 08:22:07 verdin-am62-14917616 rngd[542]: Can't open any entropy source
May 20 08:22:07 verdin-am62-14917616 rngd[542]: Maybe RNG device modules are not loaded
May 20 08:22:07 verdin-am62-14917616 systemd[1]: rngd.service: Main process exited, code=exited, status=1/FAILURE
May 20 08:22:07 verdin-am62-14917616 systemd[1]: rngd.service: Failed with result 'exit-code'.

此处的完整引导日志显示了

U-Boot SPL 2021.01-6.3.0-devel+git.1095e3e7b70c (May 15 2023 - 10:06:02 +0000)
SYSFW ABI: 3.1 (firmware rev 0x0008 '8.6.4--v08.06.04 (Chill Capybar')
SPL initial stack usage: 13408 bytes
Trying to boot from MMC1
Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
Starting ATF on ARM64 core...

NOTICE:  BL31: v2.8(release):v2.8-226-g2fcd408bb3-dirty
NOTICE:  BL31: Built : 00:42:57, Jan 13 2023

U-Boot SPL 2021.01-6.3.0-devel+git.1095e3e7b70c (May 15 2023 - 10:06:02 +0000)
SYSFW ABI: 3.1 (firmware rev 0x0008 '8.6.4--v08.06.04 (Chill Capybar')
Trying to boot from MMC1


U-Boot 2021.01-6.3.0-devel+git.1095e3e7b70c (May 15 2023 - 10:06:02 +0000)

SoC:   AM62X SR1.0 GP
DRAM:  1 GiB
MMC:   mmc@fa10000: 0, mmc@fa00000: 1, mmc@fa20000: 2
Loading Environment from MMC... OK
In:    serial@2800000
Out:   serial@2800000
Err:   serial@2800000
Model: Toradex 0069 Verdin AM62 Quad 1GB WB IT V1.0A
Serial#: 14917616
Carrier: Toradex Verdin Development Board V1.1A, Serial# 10754330
am65_cpsw_nuss ethernet@8000000: K3 CPSW: nuss_ver: 0x6BA01103 cpsw_ver: 0x6BA81103 ale_ver: 0x00290105 Ports:2 mdio_freq:1000000
Net:   
Warning: ethernet@8000000port@1 MAC addresses don't match:
Address in ROM is               1c:63:49:07:f1:f8
Address in environment is       00:14:2d:e3:9f:f0
eth0: ethernet@8000000port@1
Warning: ethernet@8000000port@2 MAC addresses don't match:
Address in ROM is               1c:63:49:07:f1:f8
Address in environment is       00:14:2d:f3:9f:f0
, eth1: ethernet@8000000port@2
Hit any key to stop autoboot:  0 
MMC: no card present
switch to partitions #0, OK
mmc0(part 0) is current device
Scanning mmc 0:1...
Found U-Boot script /boot.scr
6003 bytes read in 11 ms (532.2 KiB/s)
## Executing script at 90280000
Loading DeviceTree: k3-am625-verdin-nonwifi-dev.dtb
66480 bytes read in 14 ms (4.5 MiB/s)
155 bytes read in 9 ms (16.6 KiB/s)
Applying Overlay: verdin-am62_spidev_overlay.dtbo
560 bytes read in 9 ms (60.5 KiB/s)
7756624 bytes read in 97 ms (76.3 MiB/s)
Bootargs: root=PARTUUID=b49ad018-02 ro rootwait console=tty1 console=ttyS2,115200 consoleblank=0
   Uncompressing Kernel Image
## Flattened Device Tree blob at 90200000
   Booting using the fdt blob at 0x90200000
   Loading Device Tree to 00000000b7ec8000, end 00000000b7efbfff ... OK

Starting kernel ...

[    0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
[    0.000000] Linux version 5.10.168-00097-g8f7291dacb2c (francesco@francesco-nb) (aarch64-linux-gnu-gcc (Ubuntu 9.4.0-1ubuntu1~20.04.1) 9.4.0, GNU ld (GNU Binutils for Ubuntu) 2.34) #15 
SMP PREEMPT Thu May 25 16:53:42 CEST 2023
[    0.000000] Machine model: Toradex Verdin AM62 on Verdin Development Board
[    0.000000] efi: UEFI not found.
[    0.000000] Reserved memory: created DMA memory pool at 0x000000009c800000, size 3 MiB
[    0.000000] OF: reserved mem: initialized node ipc-memories@9c800000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x000000009cb00000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node m4f-dma-memory@9cb00000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x000000009cc00000, size 14 MiB
[    0.000000] OF: reserved mem: initialized node m4f-memory@9cc00000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x000000009da00000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node r5f-dma-memory@9da00000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x000000009db00000, size 12 MiB
[    0.000000] OF: reserved mem: initialized node r5f-memory@9db00000, compatible id shared-dma-pool
[    0.000000] Zone ranges:
[    0.000000]   DMA      [mem 0x0000000080000000-0x00000000bfffffff]
[    0.000000]   DMA32    empty
[    0.000000]   Normal   empty
[    0.000000] Movable zone start for each node
[    0.000000] Early memory node ranges
[    0.000000]   node   0: [mem 0x0000000080000000-0x000000009c7fffff]
[    0.000000]   node   0: [mem 0x000000009c800000-0x000000009e6fffff]
[    0.000000]   node   0: [mem 0x000000009e700000-0x000000009e77ffff]
[    0.000000]   node   0: [mem 0x000000009e780000-0x000000009fffffff]
[    0.000000]   node   0: [mem 0x00000000a0000000-0x00000000bfffffff]
[    0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000000bfffffff]
[    0.000000] cma: Reserved 128 MiB at 0x00000000afc00000
[    0.000000] psci: probing for conduit method from DT.
[    0.000000] psci: PSCIv1.1 detected in firmware.
[    0.000000] psci: Using standard PSCI v0.2 function IDs
[    0.000000] psci: Trusted OS migration not required
[    0.000000] psci: SMC Calling Convention v1.2
[    0.000000] percpu: Embedded 22 pages/cpu s51288 r8192 d30632 u90112
[    0.000000] Detected VIPT I-cache on CPU0
[    0.000000] CPU features: detected: ARM erratum 845719
[    0.000000] CPU features: detected: GIC system register CPU interface
[    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 258048
[    0.000000] Kernel command line: root=PARTUUID=b49ad018-02 ro rootwait console=tty1 console=ttyS2,115200 consoleblank=0
[    0.000000] Dentry cache hash table entries: 131072 (order: 8, 1048576 bytes, linear)
[    0.000000] Inode-cache hash table entries: 65536 (order: 7, 524288 bytes, linear)
[    0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
[    0.000000] Memory: 820672K/1048576K available (10688K kernel code, 1262K rwdata, 4384K rodata, 2048K init, 428K bss, 96832K reserved, 131072K cma-reserved)
[    0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
[    0.000000] rcu: Preemptible hierarchical RCU implementation.
[    0.000000] rcu:     RCU event tracing is enabled.
[    0.000000] rcu:     RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=4.
[    0.000000]  Trampoline variant of Tasks RCU enabled.
[    0.000000]  Tracing variant of Tasks RCU enabled.
[    0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[    0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
[    0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[    0.000000] GICv3: GIC: Using split EOI/Deactivate mode
[    0.000000] GICv3: 256 SPIs implemented
[    0.000000] GICv3: 0 Extended SPIs implemented
[    0.000000] GICv3: Distributor has no Range Selector support
[    0.000000] GICv3: 16 PPIs implemented
[    0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000001880000
[    0.000000] ITS [mem 0x01820000-0x0182ffff]
[    0.000000] GIC: enabling workaround for ITS: Socionext Synquacer pre-ITS
[    0.000000] ITS@0x0000000001820000: Devices Table too large, reduce ids 20->19
[    0.000000] ITS@0x0000000001820000: allocated 524288 Devices @80800000 (flat, esz 8, psz 64K, shr 0)
[    0.000000] ITS: using cache flushing for cmd queue
[    0.000000] GICv3: using LPI property table @0x0000000080030000
[    0.000000] GIC: using cache flushing for LPI property table
[    0.000000] GICv3: CPU0: using allocated LPI pending table @0x0000000080040000
[    0.000000] arch_timer: cp15 timer(s) running at 200.00MHz (phys).
[    0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x2e2049d3e8, max_idle_ns: 440795210634 ns
[    0.000004] sched_clock: 56 bits at 200MHz, resolution 5ns, wraps every 4398046511102ns
[    0.000364] Console: colour dummy device 80x25
[    0.000878] printk: console [tty1] enabled
[    0.000938] Calibrating delay loop (skipped), value calculated using timer frequency.. 400.00 BogoMIPS (lpj=800000)
[    0.000962] pid_max: default: 32768 minimum: 301
[    0.001060] LSM: Security Framework initializing
[    0.001130] Mount-cache hash table entries: 2048 (order: 2, 16384 bytes, linear)
[    0.001154] Mountpoint-cache hash table entries: 2048 (order: 2, 16384 bytes, linear)
[    0.003018] rcu: Hierarchical SRCU implementation.
[    0.003640] Platform MSI: msi-controller@1820000 domain created
[    0.004033] PCI/MSI: /bus@f0000/interrupt-controller@1800000/msi-controller@1820000 domain created
[    0.004140] EFI services will not be available.
[    0.004499] smp: Bringing up secondary CPUs ...
[    0.005146] Detected VIPT I-cache on CPU1
[    0.005187] GICv3: CPU1: found redistributor 1 region 0:0x00000000018a0000
[    0.005203] GICv3: CPU1: using allocated LPI pending table @0x0000000080050000
[    0.005270] CPU1: Booted secondary processor 0x0000000001 [0x410fd034]
[    0.005951] Detected VIPT I-cache on CPU2
[    0.005978] GICv3: CPU2: found redistributor 2 region 0:0x00000000018c0000
[    0.005990] GICv3: CPU2: using allocated LPI pending table @0x0000000080060000
[    0.006026] CPU2: Booted secondary processor 0x0000000002 [0x410fd034]
[    0.006601] Detected VIPT I-cache on CPU3
[    0.006625] GICv3: CPU3: found redistributor 3 region 0:0x00000000018e0000
[    0.006635] GICv3: CPU3: using allocated LPI pending table @0x0000000080070000
[    0.006667] CPU3: Booted secondary processor 0x0000000003 [0x410fd034]
[    0.006734] smp: Brought up 1 node, 4 CPUs
[    0.006845] SMP: Total of 4 processors activated.
[    0.006857] CPU features: detected: 32-bit EL0 Support
[    0.006868] CPU features: detected: CRC32 instructions
[    0.014358] CPU: All CPU(s) started at EL2
[    0.014394] alternatives: patching kernel code
[    0.015616] devtmpfs: initialized
[    0.023587] KASLR disabled due to lack of seed
[    0.023810] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[    0.023841] futex hash table entries: 1024 (order: 4, 65536 bytes, linear)
[    0.027855] pinctrl core: initialized pinctrl subsystem
[    0.028646] DMI not present or invalid.
[    0.029349] NET: Registered protocol family 16
[    0.031112] DMA: preallocated 128 KiB GFP_KERNEL pool for atomic allocations
[    0.031246] DMA: preallocated 128 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
[    0.031366] DMA: preallocated 128 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
[    0.032014] thermal_sys: Registered thermal governor 'step_wise'
[    0.032019] thermal_sys: Registered thermal governor 'power_allocator'
[    0.032500] cpuidle: using governor menu
[    0.032749] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[    0.032864] ASID allocator initialised with 65536 entries
[    0.059535] HugeTLB registered 1.00 GiB page size, pre-allocated 0 pages
[    0.059577] HugeTLB registered 32.0 MiB page size, pre-allocated 0 pages
[    0.059589] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages
[    0.059601] HugeTLB registered 64.0 KiB page size, pre-allocated 0 pages
[    0.060626] cryptd: max_cpu_qlen set to 1000
[    0.063624] k3-chipinfo 43000014.chipid: Family:AM62X rev:SR1.0 JTAGID[0x0bb7e02f] Detected
[    0.064230] On-module +V3.3: supplied by +V_SODIMM
[    0.066005] iommu: Default domain type: Translated 
[    0.066361] SCSI subsystem initialized
[    0.066840] mc: Linux media interface: v0.10
[    0.066874] videodev: Linux video capture interface: v2.00
[    0.066920] pps_core: LinuxPPS API ver. 1 registered
[    0.066931] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[    0.066955] PTP clock support registered
[    0.066997] EDAC MC: Ver: 3.0.0
[    0.067677] omap-mailbox 29000000.mailbox: omap mailbox rev 0x66fc9100
[    0.068166] FPGA manager framework
[    0.068263] Advanced Linux Sound Architecture Driver Initialized.
[    0.069204] clocksource: Switched to clocksource arch_sys_counter
[    0.069417] VFS: Disk quotas dquot_6.6.0
[    0.069473] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[    0.074890] NET: Registered protocol family 2
[    0.075115] IP idents hash table entries: 16384 (order: 5, 131072 bytes, linear)
[    0.076000] tcp_listen_portaddr_hash hash table entries: 512 (order: 1, 8192 bytes, linear)
[    0.076055] TCP established hash table entries: 8192 (order: 4, 65536 bytes, linear)
[    0.076122] TCP bind hash table entries: 8192 (order: 5, 131072 bytes, linear)
[    0.076279] TCP: Hash tables configured (established 8192 bind 8192)
[    0.076457] UDP hash table entries: 512 (order: 2, 16384 bytes, linear)
[    0.076496] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes, linear)
[    0.076649] NET: Registered protocol family 1
[    0.077119] RPC: Registered named UNIX socket transport module.
[    0.077137] RPC: Registered udp transport module.
[    0.077146] RPC: Registered tcp transport module.
[    0.077156] RPC: Registered tcp NFSv4.1 backchannel transport module.
[    0.077171] NET: Registered protocol family 44
[    0.077229] PCI: CLS 0 bytes, default 64
[    0.078059] hw perfevents: enabled with armv8_cortex_a53 PMU driver, 7 counters available
[    0.081965] Initialise system trusted keyrings
[    0.082209] workingset: timestamp_bits=46 max_order=18 bucket_order=0
[    0.085848] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[    0.086416] NFS: Registering the id_resolver key type
[    0.086464] Key type id_resolver registered
[    0.086475] Key type id_legacy registered
[    0.086542] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[    0.086555] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...
[    0.086760] 9p: Installing v9fs 9p2000 file system support
[    0.121904] Key type asymmetric registered
[    0.121932] Asymmetric key parser 'x509' registered
[    0.121988] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 244)
[    0.122004] io scheduler mq-deadline registered
[    0.122014] io scheduler kyber registered
[    0.124196] pinctrl-single 4084000.pinctrl: 34 pins, size 136
[    0.124665] pinctrl-single f4000.pinctrl: 171 pins, size 684
[    0.131833] Serial: 8250/16550 driver, 10 ports, IRQ sharing enabled
[    0.145672] brd: module loaded
[    0.152800] loop: module loaded
[    0.153820] megasas: 07.714.04.00-rc1
[    0.156854] tun: Universal TUN/TAP device driver, 1.6
[    0.157116] igbvf: Intel(R) Gigabit Virtual Function Network Driver
[    0.157131] igbvf: Copyright (c) 2009 - 2012 Intel Corporation.
[    0.158023] VFIO - User Level meta-driver version: 0.3
[    0.159130] i2c /dev entries driver
[    0.161068] sdhci: Secure Digital Host Controller Interface driver
[    0.161091] sdhci: Copyright(c) Pierre Ossman
[    0.161511] sdhci-pltfm: SDHCI platform and OF driver helper
[    0.162608] ledtrig-cpu: registered to indicate activity on CPUs
[    0.162978] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping ....
[    0.164543] optee: probing for conduit method.
[    0.164595] optee: revision 3.20 (8e74d476)
[    0.164887] optee: dynamic shared memory is enabled
[    0.165144] optee: initialized driver
[    0.167366] NET: Registered protocol family 17
[    0.167540] 9pnet: Installing 9P2000 support
[    0.167627] Key type dns_resolver registered
[    0.168038] Loading compiled-in X.509 certificates
[    0.178038] ti-sci 44043000.system-controller: lpm region is required for suspend but not provided.
[    0.178122] ti-sci 44043000.system-controller: ABI: 3.1 (firmware rev 0x0008 '8.6.4--v08.06.04 (Chill Capybar')
[    0.214422] ti-sci-clk 44043000.system-controller:clock-controller: recalc-rate failed for dev=70, clk=0, ret=-19
[    0.237870] davinci-mcasp 2b00000.mcasp: IRQ common not found
[    0.240675] omap-gpmc 3b000000.memory-controller: GPMC revision 6.0
[    0.240719] gpmc_mem_init: disabling cs 0 mapped at 0x0-0x1000000
[    0.243000] omap_i2c 4900000.i2c: bus 3 rev0.12 at 100 kHz
[    0.266647] +VDD_CORE (PMIC BUCK1): supplied by +V_SODIMM
[    0.267667] +V1.8 (PMIC BUCK2): supplied by +V_SODIMM
[    0.268547] +VDD_DDR (PMIC BUCK3): supplied by +V_SODIMM
[    0.269582] +V3.3_1.8_SD (PMIC LDO1): supplied by On-module +V3.3
[    0.270792] +VDDR_CORE (PMIC LDO2): supplied by +V1.8 (PMIC BUCK2)
[    0.271947] +V1.8A (PMIC LDO3): supplied by On-module +V3.3
[    0.272820] +V2.5_ETH (PMIC LDO4): supplied by On-module +V3.3
[    0.274921] input: tps65219-pwrbutton as /devices/platform/bus@f0000/20000000.i2c/i2c-0/0-0030/tps65219-pwrbutton.1.auto/input/input0
[    0.275492] tps65219 0-0030: Setup as system-power-controller but pm_power_off function already registered, overwriting
[    0.276650] rtc-ds1307 0-0032: oscillator failed, set time!
[    0.276815] rtc-ds1307 0-0032: registered as rtc0
[    0.276970] rtc-ds1307 0-0032: hctosys: unable to read the hardware clock
[    0.279010] at24 0-0050: supply vcc not found, using dummy regulator
[    0.279407] at24 0-0050: 256 byte 24c02 EEPROM, writable, 16 bytes/write
[    0.279472] omap_i2c 20000000.i2c: bus 0 rev0.12 at 400 kHz
[    0.281313] pca953x 1-0021: supply vcc not found, using dummy regulator
[    0.281461] pca953x 1-0021: using no AI
[    0.307517] at24 1-0057: supply vcc not found, using dummy regulator
[    0.308224] at24 1-0057: 256 byte 24c02 EEPROM, writable, 16 bytes/write
[    0.308287] omap_i2c 20010000.i2c: bus 1 rev0.12 at 100 kHz
[    0.309494] omap_i2c 20020000.i2c: bus 2 rev0.12 at 100 kHz
[    0.310470] omap_i2c 20030000.i2c: bus 4 rev0.12 at 100 kHz
[    0.310861] ti-sci-intr 4210000.interrupt-controller: Interrupt Router 5 domain created
[    0.311018] ti-sci-intr bus@f0000:interrupt-controller@a00000: Interrupt Router 3 domain created
[    0.311274] ti-sci-inta 48000000.interrupt-controller: Interrupt Aggregator domain 28 created
[    0.312591] ti-udma 485c0100.dma-controller: Number of rings: 82
[    0.314641] ti-udma 485c0100.dma-controller: Channels: 48 (bchan: 18, tchan: 12, rchan: 18)
[    0.317143] ti-udma 485c0000.dma-controller: Number of rings: 150
[    0.320821] ti-udma 485c0000.dma-controller: Channels: 35 (tchan: 20, rchan: 15)
[    0.323575] 4a00000.serial: ttyS3 at MMIO 0x4a00000 (irq = 15, base_baud = 3000000) is a 8250
[    0.324909] 2800000.serial: ttyS2 at MMIO 0x2800000 (irq = 29, base_baud = 3000000) is a 8250
[    1.697510] printk: console [ttyS2] enabled
[    1.703196] 2810000.serial: ttyS0 at MMIO 0x2810000 (irq = 30, base_baud = 3000000) is a 8250
[    1.720479] davinci_mdio 8000f00.mdio: Configuring MDIO in manual mode
[    1.765209] davinci_mdio 8000f00.mdio: davinci mdio revision 9.7, bus freq 1000000
[    1.773913] am65-cpsw-nuss 8000000.ethernet: initializing am65 cpsw nuss version 0x6BA01103, cpsw version 0x6BA81103 Ports: 3 quirks:00000006
[    1.786830] am65-cpsw-nuss 8000000.ethernet: initialized cpsw ale version 1.5
[    1.793968] am65-cpsw-nuss 8000000.ethernet: ALE Table size 512
[    1.800647] am65-cpsw-nuss 8000000.ethernet: CPTS ver 0x4e8a010c, freq:500000000, add_val:1 pps:0
[    1.810965] am65-cpsw-nuss 8000000.ethernet: set new flow-id-base 19
[    1.821263] rtc-ti-k3 2b1f0000.rtc: registered as rtc1
[    1.930482] davinci-mcasp 2b00000.mcasp: IRQ common not found
[    1.930937] mmc0: CQHCI version 5.10
[    1.942452] gpio-414 (CTRL_SLEEP_MOCI#): hogged as output/high
[    1.953702] On-module +V1.2_DSI: supplied by +V1.8 (PMIC BUCK2)
[    1.960031] On-module +V1.8_DSI: supplied by +V1.8 (PMIC BUCK2)
[    1.966130] On-module +V1.0_ETH: supplied by +V1.8 (PMIC BUCK2)
[    1.972229] On-module +V1.8_ETH: supplied by +V1.8 (PMIC BUCK2)
[    1.979395] davinci_mdio 8000f00.mdio: Configuring MDIO in manual mode
[    1.981259] mmc0: SDHCI controller on fa10000.mmc [fa10000.mmc] using ADMA 64-bit
[    2.025219] davinci_mdio 8000f00.mdio: davinci mdio revision 9.7, bus freq 1000000
[    2.039353] davinci_mdio 8000f00.mdio: phy[0]: device 8000f00.mdio:00, driver TI DP83867
[    2.047478] davinci_mdio 8000f00.mdio: phy[7]: device 8000f00.mdio:07, driver Microchip KSZ9131 Gigabit PHY
[    2.058249] debugfs: Directory 'pd:53' with parent 'pm_genpd' already present!
[    2.059089] mmc1: CQHCI version 5.10
[    2.065549] debugfs: Directory 'pd:52' with parent 'pm_genpd' already present!
[    2.076607] debugfs: Directory 'pd:51' with parent 'pm_genpd' already present!
[    2.076670] mmc0: Command Queue Engine enabled
[    2.084176] debugfs: Directory 'pd:182' with parent 'pm_genpd' already present!
[    2.088325] mmc0: new HS200 MMC card at address 0001
[    2.097915] input: gpio-keys as /devices/platform/gpio-keys/input/input1
[    2.101317] mmcblk0: mmc0:0001 S0J56X 14.8 GiB 
[    2.112205] mmcblk0boot0: mmc0:0001 S0J56X partition 1 31.5 MiB
[    2.118394] mmcblk0boot1: mmc0:0001 S0J56X partition 2 31.5 MiB
[    2.124536] mmcblk0rpmb: mmc0:0001 S0J56X partition 3 4.00 MiB, chardev (238:0)
[    2.134913] ti-sci-clk 44043000.system-controller:clock-controller: is_prepared failed for dev=70, clk=0, ret=-19
[    2.135178]  mmcblk0: p1 p2
[    2.153930] ALSA device list:
[    2.156918]   No soundcards found.
[    3.591398] sdhci-am654 fa00000.mmc: Power on failed
[    3.626985] mmc1: SDHCI controller on fa00000.mmc [fa00000.mmc] using ADMA 64-bit
[    3.642670] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
[    3.650880] VFS: Mounted root (ext4 filesystem) readonly on device 179:2.
[    3.659632] devtmpfs: mounted
[    3.664055] Freeing unused kernel memory: 2048K
[    3.669279] Run /sbin/init as init process
[    3.765371] systemd[1]: System time before build time, advancing clock.
[    3.954131] NET: Registered protocol family 10
[    3.959819] Segment Routing with IPv6
[    3.980153] systemd[1]: systemd 250.5+ running in system mode (+PAM -AUDIT -SELINUX -APPARMOR +IMA -SMACK +SECCOMP -GCRYPT -GNUTLS -OPENSSL +ACL +BLKID -CURL -ELFUTILS -FIDO2 -IDN2 -IDN
 -IPTC +KMOD -LIBCRYPTSETUP +LIBFDISK -PCRE2 -PWQUALITY -P11KIT -QRENCODE -BZIP2 -LZ4 -XZ -ZLIB +ZSTD -BPF_FRAMEWORK +XKBCOMMON +UTMP +SYSVINIT default-hierarchy=hybrid)
[    4.012132] systemd[1]: Detected architecture arm64.

Welcome to TDX Wayland with XWayland 6.3.0-devel-20230518+build.289 (kirkstone)!

[    4.065849] systemd[1]: Hostname set to <verdin-am62-14917616>.
[    4.385410] systemd[1]: Queued start job for default target Graphical Interface.
[    4.436178] systemd[1]: Created slice Slice /system/getty.
[  OK  ] Created slice Slice /system/getty.
[    4.459509] systemd[1]: Created slice Slice /system/modprobe.
[  OK  ] Created slice Slice /system/modprobe.
[    4.483373] systemd[1]: Created slice Slice /system/serial-getty.
[  OK  ] Created slice Slice /system/serial-getty.
[    4.507047] systemd[1]: Created slice User and Session Slice.
[  OK  ] Created slice User and Session Slice.
[    4.529748] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
[  OK  ] Started Dispatch Password �…ts to Console Directory Watch.
[    4.553537] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
[  OK  ] Started Forward Password R�…uests to Wall Directory Watch.
[    4.577548] systemd[1]: Reached target Host and Network Name Lookups.
[  OK  ] Reached target Host and Network Name Lookups.
[    4.601333] systemd[1]: Reached target Path Units.
[  OK  ] Reached target Path Units.
[    4.617345] systemd[1]: Reached target Remote File Systems.
[  OK  ] Reached target Remote File Systems.
[    4.637323] systemd[1]: Reached target Slice Units.
[  OK  ] Reached target Slice Units.
[    4.653346] systemd[1]: Reached target Swaps.
[  OK  ] Reached target Swaps.
[    4.690963] systemd[1]: Listening on RPCbind Server Activation Socket.
[  OK  ] Listening on RPCbind Server Activation Socket.
[    4.713541] systemd[1]: Reached target RPC Port Mapper.
[  OK  ] Reached target RPC Port Mapper.
[    4.734100] systemd[1]: Listening on Syslog Socket.
[  OK  ] Listening on Syslog Socket.
[    4.749733] systemd[1]: Listening on initctl Compatibility Named Pipe.
[  OK  ] Listening on initctl Compatibility Named Pipe.
[    4.777361] systemd[1]: Journal Audit Socket was skipped because of a failed condition check (ConditionSecurity=audit).
[    4.789035] systemd[1]: Listening on Journal Socket (/dev/log).
[  OK  ] Listening on Journal Socket (/dev/log).
[    4.810036] systemd[1]: Listening on Journal Socket.
[  OK  ] Listening on Journal Socket.
[    4.826171] systemd[1]: Listening on Network Service Netlink Socket.
[  OK  ] Listening on Network Service Netlink Socket.
[    4.850071] systemd[1]: Listening on udev Control Socket.
[  OK  ] Listening on udev Control Socket.
[    4.873804] systemd[1]: Listening on udev Kernel Socket.
[  OK  ] Listening on udev Kernel Socket.
[    4.893919] systemd[1]: Listening on User Database Manager Socket.
[  OK  ] Listening on User Database Manager Socket.
[    4.921648] systemd[1]: Mounting Huge Pages File System...
         Mounting Huge Pages File System...
[    4.941703] systemd[1]: Mounting POSIX Message Queue File System...
         Mounting POSIX Message Queue File System...
[    4.969688] systemd[1]: Mounting Kernel Debug File System...
         Mounting Kernel Debug File System...
[    4.993855] systemd[1]: Kernel Trace File System was skipped because of a failed condition check (ConditionPathExists=/sys/kernel/tracing).
[    5.014919] systemd[1]: Mounting Temporary Directory /tmp...
         Mounting Temporary Directory /tmp...
[    5.035091] systemd[1]: Starting Create List of Static Device Nodes...
         Starting Create List of Static Device Nodes...
[    5.062233] systemd[1]: Starting Load Kernel Module configfs...
         Starting Load Kernel Module configfs...
[    5.082423] systemd[1]: Starting Load Kernel Module drm...
         Starting Load Kernel Module drm...
[    5.102074] systemd[1]: Starting Load Kernel Module fuse...
         Starting Load Kernel Module fuse...
[    5.130714] systemd[1]: Starting RPC Bind...
         Starting RPC Bind...
[    5.142192] fuse: init (API version 7.32)
[    5.151889] systemd[1]: Starting File System Check on Root Device...
         Starting File System Check on Root Device...
[    5.180990] systemd[1]: Starting Journal Service...
         Starting Journal Service...
[    5.197698] systemd[1]: Starting Load Kernel Modules...
         Starting Load Kernel Modules...
[    5.210153] systemd[1]: Starting Generate network units from Kernel command line...
         Starting Generate network �…ts from Kernel command line...
[    5.225657] systemd[1]: Starting Coldplug All udev Devices...
         Starting Coldplug All udev Devices...
[    5.253349] systemd[1]: Started RPC Bind.
[  OK  ] Started RPC Bind.
[    5.274631] systemd[1]: Mounted Huge Pages File System.
[  OK  ] Mounted Huge Pages File System.
[    5.302222] systemd[1]: Mounted POSIX Message Queue File System.
[  OK  ] Mounted POSIX Message Queue File System.
[    5.326261] systemd[1]: Started Journal Service.
[  OK  ] Started Journal Service.
[  OK  ] Mounted Kernel Debug File System.
[  OK  ] Mounted Temporary Directory /tmp.
[  OK  ] Finished Create List of Static Device Nodes.
[  OK  ] Finished Load Kernel Module configfs.
[  OK  ] Finished Load Kernel Module drm.
[  OK  ] Finished Load Kernel Module fuse.
[  OK  ] Finished File System Check on Root Device.
[  OK  ] Finished Load Kernel Modules.
[  OK  ] Finished Generate network units from Kernel command line.
         Mounting FUSE Control File System...
         Mounting Kernel Configuration File System...
         Starting Remount Root and Kernel File Systems...
         Starting Apply Kernel Variables...
[    5.585422] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)
[  OK  ] Mounted FUSE Control File System.
[  OK  ] Mounted Kernel Configuration File System.
[  OK  ] Finished Remount Root and Kernel File Systems.
[  OK  ] Finished Apply Kernel Variables.
         Starting Flush Journal to Persistent Storage...
[    5.700298] systemd-journald[200]: Received client request to flush runtime journal.
         Starting Create Static Device Nodes in /dev...
[  OK  ] Finished Flush Journal to Persistent Storage.
[  OK  ] Finished Create Static Device Nodes in /dev.
[  OK  ] Reached target Preparation for Local File Systems.
         Mounting /var/volatile...
         Starting Rule-based Manage�…for Device Events and Files...
[  OK  ] Finished Coldplug All udev Devices.
[  OK  ] Mounted /var/volatile.
         Starting Wait for udev To �…plete Device Initialization...
         Starting Load/Save Random Seed...
[  OK  ] Reached target Local File Systems.
         Starting Create Volatile Files and Directories...
[  OK  ] Started Rule-based Manager for Device Events and Files.
[  OK  ] Finished Create Volatile Files and Directories.
         Starting Network Time Synchronization...
         Starting Record System Boot/Shutdown in UTMP...
[  OK  ] Finished Record System Boot/Shutdown in UTMP.
[    6.296399] lm75 0-0048: supply vs not found, using dummy regulator
[    6.323505] ina2xx 1-0040: power monitor ina219 (Rshunt = 10000 uOhm)
[    6.327678] hwmon hwmon1: temp1_input not attached to any thermal zone
[    6.339228] lm75 0-0048: hwmon1: sensor 'tmp1075'
[    6.345802] lm75 1-004f: supply vs not found, using dummy regulator
[    6.361922] hwmon hwmon2: temp1_input not attached to any thermal zone
[    6.368629] lm75 1-004f: hwmon2: sensor 'tmp75c'
[    6.389118] CAN device driver interface
[    6.450034] m_can_platform 20701000.can: m_can device registered (irq=44, version=32)
[    6.536854] systemd-journald[200]: Oldest entry in /run/log/journal/3bbcba0502d64fd8836e11adf551d470/system.journal is older than the configured file retention duration (1month), sugges
ting rotation.
[  OK  ] Started Network Time Synchronizatio[    6.563084] systemd-journald[200]: /run/log/journal/3bbcba0502d64fd8836e11adf551d470/system.journal: Journal header limits reached or header 
out-of-date, rotating.
n.
[  OK  ] Reached target System Time Set.
[    6.628645] k3-m4-rproc 5000000.m4fss: assigned reserved memory node m4f-dma-memory@9cb00000
[    6.641019] k3-m4-rproc 5000000.m4fss: configured M4 for remoteproc mode
[    6.652740] k3-m4-rproc 5000000.m4fss: local reset is deasserted for device
[    6.669623] remoteproc remoteproc0: 5000000.m4fss is available
[    6.684841] remoteproc remoteproc0: Direct firmware load for am62-mcu-m4f0_0-fw failed with error -2
[    6.694135] remoteproc remoteproc0: powering up 5000000.m4fss
[    6.703619] remoteproc remoteproc0: Direct firmware load for am62-mcu-m4f0_0-fw failed with error -2
[    6.713186] remoteproc remoteproc0: request_firmware failed: -2
[    6.771073] platform 78000000.r5f: R5F core may have been powered on by a different host, programmed state (0) != actual state (1)
[    6.784928] platform 78000000.r5f: configured R5F for IPC-only mode
[    6.793328] platform 78000000.r5f: assigned reserved memory node r5f-dma-memory@9da00000
[    6.810681] remoteproc remoteproc1: 78000000.r5f is available
[    6.819748] remoteproc remoteproc1: attaching to 78000000.r5f
[    6.832575] platform 78000000.r5f: R5F core initialized in IPC-only mode
[    6.841707]  remoteproc1#vdev0buffer: assigned reserved memory node r5f-dma-memory@9da00000
[    6.854198] virtio_rpmsg_bus virtio0: rpmsg host is online
[    6.854860] virtio_rpmsg_bus virtio0: creating channel ti.ipc4.ping-pong addr 0xd
[    6.869374]  remoteproc1#vdev0buffer: registered virtio0 (type 7)
[    6.871477] virtio_rpmsg_bus virtio0: creating channel rpmsg_chrdev addr 0xe
[    6.877928] remoteproc remoteproc1: remote processor 78000000.r5f is now attached
[    7.721271] random: crng init done
[  OK  ] Finished Load/Save Random Seed.
[    7.821618] remoteproc remoteproc2: 30074000.pru is available
[    7.828950] omap_rng 40910000.rng: Unable to enable the clk: -19
[    7.832257] remoteproc remoteproc3: 30078000.pru is available
[    7.835390] ------------[ cut here ]------------
[    7.845468] clk:70:0 already disabled
[    7.849228] WARNING: CPU: 0 PID: 223 at drivers/clk/clk.c:969 clk_core_disable+0xb0/0xb8
[    7.857323] Modules linked in: omap_rng(+) pru_rproc rng_core snd_soc_simple_card crct10dif_ce snd_soc_simple_card_utils dwc3_am62 extcon_usb_gpio ti_k3_r5_remoteproc virtio_rpmsg_bus r
ti_wdt j721e_csi2rx videobuf2_dma_contig ti_k3_m4_remoteproc videobuf2_memops sa2ul videobuf2_v4l2 sha512_generic mcrc authenc videobuf2_common cdns_dphy pruss m_can_platform m_can can_dev
 snd_soc_nau8822 ina2xx lm75 sch_fq_codel libcomposite udc_core usb_common fuse ipv6
[    7.897531] CPU: 0 PID: 223 Comm: systemd-udevd Not tainted 5.10.168-00097-g8f7291dacb2c #15
[    7.905965] Hardware name: Toradex Verdin AM62 on Verdin Development Board (DT)
[    7.913275] pstate: 60000085 (nZCv daIf -PAN -UAO -TCO BTYPE=--)
[    7.919283] pc : clk_core_disable+0xb0/0xb8
[    7.923461] lr : clk_core_disable+0xb0/0xb8
[    7.927635] sp : ffff80001161b8c0
[    7.930941] x29: ffff80001161b8c0 x28: 0000000000000100 
[    7.936246] x27: ffff8000100f7c08 x26: 0000000000000003 
[    7.941549] x25: ffff8000111a4138 x24: 0000000000000056 
[    7.946854] x23: ffff0000003d1800 x22: ffff0000003d1810 
[    7.952157] x21: ffff000003952a80 x20: ffff000000f19900 
[    7.957461] x19: ffff000000f19900 x18: 0000000000000010 
[    7.962765] x17: 0000000000000000 x16: 0000000000000000 
[    7.968068] x15: ffff000000eecc90 x14: 0000000000000172 
[    7.973371] x13: ffff000000eecc90 x12: 00000000ffffffea 
[    7.978674] x11: ffff800011160770 x10: ffff800011148730 
[    7.983977] x9 : ffff800011148788 x8 : 0000000000017fe8 
[    7.989281] x7 : c0000000ffffefff x6 : 0000000000000001 
[    7.994583] x5 : ffff00003fd7cab8 x4 : 0000000000000000 
[    7.999887] x3 : 0000000000000027 x2 : 0000000000000023 
[    8.005190] x1 : 0000000000000000 x0 : 0000000000000000 
[    8.010494] Call trace:
[    8.012936]  clk_core_disable+0xb0/0xb8
[    8.016763]  clk_core_disable_lock+0x24/0x40
[    8.021024]  clk_disable+0x20/0x30
[    8.024428]  omap_rng_probe+0x28c/0x378 [omap_rng]
[    8.029214]  platform_drv_probe+0x54/0xa8
[    8.033214]  really_probe+0xf0/0x500
[    8.036782]  driver_probe_device+0xf4/0x160
[    8.040954]  device_driver_attach+0x74/0x80
[    8.045127]  __driver_attach+0xc8/0x188
[    8.048957]  bus_for_each_dev+0x70/0xc8
[    8.052784]  driver_attach+0x24/0x30
[    8.056352]  bus_add_driver+0x144/0x230
[    8.060180]  driver_register+0x64/0x120
[    8.064006]  __platform_driver_register+0x48/0x58
[    8.068704]  omap_rng_driver_init+0x24/0x1000 [omap_rng]
[    8.074007]  do_one_initcall+0x54/0x1b8
[    8.077836]  do_init_module+0x44/0x1f0
[    8.081576]  load_module+0x21d0/0x2830
[    8.085315]  __do_sys_finit_module+0xbc/0x128
[    8.089663]  __arm64_sys_finit_module+0x20/0x30
[    8.094187]  el0_svc_common.constprop.0+0x78/0x1c8
[    8.098968]  do_el0_svc+0x24/0xa0
[    8.102278]  el0_svc+0x14/0x20
[    8.105325]  el0_sync_handler+0xb0/0xb8
[    8.109151]  el0_sync+0x180/0x1c0
[    8.112459] ---[ end trace ad859cb918a80adb ]---
[    8.117804] ------------[ cut here ]------------
[    8.122684] clk:70:0 already unprepared
[    8.128317] WARNING: CPU: 0 PID: 223 at drivers/clk/clk.c:828 clk_core_unprepare+0xf0/0x110
[    8.136720] Modules linked in: irq_pruss_intc omap_rng(+) pru_rproc rng_core snd_soc_simple_card crct10dif_ce snd_soc_simple_card_utils dwc3_am62 extcon_usb_gpio ti_k3_r5_remoteproc vir
tio_rpmsg_bus rti_wdt j721e_csi2rx videobuf2_dma_contig ti_k3_m4_remoteproc videobuf2_memops sa2ul videobuf2_v4l2 sha512_generic mcrc authenc videobuf2_common cdns_dphy pruss m_can_platfor
m m_can can_dev snd_soc_nau8822 ina2xx lm75 sch_fq_codel libcomposite udc_core usb_common fuse ipv6
[    8.178247] CPU: 0 PID: 223 Comm: systemd-udevd Tainted: G        W         5.10.168-00097-g8f7291dacb2c #15
[    8.188062] Hardware name: Toradex Verdin AM62 on Verdin Development Board (DT)
[    8.195363] pstate: 60000005 (nZCv daif -PAN -UAO -TCO BTYPE=--)
[    8.201370] pc : clk_core_unprepare+0xf0/0x110
[    8.205807] lr : clk_core_unprepare+0xf0/0x110
[    8.210241] sp : ffff80001161b8d0
[    8.213545] x29: ffff80001161b8d0 x28: 0000000000000100 
[    8.218851] x27: ffff8000100f7c08 x26: 0000000000000003 
[    8.224155] x25: ffff8000111a4138 x24: 0000000000000056 
[    8.229457] x23: ffff0000003d1800 x22: ffff0000003d1810 
[    8.234760] x21: ffff000003952a80 x20: ffff000002ad7600 
[    8.240063] x19: ffff000000f19900 x18: fffffe0000062e80 
[    8.245367] x17: 0000000000000000 x16: 0000000000000000 
[    8.250670] x15: 0000b41871b1ac84 x14: 000000000000019d 
[    8.255973] x13: 000000000000019d x12: 0000000000000000 
[    8.261276] x11: 0000000000000001 x10: 00000000000009f0 
[    8.266580] x9 : ffff80001161b600 x8 : ffff000000eed190 
[    8.271884] x7 : ffff00000351b200 x6 : 00000000000003db 
[    8.277188] x5 : 0000000000000000 x4 : ffff00003fd7cab8 
[    8.282491] x3 : ffff00003fd839f8 x2 : ffff00003fd7cab8 
[    8.287794] x1 : 0000000000000000 x0 : 0000000000000000 
[    8.293099] Call trace:
[    8.295542]  clk_core_unprepare+0xf0/0x110
[    8.299633]  clk_unprepare+0x2c/0x48
[    8.303210]  omap_rng_probe+0x294/0x378 [omap_rng]
[    8.307998]  platform_drv_probe+0x54/0xa8
[    8.311998]  really_probe+0xf0/0x500
[    8.315565]  driver_probe_device+0xf4/0x160
[    8.319738]  device_driver_attach+0x74/0x80
[    8.323913]  __driver_attach+0xc8/0x188
[    8.327744]  bus_for_each_dev+0x70/0xc8
[    8.331571]  driver_attach+0x24/0x30
[    8.335138]  bus_add_driver+0x144/0x230
[    8.338965]  driver_register+0x64/0x120
[    8.342793]  __platform_driver_register+0x48/0x58
[    8.347489]  omap_rng_driver_init+0x24/0x1000 [omap_rng]
[    8.352793]  do_one_initcall+0x54/0x1b8
[    8.356623]  do_init_module+0x44/0x1f0
[    8.360362]  load_module+0x21d0/0x2830
[    8.364102]  __do_sys_finit_module+0xbc/0x128
[    8.368449]  __arm64_sys_finit_module+0x20/0x30
[    8.372973]  el0_svc_common.constprop.0+0x78/0x1c8
[    8.377754]  do_el0_svc+0x24/0xa0
[    8.381064]  el0_svc+0x14/0x20
[    8.384109]  el0_sync_handler+0xb0/0xb8
[    8.387936]  el0_sync+0x180/0x1c0
[    8.391245] ---[ end trace ad859cb918a80adc ]---
[    8.397322] omap_rng 40910000.rng: initialization failed.
[    8.429764] cdns-csi2rx: probe of 30101000.csi-bridge failed with error -22
[    8.447456] dwc3 31000000.usb: Configuration mismatch. dr_mode forced to gadget
[    8.543305] usbcore: registered new interface driver usbfs
[    8.549172] usbcore: registered new interface driver hub
[    8.554849] usbcore: registered new device driver usb
[    8.600987] xhci-hcd xhci-hcd.3.auto: xHCI Host Controller
[    8.606624] xhci-hcd xhci-hcd.3.auto: new USB bus registered, assigned bus number 1
[    8.614613] xhci-hcd xhci-hcd.3.auto: hcc params 0x0258fe6d hci version 0x110 quirks 0x0000000000010010
[    8.624270] xhci-hcd xhci-hcd.3.auto: irq 552, io mem 0x31100000
[    8.630700] xhci-hcd xhci-hcd.3.auto: xHCI Host Controller
[    8.636410] xhci-hcd xhci-hcd.3.auto: new USB bus registered, assigned bus number 2
[    8.644183] xhci-hcd xhci-hcd.3.auto: Host supports USB 3.0 SuperSpeed
[    8.650972] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 5.10
[    8.659359] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[    8.666755] usb usb1: Product: xHCI Host Controller
[    8.671752] usb usb1: Manufacturer: Linux 5.10.168-00097-g8f7291dacb2c xhci-hcd
[    8.679182] usb usb1: SerialNumber: xhci-hcd.3.auto
[    8.684989] hub 1-0:1.0: USB hub found
[    8.688892] hub 1-0:1.0: 1 port detected
[    8.693757] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM.
[    8.702141] usb usb2: New USB device found, idVendor=1d6b, idProduct=0003, bcdDevice= 5.10
[    8.710506] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[    8.717834] usb usb2: Product: xHCI Host Controller
[    8.722870] usb usb2: Manufacturer: Linux 5.10.168-00097-g8f7291dacb2c xhci-hcd
[    8.730238] usb usb2: SerialNumber: xhci-hcd.3.auto
[    8.736190] hub 2-0:1.0: USB hub found
[    8.740168] hub 2-0:1.0: config failed, hub doesn't have any ports! (err -19)
[  OK  ] Created slice Slice /system/systemd-fsck.
[    8.949295] usb 1-1: new high-speed USB device number 2 using xhci-hcd
[  OK  ] Found device /dev/mmcblk0p1.
[  OK  ] Finished Wait for udev To Complete Device Initialization.
[  OK  ] Started Hardware RNG Entropy Gatherer Daemon.
[  OK  ] Reached target System Initialization.
[  OK  ] Started Daily Cleanup of Temporary Directories.
[  OK  ] Reached target Timer Units.
[  OK  ] Listening on Avahi mDNS/DNS-SD Stac[    9.101869] usb 1-1: New USB device found, idVendor=0424, idProduct=2744, bcdDevice= 2.21
k Activation Socket.
[    9.112420] usb 1-1: New USB device strings: Mfr=1, Product=2, SerialNumber=0
[    9.121745] usb 1-1: Product: USB2744
[    9.125487] usb 1-1: Manufacturer: Microchip Tech
[  OK  ] Listening on D-Bus System Message Bus Socket.
[  OK  ] Listening on dropbear.socket.
[  OK  ] Listening on GPS (Global P�…ioning System) Daemon Sockets.
[    9.195317] hub 1-1:1.0: USB hub found
[    9.199291] hub 1-1:1.0: 4 ports detected
         Starting Weston socket...
         Starting File System Check on /dev/mmcblk0p1...
[  OK  ] Listening on Weston socket.
[  OK  ] Reached target Socket Units.
[  OK  ] Reached target Basic System.
         Starting Save/Restore Sound Card State...
[  OK  ] Started Kernel Logging Service.
[  OK  ] Started System Logging Service.
         Starting D-Bus System Message Bus...
         Starting IPv6 Packet Filtering Framework...
         Starting IPv4 Packet Filtering Framework...
         Starting Telephony service...
         Starting User Login Management...
[  OK  ] Started Timestamping service.
         Starting Load default USB gadget schema g1.schema...
[  OK  ] Finished File System Check on /dev/mmcblk0p1.
[  OK  ] Started D-Bus System Message Bus.
[  OK  ] Finished Save/Restore Sound Card State.
[  OK  ] Finished IPv6 Packet Filtering Framework.
[  OK  ] Finished IPv4 Packet Filtering Framework.
[  OK  ] Reached target Preparation for Network.
[  OK  ] Reached target Sound Card.
[    9.549342] usb 1-1.2: new full-speed USB device number 3 using xhci-hcd
[    9.553508] Bluetooth: Core ver 2.22
[    9.559922] NET: Registered protocol family 31
[    9.565184] Bluetooth: HCI device and connection manager initialized
[    9.565431] Bluetooth: HCI socket layer initialized
[    9.565442] Bluetooth: L2CAP socket layer initialized
[    9.565480] Bluetooth: SCO socket layer initialized
[    9.586468] using random self ethernet address
[  OK  ] Listening on Load/Save RF �…itch S[    9.594067] using random host ethernet address
tatus /dev/rfkill Watch.
         Mounting /media/BOOT-mmcblk0p1...
         Starting Connection service...
[    9.661102] usb 1-1.2: New USB device found, idVendor=046d, idProduct=c52b, bcdDevice=24.00
[    9.669814] usb 1-1.2: New USB device strings: Mfr=1, Product=2, SerialNumber=0
[    9.669822] usb 1-1.2: Product: USB Receiver
[    9.669826] usb 1-1.2: Manufacturer: Logitech
[  OK  ] Mounted /media/BOOT-mmcblk0p1.
[  OK  ] Started Telephony service.
         Mounting /boot...
[  OK  ] Mounted /boot.
[    9.782767] usb0: HOST MAC 62:2c:14:fe:63:53
[    9.782777] usb0: MAC 62:d0:d8:13:63:9e
[  OK  ] Finished Load default USB gadget schema g1.schema.
[  OK  ] Started User Login Management.
[    9.834097] input: Logitech USB Receiver as /devices/platform/bus@f0000/f910000.dwc3-usb/31100000.usb/xhci-hcd.3.auto/usb1/1-1/1-1.2/1-1.2:1.0/0003:046D:C52B.0001/input/input2
[  OK  ] Started Connection service.
[    9.864633] usb 1-1.4: new high-speed USB device number 4 using xhci-hcd
[  OK  ] Reached target Hardware activated USB gadget.
[    9.910322] hid-generic 0003:046D:C52B.0001: input: USB HID v1.11 Keyboard [Logitech USB Receiver] on usb-xhci-hcd.3.auto-1.2/input0
         Starting Avahi mDNS/DNS-SD Stack...
[    9.929563] input: Logitech USB Receiver Mouse as /devices/platform/bus@f0000/f910000.dwc3-usb/31100000.usb/xhci-hcd.3.auto/usb1/1-1/1-1.2/1-1.2:1.1/0003:046D:C52B.0002/input/input3
         Starting Network Configuration...
[    9.947656] input: Logitech USB Receiver Consumer Control as /devices/platform/bus@f0000/f910000.dwc3-usb/31100000.usb/xhci-hcd.3.auto/usb1/1-1/1-1.2/1-1.2:1.1/0003:046D:C52B.0002/input
/input4
[    9.970224] usb 1-1.4: New USB device found, idVendor=0424, idProduct=2740, bcdDevice= 2.00
[    9.978804] usb 1-1.4: New USB device strings: Mfr=1, Product=2, SerialNumber=0
[    9.990898] usb 1-1.4: Product: Hub Controller
[    9.996428] usb 1-1.4: Manufacturer: Microchip Tech
[    9.997845] am65-cpsw-nuss 8000000.ethernet eth0: PHY [8000f00.mdio:00] driver [TI DP83867] (irq=375)
         Starting WPA supplicant...
[   10.016975] am65-cpsw-nuss 8000000.ethernet eth0: configuring for phy/rgmii-rxid link mode
[   10.035304] input: Logitech USB Receiver System Control as /devices/platform/bus@f0000/f910000.dwc3-usb/31100000.usb/xhci-hcd.3.auto/usb1/1-1/1-1.2/1-1.2:1.1/0003:046D:C52B.0002/input/i
nput5
[  OK  ] Started Avahi mDNS/DNS-SD Stack.
[   10.059324] hid-generic 0003:046D:C52B.0002: input,hiddev96: USB HID v1.11 Mouse [Logitech USB Receiver] on usb-xhci-hcd.3.auto-1.2/input1
[   10.072205] am65-cpsw-nuss 8000000.ethernet eth1: PHY [8000f00.mdio:07] driver [Microchip KSZ9131 Gigabit PHY] (irq=388)
[   10.084719] am65-cpsw-nuss 8000000.ethernet eth1: configuring for phy/rgmii-rxid link mode
         Starting Hostname Service...
[   10.100202] hid-generic 0003:046D:C52B.0003: hiddev97: USB HID v1.11 Device [Logitech USB Receiver] on usb-xhci-hcd.3.auto-1.2/input2
[   10.115105] usbcore: registered new interface driver usbhid
[   10.123108] usbhid: USB HID core driver
[  OK  ] Started WPA supplicant.
[   10.354488] cfg80211: Loading compiled-in X.509 certificates for regulatory database
[   10.371568] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
[  OK  ] Started Network Configuration.
[  OK  ] Reached target Network.
[  OK  ] Started NFS status monitor for NFSv2/3 locking..
         Starting Permit User Sessions...
[  OK  ] Finished Permit User Sessions.
[  OK  ] Started Getty on tty1.
[  OK  ] Started Serial Getty on ttyS0.
[  OK  ] Started Serial Getty on ttyS2.
[  OK  ] Reached target Login Prompts.
[  OK  ] Reached target Multi-User System.
         Starting Weston, a Wayland�…ositor, as a system service...
[  OK  ] Started Hostname Service.
         Starting User Database Manager...
[   10.813953] IPv6: ADDRCONF(NETDEV_CHANGE): usb0: link becomes ready
[  OK  ] Started User Database Manager.
[  OK  ] Created slice User Slice of UID 0.
         Starting User Runtime Directory /run/user/0...
[  OK  ] Finished User Runtime Directory /run/user/0.
         Starting User Manager for UID 0...
[  OK  ] Started User Manager for UID 0.
[  OK  ] Started Session c1 of User root.
[FAILED] Failed to start Weston, a �…mpositor, as a system service.
See 'systemctl status weston.service' for details.
[DEPEND] Dependency failed for Start a wayland application.
[  OK  ] Reached target Graphical Interface.
         Starting Record Runlevel Change in UTMP...
[  OK  ] Finished Record Runlevel Change in UTMP.

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

                +/-电源域=<&K3_PDS 70 TI_SCI_PD_shared>;

    为什么您必须删除此 DT 属性?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我认为基于这个原因: https://lore.kernel.org/all/20230417133308.1990057-1-kamlesh@ti.com/

    当然、 如果我没有删除加密节点未正确探测的属性、则只是 EPROBE_DEPEND 永久。

    root@verdin-am62-14917616:~# cat /sys/kernel/debug/devices_deferred 
    40900000.crypto
    

    我应该在这里做一些不同的事情吗?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    好的、我将在下周尝试重现并返回给您。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    有更新吗? 您能否确认这是一个影响 TI EVM 而不是我的集成的一般问题?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    +//            power-domain =<&K3_PDS 70 TI_SCI_PD_shared>;

    您可能不应删除该线路、需要该线路为加密模块启用电源。 但是、索引"70"未在 TI SCI 用户指南中列出、这使我很想知道是否可以在 Linux 中访问加密模块。

    我将对此进行深入研究、一旦有了更新、就会向您回复。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    在电源域存在的情况下、加密驱动器永远不会进行探测、正如我所说的那样。

    尽管这是我测试没有这个变化和没有任何变化。

    来自 Vignesh Raghavendra ,在 lore.kernel.org/.../中

    更新的固件似乎讨厌 SA3UL PD 控制
    请求。 但较旧的固件只是忽略了该调用,因为 SA3UL PD
    默认为 on。 因此、单独这个 DT 补丁不会有
    前向/后向兼容性。 


  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    来自 Vignesh Raghavendra ,在 lore.kernel.org/.../

    感谢您的关注。 现在、我了解为什么应该删除该 DT 节点。

    我将在内部进行检查、以了解是否应通过此 DT 更改探测加密驱动程序。 我会继续向您发布信息。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    您指向内核社区对话的链接暗示了该解决方案,rng 节点中的"Clocks"属性也应该删除。 请查看下面的完整 DT 补丁。

    diff --git a/arch/arm64/boot/dts/ti/k3-am62-main.dtsi b/arch/arm64/boot/dts/ti/k3-am62-main.dtsi
    index 510775e9a88f..1b313b54908a 100644
    --- a/arch/arm64/boot/dts/ti/k3-am62-main.dtsi
    +++ b/arch/arm64/boot/dts/ti/k3-am62-main.dtsi
    @@ -179,7 +179,6 @@ k3_reset: reset-controller {
            crypto: crypto@40900000 {
                    compatible = "ti,am62-sa3ul";
                    reg = <0x00 0x40900000 0x00 0x1200>;
    -               power-domains = <&k3_pds 70 TI_SCI_PD_SHARED>;
                    #address-cells = <2>;
                    #size-cells = <2>;
                    ranges = <0x00 0x40900000 0x00 0x40900000 0x00 0x30000>;
    @@ -192,8 +191,6 @@ rng: rng@40910000 {
                            compatible = "inside-secure,safexcel-eip76";
                            reg = <0x00 0x40910000 0x00 0x7d>;
                            interrupts = <GIC_SPI 129 IRQ_TYPE_LEVEL_HIGH>;
    -                       clocks = <&k3_clks 70 0>;
    -                       status = "disabled";
                    };
            };

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    谢谢、通过快速测试、它可以解决我报告的问题。

    还有几个问题需要回答、

    1.您能解释为什么需要移除这个时钟吗?

    2.您打算如何将此修复程序集成到 TI Linux 内核(v6.1或 v5.10)中?

    3.您打算如何将 HW RNG 支持集成到主线 Linux 内核中?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    1. 您能解释为什么需要删除此时钟吗?

    这与 Vignesh 评论删除了"电源域"属性的原因相同、DM 固件已为加密模块启用电源域和时钟、也不希望内核驱动程序请求"时钟"。

    2. 您打算如何将此修复程序集成到 TI Linux 内核(v6.1或 v5.10)中?

    我会向我们的软件开发团队提交错误通知单、以便在 TI 内核 v6.1中修复该问题。

    3. 您计划如何将 HW RNG 支持集成到主线 Linux 内核中?

    我将向我们的软件开发团队提出这方面的问题、并马上与您联系。