This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TDA4AL-Q1:如何配置 I2C2节点属性以启用 I2C2?

Guru**** 1472385 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1250510/tda4al-q1-how-to-configure-i2c2-node-property-for-enable-i2c2

器件型号:TDA4AL-Q1

您好!

目前、我们可以通过 i2c 刻录以太网固件。 现在、需要通过9068读取 SOC 的寄存器。 硬件已进行相应配置、但未在 Linux 软件中启用 I2C2、并且 i2cdetect 无法读取地址9068。 如何在 tda4-s2/linux sdk/board support/linux/arch/arm64/boot/dts/ti/k3-j721s2通用处理器板中配置与 I2C2node 相对应的属性和属性值。 DTS 文件。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    这是定制电路板还是 TI EVM? 多路复用器可能发生变化。 除此之外、我们需要将正确的引脚多路复用器连接到 MAIN_i2c2节点并将状态设置为
    设置为"可以"、表示 MAIN_i2c2器件树节点。

    此致、
    基尔西

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    这是一个定制的电路板。我做了以下修改,并在闪存机器之前编译了它。 开发板在启动期间可能会卡住、无法正常进入 Linux。我想问一下我的修改是否合理?

     -- a/board-support/linux/arch/arm64/boot/dts/ti/k3-j721s2-common-proc-board.dts
    ++ b/board-support/linux/arch/arm64/boot/dts/ti/k3-j721s2-common-proc-board.dts
    @@-320、6 +320、13 @@
    >;
    };

    + main_i2c2_pins_default:main-i2c2-pins-default {
    + pinctrl-single、pins =<
    + J721S2_IOPAD (0x04c、PIN_INPUT_PULLUP、13)/*(V27) I2C4_SCL */
    + J721S2_IOPAD (0x050、PIN_INPUT_PULLUP、13)/*(W27) I2C4_SDA */
    +>;
    +};
    +
    MAIN_i2c4_PINS_DEFAULT:MAIN-i2c4-PINS-DEFAULT{
    PINCCTRL-SINGLE、PINS =<
    //J721S2_IOPAD (0x014、PIN_INPUT_PULLUP、8)/*(AD25) I2C4_SCL */
    @@-548,7 +555,10 @@
    };

    &main_i2c2{
    -状态="已禁用";
    + pinctrl-names ="默认";
    + pinctrl-0 =<&main_i2c2_pins_default>;
    +时钟频率=<400000>;
    +
    };

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    您能否共享启动日志和故障点?

    pinmux 有2个可能的选项。

    您能否确保在定制板上使用的 V27/W27?

    -基尔西

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    U-Boot SPL 2021.01 (Jul 20 2023 - 18:02:11 +0800)
    ti_sci system-controller@44083000: Message not acknowledgedSYSFW ABI: 3.1 (firmware rev 0x0008 '8.6.3--v08.06.03 (Chill Capybar')
    EEPROM not available at 0x50, trying to read at 0x51
    Reading on-board EEPROM at 0x51 failed -19
    SPL initial stack usage: 13472 bytes
    Trying to boot from MMC2
    Starting ATF on ARM64 core...
    
    NOTICE:  BL31: v2.8(release):7953b4f
    NOTICE:  BL31: Built : 10:56:05, May 29 2023
    I/TC:
    I/TC: OP-TEE version: 97dc684 (gcc version 9.4.0 (Ubuntu 9.4.0-1ubuntu1~20.04.1)) #1 Mon May 29 02:56:44 UTC 2023 aarch64
    I/TC: WARNING: This OP-TEE configuration might be insecure!
    I/TC: WARNING: Please check optee.readthedocs.io/.../porting_guidelines.html
    I/TC: Primary CPU initializing
    I/TC: SYSFW ABI: 3.1 (firmware rev 0x0008 '8.6.3--v08.06.03 (Chill Capybar')
    I/TC: HUK Initialized
    I/TC: Activated SA2UL device
    I/TC: Fixing SA2UL firewall owner for GP device
    I/TC: Enabled firewalls for SA2UL TRNG device
    I/TC: SA2UL TRNG initialized
    I/TC: SA2UL Drivers initialized
    I/TC: Primary CPU switching to normal world boot
    
    U-Boot SPL 2021.01 (Jul 20 2023 - 18:46:46 +0800)
    ti_sci system-controller@44083000: Message not acknowledgedSYSFW ABI: 3.1 (firmware rev 0x0008 '8.6.3--v08.06.03 (Chill Capybar')
    EEPROM not available at 0x50, trying to read at 0x51
    Reading on-board EEPROM at 0x51 failed -19
    Trying to boot from MMC2
    
    
    U-Boot 2021.01 (Jul 20 2023 - 18:46:46 +0800)
    
    SoC:   J721S2 SR1.0 GP
    Model: Texas Instruments J721S2 EVM
    EEPROM not available at 0x50, trying to read at 0x51
    Reading on-board EEPROM at 0x51 failed -19
    Board: J721S2X-PM1-SOM rev E1
    DRAM:  4 GiB
    Flash: 0 Bytes
    MMC:   mmc@4f80000: 0, mmc@4fb0000: 1
    In:    serial@2800000
    Out:   serial@2800000
    Err:   serial@2800000
    Failed to probe am65_cpsw_nuss driver
    EEPROM not available at 0x50, trying to read at 0x51
    Reading on-board EEPROM at 0x51 failed -19
    Net:   No ethernet found.
    Hit any key to stop autoboot:  0
    switch to partitions #0, OK
    mmc1 is current device
    SD/MMC found on device 1
    Failed to load 'boot.scr'
    56 bytes read in 7 ms (7.8 KiB/s)
    Loaded env from uEnv.txt
    Importing environment from mmc1 ...
    k3_r5f_rproc r5f@41000000: Core 1 is already in use. No rproc commands work
    k3_r5f_rproc r5f@41400000: Core 2 is already in use. No rproc commands work
    719944 bytes read in 40 ms (17.2 MiB/s)
    Load Remote Processor 2 with data@addr=0x82000000 719944 bytes: Success!
    306092 bytes read in 22 ms (13.3 MiB/s)
    Load Remote Processor 3 with data@addr=0x82000000 306092 bytes: Success!
    Failed to load '/lib/firmware/j721s2-main-r5f1_0-fw'
    Failed to load '/lib/firmware/j721s2-main-r5f1_1-fw'
    14815296 bytes read in 621 ms (22.8 MiB/s)
    Load Remote Processor 6 with data@addr=0x82000000 14815296 bytes: Success!
    9760696 bytes read in 413 ms (22.5 MiB/s)
    Load Remote Processor 7 with data@addr=0x82000000 9760696 bytes: Success!
    19964416 bytes read in 831 ms (22.9 MiB/s)
    85134 bytes read in 11 ms (7.4 MiB/s)
    10329 bytes read in 8 ms (1.2 MiB/s)
    ## Flattened Device Tree blob at 88000000
       Booting using the fdt blob at 0x88000000
       Loading Device Tree to 000000008fee8000, end 000000008fffffff ... OK
    
    Starting kernel ...
    
    [    0.000000] Booting Linux on physical CPU 0x0000000000 [0x411fd080]
    [    0.000000] Linux version 5.10.162-g76b3e88d56 (linfei@linfei-Vostro-3671) (aarch64-none-linux-gnu-gcc (GNU Toolchain for the A-profile Architecture 9.2-2019.12 (arm-9.10)) 9.2.1 20191025, GNU ld (GNU Toolchain for the A-profile Architecture 9.2-2019.12 (arm-9.10)) 2.33.1.20191209) #1 SMP PREEMPT Thu Jul 20 17:50:15 CST 2023
    [    0.000000] Machine model: Texas Instruments J721S2 EVM
    [    0.000000] earlycon: ns16550a0 at MMIO32 0x0000000002800000 (options '')
    [    0.000000] printk: bootconsole [ns16550a0] enabled
    [    0.000000] efi: UEFI not found.
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000a0000000, size 1 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a0000000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000a0100000, size 15 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a0100000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000a1000000, size 1 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a1000000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000a1100000, size 15 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a1100000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000a2000000, size 1 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a2000000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000a2100000, size 31 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a2100000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000a4000000, size 1 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a4000000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000a4100000, size 31 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a4100000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000a6000000, size 1 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a6000000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000a6100000, size 15 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a6100000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000a7000000, size 1 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a7000000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000a7100000, size 15 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a7100000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000a8000000, size 32 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-rtos-ipc-memory-region@a8000000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000aa000000, size 96 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-dma-memory@aa000000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000b0000000, size 1 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-c71-dma-memory@b0000000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000b0100000, size 95 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-c71_0-memory@b0100000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000b6000000, size 1 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-c71_1-dma-memory@b6000000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000b6100000, size 31 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-c71_1-memory@b6100000, compatible id shared-dma-pool
    [    0.000000] OF: reserved mem: initialized node vision_apps_shared-memories, compatible id dma-heap-carveout
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000d8000000, size 64 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-core-heap-memory-lo@d8000000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x0000000880000000, size 704 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-core-heap-memory-hi@880000000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created CMA memory pool at 0x00000008ac000000, size 896 MiB
    [    0.000000] OF: reserved mem: initialized node linux-cma-buffers@8ac000000, compatible id shared-dma-pool
    [    0.000000] Zone ranges:
    [    0.000000]   DMA      [mem 0x0000000080000000-0x00000000ffffffff]
    [    0.000000]   DMA32    empty
    [    0.000000]   Normal   [mem 0x0000000100000000-0x00000008ffffefff]
    [    0.000000] Movable zone start for each node
    [    0.000000] Early memory node ranges
    [    0.000000]   node   0: [mem 0x0000000080000000-0x000000009e7fffff]
    [    0.000000]   node   0: [mem 0x000000009e800000-0x00000000b7ffffff]
    [    0.000000]   node   0: [mem 0x00000000b8000000-0x00000000d7ffffff]
    [    0.000000]   node   0: [mem 0x00000000d8000000-0x00000000dbffffff]
    [    0.000000]   node   0: [mem 0x00000000dc000000-0x00000000ffffefff]
    [    0.000000]   node   0: [mem 0x0000000880000000-0x00000008abffffff]
    [    0.000000]   node   0: [mem 0x00000008ac000000-0x00000008ffffefff]
    [    0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000008ffffefff]
    [    0.000000] On node 0, zone Normal: 1 pages in unavailable ranges
    [    0.000000] On node 0, zone Normal: 1 pages in unavailable ranges
    [    0.000000] psci: probing for conduit method from DT.
    [    0.000000] psci: PSCIv1.1 detected in firmware.
    [    0.000000] psci: Using standard PSCI v0.2 function IDs
    [    0.000000] psci: Trusted OS migration not required
    [    0.000000] psci: SMC Calling Convention v1.2
    [    0.000000] percpu: Embedded 22 pages/cpu s50392 r8192 d31528 u90112
    [    0.000000] Detected PIPT I-cache on CPU0
    [    0.000000] CPU features: detected: GIC system register CPU interface
    [    0.000000] CPU features: detected: EL2 vector hardening
    [    0.000000] CPU features: detected: ARM errata 1165522, 1319367, or 1530923
    [    0.000000] CPU features: detected: Spectre-BHB
    [    0.000000] CPU features: detected: ARM erratum 1742098
    [    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 1032190
    [    0.000000] Kernel command line: console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000 mtdparts=47040000.spi.0:512k(ospi.tiboot3),2m(ospi.tispl),4m(ospi.u-boot),256k(ospi.env),256k(ospi.env.backup),57088k@8m(ospi.rootfs),256k(ospi.phypattern);47034000.hyperbus:512k(hbmc.tiboot3),2m(hbmc.tispl),4m(hbmc.u-boot),256k(hbmc.env),-@8m(hbmc.rootfs) root=PARTUUID=8a1e00fd-02 rw rootfstype=ext4 rootwait
    [    0.000000] Dentry cache hash table entries: 524288 (order: 10, 4194304 bytes, linear)
    [    0.000000] Inode-cache hash table entries: 262144 (order: 9, 2097152 bytes, linear)
    [    0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
    [    0.000000] software IO TLB: mapped [mem 0x00000000fbfff000-0x00000000fffff000] (64MB)
    [    0.000000] Memory: 1383896K/4194296K available (11712K kernel code, 1192K rwdata, 4468K rodata, 1984K init, 456K bss, 1892896K reserved, 917504K cma-reserved)
    [    0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
    [    0.000000] rcu: Preemptible hierarchical RCU implementation.
    [    0.000000] rcu:     RCU event tracing is enabled.
    [    0.000000] rcu:     RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=2.
    [    0.000000]  Trampoline variant of Tasks RCU enabled.
    [    0.000000]  Tracing variant of Tasks RCU enabled.
    [    0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
    [    0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2
    [    0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
    [    0.000000] GICv3: GIC: Using split EOI/Deactivate mode
    [    0.000000] GICv3: 960 SPIs implemented
    [    0.000000] GICv3: 0 Extended SPIs implemented
    [    0.000000] GICv3: Distributor has no Range Selector support
    [    0.000000] GICv3: 16 PPIs implemented
    [    0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000001900000
    [    0.000000] ITS [mem 0x01820000-0x0182ffff]
    [    0.000000] GIC: enabling workaround for ITS: Socionext Synquacer pre-ITS
    [    0.000000] ITS@0x0000000001820000: Devices Table too large, reduce ids 20->19
    [    0.000000] ITS@0x0000000001820000: allocated 524288 Devices @8e4800000 (flat, esz 8, psz 64K, shr 0)
    [    0.000000] ITS: using cache flushing for cmd queue
    [    0.000000] GICv3: using LPI property table @0x00000008e4030000
    [    0.000000] GIC: using cache flushing for LPI property table
    [    0.000000] GICv3: CPU0: using allocated LPI pending table @0x00000008e4040000
    [    0.000000] arch_timer: cp15 timer(s) running at 200.00MHz (phys).
    [    0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x2e2049d3e8, max_idle_ns: 440795210634 ns
    [    0.000002] sched_clock: 56 bits at 200MHz, resolution 5ns, wraps every 4398046511102ns
    [    0.008404] Console: colour dummy device 80x25
    [    0.012973] Calibrating delay loop (skipped), value calculated using timer frequency.. 400.00 BogoMIPS (lpj=800000)
    [    0.023644] pid_max: default: 32768 minimum: 301
    [    0.028405] LSM: Security Framework initializing
    [    0.033169] Mount-cache hash table entries: 8192 (order: 4, 65536 bytes, linear)
    [    0.040757] Mountpoint-cache hash table entries: 8192 (order: 4, 65536 bytes, linear)
    [    0.049724] rcu: Hierarchical SRCU implementation.
    [    0.054821] Platform MSI: msi-controller@1820000 domain created
    [    0.061059] PCI/MSI: /bus@100000/interrupt-controller@1800000/msi-controller@1820000 domain created
    [    0.070367] EFI services will not be available.
    [    0.075116] smp: Bringing up secondary CPUs ...
    I/TC: Secondary CPU 1 initializing
    I/TC: Secondary CPU 1 switching to normal world boot
    [    0.088230] Detected PIPT I-cache on CPU1
    [    0.088257] GICv3: CPU1: found redistributor 1 region 0:0x0000000001920000
    [    0.088269] GICv3: CPU1: using allocated LPI pending table @0x00000008e4050000
    [    0.088312] CPU1: Booted secondary processor 0x0000000001 [0x411fd080]
    [    0.088380] smp: Brought up 1 node, 2 CPUs
    [    0.117731] SMP: Total of 2 processors activated.
    [    0.122537] CPU features: detected: 32-bit EL0 Support
    [    0.127793] CPU features: detected: CRC32 instructions
    [    0.142874] CPU: All CPU(s) started at EL2
    [    0.147082] alternatives: patching kernel code
    [    0.152241] devtmpfs: initialized
    [    0.160615] KASLR disabled due to lack of seed
    [    0.165287] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
    [    0.175256] futex hash table entries: 512 (order: 3, 32768 bytes, linear)
    [    0.197971] pinctrl core: initialized pinctrl subsystem
    [    0.203701] DMI not present or invalid.
    [    0.208003] NET: Registered protocol family 16
    [    0.213503] DMA: preallocated 512 KiB GFP_KERNEL pool for atomic allocations
    [    0.220817] DMA: preallocated 512 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
    [    0.228827] DMA: preallocated 512 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
    [    0.236972] ramoops: using module parameters
    [    0.241400] ramoops ramoops: no room for dmesg mem region (0xffffffffffffe000@0xdd000000) in (0x40000@0xdd000000)
    [    0.251901] ramoops: probe of ramoops failed with error -12
    [    0.257808] thermal_sys: Registered thermal governor 'step_wise'
    [    0.257811] thermal_sys: Registered thermal governor 'power_allocator'
    [    0.264474] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
    [    0.278126] ASID allocator initialised with 65536 entries
    [    0.284352] printk: console [ramoops-1] enabled
    [    0.288988] pstore: Registered ramoops as persistent store backend
    [    0.295303] ramoops: using 0x40000@0xdd000000, ecc: 0
    [    0.316721] HugeTLB registered 1.00 GiB page size, pre-allocated 0 pages
    [    0.323587] HugeTLB registered 32.0 MiB page size, pre-allocated 0 pages
    [    0.330440] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages
    [    0.337289] HugeTLB registered 64.0 KiB page size, pre-allocated 0 pages
    [    0.344896] cryptd: max_cpu_qlen set to 1000
    [    0.351182] k3-chipinfo 43000014.chipid: Family:J721S2 rev:SR1.0 JTAGID[0x0bb7502f] Detected
    [    0.360336] vsys_3v3: supplied by evm_12v0
    [    0.364779] vsys_5v0: supplied by evm_12v0
    [    0.369649] iommu: Default domain type: Translated
    [    0.374810] SCSI subsystem initialized
    [    0.378745] usbcore: registered new interface driver usbfs
    [    0.384373] usbcore: registered new interface driver hub
    [    0.389814] usbcore: registered new device driver usb
    [    0.395272] mc: Linux media interface: v0.10
    [    0.399649] videodev: Linux video capture interface: v2.00
    [    0.405285] pps_core: LinuxPPS API ver. 1 registered
    [    0.410357] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
    [    0.419696] PTP clock support registered
    [    0.423716] EDAC MC: Ver: 3.0.0
    [    0.427582] FPGA manager framework
    [    0.431109] Advanced Linux Sound Architecture Driver Initialized.
    [    0.437806] clocksource: Switched to clocksource arch_sys_counter
    [    0.444174] VFS: Disk quotas dquot_6.6.0
    [    0.448222] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
    [    0.458114] Carveout Heap: Exported 512 MiB at 0x00000000b8000000
    [    0.464419] NET: Registered protocol family 2
    [    0.469212] IP idents hash table entries: 65536 (order: 7, 524288 bytes, linear)
    [    0.477885] tcp_listen_portaddr_hash hash table entries: 2048 (order: 3, 32768 bytes, linear)
    [    0.486662] TCP established hash table entries: 32768 (order: 6, 262144 bytes, linear)
    [    0.494872] TCP bind hash table entries: 32768 (order: 7, 524288 bytes, linear)
    [    0.502668] TCP: Hash tables configured (established 32768 bind 32768)
    [    0.509533] UDP hash table entries: 2048 (order: 4, 65536 bytes, linear)
    [    0.516439] UDP-Lite hash table entries: 2048 (order: 4, 65536 bytes, linear)
    [    0.523866] NET: Registered protocol family 1
    [    0.528666] RPC: Registered named UNIX socket transport module.
    [    0.534730] RPC: Registered udp transport module.
    [    0.539551] RPC: Registered tcp transport module.
    [    0.544357] RPC: Registered tcp NFSv4.1 backchannel transport module.
    [    0.550941] NET: Registered protocol family 44
    [    0.555494] PCI: CLS 0 bytes, default 64
    [    0.559928] hw perfevents: enabled with armv8_cortex_a72 PMU driver, 7 counters available
    [    0.570738] Initialise system trusted keyrings
    [    0.575389] workingset: timestamp_bits=46 max_order=20 bucket_order=0
    [    0.583688] squashfs: version 4.0 (2009/01/31) Phillip Lougher
    [    0.590037] NFS: Registering the id_resolver key type
    [    0.595232] Key type id_resolver registered
    [    0.599510] Key type id_legacy registered
    [    0.603646] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
    [    0.610498] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...
    [    0.618165] 9p: Installing v9fs 9p2000 file system support
    [    0.643749] Key type asymmetric registered
    [    0.647940] Asymmetric key parser 'x509' registered
    [    0.652943] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 243)
    [    0.660503] io scheduler mq-deadline registered
    [    0.665129] io scheduler kyber registered
    [    0.670824] pinctrl-single 4301c000.pinctrl: 101 pins, size 404
    [    0.677064] pinctrl-single 11c000.pinctrl: 72 pins, size 288
    [    0.687953] Serial: 8250/16550 driver, 10 ports, IRQ sharing enabled
    [    0.701256] brd: module loaded
    [    0.708523] loop: module loaded
    [    0.712503] megasas: 07.714.04.00-rc1
    [    0.718398] tun: Universal TUN/TAP device driver, 1.6
    [    0.723892] igbvf: Intel(R) Gigabit Virtual Function Network Driver
    [    0.730305] igbvf: Copyright (c) 2009 - 2012 Intel Corporation.
    [    0.736391] sky2: driver version 1.30
    [    0.740828] VFIO - User Level meta-driver version: 0.3
    [    0.746772] i2c /dev entries driver
    [    0.751284] sdhci: Secure Digital Host Controller Interface driver
    [    0.757618] sdhci: Copyright(c) Pierre Ossman
    [    0.762402] sdhci-pltfm: SDHCI platform and OF driver helper
    [    0.768826] ledtrig-cpu: registered to indicate activity on CPUs
    [    0.775199] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping ....
    [    0.782126] ashmem: initialized
    [    0.786248] optee: probing for conduit method.
    I/TC: Reserved shared memory is enabled
    I/TC: Dynamic shared memory is enabled
    I/TC: Normal World virtualization support is disabled
    I/TC: Asynchronous notifications are disabled
    [    0.790820] optee: revision 3.20 (97dc6845)
    [    0.807215] optee: dynamic shared memory is enabled
    [    0.816706] optee: initialized driver
    [    0.822009] NET: Registered protocol family 17
    [    0.826651] 9pnet: Installing 9P2000 support
    [    0.831056] Key type dns_resolver registered
    [    0.835551] Loading compiled-in X.509 certificates
    [    0.841683] pstore: Invalid compression size for deflate: 0
    [    0.854319] ti-sci 44083000.system-controller: ABI: 3.1 (firmware rev 0x0008 '8.6.3--v08.06.03 (Chill Capybar')
    [    0.892801] omap_i2c 42120000.i2c: bus 0 rev0.12 at 100 kHz
    [    0.899011] omap_i2c 40b00000.i2c: bus 1 rev0.12 at 100 kHz
    [    0.905113] omap_i2c 40b10000.i2c: bus 2 rev0.12 at 100 kHz
    [    0.911490] pca953x 3-0021: supply vcc not found, using dummy regulator
    [    0.918331] pca953x 3-0021: using no AI
    [    0.945847] pca953x 3-0021: failed writing register
    [    0.950901] pca953x: probe of 3-0021 failed with error -121
    [    0.956842] pca953x 3-0020: supply vcc not found, using dummy regulator
    [    0.963657] pca953x 3-0020: using no AI
    [    0.967631] pca953x 3-0020: failed writing register
    [    0.972667] pca953x: probe of 3-0020 failed with error -121
    [    0.978556] pca953x 3-0022: supply vcc not found, using dummy regulator
    [    0.985360] pca953x 3-0022: using AI
    [    0.989066] pca953x 3-0022: failed writing register
    [    0.994093] pca953x: probe of 3-0022 failed with error -121
    [    0.999831] omap_i2c 2000000.i2c: bus 3 rev0.12 at 400 kHz
    [    1.006046] omap_i2c 2020000.i2c: bus 4 rev0.12 at 400 kHz
    [    1.012504] ti-sci-intr 42200000.interrupt-controller: Interrupt Router 125 domain created
    [    1.021080] ti-sci-intr bus@100000:interrupt-controller@a00000: Interrupt Router 148 domain created
    [    1.030426] ti-sci-intr 310e0000.interrupt-controller: Interrupt Router 227 domain created
    [    1.039098] ti-sci-inta 33d00000.msi-controller: Interrupt Aggregator domain 265 created
    [    1.048914] j721e-pcie 2910000.pcie: host bridge /bus@100000/pcie@2910000 ranges:
    [    1.056598] j721e-pcie 2910000.pcie:       IO 0x0018001000..0x0018010fff -> 0x0018001000
    [    1.064876] j721e-pcie 2910000.pcie:      MEM 0x0018011000..0x001fffffff -> 0x0018011000
    [    1.073162] j721e-pcie 2910000.pcie:   IB MEM 0x0000000000..0xffffffffffff -> 0x0000000000
    [    1.082262] ti-udma 311a0000.dma-controller: Number of rings: 48
    [    1.089064] ti-udma 311a0000.dma-controller: Channels: 24 (bchan: 0, tchan: 8, rchan: 16)
    [    1.098385] k3-ringacc 2b800000.ringacc: Ring Accelerator probed rings:286, gp-rings[96,20] sci-dev-id:272
    [    1.108271] k3-ringacc 2b800000.ringacc: dma-ring-reset-quirk: disabled
    [    1.115035] k3-ringacc 2b800000.ringacc: RA Proxy rev. 66349100, num_proxies:64
    [    1.124019] k3-ringacc 3c000000.ringacc: Ring Accelerator probed rings:1024, gp-rings[878,128] sci-dev-id:259
    [    1.134185] k3-ringacc 3c000000.ringacc: dma-ring-reset-quirk: disabled
    [    1.140947] k3-ringacc 3c000000.ringacc: RA Proxy rev. 66349100, num_proxies:64
    [    1.148653] omap8250 40a00000.serial: failed to get alias
    [    1.154427] pinctrl-single 11c000.pinctrl: pin PIN19 already requested by 2020000.i2c; cannot claim for 2800000.serial
    [    1.165376] pinctrl-single 11c000.pinctrl: pin-19 (2800000.serial) status -22
    [    1.172671] pinctrl-single 11c000.pinctrl: could not request pin 19 (PIN19) from group main_uart0_pins_default  on device pinctrl-single
    [    1.185205] omap8250 2800000.serial: Error applying setting, reverse things back
    [    1.192773] omap8250: probe of 2800000.serial failed with error -22
    [    1.202928] davinci_mdio 46000f00.mdio: Configuring MDIO in manual mode
    [    1.249814] davinci_mdio 46000f00.mdio: davinci mdio revision 9.7, bus freq 1000000
    [    1.257646] davinci_mdio 46000f00.mdio: no live phy, scanning all
    [    1.274759] am65-cpsw-nuss 46000000.ethernet: initializing am65 cpsw nuss version 0x6BA02102, cpsw version 0x6BA82102 Ports: 2 quirks:00000000
    [    1.287952] am65-cpsw-nuss 46000000.ethernet: initialized cpsw ale version 1.4
    [    1.295342] am65-cpsw-nuss 46000000.ethernet: ALE Table size 64
    [    1.301858] am65-cpsw-nuss 46000000.ethernet: CPTS ver 0x4e8a010b, freq:500000000, add_val:1 pps:0
    [    1.312514] am65-cpts 310d0000.cpts: CPTS ver 0x4e8a010c, freq:200000000, add_val:4 pps:0
    [    1.422660] mmc0: CQHCI version 5.10
    [    1.429927] vdd_mmc1: supplied by vsys_3v3
    [    1.435204] omap-mailbox 31f80000.mailbox: omap mailbox rev 0x66fca100
    [    1.442278] omap-mailbox 31f81000.mailbox: omap mailbox rev 0x66fca100
    [    1.449273] omap-mailbox 31f82000.mailbox: omap mailbox rev 0x66fca100
    [    1.456256] omap-mailbox 31f84000.mailbox: omap mailbox rev 0x66fca100
    [    1.463222] j721e-pcie 2910000.pcie: host bridge /bus@100000/pcie@2910000 ranges:
    [    1.466858] mmc0: SDHCI controller on 4f80000.mmc [4f80000.mmc] using ADMA 64-bit
    [    1.470890] j721e-pcie 2910000.pcie:       IO 0x0018001000..0x0018010fff -> 0x0018001000
    [    1.486807] j721e-pcie 2910000.pcie:      MEM 0x0018011000..0x001fffffff -> 0x0018011000
    [    1.495090] j721e-pcie 2910000.pcie:   IB MEM 0x0000000000..0xffffffffffff -> 0x0000000000
    [    1.504506] ti-udma 285c0000.dma-controller: Channels: 26 (tchan: 13, rchan: 13, gp-rflow: 8)
    [    1.514885] ti-udma 31150000.dma-controller: Channels: 60 (tchan: 30, rchan: 30, gp-rflow: 16)
    [    1.526019] davinci_mdio 46000f00.mdio: Configuring MDIO in manual mode
    [    1.569816] davinci_mdio 46000f00.mdio: davinci mdio revision 9.7, bus freq 1000000
    [    1.577648] davinci_mdio 46000f00.mdio: no live phy, scanning all
    [    1.594875] am65-cpsw-nuss 46000000.ethernet: initializing am65 cpsw nuss version 0x6BA02102, cpsw version 0x6BA82102 Ports: 2 quirks:00000000
    [    1.608069] am65-cpsw-nuss 46000000.ethernet: initialized cpsw ale version 1.4
    [    1.615459] am65-cpsw-nuss 46000000.ethernet: ALE Table size 64
    [    1.621686] mmc0: Command Queue Engine enabled
    [    1.622028] am65-cpsw-nuss 46000000.ethernet: CPTS ver 0x4e8a010b, freq:500000000, add_val:1 pps:0
    [    1.626255] mmc0: new DDR MMC card at address 0001
    [    1.640661] mmcblk0: mmc0:0001 DG4008 7.09 GiB
    [    1.645477] mmcblk0boot0: mmc0:0001 DG4008 partition 1 31.9 MiB
    [    1.651687] mmcblk0boot1: mmc0:0001 DG4008 partition 2 31.9 MiB
    [    1.657868] mmcblk0rpmb: mmc0:0001 DG4008 partition 3 4.00 MiB, chardev (236:0)
    [    1.657905] am65-cpsw-nuss 46000000.ethernet: set new flow-id-base 48
    [    1.666710]  mmcblk0: p1 p2
    [    1.677324] j721e-pcie 2910000.pcie: host bridge /bus@100000/pcie@2910000 ranges:
    [    1.677537] mmc1: CQHCI version 5.10
    [    1.685020] j721e-pcie 2910000.pcie:       IO 0x0018001000..0x0018010fff -> 0x0018001000
    [    1.696953] j721e-pcie 2910000.pcie:      MEM 0x0018011000..0x001fffffff -> 0x0018011000
    [    1.705238] j721e-pcie 2910000.pcie:   IB MEM 0x0000000000..0xffffffffffff -> 0x0000000000
    [    1.714954] j721e-pcie 2910000.pcie: host bridge /bus@100000/pcie@2910000 ranges:
    [    1.722642] j721e-pcie 2910000.pcie:       IO 0x0018001000..0x0018010fff -> 0x0018001000
    [    1.730927] mmc1: SDHCI controller on 4fb0000.mmc [4fb0000.mmc] using ADMA 64-bit
    [    1.738669] j721e-pcie 2910000.pcie:      MEM 0x0018011000..0x001fffffff -> 0x0018011000
    [    1.747013] j721e-pcie 2910000.pcie:   IB MEM 0x0000000000..0xffffffffffff -> 0x0000000000
    [    1.756473] j721e-pcie 2910000.pcie: host bridge /bus@100000/pcie@2910000 ranges:
    [    1.764159] j721e-pcie 2910000.pcie:       IO 0x0018001000..0x0018010fff -> 0x0018001000
    [    1.772502] j721e-pcie 2910000.pcie:      MEM 0x0018011000..0x001fffffff -> 0x0018011000
    [    1.780843] j721e-pcie 2910000.pcie:   IB MEM 0x0000000000..0xffffffffffff -> 0x0000000000
    [    1.789630] debugfs: Directory 'pd:39' with parent 'pm_genpd' already present!
    [    1.797205] debugfs: Directory 'pd:38' with parent 'pm_genpd' already present!
    [    1.805148] debugfs: Directory 'pd:276' with parent 'pm_genpd' already present!
    [    1.813226] debugfs: Directory 'pd:154' with parent 'pm_genpd' already present!
    [    1.827606] ALSA device list:
    [    1.830657]   No soundcards found.
    [    1.834183] Warning: unable to open an initial console.
    [    1.839637] Waiting for root device PARTUUID=8a1e00fd-02...
    [    1.870261] mmc1: new ultra high speed DDR50 SDXC card at address aaaa
    [    1.877416] mmcblk1: mmc1:aaaa SD64G 59.5 GiB
    [    1.884125]  mmcblk1: p1 p2
    [    1.888711] j721e-pcie 2910000.pcie: host bridge /bus@100000/pcie@2910000 ranges:
    [    1.896405] j721e-pcie 2910000.pcie:       IO 0x0018001000..0x0018010fff -> 0x0018001000
    [    1.904684] j721e-pcie 2910000.pcie:      MEM 0x0018011000..0x001fffffff -> 0x0018011000
    [    1.912969] j721e-pcie 2910000.pcie:   IB MEM 0x0000000000..0xffffffffffff -> 0x0000000000
    [    2.154790] EXT4-fs (mmcblk1p2): recovery complete
    [    2.162440] EXT4-fs (mmcblk1p2): mounted filesystem with ordered data mode. Opts: (null)
    [    2.170767] VFS: Mounted root (ext4 filesystem) on device 179:98.
    [    2.178354] devtmpfs: mounted
    [    2.182503] Freeing unused kernel memory: 1984K
    [    2.187260] Run /sbin/init as init process
    [    2.352898] systemd[1]: System time before build time, advancing clock.
    [    2.406311] NET: Registered protocol family 10
    [    2.411469] Segment Routing with IPv6
    [    2.442409] systemd[1]: systemd 244.5+ running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR -SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN2 -IDN -PCRE2 default-hierarchy=hybrid)
    [    2.464744] systemd[1]: Detected architecture arm64.
    [    2.488739] systemd[1]: Set hostname to <j721s2-evm>.
    [    2.658178] systemd[1]: /lib/systemd/system/irqbalanced.service:6: Unknown key name 'ConditionCPUs' in section 'Unit', ignoring.
    [    2.680461] systemd[1]: /lib/systemd/system/docker.socket:6: ListenStream= references a path below legacy directory /var/run/, updating /var/run/docker.sock \A1\FA /run/docker.sock; please update the unit file accordingly.
    [    2.705950] systemd[1]: /etc/systemd/system/auto-cam.service:2: Unknown key name 'Descriptiot' in section 'Unit', ignoring.
    [    2.760743] random: systemd: uninitialized urandom read (16 bytes read)
    [    2.769557] systemd[1]: Created slice system-getty.slice.
    [    2.775318] random: systemd: uninitialized urandom read (16 bytes read)
    [    2.782986] systemd[1]: Created slice system-serial\x2dgetty.slice.
    [    2.789495] random: systemd: uninitialized urandom read (16 bytes read)
    [    2.796977] systemd[1]: Created slice User and Session Slice.
    [    2.803072] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
    [    2.811295] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
    [    2.819159] systemd[1]: Reached target Paths.
    [    2.823682] systemd[1]: Reached target Remote File Systems.
    [    2.829429] systemd[1]: Reached target Slices.
    [    2.834027] systemd[1]: Reached target Swap.
    [    2.852213] systemd[1]: Listening on RPCbind Server Activation Socket.
    [    2.859106] systemd[1]: Reached target RPC Port Mapper.
    [    2.867261] systemd[1]: Listening on Process Core Dump Socket.
    [    2.873482] systemd[1]: Listening on initctl Compatibility Named Pipe.
    [    2.882333] systemd[1]: Condition check resulted in Journal Audit Socket being skipped.
    [    2.891011] systemd[1]: Listening on Journal Socket (/dev/log).
    [    2.897423] systemd[1]: Listening on Journal Socket.
    [    2.902914] systemd[1]: Listening on Network Service Netlink Socket.
    [    2.909696] systemd[1]: Listening on udev Control Socket.
    [    2.915415] systemd[1]: Listening on udev Kernel Socket.
    [    2.923730] systemd[1]: Mounting Huge Pages File System...
    [    2.932517] systemd[1]: Mounting POSIX Message Queue File System...
    [    2.941980] systemd[1]: Mounting Kernel Debug File System...
    [    2.952055] systemd[1]: Mounting Temporary Directory (/tmp)...
    [    2.961207] systemd[1]: Starting Create list of static device nodes for the current kernel...
    [    2.974691] systemd[1]: Starting Start psplash boot splash screen...
    [    2.984476] systemd[1]: Starting RPC Bind...
    [    2.989126] systemd[1]: Condition check resulted in File System Check on Root Device being skipped.
    [    3.000687] systemd[1]: Starting Journal Service...
    [    3.013800] systemd[1]: Starting Load Kernel Modules...
    [    3.023155] systemd[1]: Starting Remount Root and Kernel File Systems...
    [    3.033333] systemd[1]: Starting udev Coldplug all Devices...
    [    3.049355] systemd[1]: Started RPC Bind.
    [    3.049976] cryptodev: loading out-of-tree module taints kernel.
    [    3.060340] EXT4-fs (mmcblk1p2): re-mounted. Opts: (null)
    [    3.060354] systemd[1]: Mounted Huge Pages File System.
    [    3.072344] cryptodev: driver 1.10 loaded.
    [    3.078575] systemd[1]: Mounted POSIX Message Queue File System.
    [    3.089728] systemd[1]: Mounted Kernel Debug File System.
    [    3.102712] systemd[1]: Mounted Temporary Directory (/tmp).
    [    3.110368] systemd[1]: Started Create list of static device nodes for the current kernel.
    [    3.119799] systemd[1]: psplash-start.service: Main process exited, code=exited, status=255/EXCEPTION
    [    3.129909] systemd[1]: psplash-start.service: Failed with result 'exit-code'.
    [    3.138816] systemd[1]: Failed to start Start psplash boot splash screen.
    [    3.146003] systemd[1]: Dependency failed for Start psplash-systemd progress communication helper.
    [    3.155464] systemd[1]: psplash-systemd.service: Job psplash-systemd.service/start failed with result 'dependency'.
    [    3.166995] systemd[1]: Started Journal Service.
    [    3.202295] systemd-journald[167]: Received client request to flush runtime journal.
    [    3.707643] random: crng init done
    [    3.711216] random: 72 urandom warning(s) missed due to ratelimiting
    [    3.722573] j721e-pcie 2910000.pcie: host bridge /bus@100000/pcie@2910000 ranges:
    [    3.732542] j721e-pcie 2910000.pcie:       IO 0x0018001000..0x0018010fff -> 0x0018001000
    [    3.748152] j721e-pcie 2910000.pcie:      MEM 0x0018011000..0x001fffffff -> 0x0018011000
    [    3.759248] j721e-pcie 2910000.pcie:   IB MEM 0x0000000000..0xffffffffffff -> 0x0000000000
    [    3.771605] j721e-pcie 2910000.pcie: host bridge /bus@100000/pcie@2910000 ranges:
    [    3.781366] j721e-pcie 2910000.pcie:       IO 0x0018001000..0x0018010fff -> 0x0018001000
    [    3.796473] j721e-pcie 2910000.pcie:      MEM 0x0018011000..0x001fffffff -> 0x0018011000
    [    3.806294] CAN device driver interface
    [    3.809040] j721e-pcie 2910000.pcie:   IB MEM 0x0000000000..0xffffffffffff -> 0x0000000000
    [    3.827027] j721e-pcie 2910000.pcie: host bridge /bus@100000/pcie@2910000 ranges:
    [    3.839364] j721e-pcie 2910000.pcie:       IO 0x0018001000..0x0018010fff -> 0x0018001000
    [    3.849380] j721e-pcie 2910000.pcie:      MEM 0x0018011000..0x001fffffff -> 0x0018011000
    [    3.858531] j721e-pcie 2910000.pcie:   IB MEM 0x0000000000..0xffffffffffff -> 0x0000000000
    [    3.875253] cdns-mhdp8546 a000000.dp-bridge: no PHY configured
    [    3.887214] mmc1: Got data interrupt 0x00000002 even though no data operation was in progress.
    [    3.896037] mmc1: sdhci: ============ SDHCI REGISTER DUMP ===========
    [    3.902622] mmc1: sdhci: Sys addr:  0x000000f0 | Version:  0x00001004
    [    3.909204] mmc1: sdhci: Blk size:  0x00007200 | Blk cnt:  0x00000080
    [    3.915785] mmc1: sdhci: Argument:  0x00000000 | Trn mode: 0x00000033
    [    3.922364] mmc1: sdhci: Present:   0x01f70000 | Host ctl: 0x0000001f
    [    3.928943] mmc1: sdhci: Power:     0x0000000f | Blk gap:  0x00000080
    [    3.935522] mmc1: sdhci: Wake-up:   0x00000000 | Clock:    0x00000207
    [    3.942101] mmc1: sdhci: Timeout:   0x00000000 | Int stat: 0x00000000
    [    3.948680] mmc1: sdhci: Int enab:  0x03ff008b | Sig enab: 0x03ff008b
    [    3.955259] mmc1: sdhci: ACmd stat: 0x00000000 | Slot int: 0x00000000
    [    3.961839] mmc1: sdhci: Caps:      0x3de8c801 | Caps_1:   0x18002407
    [    3.968418] mmc1: sdhci: Cmd:       0x00000c1a | Max curr: 0x00000000
    [    3.974997] mmc1: sdhci: Resp[0]:   0x00000b00 | Resp[1]:  0x01dbd37f
    [    3.981577] mmc1: sdhci: Resp[2]:   0x325b5900 | Resp[3]:  0x00000900
    [    3.988155] mmc1: sdhci: Host ctl2: 0x0000000c
    [    3.992691] mmc1: sdhci: ADMA Err:  0x00000000 | ADMA Ptr: 0x00000008e599320c
    [    3.999980] mmc1: sdhci: ============================================
    [    4.030088] k3-dsp-rproc 64800000.dsp: assigned reserved memory node vision-apps-c71-dma-memory@b0000000
    [    4.040642] alloc_contig_range: [8ac100, 8ac400) PFNs busy
    [    4.047349] alloc_contig_range: [8ac200, 8ac500) PFNs busy
    [    4.047418] j721e-pcie 2910000.pcie: host bridge /bus@100000/pcie@2910000 ranges:
    [    4.067357] j721e-pcie 2910000.pcie:       IO 0x0018001000..0x0018010fff -> 0x0018001000
    [    4.079811] j721e-pcie 2910000.pcie:      MEM 0x0018011000..0x001fffffff -> 0x0018011000
    [    4.093905] j721e-pcie 2910000.pcie:   IB MEM 0x0000000000..0xffffffffffff -> 0x0000000000
    [    4.094680] k3-dsp-rproc 64800000.dsp: configured DSP for IPC-only mode
    [    4.110346] remoteproc remoteproc0: 64800000.dsp is available
    [    4.117112] remoteproc remoteproc0: attaching to 64800000.dsp
    [    4.123140] cdns-mhdp8546 a000000.dp-bridge: no PHY configured
    [    4.123937] remoteproc remoteproc0: unsupported resource 65538
    [    4.136763] k3-dsp-rproc 64800000.dsp: DSP initialized in IPC-only mode
    [    4.144758]  remoteproc0#vdev0buffer: assigned reserved memory node vision-apps-c71-dma-memory@b0000000
    [    4.155229] virtio_rpmsg_bus virtio0: rpmsg host is online
    [    4.160938] virtio_rpmsg_bus virtio0: creating channel rpmsg_chrdev addr 0xd
    [    4.162060] PVR_K:  198: Read BVNC 36.53.104.796 from HW device registers
    [    4.169150]  remoteproc0#vdev0buffer: registered virtio0 (type 7)
    [    4.181577] remoteproc remoteproc0: remote processor 64800000.dsp is now attached
    [    4.181620] j721e-pcie 2910000.pcie: host bridge /bus@100000/pcie@2910000 ranges:
    [    4.197031] j721e-pcie 2910000.pcie:       IO 0x0018001000..0x0018010fff -> 0x0018001000
    [    4.206403] k3-dsp-rproc 65800000.dsp: assigned reserved memory node vision-apps-c71_1-dma-memory@b6000000
    [    4.207497] PVR_K:  198: RGX Device registered BVNC 36.53.104.796 with 1 core in the system
    [    4.216341] j721e-pcie 2910000.pcie:      MEM 0x0018011000..0x001fffffff -> 0x0018011000
    [    4.225262] platform 41000000.r5f: R5F core may have been powered on by a different host, programmed state (0) != actual state (1)
    [    4.243718] j721e-pcie 2910000.pcie:   IB MEM 0x0000000000..0xffffffffffff -> 0x0000000000
    [    4.245700] platform 41000000.r5f: configured R5F for IPC-only mode
    [    4.254774] [drm] Initialized pvr 1.15.6133109 20170530 for 4e20000000.gpu on minor 0
    [    4.263792] k3-dsp-rproc 65800000.dsp: configured DSP for IPC-only mode
    [    4.270164] alloc_contig_range: [8ac300, 8ac600) PFNs busy
    [    4.275608] platform 41000000.r5f: assigned reserved memory node vision-apps-r5f-dma-memory@a0000000
    [    4.290652] cdns-mhdp8546 a000000.dp-bridge: no PHY configured
    [    4.290669] remoteproc remoteproc1: 65800000.dsp is available
    [    4.307042] j721e-pcie 2910000.pcie: host bridge /bus@100000/pcie@2910000 ranges:
    [    4.313287] remoteproc remoteproc2: 41000000.r5f is available
    [    4.320802] j721e-pcie 2910000.pcie:       IO 0x0018001000..0x0018010fff -> 0x0018001000
    [    4.321581] remoteproc remoteproc1: attaching to 65800000.dsp
    [    4.333957] j721e-pcie 2910000.pcie:      MEM 0x0018011000..0x001fffffff -> 0x0018011000
    [    4.336454] remoteproc remoteproc2: attaching to 41000000.r5f
    [    4.349700] j721e-pcie 2910000.pcie:   IB MEM 0x0000000000..0xffffffffffff -> 0x0000000000
    [    4.350277] remoteproc remoteproc1: unsupported resource 65538
    [    4.360400] platform 41000000.r5f: R5F core initialized in IPC-only mode
    [    4.364270] k3-dsp-rproc 65800000.dsp: DSP initialized in IPC-only mode
    [    4.379027]  remoteproc1#vdev0buffer: assigned reserved memory node vision-apps-c71_1-dma-memory@b6000000
    [    4.388940] cdns-mhdp8546 a000000.dp-bridge: no PHY configured
    [    4.389432] virtio_rpmsg_bus virtio1: rpmsg host is online
    [    4.400661] virtio_rpmsg_bus virtio1: creating channel rpmsg_chrdev addr 0xd
    [    4.408414]  remoteproc1#vdev0buffer: registered virtio1 (type 7)
    [    4.414898] remoteproc remoteproc1: remote processor 65800000.dsp is now attached
    [    4.425123]  remoteproc2#vdev0buffer: assigned reserved memory node vision-apps-r5f-dma-memory@a0000000
    [    4.434979] j721e-pcie 2910000.pcie: host bridge /bus@100000/pcie@2910000 ranges:
    [    4.435987] virtio_rpmsg_bus virtio2: rpmsg host is online
    [    4.448412]  remoteproc2#vdev0buffer: registered virtio2 (type 7)
    [    4.448474] j721e-pcie 2910000.pcie:       IO 0x0018001000..0x0018010fff -> 0x0018001000
    [    4.455638] remoteproc remoteproc2: remote processor 41000000.r5f is now attached
    [    4.469886] j721e-pcie 2910000.pcie:      MEM 0x0018011000..0x001fffffff -> 0x0018011000
    [    4.470702] virtio_rpmsg_bus virtio2: creating channel rpmsg_chrdev addr 0xd
    [    4.490028] j721e-pcie 2910000.pcie:   IB MEM 0x0000000000..0xffffffffffff -> 0x0000000000
    [    4.495366] platform 5c00000.r5f: configured R5F for IPC-only mode
    [    4.508711] cdns-mhdp8546 a000000.dp-bridge: no PHY configured
    [    4.528952] j721e-pcie 2910000.pcie: host bridge /bus@100000/pcie@2910000 ranges:
    [    4.544328] j721e-pcie 2910000.pcie:       IO 0x0018001000..0x0018010fff -> 0x0018001000
    [    4.557887] j721e-pcie 2910000.pcie:      MEM 0x0018011000..0x001fffffff -> 0x0018011000
    [    4.572370] j721e-pcie 2910000.pcie:   IB MEM 0x0000000000..0xffffffffffff -> 0x0000000000
    [    4.597940] platform 5c00000.r5f: assigned reserved memory node vision-apps-r5f-dma-memory@a2000000
    [    4.615276] m_can_platform 40528000.can: m_can device registered (irq=19, version=32)
    [    4.625687] remoteproc remoteproc3: 5c00000.r5f is available
    [    4.630213] m_can_platform 40568000.can: m_can device registered (irq=21, version=32)
    [    4.635376] remoteproc remoteproc3: attaching to 5c00000.r5f
    [    4.650872] platform 5c00000.r5f: R5F core initialized in IPC-only mode
    [    4.651623] cdns-mhdp8546 a000000.dp-bridge: no PHY configured
    [    4.667098]  remoteproc3#vdev0buffer: assigned reserved memory node vision-apps-r5f-dma-memory@a2000000
    [    4.677276] m_can_platform 2701000.can: m_can device registered (irq=34, version=32)
    [    4.688118] m_can_platform 2711000.can: m_can device registered (irq=36, version=32)
    [    4.698323] virtio_rpmsg_bus virtio3: rpmsg host is online
    [    4.711369] m_can_platform 2721000.can: m_can device registered (irq=38, version=32)
    [    4.711738]  remoteproc3#vdev0buffer: registered virtio3 (type 7)
    [    4.724684] m_can_platform 27d1000.can: m_can device registered (irq=40, version=32)
    [    4.730384] remoteproc remoteproc3: remote processor 5c00000.r5f is now attached
    [    4.740945] m_can_platform 2681000.can: m_can device registered (irq=42, version=32)
    [    4.754170] m_can_platform 2691000.can: m_can device registered (irq=44, version=32)
    [    4.772026] m_can_platform 26a1000.can: m_can device registered (irq=46, version=32)
    [    4.781304] platform 5d00000.r5f: configured R5F for IPC-only mode
    [    4.788014] platform 5d00000.r5f: assigned reserved memory node vision-apps-r5f-dma-memory@a4000000
    [    4.789924] j721e-pcie 2910000.pcie: host bridge /bus@100000/pcie@2910000 ranges:
    [    4.799365] j721e-pcie 2910000.pcie:       IO 0x0018001000..0x0018010fff -> 0x0018001000
    [    4.816817] j721e-pcie 2910000.pcie:      MEM 0x0018011000..0x001fffffff -> 0x0018011000
    [    4.827480] j721e-pcie 2910000.pcie:   IB MEM 0x0000000000..0xffffffffffff -> 0x0000000000
    [    4.840662] cdns-mhdp8546 a000000.dp-bridge: no PHY configured
    [    4.858800] remoteproc remoteproc4: 5d00000.r5f is available
    [    4.903137] remoteproc remoteproc4: attaching to 5d00000.r5f
    [    4.909392] platform 5d00000.r5f: R5F core initialized in IPC-only mode
    [    4.918015] virtio_rpmsg_bus virtio3: creating channel rpmsg_chrdev addr 0xd
    [    4.928048]  remoteproc4#vdev0buffer: assigned reserved memory node vision-apps-r5f-dma-memory@a4000000
    [    4.938421] virtio_rpmsg_bus virtio4: rpmsg host is online
    [    4.947039]  remoteproc4#vdev0buffer: registered virtio4 (type 7)
    [    4.953572] j721e-pcie 2910000.pcie: host bridge /bus@100000/pcie@2910000 ranges:
    [    4.962122] j721e-pcie 2910000.pcie:       IO 0x0018001000..0x0018010fff -> 0x0018001000
    [    4.966586] remoteproc remoteproc4: remote processor 5d00000.r5f is now attached
    [    4.970507] j721e-pcie 2910000.pcie:      MEM 0x0018011000..0x001fffffff -> 0x0018011000
    [    4.987397] j721e-pcie 2910000.pcie:   IB MEM 0x0000000000..0xffffffffffff -> 0x0000000000
    [    4.996625] virtio_rpmsg_bus virtio3: creating channel rpmsg_chrdev addr 0x15
    [    5.004486] cdns-mhdp8546 a000000.dp-bridge: no PHY configured
    [    5.010660] virtio_rpmsg_bus virtio3: creating channel ti.ipc4.ping-pong addr 0xe
    [    5.018625] virtio_rpmsg_bus virtio4: creating channel rpmsg_chrdev addr 0xd
    [    5.025993] virtio_rpmsg_bus virtio4: creating channel rpmsg_chrdev addr 0x15
    [    5.035915] virtio_rpmsg_bus virtio4: creating channel ti.ipc4.ping-pong addr 0xe
    [    5.043770] virtio_rpmsg_bus virtio0: creating channel rpmsg_chrdev addr 0x15
    [    5.051250] virtio_rpmsg_bus virtio0: creating channel ti.ipc4.ping-pong addr 0xe
    [    5.059101] virtio_rpmsg_bus virtio1: creating channel rpmsg_chrdev addr 0x15
    [    5.066568] virtio_rpmsg_bus virtio1: creating channel ti.ipc4.ping-pong addr 0xe
    [    5.074401] virtio_rpmsg_bus virtio2: creating channel rpmsg_chrdev addr 0x15
    [    5.081956] virtio_rpmsg_bus virtio2: creating channel ti.ipc4.ping-pong addr 0xe
    [    5.094121] j721e-pcie 2910000.pcie: host bridge /bus@100000/pcie@2910000 ranges:
    [    5.101862] j721e-pcie 2910000.pcie:       IO 0x0018001000..0x0018010fff -> 0x0018001000
    [    5.110205] j721e-pcie 2910000.pcie:      MEM 0x0018011000..0x001fffffff -> 0x0018011000
    [    5.121059] j721e-pcie 2910000.pcie:   IB MEM 0x0000000000..0xffffffffffff -> 0x0000000000
    [    5.134027] cdns-mhdp8546 a000000.dp-bridge: no PHY configured
    [    5.145724] platform 5e00000.r5f: configured R5F for remoteproc mode
    [    5.254083] platform 5e00000.r5f: assigned reserved memory node vision-apps-r5f-dma-memory@a6000000
    [    5.301604] remoteproc remoteproc5: 5e00000.r5f is available
    [    5.310674] remoteproc remoteproc5: Direct firmware load for j721s2-main-r5f1_0-fw failed with error -2
    [    5.323210] platform 5f00000.r5f: configured R5F for remoteproc mode
    [    5.323407] remoteproc remoteproc5: powering up 5e00000.r5f
    [    5.340939] remoteproc remoteproc5: Direct firmware load for j721s2-main-r5f1_0-fw failed with error -2
    [    5.352591] remoteproc remoteproc5: request_firmware failed: -2
    [    5.411075] platform 5f00000.r5f: assigned reserved memory node vision-apps-r5f-dma-memory@a7000000
    [    5.505127] remoteproc remoteproc6: 5f00000.r5f is available
    [    5.516604] remoteproc remoteproc6: Direct firmware load for j721s2-main-r5f1_1-fw failed with error -2
    [    5.528360] remoteproc remoteproc6: powering up 5f00000.r5f
    [    5.535406] remoteproc remoteproc6: Direct firmware load for j721s2-main-r5f1_1-fw failed with error -2
    [    5.546733] remoteproc remoteproc6: request_firmware failed: -2
    [    5.554588] j721e-pcie 2910000.pcie: host bridge /bus@100000/pcie@2910000 ranges:
    [    5.564286] j721e-pcie 2910000.pcie:       IO 0x0018001000..0x0018010fff -> 0x0018001000
    [    5.572700] j721e-pcie 2910000.pcie:      MEM 0x0018011000..0x001fffffff -> 0x0018011000
    [    5.581094] j721e-pcie 2910000.pcie:   IB MEM 0x0000000000..0xffffffffffff -> 0x0000000000
    [    5.590438] cdns-mhdp8546 a000000.dp-bridge: no PHY configured
    [    5.842764] j721e-pcie 2910000.pcie: host bridge /bus@100000/pcie@2910000 ranges:
    [    5.853486] j721e-pcie 2910000.pcie:       IO 0x0018001000..0x0018010fff -> 0x0018001000
    [    5.868490] j721e-pcie 2910000.pcie:      MEM 0x0018011000..0x001fffffff -> 0x0018011000
    [    5.881776] j721e-pcie 2910000.pcie:   IB MEM 0x0000000000..0xffffffffffff -> 0x0000000000
    [    5.898659] cdns-mhdp8546 a000000.dp-bridge: no PHY configured
    [    5.910178] j721e-pcie 2910000.pcie: host bridge /bus@100000/pcie@2910000 ranges:
    [    5.922287] j721e-pcie 2910000.pcie:       IO 0x0018001000..0x0018010fff -> 0x0018001000
    [    5.936503] j721e-pcie 2910000.pcie:      MEM 0x0018011000..0x001fffffff -> 0x0018011000
    [    5.949746] j721e-pcie 2910000.pcie:   IB MEM 0x0000000000..0xffffffffffff -> 0x0000000000
    [    5.969216] cdns-mhdp8546 a000000.dp-bridge: no PHY configured
    [    5.978915] j721e-pcie 2910000.pcie: host bridge /bus@100000/pcie@2910000 ranges:
    [    5.986609] j721e-pcie 2910000.pcie:       IO 0x0018001000..0x0018010fff -> 0x0018001000
    [    6.001450] j721e-pcie 2910000.pcie:      MEM 0x0018011000..0x001fffffff -> 0x0018011000
    [    6.015882] j721e-pcie 2910000.pcie:   IB MEM 0x0000000000..0xffffffffffff -> 0x0000000000
    [    6.027914] cdns-mhdp8546 a000000.dp-bridge: no PHY configured
    [    6.039428] j721e-pcie 2910000.pcie: host bridge /bus@100000/pcie@2910000 ranges:
    [    6.050020] j721e-pcie 2910000.pcie:       IO 0x0018001000..0x0018010fff -> 0x0018001000
    [    6.061884] j721e-pcie 2910000.pcie:      MEM 0x0018011000..0x001fffffff -> 0x0018011000
    [    6.073881] j721e-pcie 2910000.pcie:   IB MEM 0x0000000000..0xffffffffffff -> 0x0000000000
    [    6.180128] xhci-hcd xhci-hcd.2.auto: xHCI Host Controller
    [    6.255072] xhci-hcd xhci-hcd.2.auto: new USB bus registered, assigned bus number 1
    [    6.269445] xhci-hcd xhci-hcd.2.auto: hcc params 0x200073c9 hci version 0x100 quirks 0x0000002000010010
    [    6.284147] xhci-hcd xhci-hcd.2.auto: irq 514, io mem 0x06010000
    [    6.293883] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 5.10
    [    6.303530] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
    [    6.316159] usb usb1: Product: xHCI Host Controller
    [    6.321232] usb usb1: Manufacturer: Linux 5.10.162-g76b3e88d56 xhci-hcd
    [    6.330350] usb usb1: SerialNumber: xhci-hcd.2.auto
    [    6.339211] hub 1-0:1.0: USB hub found
    [    6.350083] hub 1-0:1.0: 1 port detected
    [    6.354830] cdns-mhdp8546 a000000.dp-bridge: no PHY configured
    [    6.362662] xhci-hcd xhci-hcd.2.auto: xHCI Host Controller
    [    6.368521] j721e-pcie 2910000.pcie: host bridge /bus@100000/pcie@2910000 ranges:
    [    6.376328] j721e-pcie 2910000.pcie:       IO 0x0018001000..0x0018010fff -> 0x0018001000
    [    6.384669] j721e-pcie 2910000.pcie:      MEM 0x0018011000..0x001fffffff -> 0x0018011000
    [    6.389614] xhci-hcd xhci-hcd.2.auto: new USB bus registered, assigned bus number 2
    [    6.395157] j721e-pcie 2910000.pcie:   IB MEM 0x0000000000..0xffffffffffff -> 0x0000000000
    [    6.410188] cdns-mhdp8546 a000000.dp-bridge: no PHY configured
    [    6.419599] j721e-pcie 2910000.pcie: host bridge /bus@100000/pcie@2910000 ranges:
    [    6.427857] j721e-pcie 2910000.pcie:       IO 0x0018001000..0x0018010fff -> 0x0018001000
    [    6.436222] j721e-pcie 2910000.pcie:      MEM 0x0018011000..0x001fffffff -> 0x0018011000
    [    6.447034] j721e-pcie 2910000.pcie:   IB MEM 0x0000000000..0xffffffffffff -> 0x0000000000
    [    6.450985] xhci-hcd xhci-hcd.2.auto: Host supports USB 3.0 SuperSpeed
    [    6.462988] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM.
    [    6.471558] usb usb2: New USB device found, idVendor=1d6b, idProduct=0003, bcdDevice= 5.10
    [    6.484255] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
    [    6.494287] usb usb2: Product: xHCI Host Controller
    [    6.510591] usb usb2: Manufacturer: Linux 5.10.162-g76b3e88d56 xhci-hcd
    [    6.517475] usb usb2: SerialNumber: xhci-hcd.2.auto
    [    6.517909] hub 2-0:1.0: USB hub found
    [    6.517940] hub 2-0:1.0: 1 port detected
    [    6.518556] cdns-mhdp8546 a000000.dp-bridge: no PHY configured
    [    6.519919] j721e-pcie 2910000.pcie: host bridge /bus@100000/pcie@2910000 ranges:
    [    6.548024] j721e-pcie 2910000.pcie:       IO 0x0018001000..0x0018010fff -> 0x0018001000
    [    6.556567] j721e-pcie 2910000.pcie:      MEM 0x0018011000..0x001fffffff -> 0x0018011000
    [    6.564981] j721e-pcie 2910000.pcie:   IB MEM 0x0000000000..0xffffffffffff -> 0x0000000000
    [    6.577744] cdns-mhdp8546 a000000.dp-bridge: no PHY configured
    [    6.590090] j721e-pcie 2910000.pcie: host bridge /bus@100000/pcie@2910000 ranges:
    [    6.597866] j721e-pcie 2910000.pcie:       IO 0x0018001000..0x0018010fff -> 0x0018001000
    [    6.606342] j721e-pcie 2910000.pcie:      MEM 0x0018011000..0x001fffffff -> 0x0018011000
    [    6.614776] j721e-pcie 2910000.pcie:   IB MEM 0x0000000000..0xffffffffffff -> 0x0000000000
    [    6.746236] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
    [    7.179578] Bluetooth: Core ver 2.22
    [    7.187051] NET: Registered protocol family 31
    [    7.193925] Bluetooth: HCI device and connection manager initialized
    [    7.205909] Bluetooth: HCI socket layer initialized
    [    7.210985] Bluetooth: L2CAP socket layer initialized
    [    7.216251] Bluetooth: SCO socket layer initialized
    [    7.328136] am65-cpsw-nuss 46000000.ethernet eth0: configuring for fixed/rgmii-id link mode
    [    7.356191] am65-cpsw-nuss 46000000.ethernet eth0: Link is Up - 1Gbps/Full - flow control off
    [   12.788698] file system registered
    [   13.835627] read descriptors
    [   13.845818] read strings

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Li

    此故障似乎与 I2C2无关。 您能否共享导致此引导失败的确切差异修补程序? 此外、如果没有 i2c2更改、此启动是否正常?

    此致、

    基尔西  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    此版本可以正常启动、无需任何修改。 我的修改如下:

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Li

    我怀疑您的电路板使用 i2c2引脚实现了其他目的。 您能否检查 i2c2引脚是否用于与 i2c2配置混淆的任何其他模块?

    此致、

    基尔西