This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TMDXIDK5718:AM5718

Guru**** 670150 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1248807/tmdxidk5718-am5718

器件型号:TMDXIDK5718

您好!

我正在尝试在 CCS 中运行 Hello World、但收到此错误。

Cortex_M4_IPU1_C0: GEL Output: --->>> AM571x Cortex M4 Startup Sequence In Progress... <<<---
Cortex_M4_IPU1_C0: GEL Output: --->>> AM571x Cortex M4 Startup Sequence DONE! <<<---
Cortex_M4_IPU1_C1: GEL Output: --->>> AM571x Cortex M4 Startup Sequence In Progress... <<<---
Cortex_M4_IPU1_C1: GEL Output: --->>> AM571x Cortex M4 Startup Sequence DONE! <<<---
C66xx_DSP: GEL Output: --->>> AM571x C66x DSP Startup Sequence In Progress... <<<---
C66xx_DSP: GEL Output: --->>> AM571x C66x DSP Startup Sequence DONE! <<<---
CortexA15_0: GEL Output: --->>> AM571x Cortex A15 Startup Sequence In Progress... <<<---
CortexA15_0: GEL Output: --->>> AM571x Cortex A15 Startup Sequence DONE! <<<---
IcePick_D: GEL Output: Ipu RTOS is released from Wait-In-Reset. 
IcePick_D: GEL Output: Ipu SIMCOP is released from Wait-In-Reset. 
IcePick_D: GEL Output: IVAHD C66 is released from Wait-In-Reset. 
IcePick_D: GEL Output: IVAHD ICONT1 is released from Wait-In-Reset. 
IcePick_D: GEL Output: IVAHD ICONT2 is released from Wait-In-Reset. 
CS_DAP_DebugSS: GEL Output: --->>> CONFIGURE DEBUG DPLL settings to 1.9 GHZs  <<<---
CS_DAP_DebugSS: GEL Output: > Setup DebugSS 1.9GHz in progress...
CS_DAP_DebugSS: GEL Output: < Done with Setup DebugSS Trace export clock (TPIU) to 97MHz 
CS_DAP_DebugSS: GEL Output: < Done with Setup DebugSS PLL Clocking 1.9GHz 
CS_DAP_DebugSS: GEL Output: < Done with Setup DebugSS ATB Clocking 380MHz 
CS_DAP_DebugSS: GEL Output: < Done with Setup DebugSS Trace export clock (TPIU) to 97MHz 
CS_DAP_DebugSS: GEL Output: --->>> TURNING ON L3_INSTR and L3_3 clocks required for debug instrumention <<<<<<----
CS_DAP_DebugSS: GEL Output: ---<<< L3 instrumentation clocks are enabled >>>> ---
CS_DAP_DebugSS: GEL Output: --->>> Mapping TIMER supsend sources to default cores <<<<<<----
CS_DAP_PC: GEL Output: Cortex-A15 1 is not in WIR mode so nothing to do.
CortexA15_0: GEL Output: --->>> AM571x Target Connect Sequence Begins ... <<<---
CortexA15_0: GEL Output: 	--->>> AM571x PG2.0 GP device <<<---
CortexA15_0: GEL Output: --->>> PRCM Clock Configuration for OPPNOM in progress... <<<---
CortexA15_0: GEL Output: 	Cortex A15 DPLL OPP 0 clock config is in progress...
CortexA15_0: GEL Output: 	Cortex A15 DPLL is already locked, now unlocking...  
CortexA15_0: GEL Output: 	Cortex A15 DPLL OPP 0 is DONE!
CortexA15_0: GEL Output: 	IVA DPLL OPP 0 clock config is in progress...
CortexA15_0: GEL Output: 	IVA DPLL OPP 0 is DONE!
CortexA15_0: GEL Output: 	PER DPLL OPP 0 clock config in progress...
CortexA15_0: GEL Output: 	PER DPLL already locked, now unlocking  
CortexA15_0: GEL Output: 	PER DPLL OPP 0 is DONE!
CortexA15_0: GEL Output: 	CORE DPLL OPP 0 clock config is in progress...
CortexA15_0: GEL Output: 	CORE DPLL OPP  already locked, now unlocking....  
CortexA15_0: GEL Output: 	CORE DPLL OPP 0 is DONE!
CortexA15_0: GEL Output: 	ABE DPLL OPP 0 clock config in progress...
CortexA15_0: GEL Output: 	ABE DPLL OPP 0 is DONE!
CortexA15_0: GEL Output: 	GMAC DPLL OPP 0 clock config is in progress...
CortexA15_0: GEL Output: 	GMAC DPLL OPP 0 is DONE!
CortexA15_0: GEL Output: 	GPU DPLL OPP 0 clock config is in progress...
CortexA15_0: GEL Output: 	GPU DPLL OPP 0 is DONE!
CortexA15_0: GEL Output: 	DSP DPLL OPP 0 clock config is in progress...
CortexA15_0: GEL Output: 	DSP DPLL OPP 0 is DONE!
CortexA15_0: GEL Output: 	PCIE_REF DPLL OPP 0 clock config is in progress...
CortexA15_0: GEL Output: 	PCIE_REF DPLL OPP 0 is DONE!
CortexA15_0: GEL Output: --->>> PRCM Clock Configuration for OPP 0 is DONE! <<<---
CortexA15_0: GEL Output: --->>> PRCM Configuration for all modules in progress... <<<---
CortexA15_0: GEL Output: --->>> PRCM Configuration for all modules is DONE! <<<---
CortexA15_0: GEL Output: --->>> DDR3 Initialization is in progress ... <<<---
CortexA15_0: GEL Output: 	DDR DPLL clock config for 666MHz is in progress...
CortexA15_0: GEL Output: 	DDR DPLL clock config for 666MHz is in DONE!
CortexA15_0: GEL Output:        Launch full leveling
CortexA15_0: GEL Output:        Updating slave ratios in PHY_STATUSx registers
CortexA15_0: GEL Output:        as per HW leveling output
CortexA15_0: GEL Output:        HW leveling is now disabled. Using slave ratios from 
CortexA15_0: GEL Output:        PHY_STATUSx registers
CortexA15_0: GEL Output: --->>> DDR3 Initialization is DONE! <<<---
CortexA15_0: GEL Output: --->>> Mapping TIMER supsend sources to default cores <<<<<<----
CortexA15_0: GEL Output: --->>> IPU1SS Initialization is in progress ... <<<---
CortexA15_0: GEL Output: --->>> IPU1SS Initialization is DONE! <<<---
CortexA15_0: GEL Output: --->>> IPU2SS Initialization is in progress ... <<<---
CortexA15_0: GEL Output: --->>> IPU2SS Initialization is DONE! <<<---
CortexA15_0: GEL Output: --->>> DSP1SS Initialization is in progress ... <<<---
CortexA15_0: GEL Output: DEBUG: Clock is active ... 
CortexA15_0: GEL Output: DEBUG: Checking for data integrity in DSPSS L2RAM ... 
CortexA15_0: GEL Output: DEBUG: Data integrity check in GEM L2RAM is sucessful! 
CortexA15_0: GEL Output: --->>> DSP1SS Initialization is DONE! <<<---
CortexA15_0: GEL Output: --->>> IVAHD Initialization is in progress ... <<<---
CortexA15_0: GEL Output: DEBUG: Clock is active ... 
CortexA15_0: GEL Output: --->>> IVAHD Initialization is DONE! ... <<<---
CortexA15_0: GEL Output: --->>> PRUSS 1 and 2 Initialization is in progress ... <<<---
CortexA15_0: GEL Output: --->>> PRUSS 1 and 2 Initialization is in complete ... <<<---
CortexA15_0: GEL Output: --->>> AM571x Target Connect Sequence DONE !!!!!  <<<---
CortexA15_0: File Loader: Verification failed: Values at address 0x00000020 do not match Please verify target memory and memory map.
CortexA15_0: GEL: File: C:\Users\223106495\Hello\Hola\Debug\Hola.out: a data verification error occurred, file load failed.
CortexA15_0: Unable to terminate memory download: NULL buffer pointer at 0x3aa4 (Emulation package 9.11.0.00128) 

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    您能否分享您遵循的程序? 您是否参考了任何文档?

    此致、
    帕尔特

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    大家好,帕斯

    我遵循这些步骤

    https://wiki.phytec.com/display/public/PRODUCTINFO/BSP-RTOS-TI-AM57x-PD17.1.x+Quickstart#BSPRTOSTIAM57xPD17.1.xQuickstart-CreateSimpleCCSProjectCreateaSimpleCodeComposerStudioProject

    此致、

    Jafet S

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    请查看文档 https://dev.ti.com/tirex/explore/node?node=A__AMDlrna5YiUganvfervUxw__com.ti.JACINTO_ACADEMY_AM574X__DKJrkRU__LATEST 、看看这是否有帮助。

    我正尝试在 CCS 中运行 Hello World,但收到此错误。

    此外、您是在什么时间点收到此误差? 是在加载应用程序之前还是在 A15上加载应用程序之后?

    此致、
    帕尔特

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    我按照这些步骤操作、但我在加载文件时收到错误消息。  

    我在调试后收到此错误。  

    IcePick_D: GEL: Error loading file 'C:\ti\ccs1230\ccs\ccs_base\emulation\boards\am571x\gel\AM571x_ICEPickD_Utility.gel': unable to open GEL file 'C:\ti\ccs1230\ccs\ccs_base\emulation\boards\am571x\gel\AM571x_ICEPickD_Utility.gel'
    Cortex_M4_IPU1_C0: GEL Output: --->>> AM571x Cortex M4 Startup Sequence In Progress... <<<---
    Cortex_M4_IPU1_C0: GEL Output: --->>> AM571x Cortex M4 Startup Sequence DONE! <<<---
    Cortex_M4_IPU1_C1: GEL Output: --->>> AM571x Cortex M4 Startup Sequence In Progress... <<<---
    Cortex_M4_IPU1_C1: GEL Output: --->>> AM571x Cortex M4 Startup Sequence DONE! <<<---
    C66xx_DSP: GEL Output: --->>> AM571x C66x DSP Startup Sequence In Progress... <<<---
    C66xx_DSP: GEL Output: --->>> AM571x C66x DSP Startup Sequence DONE! <<<---
    CS_DAP_DebugSS: GEL: Error loading file 'C:\ti\ccs1230\ccs\ccs_base\emulation\boards\am571x\gel\AM571x_dap_startup.gel': unable to open GEL file 'C:\ti\ccs1230\ccs\ccs_base\emulation\boards\am571x\gel\AM571x_dap_startup.gel'
    CortexA15_0: GEL Output: --->>> AM571x Cortex A15 Startup Sequence In Progress... <<<---
    CortexA15_0: GEL Output: --->>> AM571x Cortex A15 Startup Sequence DONE! <<<---
    

    然后、我连接到目标。  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    您正在使用哪个 CCS 版本? 您能否确认 AM571x_DAP_startup.gel 是否存在?

    此致、
    帕尔特

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    使用 Code Composer Studio 12.4.0的 IM

    我可以在哪里搜索该文件?

    尊重,

    Jafet

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    请检查以下路径:C:\ti\ccs1230\ccs\ccs_base\emulation\boards\am571x\gel

    此致、
    帕尔特

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    我没有板文件夹、

    尊重  

    Jafet S

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    看起来 CCS 未正确安装。 您可以尝试重新安装 CCS 吗?

    此致、
    帕尔特

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    感谢您的观看、

    现在我有版本12.4.0、且 GEL 文件夹中包含此文件。

    此致、

    Jafet S

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    您是否能够立即连接? 我们可以关闭该主题吗?

    此致、
    帕尔特