This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] PROCESSOR-SDK-J784S4:使用 Yocto 构建 SDK 时出现问题

Guru**** 2008950 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1252891/processor-sdk-j784s4-issue-building-sdk-with-yocto

器件型号:PROCESSOR-SDK-J784S4

大家好、TI 我将在 SDK 中执行以下步骤:

software-dl.ti.com/.../Overview_Building_the_SDK.html

我已下载  gcc-arm-9.2-2019.12-x86_64-aarch64-none-linux-gnu/和 gcc-arm-9.2-2019.12-x86_64-arm-none-linux-gnueabihf/并运行以下命令:

Fullscreen
1
2
3
4
5
6
7
8
9
10
11
12
13
./oe-layertool-setup.sh -f configs/processor-sdk-linux/processor-sdk-linux-08_06_01.txt
cd build
cat >> conf/local.conf << EOF
INHERIT += "own-mirrors"
SOURCE_MIRROR_URL = "">software-dl.ti.com/.../"
ARAGO_BRAND = "psdkla"
BB_NUMBER_THREADS ?= "8"
PARALLEL_MAKE ?= "-j 8"
DISTRO_FEATURES_append = " virtualization"
EOF
. conf/setenv
TOOLCHAIN_BASE=~/ MACHINE=j784s4-evm bitbake -k tisdk-tiny-image
XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

尝试构建 SDK 时不断出现以下错误:

Fullscreen
1
2
3
4
5
6
7
8
dev@0403e56a5796:~/ti-processor-sdk-linux-j784s4-evm-08_06_01_02/yocto-build/build$ TOOLCHAIN_BASE=/home/dev MACHINE=j784s4 bitbake -k tisdk-tiny-image
ERROR: Unable to start bitbake server (None)
ERROR: Server log for this session (/home/dev/ti-processor-sdk-linux-j784s4-evm-08_06_01_02/yocto-build/build/bitbake-cookerdaemon.log):
--- Starting bitbake server pid 27374 at 2023-07-26 15:31:14.693028 ---
ERROR: Failed to obtain external Arm toolchain version: Execution of '${DEF_TOOLCHAIN_PATH}/bin/INVALID-linux-gcc -v' failed: command not found
ERROR: Failed to obtain external Arm toolchain version: Execution of '${DEF_TOOLCHAIN_PATH}/bin/INVALID-linux-gcc -v' failed: command not found
ERROR: Error: EXTERNAL_TOOLCHAIN path '${DEF_TOOLCHAIN_PATH}' does not exist
XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Emily:

    请给我们的专家留出一些时间来解决该问题。  

    感谢您的耐心等待、

    Fabiana Jaimes

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    此问题已解决。 我将 gcc 工具链添加到 PATH 中、并确保机床末端具有"-evm"