主题中讨论的其他器件:AM625
您好、TI!
使用此新票据约定安全启动转换。
我制造出了安全器件、但内核映像和 DTB 无法加载。
请帮我解决这个问题。
请查找已连接的日志:
U-Boot 2023.04-00001-gf5b119738d-dirty (Mar 22 2024 - 19:14:21 +0530) SoC: AM62X SR1.0 HS-SE Model: Texas Instruments AM625 SK EEPROM not available at 80, trying to read at 81 Reading on-board EEPROM at 0x51 failed -121 DRAM: 2 GiB Core: 71 devices, 31 uclasses, devicetree: separate MMC: mmc@fa10000: 0, mmc@fa00000: 1 Loading Environment from nowhere... OK In: serial Out: serial Err: serial EEPROM not available at 80, trying to read at 81 Reading on-board EEPROM at 0x51 failed -121 Net: eth0: ethernet@8000000port@1 Hit any key to stop autoboot: 0 => setenv dfu_alt_info ${dfu_alt_info_emmc} => dfu 0 mmc 0 generic_phy_get_bulk : no phys property #############################################################################################� U-Boot SPL 2023.04-00001-gf5b119738d-dirty (Mar 21 2024 - 10:23:43 +0530) SYSFW ABI: 3.1 (firmware rev 0x0009 '9.0.5--v09.00.05 (Kool Koala)') SPL initial stack usage: 13376 bytes Trying to boot from MMC1 Authentication passed Authentication passed Authentication passed Authentication passed Authentication passed Starting ATF on ARM64 core... NOTICE: BL31: v2.8(release):v2.8-226-g2fcd408bb3-dirty NOTICE: BL31: Built : 00:42:57, Jan 13 2023 U-Boot SPL 2023.04-00001-gf5b119738d-dirty (Mar 22 2024 - 19:14:21 +0530) SYSFW ABI: 3.1 (firmware rev 0x0009 '9.0.5--v09.00.05 (Kool Koala)') SPL initial stack usage: 1856 bytes MMC: no card present ** Bad device specification mmc 1 ** Couldn't find partition mmc 1:1 Error: could not access storage. Trying to boot from MMC1 Authentication passed Authentication passed U-Boot 2023.04-00001-gf5b119738d-dirty (Mar 22 2024 - 19:14:21 +0530) SoC: AM62X SR1.0 HS-SE Model: Texas Instruments AM625 SK EEPROM not available at 80, trying to read at 81 Reading on-board EEPROM at 0x51 failed -121 DRAM: 2 GiB Core: 71 devices, 31 uclasses, devicetree: separate MMC: mmc@fa10000: 0, mmc@fa00000: 1 Loading Environment from nowhere... OK In: serial Out: serial Err: serial EEPROM not available at 80, trying to read at 81 Reading on-board EEPROM at 0x51 failed -121 Net: eth0: ethernet@8000000port@1 Hit any key to stop autoboot: 0 => setenv dfu_alt_info ${dfu_alt_info_emmc} => dfu 0 mmc 0 generic_phy_get_bulk : no phys property #############################################################################################K Ctrl+C to exit ... => boot switch to partitions #0, OK mmc0(part 0) is current device SD/MMC found on device 0 Failed to load 'boot.scr' Can't set block device ## Error: "main_cpsw0_qsgmii_phyinit" not defined 37950546 bytes read in 574 ms (63.1 MiB/s) name_fit_config=conf-ti_k3-am625-sk.dtb ## Loading kernel from FIT Image at 90000000 ... Using 'conf-ti_k3-am625-sk.dtb' configuration Verifying Hash Integrity ... fit_config_verify_required_keys: No signature node found: FDTD Bad Data Hash ERROR: can't get kernel image! switch to partitions #0, OK mmc0(part 0) is current device Scanning mmc 0:1... MMC: no card present No EFI system partition No EFI system partition
谢谢。
纳雷什。