This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] AM69、无法从 uboot 引导 Linux FS

Guru**** 2581075 points
Other Parts Discussed in Thread: SK-AM69, AM69

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1321075/am69-cannot-boot-linux-fs-from-uboot

主题中讨论的其他器件:AM69、SK-AM69

您好!  

我从 TI 网站下载了 AM69 SDK、只是想在重新构建之前使用 bl32来重新构建它(也没有任何更改)。

我从开球内核开始  

使 CFG_ARM64_CORE=y CFG_TEE_BIKENCE=n cross_COMPILE32=arm-none-linux-gnueabihf- cross_COMPILE64=aarch64-none-linux-gnu- O=out/arm platform=k3-j784s4

在该 u-boot 之后

make u-boot uBoot_TEE="/home/ti-processor-sdk-linux-j784s4-evm-09_01_00_06/board-support/optee-os-4.0.0 +gitAUTOINC+2a5b1d1232/out/arm/core/te-pager_v2.bin"

我有 HS-FS FS 电路板、因此我将 tiboot3-j784s4-hs-fs-evm.bin 和 tiboot3.bin 放置在 SD 卡的引导分区中、该分区与 hs-fs bin 以及 a72:tispl.bin 和 u-boot.img 链接。

我正在从 SDCard 引导、并且遇到了这个问题

it any key to stop autoboot:  0
switch to partitions #0, OK
mmc1 is current device
SD/MMC found on device 1
Failed to load 'boot.scr'
1329 bytes read in 2 ms (648.4 KiB/s)
Loaded env from uEnv.txt
Importing environment from mmc1 ...
Running uenvcmd ...
1 bytes read in 2 ms (0 Bytes/s)
Already setup.
GPIO: 'gpio@22_17' not found
Command 'gpio' failed: Error -22
GPIO: 'gpio@22_16' not found
Command 'gpio' failed: Error -22
k3_r5f_rproc r5f@41000000: Core 1 is already in use. No rproc commands work
Failed to load '/lib/firmware/j784s4-mcu-r5f0_1-fw'
597188 bytes read in 16 ms (35.6 MiB/s)
Warning: Did not detect image signing certificate. Skipping authentication to prevent boot failure. This will fail on Security Enforcing(HS-SE) d
Load Remote Processor 2 with data@addr=0x82000000 597188 bytes: Success!
301996 bytes read in 9 ms (32 MiB/s)
Warning: Did not detect image signing certificate. Skipping authentication to prevent boot failure. This will fail on Security Enforcing(HS-SE) d
Load Remote Processor 3 with data@addr=0x82000000 301996 bytes: Success!
179128 bytes read in 8 ms (21.4 MiB/s)
Warning: Did not detect image signing certificate. Skipping authentication to prevent boot failure. This will fail on Security Enforcing(HS-SE) d
Load Remote Processor 4 with data@addr=0x82000000 179128 bytes: Success!
179128 bytes read in 8 ms (21.4 MiB/s)
Warning: Did not detect image signing certificate. Skipping authentication to prevent boot failure. This will fail on Security Enforcing(HS-SE) d
Load Remote Processor 5 with data@addr=0x82000000 179128 bytes: Success!
596856 bytes read in 13 ms (43.8 MiB/s)
Warning: Did not detect image signing certificate. Skipping authentication to prevent boot failure. This will fail on Security Enforcing(HS-SE) d
Load Remote Processor 6 with data@addr=0x82000000 596856 bytes: Success!
179128 bytes read in 8 ms (21.4 MiB/s)
Warning: Did not detect image signing certificate. Skipping authentication to prevent boot failure. This will fail on Security Enforcing(HS-SE) d
Load Remote Processor 7 with data@addr=0x82000000 179128 bytes: Success!
14684456 bytes read in 79 ms (177.3 MiB/s)
Warning: Did not detect image signing certificate. Skipping authentication to prevent boot failure. This will fail on Security Enforcing(HS-SE) d
Load Remote Processor 8 with data@addr=0x82000000 14684456 bytes: Success!
14946600 bytes read in 80 ms (178.2 MiB/s)
Warning: Did not detect image signing certificate. Skipping authentication to prevent boot failure. This will fail on Security Enforcing(HS-SE) d
Load Remote Processor 9 with data@addr=0x82000000 14946600 bytes: Success!
14553384 bytes read in 76 ms (182.6 MiB/s)
Warning: Did not detect image signing certificate. Skipping authentication to prevent boot failure. This will fail on Security Enforcing(HS-SE) d
Load Remote Processor 10 with data@addr=0x82000000 14553384 bytes: Success!
14553384 bytes read in 75 ms (185.1 MiB/s)
Warning: Did not detect image signing certificate. Skipping authentication to prevent boot failure. This will fail on Security Enforcing(HS-SE) d
Load Remote Processor 11 with data@addr=0x82000000 14553384 bytes: Success!
19079680 bytes read in 197 ms (92.4 MiB/s)
Failed to load '/boot/dtb/ti/k3-am69-sk.dtb'
libfdt fdt_check_header(): FDT_ERR_BADMAGIC
No FDT memory address configured. Please configure
the FDT address via "fdt addr <address>" command.
Aborting!
Failed to load '/boot/dtb/ti/k3-am69-sk-ddr-mem-carveout.dtbo'
Failed to load '/boot/dtb/ti/k3-j784s4-edgeai-apps.dtbo'
ERROR: Did not find a cmdline Flattened Device Tree
Could not find a valid device tree
switch to partitions #0, OK
mmc0(part 0) is current device
** No partition table - mmc 0 **
Couldn't find partition mmc 0:1
switch to partitions #0, OK
mmc1 is current device
Scanning mmc 1:1...
No EFI system partition
No EFI system partition
Failed to persist EFI variables
BootOrder not defined
EFI boot manager: Cannot load any image
starting USB...
Bus usb@6000000: cdns-usb3-host usb@6000000: Unable to get USB2 phy (ret -61)
cdns-usb3-host usb@6000000: DRD version v1 (ID: 0004024e, rev: 00000200)
Register 2000840 NbrPorts 2
Starting the controller
USB XHCI 1.00
scanning bus usb@6000000 for devices... 3 USB Device(s) found
       scanning usb for storage devices... 0 Storage Device(s) found

Device 0: unknown device
k3-navss-ringacc ringacc@2b800000: Ring Accelerator probed rings:286, gp-rings[96,20] sci-dev-id:328
k3-navss-ringacc ringacc@2b800000: dma-ring-reset-quirk: disabled
am65_cpsw_nuss_port ethernet@46000000port@1: K3 CPSW: rflow_id_base: 2
ethernet@46000000port@1 Waiting for PHY auto negotiation to complete......... TIMEOUT !
am65_cpsw_nuss_port ethernet@46000000port@1: phy_startup failed
am65_cpsw_nuss_port ethernet@46000000port@1: am65_cpsw_start end error
missing environment variable: pxeuuid
Retrieving file: pxelinux.cfg/01-08-04-b4-2e-8f-2f
am65_cpsw_nuss_port ethernet@46000000port@1: K3 CPSW: rflow_id_base: 2
ethernet@46000000port@1 Waiting for PHY auto negotiation to complete......... TIMEOUT !
am65_cpsw_nuss_port ethernet@46000000port@1: phy_startup failed
am65_cpsw_nuss_port ethernet@46000000port@1: am65_cpsw_start end error
Retrieving file: pxelinux.cfg/00000000

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    问题可能在这里

    加载"/boot/dtb/ti/k3-am69-sk.dtb "失败
    libfdt FDT_check_header ():FDT_ERR_BADMAGIC
    未配置 FDT 存储器地址。 请配置
    通过"FDT addr "添加 FDT 地址

    "命令。
    正在中止!  

    但问题是、为什么它可以与 TI 交付的 SD 卡中捆绑的映像一起使用

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    另一个提示是 uboot 不会发现 SD 卡  

    => MMC 列表
    MMC@4f80000:0
    MMC@4fb0000:1

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    此处是来自预构建映像的 env 配置,该映像由 TI 捆绑在 SD 卡中。 但与传统的略有不同、

    => printenv
    addr_fit=0x90000000
    arch=arm
    args_all=setenv optargs earlycon=ns16550a,mmio32,0x02880000 ${mtdparts}
    args_mmc=run finduuid;setenv bootargs console=${console} ${optargs} root=PARTUUID=${uuid} rw rootfstype=${mmcrootfstype}
    args_ufs=setenv devtype scsi;setenv bootpart 1:1;run ufs_finduuid;setenv bootargs console = ${console} ${optargs}root=PARTUUID=${uuid} rw rootfstype=${scsirootfstype};setenv devtype scsi;setenv bootpart 1:1
    baudrate=115200
    board=j784s4
    board_name=am69-sk
    board_rev=E3
    board_serial=0151
    board_software_revision=01
    boot=mmc
    boot_fdt=try
    boot_fit=1
    boot_rprocs=if test ${dorprocboot} -eq 1 && test ${boot} = mmc; then rproc init;run boot_rprocs_mmc;fi;
    boot_rprocs_mmc=env set rproc_id;env set rproc_fw;env set secure_suffix;if test ${boot_fit} -eq 1; then env set secure_suffix -sec;fi;for i in ${rproc_fw_binaries}; do if test -z "${rproc_id}" ; then env set rproc_id $i;else env set rproc_fw $i${secure_suffix};run rproc_load_and_boot_one;env set rproc_id;env set rproc_fw;fi;done
    bootcmd=run findfdt; run envboot; run init_${boot}; run main_cpsw0_qsgmii_phyinit; run boot_rprocs; if test ${boot_fit} -eq 1; then run get_fit_${boot}; run get_overlaystring; run run_fit; else; run get_kern_${boot}; run get_fdt_${boot}; run get_overlay_${boot}; run run_kern; fi;
    bootdelay=2
    bootdir=/boot
    bootenvfile=uEnv.txt
    bootm_size=0x10000000
    bootpart=1:2
    bootscript=echo Running bootscript from mmc${mmcdev} ...; source ${loadaddr}
    console=ttyS2,115200n8
    cpu=armv8
    default_device_tree=k3-j784s4-evm.dtb
    dfu_alt_info_emmc=rawemmc raw 0 0x800000 mmcpart 1;rootfs part 0 1 mmcpart 0;tiboot3.bin.raw raw 0x0 0x400 mmcpart 1;tispl.bin.raw raw 0x400 0x1000 mmcpart 1;u-boot.img.raw raw 0x1400 0x2000 mmcpart 1;u-env.raw raw 0x3400 0x100 mmcpart 1;sysfw.itb.raw raw 0x3600 0x800 mmcpart 1
    dfu_alt_info_mmc=boot part 1 1;rootfs part 1 2;tiboot3.bin fat 1 1;tispl.bin fat 1 1;u-boot.img fat 1 1;uEnv.txt fat 1 1;sysfw.itb fat 1 1
    dfu_alt_info_ospi=tiboot3.bin raw 0x0 0x080000;tispl.bin raw 0x080000 0x200000;u-boot.img raw 0x280000 0x400000;u-boot-env raw 0x680000 0x020000;sysfw.itb raw 0x6c0000 0x100000;rootfs raw 0x800000 0x3800000
    dfu_alt_info_ram=tispl.bin ram 0x80080000 0x200000;u-boot.img ram 0x81000000 0x400000
    do_main_cpsw0_qsgmii_phyinit=1
    dorprocboot=0
    dtboaddr=0x89000000
    envboot=mmc dev ${mmcdev}; if mmc rescan; then echo SD/MMC found on device ${mmcdev};if run loadbootscript; then run bootscript;else if run loadbootenv; then echo Loaded env from ${bootenvfile};run importbootenv;fi;if test -n $uenvcmd; then echo Running uenvcmd ...;run uenvcmd;fi;fi;fi;
    ethaddr=08:04:b4:2e:8f:2f
    fdt_addr_r=0x88000000
    fdtaddr=0x88000000
    fdtcontroladdr=fdeae070
    fdtoverlay_addr_r=0x80200000
    findfdt=setenv name_fdt ${default_device_tree};if test $board_name = am69-sk; then setenv name_fdt k3-am69-sk.dtb; fi;if test $board_name = j784s4; then setenv name_fdt k3-j784s4-evm.dtb; fi;setenv fdtfile ${name_fdt}
    finduuid=part uuid ${boot} ${bootpart} uuid
    get_fdt_mmc=load mmc ${bootpart} ${fdtaddr} ${bootdir}/${name_fdt}
    get_fdt_ufs=load ${devtype} ${bootpart} ${fdtaddr} ${bootdir}/${fdtfile}
    get_fit_mmc=load mmc ${bootpart} ${addr_fit} ${bootdir}/${name_fit}
    get_kern_mmc=load mmc ${bootpart} ${loadaddr} ${bootdir}/${name_kern}
    get_kern_ufs=load ${devtype} ${bootpart} ${loadaddr} ${bootdir}/${name_kern}
    get_overlay_mmc=fdt address ${fdtaddr};fdt resize 0x100000;for overlay in $name_overlays;do;load mmc ${bootpart} ${dtboaddr} ${bootdir}/${overlay} && fdt apply ${dtboaddr};done;
    get_overlay_ufs=fdt address ${fdtaddr};fdt resize 0x100000;for overlay in $name_overlays;do;load scsi ${bootpart} ${dtboaddr} ${bootdir}/${overlay} && fdt apply ${dtboaddr};done;
    get_overlaystring=for overlay in $name_overlays;do;setenv overlaystring ${overlaystring}'#'${overlay};done;
    importbootenv=echo Importing environment from mmc${mmcdev} ...; env import -t ${loadaddr} ${filesize}
    init_main_cpsw0_qsgmii_phy=gpio set gpio@22_17;gpio clear gpio@22_16
    init_mmc=run args_all args_mmc
    init_ufs=ufs init; scsi scan; run args_ufs
    kernel_addr_r=0x82000000
    loadaddr=0x82000000
    loadbootenv=fatload mmc ${mmcdev} ${loadaddr} ${bootenvfile}
    loadbootscript=load mmc ${mmcdev} ${loadaddr} boot.scr
    loadfdt=load ${devtype} ${bootpart} ${fdtaddr} ${bootdir}/${fdtfile}
    loadimage=load ${devtype} ${bootpart} ${loadaddr} ${bootdir}/${bootfile}
    main_cpsw0_qsgmii_phyinit=if test ${do_main_cpsw0_qsgmii_phyinit} -eq 1 && test ${dorprocboot} -eq 1 && test ${boot} = mmc; then run init_main_cpsw0_qsgmii_phy; run toggle_mux2_ethfw;fi;
    mmcboot=mmc dev ${mmcdev}; devnum=${mmcdev}; devtype=mmc; if mmc rescan; then echo SD/MMC found on device ${mmcdev};if run loadimage; then run args_mmc; if test ${boot_fit} -eq 1; then run run_fit; else run mmcloados;fi;fi;fi;
    mmcdev=1
    mmcloados=if test ${boot_fdt} = yes || test ${boot_fdt} = try; then if run loadfdt; then bootz ${loadaddr} - ${fdtaddr}; else if test ${boot_fdt} = try; then bootz; else echo WARN: Cannot load the DT; fi; fi; else bootz; fi;
    mmcrootfstype=ext4 rootwait
    mtdids=nor0=47040000.spi.0,nor0=47034000.hyperbus
    mtdparts=mtdparts=47040000.spi.0:512k(ospi.tiboot3),2m(ospi.tispl),4m(ospi.u-boot),256k(ospi.env),256k(ospi.env.backup),57088k@8m(ospi.rootfs),256k(ospi.phypattern);47034000.hyperbus:512k(hbmc.tiboot3),2m(hbmc.tispl),4m(hbmc.u-boot),256k(hbmc.env),-@8m(hbmc.rootfs)
    name_fit=fitImage
    name_kern=Image
    partitions=uuid_disk=${uuid_gpt_disk};name=rootfs,start=0,size=-,uuid=${uuid_gpt_rootfs}
    pxefile_addr_r=0x80100000
    ramdisk_addr_r=0x88080000
    rd_spec=-
    rdaddr=0x88080000
    rproc_fw_binaries=2 /lib/firmware/j784s4-main-r5f0_0-fw 3 /lib/firmware/j784s4-main-r5f0_1-fw 4 /lib/firmware/j784s4-main-r5f1_0-fw 5 /lib/firmware/j784s4-main-r5f1_1-fw 6 /lib/firmware/j784s4-main-r5f2_0-fw 7 /lib/firmware/j784s4-main-r5f2_1-fw 8 /lib/firmware/j784s4-c71_0-fw 9 /lib/firmware/j784s4-c71_1-fw 10 /lib/firmware/j784s4-c71_2-fw 11 /lib/firmware/j784s4-c71_3-fw
    rproc_load_and_boot_one=if load mmc ${bootpart} $loadaddr ${rproc_fw}; then if rproc load ${rproc_id} ${loadaddr} ${filesize}; then rproc start ${rproc_id};fi;fi
    run_fit=bootm ${addr_fit}#${fdtfile}${overlaystring}
    run_kern=booti ${loadaddr} ${rd_spec} ${fdtaddr}
    scriptaddr=0x80000000
    scsirootfstype=ext4 rootwait
    serial#=0000000000000151
    soc=k3
    stderr=serial@2880000
    stdin=serial@2880000
    stdout=serial@2880000
    toggle_mux2_ethfw=gpio set gpio@22_13; gpio set gpio@22_14;gpio set gpio@22_15
    ufs_finduuid=part uuid scsi ${bootpart} uuid
    update_to_fit=setenv loadaddr ${addr_fit}; setenv bootfile ${name_fit}
    vendor=ti
    
    Environment size: 6518/131067 bytes
    

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Marcin:

    您是否可以通过将 tiboot3-j784s4-hs-fs-evm.bin 重命名为 tiboot3.bin 来尝试将 tiboot3.bin 替换为 tiboot3-j784s4-hs-fs-evm.bin?

    谢谢!

    法比亚纳

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我已经这么做了、正如我在这里提到的 FS、"我有 HS-FS 板、所以我将 tiboot3-j784s4-hs-fs-evm.bin 和 tiboot3.bin 放置在 SD 卡的引导分区中、它与 hs-fs bin 链接"、因此、基本上我采用了  tiboot3-j784s4-hs-fs-evm.bin 复制它并将副本重命名为 tiboot3.bin、 两个文件都放在 SD 卡上、就像在随电路板提供的 SD 卡上一样。 这意味着它在这里不是解决方案、  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    如您所见 、K3-AM69-SK.DTB 位于2个分区上  

    ls mmc 1:2
    <DIR>       4096 .
    <DIR>       4096 ..
    <DIR>      16384 lost+found
    <DIR>       4096 bin
    <DIR>       4096 boot
    <DIR>       4096 dev
    <DIR>       4096 etc
    <DIR>       4096 home
    <DIR>       4096 include
    <SYM>         20 init
    <DIR>       4096 lib
    <SYM>         19 linuxrc
    <DIR>       4096 media
    <DIR>       4096 mnt
    <DIR>       4096 opt
    <DIR>       4096 proc
    <DIR>       4096 run
    <DIR>       4096 sbin
    <DIR>       4096 sys
    <DIR>       4096 tmp
    <DIR>       4096 usr
    <DIR>       4096 var
    <DIR>       4096 .cache
    <DIR>       4096 data
    => ls mmc 1:2 boot
    <DIR>       4096 .
    <DIR>       4096 ..
    <SYM>         26 Image
            19079680 Image-5.10.162-g76b3e88d56
    <SYM>         29 fitImage
             8307211 fitImage-5.10.162-g76b3e88d56
                3639 k3-am69-sk-csi2-ov5640.dtbo
               13811 k3-am69-sk-ddr-mem-carveout.dtbo
                3596 k3-am69-sk-fpdlink-fusion.dtbo
                3149 k3-am69-sk-rpi-cam-imx219.dtbo
                1936 k3-am69-sk-rpi-hdr-ehrpwm.dtbo
               90726 k3-am69-sk.dtb
                2471 k3-j721e-fpdlink-imx390-cm-0-0.dtbo
                2471 k3-j721e-fpdlink-imx390-cm-0-1.dtbo
                2471 k3-j721e-fpdlink-imx390-cm-0-2.dtbo
                2471 k3-j721e-fpdlink-imx390-cm-0-3.dtbo
                2471 k3-j721e-fpdlink-imx390-cm-1-0.dtbo
                2471 k3-j721e-fpdlink-imx390-cm-1-1.dtbo
                2471 k3-j721e-fpdlink-imx390-cm-1-2.dtbo
                2471 k3-j721e-fpdlink-imx390-cm-1-3.dtbo
                2471 k3-j721e-fpdlink-imx390-rcm-0-0.dtbo
                2471 k3-j721e-fpdlink-imx390-rcm-0-1.dtbo
                2471 k3-j721e-fpdlink-imx390-rcm-0-2.dtbo
                2471 k3-j721e-fpdlink-imx390-rcm-0-3.dtbo
                2471 k3-j721e-fpdlink-imx390-rcm-1-0.dtbo
                2471 k3-j721e-fpdlink-imx390-rcm-1-1.dtbo
                2471 k3-j721e-fpdlink-imx390-rcm-1-2.dtbo
                2471 k3-j721e-fpdlink-imx390-rcm-1-3.dtbo
               13306 k3-j784s4-edgeai-apps.dtbo
                1614 k3-j784s4-evm-csi2-ov5640.dtbo
               99385 k3-j784s4-evm.dtb
                3155 k3-j784s4-fpdlink-fusion.dtbo
               14313 k3-j784s4-vision-apps.dtbo 

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Marcin:

    您使用的是 SK-AM69还是 AM69 EVM?

    谢谢!

    法比亚纳

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    SK-AM69、我使用的是 SDK  

    TI-PROCESSOR-SDK-LINUX-EDGEAI-J784s4-EVM-09_01_00_06-Linux-x86

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我已经决定重新构建内核以便能够访问 dtb 目录,它的问题消失了,但显示了新的  

    Working FDT set to 88000000
    11348 bytes read in 5 ms (2.2 MiB/s)
    10290 bytes read in 5 ms (2 MiB/s)
    failed on fdt_overlay_apply(): FDT_ERR_NOTFOUND
    ERROR: Did not find a cmdline Flattened Device Tree
    Could not find a valid device tree
    switch to partitions #0, OK
    mmc0(part 0) is current device
    ** No partition table - mmc 0 **
    Couldn't find partition mmc 0:1
    switch to partitions #0, OK
    mmc1 is current device
    Scanning mmc 1:1...
    No EFI system partition
    No EFI system partition
    Failed to persist EFI variables
    BootOrder not defined
    EFI boot manager: Cannot load any image
    starting USB...
    Bus usb@6000000: cdns-usb3-host usb@6000000: Unable to get USB2 phy (ret -61)
    cdns-usb3-host usb@6000000: DRD version v1 (ID: 0004024e, rev: 00000200)
    Register 2000840 NbrPorts 2
    Starting the controller
    USB XHCI 1.00
    scanning bus usb@6000000 for devices... 3 USB Device(s) found
           scanning usb for storage devices... 0 Storage Device(s) found
    
    Device 0: unknown device
    k3-navss-ringacc ringacc@2b800000: Ring Accelerator probed rings:286, gp-rings[96,20] sci-dev-id:328
    k3-navss-ringacc ringacc@2b800000: dma-ring-reset-quirk: disabled
    

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    箱关闭,重要的注意,它是不足以编译 u-boot。 必须采用默认 FS、并用其覆盖 SD 卡。 它可以解决一切问题。 我认为 最好在这里添加此信息 https://software-dl.ti.com/jacinto7/esd/processor-sdk-linux-am69/09_00_00_06/exports/docs/linux/Foundational_Components -Boot/UGGeneral-Info.html