您好!
在`将` tispl.bin 中嵌入的默认演示应用程序替换为 SDK 8.6中的另一个固件(ti-processor-sdk-rtos-j721e-evm-08_06_01_03)时、我们面临一些问题、例如从任何 mcusw 演示版本编译(编译为在 mcu1_0中运行)。
从 Linux SDK 8.6 (ti-processor-sdk-linux-j7-evm-08_06_01_02)生成 u-boot 后、我们在 DFU 中设置引导模式并传递生成的映像、在加载新的`tispl.bin`后获取以下输出:
init_env from device 18 not supported! Starting ATF on ARM64 core... NOTICE: BL31: v2.8(release):v2.8-226-g2fcd408bb3-dirty NOTICE: BL31: Built : 15:40:55, May 2 2023 I/TC: I/TC: OP-TEE version: 3.20.0 (gcc version 9.2.1 20191025 (GNU Toolchain for the A-profile Architecture 9.2-2019.12 (arm-9.10))) #1 Tue May 2 15:41:00 UTC 2023 aarch64 I/TC: WARNING: This OP-TEE configuration might be insecure! I/TC: WARNING: Please check optee.readthedocs.io/.../porting_guidelines.html I/TC: Primary CPU initializing I/TC: SYSFW ABI: 3.1 (firmware rev 0x0008 '8.6.3--v08.06.03 (Chill Capybar') I/TC: HUK Initialized E/TC:0 0 k3_sec_proxy_verify_thread:108 Queue is busy E/TC:0 0 k3_sec_proxy_recv:196 Thread SEC_PROXY_RESPONSE_THREAD verification failed. ret = -65523 E/TC:0 0 ti_sci_get_response:101 Message receive failed (-65523) E/TC:0 0 ti_sci_do_xfer:150 Failed to get response (-65523) E/TC:0 0 sa2ul_init:59 Failed to get SA2UL device E/TC:0 0 call_initcalls:43 Initcall __text_start + 0x00063c20 failed I/TC: Primary CPU switching to normal world boot E/TC:0 0 E/TC:0 0 Core data-abort at address 0x10 (translation fault) E/TC:0 0 esr 0x96000005 ttbr0 0x9e894000 ttbr1 0x00000000 cidr 0x0 E/TC:0 0 cpu #0 cpsr 0x800003c4 E/TC:0 0 x0 000000009e867000 x1 0000000000000010 E/TC:0 0 x2 0000000000000000 x3 0000000000000000 E/TC:0 0 x4 0000000000000001 x5 0000000000ffffff E/TC:0 0 x6 0000000000000002 x7 000000009e89c190 E/TC:0 0 x8 000000009e89c190 x9 000000009e884d70 E/TC:0 0 x10 0000000000000000 x11 0000000000000000 E/TC:0 0 x12 000000009e89c100 x13 000000000000000a E/TC:0 0 x14 00000000ffffffff x15 0000000000000020 E/TC:0 0 x16 000000009e813c40 x17 0000000000000000 E/TC:0 0 x18 0000000000000000 x19 000000009e89eca0 E/TC:0 0 x20 000000009e89eca8 x21 0000000000000007 E/TC:0 0 x22 000000009e873000 x23 000000009e8736a0 E/TC:0 0 x24 0000000100000000 x25 0000000000000000 E/TC:0 0 x26 0000000000000000 x27 0000000000000000 E/TC:0 0 x28 0000000000000000 x29 000000009e89ec30 E/TC:0 0 x30 000000009e80e3ac elr 000000009e80e3cc E/TC:0 0 sp_el0 000000009e89ec30 E/TC:0 0 TEE load address @ 0x9e800000 E/TC:0 0 Call stack: E/TC:0 0 0x9e80e3cc E/TC:0 0 Panic 'unhandled pageable abort' at core/arch/arm/kernel/abort.c:572 <abort_handler> E/TC:0 0 TEE load address @ 0x9e800000 E/TC:0 0 Call stack: E/TC:0 0 0x9e8087dc E/TC:0 0 0x9e81506c E/TC:0 0 0x9e807fd8 E/TC:0 0 0x9e805520
我们是否需要执行任何额外步骤来使 MCU 岛与主域 A72 (QNX 7.1)之间进行引导? 在 MCU 岛中、SDK 中是否有可通过 DFU 引导的任何软件演示?
非常感谢