This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] AM625:如何自动执行整个 DFU-EMMC 刷写过程。

Guru**** 2554690 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1359436/am625-how-to-automate-the-complete-dfu-emmc-flashing-process

器件型号:AM625
主题中讨论的其他器件:CSD

您好!

我已成功按照为 DFU 刷写脚本提供的步骤操作、在成功刷写 rootfs 后、我需要在 UART 控制台中执行特定命令。 但是、我的目标是自动执行整个刷写过程、无需在 UART 控制台中手动键入任何命令。

刷写脚本后、我需要在 UART 终端中执行以下步骤:

To give the ROM access to the boot partition, the following commands must be used for the first time:
        => mmc partconf 0 1 1 1
        => mmc bootbus 0 2 0 0

The above command sets up the EXT_CSD register of eMMC flash and enables boot from boot0 partition.

Power the EVM off. Set the boot switches [SW2:SW1] to eMMC boot. When the board is powering on, hit any key to stop u-boot auto-booting. Enter the following u-boot commands. Alternatively, these u-boot commands may also be built into u-boot.

To boot kernel from eMMC, use the following commands after writing rootfs to user partition:

setenv mmcdev 0
setenv bootpart 0
boot
The board should now boot from eMMC with the updated files.

如何将这些命令集成到 DFU-Flashing 脚本中以自动执行此过程?

谢谢。

Abhijeet