This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] J721EXSOMXEVM:用于 Jacinto 7 TDA4VM 入门套件的"无以太网接口

Guru**** 2555160 points
Other Parts Discussed in Thread: TDA4VM

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1361605/j721exsomxevm-bsp-for-jacinto-7-tda4vm-starter-kit-without-ethernet-interface-available

器件型号:J721EXSOMXEVM
主题中讨论的其他器件:TDA4VM

尊敬的论坛:

我目前正在关注 BSP 用户手册(BSP 链接)中的实例。 我能够启动电路板、但生成的 QNX 映像不包含用于以太网连接的接口。

QNX 软件中心软件包 ID 为:  com.qnx.qnx800.bsp.hw.ti_j721e_tda4vm_sk

这是 ifconfig 的输出:

# ifconfig
enc0: flags=0<> metric 0 mtu 1536
        groups: enc
        nd6 options=21<PERFORMNUD,AUTO_LINKLOCAL>
lo0: flags=8049<UP,LOOPBACK,RUNNING,MULTICAST> metric 0 mtu 16384
        options=680003<RXCSUM,TXCSUM,LINKSTATE,RXCSUM_IPV6,TXCSUM_IPV6>
        inet 127.0.0.1 netmask 0xff000000
        inet6 ::1 prefixlen 128
        inet6 fe80::1%lo0 prefixlen 64 scopeid 0x2
        groups: lo
        nd6 options=21<PERFORMNUD,AUTO_LINKLOCAL>
pflog0: flags=0<> metric 0 mtu 33144
        groups: pflog
pfsync0: flags=0<> metric 0 mtu 1500
        syncpeer: 0.0.0.0 maxupd: 128 defer: off
        syncok: 1
        groups: pfsync

这样、我看不到任何可用于配置以太网端口 IP 的接口。

我执行的步骤如下:

  1. 从软件中心下载了 BSP。
  2. 并生成 BSP。
  3. 下载 Linux SDK 和 SD 卡映像
  4. 如指南中所述、通过刷写 SD 卡映像并将 DTB (来自 Linux SDK)和编译后的 BSP 复制到 SDCard 中来生成该映像。

这是引导日志:

U-Boot SPL 2023.04-g756ba776d4 (Jul 13 2023 - 05:36:12 +0000)
SYSFW ABI: 3.1 (firmware rev 0x0009 '9.0.6--v09.00.06 (Kool Koala)')
Trying to boot from MMC2
Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
Loading Environment from nowhere... OK
Starting ATF on ARM64 core...

NOTICE:  BL31: v2.8(release):v2.8-226-g2fcd408bb3-dirty
NOTICE:  BL31: Built : 00:42:57, Jan 13 2023
I/TC: 
I/TC: OP-TEE version: 3.20.0 (gcc version 11.3.0 (GCC)) #1 Fri Jan 20 15:42:54 UTC 2023 aarch64
I/TC: WARNING: This OP-TEE configuration might be insecure!
I/TC: WARNING: Please check optee.readthedocs.io/.../porting_guidelines.html
I/TC: Primary CPU initializing
I/TC: SYSFW ABI: 3.1 (firmware rev 0x0009 '9.0.6--v09.00.06 (Kool Koala)')
I/TC: HUK Initialized
I/TC: Activated SA2UL device
I/TC: Fixing SA2UL firewall owner for GP device
I/TC: Enabled firewalls for SA2UL TRNG device
I/TC: SA2UL TRNG initialized
I/TC: SA2UL Drivers initialized
I/TC: Primary CPU switching to normal world boot

U-Boot SPL 2023.04-g756ba776d4 (Jul 13 2023 - 05:36:12 +0000)
SYSFW ABI: 3.1 (firmware rev 0x0009 '9.0.6--v09.00.06 (Kool Koala)')
Detected: J7X-BASE-CPB rev A
Detected: J7X-VSC8514-ETH rev E2
Trying to boot from MMC2
Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted


U-Boot 2023.04-g756ba776d4 (Jul 13 2023 - 05:36:12 +0000)

SoC:   J721E SR1.1 GP
Model: Texas Instruments K3 J721E SoC
Board: J721EX-PM2-SOM rev A
DRAM:  4 GiB
Core:  125 devices, 34 uclasses, devicetree: separate
Flash: 0 Bytes
MMC:   mmc@4f80000: 0, mmc@4fb0000: 1
Loading Environment from nowhere... OK
In:    serial@2800000
Out:   serial@2800000
Err:   serial@2800000
am65_cpsw_nuss ethernet@46000000: K3 CPSW: nuss_ver: 0x6BA00101 cpsw_ver: 0x6BA80100 ale_ver: 0x00293904 Ports:1 mdio_freq:1000000
Detected: J7X-BASE-CPB rev A
Detected: J7X-VSC8514-ETH rev E2
cdns,sierra serdes@5000000: sierra probed
Net:   eth0: ethernet@46000000port@1
Hit any key to stop autoboot:  0 
switch to partitions #0, OK
mmc1 is current device
SD/MMC found on device 1
Failed to load 'boot.scr'
1554 bytes read in 24 ms (62.5 KiB/s)
Loaded env from uEnv.txt
Importing environment from mmc1 ...
Running uenvcmd ...
Device: mmc@4fb0000
Manufacturer ID: 74
OEM: 4a60
Name: SD32G 
Bus Speed: 100000000
Mode: UHS SDR50 (100MHz)
Rd Block Len: 512
SD version 3.0
High Capacity: Yes
Capacity: 29.1 GiB
Bus Width: 4-bit
Erase Group Size: 512 Bytes
102536 bytes read in 27 ms (3.6 MiB/s)
13912460 bytes read in 314 ms (42.3 MiB/s)
## Starting application at 0x80080000 ...
Hypervisor support disabled
MMU: 16-bit ASID 44-bit PA TCR_EL1=00000014b5183519
ARM GIC-500 r1p1, arch v3.0 detected
gic_v3_lpi_add_entry for vectors 8192 -> 8447, Ok
gic_v3_lpi_add_entry for vectors 8448 -> 65535, Ok
No SPI intrinfo. Add default entry for 32 -> 991 vectors, Ok
LPI config table #1 @ 0000000080013000, callout vaddr: ffffff8040251000
aarch64_cpuspeed: core speed 2000
cpu0: MPIDR=0000000080000000
cpu0: MIDR=411fd080 Cortex-A72 r1p0
cpu0: CWG=4 ERG=4 Dminline=4 Iminline=4 PIPT
cpu0: CLIDR=a200023 LoUU=1 LoC=2 LoUIS=1
cpu0: L1 Icache 48K linesz=64 set/way=256/3
cpu0: L1 Dcache 32K linesz=64 set/way=256/2
cpu0: L2 Unified 1024K linesz=64 set/way=1024/16
Enabling ITS 0
ITS queue at 0000000080030000, num slots: 256
Issue MAPC/SYNC/INVALL commands for ICID 0
update CWRITER to 0x00000060
Waiting for all commands to be processed ... Done in 1 tries
Enable LPIs in GICR_CTLR @ 0000000001900000 for CPU0
Total Available L3 cache (MSMC SRAM): 0 bytes
Loading IFS...decompressing...done
I/TC: Secondary CPU 1 initializing
I/TC: Secondary CPU 1 switching to normal world boot
aarch64_cpuspeed: core speed 2000
cpu1: MPIDR=0000000080000001
cpu1: MIDR=411fd080 Cortex-A72 r1p0
cpu1: CWG=4 ERG=4 Dminline=4 Iminline=4 PIPT
cpu1: CLIDR=a200023 LoUU=1 LoC=2 LoUIS=1
cpu1: L1 Icache 48K linesz=64 set/way=256/3
cpu1: L1 Dcache 32K linesz=64 set/way=256/2
cpu1: L2 Unified 1024K linesz=64 set/way=1024/16
ITS 0 already Enabled
ITS queue at 0000000080030000, num slots: 256
Issue MAPC/SYNC/INVALL commands for ICID 1
update CWRITER to 0x000000c0
Waiting for all commands to be processed ... Done in 1 tries
Enable LPIs in GICR_CTLR @ 0000000001920000 for CPU1

System page at phys:0000000080023000 user:ffffff8040276000 kern:ffffff8040272000
Starting next program at vffffff806008e910
syspage::hypinfo::flags=0x00000000
 
Welcome to QNX 8.0.0 on TI_J721E_Starter_Kit_Board !
 
Starting I2C driver ...
Starting PCI Server ...
Start serial driver
Starting MMC/SD memory card driver... SD
Starting Flash driver...
Starting XHCI driver on USB3SS0 and USB3SS1
Starting devf-ram filesystem ...
Starting networking ...
Starting DHCP client ...
Starting SSH daemon ...
Starting devc-pty manager ...
Starting qconn daemon ...
Starting shell ...

您能不能告诉我如何在这些条件下配置以太网接口?